diff --git a/ext/x264/gstx264enc.c b/ext/x264/gstx264enc.c
index 1f1bb45951e2cfa9a31ebfb14893c4d15d0636c7..ea3cf0bf9ca3581209b8c45c0828f50fd2ced27b 100644 (file)
--- a/ext/x264/gstx264enc.c
+++ b/ext/x264/gstx264enc.c
* of the encoding. This will similarly be the case if this target bitrate
* is to obtained in multiple (2 or 3) pass encoding.
* Alternatively, one may choose to perform Constant Quantizer or Quality encoding,
- * in which case the #GstX264Enc:quantizer property controls much of the outcome.
+ * in which case the #GstX264Enc:quantizer property controls much of the outcome, in that case #GstX264Enc:bitrate is the maximum bitrate.
*
* The H264 profile that is eventually used depends on a few settings.
* If #GstX264Enc:dct8x8 is enabled, then High profile is used.
* Otherwise, if #GstX264Enc:cabac entropy coding is enabled or #GstX264Enc:bframes
* are allowed, then Main Profile is in effect, and otherwise Baseline profile
- * applies. As such, Main is presently the default profile, which is fine for
- * most players and settings, but in some cases (e.g. hardware platforms)
- * a more restricted profile/level may be necessary.
+ * applies. The main profile is imposed by default,
+ * which is fine for most software players and settings,
+ * but in some cases (e.g. hardware platforms) a more restricted profile/level
+ * may be necessary. The recommended way to set a profile is to set it in the
+ * downstream caps.
*
* If a preset/tuning are specified then these will define the default values and
* the property defaults will be ignored. After this the option-string property is
* applied, followed by the user-set properties, fast first pass restrictions and
* finally the profile restrictions.
*
+ * <note>Some settings, including the default settings, may lead to quite
+ * some latency (i.e. frame buffering) in the encoder. This may cause problems
+ * with pipeline stalling in non-trivial pipelines, because the encoder latency
+ * is often considerably higher than the default size of a simple queue
+ * element. Such problems are caused by one of the queues in the other
+ * non-x264enc streams/branches filling up and blocking upstream. They can
+ * be fixed by relaxing the default time/size/buffer limits on the queue
+ * elements in the non-x264 branches, or using a (single) multiqueue element
+ * for all branches. Also see the last example below.
+ * </note>
+ *
* <refsect2>
* <title>Example pipeline</title>
* |[
* ]| This example pipeline will encode a test video source to H264 using fixed
* quantization, and muxes it in a Matroska container.
* |[
- * gst-launch -v videotestsrc num-buffers=1000 ! x264enc pass=5 quantizer=25 speed-preset=6 profile=1 ! \
+ * gst-launch -v videotestsrc num-buffers=1000 ! x264enc pass=5 quantizer=25 speed-preset=6 ! video/x-h264, profile=baseline ! \
* qtmux ! filesink location=videotestsrc.mov
* ]| This example pipeline will encode a test video source to H264 using
* constant quality at around Q25 using the 'medium' speed/quality preset and
* restricting the options used so that the output is H.264 Baseline Profile
* compliant and finally multiplexing the output in Quicktime mov format.
+ * |[
+ * gst-launch -v videotestsrc num-buffers=1000 ! tee name=t ! queue ! xvimagesink \
+ * t. ! queue ! x264enc rc-lookahead=5 ! fakesink
+ * ]| This example pipeline will encode a test video source to H264 while
+ * displaying the input material at the same time. As mentioned above,
+ * specific settings are needed in this case to avoid pipeline stalling.
+ * Depending on goals and context, other approaches are possible, e.g.
+ * tune=zerolatency might be configured, or queue sizes increased.
* </refsect2>
*/
#include "gstx264enc.h"
+#include <gst/pbutils/pbutils.h>
+
+#if X264_BUILD >= 71
+#define X264_DELAYED_FRAMES_API
+#endif
+
#if X264_BUILD >= 76
#define X264_ENC_NALS 1
#endif
#define X264_MB_RC
#endif
+#if X264_BUILD >= 78
+/* b-pyramid was available before but was changed from boolean here */
+#define X264_B_PYRAMID
+#endif
+
#if X264_BUILD >= 80
#define X264_ENH_THREADING
#endif
ARG_TUNE,
};
-#define ARG_THREADS_DEFAULT 1
+#define ARG_THREADS_DEFAULT 0 /* 0 means 'auto' which is 1.5x number of CPU cores */
#define ARG_PASS_DEFAULT 0
#define ARG_QUANTIZER_DEFAULT 21
#define ARG_MULTIPASS_CACHE_FILE_DEFAULT "x264.log"
#define ARG_RC_MB_TREE_DEFAULT TRUE
#define ARG_RC_LOOKAHEAD_DEFAULT 40
#define ARG_INTRA_REFRESH_DEFAULT FALSE
-#define ARG_PROFILE_DEFAULT 1 /* Main profile matches current defaults */
+#define ARG_PROFILE_DEFAULT 2 /* 'Main Profile' - matches profile of property defaults */
#define ARG_OPTION_STRING_DEFAULT ""
static GString *x264enc_defaults;
-#define ARG_SPEED_PRESET_DEFAULT 0 /* no preset */
+#define ARG_SPEED_PRESET_DEFAULT 6 /* 'medium' preset - matches x264 CLI default */
#define ARG_PSY_TUNE_DEFAULT 0 /* no psy tuning */
#define ARG_TUNE_DEFAULT 0 /* no tuning */
+enum
+{
+ GST_X264_ENC_STREAM_FORMAT_FROM_PROPERTY,
+ GST_X264_ENC_STREAM_FORMAT_AVC,
+ GST_X264_ENC_STREAM_FORMAT_BYTE_STREAM
+};
+
enum
{
GST_X264_ENC_PASS_CBR = 0,
static const GEnumValue pass_types[] = {
{GST_X264_ENC_PASS_CBR, "Constant Bitrate Encoding", "cbr"},
- {GST_X264_ENC_PASS_QUANT, "Constant Quantizer", "quant"},
+ {GST_X264_ENC_PASS_QUANT, "Constant Quantizer (debugging only)", "quant"},
{GST_X264_ENC_PASS_QUAL, "Constant Quality", "qual"},
{GST_X264_ENC_PASS_PASS1, "VBR Encoding - Pass 1", "pass1"},
{GST_X264_ENC_PASS_PASS2, "VBR Encoding - Pass 2", "pass2"},
{0x0, "No tuning", "none"},
{0x1, "Still image", "stillimage"},
{0x2, "Fast decode", "fastdecode"},
- {0x4, "Zero latency", "zerolatency"},
+ {0x4, "Zero latency (requires constant framerate)", "zerolatency"},
{0, NULL, NULL},
};
static GType tune_type = 0;
if (!tune_type) {
- tune_type = g_flags_register_static ("GstX264EncTune", tune_types);
+ tune_type = g_flags_register_static ("GstX264EncTune", tune_types + 1);
}
return tune_type;
}
{
int i = 1;
- if (x264enc->tunings && x264enc->tunings->len)
+ if (x264enc->tunings)
g_string_free (x264enc->tunings, TRUE);
if (x264enc->psy_tune) {
GST_PAD_SINK,
GST_PAD_ALWAYS,
GST_STATIC_CAPS ("video/x-raw-yuv, "
- "format = (fourcc) I420, "
+ "format = (fourcc) { I420, YV12 }, "
"framerate = (fraction) [0, MAX], "
"width = (int) [ 16, MAX ], " "height = (int) [ 16, MAX ]")
);
"framerate = (fraction) [0/1, MAX], "
"width = (int) [ 1, MAX ], " "height = (int) [ 1, MAX ], "
"stream-format = (string) { byte-stream, avc }, "
- "alignment = (string) { au }")
+ "alignment = (string) { au }, "
+ "profile = (string) { high-10, high, main, constrained-baseline, "
+ "high-10-intra }")
);
static void gst_x264_enc_finalize (GObject * object);
static void gst_x264_enc_close_encoder (GstX264Enc * encoder);
static gboolean gst_x264_enc_sink_set_caps (GstPad * pad, GstCaps * caps);
+static GstCaps *gst_x264_enc_sink_get_caps (GstPad * pad);
static gboolean gst_x264_enc_sink_event (GstPad * pad, GstEvent * event);
static gboolean gst_x264_enc_src_event (GstPad * pad, GstEvent * event);
static GstFlowReturn gst_x264_enc_chain (GstPad * pad, GstBuffer * buf);
"Josef Zlomek <josef.zlomek@itonis.tv>, "
"Mark Nauwelaerts <mnauw@users.sf.net>");
- gst_element_class_add_pad_template (element_class,
- gst_static_pad_template_get (&src_factory));
- gst_element_class_add_pad_template (element_class,
- gst_static_pad_template_get (&sink_factory));
+ gst_element_class_add_static_pad_template (element_class, &src_factory);
+ gst_element_class_add_static_pad_template (element_class, &sink_factory);
}
/* don't forget to free the string after use */
g_object_class_install_property (gobject_class, ARG_PASS,
g_param_spec_enum ("pass", "Encoding pass/type",
"Encoding pass/type", GST_X264_ENC_PASS_TYPE,
- ARG_PASS_DEFAULT, G_PARAM_READWRITE));
+ ARG_PASS_DEFAULT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_object_class_install_property (gobject_class, ARG_QUANTIZER,
g_param_spec_uint ("quantizer", "Constant Quantizer",
"Constant quantizer or quality to apply",
- 1, 50, ARG_QUANTIZER_DEFAULT, G_PARAM_READWRITE));
+ 1, 50, ARG_QUANTIZER_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_object_class_install_property (gobject_class, ARG_BITRATE,
g_param_spec_uint ("bitrate", "Bitrate", "Bitrate in kbit/sec", 1,
- 100 * 1024, ARG_BITRATE_DEFAULT, G_PARAM_READWRITE));
+ 100 * 1024, ARG_BITRATE_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS |
+ GST_PARAM_MUTABLE_PLAYING));
g_object_class_install_property (gobject_class, ARG_VBV_BUF_CAPACITY,
g_param_spec_uint ("vbv-buf-capacity", "VBV buffer capacity",
"Size of the VBV buffer in milliseconds",
- 300, 10000, ARG_VBV_BUF_CAPACITY_DEFAULT, G_PARAM_READWRITE));
+ 0, 10000, ARG_VBV_BUF_CAPACITY_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS |
+ GST_PARAM_MUTABLE_PLAYING));
#ifdef X264_PRESETS
g_object_class_install_property (gobject_class, ARG_SPEED_PRESET,
"Preset name for speed/quality tradeoff options (can affect decode "
"compatibility - impose restrictions separately for your target decoder)",
GST_X264_ENC_SPEED_PRESET_TYPE, ARG_SPEED_PRESET_DEFAULT,
- G_PARAM_READWRITE));
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_object_class_install_property (gobject_class, ARG_PSY_TUNE,
g_param_spec_enum ("psy-tune", "Psychovisual tuning preset",
"Preset name for psychovisual tuning options",
- GST_X264_ENC_PSY_TUNE_TYPE, ARG_PSY_TUNE_DEFAULT, G_PARAM_READWRITE));
+ GST_X264_ENC_PSY_TUNE_TYPE, ARG_PSY_TUNE_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_object_class_install_property (gobject_class, ARG_TUNE,
g_param_spec_flags ("tune", "Content tuning preset",
"Preset name for non-psychovisual tuning options",
- GST_X264_ENC_TUNE_TYPE, ARG_TUNE_DEFAULT, G_PARAM_READWRITE));
+ GST_X264_ENC_TUNE_TYPE, ARG_TUNE_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_object_class_install_property (gobject_class, ARG_PROFILE,
g_param_spec_enum ("profile", "H.264 profile",
"Apply restrictions to meet H.264 Profile constraints. This will "
- "override other properties if necessary.",
- GST_X264_ENC_PROFILE_TYPE, ARG_PROFILE_DEFAULT, G_PARAM_READWRITE));
+ "override other properties if necessary. This will only be used "
+ "if downstream elements do not specify a profile in their caps (DEPRECATED)",
+ GST_X264_ENC_PROFILE_TYPE, ARG_PROFILE_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
#endif /* X264_PRESETS */
g_object_class_install_property (gobject_class, ARG_OPTION_STRING,
g_param_spec_string ("option-string", "Option string",
"String of x264 options (overridden by element properties)",
- ARG_OPTION_STRING_DEFAULT, G_PARAM_READWRITE));
+ ARG_OPTION_STRING_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
/* options for which we _do_ use string equivalents */
g_object_class_install_property (gobject_class, ARG_THREADS,
g_param_spec_uint ("threads", "Threads",
"Number of threads used by the codec (0 for automatic)",
- 0, 4, ARG_THREADS_DEFAULT, G_PARAM_READWRITE));
+ 0, 4, ARG_THREADS_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
/* NOTE: this first string append doesn't require the ':' delimiter but the
* rest do */
g_string_append_printf (x264enc_defaults, "threads=%d", ARG_THREADS_DEFAULT);
g_object_class_install_property (gobject_class, ARG_SLICED_THREADS,
g_param_spec_boolean ("sliced-threads", "Sliced Threads",
"Low latency but lower efficiency threading",
- ARG_SLICED_THREADS_DEFAULT, G_PARAM_READWRITE));
+ ARG_SLICED_THREADS_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":sliced-threads=%d",
ARG_SLICED_THREADS_DEFAULT);
g_object_class_install_property (gobject_class, ARG_SYNC_LOOKAHEAD,
g_param_spec_int ("sync-lookahead", "Sync Lookahead",
"Number of buffer frames for threaded lookahead (-1 for automatic)",
- -1, 250, ARG_SYNC_LOOKAHEAD_DEFAULT, G_PARAM_READWRITE));
+ -1, 250, ARG_SYNC_LOOKAHEAD_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":sync-lookahead=%d",
ARG_SYNC_LOOKAHEAD_DEFAULT);
#endif
g_object_class_install_property (gobject_class, ARG_STATS_FILE,
g_param_spec_string ("stats-file", "Stats File",
"Filename for multipass statistics (deprecated, use multipass-cache-file)",
- ARG_STATS_FILE_DEFAULT, G_PARAM_READWRITE));
+ ARG_STATS_FILE_DEFAULT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_object_class_install_property (gobject_class, ARG_MULTIPASS_CACHE_FILE,
g_param_spec_string ("multipass-cache-file", "Multipass Cache File",
"Filename for multipass cache file",
- ARG_MULTIPASS_CACHE_FILE_DEFAULT, G_PARAM_READWRITE));
+ ARG_MULTIPASS_CACHE_FILE_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":stats=%s",
ARG_MULTIPASS_CACHE_FILE_DEFAULT);
g_object_class_install_property (gobject_class, ARG_BYTE_STREAM,
g_param_spec_boolean ("byte-stream", "Byte Stream",
"Generate byte stream format of NALU", ARG_BYTE_STREAM_DEFAULT,
- G_PARAM_READWRITE));
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":annexb=%d",
ARG_BYTE_STREAM_DEFAULT);
#ifdef X264_INTRA_REFRESH
g_object_class_install_property (gobject_class, ARG_INTRA_REFRESH,
g_param_spec_boolean ("intra-refresh", "Intra Refresh",
"Use Periodic Intra Refresh instead of IDR frames",
- ARG_INTRA_REFRESH_DEFAULT, G_PARAM_READWRITE));
+ ARG_INTRA_REFRESH_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":intra-refresh=%d",
ARG_INTRA_REFRESH_DEFAULT);
#endif
g_object_class_install_property (gobject_class, ARG_ME,
g_param_spec_enum ("me", "Motion Estimation",
"Integer pixel motion estimation method", GST_X264_ENC_ME_TYPE,
- ARG_ME_DEFAULT, G_PARAM_READWRITE));
+ ARG_ME_DEFAULT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":me=%s",
x264_motion_est_names[ARG_ME_DEFAULT]);
g_object_class_install_property (gobject_class, ARG_SUBME,
g_param_spec_uint ("subme", "Subpixel Motion Estimation",
- "Subpixel motion estimation and partition decision quality: 1=fast, 6=best",
- 1, 6, ARG_SUBME_DEFAULT, G_PARAM_READWRITE));
+ "Subpixel motion estimation and partition decision quality: 1=fast, 10=best",
+ 1, 10, ARG_SUBME_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":subme=%d", ARG_SUBME_DEFAULT);
g_object_class_install_property (gobject_class, ARG_ANALYSE,
g_param_spec_flags ("analyse", "Analyse", "Partitions to consider",
- GST_X264_ENC_ANALYSE_TYPE, ARG_ANALYSE_DEFAULT, G_PARAM_READWRITE));
+ GST_X264_ENC_ANALYSE_TYPE, ARG_ANALYSE_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
partitions = gst_x264_enc_build_partitions (ARG_ANALYSE_DEFAULT);
if (partitions) {
g_string_append_printf (x264enc_defaults, ":partitions=%s", partitions);
g_object_class_install_property (gobject_class, ARG_DCT8x8,
g_param_spec_boolean ("dct8x8", "DCT8x8",
"Adaptive spatial transform size", ARG_DCT8x8_DEFAULT,
- G_PARAM_READWRITE));
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":8x8dct=%d", ARG_DCT8x8_DEFAULT);
g_object_class_install_property (gobject_class, ARG_REF,
g_param_spec_uint ("ref", "Reference Frames",
"Number of reference frames",
- 1, 12, ARG_REF_DEFAULT, G_PARAM_READWRITE));
+ 1, 12, ARG_REF_DEFAULT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":ref=%d", ARG_REF_DEFAULT);
g_object_class_install_property (gobject_class, ARG_BFRAMES,
g_param_spec_uint ("bframes", "B-Frames",
"Number of B-frames between I and P",
- 0, 4, ARG_BFRAMES_DEFAULT, G_PARAM_READWRITE));
+ 0, 4, ARG_BFRAMES_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":bframes=%d", ARG_BFRAMES_DEFAULT);
g_object_class_install_property (gobject_class, ARG_B_ADAPT,
g_param_spec_boolean ("b-adapt", "B-Adapt",
"Automatically decide how many B-frames to use",
- ARG_B_ADAPT_DEFAULT, G_PARAM_READWRITE));
+ ARG_B_ADAPT_DEFAULT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":b-adapt=%d", ARG_B_ADAPT_DEFAULT);
g_object_class_install_property (gobject_class, ARG_B_PYRAMID,
g_param_spec_boolean ("b-pyramid", "B-Pyramid",
"Keep some B-frames as references", ARG_B_PYRAMID_DEFAULT,
- G_PARAM_READWRITE));
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
+#ifdef X264_B_PYRAMID
+ g_string_append_printf (x264enc_defaults, ":b-pyramid=%s",
+ x264_b_pyramid_names[ARG_B_PYRAMID_DEFAULT]);
+#else
g_string_append_printf (x264enc_defaults, ":b-pyramid=%d",
ARG_B_PYRAMID_DEFAULT);
+#endif /* X264_B_PYRAMID */
g_object_class_install_property (gobject_class, ARG_WEIGHTB,
g_param_spec_boolean ("weightb", "Weighted B-Frames",
"Weighted prediction for B-frames", ARG_WEIGHTB_DEFAULT,
- G_PARAM_READWRITE));
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":weightb=%d", ARG_WEIGHTB_DEFAULT);
g_object_class_install_property (gobject_class, ARG_SPS_ID,
g_param_spec_uint ("sps-id", "SPS ID",
"SPS and PPS ID number",
- 0, 31, ARG_SPS_ID_DEFAULT, G_PARAM_READWRITE));
+ 0, 31, ARG_SPS_ID_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":sps-id=%d", ARG_SPS_ID_DEFAULT);
g_object_class_install_property (gobject_class, ARG_AU_NALU,
g_param_spec_boolean ("aud", "AUD",
"Use AU (Access Unit) delimiter", ARG_AU_NALU_DEFAULT,
- G_PARAM_READWRITE));
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":aud=%d", ARG_AU_NALU_DEFAULT);
g_object_class_install_property (gobject_class, ARG_TRELLIS,
g_param_spec_boolean ("trellis", "Trellis quantization",
"Enable trellis searched quantization", ARG_TRELLIS_DEFAULT,
- G_PARAM_READWRITE));
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":trellis=%d", ARG_TRELLIS_DEFAULT);
g_object_class_install_property (gobject_class, ARG_KEYINT_MAX,
g_param_spec_uint ("key-int-max", "Key-frame maximal interval",
"Maximal distance between two key-frames (0 for automatic)",
- 0, G_MAXINT, ARG_KEYINT_MAX_DEFAULT, G_PARAM_READWRITE));
+ 0, G_MAXINT, ARG_KEYINT_MAX_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":keyint=%d",
ARG_KEYINT_MAX_DEFAULT);
g_object_class_install_property (gobject_class, ARG_CABAC,
g_param_spec_boolean ("cabac", "Use CABAC", "Enable CABAC entropy coding",
- ARG_CABAC_DEFAULT, G_PARAM_READWRITE));
+ ARG_CABAC_DEFAULT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":cabac=%d", ARG_CABAC_DEFAULT);
g_object_class_install_property (gobject_class, ARG_QP_MIN,
g_param_spec_uint ("qp-min", "Minimum Quantizer",
- "Minimum quantizer", 1, 51, ARG_QP_MIN_DEFAULT, G_PARAM_READWRITE));
+ "Minimum quantizer", 1, 51, ARG_QP_MIN_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":qpmin=%d", ARG_QP_MIN_DEFAULT);
g_object_class_install_property (gobject_class, ARG_QP_MAX,
g_param_spec_uint ("qp-max", "Maximum Quantizer",
- "Maximum quantizer", 1, 51, ARG_QP_MAX_DEFAULT, G_PARAM_READWRITE));
+ "Maximum quantizer", 1, 51, ARG_QP_MAX_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":qpmax=%d", ARG_QP_MAX_DEFAULT);
g_object_class_install_property (gobject_class, ARG_QP_STEP,
g_param_spec_uint ("qp-step", "Maximum Quantizer Difference",
"Maximum quantizer difference between frames",
- 1, 50, ARG_QP_STEP_DEFAULT, G_PARAM_READWRITE));
+ 1, 50, ARG_QP_STEP_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":qpstep=%d", ARG_QP_STEP_DEFAULT);
g_object_class_install_property (gobject_class, ARG_IP_FACTOR,
g_param_spec_float ("ip-factor", "IP-Factor",
"Quantizer factor between I- and P-frames",
- 0, 2, ARG_IP_FACTOR_DEFAULT, G_PARAM_READWRITE));
+ 0, 2, ARG_IP_FACTOR_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":ip-factor=%f",
ARG_IP_FACTOR_DEFAULT);
g_object_class_install_property (gobject_class, ARG_PB_FACTOR,
g_param_spec_float ("pb-factor", "PB-Factor",
"Quantizer factor between P- and B-frames", 0, 2,
- ARG_PB_FACTOR_DEFAULT, G_PARAM_READWRITE));
+ ARG_PB_FACTOR_DEFAULT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":pb-factor=%f",
ARG_PB_FACTOR_DEFAULT);
#ifdef X264_MB_RC
g_object_class_install_property (gobject_class, ARG_RC_MB_TREE,
g_param_spec_boolean ("mb-tree", "Macroblock Tree",
"Macroblock-Tree ratecontrol",
- ARG_RC_MB_TREE_DEFAULT, G_PARAM_READWRITE));
+ ARG_RC_MB_TREE_DEFAULT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":mbtree=%d",
ARG_RC_MB_TREE_DEFAULT);
g_object_class_install_property (gobject_class, ARG_RC_LOOKAHEAD,
g_param_spec_int ("rc-lookahead", "Rate Control Lookahead",
"Number of frames for frametype lookahead", 0, 250,
- ARG_RC_LOOKAHEAD_DEFAULT, G_PARAM_READWRITE));
+ ARG_RC_LOOKAHEAD_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":rc-lookahead=%d",
ARG_RC_LOOKAHEAD_DEFAULT);
#endif
g_object_class_install_property (gobject_class, ARG_NR,
g_param_spec_uint ("noise-reduction", "Noise Reduction",
"Noise reduction strength",
- 0, 100000, ARG_NR_DEFAULT, G_PARAM_READWRITE));
+ 0, 100000, ARG_NR_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":nr=%d", ARG_NR_DEFAULT);
g_object_class_install_property (gobject_class, ARG_INTERLACED,
g_param_spec_boolean ("interlaced", "Interlaced",
- "Interlaced material", ARG_INTERLACED_DEFAULT, G_PARAM_READWRITE));
+ "Interlaced material", ARG_INTERLACED_DEFAULT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_string_append_printf (x264enc_defaults, ":interlaced=%d",
ARG_INTERLACED_DEFAULT);
encoder->sinkpad = gst_pad_new_from_static_template (&sink_factory, "sink");
gst_pad_set_setcaps_function (encoder->sinkpad,
GST_DEBUG_FUNCPTR (gst_x264_enc_sink_set_caps));
+ gst_pad_set_getcaps_function (encoder->sinkpad,
+ GST_DEBUG_FUNCPTR (gst_x264_enc_sink_get_caps));
gst_pad_set_event_function (encoder->sinkpad,
GST_DEBUG_FUNCPTR (gst_x264_enc_sink_event));
gst_pad_set_chain_function (encoder->sinkpad,
encoder->x264enc = NULL;
encoder->width = 0;
encoder->height = 0;
+ encoder->current_byte_stream = GST_X264_ENC_STREAM_FORMAT_FROM_PROPERTY;
GST_OBJECT_LOCK (encoder);
encoder->i_type = X264_TYPE_AUTO;
#define FREE_STRING(ptr) \
if (ptr) \
- ptr = (GString *)g_string_free (ptr, TRUE);
+ g_string_free (ptr, TRUE);
FREE_STRING (encoder->tunings);
FREE_STRING (encoder->option_string);
encoder->option_string->str);
if (gst_x264_enc_parse_options (encoder,
encoder->option_string->str) == FALSE) {
- GST_DEBUG_OBJECT (encoder,
- "Failed to parse internal option string. This could be due to use of an "
- "old libx264 version.", encoder->option_string->str);
+ GST_DEBUG_OBJECT (encoder, "Failed to parse internal option string. "
+ "This could be due to use of an old libx264 version. Option string "
+ "was: %s", encoder->option_string->str);
}
}
case GST_X264_ENC_PASS_QUAL:
encoder->x264param.rc.i_rc_method = X264_RC_CRF;
encoder->x264param.rc.f_rf_constant = encoder->quantizer;
+ encoder->x264param.rc.i_vbv_max_bitrate = encoder->bitrate;
+ encoder->x264param.rc.i_vbv_buffer_size
+ = encoder->x264param.rc.i_vbv_max_bitrate
+ * encoder->vbv_buf_capacity / 1000;
break;
case GST_X264_ENC_PASS_CBR:
case GST_X264_ENC_PASS_PASS1:
encoder->x264param.rc.i_rc_method = X264_RC_ABR;
encoder->x264param.rc.i_bitrate = encoder->bitrate;
encoder->x264param.rc.i_vbv_max_bitrate = encoder->bitrate;
- encoder->x264param.rc.i_vbv_buffer_size
- = encoder->x264param.rc.i_vbv_max_bitrate
+ encoder->x264param.rc.i_vbv_buffer_size =
+ encoder->x264param.rc.i_vbv_max_bitrate
* encoder->vbv_buf_capacity / 1000;
pass = encoder->pass & 0xF;
break;
break;
}
+#if X264_BUILD >= 81 && X264_BUILD < 106
+ /* When vfr is disabled, libx264 ignores buffer timestamps. This causes
+ * issues with rate control in libx264 with our nanosecond timebase. This
+ * has been fixed upstream in libx264 but this workaround is required for
+ * pre-fix versions. */
+ if (!encoder->x264param.b_vfr_input) {
+ if (encoder->x264param.i_fps_num == 0) {
+ GST_ELEMENT_ERROR (encoder, STREAM, ENCODE,
+ ("Constant framerate is required."),
+ ("The framerate caps (%d/%d) indicate VFR but VFR is disabled in libx264. (Is the zerolatency tuning in use?)",
+ encoder->x264param.i_fps_num, encoder->x264param.i_fps_den));
+ return FALSE;
+ }
+ encoder->x264param.i_timebase_num = encoder->x264param.i_fps_den;
+ encoder->x264param.i_timebase_den = encoder->x264param.i_fps_num;
+ }
+#endif
+
#ifdef X264_PRESETS
- if (encoder->profile
- && x264_param_apply_profile (&encoder->x264param,
- x264_profile_names[encoder->profile - 1])) {
- GST_WARNING_OBJECT (encoder, "Bad profile name: %s",
- x264_profile_names[encoder->profile - 1]);
+ if (encoder->peer_profile) {
+ if (x264_param_apply_profile (&encoder->x264param, encoder->peer_profile))
+ GST_WARNING_OBJECT (encoder, "Bad downstream profile name: %s",
+ encoder->peer_profile);
+ } else if (encoder->profile) {
+ if (x264_param_apply_profile (&encoder->x264param,
+ x264_profile_names[encoder->profile - 1]))
+ GST_WARNING_OBJECT (encoder, "Bad profile name: %s",
+ x264_profile_names[encoder->profile - 1]);
}
#endif /* X264_PRESETS */
+ /* If using an intra profile, all frames are intra frames */
+ if (encoder->peer_intra_profile)
+ encoder->x264param.i_keyint_max = encoder->x264param.i_keyint_min = 1;
+
+ /* Enforce level limits if they were in the caps */
+ if (encoder->peer_level) {
+ encoder->x264param.i_level_idc = encoder->peer_level->level_idc;
+
+ encoder->x264param.rc.i_bitrate = MIN (encoder->x264param.rc.i_bitrate,
+ encoder->peer_level->bitrate);
+ encoder->x264param.rc.i_vbv_max_bitrate =
+ MIN (encoder->x264param.rc.i_vbv_max_bitrate,
+ encoder->peer_level->bitrate);
+ encoder->x264param.rc.i_vbv_buffer_size =
+ MIN (encoder->x264param.rc.i_vbv_buffer_size, encoder->peer_level->cpb);
+ encoder->x264param.analyse.i_mv_range =
+ MIN (encoder->x264param.analyse.i_mv_range,
+ encoder->peer_level->mv_range);
+
+ if (encoder->peer_level->frame_only) {
+ encoder->x264param.b_interlaced = FALSE;
+#if X264_BUILD >= 95
+ encoder->x264param.b_fake_interlaced = FALSE;
+#endif
+ }
+ }
+
+ encoder->reconfig = FALSE;
+
GST_OBJECT_UNLOCK (encoder);
encoder->x264enc = x264_encoder_open (&encoder->x264param);
}
}
+static gboolean
+gst_x264_enc_set_profile_and_level (GstX264Enc * encoder, GstCaps * caps)
+{
+ x264_nal_t *nal;
+ int i_nal;
+ int header_return;
+ gint sps_ni = 0;
+ guint8 *sps;
+
+
+ header_return = x264_encoder_headers (encoder->x264enc, &nal, &i_nal);
+ if (header_return < 0) {
+ GST_ELEMENT_ERROR (encoder, STREAM, ENCODE, ("Encode x264 header failed."),
+ ("x264_encoder_headers return code=%d", header_return));
+ return FALSE;
+ }
+
+ /* old x264 returns SEI, SPS and PPS, newer one has SEI last */
+ if (i_nal == 3 && nal[sps_ni].i_type != 7)
+ sps_ni = 1;
+
+ /* old style API: nal's are not encapsulated, and have no sync/size prefix,
+ * new style API: nal's are encapsulated, and have 4-byte size prefix */
+#ifndef X264_ENC_NALS
+ sps = nal[sps_ni].p_payload;
+#else
+ sps = nal[sps_ni].p_payload + 4;
+ /* skip NAL unit type */
+ sps++;
+#endif
+
+ gst_codec_utils_h264_caps_set_level_and_profile (caps, sps, 3);
+
+ return TRUE;
+}
+
/*
* Returns: Buffer with the stream headers.
*/
@@ -1287,7 +1453,14 @@ gst_x264_enc_set_src_caps (GstX264Enc * encoder, GstPad * pad, GstCaps * caps)
structure = gst_caps_get_structure (outcaps, 0);
- if (!encoder->byte_stream) {
+ if (encoder->current_byte_stream == GST_X264_ENC_STREAM_FORMAT_FROM_PROPERTY) {
+ if (encoder->byte_stream) {
+ encoder->current_byte_stream = GST_X264_ENC_STREAM_FORMAT_BYTE_STREAM;
+ } else {
+ encoder->current_byte_stream = GST_X264_ENC_STREAM_FORMAT_AVC;
+ }
+ }
+ if (encoder->current_byte_stream == GST_X264_ENC_STREAM_FORMAT_AVC) {
buf = gst_x264_enc_header_buf (encoder);
if (buf != NULL) {
gst_caps_set_simple (outcaps, "codec_data", GST_TYPE_BUFFER, buf, NULL);
@@ -1300,6 +1473,11 @@ gst_x264_enc_set_src_caps (GstX264Enc * encoder, GstPad * pad, GstCaps * caps)
}
gst_structure_set (structure, "alignment", G_TYPE_STRING, "au", NULL);
+ if (!gst_x264_enc_set_profile_and_level (encoder, outcaps)) {
+ gst_caps_unref (outcaps);
+ return FALSE;
+ }
+
res = gst_pad_set_caps (pad, outcaps);
gst_caps_unref (outcaps);
gst_x264_enc_sink_set_caps (GstPad * pad, GstCaps * caps)
{
GstX264Enc *encoder = GST_X264_ENC (GST_OBJECT_PARENT (pad));
+ GstVideoFormat format;
gint width, height;
gint fps_num, fps_den;
gint par_num, par_den;
gint i;
+ GstCaps *peer_caps;
+ const GstCaps *template_caps;
+ GstCaps *allowed_caps = NULL;
+ gboolean level_ok = TRUE;
/* get info from caps */
- /* only I420 supported for now; so apparently claims x264enc ? */
- if (!gst_video_format_parse_caps (caps, &encoder->format, &width, &height) ||
- encoder->format != GST_VIDEO_FORMAT_I420)
+ if (!gst_video_format_parse_caps (caps, &format, &width, &height))
return FALSE;
if (!gst_video_parse_caps_framerate (caps, &fps_num, &fps_den))
return FALSE;
par_den = 1;
}
- /* If the encoder is initialized, do not
- reinitialize it again if not necessary */
+ /* If the encoder is initialized, do not reinitialize it again if not
+ * necessary */
if (encoder->x264enc) {
if (width == encoder->width && height == encoder->height
&& fps_num == encoder->fps_num && fps_den == encoder->fps_den
}
/* store input description */
+ encoder->format = format;
encoder->width = width;
encoder->height = height;
encoder->fps_num = fps_num;
encoder->par_num = par_num;
encoder->par_den = par_den;
- /* prepare a cached image description */
+ /* prepare a cached image description */
encoder->image_size = gst_video_format_get_size (encoder->format, width,
height);
for (i = 0; i < 3; ++i) {
- /* only offsets now, is shifted later */
+ /* only offsets now, is shifted later. Offsets will be for Y, U, V so we
+ * can just feed YV12 as I420 to the decoder later */
encoder->offset[i] = gst_video_format_get_component_offset (encoder->format,
i, width, height);
encoder->stride[i] = gst_video_format_get_row_stride (encoder->format,
i, width);
}
+ encoder->peer_profile = NULL;
+ encoder->peer_intra_profile = FALSE;
+ encoder->peer_level = NULL;
+
+ /* FIXME: Remove THIS bit in 0.11 when the profile property is removed */
+ peer_caps = gst_pad_peer_get_caps_reffed (encoder->srcpad);
+ if (peer_caps) {
+ gint i;
+ gboolean has_profile_or_level_or_format = FALSE;
+
+ for (i = 0; i < gst_caps_get_size (peer_caps); i++) {
+ GstStructure *s = gst_caps_get_structure (peer_caps, i);
+
+ if (gst_structure_has_name (s, "video/x-h264") &&
+ (gst_structure_has_field (s, "profile") ||
+ gst_structure_has_field (s, "level") ||
+ gst_structure_has_field (s, "stream-format"))) {
+ has_profile_or_level_or_format = TRUE;
+ break;
+ }
+ }
+
+ if (has_profile_or_level_or_format) {
+ template_caps = gst_pad_get_pad_template_caps (encoder->srcpad);
+
+ allowed_caps = gst_caps_intersect (peer_caps, template_caps);
+ }
+
+ gst_caps_unref (peer_caps);
+ }
+
+ /* Replace the bit since FIXME with this
+ * allowed_caps = gst_pad_get_allowed_caps (encoder->srcpad);
+ */
+
+ if (allowed_caps) {
+ GstStructure *s;
+ const gchar *profile;
+ const gchar *level;
+ const gchar *stream_format;
+
+ if (gst_caps_is_empty (allowed_caps)) {
+ gst_caps_unref (allowed_caps);
+ return FALSE;
+ }
+
+ allowed_caps = gst_caps_make_writable (allowed_caps);
+ gst_pad_fixate_caps (encoder->srcpad, allowed_caps);
+ s = gst_caps_get_structure (allowed_caps, 0);
+
+ profile = gst_structure_get_string (s, "profile");
+ if (profile) {
+ if (!strcmp (profile, "constrained-baseline")) {
+ encoder->peer_profile = "baseline";
+ } else if (!strcmp (profile, "high-10-intra")) {
+ encoder->peer_intra_profile = TRUE;
+ encoder->peer_profile = "high10";
+ } else if (!strcmp (profile, "high-10")) {
+ encoder->peer_profile = "high10";
+ } else if (!strcmp (profile, "high")) {
+ encoder->peer_profile = "high";
+ } else if (!strcmp (profile, "main")) {
+ encoder->peer_profile = "main";
+ } else {
+ g_assert_not_reached ();
+ }
+ }
+
+ level = gst_structure_get_string (s, "level");
+ if (level) {
+ int level_idc = gst_codec_utils_h264_get_level_idc (level);
+
+ if (level_idc) {
+ gint i;
+
+ for (i = 0; x264_levels[i].level_idc; i++) {
+ if (level_idc == x264_levels[i].level_idc) {
+ int mb_width = (width + 15) / 16;
+ int mb_height = (height + 15) / 16;
+ int mbs = mb_width * mb_height;
+
+ if (x264_levels[i].frame_size < mbs ||
+ x264_levels[i].frame_size * 8 < mb_width * mb_width ||
+ x264_levels[i].frame_size * 8 < mb_height * mb_height) {
+ GST_WARNING_OBJECT (encoder,
+ "Frame size larger than level %s allows", level);
+ level_ok = FALSE;
+ break;
+ }
+
+ if (fps_den &&
+ x264_levels[i].mbps < (gint64) mbs * fps_num / fps_den) {
+ GST_WARNING_OBJECT (encoder,
+ "Macroblock rate higher than level %s allows", level);
+ level_ok = FALSE;
+ break;
+ }
+
+ encoder->peer_level = &x264_levels[i];
+ break;
+ }
+ }
+ }
+ }
+
+ stream_format = gst_structure_get_string (s, "stream-format");
+ encoder->current_byte_stream = GST_X264_ENC_STREAM_FORMAT_FROM_PROPERTY;
+ if (stream_format) {
+ if (!strcmp (stream_format, "avc")) {
+ encoder->current_byte_stream = GST_X264_ENC_STREAM_FORMAT_AVC;
+ g_string_append_printf (encoder->option_string, ":annexb=0");
+ } else if (!strcmp (stream_format, "byte-stream")) {
+ encoder->current_byte_stream = GST_X264_ENC_STREAM_FORMAT_BYTE_STREAM;
+ g_string_append_printf (encoder->option_string, ":annexb=1");
+ } else {
+ /* means we have both in caps and _FROM_PROPERTY should be the option */
+ }
+ }
+
+ gst_caps_unref (allowed_caps);
+ }
+
+ if (!level_ok)
+ return FALSE;
+
if (!gst_x264_enc_init_encoder (encoder))
return FALSE;
return TRUE;
}
+static GstCaps *
+gst_x264_enc_sink_get_caps (GstPad * pad)
+{
+ GstX264Enc *encoder;
+ GstPad *peer;
+ GstCaps *caps;
+
+ encoder = GST_X264_ENC (gst_pad_get_parent (pad));
+ if (!encoder)
+ return gst_caps_new_empty ();
+
+ peer = gst_pad_get_peer (encoder->srcpad);
+ if (peer) {
+ const GstCaps *templcaps;
+ GstCaps *peercaps;
+ guint i, n;
+
+ peercaps = gst_pad_get_caps (peer);
+
+ /* Translate peercaps to YUV */
+ peercaps = gst_caps_make_writable (peercaps);
+ n = gst_caps_get_size (peercaps);
+ for (i = 0; i < n; i++) {
+ GstStructure *s = gst_caps_get_structure (peercaps, i);
+
+ gst_structure_set_name (s, "video/x-raw-yuv");
+ gst_structure_remove_field (s, "stream-format");
+ gst_structure_remove_field (s, "alignment");
+ }
+
+ templcaps = gst_pad_get_pad_template_caps (pad);
+
+ caps = gst_caps_intersect (peercaps, templcaps);
+ gst_caps_unref (peercaps);
+ gst_object_unref (peer);
+ peer = NULL;
+ } else {
+ caps = gst_caps_copy (gst_pad_get_pad_template_caps (pad));
+ }
+
+ /* If we already have caps return them */
+ if (GST_PAD_CAPS (pad) && gst_caps_can_intersect (GST_PAD_CAPS (pad), caps)) {
+ GstCaps *tmpcaps = gst_caps_copy (GST_PAD_CAPS (pad));
+
+ gst_caps_merge (tmpcaps, caps);
+ caps = tmpcaps;
+ }
+
+ gst_object_unref (encoder);
+
+ return caps;
+}
+
static gboolean
gst_x264_enc_src_event (GstPad * pad, GstEvent * event)
{
case GST_EVENT_EOS:
gst_x264_enc_flush_frames (encoder, TRUE);
break;
+ case GST_EVENT_TAG:{
+ GstTagList *tags = NULL;
+
+ event =
+ GST_EVENT (gst_mini_object_make_writable (GST_MINI_OBJECT (event)));
+
+ gst_event_parse_tag (event, &tags);
+ /* drop codec/video-codec and replace encoder/encoder-version */
+ gst_tag_list_remove_tag (tags, GST_TAG_VIDEO_CODEC);
+ gst_tag_list_remove_tag (tags, GST_TAG_CODEC);
+ gst_tag_list_add (tags, GST_TAG_MERGE_REPLACE, GST_TAG_ENCODER, "x264",
+ GST_TAG_ENCODER_VERSION, X264_BUILD, NULL);
+ /* push is done below */
+ break;
/* no flushing if flush received,
* buffers in encoder are considered (in the) past */
+ }
case GST_EVENT_CUSTOM_DOWNSTREAM:{
const GstStructure *s;
s = gst_event_get_structure (event);
#endif
int encoder_return;
GstFlowReturn ret;
- GstClockTime timestamp;
GstClockTime duration;
guint8 *data;
GstEvent *forcekeyunit_event = NULL;
if (G_UNLIKELY (encoder->x264enc == NULL))
return GST_FLOW_NOT_NEGOTIATED;
+ GST_OBJECT_LOCK (encoder);
+ if (encoder->reconfig) {
+ encoder->reconfig = FALSE;
+ if (x264_encoder_reconfig (encoder->x264enc, &encoder->x264param) < 0)
+ GST_WARNING_OBJECT (encoder, "Could not reconfigure");
+ }
+ GST_OBJECT_UNLOCK (encoder);
+
encoder_return = x264_encoder_encode (encoder->x264enc,
&nal, i_nal, pic_in, &pic_out);
nal_size =
x264_nal_encode (encoder->buffer + i_size + 4, &i_data, 0, &nal[i]);
- if (encoder->byte_stream)
+ g_assert (encoder->current_byte_stream !=
+ GST_X264_ENC_STREAM_FORMAT_FROM_PROPERTY);
+ if (encoder->current_byte_stream == GST_X264_ENC_STREAM_FORMAT_BYTE_STREAM)
GST_WRITE_UINT32_BE (encoder->buffer + i_size, 1);
else
GST_WRITE_UINT32_BE (encoder->buffer + i_size, nal_size);
in_buf = g_queue_pop_head (encoder->delay);
if (in_buf) {
- timestamp = GST_BUFFER_TIMESTAMP (in_buf);
duration = GST_BUFFER_DURATION (in_buf);
gst_buffer_unref (in_buf);
} else {
if (encoder->x264enc)
do {
flow_ret = gst_x264_enc_encode_frame (encoder, NULL, &i_nal, send);
+#ifdef X264_DELAYED_FRAMES_API
+ } while (flow_ret == GST_FLOW_OK
+ && x264_encoder_delayed_frames (encoder->x264enc) > 0);
+#else
+ /* note that this doesn't flush all frames for > 1 delayed frame */
} while (flow_ret == GST_FLOW_OK && i_nal > 0);
+#endif
/* in any case, make sure the delay queue is emptied */
while (!g_queue_is_empty (encoder->delay))
return ret;
}
+
+
+static void
+gst_x264_enc_reconfig (GstX264Enc * encoder)
+{
+ switch (encoder->pass) {
+ case GST_X264_ENC_PASS_QUAL:
+ encoder->x264param.rc.f_rf_constant = encoder->quantizer;
+ encoder->x264param.rc.i_vbv_max_bitrate = encoder->bitrate;
+ encoder->x264param.rc.i_vbv_buffer_size
+ = encoder->x264param.rc.i_vbv_max_bitrate
+ * encoder->vbv_buf_capacity / 1000;
+ break;
+ case GST_X264_ENC_PASS_CBR:
+ case GST_X264_ENC_PASS_PASS1:
+ case GST_X264_ENC_PASS_PASS2:
+ case GST_X264_ENC_PASS_PASS3:
+ default:
+ encoder->x264param.rc.i_bitrate = encoder->bitrate;
+ encoder->x264param.rc.i_vbv_max_bitrate = encoder->bitrate;
+ encoder->x264param.rc.i_vbv_buffer_size
+ = encoder->x264param.rc.i_vbv_max_bitrate
+ * encoder->vbv_buf_capacity / 1000;
+ break;
+ }
+
+ encoder->reconfig = TRUE;
+}
+
static void
gst_x264_enc_set_property (GObject * object, guint prop_id,
const GValue * value, GParamSpec * pspec)
GST_OBJECT_LOCK (encoder);
/* state at least matters for sps, bytestream, pass,
* and so by extension ... */
+
state = GST_STATE (encoder);
- if (state != GST_STATE_READY && state != GST_STATE_NULL)
+ if ((state != GST_STATE_READY && state != GST_STATE_NULL) &&
+ !(pspec->flags & GST_PARAM_MUTABLE_PLAYING))
goto wrong_state;
switch (prop_id) {
break;
case ARG_QUANTIZER:
encoder->quantizer = g_value_get_uint (value);
+ gst_x264_enc_reconfig (encoder);
break;
case ARG_BITRATE:
encoder->bitrate = g_value_get_uint (value);
+ gst_x264_enc_reconfig (encoder);
break;
case ARG_VBV_BUF_CAPACITY:
encoder->vbv_buf_capacity = g_value_get_uint (value);
+ gst_x264_enc_reconfig (encoder);
break;
case ARG_SPEED_PRESET:
encoder->speed_preset = g_value_get_enum (value);
break;
case ARG_B_PYRAMID:
encoder->b_pyramid = g_value_get_boolean (value);
+#ifdef X264_B_PYRAMID
+ g_string_append_printf (encoder->option_string, ":b-pyramid=%s",
+ x264_b_pyramid_names[encoder->b_pyramid]);
+#else
g_string_append_printf (encoder->option_string, ":b-pyramid=%d",
encoder->b_pyramid);
+#endif /* X264_B_PYRAMID */
break;
case ARG_WEIGHTB:
encoder->weightb = g_value_get_boolean (value);
/* ERROR */
wrong_state:
{
- GST_DEBUG_OBJECT (encoder, "setting property in wrong state");
+ GST_WARNING_OBJECT (encoder, "setting property in wrong state");
GST_OBJECT_UNLOCK (encoder);
}
}