]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gst-plugins-ugly0-10.git/commitdiff
formatting: trim trailing whitespace
authorStefan Kost <ensonic@users.sf.net>
Thu, 17 Feb 2011 16:06:51 +0000 (18:06 +0200)
committerStefan Kost <ensonic@users.sf.net>
Thu, 17 Feb 2011 16:06:51 +0000 (18:06 +0200)
ext/mad/gstmad.c
ext/mpeg2dec/gstmpeg2dec.c

index e931f163eac3669db62ceb34d339d2a221ea75e5..d6e4485d6a418a8a0739ea71eb974635e7d59691 100644 (file)
@@ -1038,10 +1038,10 @@ gst_mad_check_restart (GstMad * mad)
 }
 
 
-/* The following code has been taken from 
+/* The following code has been taken from
  * rhythmbox/metadata/monkey-media/stream-info-impl/id3-vfs/mp3bitrate.c
  * which took it from xine-lib/src/demuxers/demux_mpgaudio.c
- * This code has been kindly relicensed to LGPL by Thibaut Mattern and 
+ * This code has been kindly relicensed to LGPL by Thibaut Mattern and
  * Bastien Nocera
  */
 #define BE_32(x) GST_READ_UINT32_BE(x)
@@ -1642,11 +1642,11 @@ gst_mad_chain (GstPad * pad, GstBuffer * buffer)
 
           /* We are using the incoming timestamps to generate the outgoing ones
            * if available. However some muxing formats are not precise enough
-           * to allow us to generate a perfect stream. When converting the 
+           * to allow us to generate a perfect stream. When converting the
            * timestamp to a number of encoded samples so far we are introducing
-           * a lot of potential error compared to our accumulated number of 
-           * samples encoded. If the difference between those 2 numbers is 
-           * bigger than half a frame we then use the incoming timestamp 
+           * a lot of potential error compared to our accumulated number of
+           * samples encoded. If the difference between those 2 numbers is
+           * bigger than half a frame we then use the incoming timestamp
            * as a reference, otherwise we continue using our accumulated samples
            * counter */
           if (ABS (mad->total_samples - total) > nsamples / 2) {
index 44668fb4ab24859b22bd4fc17eee045230f494c4..a6efa14c6110f17a6724dad3057b303ee7d1389a 100644 (file)
@@ -612,7 +612,7 @@ handle_sequence (GstMpeg2dec * mpeg2dec, const mpeg2_info_t * info)
 
   init_dummybuf (mpeg2dec);
 
-  /* Pump in some null buffers, because otherwise libmpeg2 doesn't 
+  /* Pump in some null buffers, because otherwise libmpeg2 doesn't
    * initialise the discard_fbuf->id */
   mpeg2_set_buf (mpeg2dec->decoder, mpeg2dec->dummybuf, NULL);
   mpeg2_set_buf (mpeg2dec->decoder, mpeg2dec->dummybuf, NULL);