author | Thomas Vander Stichele <thomas@apestaart.org> | |
Mon, 17 Dec 2001 18:37:01 +0000 (18:37 +0000) | ||
committer | Thomas Vander Stichele <thomas@apestaart.org> | |
Mon, 17 Dec 2001 18:37:01 +0000 (18:37 +0000) |
Original commit message from CVS:
building up speed
building up speed
INSTALL | [new file with mode: 0644] | patch | blob |
Makefile.am | [new file with mode: 0644] | patch | blob |
acconfig.h | [new file with mode: 0644] | patch | blob |
autogen.sh | [new file with mode: 0755] | patch | blob |
configure.ac | [new file with mode: 0644] | patch | blob |
diff --git a/INSTALL b/INSTALL
--- /dev/null
+++ b/INSTALL
@@ -0,0 +1,182 @@
+Basic Installation
+==================
+
+ These are generic installation instructions.
+
+ The `configure' shell script attempts to guess correct values for
+various system-dependent variables used during compilation. It uses
+those values to create a `Makefile' in each directory of the package.
+It may also create one or more `.h' files containing system-dependent
+definitions. Finally, it creates a shell script `config.status' that
+you can run in the future to recreate the current configuration, a file
+`config.cache' that saves the results of its tests to speed up
+reconfiguring, and a file `config.log' containing compiler output
+(useful mainly for debugging `configure').
+
+ If you need to do unusual things to compile the package, please try
+to figure out how `configure' could check whether to do them, and mail
+diffs or instructions to the address given in the `README' so they can
+be considered for the next release. If at some point `config.cache'
+contains results you don't want to keep, you may remove or edit it.
+
+ The file `configure.in' is used to create `configure' by a program
+called `autoconf'. You only need `configure.in' if you want to change
+it or regenerate `configure' using a newer version of `autoconf'.
+
+The simplest way to compile this package is:
+
+ 1. `cd' to the directory containing the package's source code and type
+ `./configure' to configure the package for your system. If you're
+ using `csh' on an old version of System V, you might need to type
+ `sh ./configure' instead to prevent `csh' from trying to execute
+ `configure' itself.
+
+ Running `configure' takes awhile. While running, it prints some
+ messages telling which features it is checking for.
+
+ 2. Type `make' to compile the package.
+
+ 3. Optionally, type `make check' to run any self-tests that come with
+ the package.
+
+ 4. Type `make install' to install the programs and any data files and
+ documentation.
+
+ 5. You can remove the program binaries and object files from the
+ source code directory by typing `make clean'. To also remove the
+ files that `configure' created (so you can compile the package for
+ a different kind of computer), type `make distclean'. There is
+ also a `make maintainer-clean' target, but that is intended mainly
+ for the package's developers. If you use it, you may have to get
+ all sorts of other programs in order to regenerate files that came
+ with the distribution.
+
+Compilers and Options
+=====================
+
+ Some systems require unusual options for compilation or linking that
+the `configure' script does not know about. You can give `configure'
+initial values for variables by setting them in the environment. Using
+a Bourne-compatible shell, you can do that on the command line like
+this:
+ CC=c89 CFLAGS=-O2 LIBS=-lposix ./configure
+
+Or on systems that have the `env' program, you can do it like this:
+ env CPPFLAGS=-I/usr/local/include LDFLAGS=-s ./configure
+
+Compiling For Multiple Architectures
+====================================
+
+ You can compile the package for more than one kind of computer at the
+same time, by placing the object files for each architecture in their
+own directory. To do this, you must use a version of `make' that
+supports the `VPATH' variable, such as GNU `make'. `cd' to the
+directory where you want the object files and executables to go and run
+the `configure' script. `configure' automatically checks for the
+source code in the directory that `configure' is in and in `..'.
+
+ If you have to use a `make' that does not supports the `VPATH'
+variable, you have to compile the package for one architecture at a time
+in the source code directory. After you have installed the package for
+one architecture, use `make distclean' before reconfiguring for another
+architecture.
+
+Installation Names
+==================
+
+ By default, `make install' will install the package's files in
+`/usr/local/bin', `/usr/local/man', etc. You can specify an
+installation prefix other than `/usr/local' by giving `configure' the
+option `--prefix=PATH'.
+
+ You can specify separate installation prefixes for
+architecture-specific files and architecture-independent files. If you
+give `configure' the option `--exec-prefix=PATH', the package will use
+PATH as the prefix for installing programs and libraries.
+Documentation and other data files will still use the regular prefix.
+
+ In addition, if you use an unusual directory layout you can give
+options like `--bindir=PATH' to specify different values for particular
+kinds of files. Run `configure --help' for a list of the directories
+you can set and what kinds of files go in them.
+
+ If the package supports it, you can cause programs to be installed
+with an extra prefix or suffix on their names by giving `configure' the
+option `--program-prefix=PREFIX' or `--program-suffix=SUFFIX'.
+
+Optional Features
+=================
+
+ Some packages pay attention to `--enable-FEATURE' options to
+`configure', where FEATURE indicates an optional part of the package.
+They may also pay attention to `--with-PACKAGE' options, where PACKAGE
+is something like `gnu-as' or `x' (for the X Window System). The
+`README' should mention any `--enable-' and `--with-' options that the
+package recognizes.
+
+ For packages that use the X Window System, `configure' can usually
+find the X include and library files automatically, but if it doesn't,
+you can use the `configure' options `--x-includes=DIR' and
+`--x-libraries=DIR' to specify their locations.
+
+Specifying the System Type
+==========================
+
+ There may be some features `configure' can not figure out
+automatically, but needs to determine by the type of host the package
+will run on. Usually `configure' can figure that out, but if it prints
+a message saying it can not guess the host type, give it the
+`--host=TYPE' option. TYPE can either be a short name for the system
+type, such as `sun4', or a canonical name with three fields:
+ CPU-COMPANY-SYSTEM
+
+See the file `config.sub' for the possible values of each field. If
+`config.sub' isn't included in this package, then this package doesn't
+need to know the host type.
+
+ If you are building compiler tools for cross-compiling, you can also
+use the `--target=TYPE' option to select the type of system they will
+produce code for and the `--build=TYPE' option to select the type of
+system on which you are compiling the package.
+
+Sharing Defaults
+================
+
+ If you want to set default values for `configure' scripts to share,
+you can create a site shell script called `config.site' that gives
+default values for variables like `CC', `cache_file', and `prefix'.
+`configure' looks for `PREFIX/share/config.site' if it exists, then
+`PREFIX/etc/config.site' if it exists. Or, you can set the
+`CONFIG_SITE' environment variable to the location of the site script.
+A warning: not all `configure' scripts look for a site script.
+
+Operation Controls
+==================
+
+ `configure' recognizes the following options to control how it
+operates.
+
+`--cache-file=FILE'
+ Use and save the results of the tests in FILE instead of
+ `./config.cache'. Set FILE to `/dev/null' to disable caching, for
+ debugging `configure'.
+
+`--help'
+ Print a summary of the options to `configure', and exit.
+
+`--quiet'
+`--silent'
+`-q'
+ Do not print messages saying which checks are being made. To
+ suppress all normal output, redirect it to `/dev/null' (any error
+ messages will still be shown).
+
+`--srcdir=DIR'
+ Look for the package's source code in directory DIR. Usually
+ `configure' can determine that directory automatically.
+
+`--version'
+ Print the version of Autoconf used to generate the `configure'
+ script, and exit.
+
+`configure' also accepts some other, not widely useful, options.
diff --git a/Makefile.am b/Makefile.am
--- /dev/null
+++ b/Makefile.am
@@ -0,0 +1,3 @@
+SUBDIRS=sys
+
+DIST_SUBDIRS=sys
diff --git a/acconfig.h b/acconfig.h
--- /dev/null
+++ b/acconfig.h
@@ -0,0 +1,60 @@
+#undef PACKAGE
+#undef VERSION
+#undef GST_VERSION_RELEASE
+
+/* Gettext stuff */
+#undef ENABLE_NLS
+#undef HAVE_CATGETS
+#undef HAVE_GETTEXT
+#undef HAVE_LC_MESSAGES
+#undef HAVE_STPCPY
+
+#undef USE_GLIB2
+#undef HAVE_LIBXML2
+
+#undef PLUGINS_DIR
+#undef PLUGINS_BUILDDIR
+#undef PLUGINS_USE_BUILDDIR
+
+#undef GST_CONFIG_DIR
+#undef GST_WIN32_LIBDIR
+
+#undef HAVE_CPU_I386
+#undef HAVE_CPU_PPC
+#undef HAVE_CPU_ALPHA
+#undef HAVE_CPU_ARM
+#undef HAVE_CPU_SPARC
+
+#undef HAVE_RDTSC
+
+#undef HAVE_LIBGHTTP
+#undef HAVE_LIBMMX
+#undef HAVE_LIBXV
+#undef HAVE_OSS
+#undef HAVE_XAUDIO
+#undef HAVE_LIBDVDREAD
+#undef HAVE_VORBIS
+#undef HAVE_AALIB
+#undef HAVE_LIBMAD
+#undef HAVE_LIBMIKMOD
+#undef HAVE_LIBJPEG
+#undef HAVE_LIBGSM
+#undef HAVE_LIBSDL
+#undef HAVE_LIBHERMES
+#undef HAVE_NASM
+#undef HAVE_A52DEC
+#undef HAVE_MPEG2DEC
+#undef HAVE_FLACLIB
+#undef HAVE_LIBRTP
+#undef HAVE_LINUX_CDROM
+#undef HAVE_LINUX_VIDEODEV
+#undef HAVE_LIBSDL
+#undef HAVE_LIBOPENQUICKTIME
+
+#undef HAVE_ATOMIC_H
+
+#undef GST_DEBUG_ENABLED
+#undef GST_INFO_ENABLED
+#undef GST_DEBUG_COLOR
+
+#undef GST_DISABLE_LOADSAVE
diff --git a/autogen.sh b/autogen.sh
--- /dev/null
+++ b/autogen.sh
@@ -0,0 +1,167 @@
+#!/bin/bash
+# Run this to generate all the initial makefiles, etc.
+
+DIE=0
+package=gstreamer-plugins
+srcfile=own/sinesrc/gstsinesrc.c
+#DEBUG=defined
+if test "x$1" = "x-d"; then echo "+ debug output enabled"; DEBUG=defined; fi
+
+debug ()
+# print out a debug message if DEBUG is a defined variable
+{
+ if test ! -z "$DEBUG"
+ then
+ echo "DEBUG: $1"
+ fi
+}
+
+version_check ()
+# check the version of a package
+# first argument : package name (executable)
+# second argument : source download url
+# rest of arguments : major, minor, micro version
+{
+ PACKAGE=$1
+ URL=$2
+ MAJOR=$3
+ MINOR=$4
+ MICRO=$5
+
+ WRONG=
+
+ debug "major $MAJOR minor $MINOR micro $MICRO"
+ VERSION=$MAJOR
+ if test ! -z "$MINOR"; then VERSION=$VERSION.$MINOR; else MINOR=0; fi
+ if test ! -z "$MICRO"; then VERSION=$VERSION.$MICRO; else MICRO=0; fi
+
+ debug "major $MAJOR minor $MINOR micro $MICRO"
+ echo -n "+ checking for $1 >= $VERSION ... "
+ ($PACKAGE --version) < /dev/null > /dev/null 2>&1 ||
+ {
+ echo
+ echo "You must have $PACKAGE installed to compile $package."
+ echo "Download the appropriate package for your distribution,"
+ echo "or get the source tarball at $URL"
+ return 1
+ }
+ # the following line is carefully crafted sed magic
+ pkg_version=`$PACKAGE --version|head -n 1|sed 's/^[a-zA-z\.\ ()]*//;s/ .*$//'`
+ debug "pkg_version $pkg_version"
+ pkg_major=`echo $pkg_version | cut -d. -f1`
+ pkg_minor=`echo $pkg_version | cut -d. -f2`
+ pkg_micro=`echo $pkg_version | cut -d. -f3`
+ test -z "$pkg_minor" && pkg_minor=0
+ test -z "$pkg_micro" && pkg_micro=0
+
+ debug "found major $pkg_major minor $pkg_minor micro $pkg_micro"
+
+ #start checking the version
+ debug "version check"
+
+ if [ ! "$pkg_major" \> "$MAJOR" ]; then
+ debug "$pkg_major <= $MAJOR"
+ if [ "$pkg_major" \< "$MAJOR" ]; then
+ WRONG=1
+ elif [ ! "$pkg_minor" \> "$MINOR" ]; then
+ if [ "$pkg_minor" \< "$MINOR" ]; then
+ WRONG=1
+ elif [ "$pkg_micro" \< "$MICRO" ]; then
+ WRONG=1
+ fi
+ fi
+ fi
+
+ if test ! -z "$WRONG"; then
+ echo "found $pkg_version, not ok !"
+ echo
+ echo "You must have $PACKAGE $VERSION or greater to compile $package."
+ echo "Get the latest version from $URL"
+ return 1
+ else
+ echo "found $pkg_version, ok."
+ fi
+}
+
+# autoconf 2.52d has a weird issue involving a yes:no error
+# so don't allow it's use
+ac_version=`autoconf --version|head -n 1|sed 's/^[a-zA-z\.\ ()]*//;s/ .*$//'`
+if test "$ac_version" = "2.52d"; then
+ echo "autoconf 2.52d has an issue with our current build."
+ echo "We don't know who's to blame however. So until we do, get a"
+ echo "regular version. RPM's of a working version are on the gstreamer site."
+ exit 1
+fi
+
+
+version_check "autoconf" "ftp://ftp.gnu.org/pub/gnu/autoconf/" 2 52 || DIE=1
+version_check "automake" "ftp://ftp.gnu.org/pub/gnu/automake/" 1 5 || DIE=1
+version_check "libtool" "ftp://ftp.gnu.org/pub/gnu/libtool/" 1 4 0 || DIE=1
+version_check "pkg-config" "http://www.freedesktop.org/software/pkgconfig" 0 8 0 || DIE=1
+
+if test "$DIE" -eq 1; then
+ exit 1
+fi
+
+test -f $srcfile || {
+ echo "You must run this script in the top-level $package directory"
+ exit 1
+}
+
+if test -z "$*"; then
+ echo "I am going to run ./configure with no arguments - if you wish "
+ echo "to pass any to it, please specify them on the $0 command line."
+fi
+
+echo "+ creating acinclude.m4"
+cat m4/*.m4 > acinclude.m4
+
+echo "+ running aclocal ..."
+aclocal $ACLOCAL_FLAGS || {
+ echo
+ echo "aclocal failed - check that all needed development files are present on system"
+ exit 1
+}
+
+# FIXME : why does libtoolize keep complaining about aclocal ?
+echo "+ running libtoolize ..."
+libtoolize --copy --force
+
+echo "+ running autoheader ... "
+autoheader || {
+ echo
+ echo "autoheader failed"
+ exit 1
+}
+echo "+ running autoconf ... "
+autoconf || {
+ echo
+ echo "autoconf failed"
+ exit 1
+}
+echo "+ running automake ... "
+automake -a -c || {
+ echo
+ echo "automake failed"
+ exit 1
+}
+
+# now remove the cache, because it can be considered dangerous in this case
+#echo "+ removing config.cache ... "
+#rm -f config.cache
+
+CONFIGURE_OPT='--enable-maintainer-mode --enable-plugin-builddir --enable-debug --enable-DEBUG'
+
+echo "+ running configure ... "
+echo "./configure default flags: $CONFIGURE_OPT"
+echo "using: $CONFIGURE_OPT $@"
+echo
+
+./configure $CONFIGURE_OPT "$@" || {
+ echo
+ echo "configure failed"
+ exit 1
+}
+
+echo
+echo "Now type 'make' to compile $package."
diff --git a/configure.ac b/configure.ac
--- /dev/null
+++ b/configure.ac
@@ -0,0 +1,1219 @@
+dnl autoconf configuration file for plugins
+AC_INIT
+AC_CONFIG_SRCDIR([configure.ac])
+
+AC_CANONICAL_TARGET([])
+
+AM_CONFIG_HEADER(config.h)
+
+GST_VERSION_MAJOR=0
+GST_VERSION_MINOR=3
+GST_VERSION_MICRO=02
+
+dnl we use the release tag during CVS development
+GST_VERSION_RELEASE=`date +%Y%m%d`
+
+GST_VERSION=$GST_VERSION_MAJOR.$GST_VERSION_MINOR.$GST_VERSION_MICRO
+
+PACKAGE=gstreamer-plugins
+VERSION=$GST_VERSION
+
+AC_DEFINE_UNQUOTED(PACKAGE, "$PACKAGE")
+AC_DEFINE_UNQUOTED(VERSION, "$VERSION")
+AC_SUBST(PACKAGE)
+AC_SUBST(VERSION)
+AC_DEFINE_UNQUOTED(GST_VERSION_RELEASE, "$GST_VERSION_RELEASE")
+AC_SUBST(GST_VERSION_RELEASE)
+
+dnl libtool
+GST_CURRENT=1
+GST_REVISION=0
+GST_AGE=0
+GST_LIBVERSION=$GST_CURRENT:$GST_REVISION:$GST_AGE
+
+AM_INIT_AUTOMAKE($PACKAGE, $VERSION)
+dnl Add parameters for aclocal
+dnl (This must come after AM_INIT_AUTOMAKE, since it modifies ACLOCAL)
+ACLOCAL="$ACLOCAL $ACLOCAL_FLAGS"
+
+AC_SUBST(GST_VERSION_MAJOR)
+AC_SUBST(GST_VERSION_MINOR)
+AC_SUBST(GST_VERSION_MICRO)
+AC_SUBST(GST_VERSION)
+
+AC_SUBST(GST_CURRENT)
+AC_SUBST(GST_REVISION)
+AC_SUBST(GST_AGE)
+AC_SUBST(GST_LIBVERSION)
+
+AM_MAINTAINER_MODE
+
+AC_PROG_CC
+AM_PROG_CC_STDC
+AM_PROG_AS
+AS="${CC}"
+AC_PROG_CXX
+AC_PROG_CXXCPP
+AC_ISC_POSIX
+
+dnl We disable static building for development, for time savings
+dnl *NOTE*: dnl this line before release, so release does static too
+AM_DISABLE_STATIC
+AC_LIBTOOL_DLOPEN
+AM_PROG_LIBTOOL
+
+AC_HEADER_STDC([])
+
+dnl ###########################################
+dnl # Super Duper options for plugin building #
+dnl ###########################################
+
+dnl experimental plugins; stuff that hasn't had the dust settle yet
+AC_ARG_ENABLE(experimental,
+[ --enable-experimental enable building of experimental plugins],
+[case "${enableval}" in
+ yes) EXPERIMENTAL="yes" ;;
+ no) EXPERIMENTAL="no" ;;
+esac],
+[EXPERIMENTAL=no]) dnl Default value
+
+if test "x$EXPERIMENTAL" = "$xyes"; then
+ AC_MSG_WARN(building experimental plugins)
+ USE_LIBMIKMOD="yes"
+else
+ AC_MSG_NOTICE(not building experimental plugins)
+ USE_LIBMIKMOD="no"
+fi
+
+dnl broken plugins; stuff that doesn't seem to build at the moment
+AC_ARG_ENABLE(broken,
+[ --enable-broken enable building of broken plugins],
+[case "${enableval}" in
+ yes) BROKEN="yes" ;;
+ no) BROKEN="no" ;;
+esac],
+[BROKEN=no]) dnl Default value
+
+if test "x$broken-plugins" = "$xyes"; then
+ AC_MSG_WARN(building broken plugins)
+ USE_ARTS="yes"
+ USE_ARTSC="yes"
+else
+ AC_MSG_NOTICE(not building broken plugins)
+ USE_ARTS="no"
+ USE_ARTSC="no"
+fi
+
+
+
+dnl ##############################
+dnl # Do automated configuration #
+dnl ##############################
+
+dnl Check for tools:
+dnl ================
+
+dnl Check for nasm
+AC_PATH_PROG(NASM_PATH, nasm, no)
+AC_SUBST(NASM_PATH)
+if test x$NASM_PATH = xno; then
+ AC_MSG_WARN(Couldn't find nasm)
+ HAVE_NASM="no"
+else
+ AC_DEFINE(HAVE_NASM, 1, [Define if NASM, the netwide assembler, is available])
+ HAVE_NASM="yes"
+fi
+
+dnl fix pkg-config's broken default search path
+if test -z $PKG_CONFIG_PATH; then
+ PKG_CONFIG_PATH=/usr/local/lib/pkgconfig:/usr/lib/pkgconfig
+fi
+export PKG_CONFIG_PATH
+
+dnl Check for pkgconfig
+AC_CHECK_PROG(HAVE_PKGCONFIG, pkg-config, true, false)
+
+dnl dnl check for gtk-doc
+dnl AC_ARG_WITH(html-dir, [ --with-html-dir=PATH path to installed docs ])
+dnl
+dnl if test "x$with_html_dir" = "x" ; then
+dnl HTML_DIR='${datadir}/gst/html'
+dnl else
+dnl HTML_DIR=$with_html_dir
+dnl fi
+dnl
+dnl AC_SUBST(HTML_DIR)
+dnl
+dnl AC_CHECK_PROG(HAVE_GTK_DOC, gtkdoc-mkdb, true, false)
+dnl gtk_doc_min_version=0.6
+dnl if $HAVE_GTK_DOC ; then
+dnl gtk_doc_version=`gtkdoc-mkdb --version`
+dnl AC_MSG_CHECKING([gtk-doc version ($gtk_doc_version) >= $gtk_doc_min_version])
+dnl if perl <<EOF ; then
+dnl exit (("$gtk_doc_version" =~ /^[[0-9]]+\.[[0-9]]+$/) &&
+dnl ("$gtk_doc_version" >= "$gtk_doc_min_version") ? 0 : 1);
+dnl EOF
+dnl AC_MSG_RESULT(yes)
+dnl else
+dnl AC_MSG_RESULT(no)
+dnl HAVE_GTK_DOC=false
+dnl fi
+dnl fi
+dnl GTK_DOC_SCANOBJ=gtkdoc-scanobj
+dnl
+dnl AC_SUBST(HAVE_GTK_DOC)
+dnl AC_SUBST(GTK_DOC_SCANOBJ)
+dnl
+dnl dnl check for docbook tools
+dnl AC_CHECK_PROG(HAVE_XSLTPROC, xsltproc, true, false)
+dnl AC_CHECK_PROG(HAVE_PDFTOPS, pdftops, true, false)
+dnl dnl this does not yet work properly, at least on debain -- wingo
+dnl HAVE_PDFXMLTEX=false
+dnl
+dnl dnl check for image conversion tool
+dnl AC_CHECK_PROG(HAVE_FIG2DEV, fig2dev, true, false)
+dnl
+dnl dnl The following is a hack: if fig2dev doesn't display an error message
+dnl dnl for the desired type, we assume it supports it.
+dnl HAVE_FIG2DEV_PNG=false
+dnl if test "x$HAVE_FIG2DEV" = "xtrue" ; then
+dnl fig2dev_quiet=`fig2dev -L png </dev/null 2>&1 >/dev/null`
+dnl if test "x$fig2dev_quiet" = "x" ; then
+dnl HAVE_FIG2DEV_PNG=true
+dnl fi
+dnl fi
+dnl HAVE_FIG2DEV_PDF=false
+dnl if test "x$HAVE_FIG2DEV" = "xtrue" ; then
+dnl fig2dev_quiet=`fig2dev -L pdf </dev/null 2>&1 >/dev/null`
+dnl if test "x$fig2dev_quiet" = "x" ; then
+dnl HAVE_FIG2DEV_PDF=true
+dnl fi
+dnl fi
+dnl
+
+dnl Set up conditionals for (target) architecture:
+dnl ==============================================
+
+dnl Determine CPU
+case "x${target_cpu}" in
+ xi?86 | k?) HAVE_CPU_I386=yes
+ AC_DEFINE(HAVE_CPU_I386, 1, [Define if the target CPU is an x86])
+ dnl FIXME could use some better detection
+ dnl (ie CPUID)
+ case "x${target_cpu}" in
+ xi386 | xi486) ;;
+ *) AC_DEFINE(HAVE_RDTSC) ;;
+ esac ;;
+ xpowerpc) HAVE_CPU_PPC=yes
+ AC_DEFINE(HAVE_CPU_PPC, 1, [Define if the target CPU is a PPC]) ;;
+ xalpha) HAVE_CPU_ALPHA=yes
+ AC_DEFINE(HAVE_CPU_ALPHA, 1, [Define if the target CPU is an Alpha]) ;;
+ xarm*) HAVE_CPU_ARM=yes
+ AC_DEFINE(HAVE_CPU_ARM, 1, [Define if the target CPU is an ARM]) ;;
+ xsparc*) HAVE_CPU_SPARC=yes
+ AC_DEFINE(HAVE_CPU_SPARC, 1, [Define if the target CPU is a PPC]) ;;
+ xmips*) HAVE_CPU_MIPS=yes
+ AC_DEFINE(HAVE_CPU_MIPS, 1, [Define if the target CPU is a MIPS]) ;;
+ xhppa*) HAVE_CPU_HPPA=yes
+ AC_DEFINE(HAVE_CPU_HPPA, 1, [Define if the target CPU is a HPPA]) ;;
+esac
+
+dnl Determine endianness
+AC_C_BIGENDIAN
+
+dnl Check for MMX-capable compiler
+AC_MSG_CHECKING(for MMX-capable compiler)
+AC_TRY_RUN([
+#include "include/mmx.h"
+
+main()
+{ movq_r2r(mm0, mm1); return 0; }
+],
+[
+HAVE_LIBMMX="yes"
+AC_MSG_RESULT(yes)
+],
+HAVE_LIBMMX="no"
+AC_MSG_RESULT(no)
+,
+HAVE_LIBMMX="no"
+AC_MSG_RESULT(no)
+)
+
+dnl
+dnl We should really use AC_SYS_LARGEFILE, but the problem is
+dnl many of the plugins don't include "config.h". To assure
+dnl binary compatibility, it is necessary that all gstreamer
+dnl code be compiled with the same sizeof(off_t), so we use
+dnl the following crude hack.
+dnl
+
+AC_MSG_CHECKING(for large file support)
+AC_TRY_RUN([
+#define _LARGEFILE_SOURCE
+#define _FILE_OFFSET_BITS 64
+#include <sys/types.h>
+int main () { return !(sizeof(off_t) == 8); }
+],
+[
+AC_MSG_RESULT(yes)
+GST_CFLAGS="$GST_CFLAGS -D_LARGEFILE_SOURCE -D_FILE_OFFSET_BITS=64"
+],
+[
+AC_MSG_RESULT(no)
+],
+[
+AC_MSG_RESULT(no)
+])
+
+dnl Check for essential libraries first:
+dnl ====================================
+
+dnl Check for glib2
+translit(dnm, m, l) AM_CONDITIONAL(USE_GLIB2, true)
+GST_CHECK_FEATURE(GLIB2, [use of glib-2.0 and GObject], , [
+ PKG_CHECK_MODULES(GLIB2, glib-2.0 gobject-2.0 gthread-2.0 gmodule-2.0,
+ HAVE_GLIB2=yes,HAVE_GLIB2=no)
+ GLIB_LIBS=$GLIB2_LIBS
+ GLIB_CFLAGS=$GLIB2_CFLAGS
+ AC_SUBST(GLIB_LIBS)
+ AC_SUBST(GLIB_CFLAGS)
+], disabled, [
+ AC_DEFINE(USE_GLIB2)
+ GST_CFLAGS="$GST_CFLAGS -DUSE_GLIB2"
+])
+AC_SUBST(USE_GLIB2)
+
+if test x$USE_GLIB2 = xno; then
+ GST_PKG_DEPS="glib >= 1.2.0, gtk+ >= 1.2.0"
+
+ dnl Check for glib and gtk
+ AM_PATH_GLIB(1.2.0,,
+ AC_MSG_ERROR(Cannot find glib: Is glib-config in path?),
+ glib gmodule gthread)
+ AM_PATH_GTK(1.2.0,,
+ AC_MSG_ERROR(Cannot find gtk: Is gtk-config in path?))
+ HAVE_GTK=yes
+
+ GLIB_LIBS="$GLIB_LIBS $GTK_LIBS"
+ GLIB_CFLAGS="$GLIB_CFLAGS $GTK_CFLAGS"
+else
+ GST_PKG_DEPS="glib-2.0 gobject-2.0 gmodule-2.0 gthread-2.0"
+
+ PKG_CHECK_MODULES(GTK2, gtk+-2.0, HAVE_GTK=yes, HAVE_GTK=no)
+
+ GTK_FLAGS=$GTK2_CFLAGS
+ GTK_LIBS=$GTK2_LIBS
+
+ if $HAVE_GTK_DOC; then
+ AC_CHECK_PROG(HAVE_GTK_DOC, gtkdoc-scangobj, true, false)
+ if $HAVE_GTK_DOC; then
+ GTK_DOC_SCANOBJ=gtkdoc-scangobj
+ fi;
+ fi
+
+ dnl FIXME: check for gnome2 - this conditional is currently
+ dnl always false.
+ AM_CONDITIONAL(USE_GNOME2, test "x$USE_GNOME2" = "xyes")
+ AC_SUBST(USE_GNOME2)
+fi
+
+AC_SUBST(GST_PKG_DEPS)
+AC_SUBST(GTK_LIBS)
+AC_SUBST(GTK_CFLAGS)
+
+dnl Check for libxml
+if test x$USE_GLIB2 = xno; then
+ LIBXML_PKG='libxml >= 1.8.1'
+ AC_PATH_PROG(XML_CONFIG, xml-config, no)
+ if test x$XML_CONFIG = xno; then
+ AC_MSG_ERROR(Couldn't find $LIBXML_PKG)
+ fi
+ XML_LIBS="`xml-config --libs`"
+ XML_CFLAGS="`xml-config --cflags`"
+ AC_CHECK_LIB(xml, xmlDocGetRootElement, :,
+ [ AC_MSG_ERROR(Need version 1.8.1 or better of libxml) ],
+ $XML_LIBS)
+else
+ LIBXML_PKG='libxml-2.0'
+ PKG_CHECK_MODULES(XML, $LIBXML_PKG, XML_CONFIG=yes, XML_CONFIG=no)
+ AC_PATH_PROG(XML_CONFIG, xml-config, no)
+ AC_DEFINE(HAVE_LIBXML2)
+ GST_CFLAGS="$GST_CFLAGS -DHAVE_LIBXML2"
+fi
+AC_SUBST(LIBXML_PKG)
+AC_SUBST(XML_LIBS)
+AC_SUBST(XML_CFLAGS)
+
+dnl ==========================================================================
+dnl ========================= Macro definitions ==============================
+dnl ==========================================================================
+
+dnl These macros should be moved out to separate files (acinclude.m4?), but
+dnl can't currently be because of the SUBSTFOR magic.
+
+dnl Perform a check for existence of ARTS
+dnl Richard Boulton <richard-alsa@tartarus.org>
+dnl Last modification: 26/06/2001
+dnl GST_CHECK_FEATURE(FEATURE-NAME, FEATURE-DESCRIPTION,
+dnl DEPENDENT-PLUGINS, TEST-FOR-FEATURE)
+dnl
+dnl This check was written for GStreamer: it should be renamed and checked
+dnl for portability if you decide to use it elsewhere.
+dnl
+AC_DEFUN(GST_CHECK_ARTS,
+[
+dnl Set the flags
+ARTS_LIBS="-L/usr/local/lib -L/usr/lib -lmcop -lartsflow -lartsflow_idl"
+ARTS_CFLAGS="-I/usr/local/include/arts -I/usr/include/kde/arts -I/usr/include/arts"
+ARTS_MCOPFLAGS=$ARTS_CFLAGS
+dnl There's no arts-config script, so we make a guess based on the artsc-config
+AC_PATH_PROG(ARTSC_CONFIG, artsc-config, no)
+if test x$ARTSC_CONFIG = xyes; then
+ ARTS_ARTSC_CFLAGS=`artsc-config --cflags | sed 's/artsc/arts/g'`
+ ARTS_CFLAGS="$ARTS_CFLAGS $ARTS_ARTSC_CFLAGS"
+ ARTS_MCOPFLAGS="$ARTS_MCOPFLAGS $ARTS_ARTSC_CFLAGS"
+fi
+AC_SUBST(ARTS_LIBS)
+AC_SUBST(ARTS_CFLAGS)
+AC_SUBST(ARTS_MCOPFLAGS)
+
+dnl Now check if it exists
+AC_LANG_PUSH(C++)
+HAVE_ARTS=yes
+dnl FIXME: Can't get this test to pass, so commented it out. Rely on header check.
+dnl AC_CHECK_LIB(artsflow, convert_stereo_2float_i16le, :, HAVE_ARTS=no, $LIBS)
+
+dnl AC_CHECK_HEADER uses CPPFLAGS, but not CFLAGS.
+dnl FIXME: ensure only suitable flags result from artsc-config --cflags
+AC_CHECK_HEADER(artsflow.h, :, HAVE_ARTS=no)
+
+AC_LANG_POP(C++)
+dnl Check for the idl generator
+AC_CHECK_PROG(HAVE_MCOPIDL, mcopidl, yes, no)
+if test x$HAVE_MCOPIDL = xno; then
+ HAVE_ARTS=no
+fi
+])
+
+dnl ==========================================================================
+dnl ========================= End macro definitions ==========================
+dnl ==========================================================================
+
+
+dnl Next, check for the optional libraries:
+dnl These are all libraries used in building plugins
+dnl ================================================
+dnl let's try and sort them alphabetically, shall we ?
+
+echo
+echo
+AC_MSG_NOTICE(Checking for plugin libraries)
+
+dnl *** a52dec ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_A52DEC, true)
+GST_CHECK_FEATURE(A52DEC, [a52dec], a52dec, [
+GST_CHECK_LIBHEADER(A52DEC, a52, a52_init, -lm, a52dec/a52.h, A52DEC_LIBS="-la52")
+])
+
+dnl *** aalib ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_AALIB, true)
+GST_CHECK_FEATURE(AALIB, [aasink plugin], aasink, [
+ AM_PATH_AALIB(, HAVE_AALIB=yes, HAVE_AALIB=no)
+])
+
+dnl *** alsa ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_ALSA, true)
+GST_CHECK_FEATURE(ALSA, [alsa plugins], gstalsa, [
+AM_PATH_ALSA(0.9.0, HAVE_ALSA=yes, HAVE_ALSA=no)
+])
+
+dnl *** arts ***
+dnl translit(dnm, m, l) AM_CONDITIONAL(USE_ARTS, true)
+dnl GST_CHECK_FEATURE(ARTS, [arts plugins], arts, [GST_CHECK_ARTS()])
+
+dnl *** artsc ***
+dnl translit(dnm, m, l) AM_CONDITIONAL(USE_ARTSC, true)
+dnl GST_CHECK_FEATURE(ARTSC, [artsd plugins], artsdsink, [GST_CHECK_ARTSC()])
+
+dnl *** audiofile ***
+dnl this check uses the GST_CHECK_CONFIGPROG macro
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBAUDIOFILE, true)
+GST_CHECK_FEATURE(LIBAUDIOFILE, [audiofile], afsink afsrc, [
+translit(dnm, m, l) AC_SUBST(LIBAUDIOFILE_LIBS)
+translit(dnm, m, l) AC_SUBST(LIBAUDIOFILE_CFLAGS)
+GST_CHECK_CONFIGPROG(LIBAUDIOFILE, audiofile-config)
+])
+
+dnl *** avifile ***
+dnl this check uses the GST_CHECK_CONFIGPROG macro
+translit(dnm, m, l) AM_CONDITIONAL(USE_AVIFILE, true)
+GST_CHECK_FEATURE(AVIFILE, [avifile], windec winenc, [
+translit(dnm, m, l) AC_SUBST(AVIFILE_LIBS)
+translit(dnm, m, l) AC_SUBST(AVIFILE_CFLAGS)
+GST_CHECK_CONFIGPROG(AVIFILE, avifile-config)
+])
+
+dnl *** CDParanoia ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_CDPARANOIA, true)
+GST_CHECK_FEATURE(CDPARANOIA, [CDParanoia], cdparanoia, [
+ GST_CHECK_LIBHEADER(CDPARANOIA, cdda_interface, cdda_open, , cdda_interface.h, CDPARANOIA_LIBS="-lcdda_interface -lcdda_paranoia")
+])
+dnl FIXME : add second check somehow if that is necessary
+dnl AC_CHECK_LIB(cdda_paranoia, paranoia_init, : , HAVE_CDPARANOIA=no, -lcdda_interface )
+dnl AC_CHECK_HEADER(cdda_paranoia.h, :, HAVE_CDPARANOIA=no)
+
+dnl *** dvdread ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBDVDREAD, true)
+GST_CHECK_FEATURE(LIBDVDREAD, [dvdread library], libdvdread, [
+ GST_CHECK_LIBHEADER(LIBDVDREAD, dvdread, DVDOpen, , dvdread/dvd_reader.h, LIBDVDREAD_LIBS="-ldvdread")
+])
+
+dnl **** ESound ****
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBESD, true)
+GST_CHECK_FEATURE(LIBESD, [esound plugins], esdsrc esdsink, [
+ AM_PATH_ESD(0.2.12, HAVE_LIBESD=yes, HAVE_LIBESD=no)
+])
+
+dnl *** FLAC ***
+dnl thomas : checking for compile with main instead of actual function,
+dnl since that made autoconf break (for version 2.13)
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBFLAC, true)
+GST_CHECK_FEATURE(FLACLIB, [FLAC lossless audio], flacenc flacdec, [
+ GST_CHECK_LIBHEADER(FLACLIB, FLAC, main, -lm, FLAC/all.h, LIBFLAC_LIBS="-lFLAC")
+])
+
+dnl
+dnl *** Gnome VFS ***
+dnl this check uses the GST_CHECK_CONFIGPROG macro with gnome-config vfs
+translit(dnm, m, l) AM_CONDITIONAL(USE_GNOME_VFS, true)
+GST_CHECK_FEATURE(GNOME_VFS, [Gnome VFS], gnomevfssrc, [
+translit(dnm, m, l) AC_SUBST(GNOME_VFS_LIBS)
+translit(dnm, m, l) AC_SUBST(GNOME_VFS_CFLAGS)
+GST_CHECK_CONFIGPROG(GNOME_VFS, gnome-config vfs)
+])
+
+dnl *** gsm ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBGSM, true)
+GST_CHECK_FEATURE(LIBGSM, [GSM library], gsmenc gsmdec, [
+GST_CHECK_LIBHEADER(LIBGSM, gsm, gsm_create, , gsm/gsm.h, LIBGSM_LIBS="-lgsm")
+])
+
+dnl *** Hermes ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBHERMES, true)
+GST_CHECK_FEATURE(LIBHERMES, [Hermes library], colorspace, [
+GST_CHECK_LIBHEADER(LIBHERMES, Hermes, Hermes_ConverterInstance, , Hermes/Hermes.h, LIBHERMES_LIBS="-lHermes")
+], AC_SUBST(LIBHERMES_LIBS))
+
+dnl *** lame ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBLAME, true)
+GST_CHECK_FEATURE(LIBLAME, [lame mp3 encoder library], lame, [
+GST_CHECK_LIBHEADER(LIBLAME, mp3lame, lame_init, -lm, lame/lame.h, LIBLAME_LIBS="-lmp3lame")
+])
+
+dnl AC_SUBST(HAVE_LIBLAME)
+
+dnl *** libdv ***
+dnl FIXME : check if those GLIB thingies are ok
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBDV, true)
+GST_CHECK_FEATURE(LIBDV, [dv library], dv, [
+GST_CHECK_LIBHEADER(LIBDV, dv, dv_init, -lm $GLIB_LIBS $GLIB_CFLAGS, libdv/dv.h, LIBDV_LIBS="-ldv")
+])
+dnl FIXME : check if these CPP flags can be dealt with otherwise
+dnl libdvcheck_save_CPPFLAGS="$CPPFLAGS"
+dnl CPPFLAGS="$CPPFLAGS $GLIB_CFLAGS"
+dnl AC_CHECK_HEADER(libdv/dv.h, :, HAVE_LIBDV=no)
+dnl CPPFLAGS="$libdvcheck_save_CPPFLAGS"
+
+dnl *** libjpeg ***
+dnl FIXME: we could use header checks here as well IMO
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBJPEG, true)
+GST_CHECK_FEATURE(LIBJPEG, [libjpeg], jpegenc jpegdec, [
+ AC_CHECK_LIB(jpeg, jpeg_set_defaults, HAVE_LIBJPEG="yes", HAVE_LIBJPEG="no")
+])
+
+dnl *** mad ***
+dnl FIXME: we could use header checks here as well IMO
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBMAD, true)
+GST_CHECK_FEATURE(LIBMAD, [mad], mad, [
+AC_CHECK_LIB(mad, mad_decoder_finish, HAVE_LIBMAD="yes")
+])
+
+dnl *** mikmod ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBMIKMOD, true)
+GST_CHECK_FEATURE(LIBMIKMOD, [mikmod plugin], mikmod, [
+ AM_PATH_LIBMIKMOD(, HAVE_LIBMIKMOD=yes, HAVE_LIBMIKMOD=no)
+])
+
+dnl *** mpeg2dec ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_MPEG2DEC, true)
+GST_CHECK_FEATURE(MPEG2DEC, [mpeg2dec], mpeg2dec, [
+ GST_CHECK_LIBHEADER(MPEG2DEC, mpeg2, mpeg2_init,, mpeg2dec/mpeg2.h, MPEG2DEC_LIBS="-lmpeg2")
+])
+
+dnl *** OSS audio ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_OSS, true)
+GST_CHECK_FEATURE(OSS, [OSS audio], osssrc osssink, [
+ AC_CHECK_HEADER(sys/soundcard.h, HAVE_OSS="yes", HAVE_OSS="no")
+])
+
+dnl *** quicktime ***
+dnl FIXME: make this be called openquicktime
+translit(dnm, m, l) AM_CONDITIONAL(USE_QUICKTIME, true)
+GST_CHECK_FEATURE(QUICKTIME, [Open Quicktime], quicktime_parser quicktime_decoder quicktime_demux,[
+ GST_CHECK_LIBHEADER(QUICKTIME, openquicktime, quicktime_init,, openquicktime/openquicktime.h, QUICKTIME_LIBS="-lopenquicktime")
+])
+
+dnl *** raw1394 ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_RAW1394, true)
+GST_CHECK_FEATURE(RAW1394, [raw1394 library], dv1394src, [
+ GST_CHECK_LIBHEADER(RAW1394, raw1934, raw1934_get_handle,, libraw1394/raw1394.h, RAW1394_LIBS="-raw1394")
+])
+
+dnl Check for librtp
+dnl FIXME : adapt and make it work
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBRTP, true)
+GST_CHECK_FEATURE(LIBRTP, [RTP library], rtpenc rtpdec,[
+ AC_CHECK_LIB(rtp, rtp_packet_new_take_data, HAVE_LIBRTP=yes, HAVE_LIBRTP=no, $GLIB_LIBS $GLIB_CFLAGS)
+])
+dnl FIXME header check needs to use GLIB_CFLAGS in order to succeed for rtp
+dnl AC_CHECK_HEADERS(rtp/rtp.h, HAVE_LIBRTP=yes, HAVE_LIBRTP=no)
+dnl AC_CHECK_HEADERS(rtp/rtp-packet.h, :, HAVE_LIBRTP=no)
+dnl AC_CHECK_HEADERS(rtp/rtcp-packet.h, :, HAVE_LIBRTP=no)
+dnl AC_CHECK_HEADERS(rtp/rtp-audio.h, :, HAVE_LIBRTP=no)
+
+
+dnl *** SDL ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBSDL, true)
+GST_CHECK_FEATURE(LIBSDL, [SDL plugin], sdlvideosink, [
+ AM_PATH_SDL(, HAVE_LIBSDL=yes, HAVE_LIBSDL=no)
+])
+
+dnl *** shout ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBSHOUT, true)
+GST_CHECK_FEATURE(LIBSHOUT, [shout plugin], icecastsend, [
+ GST_CHECK_LIBHEADER(LIBSHOUT, shout, shout_init_connection,, shout/shout.h, LIBSHOUT_LIBS="-lshout")
+])
+
+dnl for sidplay
+dnl FIXME : make this work
+dnl AC_PATH_LIBSIDPLAY
+
+
+dnl *** vorbis ***
+dnl AM_PATH_VORBIS only takes two options
+translit(dnm, m, l) AM_CONDITIONAL(USE_VORBIS, true)
+GST_CHECK_FEATURE(VORBIS, [vorbis plugin], vorbisenc vorbisdec, [
+ AM_PATH_VORBIS(HAVE_VORBIS=yes, HAVE_VORBIS=no)
+])
+
+dnl *** xmms ***
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBXMMS, true)
+GST_CHECK_FEATURE(LIBXMMS, [xmms plugin], xmms, [
+ AM_PATH_XMMS(0.1.0, HAVE_LIBXMMS=yes, HAVE_LIBXMMS=no)
+])
+
+dnl Check for libgdk-pixbuf
+dnl FIXME: not sure that this is still used anywhere.
+dnl DELETEME
+dnl translit(dnm, m, l) AM_CONDITIONAL(USE_GDK_PIXBUF, true)
+dnl GST_CHECK_FEATURE(GDK_PIXBUF, [use gdk pixbuf], , [
+dnl translit(dnm, m, l) AC_SUBST(GDK_PIXBUF_LIBS)
+dnl translit(dnm, m, l) AC_SUBST(GDK_PIXBUF_CFLAGS)
+dnl GST_CHECK_CONFIGPROG(GDK_PIXBUF, gdk-pixbuf-config)
+dnl ])
+dnl
+
+
+if test x$USE_GLIB2 = xyes; then
+ dnl we don't support gnome/gtk with glib2.0 yet
+ GNOME_LIBS=
+ GNOME_CFLAGS=
+ HAVE_GNOME=no
+ AC_MSG_WARN(gnome disabled for glib2.0)
+else
+ dnl Check for libgnome
+ GST_CHECK_CONFIGPROG(GNOME, gnome-config, gnome gnomeui)
+fi
+AC_SUBST(GNOME_LIBS)
+AC_SUBST(GNOME_CFLAGS)
+AC_SUBST(HAVE_GNOME)
+
+dnl Check for libghttp
+translit(dnm, m, l) AM_CONDITIONAL(USE_LIBGHTTP, true)
+GST_CHECK_FEATURE(LIBGHTTP, [libghttp plugins], gsthttpsrc, [
+ dnl FIXME: need to check for header
+ GHTTP_LIBS=
+ GST_HTTPSRC_GET_TYPE=
+ if test x$USE_GLIB2 = xyes; then
+ AC_MSG_WARN(ghttp disabled for glib2.0)
+ else
+ AC_CHECK_LIB(ghttp, ghttp_request_new,
+ [GHTTP_LIBS="-lghttp"
+ GST_HTTPSRC_GET_TYPE="gst_httpsrc_get_type"
+ HAVE_LIBGHTTP=yes
+ ], :, $LIBS)
+ fi
+ AC_SUBST(GHTTP_LIBS)
+ AC_SUBST(GST_HTTPSRC_GET_TYPE)
+])
+
+
+dnl thomas : adding an arts check taken from xine with it's own .m4
+dnl FIXME: put this higher up
+dnl AM_PATH_ARTS(, HAVE_ARTS=yes, HAVE_ARTS=no)
+
+dnl also define ARTS_MCOPFLAGS
+dnl ARTS_MCOPFLAGS="$ARTS_CFLAGS"
+dnl AC_SUBST(ARTS_MCOPFLAGS)
+
+dnl Check for libglade with gnome support; no libglade for glib2.0
+HAVE_LIBGLADE_GNOME="no"
+if test x$USE_GLIB2 = xyes; then
+ AC_MSG_WARN(libglade disabled for glib2.0)
+ PKG_CHECK_MODULES(LIBGLADE_GNOME, libglade-2.0 libgnomeui-2.0, HAVE_LIBGLADE_GNOME=yes, HAVE_LIBGLADE_GNOME=no)
+ if test x$HAVE_LIBGLADE_GNOME = xno; then
+ AC_MSG_WARN(Couldn't find libglade-2.0 - Can't build gstplay)
+ LIBGLADE_GNOME_LIBS=
+ LIBGLADE_GNOME_CFLAGS=
+ fi;
+else
+ AM_PATH_LIBGLADE(HAVE_LIBGLADE_GNOME="yes", HAVE_LIBGLADE_GNOME="no", gnome)
+ if test x$HAVE_LIBGLADE_GNOME = xno; then
+ AC_MSG_WARN(Couldn't find libglade-config - Can't build gstplay)
+ else
+ LIBGLADE_GNOME_LIBS=$LIBGLADE_LIBS
+ LIBGLADE_GNOME_CFLAGS=$LIBGLADE_CFLAGS
+ AC_TRY_LINK([#include <glade/glade.h>],[glade_gnome_init();],
+ HAVE_LIBGLADE_GNOME="yes"
+ AC_MSG_WARN(
+ [Couldn't find gnome libraries for libglade - Can't build gstmediaplay and gsteditor])
+ )
+ fi
+fi
+AC_SUBST(HAVE_LIBGLADE_GNOME)
+AC_SUBST(LIBGLADE_GNOME_LIBS)
+AC_SUBST(LIBGLADE_GNOME_CFLAGS)
+
+dnl Check for atomic.h
+dnl Note: use AC_CHECK_HEADER not AC_CHECK_HEADERS, because the latter
+dnl defines the wrong default symbol as well (HAVE_ASM_ATOMIC_H)
+AC_CHECK_HEADER(asm/atomic.h, HAVE_ATOMIC_H=yes, HAVE_ATOMIC_H=no)
+dnl Do a compile to check that it has atomic_set (eg, linux 2.0 didn't)
+if test x$HAVE_ATOMIC_H = xyes; then
+ AC_TRY_RUN([
+#include "asm/atomic.h"
+main() { atomic_t t; atomic_set(&t,0); atomic_inc(&t); atomic_add(1,&t);return 0;}
+ ],, [
+ # Not successful
+ if test x$HAVE_ATOMIC_H = xyes; then
+ AC_MSG_WARN(Atomic reference counting is out of date: doing without.)
+ fi
+ HAVE_ATOMIC_H=no
+ ], [
+ # Cross compiling
+ AC_MSG_RESULT(yes)
+ AC_MSG_WARN(Can't check properly for atomic reference counting. Assuming OK.)
+ ])
+fi
+
+
+dnl Check for X11 extensions
+AC_PATH_XTRA
+if test "-DX_DISPLAY_MISSING" = "$X_CFLAGS"; then
+ AC_MSG_ERROR(can not find X11)
+fi
+AC_SUBST(X_CFLAGS)
+AC_SUBST(X_PRE_LIBS)
+AC_SUBST(X_EXTRA_LIBS)
+AC_SUBST(X_LIBS)
+
+
+dnl Check for the Xv library
+xvsave_LIBS=${LIBS}
+AC_CHECK_LIB(Xv, XvQueryExtension,
+ HAVE_LIBXV=yes,
+ HAVE_LIBXV=no,
+ $X_LIBS $X_PRE_LIBS -lXext -lX11 $X_EXTRA_LIBS
+)
+LIBS=${xvsave_LIBS}
+AC_CHECK_HEADER(X11/extensions/Xv.h, :, HAVE_LIBXV=no)
+AC_CHECK_HEADER(X11/extensions/Xvlib.h, :, HAVE_LIBXV=no)
+
+dnl Check for linux/cdrom.h
+AC_CHECK_HEADER(linux/cdrom.h,
+ HAVE_LINUX_CDROM=yes, HAVE_LINUX_CDROM=no
+)
+
+dnl Check for linux/videodev.h
+AC_CHECK_HEADER(linux/videodev.h,
+ HAVE_LINUX_VIDEODEV=yes, HAVE_LINUX_VIDEODEV=no
+)
+
+
+dnl ######################################################################
+dnl # Check command line parameters, and set shell variables accordingly #
+dnl ######################################################################
+
+AC_ARG_ENABLE(libmmx,
+[ --enable-libmmx use libmmx, if available],
+[case "${enableval}" in
+ yes) USE_LIBMMX=$HAVE_LIBMMX ;;
+ no) USE_LIBMMX=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-libmmx) ;;
+esac],
+[USE_LIBMMX=$HAVE_LIBMMX]) dnl Default value
+
+AC_ARG_ENABLE(atomic,
+[ --enable-atomic use atomic reference counting header],
+[case "${enableval}" in
+ yes) USE_ATOMIC_H=$HAVE_ATOMIC_H;;
+ noset) USE_ATOMIC_H=$HAVE_ATOMIC_H;;
+ no) USE_ATOMIC_H=no;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-atomic) ;;
+esac],
+[USE_ATOMIC_H=$HAVE_ATOMIC_H]) dnl Default value
+
+AC_ARG_ENABLE(plugin-builddir,
+[ --enable-plugin-builddir allow tests/demos to use non-installed plugins ],
+[case "${enableval}" in
+ yes) PLUGINS_USE_BUILDDIR=yes ;;
+ no) PLUGINS_USE_BUILDDIR=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-plugin-builddir) ;;
+esac],
+[PLUGINS_USE_BUILDDIR=no]) dnl Default value
+
+AC_ARG_ENABLE(debug,
+[ --enable-debug compile with -g debugging info],
+[case "${enableval}" in
+ yes) USE_DEBUG=yes ;;
+ no) USE_DEBUG=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-debug) ;;
+esac],
+[USE_DEBUG=no]) dnl Default value
+
+AC_ARG_ENABLE(DEBUG,
+[ --enable-DEBUG compiles in a large number of debugging messages],
+[case "${enableval}" in
+ yes) ENABLE_DEBUG=yes ;;
+ no) ENABLE_DEBUG=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-DEBUG) ;;
+esac],
+[ENABLE_DEBUG=no]) dnl Default value
+if test x$ENABLE_DEBUG = xyes; then
+ AC_DEFINE(GST_DEBUG_ENABLED, 1, [Define if DEBUG statements should be compiled in])
+fi
+
+AC_ARG_ENABLE(INFO,
+[ --disable-INFO disables compilation of informational messages],
+[case "${enableval}" in
+ yes) ENABLE_INFO=yes ;;
+ no) ENABLE_INFO=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-INFO) ;;
+esac],
+[ENABLE_INFO=yes]) dnl Default value
+if test x$ENABLE_INFO = xyes; then
+ AC_DEFINE(GST_INFO_ENABLED, 1, [Define if INFO statements should be compiled in])
+fi
+
+AC_ARG_ENABLE(debug-color,
+[ --disable-debug-color disables color output of DEBUG and INFO output],
+[case "${enableval}" in
+ yes) ENABLE_DEBUG_COLOR=yes ;;
+ no) ENABLE_DEBUG_COLOR=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-debug-color) ;;
+esac],
+[ENABLE_DEBUG_COLOR=yes]) dnl Default value
+if test "x$ENABLE_DEBUG_COLOR" = xyes; then
+ AC_DEFINE(GST_DEBUG_COLOR, 1, [Define if debugging messages should be colorized])
+fi
+
+AC_ARG_ENABLE(profiling,
+[ --enable-profiling adds -pg to compiler commandline, for profiling],
+[case "${enableval}" in
+ yes) USE_PROFILING=yes ;;
+ no) UES_PROFILING=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-profiling) ;;
+esac],
+[USE_PROFILING=no]) dnl Default value
+
+dnl default to building registry in the source tree if we are enabling plugin build dir
+if test "x$PLUGINS_USE_BUILDDIR"="xyes"; then
+ GST_CONFIG_DIR=`pwd`
+else
+ GST_CONFIG_DIR=/etc/gstreamer
+fi
+AC_ARG_WITH(configdir,
+[ --with-configdir specify path to use for configdir],
+[case "${withval}" in
+ yes) AC_MSG_ERROR(bad value ${withval} for --with-configdir) ;;
+ no) AC_MSG_ERROR(bad value ${withval} for --with-configdir) ;;
+ *) GST_CONFIG_DIR="${withval}" ;;
+esac],
+[:]) dnl Default value
+
+dnl Default value
+GST_WIN32_LIBDIR="/usr/lib/win32"
+AC_ARG_WITH(win32_libdir,
+[ --with-win32-libdir specify location for win32 DLLs],
+[case "${withval}" in
+ yes) AC_MSG_ERROR(bad value ${withval} for --with-win32-libdir) ;;
+ no) AC_MSG_ERROR(bad value ${withval} for --with-win32-libdir) ;;
+ *) GST_WIN32_LIBDIR="${withval}" ;;
+esac],
+[:]) dnl Default value
+
+AC_ARG_ENABLE(docs-build,
+[ --enable-docs-build enable building of documentation],
+[case "${enableval}" in
+ yes) if $HAVE_GTK_DOC; then BUILD_DOCS=yes; else AC_MSG_ERROR([you don't have gtk-doc, so don't use --docs-build]); fi; ;;
+ no) BUILD_DOCS=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-docs-build) ;;
+esac],
+[BUILD_DOCS=no]) dnl Default value
+
+AC_ARG_ENABLE(plugin-docs,
+[ --enable-plugin-docs enable the building of plugin documentation
+ (this is currently broken, so off by default)],
+[case "${enableval}" in
+ yes) BUILD_PLUGIN_DOCS=yes ;;
+ no) BUILD_PLUGIN_DOCS=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-plugin-docs) ;;
+esac],
+[BUILD_PLUGIN_DOCS=no]) dnl Default value
+
+AC_ARG_ENABLE(tests,
+[ --disable-tests disable building test apps],
+[case "${enableval}" in
+ yes) BUILD_TESTS=yes ;;
+ no) BUILD_TESTS=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --disable-tests) ;;
+esac],
+[BUILD_TESTS=yes]) dnl Default value
+
+AC_ARG_ENABLE(examples,
+[ --disable-examples disable building examples],
+[case "${enableval}" in
+ yes) BUILD_EXAMPLES=yes ;;
+ no) BUILD_EXAMPLES=no ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --disable-examples) ;;
+esac],
+[BUILD_EXAMPLES=yes]) dnl Default value
+
+dnl Next, check for the optional components:
+dnl ========================================
+
+
+AC_DEFUN(GST_SUBSYSTEM_DISABLE,
+[dnl
+dnl Add a subsystem --disable flag and all the necessary symbols and substitions
+dnl
+AC_ARG_ENABLE(translit([$1], A-Z, a-z),
+[ ]builtin(format, --disable-%-17s disable %s, translit([$1], A-Z, a-z), $2),
+[ case "${enableval}" in
+ yes) GST_DISABLE_[$1]=no ;;
+ no) GST_DISABLE_[$1]=yes ;;
+ *) AC_MSG_ERROR(bad value ${enableval} for --enable-translit([$1], A-Z, a-z)) ;;
+ esac],
+[GST_DISABLE_[$1]=no]) dnl Default value
+if test x$GST_DISABLE_[$1] = xyes; then
+ AC_DEFINE(GST_DISABLE_[$1], 1, [Disable $2])
+ GST_DISABLE_[$1]_DEFINE=-DGST_DISABLE_[$1]
+fi
+AM_CONDITIONAL(GST_DISABLE_[$1], test x$GST_DISABLE_[$1] = xyes)
+AC_SUBST(GST_DISABLE_[$1]_DEFINE)
+GST_SUBSYSTEM_DISABLE_DEFINES="$GST_SUBSYTEM_DISABLE_DEFINES $GST_DISABLE_[$1]_DEFINE"
+])
+
+translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_LOADSAVE, true)
+GST_SUBSYSTEM_DISABLE(LOADSAVE,[pipeline XML load/save])
+translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_TYPEFIND, true)
+GST_SUBSYSTEM_DISABLE(TYPEFIND,[typefind plugin],)
+translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_AUTOPLUG, true)
+GST_SUBSYSTEM_DISABLE(AUTOPLUG,[autoplugger subsystem])
+translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_PARSE, true)
+GST_SUBSYSTEM_DISABLE(PARSE,[command-line parser])
+translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_TRACE, true)
+GST_SUBSYSTEM_DISABLE(TRACE,[tracing subsystem])
+translit(dnm, m, l) AM_CONDITIONAL(GST_DISABLE_REGISTRY, true)
+GST_SUBSYSTEM_DISABLE(REGISTRY,[plugin registry])
+
+GST_CFLAGS="$GST_CFLAGS $GST_SUBSYSTEM_DISABLE_DEFINES"
+
+
+dnl ################################################
+dnl # Set defines according to variables set above #
+dnl ################################################
+
+
+dnl These should be "USE_*" instead of "HAVE_*", but some packages expect
+dnl HAVE_ and it is likely to be easier to stick with the old name
+if test "x$USE_LIBGHTTP" = xyes; then
+ AC_DEFINE(HAVE_LIBGHTTP, 1, [Define if ghttp library is available])
+fi
+
+if test "x$USE_LIBMMX" = xyes; then
+ AC_DEFINE(HAVE_LIBMMX, 1, [Define if libmmx is available])
+fi
+
+if test "x$USE_ATOMIC_H" = xyes; then
+ AC_DEFINE(HAVE_ATOMIC_H, 1, [Define if atomic.h header file is available])
+fi
+
+if test "x$PLUGINS_USE_BUILDDIR" = xyes; then
+ AC_DEFINE(PLUGINS_USE_BUILDDIR, 1, [Define if plugins should be loaded from the build tree - only developers should use this])
+fi
+
+dnl if test "x$USE_DEBUG" = xyes; then
+dnl CFLAGS="$CFLAGS -g"
+dnl fi
+
+if test "x$USE_PROFILING" = xyes; then
+dnl CFLAGS="$CFLAGS -pg -fprofile-arcs"
+ FOMIT_FRAME_POINTER=""
+else
+ FOMIT_FRAME_POINTER="-fomit-frame-pointer"
+fi
+
+dnl
+dnl AC_SUBST(FOMIT_FRAME_POINTER)
+dnl
+
+if test "x$HAVE_LIBXV" = xyes; then
+ AC_DEFINE(HAVE_LIBXV)
+fi
+
+if test "x$HAVE_OSS" = xyes; then
+ AC_DEFINE(HAVE_OSS)
+fi
+
+if test "x$HAVE_XAUDIO" = xyes; then
+ AC_DEFINE(HAVE_XAUDIO)
+fi
+
+if test "x$HAVE_LIBMAD" = xyes; then
+ AC_DEFINE(HAVE_LIBMAD)
+fi
+
+if test "x$HAVE_LIBMIKMOD" = xyes; then
+ AC_DEFINE(HAVE_LIBMIKMOD)
+fi
+
+if test "x$HAVE_VORBIS" = xyes; then
+ AC_DEFINE(HAVE_VORBIS)
+fi
+
+if test "x$HAVE_AALIB" = "xyes"; then
+ AC_DEFINE(HAVE_AALIB)
+fi
+
+if test "x$HAVE_LIBJPEG" = xyes; then
+ AC_DEFINE(HAVE_LIBJPEG)
+fi
+
+if test "x$HAVE_LIBSDL" = xyes; then
+ AC_DEFINE(HAVE_LIBSDL)
+fi
+
+if test "x$HAVE_LIBHERMES" = "xyes"; then
+ AC_DEFINE(HAVE_LIBHERMES)
+fi
+
+if test "x$HAVE_LIBDVDREAD" = xyes; then
+ AC_DEFINE(HAVE_LIBDVDREAD)
+fi
+
+if test "x$HAVE_LINUX_CDROM" = xyes; then
+ AC_DEFINE(HAVE_LINUX_CDROM)
+fi
+
+if test "x$HAVE_LINUX_VIDEODEV" = xyes; then
+ AC_DEFINE(HAVE_LINUX_VIDEODEV)
+fi
+
+if test "x$HAVE_MPEG2DEC" = xyes; then
+ AC_DEFINE(HAVE_MPEG2DEC)
+fi
+
+if test "x$HAVE_A52DEC" = xyes; then
+ AC_DEFINE(HAVE_A52DEC)
+fi
+
+if test "x$HAVE_FLACLIB" = xyes; then
+ AC_DEFINE(HAVE_FLACLIB)
+fi
+
+if test "x$HAVE_LIBGSM" = xyes; then
+ AC_DEFINE(HAVE_LIBGSM)
+fi
+
+dnl #############################
+dnl # Set automake conditionals #
+dnl #############################
+
+dnl These should be "USE_*" instead of "HAVE_*", but some packages expect
+dnl HAVE_ and it is likely to be easier to stick with the old name
+AM_CONDITIONAL(HAVE_CPU_I386, test "x$HAVE_CPU_I386" = "xyes")
+AM_CONDITIONAL(HAVE_CPU_PPC, test "x$HAVE_CPU_PPC" = "xyes")
+AM_CONDITIONAL(HAVE_CPU_ALPHA, test "x$HAVE_CPU_ALPHA" = "xyes")
+AM_CONDITIONAL(HAVE_CPU_ARM, test "x$HAVE_CPU_ARM" = "xyes")
+AM_CONDITIONAL(HAVE_CPU_SPARC, test "x$HAVE_CPU_SPARC" = "xyes")
+AM_CONDITIONAL(HAVE_LIBMMX, test "x$USE_LIBMMX" = "xyes")
+
+AM_CONDITIONAL(HAVE_ATOMIC_H, test "x$USE_ATOMIC_H" = "xyes")
+
+AM_CONDITIONAL(EXPERIMENTAL, test "$EXPERIMENTAL" = "$xyes")
+AM_CONDITIONAL(BROKEN, test "$BROKEN" = "$xyes")
+
+AM_CONDITIONAL(HAVE_OSS, test "x$HAVE_OSS" = "xyes")
+AM_CONDITIONAL(HAVE_XAUDIO, test "x$HAVE_XAUDIO" = "xyes")
+AM_CONDITIONAL(HAVE_LIBMAD, test "x$HAVE_LIBMAD" = "xyes")
+AM_CONDITIONAL(HAVE_LIBMIKMOD, test "x$HAVE_LIBMIKMOD" = "xyes")
+AM_CONDITIONAL(HAVE_LINUX_CDROM, test "x$HAVE_LINUX_CDROM" = "xyes")
+AM_CONDITIONAL(HAVE_LINUX_VIDEODEV, test "x$HAVE_LINUX_VIDEODEV" = "xyes")
+AM_CONDITIONAL(HAVE_LIBDVDREAD, test "x$HAVE_LIBDVDREAD" = "xyes")
+AM_CONDITIONAL(HAVE_VORBIS, test "x$HAVE_VORBIS" = "xyes")
+AM_CONDITIONAL(HAVE_LIBJPEG, test "x$HAVE_LIBJPEG" = "xyes")
+AM_CONDITIONAL(HAVE_LIBSDL, test "x$HAVE_LIBSDL" = "xyes")
+AM_CONDITIONAL(HAVE_LIBHERMES, test "x$HAVE_LIBHERMES" = "xyes")
+AM_CONDITIONAL(HAVE_NASM, test "x$HAVE_NASM" = "xyes")
+AM_CONDITIONAL(HAVE_LIBGLADE_GNOME, test "x$HAVE_LIBGLADE_GNOME" = "xyes")
+AM_CONDITIONAL(HAVE_GNOME, test "x$HAVE_GNOME" = "xyes")
+AM_CONDITIONAL(HAVE_LIBXV, test "x$HAVE_LIBXV" = "xyes")
+AM_CONDITIONAL(HAVE_GTK, test "x$HAVE_GTK" = "xyes")
+AM_CONDITIONAL(HAVE_GTK_DOC, $HAVE_GTK_DOC)
+AM_CONDITIONAL(BUILD_DOCS, test "x$BUILD_DOCS" = "xyes")
+AM_CONDITIONAL(BUILD_TESTS, test "x$BUILD_TESTS" = "xyes")
+AM_CONDITIONAL(BUILD_EXAMPLES, test "x$BUILD_EXAMPLES" = "xyes")
+AM_CONDITIONAL(BUILD_PLUGIN_DOCS, test "x$BUILD_PLUGIN_DOCS" = "xyes")
+AM_CONDITIONAL(HAVE_PDFXMLTEX, $HAVE_PDFXMLTEX)
+AM_CONDITIONAL(HAVE_PDFTOPS, $HAVE_PDFTOPS)
+AM_CONDITIONAL(HAVE_XSLTPROC, $HAVE_XSLTPROC)
+AM_CONDITIONAL(HAVE_FIG2DEV_PNG, $HAVE_FIG2DEV_PNG)
+AM_CONDITIONAL(HAVE_FIG2DEV_PDF, $HAVE_FIG2DEV_PDF)
+AM_CONDITIONAL(HAVE_CDPARANOIA, test "x$HAVE_CDPARANOIA" = "xyes")
+AM_CONDITIONAL(HAVE_LIBLAME, test "x$HAVE_LIBLAME" = "xyes")
+AM_CONDITIONAL(HAVE_LIBSHOUT, test "x$HAVE_LIBSHOUT" = "xyes")
+AM_CONDITIONAL(HAVE_MPEG2DEC, test "x$HAVE_MPEG2DEC" = "xyes")
+AM_CONDITIONAL(HAVE_A52DEC, test "x$HAVE_A52DEC" = "xyes")
+dnl thomas : the next line gives errors, this is how it is in CVS
+dnl AM_CONDITIONAL(HAVE_FLAC, test "x$HAVE_FLAC" = "xyes")
+dnl thomas : the next line gives errors as well, I commented it
+dnl AM_CONDITIONAL(HAVE_LAC, test "x$HAVE_FAC" = "xyes")
+dnl thomas: the next line doesn't give errors
+AM_CONDITIONAL(HAVE_FLACLIB, test "x$HAVE_FLACLIB" = "xyes")
+AM_CONDITIONAL(HAVE_LIBRTP, test "x$HAVE_LIBRTP" = "xyes")
+AM_CONDITIONAL(HAVE_ARTS, test "x$HAVE_ARTS" = "xyes")
+AM_CONDITIONAL(HAVE_XMMS, test "x$HAVE_XMMS" = "xyes")
+AM_CONDITIONAL(HAVE_RAW1394, test "x$HAVE_RAW1394" = "xyes")
+AM_CONDITIONAL(HAVE_LIBDV, test "x$HAVE_LIBDV" = "xyes")
+AM_CONDITIONAL(HAVE_AALIB, test "x$HAVE_AALIB" = "xyes")
+AM_CONDITIONAL(HAVE_GNOME_VFS, test "x$HAVE_GNOME_VFS" = "xyes")
+AM_CONDITIONAL(HAVE_AVIFILE, test "x$HAVE_AVIFILE" = "xyes")
+AM_CONDITIONAL(HAVE_LIBOPENQUICKTIME, test "x$HAVE_LIBOPENQUICKTIME" = "xyes")
+AM_CONDITIONAL(HAVE_LIBGSM, test "x$HAVE_LIBGSM" = "xyes")
+AM_CONDITIONAL(PLUGINS_USE_BUILDDIR, test "x$PLUGINS_USE_BUILDDIR" = "xyes")
+AM_CONDITIONAL(HAVE_SIDPLAY, test "x$have_sidplay" = "xyes")
+
+
+dnl ############################
+dnl # Set up some more defines #
+dnl ############################
+
+dnl Set location of configuration dir.
+AC_DEFINE_UNQUOTED(GST_CONFIG_DIR,"$GST_CONFIG_DIR")
+AC_SUBST(GST_CONFIG_DIR)
+
+dnl Set location of windows dll dir.
+AC_DEFINE_UNQUOTED(GST_WIN32_LIBDIR,"$GST_WIN32_LIBDIR")
+AC_SUBST(GST_WIN32_LIBDIR)
+
+dnl Set location of plugin directory
+if test "x${prefix}" = "xNONE"; then
+ PLUGINS_DIR=${ac_default_prefix}/lib/gst
+else
+ PLUGINS_DIR=${prefix}/lib/gst
+fi
+AC_DEFINE_UNQUOTED(PLUGINS_DIR,"$PLUGINS_DIR")
+AC_SUBST(PLUGINS_DIR)
+
+dnl Set location of uninstalled plugin directory
+PLUGINS_BUILDDIR=`pwd`
+AC_DEFINE_UNQUOTED(PLUGINS_BUILDDIR,"$PLUGINS_BUILDDIR")
+AC_SUBST(PLUGINS_BUILDDIR)
+
+dnl Private vars for libgst only
+LIBGST_LIBS="$GST_LIBS $XML_LIBS $GLIB_LIBS"
+LIBGST_CFLAGS="$GST_CFLAGS $XML_CFLAGS $GLIB_CFLAGS"
+AC_SUBST(LIBGST_LIBS)
+AC_SUBST(LIBGST_CFLAGS)
+
+dnl Vars for everyone else
+GST_LIBS="\$(top_builddir)/gst/libgst.la $LIBGST_LIBS"
+GST_CFLAGS="-I\$(top_srcdir) -I\$(top_srcdir)/include $LIBGST_CFLAGS"
+AC_SUBST(GST_LIBS)
+AC_SUBST(GST_CFLAGS)
+
+dnl #############################
+dnl # Configure the subpackages #
+dnl #############################
+
+dnl AC_CONFIG_SUBDIRS(gist)
+dnl AC_CONFIG_SUBDIRS(plugins/mp3decode/xing/libxing)
+
+dnl ##################################################
+dnl # Prepare informative messages to display at end #
+dnl ##################################################
+
+infomessages=
+
+if test "x$PLUGINS_USE_BUILDDIR" = xyes; then
+ infomessages="$infomessages
+*** Warning: You have configured using the --enable-plugin-builddir option.
+
+This option is for development purposes only: binaries built with
+it should be used with code in the build tree only. To build an
+installable version, use ./configure without the --enable-plugin-builddir
+option. Note that the autogen.sh script supplies the plugin builddir
+option automatically - it cannot be used to configure installable builds.
+
+"
+fi
+
+dnl #########################
+dnl # Make the output files #
+dnl #########################
+
+dnl gstreamer.pc
+dnl gstreamer-uninstalled.pc
+dnl gstreamer.spec,
+dnl until ffmpeg is handled by configure plugins/ffmpeg/Makefile
+dnl components/bonobo-gstmediaplay/Makefile
+dnl someone should fix this test/misc/Makefile
+dnl wtay fix this: testsuite/threads/Makefile
+dnl testsuite/refcounting/Makefile
+AC_OUTPUT(
+Makefile
+sys/vgasink/Makefile
+sys/vcdsrc/Makefile
+sys/xvideosink/Makefile
+sys/v4l/Makefile
+sys/qcam/Makefile
+sys/Makefile
+libs/Makefile
+libs/riff/Makefile
+libs/getbits/Makefile
+libs/putbits/Makefile
+libs/idct/Makefile
+libs/audio/Makefile
+libs/bytestream/Makefile
+libs/control/Makefile
+libs/resample/Makefile
+stamp.h
+echo "$infomessages", infomessages="$infomessages"
+)
+
+echo -e "configure: *** Plugins that will be built : $GST_PLUGINS_YES"
+echo
+echo -e "configure: *** Plugins that will not be built : $GST_PLUGINS_NO"
+echo