summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b9a85c9)
raw | patch | inline | side by side (parent: b9a85c9)
author | Maciej Katafiasz <mathrick@mathrick.org> | |
Sun, 9 Jan 2005 13:50:36 +0000 (13:50 +0000) | ||
committer | Maciej Katafiasz <mathrick@mathrick.org> | |
Sun, 9 Jan 2005 13:50:36 +0000 (13:50 +0000) |
Original commit message from CVS:
Update README to give valid PKG_CONFIG_PATH instructions
Update README to give valid PKG_CONFIG_PATH instructions
ChangeLog | patch | blob | history | |
README | patch | blob | history |
diff --git a/ChangeLog b/ChangeLog
index df85f72418a6bacc6e35d7a68816a23f9749f5d2..6aa12263824da5bd62763de5573cf423cbeec11b 100644 (file)
--- a/ChangeLog
+++ b/ChangeLog
+2005-01-09 Maciej Katafiasz <mathrick@freedesktop.org>
+
+ * README: fix PKG_CONFIG_PATH instructions, what was there
+ previously was breaking default search path, not nice.
+ Fixes #163358
+
2005-01-09 Ronald S. Bultje <rbultje@ronald.bitfreak.net>
* gst/audioscale/gstaudioscale.c: (gst_audioscale_init),
index 7e76bd243ea99766b8c1890595f8f4685c9b41d6..1bd0d623fc81d3121724d27092437fd1f41f52be 100644 (file)
--- a/README
+++ b/README
- configure the source tree:
- if you installed GStreamer, then do:
./configure
- If configure complains about missing GStreamer, you should try
- ./configure --with-pkg-config-path=prefix/lib/pkgconfig
+ If configure complains about missing GStreamer, you should try the
+ following command:
+ $export PKG_CONFIG_PATH=prefix/lib/pkgconfig
where prefix should be replaced by the prefix you used to configure
- GStreamer. (Be mindful NOT to ADD a trailing / to that option !)
- If this doesn't fix it, you have other issues ;)
+ GStreamer. (Be mindful NOT to ADD a trailing / to that option !).
+ After that, rerun ./configure. If this doesn't fix it, you have other
+ issues ;)
- if you didn't install GStreamer, you can still compile the plug-ins.
Add the path to gstreamer-uninstalled.pc (which lives in the gstreamer