Update README to give valid PKG_CONFIG_PATH instructions
authorMaciej Katafiasz <mathrick@mathrick.org>
Sun, 9 Jan 2005 13:50:36 +0000 (13:50 +0000)
committerMaciej Katafiasz <mathrick@mathrick.org>
Sun, 9 Jan 2005 13:50:36 +0000 (13:50 +0000)
Original commit message from CVS:
Update README to give valid PKG_CONFIG_PATH instructions

ChangeLog
README

index df85f72418a6bacc6e35d7a68816a23f9749f5d2..6aa12263824da5bd62763de5573cf423cbeec11b 100644 (file)
--- a/ChangeLog
+++ b/ChangeLog
@@ -1,3 +1,9 @@
+2005-01-09  Maciej Katafiasz <mathrick@freedesktop.org>
+
+       * README: fix PKG_CONFIG_PATH instructions, what was there
+       previously was breaking default search path, not nice. 
+       Fixes #163358
+
 2005-01-09  Ronald S. Bultje  <rbultje@ronald.bitfreak.net>
 
        * gst/audioscale/gstaudioscale.c: (gst_audioscale_init),
 2005-01-09  Ronald S. Bultje  <rbultje@ronald.bitfreak.net>
 
        * gst/audioscale/gstaudioscale.c: (gst_audioscale_init),
diff --git a/README b/README
index 7e76bd243ea99766b8c1890595f8f4685c9b41d6..1bd0d623fc81d3121724d27092437fd1f41f52be 100644 (file)
--- a/README
+++ b/README
@@ -9,11 +9,13 @@ COMPILING FROM SOURCE
 - configure the source tree:
   - if you installed GStreamer, then do:
       ./configure
 - configure the source tree:
   - if you installed GStreamer, then do:
       ./configure
-    If configure complains about missing GStreamer, you should try
-      ./configure --with-pkg-config-path=prefix/lib/pkgconfig
+    If configure complains about missing GStreamer, you should try the 
+    following command:
+    $export PKG_CONFIG_PATH=prefix/lib/pkgconfig
     where prefix should be replaced by the prefix you used to configure
     where prefix should be replaced by the prefix you used to configure
-    GStreamer.  (Be mindful NOT to ADD a trailing / to that option !)
-    If this doesn't fix it, you have other issues ;)
+    GStreamer. (Be mindful NOT to ADD a trailing / to that option !).
+    After that, rerun ./configure. If this doesn't fix it, you have other
+    issues ;)
 
   - if you didn't install GStreamer, you can still compile the plug-ins.
     Add the path to gstreamer-uninstalled.pc (which lives in the gstreamer
 
   - if you didn't install GStreamer, you can still compile the plug-ins.
     Add the path to gstreamer-uninstalled.pc (which lives in the gstreamer