release time
authorThomas Vander Stichele <thomas@apestaart.org>
Mon, 3 Oct 2005 17:49:44 +0000 (17:49 +0000)
committerThomas Vander Stichele <thomas@apestaart.org>
Mon, 3 Oct 2005 17:49:44 +0000 (17:49 +0000)
Original commit message from CVS:
release time

ChangeLog
NEWS
README
configure.ac
ext/sidplay/Makefile.am

index 1c35817f8bd2b2dcf39f0b3b3afe3b715b85b033..d50fd3036cb83440eb2d79154535200b8f8c835e 100644 (file)
--- a/ChangeLog
+++ b/ChangeLog
@@ -1,3 +1,12 @@
+=== release 0.9.3 ===
+
+2005-10-03  Thomas Vander Stichele  <thomas at apestaart dot org>
+
+       * NEWS:
+       * README:
+       * configure.ac:
+         releasing 0.9.3, "Athos"
+
 2005-09-30  Michael Smith <msmith@fluendo.com>
 
        * gst/realmedia/rmdemux.c: (gst_rmdemux_src_event),
diff --git a/NEWS b/NEWS
index 5e3ef14c8e783488f196b21f57d6144a5cb312e2..a7e33bcc6ee019d15dc343697276e690327c5a52 100644 (file)
--- a/NEWS
+++ b/NEWS
@@ -1,4 +1,5 @@
-This is GStreamer Ugly Plug-ins 0.9.1
+This is GStreamer Ugly Plug-ins 0.9.3, "Athos".
 
-This release was tested with GStreamer Core 0.9.2 and GStreamer Base Plug-ins
-0.9.1
+Changes since 0.9.1:
+
+      * lame, rmdemux, iec958 fixes
diff --git a/README b/README
index 322a56abef07fdeb573da19a4dbce658deab809f..b73a140009e09c5bf9812c58151df947e998630f 100644 (file)
--- a/README
+++ b/README
@@ -1,46 +1,19 @@
-WHAT IT IS
-----------
-This is GStreamer Ugly Plug-ins.
 
-This package is in the 0.9.x series.  This means that this is a
-development series leading up to a stable 0.10.x series.
-You have been warned.
+GStreamer: Release notes for GStreamer Ugly Plug-ins 0.9.3 "Athos"
+        
 
-GStreamer 0.9 development series - Hung by a Thread
----------------------------------------------------
+The GStreamer team is petrified to announce a new release
+in the 0.9.x development series of the
+GStreamer Ugly Plug-ins.
 
-Starring
 
-  GSTREAMER
+The 0.9.x series is a development series and not recommended for end users.
+It is not API or ABI compatible with the stable 0.8.x series.
+It is, however, parallel installable with the 0.8.x series.
 
-The core around which all other modules revolve.  Base functionality and
-libraries, some essential elements, documentation, and testing.
 
-  BASE
+"When you have to shoot, shoot.  Don't talk."
 
-A well-groomed and well-maintained collection of GStreamer plug-ins and
-elements, spanning the range of possible types of elements one would want
-to write for GStreamer.  
-
-And introducing, for the first time ever, on the development screen ...
-
-  THE GOOD
-
- --- "Such ingratitude.  After all the times I've saved your life."
-
-A collection of plug-ins you'd want to have right next to you on the
-battlefield.  Shooting sharp and making no mistakes, these plug-ins have it
-all: good looks, good code, and good licensing.  Documented and dressed up
-in tests.  If you're looking for a role model to base your own plug-in on,
-here it is.
-
-If you find a plot hole or a badly lip-synced line of code in them,
-let us know - it is a matter of honour for us to ensure Blondie doesn't look
-like he's been walking 100 miles through the desert without water.
-
-  THE UGLY
-
-  --- "When you have to shoot, shoot.  Don't talk."
 
 There are times when the world needs a color between black and white.
 Quality code to match the good's, but two-timing, backstabbing and ready to
@@ -48,6 +21,7 @@ sell your freedom down the river.  These plug-ins might have a patent noose
 around their neck, or a lock-up license, or any other problem that makes you
 think twice about shipping them.
 
+
 We don't call them ugly because we like them less.  Does a mother love her
 son less because he's not as pretty as the other ones ? No  - she commends
 him on his great personality.  These plug-ins are the life of the party.
@@ -55,163 +29,68 @@ And we'll still step in and set them straight if you report any unacceptable
 behaviour - because there are two kinds of people in the world, my friend:
 those with a rope around their neck and the people who do the cutting.
 
-  THE BAD
-
-  --- "That an accusation?"
-
-No perfectly groomed moustache or any amount of fine clothing is going to
-cover up the truth - these plug-ins are Bad with a capital B. 
-They look fine on the outside, and might even appear to get the job done, but
-at the end of the day they're a black sheep. Without a golden-haired angel
-to watch over them, they'll probably land in an unmarked grave at the final
-showdown.
-
-Don't bug us about their quality - exercise your Free Software rights,
-patch up the offender and send us the patch on the fastest steed you can
-steal from the Confederates. Because you see, in this world, there's two
-kinds of people, my friend: those with loaded guns and those who dig.
-You dig.
-
-The Lowdown
------------
-
-  --- "I've never seen so many plug-ins wasted so badly."
-
-GStreamer Plug-ins has grown so big that it's hard to separate the wheat from
-the chaff.  Also, distributors have brought up issues about the legal status
-of some of the plug-ins we ship.  To remedy this, we've divided the previous
-set of available plug-ins into four modules:
-
-- gst-plugins-base: a small and fixed set of plug-ins, covering a wide range
-  of possible types of elements; these are continuously kept up-to-date
-  with any core changes during the development series.
-
-  - We believe distributors can safely ship these plug-ins.
-  - People writing elements should base their code on these elements.
-  - These elements come with examples, documentation, and regression tests.
-
-- gst-plugins-good: a set of plug-ins that we consider to have good quality
-  code, correct functionality, our preferred license (LGPL for the plug-in
-  code, LGPL or LGPL-compatible for the supporting library).
-
-  - We believe distributors can safely ship these plug-ins.
-  - People writing elements should base their code on these elements.
-- gst-plugins-ugly: a set of plug-ins that have good quality and correct
-  functionality, but distributing them might pose problems.  The license
-  on either the plug-ins or the supporting libraries might not be how we'd
-  like. The code might be widely known to present patent problems.
-
-  - Distributors should check if they want/can ship these plug-ins.
-  - People writing elements should base their code on these elements.
-
-- gst-plugins-bad: a set of plug-ins that aren't up to par compared to the
-  rest.  They might be close to being good quality, but they're missing
-  something - be it a good code review, some documentation, a set of tests,
-  a real live maintainer, or some actual wide use.
-  If the blanks are filled in they might be upgraded to become part of
-  either gst-plugins-good or gst-plugins-ugly, depending on the other factors.
-
-  - If the plug-ins break, you can't complain - instead, you can fix the
-    problem and send us a patch, or bribe someone into fixing them for you.
-  - New contributors can start here for things to work on.
-
-INSTALLING FROM PACKAGES
-------------------------
-You should always prefer installing from packages first.  GStreamer is
-well-maintained for a number of distributions, including Fedora, Debian,
-Ubuntu, Mandrake, Gentoo, ...
-
-Only in cases where you:
-- want to hack on GStreamer
-- want to verify that a bug has been fixed
-- do not have a sane distribution
-should you choose to build from source tarballs or CVS.
-
-Find more information about the various packages at
-http://gstreamer.freedesktop.org/download/
-
-COMPILING FROM SOURCE TARBALLS
-------------------------------
-- again, make sure that you really need to install from source !
-  If GStreamer is one of your first projects ever that you build from source,
-  consider taking on an easier project.
-
-- check output of ./configure --help to see if any options apply to you
-- run
-  ./configure
-  make
-
-  to build GStreamer.
-- if you want to install it (not required), run
-  make install
-- You should create a registry for things to work.
-  If you ran make install in the previous step, run
-  gst-register
-  as root.
-
-  If you didn't install, run
-  tools/gst-register
-  as a normal user.
-
-- try out a simple test:
-  gst-launch fakesrc num_buffers=5 ! fakesink
-  (If you didn't install GStreamer, again prefix gst-launch with tools/)
-
-  If it outputs a bunch of messages from fakesrc and fakesink, everything is
-  ok.
-
-- After this, you're ready to install gst-plugins, which will provide the
-  functionality you're probably looking for by now, so go on and read
-  that README.
-
-COMPILING FROM CVS
-------------------
-When building from CVS sources, you will need to run autogen.sh to generate 
-the build system files.
-
-You will need a set of additional tools typical for building from CVS,
-including:
-- autoconf
-- automake
-- libtool
-
-autogen.sh will check for recent enough versions and complain if you don't have
-them.  You can also specify specific versions of automake and autoconf with
---with-automake and --with-autoconf
-
-Check autogen.sh options by running autogen.sh --help
-
-autogen.sh can pass on arguments to configure - you just need to separate them
-from autogen.sh with -- between the two.
-prefix has been added to autogen.sh but will be passed on to configure because
-some build scripts like that.
-
-When you have done this once, you can use autoregen.sh to re-autogen with
-the last passed options as a handy shortcut.  Use it.
-
-After the autogen.sh stage, you can follow the directions listed in
-"COMPILING FROM SOURCE"
-
-You can also run your whole cvs stack uninstalled.  The script in
-the gstreamer module /docs/faq/gst-uninstalled) is helpful in setting
-up your environment for this.
-
-PLUG-IN DEPENDENCIES AND LICENSES
----------------------------------
-GStreamer is developed under the terms of the LGPL (see LICENSE file for
-details). Some of our plug-ins however rely on libraries which are available
-under other licenses. This means that if you are using an application which
-has a non-GPL compatible license (for instance a closed-source application)
-with GStreamer, you have to make sure not to use GPL-linked plug-ins.
-When using GPL-linked plug-ins, GStreamer is for all practical reasons
-under the GPL itself.
-
-HISTORY
--------
-The fundamental design comes from the video pipeline at Oregon Graduate
-Institute, as well as some ideas from DirectMedia.  It's based on plug-ins that
-will provide the various codec and other functionality.  The interface
-hopefully is generic enough for various companies (ahem, Apple) to release
-binary codecs for Linux, until such time as they get a clue and release the
-source.
+
+This module contains a set of plug-ins that have good quality and correct
+functionality, but distributing them might pose problems.  The license
+on either the plug-ins or the supporting libraries might not be how we'd
+like. The code might be widely known to present patent problems.
+Distributors should check if they want/can ship these plug-ins.
+
+
+Other modules containing plug-ins are:
+
+
+gst-plugins-base
+contains a basic set of well-supported plug-ins
+gst-plugins-good
+contains a set of well-supported plug-ins under our preferred license
+gst-plugins-bad
+contains a set of less supported plug-ins that haven't passed the
+    rigorous quality testing we expect
+
+
+
+  
+Features of this release
+    
+      * Parallel installability with 0.8.x series
+      * Threadsafe design and API
+      * lame, rmdemux, iec958 fixes
+
+Bugs fixed in this release
+    
+
+Download
+
+You can find source releases of gst-plugins-ugly in the download directory:
+http://gstreamer.freedesktop.org/src/gst-plugins-ugly/
+
+GStreamer Homepage
+
+More details can be found on the project's website:
+http://gstreamer.freedesktop.org/
+
+Support and Bugs
+
+We use GNOME's bugzilla for bug reports and feature requests:
+http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
+
+Developers
+
+CVS is hosted on cvs.freedesktop.org.
+All code is in CVS and can be checked out from there.
+Interested developers of the core library, plug-ins, and applications should
+subscribe to the gstreamer-devel list. If there is sufficient interest we
+will create more lists as necessary.
+
+        
+Applications
+  
+Contributors to this release
+    
+      * Flavio Oliveira
+      * Michael Smith
+      * Stefan Kost
+      * Thomas Vander Stichele
+      * Wim Taymans
\ No newline at end of file
index 5bc2d74a699b4b60a1bbb748e274680f6b2da226..b167ce3194b59113bc779145d4f48f0d311a7623 100644 (file)
@@ -12,7 +12,7 @@ AM_MAINTAINER_MODE
 
 dnl when going to/from release please set the nano (fourth number) right !
 dnl releases only do Wall, cvs and prerelease does Werror too
-AS_VERSION(gst-plugins-ugly, GST_PLUGINS_UGLY_VERSION, 0, 9, 1, 1,
+AS_VERSION(gst-plugins-ugly, GST_PLUGINS_UGLY_VERSION, 0, 9, 3, 0,
   GST_CVS="no", GST_CVS="yes")
 
 AM_INIT_AUTOMAKE($PACKAGE,$VERSION)
index 7d1ca6bba9c43ad90e7ec1ba587ff928e2584133..cbd1f5eafff3242ff6ae2d5673ee42537e40e991 100644 (file)
@@ -1,4 +1,3 @@
-
 plugin_LTLIBRARIES = libgstsid.la
 
 libgstsid_la_SOURCES = gstsiddec.cc