]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gst-plugins-ugly0-10.git/history - ChangeLog
x264enc: remove leaking "optimization"
[glsdk/gst-plugins-ugly0-10.git] / ChangeLog
2011-05-10 Tim-Philipp MüllerRelease 0.10.18 freedesktop-RELEASE-0.10.18
2011-01-21 Tim-Philipp MüllerRelease 0.10.17
2010-09-02 Tim-Philipp MüllerRelease 0.10.16
2010-05-30 Tim-Philipp MüllerRelease 0.10.15
2010-03-06 Tim-Philipp MüllerRelease 0.10.14
2009-10-21 Jan SchmidtRelease 0.10.13
2009-10-15 Jan Schmidt0.10.12.3 pre-release
2009-10-12 Jan Schmidt0.10.12.2 pre-release
2009-06-18 Jan SchmidtRelease 0.10.12
2009-03-21 Jan SchmidtRelease 0.10.11
2009-01-08 Yves Lefebvregst/mpegstream/: Fix some caps leaks. Fixes bug #564885.
2009-01-02 Alessandro Decinaext/cdio/gstcdio.c: Remove unused format argument.
2008-12-13 Tim-Philipp Müllerwin32/common/: Hardcode cpu for win32 build, just like...
2008-12-13 Edward Herveym4/Makefile.am: Removed two more .m4 that aren't shippe...
2008-12-13 Edward Herveym4/Makefile.am: inttypes.m4 hasn't been available since...
2008-12-10 Tim-Philipp Müllergst/mpegaudioparse/gstmpegaudioparse.*: Do an initial...
2008-12-04 Sebastian Drögeconfigure.ac: Apparently AC_CONFIG_MACRO_DIR breaks...
2008-12-04 Sebastian Drögeconfigure.ac: Set AC_CONFIG_MACRO_DIR to common/m4...
2008-12-01 Sebastian Drögeext/mpeg2dec/gstmpeg2dec.c: Last change introduced...
2008-11-29 Sebastian DrögeRequire gettext 0.17 because older versions don't mix...
2008-11-25 David Schleefext/mpeg2dec/gstmpeg2dec.*: Add support for 4:4:4 video...
2008-11-24 Simon Holm Thøgersenext/mpeg2dec/gstmpeg2dec.c: Add support for the STATE_S...
2008-11-20 Wim Taymansgst/asfdemux/gstasfdemux.c: Remove duplicate and broken...
2008-11-20 Jan Schmidtconfigure.ac: Back to development -> 0.10.10.1
2008-11-19 Jan SchmidtRelease 0.10.10 - "Under the House"
2008-11-17 Sebastian Drögeext/sidplay/Makefile.am: Use GST_CXXFLAGS for C++ code...
2008-11-12 Jan Schmidtconfigure.ac: 0.10.9.3 pre-release
2008-11-11 Wim Taymansgst/asfdemux/gstasfdemux.c: Only copy sane aspect ratio...
2008-11-06 Sebastian DrögeAdd bug number to the mp3parse mpeg 2.5 fix
2008-11-05 Wim Taymansext/amrnb/amrnbdec.*: Add a property to select the...
2008-11-03 Tal Shalifgst/mpegstream/: Fix memmory corruption due to not...
2008-10-30 Stefan Kosttests/check/Makefile.am: Blacklist cdiocddasrc from...
2008-10-24 Jan Schmidtconfigure.ac: oops, forgot to bump the version back...
2008-10-24 Wim Taymansgst/realmedia/rmdemux.c: Add suport for mpeg4 and aac...
2008-10-14 Michael Smithgst/mpegaudioparse/gstmpegaudioparse.c: Calculate sampl...
2008-10-14 Robin Stockerext/mpeg2dec/gstmpeg2dec.*: Prefer the container's...
2008-10-13 Stefan KostDon't install static libs for plugins. Fixes #550851...
2008-10-13 Sebastian Drögegst/mpegaudioparse/gstmpegaudioparse.c: Post a GST_ELEM...
2008-10-09 Stefan Kostext/amrnb/amrnbparse.c: use #defines for HEADER. Unref...
2008-10-08 Wim Taymansext/mad/gstmad.*: track discont on incomming buffers...
2008-09-28 Sameer Naikext/mpeg2dec/gstmpeg2dec.*: Fix compilation with -...
2008-09-28 Sameer Naikext/mad/gstmad.*: Fix compilation with --disable-index...
2008-09-27 Thijs Vermeirext/a52dec/gsta52dec.*: Fix channel re-negotiation...
2008-09-26 Wim Taymansext/amrnb/amrnbenc.*: Pass the discont flag from the...
2008-09-26 Benoit Fouetext/amrnb/amrnbparse.*: Add flush seek handler. Fixes...
2008-09-26 Benoit Fouetext/amrnb/amrnbparse.*: Fix the duration query. Fixes...
2008-09-02 Tim-Philipp Müllerpo/LINGUAS: Add 'ca' to LINGUAS.
2008-08-28 Edward Herveygst/asfdemux/gstasfdemux.c: Fix aggregated GST_FLOW_RET...
2008-08-27 Wim Taymansgst/realmedia/rdtdepay.*: Parse other values from the...
2008-08-27 Wim Taymansgst/realmedia/rdtdepay.*: Check seqnum gaps and drop...
2008-08-27 Wim Taymansgst/realmedia/rdtmanager.c: Include the new rdt jitterb...
2008-08-27 Wim Taymansgst/realmedia/rdtdepay.*: Use new RDT parsing helper...
2008-08-27 Wim Taymansgst/realmedia/: Add first support for parsing RDT messages.
2008-08-27 Wim Taymansgst/realmedia/rmdemux.*: Keep track of the first timest...
2008-08-26 Jan SchmidtRelease 0.10.9
2008-08-26 Jan Schmidtext/a52dec/gsta52dec.c: Set up a default time segment...
2008-08-12 Jan Schmidt0.10.8.2 pre-release.
2008-08-11 Michael Smithgst/asfdemux/gstasfdemux.c: Properly aggregate flow...
2008-08-07 Frederic CrozatMake sure gettext returns translations in UTF-8 encodin...
2008-07-31 Sebastian Drögegst/mpegaudioparse/gstmpegaudioparse.c: Don't recurse...
2008-07-31 Sebastian Drögeext/lame/gstlame.c: Use the default for the strict...
2008-07-29 Sebastian Drögeext/lame/gstlame.*: Get the defaults settings of LAME...
2008-07-27 Sebastian Drögeext/lame/gstlame.c: Use LAME's default for the min...
2008-07-27 Sebastian DrögePut the MPEG audio version into the caps as "mpegaudiov...
2008-07-22 Sebastian Drögeext/lame/gstlame.*: Fix build with lame >= 3.97. The...
2008-07-13 Sebastian Drögeext/mpeg2dec/gstmpeg2dec.c: Don't allow width/height...
2008-07-11 Sebastian Drögeext/sidplay/Makefile.am: Fix the build.
2008-07-08 Sebastian Drögeconfigure.ac: Don't include ERROR_CFLAGS in GST_CXXFLAG...
2008-07-05 Tal Shalifext/dvdnav/dvdnavsrc.c: Prevent double free. Fixes...
2008-07-05 Mark Nauwelaertsgst/mpegstream/: Resend tags event after a FLUSH (seek...
2008-07-03 Tim-Philipp MüllerUse correct error code for encrypted streams.
2008-07-02 Mark Nauwelaertsgst/mpegstream/gstmpegdemux.c: Bridge gaps in stream...
2008-06-27 Mark Nauwelaertsext/dvdread/dvdreadsrc.c: Allow and implement non-flush...
2008-06-26 Edward Herveygst/mpegaudioparse/gstmpegaudioparse.c: Fix build on...
2008-06-13 Stefan KostAdd missing elements to docs. Restore alphabetical...
2008-06-13 Stefan KostDo not use short_description in section docs for elemen...
2008-06-09 Sebastian Drögegst/mpegaudioparse/gstmpegaudioparse.c: Don't mark...
2008-06-02 Wim Taymansext/a52dec/gsta52dec.c: Drain queued buffers before...
2008-06-02 Wim Taymansext/a52dec/gsta52dec.*: Add segment handling, buffer...
2008-05-28 Stefan KostRandom doc of the day. Also print human readable format...
2008-05-26 Wim Taymansext/a52dec/gsta52dec.*: Mark discont on outgoing buffer...
2008-05-26 Sebastian Drögegst/mpegaudioparse/gstxingmux.c: Fix alignment issues...
2008-05-25 Tim-Philipp Müllergst/ac3parse/gstac3parse.c: Fix alignment issue which...
2008-05-25 Jan Schmidtconfigure.ac: Back to devel -> 0.10.8.1
2008-05-21 Jan SchmidtRelease 0.10.8
2008-05-19 Jan Schmidtconfigure.ac: 0.10.7.4 pre-release
2008-05-19 Edward Herveyext/mad/gstmad.c: Fix inconsistent use of rate and...
2008-05-19 Wim Taymansgst/realmedia/rmdemux.c: Flush timestamp correction...
2008-05-19 Jan SchmidtCommit 0.10.7.3 pre-rel marker
2008-05-13 Edward Herveygst/realmedia/rmdemux.c: Properly aggregate GstFlowRetu...
2008-05-10 Jan Schmidtconfigure.ac: 0.10.7.2 pre-release
2008-05-10 Edward HerveyAlways let FLUSH_START events flow downstream.
2008-05-07 Tim-Philipp Müllerconfigure.ac: Error out if we don't have the required...
2008-05-06 Wim Taymansgst/realmedia/rmdemux.c: Fix video timestamps by adjust...
2008-05-06 Wim Taymansgst/realmedia/rdtmanager.c: Set Rank to NONE so that...
2008-05-05 Sebastian Drögegst/mpegaudioparse/gstmpegaudioparse.c: Send a new...
2008-04-30 Wim Taymansgst/realmedia/rtspreal.*: Move assembly rule parsing...
2008-04-29 Michael Smithgst/realmedia/: Include generated "_stdint.h" instead...
2008-04-25 Sebastian Drögeext/sidplay/gstsiddec.cc: Cast NULL sentinels to void...
2008-04-22 Edgard LimaFix "unused var" compiler error when --disable-gst...
next