MAINTAINERS: Add
[glsdk/gst-plugins-ugly0-10.git] / configure.ac
2004-02-26 Thomas Vander Sticheleback to nano
2004-02-24 Thomas Vander SticheleI hate conflicts, this was supposed to go in yesterday
2004-02-22 Benjamin Otteconfigure.ac: export [_]*{gst,Gst,GST}.* symbols from...
2004-02-22 Ramon Garcia FernandezExport only gst_plugin_desc from plugins
2004-02-20 Thomas Vander Stichelefix gdk_pixbuf install location creation for solaris...
2004-02-20 Andy Wingogst/intfloat/, gst/oneton: Removed, replaced by audioco...
2004-02-20 Benjamin Otteext/xine/: add first version of xine plugin wrapper...
2004-02-19 David Schleefconfigure.ac: Move massink to gst-rotten
2004-02-13 Thomas Vander Stichelemove ffmpeg stuff to gst-ffmpeg module
2004-02-13 Thomas Vander Sticheleuse GST_ARCH
2004-02-12 David SchleefConvert a few inner loops to use liboil. This is curre...
2004-02-11 Thomas Vander Stichelefix ulonglong.m4 missing by upping gettext required...
2004-02-06 Thomas Vander Sticheleremove RELEASE
2004-02-04 Thomas Vander Stichelebump version
2004-02-04 Thomas Vander Sticheleappease libtool gods
2004-02-03 Benjamin Otteco/: add AX_CREATE_STDINT_H to get correct type definit...
2004-02-01 Thomas Vander Sticheleadd check for new function
2004-01-30 Benjamin Otteconfigure.ac: use AC_C_INLINE
2004-01-21 Christian Schalleradding NAS plugin
2004-01-19 Thomas Vander Sticheleputting i18n in place for plugins
2004-01-19 Benjamin OtteChangeLog
2004-01-18 Jeremy SimonCheck for libmusicbrainz
2004-01-15 David SchleefDuplicate the ext/hermes colorspace plugin, and remove...
2004-01-12 David SchleefFixes to make ext/libcaca compile.
2004-01-11 Julien Moutteconfigure.ac: Adding examples/switch/Makefile
2004-01-07 David SchleefNew source plugin based on librfb-0.1. RFB (remote...
2004-01-03 Ronald S. BultjeUpdate xvid plugin to latest xvid (1.0.0-beta3) API.
2004-01-01 Ronald S. Bultjeconfigure.ac: Fix configure check for mpeg2enc. We...
2003-12-21 Thomas Vander Stichelefix BBB's configure.ac changes
2003-12-21 Julien Moutteconfigure.ac: X_DISPLAY_MISSING is set to 1 if AC_PATH_...
2003-12-21 Ronald S. Bultjeconfigure.ac: Improve mpeg2enc detection. This is for...
2003-12-20 Thomas Vander Stichelebump back to cvs versoin
2003-12-20 Thomas Vander Stichelecommitting release stuff testing fdo cvs commits this...
2003-12-16 Thomas Vander Sticheledisable gdk_pixbuf by default
2003-12-14 Thomas Vander Stichelemake sdl depend on X
2003-12-14 Thomas Vander Sticheledistcheck fixes
2003-12-14 Thomas Vander Stichelenot done yet
2003-12-14 Thomas Vander Sticheletrademark protection
2003-12-14 Julien MoutteAdding a test app for libgstplay. It is a command line...
2003-12-14 Thomas Vander Stichelemake pixbuf loader dir configurable
2003-12-13 Christian Schallerfix build wrt to autoplug test
2003-12-11 Ronald S. BultjeThis is a first attempt at a wrapper for the lib'ified...
2003-12-09 Christophe FergeauCommitted fix for #128893 (properly detect too old...
2003-12-08 Julien MoutteAdding a new plugin: switch.
2003-12-07 Ronald S. BultjeFix v4l detection (it requires X, but X is detected...
2003-12-04 Andy Wingoremove copyright field from plugins
2003-12-03 Thomas Vander Stichelefix X dependencies
2003-12-03 Thomas Vander Stichelefixing up X test and general features test
2003-11-29 Ronald S. BultjeAdd check for faad2 (faad1 was detected, too, but we...
2003-11-27 Leif Johnsonfixing bug #127984, we require a higher version of...
2003-11-24 Benjamin Otteuse GDK_PIXBUF_CONFDIR
2003-11-24 Benjamin Ottetagging stuff and build fixes. In detail:
2003-11-23 Jeremy Simonfaad plugin needs the math library
2003-11-23 Christian Schallercommit my batch of build and spec fixes
2003-11-23 David SchleefFix gdk_pixbuf installation directory (again)
2003-11-22 Ronald S. BultjeAdd faac build
2003-11-22 David Schleeffixes to make gdk_pixbuf loader install nicely
2003-11-21 Ronald S. BultjeAdd C-based local matroska/EBML plugin, remove libmatro...
2003-11-21 Ronald S. BultjeNew libfaad (MPEG-2/4 AAC decoder) plugin
2003-11-12 Benjamin Ottefix build system for X, XShm and Xv
2003-11-12 Benjamin Otteadd -lX11 to X_LIBS so ximagesink builds
2003-11-11 Thomas Vander Sticheletest for regular shm instead of XShm
2003-11-11 Benjamin Otteinclude macro for defining GST_FUNCTION, so debugging...
2003-11-07 Thomas Vander Sticheletest and define HAVE_XSHM build ximage plugin
2003-11-06 Steve Bakerthis will make it easier to merge when you have uncommi...
2003-11-06 Benjamin Otteset default errorlevel to NONE. Make configure change...
2003-11-05 Benjamin Otteadd initial version of gdkpixbuf loader for gtk that...
2003-11-03 David SchleefAdd -DG_DISABLE_DEPRECATED to $GST_ERROR
2003-10-31 Benjamin Ottefirst bunch of conversions to new plugin_init. Includes...
2003-10-30 David SchleefRemove mpeg2enc
2003-10-30 David SchleefFix makefiles for GstPropertyProbe. Combine all interf...
2003-10-28 Benjamin Ottemerge TYPEFIND branch. Major changes:
2003-10-28 Gernot Ziegleradded glsink directory
2003-10-26 Ronald S. BultjeUpdate FFMPEG snapshot to this morning's. Asked for...
2003-10-20 David Schleefbump version to 0.7.1.1
2003-10-20 David Schleefbump to 0.7.1
2003-10-10 Ronald S. BultjeSome interface implementations for video4linux/video4li...
2003-10-01 Ronald S. BultjeNew typefind system: bytestream is now part of the...
2003-09-30 Ronald S. BultjeAdd new element: frame dropper. This element inserts...
2003-09-27 David SchleefAdd navigation
2003-09-25 Benjamin Ottesort the list of plugins that are built and don't spit...
2003-09-21 Thomas Vander Stichelemake sure gtk apps are built
2003-09-19 Christian Schalleradd versioning to gst-launch-ext and gst-visualise...
2003-09-18 Christian Schallerversion gst-launch command in gst-launch-ext
2003-09-13 David SchleefChange default program suffix to -0.7
2003-09-13 Ronald S. BultjeInterface example: a mixer
2003-09-11 David SchleefRemove all locally-defined optimization flags
2003-08-09 David SchleefDefine plugindir
2003-08-04 Ronald S. BultjeRemove mpeg1enc because A) it's FUBAR and B) we've...
2003-07-28 Thomas Vander Stichelesecond attempt fixing gdkpixbuf stuff
2003-07-27 David SchleefAdd gst-libs/ext/mplex, and check that we have C++...
2003-07-25 Angel CarpinteroAdded tcp plugin to build
2003-07-22 David Schleefenable ext/mplex
2003-07-17 David Schleef_Really_ fix my lame attempts at previous fixes for...
2003-07-17 David SchleefReenable matroska config check, 'cuz I'm dumb and accid...
2003-07-17 David SchleefReally disable Matroska this time. Reenable smoothwave...
2003-07-15 Brian CameronNow set XVIDEO_LIBS only if the Xv library is found...
2003-07-14 Ronald S. BultjeAdd matroska support to the build tree
2003-07-14 David SchleefAdd gst/overlay directory
2003-07-07 Christian SchallerA big rewrite of the spec file and some ffmpeg disting...
next