lame: fix printf format in debug statements
[glsdk/gst-plugins-ugly0-10.git] / ext / lame /
2013-05-17 Tim-Philipp Müllerlame: fix printf format in debug statements
2013-05-17 Mark Nauwelaertslame: ensure parsed output
2013-05-17 Mark Nauwelaertslame: cleanup unused instance struct fields
2013-05-17 Mark Nauwelaertslamemp3enc: ensure parsed output
2013-05-17 Mark Nauwelaertslamemp3enc: do not leak merged tags
2013-05-17 Vincent Penquerc'hvarious: fix pad template ref leaks
2013-05-17 Sebastian Drögelame: Don't get the parent class again, GST_BOILERPLATE...
2013-05-17 Sebastian Drögelame: Fix variable 'gstelement_class' set but not used...
2013-05-17 Mark Nauwelaertslame: use some more boilerplate
2013-05-17 Mark Nauwelaertslame: port to audioencoder
2013-05-17 Mark Nauwelaertslamemp3enc: use some more boilerplate
2013-05-17 Mark Nauwelaertslamemp3enc: really report bitrate rather kbitrate
2013-05-17 Mark Nauwelaertslamemp3enc: port to audioencoder
2013-05-17 Sebastian Drögelamemp3enc: Post CODEC and BITRATE tags
2011-02-03 Tim-Philipp Müllerlamemp3enc: implement sinkpad get_caps() function to...
2010-10-19 Stefan Kostvarious: canonicalize property names
2010-10-19 Stefan Kostvarious (ext): add a missing G_PARAM_STATIC_STRINGS...
2010-06-01 Tristan Matthewslamemp3enc: implement latency query
2010-03-24 Sebastian Drögebuild: Add all kinds of compiler warning flags and...
2010-03-18 Benjamin Ottegst_element_class_set_details => gst_element_class_set_...
2009-12-02 Thiago Santoslame: Avoid crash when seeking before negotiating
2009-05-14 Sebastian Drögelamemp3enc: Improve debugging a bit
2009-05-13 Tim-Philipp Müllerlamemp3enc: add Since tag to gtk-doc chunk
2009-05-10 Sebastian Drögelamemp3enc: Don't write a Xing header
2009-05-07 Christian SchallerAdd ranks to mp3 encoders
2009-05-07 Sebastian Drögelamemp3enc: Fixup the bitrate only for CBR
2009-05-06 Alessandro Decinalame: fix format string in debug statement
2009-05-05 Tim-Philipp Müllerlame: fix compilation with LAME versions < 3.98
2009-05-04 Sebastian Drögelamemp3enc: Add a note to the encoding-engine-quality...
2009-05-04 Sebastian Drögelame: Implement preset interface
2009-05-04 Sebastian Drögelamemp3enc: Remove fast-vbr property and rename vbr...
2009-05-04 Sebastian Drögelame/lamemp3enc: Fix memory leak on FLUSH_STOP
2009-05-04 Sebastian Drögelame: Deprecate the lame element
2009-05-04 Sebastian Drögelame: Update example pipelines with the new properties
2009-05-04 Sebastian Drögelame: Add lamemp3enc element with much simplified interface
2009-04-19 Edward Herveylame: Remove unneeded variable, it's assigned a value...
2008-10-13 Stefan KostDon't install static libs for plugins. Fixes #550851...
2008-08-07 Frederic CrozatMake sure gettext returns translations in UTF-8 encodin...
2008-07-31 Sebastian Drögeext/lame/gstlame.c: Use the default for the strict...
2008-07-29 Sebastian Drögeext/lame/gstlame.*: Get the defaults settings of LAME...
2008-07-27 Sebastian Drögeext/lame/gstlame.c: Use LAME's default for the min...
2008-07-27 Sebastian DrögePut the MPEG audio version into the caps as "mpegaudiov...
2008-07-22 Sebastian Drögeext/lame/gstlame.*: Fix build with lame >= 3.97. The...
2008-06-13 Stefan KostAdd missing elements to docs. Restore alphabetical...
2008-06-13 Stefan KostDo not use short_description in section docs for elemen...
2008-02-22 Tim-Philipp Müllerext/lame/gstlame.c: Fix broken GST_ELEMENT_ERROR macro...
2008-02-11 Sebastian Drögeext/lame/gstlame.c: Don't leak the allowed caps.
2008-01-17 Zaheer Abbas Meraliext/lame/gstlame.*: Fix the case where you initially...
2008-01-14 Sebastian Drögeext/lame/gstlame.c: Use gst_util_uint64_scale instead...
2008-01-14 Mark Nauwelaertsext/lame/gstlame.c: Correctly set number of channels...
2007-09-26 Tim-Philipp Müllerext/lame/gstlame.c: Fix up case where there is no peer...
2007-09-25 Tim-Philipp Müllerext/lame/gstlame.c: Use GST_PTR_FORMAT to print caps...
2007-09-24 Thomas Vander Sticheleext/lame/gstlame.c: Allow fixing the sample rate lame...
2007-03-21 Jan Schmidtext/lame/gstlame.c: Disable the bitrate checking when...
2007-02-28 Jan Schmidtext/lame/gstlame.c: Display sensible defaults and limit...
2007-02-28 Jan Schmidtext/lame/gstlame.c: Initialise the variables so gcc...
2007-02-21 Thomas Vander Sticheleext/lame/gstlame.c: Fix up bitrate checking macro....
2007-02-09 Tim-Philipp Müllerext/lame/gstlame.*: On receiving EOS, we try to push...
2006-12-30 Thomas Vander Sticheleext/lame/gstlame.c: warn when outgoing sample rate...
2006-12-14 Roland Kayext/lame/gstlame.*: Fix leak (by calling lame_init_para...
2006-11-14 Wim Taymansext/lame/gstlame.*: Make lame timestamp flushed eos...
2006-10-13 Tim-Philipp Müllerext/lame/gstlame.c: Round up not allowed bitrates to...
2006-10-13 Tim-Philipp MüllerAdd docs for lame and lame to docs. Specify allowed...
2006-10-13 Tim-Philipp MüllerAdd i18n magic to lame plugin. Throw decent error messa...
2006-08-31 Jan SchmidtAdd missing GST_LIBS to the link flags
2006-07-26 Zaheer Abbas Meraliext/lame/gstlame.c: Fix lame putting lots of 0's at...
2006-06-11 Thomas Vander Sticheleupdate build files
2006-05-06 Tim-Philipp Müllerext/lame/gstlame.*: Remove tag writing from lame (which...
2006-05-05 Andres Salomonext/lame/gstlame.c: Fix typo (comma vs. semicolon)...
2006-04-21 Ed Catmurext/lame/gstlame.c: Don't crash if we get an EOS event...
2006-04-01 Thomas Vander Sticheleconfigure.ac: rework similarly to other modules
2006-03-28 Tim-Philipp Müllerext/lame/gstlame.*: Make xingheader property non-functi...
2006-03-28 Tim-Philipp Müllerext/lame/gstlame.c: On EOS, flush encoder and send...
2006-03-15 Christophe Fergeauext/lame/gstlame.c: use GST_DEBUG_FUNCPTR more often.
2006-03-12 Christophe Fergeauext/lame/gstlame.c: mark the xing-header property as...
2006-02-16 Wim Taymansext/lame/gstlame.c: Fix up lame a bit.
2006-01-23 Tim-Philipp Müllerext/lame/gstlame.*: Contrary to what the const char...
2006-01-23 Tim-Philipp Müllerext/lame/gstlame.c: don't pass an uninitialised string...
2005-12-06 Thomas Vander Sticheleexpand tabs
2005-11-22 Thomas Vander Sticheledoh
2005-11-22 Thomas Vander Stichelefix up GValueEnum
2005-11-22 Andy WingoUpdate for gst_tag_setter API changes.
2005-11-21 Edward Herveyext/lame/gstlame.c: Don't take the stream lock
2005-10-12 Stefan Kostrenamed GST_FLAGS macros to GST_OBJECT_FLAGS moved...
2005-09-19 Wim Taymansext/lame/gstlame.c: Set caps on outgoing buffers.
2005-09-16 Thomas Vander Sticheleclean up further so we don't try to set up five times...
2005-09-02 Andy WingoAll plugins updated for element state changes.
2005-08-17 Wim Taymansconfigure.ac: Added mpegaudioparse
2005-08-16 Wim TaymansFix compile warning.
2005-07-05 Andy WingoWay, way, way too many files: Remove crack comment...
2004-10-26 Iain HolmesMemory leak fixes
2004-08-26 Zaheer Abbas Meraliext/lame/gstlame.*: Added new media support to lame
2004-08-19 Zaheer Abbas MeraliOnly enable lame presets if version of lame has presets...
2004-08-15 Zaheer Abbas Meraliext/lame/gstlame.c: describe the enum values for vbr...
2004-08-13 Zaheer Abbas Meraliext/lame/gstlame.*: add preset property to lame so...
2004-08-13 Zaheer Abbas Meraliext/lame/gstlame.c: whoops forgot break, thanks teuf
2004-08-13 Zaheer Abbas Meraliext/lame/gstlame.*: fix lame's broken vbr stuff, allow...
2004-08-12 Zaheer Abbas Meraliext/lame/gstlame.c: added getcaps function so samplerat...
2004-08-12 Zaheer Abbas Meraliext/lame/gstlame.c: revert previous fix
2004-08-12 Zaheer Abbas Meraliext/lame/gstlame.c: made source pad link function check...
next