MAINTAINERS: Add
[glsdk/gst-plugins-ugly0-10.git] / ext /
2004-02-22 Benjamin Otteconfigure.ac: export [_]*{gst,Gst,GST}.* symbols from...
2004-02-20 Andy Wingogst/intfloat/, gst/oneton: Removed, replaced by audioco...
2004-02-20 Benjamin Otteext/xine/: add first version of xine plugin wrapper...
2004-02-19 Benjamin Otteext/: use gst_tag_list_insert when you want to insert...
2004-02-19 David Schleefconfigure.ac: Move massink to gst-rotten
2004-02-14 Benjamin Otteext/mad/gstid3tag.c: remove v1 tag even if we can't...
2004-02-13 Thomas Vander Stichelemove ffmpeg stuff to gst-ffmpeg module
2004-02-05 Benjamin Otteext/mad/gstid3tag.c: skip undecodable id3v2 tag instead...
2004-02-05 Benjamin Otteext/alsa/gstalsa.c: be sure to stop the clock when...
2004-02-04 Benjamin Otteext/mad/gstid3tag.c: that should be !=, not == (fixes...
2004-02-03 Thomas Vander Sticheleso remove dep on dvdread header
2004-02-03 Benjamin Otteco/: add AX_CREATE_STDINT_H to get correct type definit...
2004-02-02 Thomas Vander Stichelechange NULL to (NULL) for GST_ELEMENT_ERROR
2004-01-30 Benjamin Otteconfigure.ac: use AC_C_INLINE
2004-01-29 Thomas Vander SticheleGST_ELEMENT_ERROR
2004-01-27 Benjamin Ottegst/asfdemux/: lot's of fixes to make data extraction...
2004-01-23 Thomas Vander Stichelefix distcheck
2004-01-21 Christian Schalleradding NAS plugin
2004-01-19 Thomas Vander Stichelefix typo
2004-01-19 Thomas Vander Sticheleparenthising NULL
2004-01-18 Thomas Vander Sticheleuse new error signal and classification
2004-01-18 Jeremy SimonCheck for libmusicbrainz
2004-01-15 Colin Waltersext/mad/gstid3tag.c (gst_id3_tag_chain): Don't nego...
2004-01-15 Benjamin Otteext/mad/gstid3tag.c: assume tag mode when pad is not...
2004-01-14 Jan SchmidtDon't issue a timestamp unless we have a PTS.
2004-01-13 Amaury Jacquotenable compilation and installation of ivorbis plugin
2004-01-12 David SchleefMake sure everybody wraps #include "config.h" in #ifdef...
2004-01-12 David SchleefFixes to make ext/libcaca compile.
2004-01-07 David SchleefNew source plugin based on librfb-0.1. RFB (remote...
2004-01-07 Benjamin Otteext/mad/gstid3tag.c: Add guard against invalid utf...
2004-01-06 Jan Schmidtext/dv/gstdvdec.c: Fix caps negotiation.
2004-01-05 David Schleefremove c99-ism
2004-01-03 Ronald S. BultjeHm, I broke compilation on 0.3.1... This really fixes it
2004-01-03 Ronald S. Bultjeext/mpeg2dec/gstmpeg2dec.c: Add support for mpeg2dec...
2004-01-02 David Schleefext/ffmpeg/gstffmpegenc.c: Negotiation fixes.
2004-01-02 David SchleefFix problem with last checkin -- remove some of the...
2004-01-02 David SchleefConvert elements to use gst_pad_use_explicit_caps(...
2003-12-31 David SchleefNegotiation fixes.
2003-12-27 Benjamin Otteext/mad/gstid3tag.c: Make id3tag use correct caps nego.
2003-12-22 David SchleefMerge CAPS branch
2003-12-15 Ronald S. BultjeFix crasher (#129287)
2003-12-15 Benjamin Ottemake tag encoding use utf-8. Use glib functions for...
2003-12-15 Benjamin Ottemake id3v1 tag reading use internal function, which...
2003-12-14 Thomas Vander Sticheledistcheck fixes
2003-12-11 Ronald S. BultjeThis is a first attempt at a wrapper for the lib'ified...
2003-12-09 Benjamin Otterework id3tag plugin to work as a) parser - just strip...
2003-12-08 Thomas Vander Sticheleconfigure fixing
2003-12-07 Christophe FergeauUses new tagging framework
2003-12-04 Andy Wingoremove copyright field from plugins
2003-12-02 David Schleefchange _connect to _link
2003-11-24 Benjamin Otteoops, we use application/x-id3 as caps for id3 tags...
2003-11-24 Benjamin Otteforgot breaks and fixed a bogus 'value used uninitialized'
2003-11-24 Benjamin Ottetagging stuff and build fixes. In detail:
2003-11-22 Ronald S. BultjeTypo
2003-11-22 Ronald S. BultjeAdd faac build
2003-11-21 Ronald S. BultjeAdd C-based local matroska/EBML plugin, remove libmatro...
2003-11-21 Ronald S. BultjeNew libfaad (MPEG-2/4 AAC decoder) plugin
2003-11-16 Leif Johnson+ checking in plugin category changes
2003-11-07 Ronald S. BultjeRemove all config.h includes from header files, add...
2003-11-03 David Schleeffixes for new plugin system
2003-11-02 Iain HolmesMpeg2dec go go go!
2003-11-02 Iain HolmesFixed lame too
2003-11-01 Iain HolmesDVDReadSrc updated as well
2003-11-01 Iain HolmesDVDNavSrc updated
2003-11-01 Iain HolmesUpdated for new changes
2003-10-31 Benjamin Ottefirst bunch of conversions to new plugin_init. Includes...
2003-10-29 David SchleefMove a few typefind functions to gst/typefind, remove...
2003-10-29 David Schleefchange gst/bytestream.h to gst/bytestream/bytestream.h
2003-10-28 Benjamin Ottemerge TYPEFIND branch. Major changes:
2003-10-09 Ronald S. BultjeFix typo in Andy's commit
2003-10-09 David SchleefTrivial fixes for GstBuffer->GstData migration
2003-10-08 Andy Wingo/GstBuffer/GstData/ in the API where you can pass event...
2003-10-07 Ronald S. BultjeMake binary work with both libmpeg2-0.3.1 and -0.3.2
2003-10-06 Ronald S. BultjeI believe this fixes 0.3.2-cvs failures; it's 0.3.1...
2003-10-03 David SchleefFix typefinding for BBB's new system
2003-10-01 Ronald S. BultjeNew typefind system: bytestream is now part of the...
2003-09-30 Ronald S. BultjeInput and output samplerate are *not* necessarily the...
2003-09-16 Thomas Vander Stichelereverting error patch before making a branch.
2003-09-15 Benjamin Otteconverted gst_element_error to new format in ext/ ...
2003-09-12 Ronald S. BultjeFix tiny caps error in lame caps - mpegversion(1) was...
2003-09-11 David SchleefRemove all locally-defined optimization flags
2003-09-11 Thomas Vander Stichelefix ocmpilation against cvs
2003-08-10 David SchleefRemove redundant plugindir definition
2003-08-02 Ronald S. Bultjegcc-2.9x fixes
2003-07-27 David SchleefMake mplex subdir dependent on USE_MPLEX
2003-07-26 Jan SchmidtUpdate the gst-launch example for the new syntax
2003-07-26 Jan Schmidthack to handle DVDNAV_WAIT event
2003-07-25 Brian CameronAdding needed license information. The patch was revie...
2003-07-25 Joshua N. PritikinProvide valuable diagnostics for seek events control...
2003-07-24 Anonymous Ignore... Don't attempt to negotiate format if our srcpad isn...
2003-07-23 David SchleefAnd also handle the case where caps have alredy been...
2003-07-23 David SchleefTry to get bufferpool _after_ sucessfully negotiating...
2003-07-22 David Schleefenable ext/mplex
2003-07-18 Christian Schallerthe real speex disting fix, the previous one was just...
2003-07-18 Christian Schallerfix it so that the SPEEX plugin gets disted
2003-07-17 David SchleefApplied patch from vishnu to remove can_seek.
2003-07-16 Andy Wingoactually recurse into sndfile if we are able big ladspa...
2003-07-14 Ronald S. BultjeAdd matroska support to the build tree
2003-07-12 Ronald S. BultjePlugin details fixes
2003-07-10 Christian Schallerfix license field of lame plugin to say LGPL, lame...
next