Release 0.10.13
Update .po files
0.10.12.3 pre-release
a52dec: Fix reference leak on all input buffers in 'dvd mode'
https://bugzilla.gnome.org/show_bug.cgi?id=598272
https://bugzilla.gnome.org/show_bug.cgi?id=598272
0.10.12.2 pre-release
docs: Remove files accidentally added
Remove the gst-plugins-ugly-plugins.args.new and
gst-plugins-ugly-plugins.signals.new files, that appear
to have been accidentally added in commit
f5d046a0b034f9bd7274291f7131ee5db1a30052
Remove the gst-plugins-ugly-plugins.args.new and
gst-plugins-ugly-plugins.signals.new files, that appear
to have been accidentally added in commit
f5d046a0b034f9bd7274291f7131ee5db1a30052
a52dec: Add some debugging for new segment events
mpeg2dec: fix warning in macosx snow leopard
mpegstream: fix warning in macosx snow leopard
mpegaudioparse: fix warning in macosx snow leopard
dvdsubdec: fix warning on macosx snow leopard
asfdemux: fix warning in macosx snow leopard
mp3parse: don't fail SEEKING query when upstream query fails for TIME format
build: fprintf, sprintf, sscanf need stdio.h
mad: add missing include to fix the build
dvdlpcm: whitespace fixes
update spec file
x264enc: adjust configure checking to changed upstream
x264enc: conditionally adjust to new upstream API
Fixes #596517.
Fixes #596517.
mpegaudioparse: prevent infinite (re)syncing
Conflicts:
gst/mpegaudioparse/gstmpegaudioparse.c
Conflicts:
gst/mpegaudioparse/gstmpegaudioparse.c
mp3parse: Refactor checking for sync. Make resyncing more reliable.
Previously, we could get false sync relatively easily - it sometimes happened
on real files. This cleans the code up a fair bit, and makes it require more
confirmation that we've found valid sync before continuing.
Previously, we could get false sync relatively easily - it sometimes happened
on real files. This cleans the code up a fair bit, and makes it require more
confirmation that we've found valid sync before continuing.
mpegaudioparse: ensure 2 valid headers in a row when resyncing
dvddemux: remove bogus ifndef
mpeg2dec: Fix GstIndex handling, incl. refcounting and NULL indizes
dvdsubparse: GstAdapter is not a GstObject and should be freed with g_object_unref
Remove Ronald Bultje from Authors field
Replaced with "GStreamer maintainers
<gstreamer-devel@lists.sourceforge.net>" or just removed,
depending on the number of other authors.
Replaced with "GStreamer maintainers
<gstreamer-devel@lists.sourceforge.net>" or just removed,
depending on the number of other authors.
asfdemux: Remove old non-built asfmux code
Remove so people don't confuse it with the new asfmux code
in -bad.
Remove so people don't confuse it with the new asfmux code
in -bad.
a52dec: Only add the MM_ACCEL_DJBFFT flag if it's defined
It's not defined for older liba52 versions.
It's not defined for older liba52 versions.
a52dec: Allow liba52 to use djbfft based IMDCT transform
liba52 in a52dec-0.7.4 does not have any MMX, MMXEXT or 3DNOW based
IMDCT transform acceleration. It does however have a software based
acceleration using the djbfft library (D.J. Bernstein's library for
fourier transforms - Extremely fast library for floating-point
convolution). So allow liba52 to use it through the MM_ACCEL_DJBFFT
flag.
The liba52 copy in MPlayer sources does have SSE, 3dnowext, 3dnow
and AltiVec implementations, but those are checked for first, and
djbfft is chosen only if none of those is available - good in the
case of some distributions including a port of the MPlayer changes
in their system a52dec library.
The down and upmix code in liba52 doesn't seem to be disturbed by
this additional MM_ACCEL flag and will still use MMX, SSE or 3DNOW
versions if passed from oil_cpu_get_flags (SSE currently is not).
Fixes bug #592787.
liba52 in a52dec-0.7.4 does not have any MMX, MMXEXT or 3DNOW based
IMDCT transform acceleration. It does however have a software based
acceleration using the djbfft library (D.J. Bernstein's library for
fourier transforms - Extremely fast library for floating-point
convolution). So allow liba52 to use it through the MM_ACCEL_DJBFFT
flag.
The liba52 copy in MPlayer sources does have SSE, 3dnowext, 3dnow
and AltiVec implementations, but those are checked for first, and
djbfft is chosen only if none of those is available - good in the
case of some distributions including a port of the MPlayer changes
in their system a52dec library.
The down and upmix code in liba52 doesn't seem to be disturbed by
this additional MM_ACCEL flag and will still use MMX, SSE or 3DNOW
versions if passed from oil_cpu_get_flags (SSE currently is not).
Fixes bug #592787.
amr: Use opencore-amr pkg-config files if possible
This makes it possible to build the plugins when the libraries
are installed at non-standard locations.
Fixes bug #591348.
This makes it possible to build the plugins when the libraries
are installed at non-standard locations.
Fixes bug #591348.
mpegaudioparse: use metadata (xing, vbri) provided bytesize for conversions
Metadata provided seek tables are consistent with metadata's view of
total size, which typically matches real size, but need not do so
(e.g. a truncated file). Fixes seeking and position reporting
in such truncated files (although duration based on metadata may then
still be incorrect).
Metadata provided seek tables are consistent with metadata's view of
total size, which typically matches real size, but need not do so
(e.g. a truncated file). Fixes seeking and position reporting
in such truncated files (although duration based on metadata may then
still be incorrect).
configure: bump core/base requirements to released versions
to avoid confusion.
to avoid confusion.
configure: Remove all mentions to the id3tag plugin which was removed
mad: make check for mad independent of the check for id3tag
Fixes bug #590432.
Fixes bug #590432.
rtpasfdepay: set padding size to the correct value
asf packets in rtp packets should come with their padding fields
set to 0 and the depayload must update them to the correct
value before pushing downstream
asf packets in rtp packets should come with their padding fields
set to 0 and the depayload must update them to the correct
value before pushing downstream
amr: Add AMR-WB decoder and AMR-NB encoder and decoder
These are based on the OpenCore codecs.
Fixes bug #584890.
These are based on the OpenCore codecs.
Fixes bug #584890.
dvdnav: remove dvdnav plugin
Remove dvdnav plugin, it has no future. resindvd is the plugin to
use for dvd playback. Note that dvdnav was never really enabled
in -ugly, you had to edit configure.ac to get it built.
Remove dvdnav plugin, it has no future. resindvd is the plugin to
use for dvd playback. Note that dvdnav was never really enabled
in -ugly, you had to edit configure.ac to get it built.
mpeg2dec: Fix unused variables compiler warnings in unit test
autogen.sh: Use printf instead of 'echo -n'. Check for automake-1.1[01]
Check for more automake command variants. Use printf instead of 'echo -n'
for portability
Check for more automake command variants. Use printf instead of 'echo -n'
for portability
Make git ignore more files
asfdemux: Refactor multiple packet pull.
This also fixes a bug by which the first buffer (in a multi-packet mode)
passed to asf_demux_parse_packet() would have a GST_BUFFER_SIZE of the
full incoming buffer and not just of the single asf packet.
Fixes corrupted frames introduced by latest commit.
This also fixes a bug by which the first buffer (in a multi-packet mode)
passed to asf_demux_parse_packet() would have a GST_BUFFER_SIZE of the
full incoming buffer and not just of the single asf packet.
Fixes corrupted frames introduced by latest commit.
asfdemux: use the right accurate field
Remove accurate variable and its faulty use because the real variable is an
instance variable.
Remove accurate variable and its faulty use because the real variable is an
instance variable.
asfdemux: Sprinkle branch prediction macros accross the code
asfdemux: Delay newsegment handling until we have a keyframe.
We now have a chance for packets to be collected before we send out the
newsegment. If we're not in accurate seeking (keyunit) it will set
the segment start/time to the keyframe's timestamp.
We now have a chance for packets to be collected before we send out the
newsegment. If we're not in accurate seeking (keyunit) it will set
the segment start/time to the keyframe's timestamp.
asfdemux: Remove useless check. We already have checked for it above.
asfdemux: No longer queue GOPs now that seeking is fixed.
We now *always* seek to the keyframe just before our requested position.
When we encounter the first keyframe and we were not accurate (therefore doing
keyframe seeking), we update the segment start position to the keyframe timestamp.
We now *always* seek to the keyframe just before our requested position.
When we encounter the first keyframe and we were not accurate (therefore doing
keyframe seeking), we update the segment start position to the keyframe timestamp.
asfdemux: Store the accurate seeking flag
asfdemux: Use the average frame duration for buffers without a duration.
This will still cause some timestamp jitter, but giving a hint as to the duration
rather than nothing seems to be a better idea.
Also, this allows some scenarios (like remuxing with asfmux) to estimate the total
duration using the accumulated packet duration (which will be correct).
This will still cause some timestamp jitter, but giving a hint as to the duration
rather than nothing seems to be a better idea.
Also, this allows some scenarios (like remuxing with asfmux) to estimate the total
duration using the accumulated packet duration (which will be correct).
asfdemux: Use index entry packet count to optimize seeking.
The simple index entries also contain the number of packets one needs
to retrieve at a given position to get a full keyframe. We therefore
use that information to retrieve all those packets in one buffer when
working in pull-mode.
The simple index entries also contain the number of packets one needs
to retrieve at a given position to get a full keyframe. We therefore
use that information to retrieve all those packets in one buffer when
working in pull-mode.
asfdemux: Do not try to free const pointer
In gst_asf_demux_chain_headers, when 'goto wrong_type' was called
asfdemux tried to free a const pointer that had been cast to a
normal pointer variable.
In gst_asf_demux_chain_headers, when 'goto wrong_type' was called
asfdemux tried to free a const pointer that had been cast to a
normal pointer variable.
asfdemux: Use presentation timestamp when searching in the index.
We need to take the preroll into account... else we end up too early.
We need to take the preroll into account... else we end up too early.
asfdemux: Convert index entry from presentation time to timestamps.
We weren't taking the preroll into account previously, meaning that we
were always seeking preroll nanoseconds too early... resulting in a lot
of dropped packets (which are before the start time).
This brings quit a bit closer to as-fast-as-possible seeking in asf files.
We weren't taking the preroll into account previously, meaning that we
were always seeking preroll nanoseconds too early... resulting in a lot
of dropped packets (which are before the start time).
This brings quit a bit closer to as-fast-as-possible seeking in asf files.
asfdemux: Fix byte array metadata handling.
We basically discard byte array metadata. Should be trivial to adapt
to storing the pointers if we need it later on.
We basically discard byte array metadata. Should be trivial to adapt
to storing the pointers if we need it later on.
asfdemux: Handle PAR/interlaced information stored in packet payload.
This is the 'other' way to store non 1/1 PAR in asf streams (by storing it
in the ASF Packet payload extensions).
This is the 'other' way to store non 1/1 PAR in asf streams (by storing it
in the ASF Packet payload extensions).
asfdemux: Store/Handle global metadata (not specific to one stream).
This allows us to store (and handle) PAR information which might be stored there.
This allows us to store (and handle) PAR information which might be stored there.
mpegaudioparse: fix Xing inverse seek table building
asfdemux: don't try to free a NULL taglist
asfdemux: post tags only after we've created our source pads
Post global tags only after we've added our source pads, so that
tag events get sent downstream in addition to tag messages posted
on the bus. This makes sure tags can be picked up automatically
when transcoding, but also by tagreadbin/playbin2. Fixes #519721.
While we're at it, also add a container-format tag.
Post global tags only after we've added our source pads, so that
tag events get sent downstream in addition to tag messages posted
on the bus. This makes sure tags can be picked up automatically
when transcoding, but also by tagreadbin/playbin2. Fixes #519721.
While we're at it, also add a container-format tag.
asfdemux: use new bytereader functions for image tag parsing
asfdemux: remove some more unused variables
rmdemux: plug buffer leaking
asfdepay: guard against dropped buffers
If a buffer was dropped, we might request data from the adapter that is not
there and then we get a NULL buffer.
If a buffer was dropped, we might request data from the adapter that is not
there and then we get a NULL buffer.
asfdemux: set DISCONT on streams
When we receive a DISCONT as input, don't clear our complete state but simply
mark a discont that will be put on the next buffer. The code will be able to
handle and throw away incomplete data.
Add some more debug info.
Remove an unused variable.
When we receive a DISCONT as input, don't clear our complete state but simply
mark a discont that will be put on the next buffer. The code will be able to
handle and throw away incomplete data.
Add some more debug info.
Remove an unused variable.
asfdepay: set DELTA_UNIT flag correctly
Only set the DELTA_UNIT flag when we are not dealing with a keyframe.
Add some more debug info.
Only set the DELTA_UNIT flag when we are not dealing with a keyframe.
Add some more debug info.
asfdemux: fix latency calculations
We need to check for -1 as an invalid timestamp, not 1.
We need to check for -1 as an invalid timestamp, not 1.
mp3parse: don't put every single frame into the index
Let's not put every single mp3 frame in our index, a few frames per
second should be more than enough. For now use an index interval
of 100ms-500ms depending on the upstream size, to keep the index at
a reasonable size. Factor out the code that adds the index entry
into a separate function for better code readability.
Let's not put every single mp3 frame in our index, a few frames per
second should be more than enough. For now use an index interval
of 100ms-500ms depending on the upstream size, to keep the index at
a reasonable size. Factor out the code that adds the index entry
into a separate function for better code readability.
mp3parse: assume seekability only if we know the upstream size
While technically upstream may be seekable even if it doesn't know
the exact size, I can't think of a use case where this distincation
is relevant in practice, so for now just assume we're not seekable
if upstream doesn't provide us with a size. Makes sure we don't
build a seek index when streaming internet radio with sources that
pretend to be seekable until you try to actually seek.
While technically upstream may be seekable even if it doesn't know
the exact size, I can't think of a use case where this distincation
is relevant in practice, so for now just assume we're not seekable
if upstream doesn't provide us with a size. Makes sure we don't
build a seek index when streaming internet radio with sources that
pretend to be seekable until you try to actually seek.
Fix x264 requirement in SPEC file
x264enc, rdtmanager: fix compilation with debugging disabled
docs: Bump common. Fix comment in the docs Makefile.am
Back to development -> 0.10.12.1
Add 0.10.12 release to the doap file
Release 0.10.12
Update .po files
Update .po files
0.10.11.2 pre-release
win32: Remove #undef inline from the win32 config.h
mad, id3mux: (re)move broken, unmaintained and unloved id3mux element
It will be reborn with a shiny new code base under its hood in -bad.
See #581756 and #565764.
It will be reborn with a shiny new code base under its hood in -bad.
See #581756 and #565764.
gitignore: Ignore some built files in the test area
docs: Update plugin inspect files
Moved 'x264enc' from -bad to -ugly
[MOVED FROM BAD 28/28] x264enc: add multipass-cache-file property
Fixes #583627
Fixes #583627
[MOVED FROM BAD 27/28] Remove wrong stuff from preset file
[MOVED FROM BAD 26/28] Add a more representative example preset file for x264
[MOVED FROM BAD 25/28] Add ranks to various muxers and encoders in -bad
[MOVED FROM BAD 24/28] x264enc: add preset support
Add preset iface and a (dummy) preset file as a starting point.
Add preset iface and a (dummy) preset file as a starting point.
[MOVED FROM BAD 23/28] x264enc: add some documentation on profile
[MOVED FROM BAD 22/28] x264enc: add force keyframe event handling
Use the GstForceKeyUnit event to force a keyframe.
Fixes #578112.
Use the GstForceKeyUnit event to force a keyframe.
Fixes #578112.
[MOVED FROM BAD 21/28] ext/x264/gstx264enc.c: Use hyphen in property name, perform safety buffer size check prior to mem access, and some mo...
Original commit message from CVS:
* ext/x264/gstx264enc.c: (gst_x264_enc_class_init),
(gst_x264_enc_header_buf), (gst_x264_enc_encode_frame):
Use hyphen in property name, perform safety buffer size check
prior to mem access, and some more parentheses in macro.
Original commit message from CVS:
* ext/x264/gstx264enc.c: (gst_x264_enc_class_init),
(gst_x264_enc_header_buf), (gst_x264_enc_encode_frame):
Use hyphen in property name, perform safety buffer size check
prior to mem access, and some more parentheses in macro.
[MOVED FROM BAD 20/28] ext/apexsink/Makefile.am: Link against -lgcrpyto for RSA_new and RSA_free.
Original commit message from CVS:
* ext/apexsink/Makefile.am:
Link against -lgcrpyto for RSA_new and RSA_free.
* ext/faac/gstfaac.c:
* ext/x264/gstx264enc.c:
Fix compiler warnings.
Original commit message from CVS:
* ext/apexsink/Makefile.am:
Link against -lgcrpyto for RSA_new and RSA_free.
* ext/faac/gstfaac.c:
* ext/x264/gstx264enc.c:
Fix compiler warnings.
14 years ago[MOVED FROM BAD 19/28] ext/x264/gstx264enc.c: Construct source caps in more conventio...
[MOVED FROM BAD 19/28] ext/x264/gstx264enc.c: Construct source caps in more conventional (and correct) manner.
Original commit message from CVS:
* ext/x264/gstx264enc.c: (gst_x264_enc_set_src_caps):
Construct source caps in more conventional (and correct) manner.
Original commit message from CVS:
* ext/x264/gstx264enc.c: (gst_x264_enc_set_src_caps):
Construct source caps in more conventional (and correct) manner.
[MOVED FROM BAD 18/28] Don't install static libs for plugins. Fixes #550851 for -bad.
Original commit message from CVS:
* ext/alsaspdif/Makefile.am:
* ext/amrwb/Makefile.am:
* ext/apexsink/Makefile.am:
* ext/arts/Makefile.am:
* ext/artsd/Makefile.am:
* ext/audiofile/Makefile.am:
* ext/audioresample/Makefile.am:
* ext/bz2/Makefile.am:
* ext/cdaudio/Makefile.am:
* ext/celt/Makefile.am:
* ext/dc1394/Makefile.am:
* ext/dirac/Makefile.am:
* ext/directfb/Makefile.am:
* ext/divx/Makefile.am:
* ext/dts/Makefile.am:
* ext/faac/Makefile.am:
* ext/faad/Makefile.am:
* ext/gsm/Makefile.am:
* ext/hermes/Makefile.am:
* ext/ivorbis/Makefile.am:
* ext/jack/Makefile.am:
* ext/jp2k/Makefile.am:
* ext/ladspa/Makefile.am:
* ext/lcs/Makefile.am:
* ext/libfame/Makefile.am:
* ext/libmms/Makefile.am:
* ext/metadata/Makefile.am:
* ext/mpeg2enc/Makefile.am:
* ext/mplex/Makefile.am:
* ext/musepack/Makefile.am:
* ext/musicbrainz/Makefile.am:
* ext/mythtv/Makefile.am:
* ext/nas/Makefile.am:
* ext/neon/Makefile.am:
* ext/ofa/Makefile.am:
* ext/polyp/Makefile.am:
* ext/resindvd/Makefile.am:
* ext/sdl/Makefile.am:
* ext/shout/Makefile.am:
* ext/snapshot/Makefile.am:
* ext/sndfile/Makefile.am:
* ext/soundtouch/Makefile.am:
* ext/spc/Makefile.am:
* ext/swfdec/Makefile.am:
* ext/tarkin/Makefile.am:
* ext/theora/Makefile.am:
* ext/timidity/Makefile.am:
* ext/twolame/Makefile.am:
* ext/x264/Makefile.am:
* ext/xine/Makefile.am:
* ext/xvid/Makefile.am:
* gst-libs/gst/app/Makefile.am:
* gst-libs/gst/dshow/Makefile.am:
* gst/aiffparse/Makefile.am:
* gst/app/Makefile.am:
* gst/audiobuffer/Makefile.am:
* gst/bayer/Makefile.am:
* gst/cdxaparse/Makefile.am:
* gst/chart/Makefile.am:
* gst/colorspace/Makefile.am:
* gst/dccp/Makefile.am:
* gst/deinterlace/Makefile.am:
* gst/deinterlace2/Makefile.am:
* gst/dvdspu/Makefile.am:
* gst/festival/Makefile.am:
* gst/filter/Makefile.am:
* gst/flacparse/Makefile.am:
* gst/flv/Makefile.am:
* gst/games/Makefile.am:
* gst/h264parse/Makefile.am:
* gst/librfb/Makefile.am:
* gst/mixmatrix/Makefile.am:
* gst/modplug/Makefile.am:
* gst/mpeg1sys/Makefile.am:
* gst/mpeg4videoparse/Makefile.am:
* gst/mpegdemux/Makefile.am:
* gst/mpegtsmux/Makefile.am:
* gst/mpegvideoparse/Makefile.am:
* gst/mve/Makefile.am:
* gst/nsf/Makefile.am:
* gst/nuvdemux/Makefile.am:
* gst/overlay/Makefile.am:
* gst/passthrough/Makefile.am:
* gst/pcapparse/Makefile.am:
* gst/playondemand/Makefile.am:
* gst/rawparse/Makefile.am:
* gst/real/Makefile.am:
* gst/rtjpeg/Makefile.am:
* gst/rtpmanager/Makefile.am:
* gst/scaletempo/Makefile.am:
* gst/sdp/Makefile.am:
* gst/selector/Makefile.am:
* gst/smooth/Makefile.am:
* gst/smoothwave/Makefile.am:
* gst/speed/Makefile.am:
* gst/speexresample/Makefile.am:
* gst/stereo/Makefile.am:
* gst/subenc/Makefile.am:
* gst/tta/Makefile.am:
* gst/vbidec/Makefile.am:
* gst/videodrop/Makefile.am:
* gst/videosignal/Makefile.am:
* gst/virtualdub/Makefile.am:
* gst/vmnc/Makefile.am:
* gst/y4m/Makefile.am:
* sys/acmenc/Makefile.am:
* sys/cdrom/Makefile.am:
* sys/dshowdecwrapper/Makefile.am:
* sys/dshowsrcwrapper/Makefile.am:
* sys/dvb/Makefile.am:
* sys/dxr3/Makefile.am:
* sys/fbdev/Makefile.am:
* sys/oss4/Makefile.am:
* sys/qcam/Makefile.am:
* sys/qtwrapper/Makefile.am:
* sys/vcd/Makefile.am:
* sys/wininet/Makefile.am:
* win32/common/config.h:
Don't install static libs for plugins. Fixes #550851 for -bad.
Original commit message from CVS:
* ext/alsaspdif/Makefile.am:
* ext/amrwb/Makefile.am:
* ext/apexsink/Makefile.am:
* ext/arts/Makefile.am:
* ext/artsd/Makefile.am:
* ext/audiofile/Makefile.am:
* ext/audioresample/Makefile.am:
* ext/bz2/Makefile.am:
* ext/cdaudio/Makefile.am:
* ext/celt/Makefile.am:
* ext/dc1394/Makefile.am:
* ext/dirac/Makefile.am:
* ext/directfb/Makefile.am:
* ext/divx/Makefile.am:
* ext/dts/Makefile.am:
* ext/faac/Makefile.am:
* ext/faad/Makefile.am:
* ext/gsm/Makefile.am:
* ext/hermes/Makefile.am:
* ext/ivorbis/Makefile.am:
* ext/jack/Makefile.am:
* ext/jp2k/Makefile.am:
* ext/ladspa/Makefile.am:
* ext/lcs/Makefile.am:
* ext/libfame/Makefile.am:
* ext/libmms/Makefile.am:
* ext/metadata/Makefile.am:
* ext/mpeg2enc/Makefile.am:
* ext/mplex/Makefile.am:
* ext/musepack/Makefile.am:
* ext/musicbrainz/Makefile.am:
* ext/mythtv/Makefile.am:
* ext/nas/Makefile.am:
* ext/neon/Makefile.am:
* ext/ofa/Makefile.am:
* ext/polyp/Makefile.am:
* ext/resindvd/Makefile.am:
* ext/sdl/Makefile.am:
* ext/shout/Makefile.am:
* ext/snapshot/Makefile.am:
* ext/sndfile/Makefile.am:
* ext/soundtouch/Makefile.am:
* ext/spc/Makefile.am:
* ext/swfdec/Makefile.am:
* ext/tarkin/Makefile.am:
* ext/theora/Makefile.am:
* ext/timidity/Makefile.am:
* ext/twolame/Makefile.am:
* ext/x264/Makefile.am:
* ext/xine/Makefile.am:
* ext/xvid/Makefile.am:
* gst-libs/gst/app/Makefile.am:
* gst-libs/gst/dshow/Makefile.am:
* gst/aiffparse/Makefile.am:
* gst/app/Makefile.am:
* gst/audiobuffer/Makefile.am:
* gst/bayer/Makefile.am:
* gst/cdxaparse/Makefile.am:
* gst/chart/Makefile.am:
* gst/colorspace/Makefile.am:
* gst/dccp/Makefile.am:
* gst/deinterlace/Makefile.am:
* gst/deinterlace2/Makefile.am:
* gst/dvdspu/Makefile.am:
* gst/festival/Makefile.am:
* gst/filter/Makefile.am:
* gst/flacparse/Makefile.am:
* gst/flv/Makefile.am:
* gst/games/Makefile.am:
* gst/h264parse/Makefile.am:
* gst/librfb/Makefile.am:
* gst/mixmatrix/Makefile.am:
* gst/modplug/Makefile.am:
* gst/mpeg1sys/Makefile.am:
* gst/mpeg4videoparse/Makefile.am:
* gst/mpegdemux/Makefile.am:
* gst/mpegtsmux/Makefile.am:
* gst/mpegvideoparse/Makefile.am:
* gst/mve/Makefile.am:
* gst/nsf/Makefile.am:
* gst/nuvdemux/Makefile.am:
* gst/overlay/Makefile.am:
* gst/passthrough/Makefile.am:
* gst/pcapparse/Makefile.am:
* gst/playondemand/Makefile.am:
* gst/rawparse/Makefile.am:
* gst/real/Makefile.am:
* gst/rtjpeg/Makefile.am:
* gst/rtpmanager/Makefile.am:
* gst/scaletempo/Makefile.am:
* gst/sdp/Makefile.am:
* gst/selector/Makefile.am:
* gst/smooth/Makefile.am:
* gst/smoothwave/Makefile.am:
* gst/speed/Makefile.am:
* gst/speexresample/Makefile.am:
* gst/stereo/Makefile.am:
* gst/subenc/Makefile.am:
* gst/tta/Makefile.am:
* gst/vbidec/Makefile.am:
* gst/videodrop/Makefile.am:
* gst/videosignal/Makefile.am:
* gst/virtualdub/Makefile.am:
* gst/vmnc/Makefile.am:
* gst/y4m/Makefile.am:
* sys/acmenc/Makefile.am:
* sys/cdrom/Makefile.am:
* sys/dshowdecwrapper/Makefile.am:
* sys/dshowsrcwrapper/Makefile.am:
* sys/dvb/Makefile.am:
* sys/dxr3/Makefile.am:
* sys/fbdev/Makefile.am:
* sys/oss4/Makefile.am:
* sys/qcam/Makefile.am:
* sys/qtwrapper/Makefile.am:
* sys/vcd/Makefile.am:
* sys/wininet/Makefile.am:
* win32/common/config.h:
Don't install static libs for plugins. Fixes #550851 for -bad.