mpeg2dec: fix spurious failure to decode some files
Parsing can return with an 'invalid' state, but this is not
actually fatal. For one, the mpeg2dec command line tool that
comes with the libmpeg2 library blithely ignores this condition
and merrily goes on. So we do this same, logging the error,
and going on with parsing. This makes something work that did
not use to work, and brings happiness to the world.
https://bugzilla.gnome.org/show_bug.cgi?id=429476
Parsing can return with an 'invalid' state, but this is not
actually fatal. For one, the mpeg2dec command line tool that
comes with the libmpeg2 library blithely ignores this condition
and merrily goes on. So we do this same, logging the error,
and going on with parsing. This makes something work that did
not use to work, and brings happiness to the world.
https://bugzilla.gnome.org/show_bug.cgi?id=429476
x264enc: Properly set the stream format in setcaps
Do not forget to set the selected format to the options string
when getting it from caps
https://bugzilla.gnome.org/show_bug.cgi?id=655223
Do not forget to set the selected format to the options string
when getting it from caps
https://bugzilla.gnome.org/show_bug.cgi?id=655223
x264enc: fix the build for older x264enc
b_fake_interlaced was introduced in x264 commit 1b48874d06 = X264_BUILD 96.
b_fake_interlaced was introduced in x264 commit 1b48874d06 = X264_BUILD 96.
x264enc: Read stream-format from the right place
Read the stream-format from "stream-format" and not from profile, also rename
the "bytestream" variable to "stream_format" so it's easier to understand.
Read the stream-format from "stream-format" and not from profile, also rename
the "bytestream" variable to "stream_format" so it's easier to understand.
x264enc: Select stream-format based on caps
Makes x264 select its stream-format based on what's available
on caps, the user selected option will be chosen as a fallback
when both options are available.
https://bugzilla.gnome.org/show_bug.cgi?id=644233
Makes x264 select its stream-format based on what's available
on caps, the user selected option will be chosen as a fallback
when both options are available.
https://bugzilla.gnome.org/show_bug.cgi?id=644233
x264: Allow renegotiation but prefer current caps
tests: Test x264enc profiles from the caps
https://bugzilla.gnome.org/show_bug.cgi?id=644233
https://bugzilla.gnome.org/show_bug.cgi?id=644233
x264: Use profile and level from caps
Enforces the profile and level from the downstream caps, also
sets them on the fixated caps
https://bugzilla.gnome.org/show_bug.cgi?id=644233
Enforces the profile and level from the downstream caps, also
sets them on the fixated caps
https://bugzilla.gnome.org/show_bug.cgi?id=644233
x264enc: fix subme property annotation - subme maximum is 10, not 6.
Although the element accepts subme values > 6, the annotation which is
visible through gst-inspect (for example) erroneously indicates 6 as the
maximum. Fix this by indicating 10 (which is the x264 max) as the maximum.
https://bugzilla.gnome.org/show_bug.cgi?id=653473
Although the element accepts subme values > 6, the annotation which is
visible through gst-inspect (for example) erroneously indicates 6 as the
maximum. Fix this by indicating 10 (which is the x264 max) as the maximum.
https://bugzilla.gnome.org/show_bug.cgi?id=653473
rtpasfdepay: fix fragmented packet handling and packet padding
Also remove a bogus assert.
Also remove a bogus assert.
synaesthesia: fix wrong debug log string (copy'n'paste)
rmdemux: target is unsigned and can't be < 0
mad: use signed when caluculating the delta
Avoids a <0 check for an unsigned variable.
Avoids a <0 check for an unsigned variable.
docs: remove obsolete commented out part
We don't have this in the other modules and its not needed.
We don't have this in the other modules and its not needed.
docs: update plugin introspection data
Now more files are merged and produced in a canonical fashion, which hopefully
creates less or no delta in the future.
Now more files are merged and produced in a canonical fashion, which hopefully
creates less or no delta in the future.
lamemp3enc: Post CODEC and BITRATE tags
Also filter any CODEC/AUDIO_CODEC tags from incoming
tag events.
Fixes bug #391543.
Also filter any CODEC/AUDIO_CODEC tags from incoming
tag events.
Fixes bug #391543.
rtpasfdepay: simplify and refactor packet parsing
Specifically, refactor buffer padding and consider marker bit for fragment
assembling.
Specifically, refactor buffer padding and consider marker bit for fragment
assembling.
rtpasfdepay: avoid re-sending header
... e.g. following a seek, which otherwise confuses downstream demuxer
expecting only a flow of data packets at this time.
... e.g. following a seek, which otherwise confuses downstream demuxer
expecting only a flow of data packets at this time.
rtpasfdepay: remove unused field
mad: Post bitrate tag whenever the bitrate changes
Also send the layer/mode/emphasis/bitrate tags as an event too.
Also send the layer/mode/emphasis/bitrate tags as an event too.
win32: define GST_PACKAGE_RELEASE_DATETIME in win32 config.h as well
Back to development
Release 0.10.18
Highlights:
- x264enc: allow changing bitrate and quantizers dynamically at runtime
- x264enc: proxy downstream caps restrictions upstream via get_caps()
- lamemp3enc: proxy downstream rate/channels restrictions upstream via get_caps()
- mad: allow build without libid3tag (which isn't really needed anyway)
- many other fixes and improvements
Highlights:
- x264enc: allow changing bitrate and quantizers dynamically at runtime
- x264enc: proxy downstream caps restrictions upstream via get_caps()
- lamemp3enc: proxy downstream rate/channels restrictions upstream via get_caps()
- mad: allow build without libid3tag (which isn't really needed anyway)
- many other fixes and improvements
x264enc: Copy the template caps, it's not allowed to increase the refcount of const caps
x264enc: do not leak peer pad reference
x264enc: No need to copy, reffing is enough
x264enc: get_caps function should return a copy of the caps
0.10.17.4 pre-release
0.10.17.3 pre-release
tests: add suppression for lame unit test
tests: add generic index-setting test
mpeg2dec: don't deadlock when setting an index
0.10.17.2 pre-release
12 years agorademux: fix two 'variable may be used uninitialized' warnings caused by -DG_DISABLE_...
rademux: fix two 'variable may be used uninitialized' warnings caused by -DG_DISABLE_ASSERT
mpegstream: fix unused-but-set-variable warnings with gcc 4.6
dvdread, sidplay, x264enc: fix unused-but-set-variable warnings with gcc 4.6
asfdemux: fix unused-but-set-variable warnings with gcc 4.6
x264enc: Implement getcaps function
This allows to set width/height/etc restrictions downstream.
This allows to set width/height/etc restrictions downstream.
android: make it ready for androgenizer
To build gstreamer for android we are now using androgenizer which
generates the needed Android.mk files.
Androgenizer can be found here: http://git.collabora.co.uk/?p=user/derek/androgenizer.git
To build gstreamer for android we are now using androgenizer which
generates the needed Android.mk files.
Androgenizer can be found here: http://git.collabora.co.uk/?p=user/derek/androgenizer.git
android: remove the android/ folder
x264enc: Allow changing the bitrate and quantitizers dynamically
https://bugzilla.gnome.org/show_bug.cgi?id=621663
https://bugzilla.gnome.org/show_bug.cgi?id=621663
x264enc: Set max bitrate in quality mode
https://bugzilla.gnome.org/show_bug.cgi?id=621663
https://bugzilla.gnome.org/show_bug.cgi?id=621663
x264enc: Make it clear that constant quantizer is for debugging only
https://bugzilla.gnome.org/show_bug.cgi?id=621663
https://bugzilla.gnome.org/show_bug.cgi?id=621663
configure.ac: redundant use of AC_MSG_RESULT()
cleaned the redundant use of AC_MSG_RESULT() in configure.ac
cleaned the redundant use of AC_MSG_RESULT() in configure.ac
autogen: wingo signed comment
dvdsubdec: Rearrange buffer allocation and pushing code a bit
This makes the code easier to read, doesn't store every buffer
in the instance until the next buffer is to be drawn and
fixes an unitialized variable compiler warning.
This makes the code easier to read, doesn't store every buffer
in the instance until the next buffer is to be drawn and
fixes an unitialized variable compiler warning.
dvdsubdec: Output only a single buffer per subpicture and set the correct duration
Fixes bug #619136.
Fixes bug #619136.
dvdsubdec: Implement clipping if the video size is smaller than the subpicture size
Fixes bug #644704.
Fixes bug #644704.
mad: build the mad plugin even if libid3tag is not available
ID3 tags are usually handled by id3demux, and should be handled
by id3demux. Tag handling in mad based on libid3tag is very basic
and mostly unnecessary really, so just build this plugin without
ID3 tag support if libid3tag is not available.
ID3 tags are usually handled by id3demux, and should be handled
by id3demux. Tag handling in mad based on libid3tag is very basic
and mostly unnecessary really, so just build this plugin without
ID3 tag support if libid3tag is not available.
dvddemux: small code cleanup
Don't duplicate the 'if' check. Makes the 2nd condition easier to read also
and avoid empty 'if' when logging is disabled.
Don't duplicate the 'if' check. Makes the 2nd condition easier to read also
and avoid empty 'if' when logging is disabled.
configure.ac: export plugin description more platform independent
Fixes #642504.
Fixes #642504.
mpeg2dec: do not fail fatally when unlinked
... as _NOT_LINKED was neither tested as fatal before nor complained about.
... as _NOT_LINKED was neither tested as fatal before nor complained about.
index: remove conditional index support
Index support cannot be disabled since commit
4bfb1fe70c6f0d5e29c17a8eeffb02f7fd083f11
in core, which removed the configure flags to disable index.
Index support cannot be disabled since commit
4bfb1fe70c6f0d5e29c17a8eeffb02f7fd083f11
in core, which removed the configure flags to disable index.
formatting: trim trailing whitespace
index: use delta frame flags instead of 0 or none
x264enc: Don't register flags with a value of 0
Flags with a value of 0 aren't meaningful and will cause
g_value_transform to go into an endless loop when trying to
convert the flags to a string
Flags with a value of 0 aren't meaningful and will cause
g_value_transform to go into an endless loop when trying to
convert the flags to a string
amrwbdec: avoid stalling on invalid frame
Skip 1 byte indicating invalid frame type index rather than stalling
on it indefinitely until EOS.
Fixes #639715.
Skip 1 byte indicating invalid frame type index rather than stalling
on it indefinitely until EOS.
Fixes #639715.
tests: add unit test for lamemp3enc negotiation issue
https://bugzilla.gnome.org/show_bug.cgi?id=641151
https://bugzilla.gnome.org/show_bug.cgi?id=641151
13 years agolamemp3enc: implement sinkpad get_caps() function to proxy rate and channels restrict...
lamemp3enc: implement sinkpad get_caps() function to proxy rate and channels restrictions from downstream
The element downstream of mp3enc might only accept certain sample rates or channels,
make sure we relay any restrictions that do exist to upstream when it does a
get_caps() on the sink pad. That way upstream elements like audioresample or
audioconvert can pick a sample rate / channel configuration that will be accepted,
instead of just negotiating to the highest, which might then be rejected.
https://bugzilla.gnome.org/show_bug.cgi?id=641151
The element downstream of mp3enc might only accept certain sample rates or channels,
make sure we relay any restrictions that do exist to upstream when it does a
get_caps() on the sink pad. That way upstream elements like audioresample or
audioconvert can pick a sample rate / channel configuration that will be accepted,
instead of just negotiating to the highest, which might then be rejected.
https://bugzilla.gnome.org/show_bug.cgi?id=641151
asfpacket: Avoid using broken duration extension
Quite a few (broken?) files have a packet duration of 1ms, which is
most definitely wrong for either audio or video packets.
We therefore avoid using that value and instead use other metrics to
determine the buffer duration (like using the extended stream properties
average frame duration if present and valid).
Quite a few (broken?) files have a packet duration of 1ms, which is
most definitely wrong for either audio or video packets.
We therefore avoid using that value and instead use other metrics to
determine the buffer duration (like using the extended stream properties
average frame duration if present and valid).
win32: fix DEFAULT_AUDIOSINK, should be direct*sound*sink
https://bugzilla.gnome.org/show_bug.cgi?id=640705
https://bugzilla.gnome.org/show_bug.cgi?id=640705
xingmux: Use FALSE instead of 0 as return value for a function returning gboolean
Fixes bug #639291.
Fixes bug #639291.
mpegstream: increase allowable gap between streams
The new delay is three times as much as the old one, and just happens
to let me properly decode my "Princess Mononoke" DVD, on which dvdreadsrc
was chocking before at 5:11.
While there, merge the constants used in two places into a define.
https://bugzilla.gnome.org/show_bug.cgi?id=539708
The new delay is three times as much as the old one, and just happens
to let me properly decode my "Princess Mononoke" DVD, on which dvdreadsrc
was chocking before at 5:11.
While there, merge the constants used in two places into a define.
https://bugzilla.gnome.org/show_bug.cgi?id=539708
x264enc: make tag event writable before modifying tag list in place
To modify an event tag is necessary to be sure that x264enc
has its own copy.
Also fix indentation.
https://bugzilla.gnome.org/show_bug.cgi?id=640272
To modify an event tag is necessary to be sure that x264enc
has its own copy.
Also fix indentation.
https://bugzilla.gnome.org/show_bug.cgi?id=640272
Back to development
Release 0.10.17
0.10.16.4 pre-release
mpeg2dec: Use the proper component value for height
0.10.16.3 pre-release
asfdemux: Handle new type of DRM'd asf files.
These are produced by the new MS PlayReady system.
https://bugzilla.gnome.org/show_bug.cgi?id=639226
These are produced by the new MS PlayReady system.
https://bugzilla.gnome.org/show_bug.cgi?id=639226
tests: never disable g_assert() and cast checks for the unit tests
The unit tests are riddled with g_assert() and friends, make sure we
don't disable assert and cast checks for the unit tests even if
this has been specified for the rest of the code base, e.g. via
--disable-glib-asserts
The unit tests are riddled with g_assert() and friends, make sure we
don't disable assert and cast checks for the unit tests even if
this has been specified for the rest of the code base, e.g. via
--disable-glib-asserts
0.10.16.2 pre-release
docs: update docs
po: update translations
configure: use $LIBM instead of hardcoding -lm
rmdemux: Initialize return variable.
In the unlikely event that height is 0 (which is invalid) we would end up
never setting the flow return.
In the unlikely event that height is 0 (which is invalid) we would end up
never setting the flow return.
realmedia: Fix unitialized variables on macosx
x264enc: Handle codec/encoder tags
Make x264enc drop video-codec and codec tags and replace
encoder/encoder-version with x264 and its build number
Fixes #621465
Make x264enc drop video-codec and codec tags and replace
encoder/encoder-version with x264 and its build number
Fixes #621465
mpeg2dec: use gst_pad_alloc_buffer() when cropping buffers
mpeg2dec: minor formatting clean-up
mpeg2dec: refactor cropping code to use libgstvideo functions
https://bugzilla.gnome.org/show_bug.cgi?id=571146
https://bugzilla.gnome.org/show_bug.cgi?id=571146
mpeg2dec: use GstVideoFormat instead of custom enum
mpeg2dec: fix LIBADD order in Makefile.am