From 9d2202097bf94b69f6f5f92c59276875c81579e1 Mon Sep 17 00:00:00 2001 From: Thomas Vander Stichele Date: Mon, 23 Sep 2002 05:49:26 +0000 Subject: [PATCH] better README Original commit message from CVS: better README --- README | 103 +++++++++++++++++++++++++++++++++++++++++++++++++++------ 1 file changed, 93 insertions(+), 10 deletions(-) diff --git a/README b/README index fb003a98..f60e0d77 100644 --- a/README +++ b/README @@ -1,18 +1,101 @@ -gst-plugins : plug-ins for GStreamer +WHAT IT IS +---------- +This is gst-plugins, a set of plug-ins for GStreamer. -* to develop against uninstalled GStreamer core : - add path to gstreamer-uninstalled.pc to PKG_CONFIG_PATH - or run configure --with-pkg-config-path=(path to gstreamer uninstalled) +COMPILING FROM SOURCE +--------------------- +- make sure you compiled and at least did a test-run of GStreamer (core) +- check output of ./configure --help to see if any options apply to you +- configure the source tree: + - if you installed GStreamer, then do: + ./configure + If configure complains about missing GStreamer, you should try + ./configure --with-pkg-config-path=prefix/lib/pkgconfig + where prefix should be replaced by the prefix you used to configure + GStreamer. (Be mindful NOT to ADD a trailing / to that option !) + If this doesn't fix it, you have other issues ;) -* to register plug-ins in source tree - run gst-register --gst-plugin-path=. + - if you didn't install GStreamer, you can still compile the plug-ins. + Add the path to gstreamer-uninstalled.pc (which lives in the gstreamer + source tree) to PKG_CONFIG_PATH + or run configure --with-pkg-config-path=(path to gstreamer uninstalled) + + - the output of configure will give you a list of plug-ins with external + dependencies (ie, depending on other libs, see below). By no means + should you try to get them all built on your first run. This is hard + enough as it is ;) Resist the urge to get the most features for now. + It doesn't list all of the non-depending plug-ins, which get built + regardless (unless you explicitly asked it not to). -* if a certain plug-in doesn't build, then redo configure with - --disable-(plug-in) - to disable it from the build +- build the tree: + make + If any plug-in causes a problem at this stage, you should re-configure + with --disable-(dependency) + and doublecheck if configure reports this plug-in as being disabled. + Then re-run make. -* Additional documentation : +- install: + - if you installed GStreamer, and want to install the plug-ins as well, run + make install + and, as root, run + gst-register + - if you installed GStreamer, but don't want to install the plug-ins, run + gst-register --gst-plugin-path=. + - if you didn't install GStreamer, then do + path/to/gstreamer/tools/gst-register --gst-plugin-path=. + (Replace path/to/gstreamer obviously) +- test: + - run + gst-launch sinesrc ! fakesink + and prefix gst-launch with the path to gstreamer/tools if you didn't install + GStreamer. + If this doesn't give any errors, you can abort it. + + - try replacing fakesink with your choice of + osssink/esdsink/artsdsink/alsasink/jacksink (depending on what output + method you have available) and see if you hear a C tone. + +- After this, you should look into installing an application, like + gst-player, gst-editor or monkey-media with rhythmbox. + +COMPILING FROM CVS +------------------ +When building from CVS sources, you will need to run autogen.sh to generate +the build system files. + +GStreamer is cutting-edge stuff. To be a CVS developer, you need +what used to be considered cutting-edge tools. + +ATM, most of us have at least these versions : + +* autoconf 2.52 (NOT 2.52d) +* automake 1.5 +* libtool 1.4 (NOT Gentoo's genetic failure 1.4.2) +* pkg-config 0.8.0 + +autogen.sh will check for these versions and complain if you don't have +them. You can also specify specific versions of automake and autoconf with +--with-automake and --with-autoconf + +Check autogen.sh options by running autogen.sh --help + +autogen.sh can pass on arguments to configure - you just need to separate them +from autogen.sh with -- between the two. +prefix has been added to autogen.sh but will be passed on to configure because +some build scripts like that. +You will probably have to pass at least --with-pkg-config-path to autogen.sh +to point to the CVS version of GStreamer. + +When you have done this once, you can use autoregen.sh to re-autogen with +the last passed options as a handy shortcut. Use it. + +After the autogen.sh stage, you can follow the directions listed in +"COMPILING FROM SOURCE" + + +PLUG-IN DEPENDENCIES AND LICENSES +--------------------------------- GStreamer is developed under the terms of the LGPL (see LICENSE file for details). Some of our plug-ins however rely on libraries which are available under other licenses. This means that if you are using an application which -- 2.39.2