glsdk/gst-plugins-ugly0-10.git
2006-06-12 Wim Taymanstests/check/elements/amrnbenc.c: Init memory before...
2006-06-12 Edward Herveygst/asfdemux/.cvsignore: More ignore
2006-06-11 Tim-Philipp... .cvsignore: Ignore files generated by 'make dist'.
2006-06-11 Thomas Vander... update build files
2006-06-11 Thomas Vander... autogen.sh: require am17
2006-06-07 Wim Taymansext/mpeg2dec/gstmpeg2dec.*: Simplify and don't leak...
2006-06-07 Wim Taymansext/mpeg2dec/gstmpeg2dec.*: Fix padtemplate as we can...
2006-06-05 Sébastien Mouttewin32/MANIFEST: Add a manifest for futures ugly win32...
2006-06-01 Stefan KostFix more gobject macros: obj<->klass, GstXXX<->GstXXXClass
2006-06-01 Stefan KostFix more gobject macros: obj<->klass, GstXXX<->GstXXXClass
2006-05-27 Tim-Philipp... README: Replace current README (containing the release...
2006-05-24 Wim Taymansext/amrnb/: Sortof first quick cleanup of all this...
2006-05-22 Tim-Philipp... gst/asfdemux/gstasf.c: Call gst_riff_init() so the...
2006-05-19 Michael Smithgst/iec958/: Write rate into the caps, for the allowed...
2006-05-18 James Doc Livingstonext/mad/gstid3tag.c: Do tag merging correctly (#339918...
2006-05-11 Jan Schmidtext/a52dec/gsta52dec.c: Add more debug
2006-05-11 Michael Smithgst/dvdlpcmdec/gstdvdlpcmdec.c: Fix timestamping for...
2006-05-10 Tim-Philipp... gst/asfdemux/gstasfdemux.c: Fix silly bug when reading...
2006-05-08 Edward Herveyautogen.sh: libtoolize on Darwin/MacOSX is called glibt...
2006-05-06 Tim-Philipp... ext/lame/gstlame.*: Remove tag writing from lame (which...
2006-05-06 Maciej KatafiaszAdd semicolons after GST_BOILERPLATE[_FULL] so that...
2006-05-05 Andres Salomonext/lame/gstlame.c: Fix typo (comma vs. semicolon)...
2006-05-04 Lutz Müllerext/mad/gstmad.c: Make mad the second element to suppor...
2006-05-02 Edward Herveyext/mpeg2dec/gstmpeg2dec.c: Remember the query duration...
2006-04-25 Stefan KostDefine GstElementDetails as const and also static ...
2006-04-25 Stefan KostDefine GstElementDetails as const and also static ...
2006-04-25 Stefan KostDefine GstElementDetails as const and also static ...
2006-04-25 Tim-Philipp... ext/dvdnav/dvdnavsrc.c: Fix name of custom event (use...
2006-04-23 Tim-Philipp... ext/mad/gstid3tag.c: Change debug category to 'id3mux'.
2006-04-22 Alexander Lancasterext/mad/gstid3tag.c: When acting as a muxer, set caps...
2006-04-21 Tim-Philipp... ext/mad/gstmad.c: .. and DEFAULT queries should work...
2006-04-21 Tim-Philipp... ext/mad/gstmad.c: Fix duration query in BYTES format...
2006-04-21 Ed Catmurext/lame/gstlame.c: Don't crash if we get an EOS event...
2006-04-21 Wim Taymansext/dvdread/dvdreadsrc.c: Move errors out of the normal...
2006-04-21 Wim Taymansgst/mpegstream/: Do state changes correctly
2006-04-13 Tim-Philipp... ext/mpeg2dec/gstmpeg2dec.c: Can't use gst_pad_alloc_buf...
2006-04-13 Tim-Philipp... gst/mpegstream/gstmpegpacketize.*: g_malloc() can't...
2006-04-12 Thomas Vander... one more suppression for FC4
2006-04-10 Michael SmithThe AMR encoder sucks giant sucky things through a...
2006-04-10 Thomas Vander... add test for amrnbenc, enable test infrastructure,...
2006-04-10 Michael Smithext/amrnb/amrnbenc.c: Plug big leak in AMR encoder.
2006-04-09 Sébastien Moutteext/mad/gstmad.c: move GstIndexEntry *entry variable...
2006-04-08 Stefan KostFix #337365 (g_type_class_ref <-> g_type_class_peek_parent)
2006-04-07 Fabrizio Gennarigst/asfdemux/gstasfdemux.c: Send newsegment event only...
2006-04-06 j^Unify the long descriptions in the plugin details ...
2006-04-05 Christian Schallerfix version numbering
2006-04-05 Christian Schalleradd dvdsub plugin to spec
2006-04-01 Thomas Vander... docs/plugins/: add siddec
2006-04-01 Thomas Vander... disable use of AS_LIBTOOL_TAGS, it doesn't work correctly
2006-04-01 Thomas Vander... ignore more
2006-04-01 Thomas Vander... update plugin inspect files
2006-04-01 Thomas Vander... rework build; add translations for v4l2
2006-04-01 Thomas Vander... configure.ac: rework similarly to other modules
2006-04-01 Thomas Vander... ignore more
2006-03-31 Thomas Vander... back to HEAD
2006-03-31 Thomas Vander... releasing 0.10.3
2006-03-30 Wim Taymansbetter/unified long descriptions
2006-03-29 Tim-Philipp... gst/mpegstream/gstmpegparse.c: Don't unref event uncond...
2006-03-28 Tim-Philipp... gst/mpegstream/gstmpegdemux.c: Don't ref NULL caps...
2006-03-28 Tim-Philipp... gst/mpegstream/: Don't leak element and pad names in...
2006-03-28 Tim-Philipp... ext/dvdread/dvdreadsrc.c: Name the structure in the...
2006-03-28 Tim-Philipp... ext/lame/gstlame.*: Make xingheader property non-functi...
2006-03-28 Tim-Philipp... ext/lame/gstlame.c: On EOS, flush encoder and send...
2006-03-27 Jürg Billeterext/dvdread/dvdreadsrc.c: Fix wrong check for started...
2006-03-27 Fabrizio Gennarigst/asfdemux/gstasfdemux.*: Subtract first timestamp...
2006-03-27 Christian Kirbachconfigure.ac: Remove CXX tag from AS_LIBTOOL_TAGS,...
2006-03-24 Tim-Philipp... gst/realmedia/rmdemux.c: Extract more tags and also...
2006-03-24 Tim-Philipp... gst/realmedia/rmdemux.c: Extra data usually goes into...
2006-03-24 Tim-Philipp... gst/realmedia/rmdemux.c: When operating in pull mode...
2006-03-24 Tim-Philipp... gst/realmedia/rmdemux.*: Handle unlinked source pads...
2006-03-23 Michal Benesgst/mpegstream/: Timestamps in mpeg stream are 32-bit...
2006-03-15 Michael Smithext/a52dec/gsta52dec.*: Fix #334550: failure to play...
2006-03-15 Christophe... ext/lame/gstlame.c: use GST_DEBUG_FUNCPTR more often.
2006-03-14 Tim-Philipp... ext/mad/gstmad.c: Include AUDIO_CODEC tag with tags...
2006-03-12 Christophe... ext/lame/gstlame.c: mark the xing-header property as...
2006-03-11 Christophe... added new element to add Xing headers to MP3 files...
2006-03-07 Alex Lancasterext/mad/gstid3tag.c: Add support for writing the GST_TA...
2006-03-02 Wim Taymansext/amrnb/: Further fancyfication.
2006-03-02 Michael Smithext/amrnb/amrnbenc.c: The AMR encoder writes into the...
2006-03-01 Jens Granseuergst/mpegstream/gstmpegparse.c: Declare variables at...
2006-03-01 Fabriziogst/asfdemux/gstasfdemux.c: Read packet size, sequence...
2006-02-28 Edward Herveygst/iec958/ac3iec.c: Set a proper klass (Codec/Muxer...
2006-02-27 Jan Schmidtconfigure.ac: Make the id3tag and mad checks check...
2006-02-27 Tim-Philipp... ext/mpeg2dec/gstmpeg2dec.*: Don't treat STATE_INVALID...
2006-02-26 Tim-Philipp... ext/dvdnav/dvdnavsrc.h: Oops. forgot to add this one.
2006-02-26 Julien Moutteext/Makefile.am: Fix dist-check.
2006-02-26 Tim-Philipp... configure.ac: Disable dvdnavsrc for now.
2006-02-26 Tim-Philipp... dvdnavsrc ported to 0.10, for the most part at least...
2006-02-23 Tim-Philipp... ext/cdio/Makefile.am: Add GST_BASE_CFLAGS and GST_BASE_...
2006-02-22 Tim-Philipp... Port dvdsubdec to 0.10
2006-02-21 Jan Schmidtgst/mpegstream/gstdvddemux.c: Push the rank up to SECON...
2006-02-20 Jan Schmidtconfigure.ac: Bump nano back to CVS
2006-02-20 Jan Schmidtconfigure.ac: releasing 0.10.2, "Season to Taste"
2006-02-19 Jan Schmidtconfigure.ac: releasing 0.10.1.3 prelease for 0.10.2
2006-02-17 Tim-Philipp... gst/asfdemux/gstasfdemux.c: In sink event handler,...
2006-02-17 Christian Schallerfix rank of asfdemux
2006-02-17 Jan Schmidtconfigure.ac: releasing 0.10.1.2 prelease for 0.10.2
2006-02-17 Christian Schallerlatest updates
2006-02-17 Tim-Philipp... ext/mpeg2dec/gstmpeg2dec.c: When we need to crop the...
2006-02-17 Tim-Philipp... ext/cdio/gstcdio.c: Init debug category (#331253).
next