1 This is GStreamer 0.10.25 "Feel the burn"
3 Changes since 0.10.24:
5 * Improve the byte-reader API
6 * GObject introspection support
7 * Improve clock accuracy on win32
8 * Optimisations in capabilities checking
9 * Optimisations and fixes in the basetransform base class
10 * new 64-bit scaling utility function variants
11 * Various bug-fixes and improvements (see ChangeLog and bugs list below)
13 Bugs fixed since 0.10.24:
15 * 583999 : [basetransform] caps refcounting problem causing GST_IS_CAPS assertion failures
16 * 566881 : [GstIndex] support/caching in GstBin
17 * 588472 : [basetransform] problems in reverse-negotiating
18 * 589173 : macros cause spurious semicolon warnings
19 * 589314 : [basetransform] clears GAP flag in passthrough mode
20 * 589524 : gst_base_transform_acceptcaps() could provide more verbose debugging output
21 * 589849 : [segment] Clipping fails to handle start=stop < segment_start correctly
22 * 589991 : [queue] limited error handling might cause pipeline appearing to hang
23 * 590045 : Query position fails when pipeline is paused and format is not time
24 * 590430 : Add support for " album artist " tags
25 * 590841 : configure script check for libxml2 is incorrect
26 * 590919 : gst_util_uint64_scale_int() and friends don't round
27 * 591045 : [basesrc] Leaking GstTask instances
28 * 591318 : ghostpad : core dump : on_src_target_notify called with an invalid ghostpad
29 * 591441 : append mode for filesink
30 * 592209 : [GstPad] Deprecated markers missing in the header for internal links function related things
31 * 592314 : core/tests/examples/streams/ does not link to pthread
32 * 593460 : Broken win32-specific systemclock code
33 * 593719 : regression: segfault when using gstrtpbin and certain video codecs
34 * 594107 : [gstbin] : use of freed message : valgrind Invalid read
35 * 594225 : [API] [bytereader] add _unchecked() variants and inline most common functions
36 * 594990 : [introspection] pkg-config file madness and another bug
37 * 595130 : checks fail
38 * 595133 : gst/gstutils check fails
39 * 595209 : Fix out-of-tree build
40 * 368536 : bin_change_state makes children go through unnecessary state changes
42 API additions since 0.10.24:
44 * gst_caps_can_intersect()
45 * gst_util_uint64_scale_int_round()
46 * gst_util_uint64_scale_int_ceil()
47 * gst_util_uint64_scale_round()
48 * gst_util_uint64_scale_ceil()
49 * gst_iterator_new_single()
50 * gst_byte_reader_skip_unchecked()
51 * gst_byte_reader_peek_*_unchecked()
52 * gst_byte_reader_get_*_unchecked()
53 * gst_byte_reader_{peek,get,dup}_data_unchecked()
54 * gst_byte_reader_get_float*_unchecked()
56 Changes since 0.10.23:
58 * Fully support nested structures in caps
59 * Support frame-by-frame stepping in sinks
60 * Add support for buffer-lists to pass around groups of buffers
61 * Use TaskPools for managing worker threads
62 * New stream-status API for finer thread control
63 * Code optimisations
64 * Many other bug-fixes and enhancements
66 Bugs fixed since 0.10.23:
68 * 580579 : crash in Volume Control: aucunes idées désolé.
69 * 527488 : [GstXML] can't load elements with request pads from XML
70 * 570233 : allow plugins caching data in the registry
71 * 584389 : don't recreate plugin feature and element factories on fi...
72 * 534208 : [API] add gst_structure_get()
73 * 545787 : [API] add gst_plugin_register_static_full() for bindings
74 * 554460 : thumbnailer crash in gst_fake_sink_event() on FLUSH_START...
75 * 559643 : Don't allow empty or NULL strings in taglists
76 * 560345 : gst_tag_list_get_string() may return NULL or empty string
77 * 560442 : GNOME Goal: Remove deprecated GLib symbols
78 * 572285 : Buffer Lists
79 * 577926 : Remove old xml registry
80 * 578908 : [fdsink] implement seeking on seekable fds
81 * 580177 : glibc 2.10 deprecates register_printf_function
82 * 580716 : race condition in gst_element_lost_state
83 * 581198 : [tags] Add gst_tag_setter_add_tag_value() and gst_tag_lis...
84 * 581281 : [GstURIHandler] Doesn't use get_type_full() at all
85 * 582010 : audiotestsrc is-live=1 ! pulsesink unreliable
86 * 582564 : [controller] Use ordered GSequence instead of GList in th...
87 * 582588 : [API] Add a way to get the pad corresponding to a taglist
88 * 582878 : [GstClock] ABI breakage in GIT on x86
89 * 583187 : [API] add gst_adapter_masked_scan_uint32() and gst_adapte...
90 * 583419 : Bad translatable string in gst-launch.c
91 * 583456 : framestep functionality
92 * 583554 : Slow down or lock if date time is changed to the past
93 * 584835 : MSVC compiler fails with 'static inline' function
94 * 584838 : basesrc: confusing QUERY_SEEKING handling
95 * 585039 : rtpool-test can't find pthreads
96 * 585075 : Compilation with MSVC fails for files including config.h ...
97 * 585137 : gst_xml_write_file() fails serialising GstStructure property
98 * 585592 : [API] add gst_byte_reader_masked_scan_uint32()
99 * 585733 : Wrong #include order in gstsegment.c
100 * 585748 : [API] add gst_tag_list_new_full() to create taglist with ...
101 * 586566 : Add GAP Flag support to gstcapsfilter
102 * 586568 : [bytereader] add misc. string functions and gst_byte_read...
103 * 587973 : use G_DIR_SEPARATOR_S instead of " /' "
104 * 587976 : Fix for gst-inspect and gst-launch when option parsing is...
105 * 588744 : [check] Stream consistency checker utility
106 * 588745 : [basesrc] Serialize tags in the dataflow
107 * 589127 : gsttask leaks the pool
108 * 590056 : [collectpads] race resulting in double flush-stop being o...
109 * 590622 : [bytereader] buffer size checks subject to wrap-around ov...
110 * 579177 : GstInfo: maintain ABI compatibility
111 * 581321 : typefind element leaks force-caps property
112 * 584118 : [gstadapter][doc] Improve documentation of gst_adapter_ma...
113 * 585433 : [queue] Can lock down if min-threshold conflicts with max...
114 * 585569 : rtsp/rtp streaming fails when skipping explicit PAUSED st...
115 * 585834 : Support for GstBufferList in ghostpads
116 * 585960 : Support for GstBufferList in gstbasesink
117 * 587052 : [filesink.c] Support for files > 4GB on windows makes file...
119 API added since 0.10.23:
121 * GST_DEBUG_CATEGORY_GET() macro
122 * gst_byte_reader_dup_data
123 * gst_byte_reader_dup_string
124 * gst_byte_reader_dup_string_utf8
125 * gst_byte_reader_dup_string_utf16
126 * gst_byte_reader_dup_string_utf32
127 * gst_byte_reader_skip_string
128 * gst_byte_reader_skip_string_utf8
129 * gst_byte_reader_skip_string_utf16
130 * gst_byte_reader_skip_string_utf32
131 * gst_byte_reader_peek_string
132 * gst_byte_reader_peek_string_utf8
133 * gst_byte_reader_get_string
134 * gst_byte_reader_get_string_utf8
135 * add gst_tag_list_new_full()
136 * add gst_tag_list_new_full_valist()
137 * add gst_byte_reader_masked_scan_uint32()
138 * add gst_plugin_get_cache_data, gst_plugin_set_cache_data
139 * gst_structure_get()
140 * gst_structure_id_get()
141 * gst_structure_get_valist()
142 * gst_structure_id_get_valist()
143 * GstSegment::gst_segment_set_running_time()
144 * Add GST_MESSAGE_SRC_NAME() macro
145 * GstSegment::gst_segment_to_position()
146 * GstEvent::gst_event_new_step()
147 * GstEvent::gst_event_parse_step()
148 * GstMessage::gst_message_new_step_done()
149 * GstMessage::gst_message_parse_step_done()
150 * gst_structure_id_new()
151 * Add gst_message_{new,parse}_tag_full() to get/set the source pad
152 * GstAdapter::gst_adapter_masked_scan_uint32()
153 * GstElement::gst_element_lost_state_full()
154 * GstAdapter::gst_adapter_prev_timestamp()
155 * gst_plugin_register_static_full()
156 * gst_tag_list_add_value()
157 * gst_tag_setter_add_tag_value()
158 * add GST_TAG_CONTAINER_FORMAT tag
159 * GstTask::gst_task_set_state()
160 * GstObject::gst_object_ref_sink()
162 Changes since 0.10.22:
163 * Support files > 4GB on Windows
164 * Controller interpolation fixes
165 * Add timer support to GstPoll and use it for clocking
166 * Attempt to typefind contents from the file extension if all else fails
167 * GStreamer revision control switched to Git
168 * Many other bug fixes and improvements
170 Bugs fixed since 0.10.22:
172 * 579177 : GstInfo: maintain ABI compatibility
173 * 163577 : [RFC] Interlaced/progressive media support in GStreamer.
174 * 574160 : collectpads does not reliably eos when last pad is removed
175 * 575598 : hierarchical pipelines accumulate segment-done wrongly
176 * 575922 : disabling subsystems cause API break
177 * 576842 : loading a broken registry file can crash
178 * 555978 : [ladspa] no elements exposed/found on Cygwin
179 * 565607 : Broken macros in gsturi.h and gstinterface.h
180 * 566936 : [ghostpads] unlink function wrongly called on target
181 * 567692 : gstinfo.h header not compatible with C++
182 * 567725 : [qtdemux] stopping at a time sometimes shows a different ...
183 * 568289 : gst_pad_template_new() leaks caps it's supposed to take o...
184 * 568438 : gst_poll_wait calling read() on control socket
185 * 568481 : GStreamer linking failures.
186 * 568632 : __MSVCRT_VERSION__ not defined with mingw, causing " stora...
187 * 568678 : filesrc doesn't logs offsets
188 * 570910 : Removing the target of a ghostpad does not re-target the ...
189 * 571227 : Add home page tag
190 * 571559 : [API] add GST_PARAM_MUTABLE_PLAYING etc. to indicate vali...
191 * 572480 : unref and copy functions should not be macros
192 * 573623 : [API] Array binary search utility function
193 * 574024 : [GstAdapter] gst_adapter_push should not accept empty buf...
194 * 574211 : gst_poll_*_control always returns FALSE on Windows
195 * 574213 : [gstcheck] fix for libcheck > 0.9.6
196 * 574241 : gst_tag_list_add and gst_tag_list_add_values behave incon...
197 * 574484 : [patch] Make caps in DOT debug graphs more readable
198 * 574623 : [dot_file_with_ts] ':' not a valid character for a filename
199 * 574805 : [capsfilter] Doesn't reset the internal suggestion with A...
200 * 575695 : build fails on OpenSolaris due to incorrect header file i...
201 * 575814 : flag for EOS on gst-launch when exiting with ctrl-c
202 * 576381 : [basesink] QoS: emergency rendering not always done
203 * 576563 : pidgin crashes on exit in gst_plugin_ext_dep_free()
204 * 576582 : A patch to enable the use of 'name' in Enum parameters
205 * 577887 : Missing GST_DISABLE_GST_DEBUG in gstregistrybinary.c
206 * 577891 : add alloc-pad property on tee
207 * 578114 : API: add two new log levels: FIXME and MEMDUMP
208 * 578201 : _gst_plugin_fault_handler_is_setup undefined under HAVE_W...
209 * 579127 : gst-launch: disable CLOCK_LOST message handling
210 * 580121 : race condition in GStreamer state changes causes problems...
211 * 361155 : Add monotonic clock
212 * 517231 : threadsafe/colored windows logging
213 * 572591 : Another batch of " differs in signedness " warnings
214 * 573823 : pad block callback if it is re-blocked while the previous...
215 * 574163 : Fix gst_pad_activate_pull deactivation with unlinked element
216 * 575682 : Add gst_pad_is_compatible()
217 * 575988 : On Windows filesink can't write files longer than 2-4 GiB...
219 API additions since 0.10.22:
221 * New FIXME and MEMDUMP debug levels
222 * gst_tag_list_get_buffer() and gst_tag_list_get_buffer_index()
223 * New tags: GST_TAG_SUBTITLE_CODEC, GST_TAG_HOMEPAGE
224 * gst_util_array_binary_search()
225 * gst_message_new_request_state(), gst_message_parse_request_state(), GST_MESSAGE_REQUEST_STATE
226 * GstPoll::gst_poll_new_timer()
227 * GstPoll::gst_poll_write_control()
228 * GstPoll::gst_poll_read_control()
230 Changes since 0.10.21:
232 * GstController improvements
233 * Extensions to the latency setting behaviours
234 * Ability for plugins to register dependencies to trigger re-scanning
235 * Optimisations in some common operations on caps and values and elsewhere
236 * Add sequence numbers to events so dependent events can be associated with
237 the event that caused them
238 * New macros for reading and writing float values
239 * Many improvements in the basesink base class
240 * Support non-default main contexts for GstBus watches
241 * Improvements in pull-mode scheduling of sinks
242 * Fixes for alignment issues on sparc
243 * Ghost pad fixes
244 * New bit-reader assistance API
245 * Many other bug fixes and improvements
247 Bugs fixed since 0.10.21:
249 * 567002 : --gst-disable-registry-update also skips registry creation
250 * 350477 : [Registry] Provide a way for plugins to delegate the 'cha...
251 * 510354 : post GST_MESSAGE_STRUCTURE_CHANGE when linking and unlink...
252 * 526044 : Crash if there is more than one watcher for a GstBus
253 * 539108 : gst_ghost_pad_new() does more than call g_object_new()
254 * 544003 : [parse] Links to wrong pad if no padtemplate name is given
255 * 544293 : rtspsrc / gstpoll regression
256 * 545714 : GST_READ_UINT_* and GST_WRITE_UINT_* are not always safe ...
257 * 548786 : [win32] search for plugins based on location of DLL
258 * 551676 : Small Memleak fix in gst_pad_link_check_compatible_unlocked
259 * 552778 : add free_func in gstbuffer instances
260 * 553554 : [base] Add a generic bit reader
261 * 553874 : query_position broken during seek
262 * 555196 : Move floating point endian conversion macros into core
263 * 555307 : Need to push latency event into the pipeline
264 * 555631 : Banshee crashes; gstreamer GST_CAPS GST_IS_CAPS warnings
265 * 556091 : libtool-2.2 and old gettext don't mix
266 * 556900 : a copy & paste bug in helloworld example
267 * 557154 : Allow totem to run without write-access to home directory
268 * 557300 : libgstnet needs to link against $(WIN32_LIBS)
269 * 557438 : Gstreamer crashes when Banshee supposed to change track
270 * 557649 : GstBaseTransform can cause ivalid memory references
271 * 559250 : segments need identifiers.
272 * 560301 : Add --plugin to gst-inspect
273 * 560360 : Excessive statting when reading binary cache
274 * 560399 : Unnecessary CRC checksum for binary registry cache
275 * 560442 : GNOME Goal: Remove deprecated GLib symbols
276 * 561501 : g_type_class_ref without unref
277 * 562170 : GstBus watch doesn't work with non-default main context
278 * 562949 : [API] Add an URI query type for querying the source/sink URI
279 * 564863 : Caps are not propagated from a ghostpad's target to the g...
280 * 567225 : volatile gonce_data in BOILERPLATE not initialized to 0
281 * 566393 : [deadlock] Setting index on a pipeline
283 API added since 0.10.21:
285 * Add bit reader and byte reader classes.
286 * gst_message_new_structure_change()
287 * gst_message_parse_structure_change()
288 * GST_BUFFER_FREE_FUNC()
289 * Add GST_READ_UINT24_(LE|BE) and GST_WRITE_UINT24_(LE|BE).
290 * GstBaseSrc::gst_base_src_set_blocksize()
291 * GstBaseSrc::gst_base_src_get_blocksize()
292 * GstBaseSink::gst_base_sink_set_blocksize()
293 * GstBaseSink::gst_base_sink_get_blocksize()
294 * GstBaseSink::blocksize
295 * GstBaseSink::gst_base_sink_do_preroll()
296 * Add gst_byte_reader_get_data and gst_byte_reader_peek_data
297 * Move float endianness conversion macros from libgstfloatcast to core
298 * gst_util_seqnum_next, gst_util_seqnum_compare
299 * gst_event_get_seqnum, gst_event_set_seqnum
300 * gst_message_get_seqnum, gst_message_set_seqnum
301 * GstSeekFlags::GST_SEEK_FLAG_SKIP
302 * gst_bin_recalculate_latency()
303 * GstBin::do-latency
304 * gst_tag_setter_reset_tags()
305 * gst_query_new_uri, gst_query_set_uri, gst_query_parse_uri
306 * add gst_plugin_add_dependency()
307 * add gst_plugin_add_dependency_simple()
310 Changes since 0.10.20:
312 * Basetransform rework
313 * Basesink synchronisation extensions
314 * New documentation
315 * Many bug fixes, enhancements and optimisations
317 Bugs fixed since 0.10.20:
319 * 481169 : [tag] add support for geo tags (gps location etc.)
320 * 520694 : adding GST_TAG_KEYWORDS
321 * 538201 : deleting the control point at ts=0 does not lower the con...
322 * 544855 : fakesrc and fakesink should call super::event()
323 * 339795 : [GstBaseTransform] Reverse negotiation issues in passthro...
324 * 348114 : [PPC64?] [gcc-4.1.2?] GST_BUFFER_IN_CAPS flag should have...
325 * 361718 : [basetransform] needs API to force renegotiation
326 * 533856 : gst_buffer_join() documentation is unclear
327 * 536978 : GTKDOC_CFLAGS should include CFLAGS
328 * 537804 : [multiqueue] wrongly reporting that the queue is full.
329 * 537812 : [check] add api to setup a pad by name
330 * 538568 : Add GST_TAG_ATTACHMENT
331 * 539772 : gst_pad_template_new() does more than call g_object_new()
332 * 542175 : gst-inspect --gst-plugins-path fails with multiple direct...
333 * 543444 : gst_base_sink_get_position can return 0 unexpectedly
334 * 543853 : Bison version check failure on OSX 10.4 Tiger
335 * 544174 : [basesrc] allow dynamic value of the seekable value.
336 * 544776 : [win32] binary registry may fail if glib is using a diffe...
337 * 545352 : gsturi is too restrictive
338 * 545603 : gst-inspect: don't print uri handler when compiled withou...
339 * 545605 : gstelementfactory: don't use uri handler code without uri...
340 * 545607 : gst: include gstconfig when using macros defined therein
341 * 545853 : [basetransform] rewrite
342 * 546328 : fractions with G_MAXINT cause failure for fixation
343 * 546822 : gstreamer doesn't tell gettext to output its translations...
344 * 547277 : filesrc detect if a file is seekable using SEEK_SET and n...
345 * 547728 : [basetransform] fail on buffer_alloc
346 * 548394 : basesink should ignore EOS during flushing
347 * 548652 : [Inconsistency] GST_TAG_LOCATION is used for different me...
348 * 549504 : Thread-safe version of gst_pad_get_internal_links()
349 * 551952 : Need 'check' package when compile
350 * 551978 : Memleak in gst_element_sync_state_with_paren
351 * 547835 : tee release_request_pad while buffer_alloc racyness
352 * 538628 : Patch: added a timeout property to fdsrc used in gst_poll...
353 * 546883 : [basetransform] ximagesink fails when resizing video window
354 * 551509 : gst_base_transform_prepare_output_buffer: assertion faile...
356 API added since 0.10.20:
358 * Add GST_TAG_ATTACHMENT for generic file attachments to streams.
359 * Add gst_base_sink_set_render_delay()
360 * Add gst_base_sink_get_render_delay()
361 * Add gst_check_setup_src_pad_by_name
362 * Add gst_check_setup_sink_pad_by_name
363 * Add gst_check_teardown_pad_by_name
364 * Add GstBaseTransform::gst_base_transform_suggest()
365 * GstBaseTransform::gst_base_transform_reconfigure()
366 * GstPad::gst_pad_set_iterate_internal_links_function()
367 * GstPad::GstPadIterIntLinkFunction
368 * GstPad::gst_pad_iterate_internal_links()
369 * GstPad::gst_pad_iterate_internal_links_default()
371 API deprecated since 0.10.20:
373 * gst_pad_get_internal_links()
374 * gst_pad_set_internal_link_function()
375 * gst_pad_get_internal_links_default()
377 Changes since 0.10.19:
379 * Add the Presets interface
380 * Use the binary registry by default
381 * Deprecate gst_element_get_pad and don't use it anywhere any more.
382 * Reverse playback fixes
383 * API to get missing element messages from parse_launch parsing.
384 * Fixes in latency calculations
385 * BaseTransform negotiation fixes
386 * New Buffering query and messages
387 * Fix multiqueue deadlocks when changing limits
388 * Remove pre-generated parser hacks and require newer flex/bison
389 * Use GSlice in more places
390 * Use static strings in property declarations everywhere to save memory
391 allocations
392 * Fix unaligned memory accesses with the binary registry and add CRC
393 checks
394 * Lots of other bug fixes
396 Bugs fixed since 0.10.19:
398 * 535069 : basesrc no longer support non-flushing seeks on itself
399 * 522882 : Add a configure option to enable/disable OPTION_PARSING i...
400 * 396779 : Preset interface for elements
401 * 359653 : GStreamer Binary Registry patch
402 * 401456 : [API] Rename gst_bin_find_unconnected_pad to gst_bin_find...
403 * 446763 : [identity] leaks events in single segment mode
404 * 459862 : typefinding coud be more efficient
405 * 461253 : Crash when gst_base_transform_prepare_output_buffer is se...
406 * 489269 : valgrind option parameter invalid for valgrind 2.2
407 * 508070 : gstreamer crashes whilst trying to read .so files in .deb...
408 * 512577 : GstTagMergeMode doc has slightly incorrect explanation
409 * 512578 : gst_tag_setter_merge_tags can mess up with KEEP_ALL merge...
410 * 514507 : gst-xmlinspect outputs text instead of xml for plugins
411 * 518022 : [libgstnet] MSVC 6.0 compile error due to socklen_t
412 * 518932 : Expose gst_segment_copy() to facilitate wrapping of GstSe...
413 * 520468 : Add a Env to enable/disable scan_and_update_registry for ...
414 * 522326 : use of 'char*' instead of 'const char*' in gst_caps_set_s...
415 * 523798 : [API] Some GstMiniObject enhancements
416 * 523806 : Should use G_PARAM_STATIC_(NAME|NICK|BLURB) when possible
417 * 523978 : Documentation fixes.
418 * 523985 : [PATCH] [identity] meta-writes buffers without meta-writa...
419 * 524659 : Add specific error code for encrypted streams (e.g. WMA/A...
420 * 525532 : [fakesink/fakesrc/identity] Uses GObject marshallers for ...
421 * 526042 : [identity] check-imperfect-timestamp doesn't handle new s...
422 * 526236 : mingw32 gstpoll compilation fix
423 * 526247 : Actually build dlls when cross-compiling with mingw32
424 * 526705 : GstIndexResolver uses nickname field as description field
425 * 526768 : Basetransform bufferalloc passing through too easily
426 * 526814 : [API] add gst_pad_add_{data,event,buffer}_probe_full() wi...
427 * 527967 : gst_gerror_get_type is not thread safe
428 * 528187 : Get missing elements from gst_parse_launch()
429 * 528868 : URI schemes/protocols should be handled case insensitive
430 * 529148 : Make gstqueue give the right min latency
431 * 530317 : GType registration error - race condition when parallel c...
432 * 530637 : queue leak on capacity change
433 * 531538 : Race between gst_bus_set_flushing and async bus watches
434 * 533490 : gst_message_new_warning() should take const gchar*
435 * 533635 : gst_event_new_tag() documentation should say it takes own...
436 * 533740 : [API] add gst_typefind_suggest_simple()
437 * 533865 : gst_element_get_pad() should really be deprecated
438 * 534258 : basesink not accumulated time in some cases.
439 * 535218 : gst_base_src_send_event will block if basesrc is blocking...
440 * 536723 : Misspelled word in error string
441 * 536744 : Must link to libdl if dladdr() is used
442 * 536780 : gcc 4.3.0 compile warnings
443 * 536857 : DATADIR definition conflicts with windows headers
444 * 525961 : Build fails on darwin
445 * 535285 : Correct reference to GST_URI_UNKNOWN in gst_element_facto...
447 API added since 0.10.19:
449 * Add GST_IS_PARAM_SPEC_MINI_OBJECT, GST_PARAM_SPEC_MINI_OBJECT
450 GST_TYPE_PARAM_MINI_OBJECT and gst_value_dup_mini_object
451 * typefind::force-caps
452 * gst_message_set_buffering_stats()
453 * gst_message_parse_buffering_stats()
454 * GST_QUERY_BUFFERING
455 * GstBufferingMode
456 * gst_query_new_buffering()
457 * gst_query_set_buffering_percent()
458 * gst_query_parse_buffering_percent()
459 * gst_query_set_buffering_stats()
460 * gst_query_parse_buffering_stats()
461 * gst_query_set_buffering_range()
462 * gst_query_parse_buffering_range()
463 * GST_STREAM_ERROR_DECRYPT
464 * GST_STREAM_ERROR_DECRYPT_NOKEY
465 * gst_segment_copy()
466 * gst_pad_add_data_probe_full()
467 * gst_pad_add_buffer_probe_full()
468 * gst_pad_add_event_probe_full()
469 * GstEvent::gst_event_has_name()
470 * GstFakeSrc:format
471 * gst_type_find_suggest_simple()
472 * GstBaseSink::gst_base_sink_wait_clock()
473 * gst_parse_launch_full()
474 * gst_parse_launchv_full()
475 * gst_parse_bin_from_description_full()
476 * gst_parse_context_new()
477 * gst_parse_context_free()
478 * gst_parse_context_get_missing_elements()
479 * gst_bin_find_unlinked_pad()
480 * GstPreset interface
482 API deprecated since 0.10.19:
484 * gst_element_get_pad -
485 use gst_element_get_static_pad or gst_element_get_request_pad
486 * gst_atomic_int_set() - g_atomic_int_set from GLib
487 * gst_bin_find_unconnected_pad()
489 Changes since 0.10.18:
491 * Fix a regression in raw fd handling
493 Bugs fixed since 0.10.18:
495 * 524041 : gstfdsrc broken in 0.10.18
497 Changes since 0.10.17:
499 * New GstPoll abstraction simplifies operations on multiple fd's/sockets
500 * Various bug fixes and corrections
502 Bugs fixed since 0.10.17:
504 * 516187 : adding gst_collect_pads_read_buffer () collectpads
505 * 516395 : gst_buffer_create_sub does not copy flags
506 * 520756 : different registry backend configurations cause build errors
507 * 498222 : configure improvements
508 * 499127 : [multiqueue] has no documentation
509 * 505417 : Add GstPoll to core
510 * 509559 : [gstinfo]_gst_debug_init() memory leak
511 * 510194 : segmentation fault when trying to link elements.
512 * 511783 : [API] [check] add gst_check_element_push_buffer_list() etc.
513 * 513964 : [GstPad] gst_pad_get_caps don't return a copy of the caps
514 * 515469 : patch to add gst_index_set_resolver_full
515 * 519584 : gst_element_implements_interface() segfaults with 'filesr...
516 * 519698 : g_free/xmlFree mismatches in gstregistryxml
517 * 520152 : Core uses non-portable size_t and ssize_t
518 * 520671 : GstPoll needs to be ported to Windows
519 * 520808 : GstPoll's API could need some changes for Windows
520 * 520877 : registrybinary.c doesn't build cleanly on Windows/MSVC
521 * 521740 : libgstreamer.def exports not up to date
522 * 522741 : regression: gst_index_entry_free() frees string it does n...
524 Changes since 0.10.16:
526 * Fix compilation on environments that have POSIX timers but not
527 monotonic clocks
529 Bugs fixed since 0.10.16:
531 * 512715 : gst/gstutils.c and HAVE_MONOTONIC_CLOCK
533 Changes since 0.10.15:
535 * Monotonic/Posix clock support
536 * Dumping of dot-file graph descriptions for debugging
537 * Clean-up of exported symbols
538 * Many bug-fixes and enhancements
540 Bugs fixed since 0.10.15:
542 * 497859 : --disable-gst-debug option fails compilation
543 * 339279 : [gst.URIHandler] interfaces with class-global virtual met...
544 * 498694 : Patches to avoid g_signal_emit(SIGNAL_HANDOFF) on identit...
545 * 498746 : basesink is forwarding downstream events
546 * 498767 : Hangs after end of tracks since 0.10.15
547 * 498924 : deprecate GST_PLUGIN_DEFINE_STATIC because it's not portable
548 * 499007 : [gst-plot-timeline] more options
549 * 499140 : Add check to ensure .def files are kept up-to-date
550 * 500143 : Some small improvements (limiting realloc and CPU usage )
551 * 500150 : [filesink] add property to enable buffering via setvbuf()
552 * 501560 : gst_(caps|structure)_from_string() crash if structure nam...
553 * 503131 : g_intern_string SUSE 10.2
554 * 503231 : Change to GST_BUFFER_FLAG_GAP meaning can break with base...
555 * 503417 : Build failure due uninitialized variable in function 'gst...
556 * 503590 : gstreamer-0.10.15 fails tests on ppc64
557 * 503675 : broken registry files written to disk
558 * 504499 : Messages from check no longer contain the test case name
559 * 505799 : iSight camera does not work in gstreamer
560 * 506643 : crash in fixate_value/gst_value_init_and_copy on empty li...
561 * 507957 : clean-up incomplete function declarations
562 * 508175 : GST_TIMEVAL_TO_TIME() and GST_TIMESPEC_TO_TIME() need to ...
563 * 510187 : gst_plugin_register_static() API review and GST_PLUGIN_DE...
564 * 510747 : Use $(MAKE) instead of make to fix the build if GNU make ...
565 * 511750 : Configure of prereleases 15.2-15.4 fail in OpenEmbedded M...
567 API additions since 0.10.15:
569 * GstIdentity::signal-handoffs
570 * gst_util_get_timestamp()
571 * gst_base_transform_set_gap_aware()
572 * GstFileSink::buffer-mode
573 * GstFileSink::buffer-size
574 * gst_plugin_register_static()
576 API deprecated since 0.10.15:
578 * GST_PLUGIN_DEFINE_STATIC()
580 Changes since 0.10.14:
582 * Changes for asynchronous sink management
583 * New ts-offset property on basesink for adjusting clock synchronisation
584 * New GstController LFO feature
585 * Fixes and improvements in latency measurement for live pipelines
586 * Additional documentation and docs fixes
587 * Faster typefinding
588 * More tag types added
589 * Improvements in various core elements and parent classes
590 * New unit tests
591 * Allow dumping pipelines as dot graphs
592 * GstStructures now support nesting
593 * URIHandler interface can now be implemented in bindings
594 * Many other bug-fixes and improvements
596 Bugs fixed since 0.10.14:
598 * 496722 : DSP/DSW files in win32/vs6 directory are in unix format
599 * 476514 : [queue] Doesn't forward EOS event in all cases
600 * 456573 : allow dumping pipelines as dot graphs
601 * 475723 : cleanup static caps correctly
602 * 480341 : Memory leak at fakesink (regression in cvs)
603 * 349410 : Problems with type handling
604 * 414539 : [API] Support more GST_TAG*_SORTNAME and remove MusicBrai...
605 * 459717 : [Controller] Add GstLFOControlSource that provides values...
606 * 459809 : [API] add GST_TAG_COMPOSER
607 * 461598 : Commit Hungarian translations from TP
608 * 461599 : Some files missing from POTFILES.in
609 * 464366 : program including gst/gstbuffer.h does not compile with -...
610 * 466595 : gst_index_add_association generates corrupted entries
611 * 469402 : File uri handling on windows broken
612 * 473846 : Deadlock if sink is unable to send first buffer
613 * 474371 : Can't build libsgtcontroller with VS6
614 * 474823 : tee unit test failure
615 * 478347 : GST_STATIC_PAD_TEMPLATE macro causes warnings with g++-4.2
616 * 478401 : gstbasesrc.c ref count bug
617 * 479784 : GST_PLUGIN_DEFINE() doesn't accept BSD and MIT/X11 licences
618 * 485343 : Implement a wait_eos function in basesink
619 * 487969 : allow nested GstStructures
620 * 492077 : Build issues on Windows/MSVC
621 * 493134 : Wrong GstObject signals registration
622 * 493983 : Build issues on Windows
623 * 494343 : pre-release vs6 patch
624 * 480858 : gstqueue code cleaning
625 * 486758 : queue element fails to re-negotiate caps upstream when si...
626 * 488201 : gst_segment_set_newsegment does not accumulate correctly
627 * 492729 : PAUSED- > PLAYING returns ASYNC when triggered from bus han...
628 * 494245 : [basesink] doesn't sync correctly if segment is in BYTES ...
630 API added since 0.10.14:
632 * gst_base_sink_get_last_buffer()
633 * GstBaseSink::last-buffer
634 * GstURIHandlerInterface::get_type_full
635 * GstURIHandlerInterface::get_protocols_full
636 * New tag: GST_TAG_ARTIST_SORTNAME
637 * New tag: GST_TAG_ALBUM_SORTNAME
638 * New tag: GST_TAG_TITLE_SORTNAME
639 * New tag: GST_TAG_COMPOSER
640 * gst_value_set_structure()
641 * gst_value_get_structure()
642 * GST_VALUE_HOLDS_STRUCTURE macro
643 * gst_bus_pop_filtered()
644 * gst_bus_timed_pop_filtered()
645 * gst_base_sink_wait_eos()
646 * gst_pad_peer_query()
647 * GstBaseSrc::do-timestamp
648 * gst_base_src_set_do_timestamp()
649 * gst_base_src_get_do_timestamp()
650 * GstBaseSink::ts-offset property
651 * gst_base_sink_set_ts_offset()
652 * gst_base_sink_get_ts_offset()
653 * GstBaseSink::async property
654 * gst_base_sink_set_async_enabled()
655 * gst_base_sink_is_async_enabled()
656 * gst_structure_get_uint()
657 * GstLFOControlSource and functions
659 Changes since 0.10.13:
661 * State change handling improvements
662 * New improved GstController API
663 * Multi-queue fixes and enhancements
664 * Fewer dynamic library relocations
665 * Various other fixes and improvements
666 * Parallel installability with 0.8.x series
667 * Threadsafe design and API
669 Bugs fixed since 0.10.13:
671 * 457322 : registry is read twice on startup
672 * 406632 : pkgconfigify the check for Check in configure.ac
673 * 423700 : [multiqueue] leaks memory when flushing
674 * 437457 : saving relocations for GstElementDetails
675 * 444648 : [API] add GstParamSpecFraction
676 * 444820 : build error with grammar.tab.c
677 * 448794 : state changes are racy with decodebin after rewrite for 0...
678 * 449197 : [capsfilter] Should set src pad caps on buffer
679 * 449226 : Incomplete ghostpads in xml session save
680 * 449493 : minor quoting fix in gst-feature.m4 macro
681 * 450711 : [GstController] Improve extensibility by providing a GstC...
682 * 451939 : [API] add GST_TAG_LICENSE_URI and GST_TAG_COPYRIGHT_URI
683 * 459501 : gst_registry_lookup_feature_locked is slow
684 * 462558 : Regression in async state change handling
685 * 462752 : make gst_element_class_set_details_simple args const
686 * 430682 : multiqueue doesn't output data on unlinked pads properly
687 * 462085 : registry feature hash can access invalid memory
688 * 357959 : buffer_alloc is not proxied through tee
689 * 374639 : GstTee doesn't handle pad list resyncs properly
690 * 449414 : [capsfilter] Copy of passed GstCaps taken instead of refe...
691 * 453732 : [PATCH] multiqueue returns wrong internally linked pads
693 API added since 0.10.13:
695 * Add GstParamSpecFraction, so elements can have fraction
696 properties without lots of painful string parsing (#444648).
697 * Add fail_unless_equals_float() and assert_equals_float()
698 * Add gst_type_register_static_full
699 * Add gst_element_class_set_details_simple
700 * Refactor GstController into the core controller which can take
701 a GstControlSource for providing actual values for timestamps.
702 * add GST_TAG_LICENSE_URI and GST_TAG_COPYRIGHT_URI (#451939)
703 * gst_element_factory_has_interface()
705 Changes since 0.10.12:
707 * Latency handling infrastructure for live playback scenarios
708 * State change handling changes
709 * GstController property handling improved
710 * Various bug fixes and improvements
711 * Parallel installability with 0.8.x series
712 * Threadsafe design and API
714 Bugs fixed since 0.10.12:
716 * 440682 : gst/gstsystemclock unit test occasionally fails
717 * 342564 : Configure options causing compilation to fail
718 * 378255 : Swedish translation updated
719 * 392804 : [API] add GST_CORE_ERROR_DISABLED
720 * 412648 : [filesink] reports wrong (byte) position after seeking
721 * 413123 : No XML dependency patch
722 * 415394 : [identity] post message for imperfect streams if check-pe...
723 * 417992 : Quickly playing/pausing messes up synchronization
724 * 420106 : [basetransform] race on shutdown: setcaps func called aft...
725 * 420206 : Collectpads causes a segv. when stopping after a pad remove
726 * 421480 : Make it possible to build without libxml2 with --disable-...
727 * 421543 : [GstPad] Doesn't check if pad accepts caps after caps change
728 * 422295 : GstController crashes with quadratic and cubic interpolat...
729 * 425400 : Multiqueue leaks memory when releasing sink pads
730 * 431150 : compilation fails with flex 2.5.4
731 * 431940 : [API] add gst_buffer_try_new_and_alloc()
732 * 432876 : current time level in queue
733 * 434926 : Multilib conflicts with gst-launch-0.10 man page
734 * 435880 : [GstBin] Property to allow bins to handle child async cha...
735 * 437563 : URIs with upper-case protocol don't play
736 * 440463 : gstbin unit test sometimes hangs waiting for ASYNC_DONE m...
737 * 441159 : Regression in state change handling
738 * 349180 : gst_parse_launch is not reentrant (or recursively callable)
739 * 414986 : Don't start the async thread for the system clock until n...
740 * 393099 : GstBuffer copy vfunc broken?
741 * 419851 : pad-added and pad-removed signals parameter type incorrect
742 * 420133 : gst_element_sync_state_with_parent should look at pending...
743 * 421177 : Possible deadlock if pad eventfunc is not specified
745 API additions since 0.10.12:
747 * gst_element_change_state()
748 * GST_STATE_TARGET
749 * GST_BASE_TRANSFORM_LOCK/UNLOCK
750 * GstClock::gst_clock_unadjust_unlocked()
751 * fakesink::num-buffers property
752 * GST_CORE_ERROR_DISABLED
753 * basesrc::prepare_seek_segment vmethod
754 * gst_buffer_try_new_and_alloc()
755 * gst_buffer_copy_metadata()
756 * GstBufferCopyFlags enum
757 * GST_BUFFER_COPY_ALL flag
758 * gst_uri_protocol_is_supported()
759 * gst_base_src_query_latency()
760 * GstQueue::pushing
761 * gst_controller_suggest_next_sync()
762 * gst_object_suggest_next_sync()
763 * basesrc::unlock_stop
764 * basesink::unlock_stop
765 * GstBin::async-handling property
766 * gst_message_new_async_start()
767 * gst_message_parse_async_start()
768 * gst_message_new_async_done()
769 * GST_MESSAGE_ASYNC_START
770 * GST_MESSAGE_ASYNC_DONE
772 Changes since 0.10.11:
774 * Add a warning if GLib threading support is not properly initialised
775 * Add support for binary registry serialisation
776 * Preliminary support for pull-mode scheduling of entire chains
777 * Add support for HPPA
778 * Collectpads fixes
779 * Lots of bug fixes
781 Bugs fixed since 0.10.11:
783 * 378931 : Bison version check doesn't work on Solaris 9
784 * 399875 : [multiqueue] dynamic growth not implemented.
785 * 339326 : pads not set to FLUSHING when created
786 * 380129 : gst_plugin_feature_load doesn't consistently ref a return...
787 * 381301 : [patch] Make GstBus watch work with any GMainContext
788 * 383382 : Removing pads from collectpads not threadsafe
789 * 383506 : Disallow CLOCK_TIME_NONE as periodic clock id interval
790 * 387073 : gst-launch videotestsrc ! ffmpegcolorspace ! ximagesink d...
791 * 387866 : [docs] Small fix for GstCollectPads docs
792 * 391278 : g_thread_init() called too late, possibly causing memory ...
793 * 391296 : [API] add gst_update_registry() to rescan registry at run...
794 * 391777 : GStreamer does not reset SEGV trap handler
795 * 391909 : Fix compilation with MinGW
796 * 399094 : gst_pad_start_task: small doc typo
797 * 401381 : GstRegistry signals documentation is missing
798 * 401781 : [API] add GST_ROUND_DOWN_* macros
799 * 402393 : [API][GstCollectPads] Allow elements to specify destroy n...
800 * 405284 : Changing state of pipeline can lock up with preroll queue...
801 * 400656 : [PATCH] filesrc seekability detection fix (NFS and 2GB+ f...
802 * 403172 : [filesrc] doesn't handle localhost file locations
803 * 404569 : [filesrc] Unexpected end of file
804 * 161922 : script to provide plugin installation info
805 * 391915 : adapter test doesn't compile with mingw
806 * 395554 : gst_tag_setter_merge_tags works at most once
807 * 403597 : [API] Add ReplayGain reference level tag
808 * 405288 : Configure checks use pkg-config directly
809 * 381492 : [SystemClock] ClockID wait_async notification broken
810 * 382592 : Multiple wait()ers break periodic clock ids
811 * 385084 : endless ghost pad pull/push activate recursion until crash
812 * 388201 : [API] add gst_adapter_copy()
814 API additions since 0.10.11:
816 * gst_update_registry()
817 * gst_adapter_copy()
818 * GST_ROUND_DOWN_* macros
819 * GstCollectDataDestroyNotify
820 * gst_query_new_latency()
821 * gst_query_set_latency()
822 * gst_query_parse_latency()
823 * gst_message_new_lost_preroll()
824 * gst_message_parse_lost_preroll()
825 * gst_message_new_prerolled()
826 * gst_message_new_latency()
827 * gst_event_new_latency()
828 * gst_event_parse_latency()
829 * GST_TAG_REFERENCE_LEVEL
830 * gst_base_sink_query_latency()
831 * gst_base_sink_get_latency()
832 * gst_bus_timed_pop()
833 * gst_message_new_info()
834 * gst_message_parse_info()
836 Bugs fixed since 0.10.10:
838 * 363095 : [BaseTransform] Outputs empty buffers
839 * 353301 : aborts in _get_element_by_uri(), probably due to buggy el...
840 * 344639 : Separate threadsafe queuing functionnality in a separate ...
841 * 347785 : [multiqueue] New multiple input-output queue
842 * 352827 : re-negotiation issues with dynamic pipelines and level or...
843 * 357180 : [libs] gst_controller_new* functions don't increase refco...
844 * 318031 : gstreamer should use gmodule-no-export in its .pc file
845 * 340878 : Registry doesn't discard removed plugin features
846 * 345496 : No GstPadDirection in files created by GstXml
847 * 356910 : Basesrc gst_base_src_activate_push not calling base_src_s...
848 * 357593 : Generated gst-element-check.m4 installed from $(srcdir)
849 * 358436 : #include is missing in gstghostpad.c and gstquery.c
850 * 358999 : [PATCH] [GstPad] Flushing on blocked pads not handled cor...
851 * 359850 : Compiling issues on sparc with Forte
852 * 360151 : Fixes compiling with forte: disable warning as error for ...
853 * 360173 : Fixes compiling with forte: warning clean up (part 1)
854 * 360467 : [API] add gst_tag_list_is_empty ()
855 * 360860 : Fixes compiling with forte: warning clean up (part 2)
856 * 361675 : Allow applications to use libxml2 and GStreamer even if ...
857 * 361720 : grammar project: error generating gstmarshal.c and gstmar...
858 * 361730 : wrong source file list in VC8 project
859 * 361732 : " win32\common\libgstreamer.def " lacks 'gst_caps_merge' entry
860 * 361769 : Deadlock in gstpad.c
861 * 364388 : size variable is not always initialized in gst_base_src_s...
862 * 366321 : GST_SEGMENT_FORMAT not defined on windows
863 * 370865 : [basesrc] update segment duration in gst_base_src_update_...
864 * 371493 : Incomplete change of printf conversion specifiers in gstr...
865 * 374475 : [PATCH] minor doc typo
866 * 377332 : [PATCH] Warning with check > = 0.9.4
867 * 357617 : [libs] gst_controller_set_from_list can return without un...
868 * 358737 : _gst_event_copy sets the wrong parent_refcount on the chi...
869 * 366212 : Fix some misspellings in gstreamer core
870 * 369366 : MacOSX printf fixes for CVS
871 * 371894 : tests/examples/typefind is broken
872 * 355499 : ensure_current_registry_forking() fails if zombie alread...
873 * 352345 : Small race condition in the queue element
874 * 357432 : [libs] GstController needs to keep controlled objects alive
875 * 358613 : sink- > file is never reset for filesink elements, even tho...
876 * 366286 : [PATCH] fix compilation on Windows
877 * 366572 : Bad declaration in headerfile
878 * 367677 : [fdsrc] skips the first byte
879 * 369942 : [PATCH] unblocking blocked pad does not release all block...
881 API added since 0.10.10:
883 * gst_element_state_change_return_get_name
884 * gst_tag_list_is_empty
885 * gst_pad_is_blocking()
886 * GST_PAD_IS_BLOCKING() macro
887 * GST_PAD_BLOCKING GstPadFlag
888 * gst_base_src_wait_playing
889 * gst_base_sink_wait_preroll
890 * gst_message_new_buffering
891 * gst_message_parse_buffering
893 Bugs fixed since 0.10.9:
895 * 349180 : gst_parse_launch is not reentrant (or recursively callable)
896 * 348455 : [filesrc] should not use mmap() by default, since it migh...
897 * 340674 : marry gst-debugs & plot-timeline.py
898 * 350449 : [GstBaseTransform] buffer_alloc should alway try downstream
899 * 352580 : implement proper caps merging
900 * 345444 : Linking to an audioconvert (pad-added callback) multiple ...
901 * 347293 : GstValueList comparison is flawed
902 * 347311 : element_unlink leaks its iterator wich will leak the src ...
903 * 348179 : gst_parse_lauch is not reentrant
904 * 348354 : failure in bison version detection breaks build
905 * 350419 : API: GST_SEGMENT_FORMAT printf extension for GstSegments
906 * 350879 : [init] Mark gstreamer as being initialized during registr...
907 * 350935 : API: add GST_TAG_EXTENDED_COMMENT
908 * 353976 : asssertion about element sanity in gst_registry_xml_write...
909 * 350432 : micro-optimising quarks
910 * 341029 : Ghostpads internal and target should be linked from the b...
911 * 345295 : [PATCH] gstreamer/libs/gst/net for Windows
912 * 347756 : Allow --disable-trace without --disable-parse
913 * 347794 : Do not reset SIGSEGV handler when --gst-disable-segtrap i...
914 * 348918 : application should decide whether or not to use fork() to...
915 * 349943 : [QOS] documentation/code mismatch
916 * 351768 : Unwanted concurent buffer modifications
917 * 352958 : pad_alloc_buffer and stream lock
918 * 353121 : gst_query_new_segment should initialize all structure fields
919 * 353122 : gst_element_get_bus refs the bus unconditionally
920 * 347385 : [ghostpad] gst_ghost_pad_new_from_template() method
921 * 348677 : Upgrade to 0.10.9 breaks existing applications (failed se...
923 API added since 0.10.9:
925 * gst_segtrap_is_enabled
926 * gst_segtrap_set_enabled
927 * gst_registry_fork_is_enabled
928 * gst_registry_fork_set_enabled
929 * gst_ghost_pad_new_from_template
930 * gst_ghost_pad_new_no_target_from_template
931 * gst_caps_merge
932 * GST_TAG_EXTENDED_COMMENT
933 * GstClockCLass:wait_jitter
934 * GST_SEGMENT_FORMAT
935 * gst_structure_id_set
936 * gst_structure_id_set_valist
938 Changes since 0.10.8:
940 * The testsuite can now generate coverage information
941 * Better support for non-linear editing
942 * Removed Glib 2.6 compatibility
943 * Performance improvements on cpus that support branch hints
944 * Bug fixes
946 Bugs fixed since 0.10.8:
948 * 346730 : some warnings about enums and macros
949 * 341029 : Ghostpads internal and target should be linked from the b...
950 * 346192 : [PATCH] Pad blocking on events
951 * 347384 : [ghostpad] padtemplates shouldn't be set automatically
952 * 344115 : [patch] make more internal data const
953 * 324176 : gst-element-check-0.x.m4 should use versioned gst-inspect
954 * 330379 : Bogus commits to basesink, basetransform, collectpads
955 * 341667 : restore_from_xml breaks pad links again after creating them
956 * 344642 : tools/gst-inspect.c does not compile if --disable-nls is ...
957 * 344748 : Fails with non-writable registry
958 * 344849 : GstController doesn't handle float properties correct
959 * 345086 : [gst-feedback] calls un-versioned tools
960 * 346097 : SIGSEGV when using --gst-plugin-load
961 * 347337 : GDP does not correctly deserialize events without a struc...
962 * 347408 : basesrc causes regressions in pull with 0 bytes
963 * 345720 : Bad performance playing files off CD
964 * 331727 : make probes and Ghostpads more elegant
965 * 343196 : basetransform not handles ro/rw buffer flagging for trans...
966 * 346663 : Segmentation error with fakesrc, fakesink and a filter
968 Changes since 0.10.7:
970 * Important fix for registry update causing applets not to load
972 Bugs fixed since 0.10.7:
974 * 344474 : Gnome Mixer Applet doesn't want to load
976 Changes since 0.10.6:
978 * Registry cache updating is now done in a fork, so no plugins are left
979 opened
980 * New version of data protocol now serializes events
981 * queue fixes
982 * win32 fixes
984 Bugs fixed since 0.10.6:
986 * 338335 : [patch] memleak in gst-utils.c (leak pads from iterator)
987 * 343598 : undefined symbol in coreindexers when using --disable-loa...
988 * 336929 : GstCollectPads does not clear/reset segment info after fl...
989 * 337100 : [fakesink] add " preroll-handoff " signal
990 * 339918 : GstTagSetter merge-mode description unclear, and implemen...
991 * 340501 : [filesrc] give primary rank
992 * 341662 : gst-launch print_tags() fix
993 * 342238 : API: gst_element_seek_simple
994 * 342321 : GST_QUERY_POSITION fails if GstBaseSrc in get_range mode
995 * 342777 : rebuilding the registry leaves all plugins in memory
996 * 342820 : gstnetclientclock.c(453): servaddr used before set
997 * 343057 : gst-launch-0.10 segfaults when passed gst-plugin-path and...
998 * 343341 : [API] add GST_TAG_PREVIEW_IMAGE
999 * 343827 : leak in gst_index_gtype_resolver
1000 * 343929 : Use of // in public header
1001 * 343988 : data protocol needs extending to handle events better
1002 * 341479 : Too many plugins loaded even for up-to-date registry
1003 * 343334 : GstCollectPads testsuite and fixes
1004 * 343538 : GstCollectPads doesn't reset EOS fields when stopped
1006 API added since 0.10.6:
1008 * gst_element_seek_simple()
1009 * GST_FLOW_CUSTOM_SUCCESS
1010 * GST_FLOW_CUSTOM_ERROR
1011 * GST_FLOW_IS_SUCCESS
1012 * gst_collect_pads_set_flushing()
1013 * GST_TAG_PREVIEW_IMAGE
1014 * gst_dp_crc()
1015 * GstDPPacketizer
1016 * GstDPVersion
1017 * GstFakeSink::preroll-handoff
1018 * GstFakeSink::use-mmap
1020 Changes since 0.10.5:
1022 * Fixes for the collectpads helper
1023 * Support for proper time recording on server-trickmode streams
1024 via the applied_rate parameter of the NewSegment event
1025 * Many bug fixes
1027 Bugs fixed since 0.10.5:
1029 * 339808 : [patch] mem-leak of bin in gstbin.c
1030 * 338339 : [patch] registry cache is always written
1031 * 339843 : [patch] fdsink should not handle short writes and non fat...
1032 * 340016 : does not build on opensolaris, must always include config...
1033 * 340079 : gst-launch wrapper fails with 'No version of tool gst-lau...
1034 * 340174 : locking problem in gstbasesink
1035 * 340460 : gst-launch no longer supports --version
1036 * 340508 : remove glib pre 2.8 hacks and compat stuff
1037 * 340604 : gst_mini_object_ref () docs make no mention of writeability
1038 * 340608 : leaking caps in padtemplate
1039 * 340697 : gstsystemclock hangs when outputting to stdout via fdsink
1040 * 340721 : API: add GST_TAG_IMAGE
1041 * 340772 : [qtdemux] bails out on Meet The Robinsons trailer
1042 * 341556 : gst-launch: print image tags in a human readable form
1043 * 339821 : [patch] serializing a GValue with a NULL buffer crashes
1045 API added since 0.10.5:
1047 * gst_adapter_take_buffer()
1048 * GST_TAG_IMAGE tag added.
1049 * gst_event_new_new_segment_full()
1050 * gst_event_parse_new_segment_full()
1051 * GstSegment::applied_rate field
1052 * gst_segment_set_newsegment_full()
1054 Changes since 0.10.4:
1056 * QoS in BaseTransform
1057 * gcc 4.1 fixes
1058 * BaseTransform reworked
1059 * Bus reworked; signal API added
1061 Bugs fixed since 0.10.4:
1063 * 131079 : [PATCH] [api] loading a class leaves elementfactory blank
1064 * 317048 : gstreamer Cygwin build fixes
1065 * 325599 : Build fails with GCC 4.1
1066 * 327315 : GStreamer CVS head files to build with GCC 4.1
1067 * 331248 : [basesink] filesink spews warnings when used with flacenc
1068 * 332151 : xml registry loader should use mmap() where possible
1069 * 332390 : [GstQueue/GstPad] queue pauses immediately when linked, p...
1070 * 332986 : Something wrong in caps checking...
1071 * 334109 : pkg-config files must link with the same check library th...
1072 * 334303 : Stale libgnomeui check in configure
1073 * 334434 : Missing functions in def files for dlls
1074 * 335195 : GST_BOILERPLATE_FULL etc isn' optimised
1075 * 335480 : start with debugging disabled
1076 * 335513 : totem goes (and stays) out of sync when running bittorrent
1077 * 336336 : [queue] Queue might block in EOS
1078 * 336945 : [filesink] throws error when writing 0 bytes
1079 * 337103 : small cleanup in gstplugin.c
1080 * 337386 : Pipeline bus is not initially flushing
1081 * 338711 : Internal data flow error with latest updates for FC5 with...
1082 * 326311 : basesink does not call the PAUSED- > PLAYING change_state f...
1083 * 326998 : GstBaseSrc's send_event handler ignores seek requests aft...
1085 API added since 0.10.4:
1087 * gst_controller_unset_all()
1088 * gst_pad_query_peer_position()
1089 * gst_pad_query_peer_duration()
1090 * gst_pad_query_peer_convert()
1091 * GstBaseSink::async_play()
1092 * GstBaseSrc::qos
1093 * gst_base_sink_set_qos_enabled()
1094 * gst_base_sink_is_qos_enabled()
1095 * gst_base_transform_update_qos()
1096 * gst_base_transform_set_qos_enabled()
1097 * gst_base_transform_is_qos_enabled()
1098 * gst_pipeline_get_delay()
1099 * gst_pipeline_set_delay()
1101 Changes since 0.10.3:
1103 * Parallel installability with 0.8.x series
1104 * Threadsafe design and API
1105 * 33% of library size removed by parse change
1106 * (Experimental) QoS features (use max-lateness on BaseSink subclasses to enable)
1108 Bugs fixed since 0.10.3:
1110 * 323542 : GStreamer 0.10 hangs at EOS for all songs
1111 * 320340 : triggering a gst_task_join from the streaming task can de...
1112 * 322628 : document thread-unsafety of gst_value_foo() + gst_value_r...
1113 * 324186 : Smarter (deterministic!) typefind decisions
1114 * 324398 : varargs/valist functions aren't bindable
1115 * 328873 : only one gst_bin_recalc_state allowed at a time
1116 * 330899 : CVS directory in make dist tarball
1117 * 330906 : API: add GST_QUERY_TYPE_NAME and GST_MESSAGE_TYPE_NAME
1118 * 330996 : basesrc emits EOS unconditionally when going to READY
1119 * 331255 : Shrinking gst_parse_launch bloat
1120 * 331898 : Basetranform is not reusable
1121 * 332045 : API: GstPipeline needs API to disable flushing of its bu...
1122 * 332277 : [filesrc] seek does not correct read position in non-mmap...
1123 * 332611 : [basesrc] needs way to prevent expensive start/stop in ch...
1124 * 332723 : New API: gst_type_find_helper_for_buffer
1125 * 333042 : New API: gst_type_find_helper_get_range
1126 * 333266 : Registry file writing rewrite
1127 * 333272 : tests should set G_SLICE=always-malloc now
1128 * 333417 : GST_BOILERPLATE_WITH_INTERFACE can't be used in C++ code
1129 * 333669 : Add pad accessor defines for GstBaseTransform
1130 * 333779 : New API: add gst_uri_has_protocol
1131 * 324818 : gst_registry_get_default doesn't sink newly created registry
1132 * 330125 : _pad_send_event does not check flushing correctly
1133 * 330684 : Add ability to emit sync-message without messing with the...
1135 API added since 0.10.3:
1137 * gst_pipeline_set_auto_flush_bus()
1138 * gst_pipeline_get_auto_flush_bus()
1139 * gst_uri_has_protocol()
1140 * gst_pipeline_set_max_lateness()
1141 * gst_pipeline_get_max_lateness()
1142 * gst_pipeline_get_sync()
1143 * gst_pipeline_do_sync()
1144 * GST_BASE_TRANSFORM_SRC_PAD()
1145 * GST_BASE_TRANSFORM_SINK_PAD()
1146 * GstBaseSrc::check_get_range()
1147 * GstBaseSink::max-lateness
1148 * gst_type_find_helper_get_range()
1149 * gst_type_find_helper_for_buffer()
1150 * GST_MESSAGE_TYPE_NAME()
1151 * GST_QUERY_TYPE_NAME()
1152 * gst_bus_enable_sync_message_emission()
1153 * gst_bus_disable_sync_message_emission()
1155 Changes since 0.10.2:
1157 * Documentation updates
1158 * Bug fixes
1159 * Base class improvements
1160 * Extra utility API
1161 * More elements ported from 0.8
1162 * Fixes for win32 build.
1164 Changes since 0.10.1:
1166 * documentation updates
1167 * bug fixes
1169 Bugs fixed since 0.10.1:
1171 * 325429 : GST_BOILERPLATE_FULL can't be used when compiling with -W...
1172 * 316086 : MinGW compilation: fileindexer depends on mmap
1174 Changes since 0.10.0:
1176 * element factory leak fixes
1177 * tests cleanup
1178 * BaseSrc seeking in other format than BYTES
1179 * collectpad fixes
1181 Bugs fixed since 0.10.0:
1183 * 322441 : getcontext() in common/m4/gst-mcsc.m4 uses incorrect stac...
1184 * 323041 : [BASESRC] basesrc does not handle a seek to non-bytes for...
1185 * 323870 : [tools] gst-feedback needs updating for 0.9/0.10
1186 * 323882 : gst-launch manpage needs updates
1187 * 323905 : use return val of g_list_append
1189 API added since 0.10.0:
1191 * GST_TYPE_STATIC_CAPS
1192 * GST_TYPE_STATIC_PAD_TEMPLATE
1193 * GstNetTimeProvider::active
1194 * gst_base_src_set_format
1196 Changes from the 0.8 series to 0.10 series:
1198 * Refcounting and API revised for thread safety, see rules in
1199 docs/design/part-MT-refcounting.txt
1201 * Scheduling is now done by the elements, they start/stop
1202 processing threads themselves. This removes the need for
1203 a separate scheduler.
1205 * State changes now happen from sink to source. This makes sure
1206 that downstream elements are ready to process data when upstream
1207 starts producing.
1209 * EOS/ERROR/... does not change the state of elements anymore. This
1210 means that when the application sets the state on an element, it
1211 remains in this state.
1213 * GMainLoop integration. Information on the state of the pipeline
1214 is now received in the mainloop via the GstBus.
1216 * Events move separate from the datastream, this allows for both
1217 in and out of sync delivery of events.
1219 * Generic _pull() replaced by _pull_region() so that random access
1220 can be made faster.
1222 * data passing happens from PAUSED, called the preroll phase. In this
1223 state no data is rendered but it is queued in the sinks.
1225 * negotiation simplified. Caps are now attached to buffers and travel
1226 along with the datastream.
1228 * GstBuffer is now subclassable.
1230 * Ghostpads now look and feel like real pads.
1232 * New Seeking/flushing policy.
1234 * Addition of base classes and helper functions in the core to abstract
1235 away the harder parts of plugin development.
1237 Changes since 0.9.7:
1239 * added Traditional Chinese translation
1241 Bugs fixed since 0.9.7:
1243 * 322874 : [PAD] pad_alloc_buffer should not call set_caps
1244 * 323222 : GStreamer 0.9.7 still checks in dirs containing 0.9
1245 * 323250 : [collectpads] debug category should be called 'collectpad...
1247 Changes since 0.9.6:
1249 * bumped major/minor to 0.10
1250 * API cleanup
1251 * PluginFeature and TypeFind leak fixes
1252 * cleaned up source tree
1253 * added plugin documentation for core elements
1254 * fixes for stripped core
1256 Bugs fixed since 0.9.6:
1258 * 320529 : [API] gst_event_new_segment mentions " stream_time " as an ...
1259 * 321917 : quicktime with two video tracks and extra foo, makes tote...
1260 * 322257 : Fix gstnet library name
1261 * 322427 : gst-compprep aborts with 'double free or corruption'
1262 * 322429 : Filesink seeking problem
1263 * 322626 : Strings in gst-launch.c adn gstdebug.c are horrid
1264 * 322708 : gst_plugin_load_file leaks a reference to a GstPlugin
1265 * 322751 : gst_ghost_pad_get_target borks on pads without target
1266 * 322842 : GStreamer-CRITICAL in GstBaseSink and GstBaseTransform
1268 Changes since 0.9.5:
1270 * API changes and clean-up
1271 * Extensive documentation updates
1272 * remove GLib 2.4 compatibility
1273 * added clock selection
1274 * added network clocking
1275 * added fd:// URI handler
1276 * added more fraction functionality
1278 Bugs fixed since 0.9.5:
1280 * 143472 : [api] gst_tag_list_foreach() takes a non-const GstTagList*
1281 * 156633 : [API] don't use same API for arrays as for normal lists
1282 * 164168 : circular pipeline fails to negotiate
1283 * 165650 : [API] gst_value_deserialize doesn't work correctly for NU...
1284 * 168438 : [API] GstIndexFilter doesn't receive user_data
1285 * 168494 : [API] gst_index_add_object() does nothing
1286 * 305291 : Obnoxious bug-filing request
1287 * 311489 : Possible gstghostpad locking problems
1288 * 319178 : [API] finish filler events and support them in GstCollect...
1289 * 319388 : 0.9 API changes tracker
1290 * 319389 : state change updates obsolete some functions
1291 * 319392 : GstEventType is not bindings-friendly
1292 * 319395 : Macro name/visibility API bugs
1293 * 319940 : Use GLIB macros for GCC extensions
1294 * 320060 : add a CORE error category for missing ELEMENTS/PLUGINS
1295 * 320097 : GST_BUFFER_FLAG_ORIGINAL should die
1296 * 320113 : [API] duration message changes
1297 * 320299 : gst_pad_send_event should take stream lock for serialized...
1298 * 320324 : [API] GST_FOURCC_FORMAT should drop leading '%'
1299 * 320423 : [API] padding for GstCollectData
1300 * 320766 : [API] collect pads API changes
1301 * 321061 : GstURI not used
1302 * 321235 : [API] GST_PAD_IS_USABLE should be removed
1303 * 321386 : [SEGFAULT] basetransform when doing reverse caps negotiation
1304 * 321452 : GstPad's " template " property is b0rked
1305 * 321528 : capsfilter: assertion `caps != NULL' failed
1306 * 321595 : GstBin doesn't clean the message queue when changing stat...
1307 * 321638 : Don't use // style comments in headers
1308 * 321648 : Wrong type check in gst_message_parse_clock_lost
1309 * 321710 : GstClock resolution functions should take a GstClockTime
1310 * 321712 : GstClock adjust function changes
1311 * 321875 : gst_plugin_check_file disappeared
1312 * 321950 : gst_registry_scan_paths lacks implementation
1313 * 321962 : [easyfix] gst_value_is_fixed uses gst_value_list_* on GST...
1314 * 322027 : [API] Rename gst_caps_structure_fixate_* to gst_structure...
1315 * 322034 : Elements should be updated not to take the stream lock in...
1316 * 322069 : Names of GstTagSetter methods should be more descriptive
1317 * 322134 : API master/slave clocks
1318 * 322139 : our elements are confused about GEnumValue and which is t...
1320 Changes since 0.9.4:
1322 * gst_bus_poll and signal watch now see the same messages
1323 * clock sync in BaseSrc class
1324 * API documentation updates
1325 * Bus reworked; signal API added
1327 Bugs fixed since 0.9.4:
1329 * 317341 : after linking ghost pads, one target pad does not have a ...
1330 * 320774 : basesrc commit broke typefinding
1332 Changes since 0.9.3:
1334 * state lock redefined
1335 * Extensive documentation updates
1336 * BaseTransform reworked
1337 * Bus reworked; signal API added
1339 Bugs fixed since 0.9.3:
1341 * 111146 : new GstThread fails on pipeline with errors
1342 * 169772 : [PATCH] GOption command-line parsing
1343 * 170777 : use GST_TYPE_DATE for GST_TAG_DATE
1344 * 315050 : [API] consider using GstClockTime instead of GTimeVal in ...
1345 * 315126 : filesrc + forced caps should be possible
1346 * 315383 : gst-launch shouldn't run broken pipelines
1347 * 317041 : GstObject flags should be made real flags
1348 * 318447 : gst_bin_iterate_sorted: Invalid call to gst_iterator_new
1350 Changes since 0.9.2:
1352 * gst-register has been removed
1353 * Extensive documentation updates
1354 * BaseTransform reworked
1355 * Bus reworked; signal API added
1357 Bugs fixed since 0.9.2:
1359 * 102980 : support incremental gst-register/compprep updates
1360 * 313897 : [0.9] registry rewrite
1361 * 314710 : gst_buffer_create_sub doesn't copy the GST_BUFFER_FLAGS
1362 * 315895 : gst_pad_query_convert src_val check
1363 * 316155 : MinGW compilation: glib-mkenums root path subtitution pro...
1364 * 316157 : MinGW compilation: Plugin exports
1366 This is GStreamer 0.9.2, "South".
1368 Bugs fixed since 0.9.1:
1370 * 121015 : [api] gst_clock_entry_new() seems broken
1371 * 134227 : [api] gst_clock_id_wait_async, wrong return code for defa...
1372 * 142209 : [build] Large file support broken
1373 * 154785 : Clock does not run if audio stream lacks data for a short...
1374 * 305256 : [API] Change gst_element_seek to not mix enum/flags types
1375 * 309253 : GST_DEBUG_FUNCPTR macro does illegal casting from functio...
1376 * 311004 : ghostpad bugginess
1377 * 311009 : valgrind shows undesired messages
1378 * 311848 : Renegotiation broken
1379 * 314708 : filesrc doesn't set GST_BUFFER_FLAG_READONLY on mmaped bu...