698ad4e2f96e58078de28a755417a9542bf872ad
[glsdk/gstreamer0-10.git] / RELEASE
2 Release notes for GStreamer 0.10.32 "Take Me to the Bonus Level"
3         
6 The GStreamer team is proud to announce a new release
7 in the 0.10.x stable series of the
8 core of the GStreamer streaming media framework.
11 The 0.10.x series is a stable series targeted at end users.
14 This module, gstreamer, only contains core functionality.
15 For actual media playback, you will need other modules.
17 gst-plugins-base
18 contains a basic set of well-supported plug-ins
19 gst-plugins-good
20 contains a set of well-supported plug-ins under our preferred license
21 gst-plugins-ugly
22 contains a set of well-supported plug-ins, but might pose problems for
23     distributors
24 gst-plugins-bad
25 contains a set of less supported plug-ins that haven't passed the
26     rigorous quality testing we expect
30   
32 Features of this release
33     
34       * GLib requirement is now >= 2.22
35       * New core element: valve (moved from -bad)
36       * New core element: input-selector (N.B. without "select-all" property, use fsfunnel instead) (moved from -bad)
37       * New core element: output-selector (with different negotiation behaviour by default, set pad-negotiation-mode=active for previous behaviour) (moved from -bad)
38       * Performance improvements for many heavily-used code paths: GstPad, GstPoll, GstClock, GstTask, basesink, basesrc, queue2, multiqueue (use atomic ops make many code-paths
39       * gobject-introspection: add annotations for most core API
40       * clock: make sync clock wait lockfree
41       * fdsrc/fdsink: reenable on MSVC
42       * registry: fix GStatBuf definition for win32 when building against older glib (fixes unnecessary rescanning of plugins at start-up)
43       * element: add a more flexible way to get request pads from elements
44       * multiqueue: return upon input when already eos
45       * object: fix creation of default name (when creating more than 100000 elements)
46       * pluginloader: fix hangs on OSX
47       * poll: fixes for (p)select backend (used e.g. on OSX)
48       * poll: refactor and make more lockfree; fixes for win32 and OSX (pselect backend)
49       * registry: don't replace valid existing plugins by blacklisted ones
50       * tags: don't produce duplicated entries when merging same value twice
51       * basesink: preroll fixes for async=false case
52       * basesink: rework position reporting code
53       * basetransform: handle downstream giving a buffer with new caps but invalid size
55 Bugs fixed in this release
56      
57       * 635785 : basesrc: fix deadlock
58       * 638599 : GST_PTR_FORMAT causes crashes if GLib-internal printf is used but system provides register_printf_specifier
59       * 503592 : gstpad.c does many ref/unref of peer pad in dataflow
60       * 564056 : Protect against umask(0177)
61       * 607513 : input-selector segfaults in g_object_notify()
62       * 632168 : [gsttask] MSVC thread names for task debugging
63       * 632447 : reduce static memory allocated by the registry
64       * 632557 : [macros] Define restrict keyword if not available
65       * 632778 : Optimisations to GstBaseSink
66       * 632779 : gstdataqueue: Only emit g_cond_signal when needed
67       * 632780 : queue: Remove useless checks from e406f7
68       * 633918 : [fakesink] [PATCH] print sink-message events like a  message and its structure
69       * 634965 : sinks render buffers in state PAUSED when async is FALSE
70       * 635001 : basesink: fix position reporting in PAUSED
71       * 636268 : configure test fails on FreeBSD
72       * 636455 : basesrc: Avoid taking object locks for just checking tag presence
73       * 637057 : [plugin-scanner] gstpoll fails with select backend
74       * 637300 : [API] request pad based on caps
75       * 637549 : build fails: ./.libs/libgstbase-0.10.so: undefined reference to `gst_clock_single_shot_id_reinit'
76       * 637776 : merging the same tag values again produces lists containing duplicates
77       * 638381 : {input,output}-selector: double-check API before release
78       * 638399 : a few typos in GStreamer
79       * 638900 : [GstPoll] Doesn't compile with MinGW
80       * 638941 : registry scan/loading race and inconsistency
82 API changed in this release
83      
84 - API additions:
85     
86       * gst_clock_single_shot_id_reinit()
87       * gst_element_request_pad()
88       * GstElementClass::request_new_pad_full()
89       * gst_poll_get_read_gpollfd()
90       * gst_value_list_merge()
91       * GST_CLOCK_DONE
93 Download
95 You can find source releases of gstreamer in the download directory:
96 http://gstreamer.freedesktop.org/src/gstreamer/
98 GStreamer Homepage
100 More details can be found on the project's website:
101 http://gstreamer.freedesktop.org/
103 Support and Bugs
105 We use GNOME's bugzilla for bug reports and feature requests:
106 http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
108 Developers
110 GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
111 Interested developers of the core library, plug-ins, and applications should
112 subscribe to the gstreamer-devel list. If there is sufficient interest we
113 will create more lists as necessary.
115         
116 Contributors to this release
117     
118       * Andoni Morales Alastruey
119       * Benjamin Gaignard
120       * Benjamin Otte
121       * David Hoyt
122       * David Schleef
123       * Edward Hervey
124       * Havard Graff
125       * Jan Schmidt
126       * Kipp Cannon
127       * Koop Mast
128       * Lasse Laukkanen
129       * Mark Nauwelaerts
130       * Michael Smith
131       * Olivier Crete
132       * Olivier Crête
133       * Raimo Järvi
134       * Sebastian Dröge
135       * Stefan Kost
136       * Thiago Santos
137       * Tim-Philipp Müller
138       * Tommi Myöhänen
139       * Wim Taymans
140       * Zhang Wanming
141       * Christian Schaller
142       * Sjoerd Simons
143