]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blob - RELEASE
queue: use statically allocated GQueue
[glsdk/gstreamer0-10.git] / RELEASE
2 Release notes for GStreamer 0.10.35 "Nuclear Fission"
3         
6 The GStreamer team is proud to announce a new release
7 in the 0.10.x stable series of the
8 core of the GStreamer streaming media framework.
11 The 0.10.x series is a stable series targeted at end users.
12 It is not API or ABI compatible with the stable 0.8.x series.
13 It is, however, parallel installable with the 0.8.x series.
16 The 0.10.x series has been reworked for threadsafety.  It also features
17 various feature additions and enhancements.
20 This module, gstreamer, only contains core functionality.
21 For actual media playback, you will need other modules.
23 gst-plugins-base
24 contains a basic set of well-supported plug-ins
25 gst-plugins-good
26 contains a set of well-supported plug-ins under our preferred license
27 gst-plugins-ugly
28 contains a set of well-supported plug-ins, but might pose problems for
29     distributors
30 gst-plugins-bad
31 contains a set of less supported plug-ins that haven't passed the
32     rigorous quality testing we expect
36   
38 Features of this release
39     
40       * work around GLib atomic ops API change
41       * some minor win32/mingw fixes
42       * don't use G_CONST_RETURN in public headers
44 Bugs fixed in this release
45      
46       * 652211 : Use const instead G_CONST_RETURN
48 Download
50 You can find source releases of gstreamer in the download directory:
51 http://gstreamer.freedesktop.org/src/gstreamer/
53 GStreamer Homepage
55 More details can be found on the project's website:
56 http://gstreamer.freedesktop.org/
58 Support and Bugs
60 We use GNOME's bugzilla for bug reports and feature requests:
61 http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
63 Developers
65 GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
66 Interested developers of the core library, plug-ins, and applications should
67 subscribe to the gstreamer-devel list. If there is sufficient interest we
68 will create more lists as necessary.
70         
71 Applications
73 Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
74 Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
75 Let us know if you want to be added to this list.
77   
78 Contributors to this release
79     
80       * David Schleef
81       * Javier Jardón
82       * Руслан Ижбулатов
83