2 GStreamer: Release notes for GStreamer 0.10.2 "If man is five"
6 The GStreamer team is proud to announce a new release
7 in the 0.10.x stable series of the
8 core of the GStreamer streaming media framework.
11 The 0.10.x series is a stable series targeted at end users.
12 It is not API or ABI compatible with the stable 0.8.x series.
13 It is, however, parallel installable with the 0.8.x series.
16 The 0.10.x series has been reworked for threadsafety. It also features
17 various feature additions and enchancements.
20 This module, gstreamer, only contains core functionality.
21 For actual media playback, you will need other modules.
23 gst-plugins-base
24 contains a basic set of well-supported plug-ins
25 gst-plugins-good
26 contains a set of well-supported plug-ins under our preferred license
27 gst-plugins-ugly
28 contains a set of well-supported plug-ins, but might pose problems for
29 distributors
30 gst-plugins-bad
31 contains a set of less supported plug-ins that haven't passed the
32 rigorous quality testing we expect
37 Features of this release
39 * Parallel installability with 0.8.x series
40 * Threadsafe design and API
41 * documentation updates
42 * bug fixes
44 Bugs fixed in this release
46 * 325429 : GST_BOILERPLATE_FULL can't be used when compiling with -W...
47 * 316086 : MinGW compilation: fileindexer depends on mmap
49 Download
51 You can find source releases of gstreamer in the download directory:
52 http://gstreamer.freedesktop.org/src/gstreamer/
54 GStreamer Homepage
56 More details can be found on the project's website:
57 http://gstreamer.freedesktop.org/
59 Support and Bugs
61 We use GNOME's bugzilla for bug reports and feature requests:
62 http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
64 Developers
66 CVS is hosted on cvs.freedesktop.org.
67 All code is in CVS and can be checked out from there.
68 Interested developers of the core library, plug-ins, and applications should
69 subscribe to the gstreamer-devel list. If there is sufficient interest we
70 will create more lists as necessary.
73 Applications
75 At this point, ports of existing applications to 0.10 are still experimental.
76 Totem HEAD has a configure option to build the 0.10 backend.
77 A patch for Rhythmbox is maintained at
79 http://bugzilla.gnome.org/show_bug.cgi?id=309609.
80 Jamboree builds against GStreamer 0.10.
81 Flumotion has been ported to 0.10 as well.
84 Contributors to this release
86 * Brian Cameron
87 * David Schleef
88 * Edward Hervey
89 * James Livingston
90 * Jan Schmidt
91 * Sebastien Moutte
92 * Stefan Kost
93 * Thomas Vander Stichele
94 * Tim-Philipp Müller
95 * Wim Taymans