2 GStreamer: Release notes for GStreamer 0.9.5 "Bike Lunch Day"
5 The GStreamer team is petrified to announce a new release
6 in the 0.9.x development series of the
7 core of the GStreamer streaming media framework.
10 The 0.9.x series is a development series and not recommended for end users.
11 It is not API or ABI compatible with the stable 0.8.x series.
12 It is, however, parallel installable with the 0.8.x series.
15 The main focus of the 0.9 series is to make GStreamer threadsafe.
18 This module, gstreamer, only contains core functionality.
19 For actual media playback, you will need other modules.
21 gst-plugins-base
22 contains a basic set of well-supported plug-ins
23 gst-plugins-good
24 contains a set of well-supported plug-ins under our preferred license
25 gst-plugins-ugly
26 contains a set of well-supported plug-ins, but might pose problems for
27 distributors
28 gst-plugins-bad
29 contains a set of less supported plug-ins that haven't passed the
30 rigorous quality testing we expect
35 Features of this release
37 * Parallel installability with 0.8.x series
38 * Threadsafe design and API
39 * gst_bus_poll and signal watch now see the same messages
40 * clock sync in BaseSrc class
41 * API documentation updates
42 * Bus reworked; signal API added
44 Bugs fixed in this release
46 * 317341 : after linking ghost pads, one target pad does not have a ...
47 * 320774 : basesrc commit broke typefinding
49 Download
51 You can find source releases of gstreamer in the download directory:
52 http://gstreamer.freedesktop.org/src/gstreamer/
54 GStreamer Homepage
56 More details can be found on the project's website:
57 http://gstreamer.freedesktop.org/
59 Support and Bugs
61 We use GNOME's bugzilla for bug reports and feature requests:
62 http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer
64 Developers
66 CVS is hosted on cvs.freedesktop.org.
67 All code is in CVS and can be checked out from there.
68 Interested developers of the core library, plug-ins, and applications should
69 subscribe to the gstreamer-devel list. If there is sufficient interest we
70 will create more lists as necessary.
73 Applications
75 At this point, ports of existing applications to 0.9 are still experimental.
76 A patch for Totem is maintained at
78 http://bugzilla.gnome.org/show_bug.cgi?id=313086.
79 A patch for Rhythmbox is maintained at
81 http://bugzilla.gnome.org/show_bug.cgi?id=309609.
82 Jamboree has a branch with the tag "jamboree-gst-0.9" that works against
83 GStreamer 0.9.
84 Flumotion has been mostly ported to 0.9 as well.
87 Contributors to this release
89 * Andy Wingo
90 * Edward Hervey
91 * Johan Dahlin
92 * Julien MOUTTE
93 * Luca Ognibene
94 * Michael Smith
95 * Stefan Kost
96 * Thomas Vander Stichele
97 * Tim-Philipp Müller
98 * Wim Taymans