1 GStreamer uses a *large* array of tools and libraries, most of which are
2 optional. We have attempted to make sure that any code that depends on
3 optional libraries doesn't get built unless you have those libraries. If
4 you find this not to be the case, please, let us know by filing a bug
5 report at http://sourceforge.net/bugs/?group_id=1936.
8 Required libraries:
9 ===================
11 glib2
12 libxml2 (also called gnome-xml, available from http://xmlsoft.org/)
14 These libraries are all central parts of gnome, and are available from the
15 ftp.gnome.org or its mirrors, amongst other places.
18 Optional libraries for Plugins:
19 ==============================
21 The vast number of optional libraries that can be used for plugins are
22 listed in the REQUIREMENTS document in the gst-plugins package.
25 Required tools:
26 ===============
28 bison >= 1.35
29 flex
31 An extra set of tools is required if you wish to build GStreamer out of
32 CVS (using autogen.sh):
34 autoconf 2.52
35 automake 1.6
36 libtool v1.4 or better
37 pkgconfig 0.9.0 (http://www.freedesktop.org/software/pkgconfig/)
40 Optional tools:
41 ===============
43 gtkdoc
44 db2html
45 fig2dev
46 xsltproc
48 To build pdf and ps version of docs
49 ===================================
50 passivetex
51 xmltex
52 tetex-dvips
54 Optional debian packages:
55 =========================
57 (This is an incomplete list, made only of problems which have been reported,
58 rather than by an audit.)
59 task-helix-gnome-dev OR libgnome-dev
61 gtk-doc-tools 0.4-0.2 -- needed to build documentation
63 Alternatively, the docbook-gnome-bin package, which is available by adding the
64 following lines to apt's sources.list (/etc/apt/sources.list):
66 deb ftp://ftp.home-of-linux.org/pub/debian gnome/
67 deb-src ftp://ftp.home-of-linux.org/pub/debian gnome/