1 GStreamer documentation notes
3 IMPORTANT
4 =========
6 Please make sure you've read and understood everything in this file
7 before you try changing documentation.
9 OVERVIEW
10 ========
12 GStreamer has two sets of documentation that we maintain:
13 * API references, using gtk-doc (gstreamer, gstreamer-libs)
14 * "books", using DocBook/XML (faq, manual, pwg)
16 DOCBOOK NOTES
17 =============
19 OK, I've grown so tired of having to coax the docs to build every time I
20 get round to it that I've decided to note down some of the things that
21 are important to know.
23 OVERVIEW
24 --------
25 * Our documentation should all be Docbook/XML. No SGML.
26 * The source for the documentation is:
27 - one or more .xml files, with the main one being gstreamer-(whatever).xml
28 - image files
29 - in .fig
30 - in .png (and maybe others)
31 * We want to generate docs in HTML, PS and PDF
32 * We want to use xml to to generate these
34 CONVENTIONS
35 -----------
36 We stick to some simple conventions for writing docbook documentation.
37 * id names:
38 - all id's start with chapter-, part-, section-, or misc-
39 - verify this is the case by looking at the generated file names in html/
40 - sections should also include the chapter name;
41 for example in a chapter called chapter-example, a section would be
42 called section-example-hello-world
43 * there are currently comments of the form <!-- synchronize with PWG -->
44 in the docbook file. Please check the relevant section of the other manual
45 when updating.
47 HOW IMAGES ARE HANDLED
48 ----------------------
49 * the format of images used is:
50 - PNG for html
51 - EPS for ps
52 - PDF for pdf
54 * images may need to be converted from their source format to the end format
56 * a file called image.entities is generated that provides two entities:
57 ℑ and &IMAGE;
58 ℑ is the file extension (png, ps, pdf)
59 * all generated images will be put in images/
61 HOW THE BUILD WORKS FOR EACH FORMAT
62 -----------------------------------
63 * HTML:
64 - xmlto html gstreamer-whatever.xml should produce the html docs.
65 - We do this in the html subdir of the doc builddir.
66 - images are copied to (builddir)/html/images
67 - PNGS should be set to all of the png's referenced for html, both
68 already there and auto-generated
70 * PS :
71 - images are converted to .ps files in EPS format. Generated images are
72 put in images/
73 - xmlto ps gstreamer-whatever.xml generates the ps file
75 * PDF :
76 There are two ways:
77 - ps2pdf is the easiest
78 - we specify ps, PS as the image type, but using xmlto the build will fail
79 because it uses ps2pdf internally and it fails to generate the images
80 By hand-generating .pdf images before xmlto we can make the build succeed.
81 (This is why image-pdf has file ext pdf but type EPS; this tricks xmlto in
82 doing the right thing)
83 xmlto pdf gstreamer-whatever.xml generates pdf (but seems to fail on the
84 FAQ, so for now we use ps2pdf)
86 HOW THE BUILD SYSTEM IS SET UP
87 ------------------------------
88 * make all should build html, ps, and pdf
89 * html is built in a subdir, with the png/ps images copied there
90 * ps and pdf are built in the current dir, in one file
92 SPELL CHECKING
93 --------------
94 * with aspell
95 * aspell -b -c --mode=sgml --lang=en <file>.xml
96 unfortunately the curses-ui of aspell (0.50.5) has problems with the xml tags
99 GTK-DOC NOTES
100 =============
102 * files under CVS control:
103 - Makefile.am
104 - gstreamer-sections.txt
105 describes which symbols later appear on one api-doc page
106 configure which symbols are shown/invisible/private
107 - gstreamer.types
108 the types file lists all get_type() functions that register the GObject types
109 - gstreamer-docs.sgml
110 defines the overall structure of the api documentation
111 - tmpl/
112 - only add the file to CVS if you have at least filled the short description
113 (filename corresponds to the <FILE> tag in the sections file)
114 - document as much as possible in the source (*.c files)
116 * what to do when adding a new piece of API:
117 - add both an entity and use the entity in gstreamer-docs.sgml
118 - add a new <SECTION> to gstreamer-sections.txt in the correct alphabetical
119 position related to the other sections (so that it is easier to locate)
120 - add all documented symbols to gstreamer-sections.txt in the proper section
121 (default),<SUBSECTION Standard>,<SUBSECTION Private>
122 - document at least the Short_Description in tmpl/.sgml
123 - document symbols where they are defined, so that when one changes the
124 definition, the chaces are good that docs are updated.
125 - document functions, signals in the .c files
126 - document structs, typedefs, enums in the .h files
128 * checklist:
129 - make sure *-sections.txt has a <TITLE> set for each <FILE>
130 - add only *one* <TITLE> to each file, when you have multiple classes in one
131 source-file, create one <FILE> section for each class
132 - the <TITLE> *must* be named like the type of the GType, when it gets
133 registered (otherwise gtkdoc introspection fails)
134 - for clarity name the <FILE> like the <TITLE>, but all lowercase
136 * what to do when trying to improve the docs
137 - compare the output of
138 grep "_get_type" gstreamer-sections.txt | sort
139 with the types in XXX.types to detect entries that
140 are maybe missing
141 - gtk docs does not warns about empty member docs!, run
142 find . -name "*.[c,h]" -exec egrep -Hn "^ +\* +@.*: *$" {} \;
143 in the project root to find them
144 - gtk docs does not warns about empty Returns: docs!, run
145 find . -name "*.[c,h]" -exec egrep -Hn "^ +\* +@Returns: *$" {} \;
146 in the project root to find them
148 * what happens during a gtk-doc build ?
149 - Scan step:
150 - based on a $(MODULE).types file:
151 - gtkdoc-scangobj creates a gtkdoc-scan binary
152 - using CC, LD, CFLAGS, LDFLAGS env var
153 - using --type-init-func and --module parameters
154 - gtkdoc-scan creates
155 - $MODULE.signals.new
156 - $MODULE.hierarchy.new
157 - $MODULE.interfaces.new
158 - $MODULE.prerequisites.new
159 - $MODULE.args.new
160 - generated source and objects get deleted
161 - gtkdoc-scangobj merges changes into the original files
162 - gtkdoc-scan
163 - extracts decls of functions, macros, enums, structs, unions from headers
164 - generates
165 - $MODULE-decl.txt
166 - $MODULE-decl-list.txt
167 - $MODULE-decl-list.txt then should get copied to $MODULE-sections.txt
168 - scan-build.stamp gets created
170 - Template generation step:
171 - gtkdoc-mktmpl --module=$MODULE
172 - reads in tmpl/*.sgml
173 - moves them to tmpl/*.sgml.bak
174 - recreates tmpl/*.sgml according to $MODULE-sections.txt
175 - moves unused stuff to $MODULE-unused.txt
176 - tmpl-build.stamp gets generated
178 * Possible errors and how to fix them
179 - Warning: multiple "IDs" for constraint linkend: gst-tag-register.
180 - check if gst_tag_register is listed more than once in -sections.txt
182 STYLE GUIDE FOR GTK-DOC
183 =======================
184 - this is in addition to gtk-doc's style-guide.txt
186 - when documenting signals, use "the #Gst..." for the object receiving the
187 signal; no trailing dot, and no "that received the signal"
188 - function/macro descriptions are descriptive, not imperative
189 ie, it uses the third person verb
190 - synopsis and description should have most-used/application functions at the
191 top
192 - functions that can return FALSE/NULL or fail should describe their failure
193 conditions like this:
194 * Returns NULL if no element with the given name is found in the bin, if
195 * the frobble was stuck in the froob, or the frizzle was frazzed.
196 - a line with function attributes should be added before Returns:
197 - can contain:
198 "MT safe." - the function is verified to be multithreadingsafe
199 "Caller owns returned reference" for refcounted classes
200 "Caller owns returned value" for other types (iterators, ..)
201 - we do this because, in contrast with GLib/GTK, we are more explicit
202 about threadsafety and related issues
203 - link to signals from the description like this:
204 * The <link linkend="GstBin-element-added">element-added</link> signal
205 - the bottom of the description should say when the doc was last reviewed
206 (version and date)
207 * Last reviewed on 2005-10-28 (0.9.4)
209 WEBSITE DOCUMENTATION
210 =====================
212 Updating the online documentation is pretty simple.
213 Make sure that you
214 a) have a working freedesktop.org account
215 b) $HOME/.ssh/config set up so that it has the right User for the Host
216 (for example, I have:
217 Host freedesktop.org
218 User thomasvs
219 c) verify this works by doing ssh freedesktop.org and being logged in without
220 a password prompt
221 d) have verified your changes build documentation locally.
223 Then, after updating any of the docs, run "make upload" from that directory.
224 Or, run "make upload" from this (docs) directory.
226 DOCUMENTING ELEMENTS
227 ====================
228 As of september 2005 we have some system to document plugins and elements
229 in the various plugin packages.
231 - in a submodule, docs go in docs/plugins
232 - template can be copied from gst-plugins-base
233 - to add plugins documentation:
234 - create docs/plugins
235 - create Makefile.am and friends, add to configure.ac
236 - create docs/version.entities.in, add to configure.ac
237 - in docs/plugins:
238 - create $(module)-plugins.types with #include <gst/gst.h>
239 - run make
240 - edit the -docs.sgml
241 - add to cvs:
242 cvs add *-plugins-docs.sgml *-plugins.args *-plugins.hierarchy *-plugins.interfaces *-plugins.prerequisites *-plugins.signals *-plugins.types inspect-build.stamp inspect.stamp scanobj-build.stamp
243 cvs add inspect
244 cvs add inspect/*.xml
245 - Additional types can be added to the documentation by placing them in
246 the .types file like this:
247 type:GstPlayBaseBin
248 This is useful for documenting plugin-private types that implement
249 signals or properties. The GType is looked up by name after all the
250 element classes have been printed - so this is only useful for types
251 that are created as a consequence of loading plugins and registering
252 the element(s).
254 - to add a plugin to be documented:
255 - make sure inspect/ has generated a inspect/plugin-xxx.xml file for it.
256 - if it has not, make sure you have pygst installed and run 'make update'.
257 and add it to CVS.
258 - add an xi:include in -docs.sgml in the Plugins chapter for that plugin
260 - to add an element to be documented:
261 - add an xi:include in the Elements chapter for the element
262 in the main -docs.sgml
263 - add a section for it in -sections.txt with
264 <SECTION>
265 <FILE>element-(element)</FILE>
266 <TITLE>(element)</TITLE>
267 GstXxx
268 <SUBSECTION Standard>
269 GstXxxClass
270 GST_XXX
271 GST_XXX_CLASS
272 GST_IS_XXX
273 GST_IS_XXX_CLASS
274 GST_TYPE_XXX
275 gst_xxx_get_type
276 </SECTION>
277 - add a gtk-doc section to the source code like:
278 /**
279 * SECTION:element-multifdsink
281 and fill it with documentation about the element, preferably inside
282 a <refsect2> docbook container.
283 - add an example:
284 - either a few pipelines, inside <programlisting>
285 - or a piece of code:
286 - create an example program (element)-example.c in the plugin dir
287 - add the full path (starting with $(top_srcdir)) for this example
288 to the EXAMPLE_CFILES variable in Makefile.am
289 - add an xinclude of a file named "element-(element)-example.xml"
290 to the docbook documentation piece in the element source code
291 - add the header to EXTRA_HFILES in Makefile.am to be able to document
292 signals and args; in that case, the object struct needs to be in
293 -sections.txt outside of the Standard Subsection (which is annoying,
294 but ...)
295 (FIXME: are we sure we can both do the xinclude from the tmpl/ sgml,
296 as well as an override from the source itself ? maybe we should just
297 make sure the xinclude is in the source itself instead ?)
298 - if the plugin has no public header, don't add the c-file, add entries to the
299 -overrides.txt file (see playbin docs in plugins-base).
300 - to rebuild the docs, do:
301 make clean
302 make update
303 make
304 - examples will only show up using gtk-doc 1.4 or later - it relies on
305 merging stuff from .sgml with inline docs. We might want to change
306 this to only get stuff from the source.
307 - you need to commit resulting files to git:
308 - changes to *.signals and *.args
309 - new files for your plugin created in inspect/
310 - if you get this warning:
311 " Documentation in template xxx for ./tmpl/element-yyy:Short_Description
312 being overridden by inline comments"
313 per-default the description from the GST_ELEMENT_DETAILS is put to the
314 Short_Description. This warning mean you have a different one in the section
315 docs as "@short_description:".
317 - the plugin-doc-list on the gstreamer homepage is updated along with other
318 web site updates.
320 - maintainer tricks:
321 - in gst-plugins-foo/docs/plugins/, run
322 make check-inspected-versions
323 to show plugins whose inspect information is not up-to-date (which is
324 usually either because they have been moved to a different module or
325 because they are not built on the maintainer's machine for some reason).
326 Whether it really makes sense to update the version number is debatable
327 (after all, the inspected information may be outdated and things may have
328 changed, in which case it would be bad to change the version number)
329 - find files that have docs
330 for file in `find . -name "*.c" -exec grep -l " * SECTION:element-" {} \; | sort`; do if [ -e ${file/.c/.h} ]; then echo ${file/.c/.h}; else echo "no header for $file"; fi; done
331 for file in `find . -name "*.cc" -exec grep -l " * SECTION:element-" {} \; | sort`; do if [ -e ${file/.cc/.h} ]; then echo ${file/.cc/.h}; else echo "no header for $file"; fi; done
332 - add those .h files to EXTRA_HFILES in Makefile.am
333 - update gst-plugins-xxx-docs.sgml
334 cd docs/plugins
335 ls -1 xml/plugin-*.xml | sort | sed -e "s/\(.*\)/ \<xi:include href=\"\1\" \/\>/"
336 ls -1 xml/element-*.xml | grep -v -- "-details.xml" | sort | sed -e "s/\(.*\)/ \<xi:include href=\"\1\" \/\>/"
337 - maybe we can generate these lists after "make update" and just xi:include
338 them in gst-plugins-xxx-docs.sgml. They should be committed to the vcs.
340 - possible errors:
341 - "multiple constraints for linkend ID":
342 check if each section in -sections.txt actually starts and ends with
343 <SECTION> and </SECTION>
344 - if a plugin does not show up:
345 - check inspect/plugin-xxx.xml and tmpl/elements-
347 RANDOM THINGS I'VE LEARNED
348 ==========================
350 * for clean builddir != srcdir separation, I wanted to use xmlto --searchpath
351 so the source xml could find the built entity file.
352 But xmlto --searchpath is (right now) for TeX input, not xml input.
353 xsltproc has a --path option (that xmlto doesn't use yet), but it
354 resolves single files to $(specified_path)/$(srcdir)/$(file)
355 For now, we need to hack around it by copying xml to the build dir.
358 (old) DOCUMENTATION BUILDING NOTES
359 ----------------------------------
361 To build the GStreamer documentation you need the following installed (based on
362 Red Hat packages). These packages comes from rawhide and are the ones that
363 will be in Red Hat 7.3/8.0
365 Docbook stuff:
366 sgml-common
367 xml-common
368 openjade (needs to be rebuilt from SRPM for Red Hat 7.2)
369 tetex-dvips
370 jadetex
371 docbook-dtds
372 docbook-style-dsssl
373 docbook-style-xsl
374 docbook-utils
376 XML stuff:
377 libxml2
378 libxml2-python
379 libxml2-devel
380 libxslt
381 libxslt-devel
382 libxslt-python
386 Gtkdoc:
387 gtk-doc
389 Other stuff:
390 transfig
391 pdftops
393 DEVHELP INTEGRATION
394 -------------------
395 Check http://www.imendio.com/projects/devhelp/
396 It's a really nice development app allowing you to look up API stuff
397 from various gtk-doc'd libraries. GStreamer is one of these ;)
399 gtk-doc generates both html API docs and the matching .devhelp(2) books.
401 IMAGES
402 ------
403 It's important to keep the original source format for images, to be able
404 to change and regenerate later on. Original files go in
405 docs/images