1 Conventions for thread a safe API
2 ---------------------------------
4 The GStreamer API is designed to be thread safe. This means that API functions
5 can be called from multiple threads at the same time. GStreamer internally uses
6 threads to perform the data passing and various asynchronous services such as
7 the clock can also use threads.
9 This design decision has implications for the usage of the API and the objects
10 which this document explains.
12 MT safety techniques
13 ~~~~~~~~~~~~~~~~~~~~
15 Several design patterns are used to guarantee object consistency in GStreamer.
16 This is an overview of the methods used in various GStreamer subsystems.
18 Refcounting:
20 All shared objects have a refcount associated with them. Each reference
21 obtained to the object should increase the refcount and each reference lost
22 should decrease the refcount.
24 The refcounting is used to make sure that when another thread destroys the
25 object, the ones which still hold a reference to the object do not read from
26 invalid memory when accessing the object.
28 Refcounting is also used to ensure that mutable data structures are only
29 modified when they are owned by the calling code.
31 It is a requirement that when two threads have a handle on an object, the
32 refcount must be more than one. This means that when one thread passes an
33 object to another thread it must increase the refcount. This requirement makes
34 sure that one thread cannot suddenly dispose the object making the other
35 thread crash when it tries to access the pointer to invalid memory.
37 Shared data structures and writability:
39 All objects have a refcount associated with them. Each reference obtained to
40 the object should increase the refcount and each reference lost should
41 decrease the refcount.
43 Each thread having a refcount to the object can safely read from the object.
44 but modifications made to the object should be preceeded with a
45 _get_writable() function call. This function will check the refcount of the
46 object and if the object is referenced by more than one instance, a copy is
47 made of the object that is then by definition only referenced from the calling
48 thread. This new copy is then modifiable without being visible to other
49 refcount holders.
51 This technique is used for information objects that, once created, never
52 change their values. The lifetime of these objects is generally short, the
53 objects are usually simple and cheap to copy/create.
55 The advantage of this method is that no reader/writers locks are needed. all
56 threads can concurrently read but writes happen locally on a new copy. In most
57 cases _get_writable() can avoid a real copy because the calling method is the
58 only one holding a reference, which makes read/write very cheap.
60 The drawback is that sometimes 1 needless copy can be done. This would happen
61 when N threads call _get_writable() at the same time, all seeing that N
62 references are held on the object. In this case 1 copy too many will be done.
63 This is not a problem in any practical situation because the copy operation is
64 fast.
66 Mutable substructures:
68 Special techniques are necessary to ensure the consistency of compound shared
69 objects. As mentioned above, shared objects need to have a reference count of
70 1 if they are to be modified. Implicit in this assumption is that all parts of
71 the shared object belong only to the object. For example, a GstStructure in
72 one GstCaps object should not belong to any other GstCaps object. This
73 condition suggests a parent-child relationship: structures can only be added
74 to parent object if they do not already have a parent object.
76 In addition, these substructures must not be modified while more than one code
77 segment has a reference on the parent object. For example, if the user creates
78 a GstStructure, adds it to a GstCaps, and the GstCaps is then referenced by
79 other code segments, the GstStructure should then become immutable, so that
80 changes to that data structure do not affect other parts of the code. This
81 means that the child is only mutable when the parent's reference count is 1,
82 as well as when the child structure has no parent.
84 The general solution to this problem is to include a field in child structures
85 pointing to the parent's atomic reference count. When set to NULL, this
86 indicates that the child has no parent. Otherwise, procedures that modify the
87 child structure must check if the parent's refcount is 1, and otherwise must
88 cause an error to be signaled.
90 Note that this is an internal implementation detail; application or plugin
91 code that calls _get_writable() on an object is guaranteed to receive an
92 object of refcount 1, which must then be writable. The only trick is that a
93 pointer to a child structure of an object is only valid while the calling code
94 has a reference on the parent object, because the parent is the owner of the
95 child.
97 Object locking:
99 For objects that contain state information and generally have a longer
100 lifetime, object locking is used to update the information contained in the
101 object.
103 All readers and writers acquire the lock before accessing the object. Only one
104 thread is allowed access the protected structures at a time.
106 Object locking is used for all objects extending from GstObject such as
107 GstElement, GstPad.
109 Object locking can be done with recursive locks or regular mutexes. Object
110 locks in GStreamer are implemented with mutexes which cause deadlocks when
111 locked recursively from the same thread. This is done because regular mutexes
112 are cheaper.
114 Atomic operations
116 Atomic operations are operations that are performed as one consistent
117 operation even when executed by multiple threads. They do however not use the
118 conventional aproach of using mutexes to protect the critical section but rely
119 on CPU features and instructions.
121 The advantages are mostly speed related since there are no heavyweight locks
122 involved. Most of these instructions also do not cause a context switch in case
123 of concurrent access but use a retry mechanism or spinlocking.
125 Disadvantages are that each of these instructions usually cause a cache flush
126 on multi-CPU machines when two processors perform concurrent access.
128 Atomic operations are generally used for refcounting and for the allocation of
129 small fixed size objects in a memchunk. They can also be used to implement a
130 lockfree list or stack.
132 Compare and swap
134 As part of the atomic operations, compare-and-swap (CAS) can be used to access
135 or update a single property or pointer in an object without having to take a
136 lock.
138 This technique is currently not used in GStreamer but might be added in the
139 future in performance critical places.
142 Objects
143 ~~~~~~~
145 * Locking involved:
147 - atomic operations for refcounting
148 - object locking
150 All objects should have a lock associated with them. This lock is used to keep
151 internal consistency when multiple threads call API function on the object.
153 For objects that extend the GStreamer base object class this lock can be
154 obtained with the macros GST_OBJECT_LOCK() and GST_OBJECT_UNLOCK(). For other object that do
155 not extend from the base GstObject class these macros can be different.
157 * refcounting
159 All new objects created have the FLOATING flag set. This means that the object
160 is not owned or managed yet by anybody other than the one holding a reference
161 to the object. The object in this state has a reference count of 1.
163 Various object methods can take ownership of another object, this means that
164 after calling a method on object A with an object B as an argument, the object
165 B is made sole property of object A. This means that after the method call you
166 are not allowed to access the object anymore unless you keep an extra
167 reference to the object. An example of such a method is the _bin_add() method.
168 As soon as this function is called in a Bin, the element passed as an argument
169 is owned by the bin and you are not allowed to access it anymore without
170 taking a _ref() before adding it to the bin. The reason being that after the
171 _bin_add() call disposing the bin also destroys the element.
173 Taking ownership of an object happens through the process of "sinking" the
174 object. the _sink() method on an object will decrease the refcount of the
175 object if the FLOATING flag is set. The act of taking ownership of an object
176 is then performed as a _ref() followed by a _sink() call on the object.
178 The float/sink process is very useful when initializing elements that will
179 then be placed under control of a parent. The floating ref keeps the object
180 alive until it is parented, and once the object is parented you can forget
181 about it.
183 also see part-relations.txt
185 * parent-child relations
187 One can create parent-child relationships with the _object_set_parent()
188 method. This method refs and sinks the object and assigns its parent property
189 to that of the managing parent.
191 The child is said to have a weak link to the parent since the refcount of the
192 parent is not increased in this process. This means that if the parent is
193 disposed it has to unset itself as the parent of the object before disposing
194 itself, else the child object holds a parent pointer to invalid memory.
196 The responsibilities for an object that sinks other objects are summarised as:
198 - taking ownership of the object
199 - call _object_set_parent() to set itself as the object parent, this call
200 will _ref() and _sink() the object.
201 - keep reference to object in a datastructure such as a list or array.
203 - on dispose
204 - call _object_unparent() to reset the parent property and unref the
205 object.
206 - remove the object from the list.
208 also see part-relations.txt
210 * Properties
212 Most objects also expose state information with public properties in the
213 object. Two types of properties might exist: accessible with or without
214 holding the object lock. All properties should only be accessed with their
215 corresponding macros. The public object properties are marked in the .h files
216 with /*< public >*/. The public properties that require a lock to be held are
217 marked with /*< public >*/ /* with <lock_type> */, where <lock_type> can be
218 "LOCK" or "STATE_LOCK" or any other lock to mark the type(s) of lock to be
219 held.
221 Example:
223 in GstPad there is a public property "direction". It can be found in the
224 section marked as public and requiring the LOCK to be held. There exists
225 also a macro to access the property.
227 struct _GstRealPad {
228 ...
229 /*< public >*/ /* with LOCK */
230 ...
231 GstPadDirection direction;
232 ...
233 };
235 #define GST_RPAD_DIRECTION(pad) (GST_REAL_PAD_CAST(pad)->direction)
237 Accessing the property is therefore allowed with the following code example:
239 GST_OBJECT_LOCK (pad);
240 direction = GST_RPAD_DIRECTION (pad);
241 GST_OBJECT_UNLOCK (pad);
243 * Property lifetime
245 All properties requiring a lock can change after releasing the associated
246 lock. This means that as long as you hold the lock, the state of the
247 object regarding the locked properties is consistent with the information
248 obtained. As soon as the lock is released, any values acquired from the
249 properties might not be valid anymore and can as best be described as a
250 snapshot of the state when the lock was held.
252 This means that all properties that require access beyond the scope of the
253 critial section should be copied or refcounted before releasing the lock.
255 Most object provide a _get_<property>() method to get a copy or refcounted
256 instance of the property value. The caller should not wory about any locks
257 but should unref/free the object after usage.
259 Example:
261 the following example correctly gets the peer pad of an element. It is
262 required to increase the refcount of the peer pad because as soon as the
263 lock is released, the peer could be unreffed and disposed, making the
264 pointer obtained in the critical section point to invalid memory.
266 GST_OBJECT_LOCK (pad);
267 peer = GST_RPAD_PEER (pad);
268 if (peer)
269 gst_object_ref (GST_OBJECT (peer));
270 GST_OBJECT_UNLOCK (pad);
271 ... use peer ...
273 if (peer)
274 gst_object_unref (GST_OBJECT (peer));
276 Note that after releasing the lock the peer might not actually be the peer
277 anymore of the pad. If you need to be sure it is, you need to extend the
278 critical section to include the operations on the peer.
280 The following code is equivalent to the above but with using the functions
281 to access object properties.
283 peer = gst_pad_get_peer (pad);
284 if (peer) {
285 ... use peer ...
287 gst_object_unref (GST_OBJECT (peer));
288 }
290 Example:
292 Accessing the name of an object makes a copy of the name. The caller of the
293 function should g_free() the name after usage.
295 GST_OBJECT_LOCK (object)
296 name = g_strdup (GST_OBJECT_NAME (object));
297 GST_OBJECT_UNLOCK (object)
298 ... use name ...
300 g_free (name);
302 or:
304 name = gst_object_get_name (object);
306 ... use name ...
308 g_free (name);
311 * Accessor methods
313 For aplications it is encouraged to use the public methods of the object. Most
314 useful operations can be performed with the methods so it is seldom required
315 to access the public fields manually.
317 All accessor methods that return an object should increase the refcount of the
318 returned object. The caller should _unref() the object after usage. Each
319 method should state this refcounting policy in the documentation.
321 * Accessing lists
323 If the object property is a list, concurrent list iteration is needed to get
324 the contents of the list. GStreamer uses the cookie mechanism to mark the last
325 update of a list. The list and the cookie are protected by the same lock. Each
326 update to a list requires the following actions:
328 - acquire lock
329 - update list
330 - update cookie
331 - release lock
333 Updating the cookie is usually done by incrementing its value by one. Since
334 cookies use guint32 its wraparound is for all practical reasons is not a
335 problem.
337 Iterating a list can safely be done by surrounding the list iteration with a
338 lock/unlock of the lock.
340 In some cases it is not a good idea to hold the lock for a long time while
341 iterating the list. The state change code for a bin in GStreamer, for example,
342 has to iterate over each element and perform a blocking call on each of them
343 potentially causing infinite bin locking. In this case the cookie can be used
344 to iterate a list.
346 Example:
348 The following algorithm iterates a list and reverses the updates in the
349 case a concurrent update was done to the list while iterating. The idea is
350 that whenever we reacquire the lock, we check for updates to the cookie to
351 decide if we are still iterating the right list.
353 GST_OBJECT_LOCK (lock);
354 /* grab list and cookie */
355 cookie = object->list_cookie;
356 list = object-list;
357 while (list) {
358 GstObject *item = GST_OBJECT (list->data);
359 /* need to ref the item before releasing the lock */
360 gst_object_ref (item);
361 GST_OBJECT_UNLOCK (lock);
363 ... use/change item here...
365 /* release item here */
366 gst_object_unref (item);
368 GST_OBJECT_LOCK (lock);
369 if (cookie != object->list_cookie) {
370 /* handle rollback caused by concurrent modification
371 * of the list here */
373 ...rollback changes to items...
375 /* grab new cookie and list */
376 cookie = object->list_cookie;
377 list = object->list;
378 }
379 else {
380 list = g_list_next (list);
381 }
382 }
383 GST_OBJECT_UNLOCK (lock);
385 * GstIterator
387 GstIterator provides an easier way of retrieving elements in a concurrent
388 list. The following code example is equivalent to the previous example.
390 Example:
392 it = _get_iterator(object);
393 while (!done) {
394 switch (gst_iterator_next (it, &item)) {
395 case GST_ITERATOR_OK:
397 ... use/change item here...
399 /* release item here */
400 gst_object_unref (item);
401 break;
402 case GST_ITERATOR_RESYNC:
403 /* handle rollback caused by concurrent modification
404 * of the list here */
406 ...rollback changes to items...
408 /* resync iterator to start again */
409 gst_iterator_resync (it);
410 break;
411 case GST_ITERATOR_DONE:
412 done = TRUE;
413 break;
414 }
415 }
416 gst_iterator_free (it);