docs/design/: Update some docs.
[glsdk/gstreamer0-10.git] / docs / design / part-TODO.txt
1 API/ABI
2 -------
4 - implement return values from events in addition to the gboolean. This should
5   be done by making the event contain a GstStructure with input/output values,
6   similar to GstQuery. A typical use case is performing a non-accurate seek to a
7   keyframe, after the seek you want to get the new stream time that will
8   actually be used to update the slider bar.
10 - make gst_pad_push_event() return a GstFlowReturn so that we can resend
11   NEWSEGMENT and other events.
13 - GstEvent, GstMessage register like GstFormat or GstQuery.
15 - query POSITION/DURATION return accuracy. Just a flag or accuracy percentage.
17 - add some sort of time/frame stepping functionality, either with a flag on
18   the seek event or some new seek event type. The idea would be to operate on
19   the current playback position instead of the current configured segment when
20   doing the seek.
21   Idea is that frame stepping forwards can be done in the sinks, ie, just
22   dropping N frames/time, sending more complicated queries upstream which can
23   ideally handle those cases more efficiently too.
25 - use | instead of + as divider in serialization of Flags
26   (gstvalue/gststructure)
28 - rethink how we handle dynamic replugging wrt segments and other events that
29   already got pushed and need to be pushed again.
31 - keep track of seeks with a counter so that we can match seek events received
32   in the demuxer srcpads. This is needed because a normal seek on a pipeline
33   will send the seek event on all sinks, which results in the demuxer receiving
34   the seek twice. If there is no way to see that the seek is the same, it will
35   perform the seek twice.
36   It would also be nice to have this same sequence number in the segment event
37   that resulted from the seek so that everything seek related can be tracked
38   properly.
40 - When an element goes to PAUSED there is no way to figure out the running time
41   when this happened. One could think that we can store this time in the
42   base_time field of the element but that causes problems when the element is
43   still using the base_time before really PAUSING. We seem to need a new element
44   field for this. The running time when an element is paused can be usefull to
45   clip late buffers instead of prerolling on them.
47 - Elements in a bin have no clue about the final state of the parent element
48   since the bin sets the target state on its children in small steps. This
49   causes problems for elements that like to know the final state (rtspsrc going
50   to PAUSED or READY is different in that we can avoid sending the useless
51   PAUSED request).
54 IMPLEMENTATION
55 --------------
57 - implement more QOS, see part-qos.txt.
59 - implement BUFFERSIZE.
61 - implement pad_block with probes.
64 DESIGN
65 ------
67 - unlinking pads in the PAUSED state needs to make sure the stream thread is not
68   executing code. Can this be done with a flush to unlock all downstream chain
69   functions? Do we do this automatically or let the app handle this?