1 Synchronisation
2 ---------------
4 This document outlines the techniques used for doing synchronised playback of
5 multiple streams.
7 Synchronisation in a GstPipeline is achieved using the following 3 components:
9 - a GstClock, which is global for all elements in a GstPipeline.
10 - Timestamps on a GstBuffer.
11 - the NEW_SEGMENT event preceding the buffers.
14 A GstClock
15 ----------
17 This object provides a counter that represents the current time in nanoseconds.
18 This value is called the absolute_time.
20 Different sources exist for this counter:
22 - the system time (with g_get_current_time() and with microsecond accuracy)
23 - an audio device (based on number of samples played)
24 - a network source based on packets received + timestamps in those packets (a
25 typical example is an RTP source)
26 - ...
28 In GStreamer any element can provide a GstClock object that can be used in the
29 pipeline. The GstPipeline object will select a clock from all the providers and
30 will distribute it to all other elements (see part-gstpipeline.txt).
32 A GstClock always counts time upwards and does not necessarily start at 0.
35 Running time
36 ------------
38 After a pipeline selected a clock it will maintain the running_time based on the
39 selected clock. This running_time represents the total time spent in the PLAYING
40 state and is calculated as follows:
42 - If the pipeline is NULL/READY, the running_time is undefined.
43 - In PAUSED, the running_time remains at the time when it was last
44 PAUSED. When the stream is PAUSED for the first time, the running_time
45 is 0.
46 - In PLAYING, the running_time is the delta between the absolute_time
47 and the base time. The base time is defined as the absolute_time minus
48 the running_time at the time when the pipeline is set to PLAYING.
49 - after a flushing seek, the running_time is set to 0 (see part-seeking.txt).
50 This is accomplished by redistributing a new base_time to the elements that
51 got flushed.
53 This algorithm captures the running_time when the pipeline is set from PLAYING
54 to PAUSED and restores this time based on the current absolute_time when going
55 back to PLAYING. This allows for both clocks that progress when in the PAUSED
56 state (systemclock) and clocks that don't (audioclock).
58 The clock and pipeline now provides a running_time to all elements that want to
59 perform synchronisation. Indeed, the running time can be observed in each
60 element (during the PLAYING state) as:
62 running_time = absolute_time - base_time
65 Timestamps
66 ----------
68 The GstBuffer timestamps and the preceeding NEW_SEGMENT event (See
69 part-streams.txt) define a transformation of the buffers to running_time as
70 follows:
72 The following notation is used:
74 B: GstBuffer
75 - B.timestamp = buffer timestamp (GST_BUFFER_TIMESTAMP)
77 NS: NEWSEGMENT event preceeding the buffers.
78 - NS.start: start field in the NEWSEGMENT event
79 - NS.rate: rate field of NEWSEGMENT event
80 - NS.abs_rate: absolute value of rate field of NEWSEGMENT event
81 - NS.time: time field in the NEWSEGMENT event
82 - NS.accum: total accumulated time of all previous NEWSEGMENT events. This
83 field is kept in the GstSegment structure.
85 Valid buffers for synchronisation are those with B.timestamp between NS.start
86 and NS.stop. All other buffers outside this range should be dropped or clipped
87 to these boundaries (see also part-segments.txt).
89 The following transformation to running_time exist:
91 if (NS.rate > 0.0)
92 running_time = (B.timestamp - NS.start) / NS.abs_rate + NS.accum
93 else
94 running_time = (NS.stop - B.timestamp) / NS.abs_rate + NS.accum
96 The first displayable buffer will yield a value of 0 (since B.timestamp ==
97 NS.start and NS.accum == 0).
99 For NS.rate > 1.0, the timestamps will be scaled down to increase the playback
100 rate. Likewise, a rate between 0.0 and 1.0 will slow down playback.
102 For negative rates, timestamps are received stop NS.stop to NS.start so that the
103 first buffer received will be transformed into running_time of 0 (B.timestamp ==
104 NS.stop and NS.accum == 0).
107 Synchronisation
108 ---------------
110 As we have seen, we can get a running_time:
112 - using the clock and the element's base_time with:
114 C.running_time = absolute_time - base_time
116 - using the buffer timestamp and the preceeding NEWSEGMENT event as (assuming
117 positive playback rate):
119 B.running_time = (B.timestamp - NS.start) / NS.abs_rate + NS.accum
121 We prefix C. and B. before the two running times to note how they were
122 calculated.
124 The task of synchronized playback is to make sure that we play be buffer with
125 B.running_time at the moment when the clock reaches the same C.running_time.
127 Thus the following must hold:
129 B.running_time = C.running_time
131 expaning:
133 B.running_time = absolute_time - base_time
135 or:
137 absolute_time = B.running_time + base_time
139 The absolute_time when a buffer with B.running_time should be played is noted
140 with B.sync_time. Thus:
142 B.sync_time = B.running_time + base_time
144 One then waits for the clock to reach B.sync_time before rendering the buffer in
145 the sink (See also part-clocks.txt).
147 For multiple streams this means that buffers with the same running_time are to
148 be displayed at the same time.
150 A demuxer must make sure that the NEWSEGMENT it emits on its output pads yield
151 the same running_time for buffers that should be played synchronized. This
152 usually means sending the same NEWSEGMENT on all pads and making sure that the
153 synchronized buffers have the same timestamps.
156 Stream time
157 -----------
159 The stream time is also known as the position in the stream and is a value
160 between 0 and the total duration of the media file.
162 It is the stream time that is used for:
164 - report the POSITION query in the pipeline
165 - the position used in seek queries
166 - the position used to synchronize controller values
168 Stream time is calculated using the buffer times and the preceeding NEWSEGMENT
169 event as follows:
171 stream_time = (B.timestamp - NS.start) * NS.abs_applied_rate + NS.time
173 For negative rates, B.timestamp will go backwards from NS.stop to NS.start,
174 making the stream time go backwards.
176 Note that the stream time is never used for synchronisation against the clock.