8c56286a600378ff13cf95801e1b8d353567eb07
1 #!/bin/bash -i
2 #
3 # this script is in git as gstreamer/docs/faq/gst-uninstalled
4 #
5 # It will set up the environment to use and develop gstreamer and projects
6 # that use gstreamer with an uninstalled git checkout of gstreamer and the
7 # plugin modules.
8 #
9 # It will set up LD_LIBRARY_PATH, DYLD_LIBRARY_PATH, PKG_CONFIG_PATH,
10 # GST_PLUGIN_PATH, GST_PLUGIN_SYSTEM_PATH, GST_REGISTRY, MANPATH, PYTHONPATH
11 # to prefer the uninstalled versions but also contain the installed ones.
12 # The only exception to this is, that no system installed plugins will be
13 # used but only the uninstalled ones.
14 #
15 # This script assumes that the relevant modules are checked out one by one
16 # under a given tree specified below in MYGST.
17 #
18 # Symlink this script in a directory in your path (for example $HOME/bin). You
19 # must name the symlink gst-something, where something is the subdirectory
20 # of MYGST that contains your gstreamer module checkouts.
21 #
22 # e.g.:
23 # - mkdir $HOME/gst/head
24 # - ln -sf gst-uninstalled $HOME/bin/gst-head
25 # - checkout copies of gstreamer modules in $HOME/gst/head
26 # - gst-head
28 # This script is run -i so that PS1 doesn't get cleared
30 # Change this variable to the location of your gstreamer git checkouts
31 MYGST=$HOME/gst
33 #
34 # Everything below this line shouldn't be edited!
35 #
37 # extract version from $0
38 # if this script is called "gst-head" then version will be "head"
39 VERSION=`echo $0 | sed s/.*gst-//g`
41 # base path under which dirs are installed
42 GST=$MYGST/$VERSION
43 if test ! -e $GST; then
44 echo "$GST does not exist !"
45 exit
46 fi
48 # set up a bunch of paths
49 PATH="\
50 $GST/gstreamer/tools:\
51 $GST/gst-plugins-base/tools:\
52 $GST/gst-player/src:\
53 $GST/gst-editor/src:\
54 $GST/prefix/bin:\
55 $PATH"
57 # /some/path: makes the dynamic linker look in . too, so avoid this
58 LD_LIBRARY_PATH=$GST/prefix/lib${LD_LIBRARY_PATH:+:$LD_LIBRARY_PATH}
59 DYLD_LIBRARY_PATH=$GST/prefix/lib${DYLD_LIBRARY_PATH:+:$DYLD_LIBRARY_PATH}
61 # GStreamer rtsp server library
62 LD_LIBRARY_PATH=$GST/gst-rtsp-server/gst/rtsp-server/.libs:$LD_LIBRARY_PATH
63 DYLD_LIBRARY_PATH=$GST/gst-rtsp-server/gst/rtsp-server/.libs:$DYLD_LIBRARY_PATH
65 # GStreamer ffmpeg libraries
66 for path in libavformat libavutil libavcodec libpostproc libavdevice
67 do
68 LD_LIBRARY_PATH=$GST/gst-ffmpeg/gst-libs/ext/ffmpeg/$path:$LD_LIBRARY_PATH
69 DYLD_LIBRARY_PATH=$GST/gst-ffmpeg/gst-libs/ext/ffmpeg/$path:$DYLD_LIBRARY_PATH
70 done
72 # GStreamer plugins base libraries
73 for path in app audio cdda fft interfaces pbutils netbuffer riff rtp rtsp sdp tag utils video
74 do
75 LD_LIBRARY_PATH=$GST/gst-plugins-base/gst-libs/gst/$path/.libs:$LD_LIBRARY_PATH
76 DYLD_LIBRARY_PATH=$GST/gst-plugins-base/gst-libs/gst/$path/.libs:$DYLD_LIBRARY_PATH
77 done
79 # GStreamer core libraries
80 for path in base net check controller dataprotocol
81 do
82 LD_LIBRARY_PATH=$GST/gstreamer/libs/gst/$path/.libs:$LD_LIBRARY_PATH
83 DYLD_LIBRARY_PATH=$GST/gstreamer/libs/gst/$path/.libs:$DYLD_LIBRARY_PATH
84 done
85 LD_LIBRARY_PATH=$GST/gstreamer/gst/.libs:$LD_LIBRARY_PATH
86 DYLD_LIBRARY_PATH=$GST/gstreamer/gst/.libs:$DYLD_LIBRARY_PATH
87 export LD_LIBRARY_PATH
88 export DYLD_LIBRARY_PATH
90 export PKG_CONFIG_PATH="\
91 $GST/prefix/lib/pkgconfig\
92 :$GST/gstreamer/pkgconfig\
93 :$GST/gst-plugins-base/pkgconfig\
94 :$GST/gst-plugins-good/pkgconfig\
95 :$GST/gst-python/pkgconfig\
96 :$GST/gst-rtsp-server/pkgconfig\
97 ${PKG_CONFIG_PATH:+:$PKG_CONFIG_PATH}"
99 export GST_PLUGIN_PATH="\
100 $GST/gstreamer/plugins\
101 :$GST/gst-plugins-base/ext\
102 :$GST/gst-plugins-base/gst\
103 :$GST/gst-plugins-base/sys\
104 :$GST/gst-plugins-good/ext\
105 :$GST/gst-plugins-good/gst\
106 :$GST/gst-plugins-good/sys\
107 :$GST/gst-plugins-ugly/ext\
108 :$GST/gst-plugins-ugly/gst\
109 :$GST/gst-plugins-ugly/sys\
110 :$GST/gst-plugins-bad/ext\
111 :$GST/gst-plugins-bad/gst\
112 :$GST/gst-plugins-bad/sys\
113 :$GST/gst-ffmpeg/ext\
114 :$GST/gnonlin/gnl\
115 :$GST/gst-openmax\
116 :$GST/gst-plugins-gl/gst\
117 :$GST/plugins\
118 ${GST_PLUGIN_PATH:+:$GST_PLUGIN_PATH}"
120 # don't use any system-installed plug-ins at all
121 export GST_PLUGIN_SYSTEM_PATH=
122 # set our registry somewhere else so we don't mess up the registry generated
123 # by an installed copy
124 rm -f $GST/gstreamer/registry.xml 2>/dev/null
125 export GST_REGISTRY=$GST/gstreamer/registry.dat
127 # once MANPATH is set, it needs at least an "empty"component to keep pulling
128 # in the system-configured man paths from man.config
129 # this still doesn't make it work for the uninstalled case, since man goes
130 # look for a man directory "nearby" instead of the directory I'm telling it to
131 export MANPATH=$GST/gstreamer/tools:$GST/prefix/share/man:$MANPATH
132 pythonver=`python -c "import sys; print sys.version[:3]"`
133 export PYTHONPATH=$GST/gst-python:$GST/prefix/lib/python$pythonver/site-packages${PYTHONPATH:+:$PYTHONPATH}
135 # totem-pl-parser
136 export PKG_CONFIG_PATH=$GST/totem-pl-parser:$PKG_CONFIG_PATH
137 export LD_LIBRARY_PATH=$GST/totem-pl-parser/plparse/.libs:$LD_LIBRARY_PATH
138 export DYLD_LIBRARY_PATH=$GST/totem-pl-parser/plparse/.libs:$DYLD_LIBRARY_PATH
140 # totem
141 export PATH=$GST/totem/src:$PATH
143 # if we got a command, run it, else start a shell
144 if test ! -z "$1";
145 then
146 $@
147 exit $?
148 fi
150 # set up prompt to help us remember we're in a subshell, cd to
151 # the gstreamer base dir and start $SHELL
152 cd $GST
153 shell=$SHELL
154 if test "x$SHELL" == "x/bin/bash"
155 then
156 # debian/ubuntu resets our PS1. bastards.
157 shell="$SHELL --noprofile"
158 fi
159 PS1="[gst-$VERSION] $PS1" $shell