6d7021906dd2da6de99a2d0ac71d3cfba5cb7bdd
1 <!-- ##### SECTION Title ##### -->
2 GstThread
4 <!-- ##### SECTION Short_Description ##### -->
5 A bin that will become a thread
7 <!-- ##### SECTION Long_Description ##### -->
8 <para>
9 A bin that will become a thread if possible when the pipeline is started
10 up. It can contain any set of GstObjects.
11 </para>
12 <para>
13 A Thread can act as a toplevel bin as it has its own scheduler.
14 </para>
16 <!-- ##### SECTION See_Also ##### -->
17 <para>
18 #GstBin, #GstPipeline
19 </para>
21 <!-- ##### ENUM GstThreadState ##### -->
22 <para>
23 Thread flags:
24 </para>
26 @GST_THREAD_STATE_SPINNING: The thread is runnning
27 @GST_THREAD_STATE_REAPING: The thread is ending.
28 @GST_THREAD_MUTEX_LOCKED:
29 @GST_THREAD_FLAG_LAST: subclass use this to start their enumeration
31 <!-- ##### STRUCT GstThread ##### -->
32 <para>
33 The GstThread object
34 </para>
37 <!-- ##### FUNCTION gst_thread_new ##### -->
38 <para>
40 </para>
42 @name:
43 @Returns:
46 <!-- ##### SIGNAL GstThread::shutdown ##### -->
47 <para>
49 </para>
51 @gstthread: the object which received the signal.
53 <!-- ##### ARG GstThread:priority ##### -->
54 <para>
55 The thread priority
56 </para>