1 /* GStreamer
2 * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3 * 2000 Wim Taymans <wtay@chello.be>
4 *
5 * gst.c: Initialization and non-pipeline operations
6 *
7 * This library is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU Library General Public
9 * License as published by the Free Software Foundation; either
10 * version 2 of the License, or (at your option) any later version.
11 *
12 * This library is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
15 * Library General Public License for more details.
16 *
17 * You should have received a copy of the GNU Library General Public
18 * License along with this library; if not, write to the
19 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20 * Boston, MA 02111-1307, USA.
21 */
23 /**
24 * SECTION:gst
25 * @short_description: Media library supporting arbitrary formats and filter
26 * graphs.
27 *
28 * GStreamer is a framework for constructing graphs of various filters
29 * (termed elements here) that will handle streaming media. Any discreet
30 * (packetizable) media type is supported, with provisions for automatically
31 * determining source type. Formatting/framing information is provided with
32 * a powerful negotiation framework. Plugins are heavily used to provide for
33 * all elements, allowing one to construct plugins outside of the GST
34 * library, even released binary-only if license require (please don't).
35 * GStreamer covers a wide range of use cases including: playback, recording,
36 * editing, serving streams, voice over ip and video calls.
37 *
38 * The <application>GStreamer</application> library should be initialized with
39 * gst_init() before it can be used. You should pass pointers to the main argc
40 * and argv variables so that GStreamer can process its own command line
41 * options, as shown in the following example.
42 *
43 * <example>
44 * <title>Initializing the gstreamer library</title>
45 * <programlisting language="c">
46 * int
47 * main (int argc, char *argv[])
48 * {
49 * // initialize the GStreamer library
50 * gst_init (&argc, &argv);
51 * ...
52 * }
53 * </programlisting>
54 * </example>
55 *
56 * It's allowed to pass two NULL pointers to gst_init() in case you don't want
57 * to pass the command line args to GStreamer.
58 *
59 * You can also use GOption to initialize your own parameters as shown in
60 * the next code fragment:
61 * <example>
62 * <title>Initializing own parameters when initializing gstreamer</title>
63 * <programlisting>
64 * static gboolean stats = FALSE;
65 * ...
66 * int
67 * main (int argc, char *argv[])
68 * {
69 * GOptionEntry options[] = {
70 * {"tags", 't', 0, G_OPTION_ARG_NONE, &tags,
71 * N_("Output tags (also known as metadata)"), NULL},
72 * {NULL}
73 * };
74 * // must initialise the threading system before using any other GLib funtion
75 * if (!g_thread_supported ())
76 * g_thread_init (NULL);
77 * ctx = g_option_context_new ("[ADDITIONAL ARGUMENTS]");
78 * g_option_context_add_main_entries (ctx, options, GETTEXT_PACKAGE);
79 * g_option_context_add_group (ctx, gst_init_get_option_group ());
80 * if (!g_option_context_parse (ctx, &argc, &argv, &err)) {
81 * g_print ("Error initializing: %s\n", GST_STR_NULL (err->message));
82 * exit (1);
83 * }
84 * g_option_context_free (ctx);
85 * ...
86 * }
87 * </programlisting>
88 * </example>
89 *
90 * Use gst_version() to query the library version at runtime or use the
91 * GST_VERSION_* macros to find the version at compile time. Optionally
92 * gst_version_string() returns a printable string.
93 *
94 * The gst_deinit() call is used to clean up all internal resources used
95 * by <application>GStreamer</application>. It is mostly used in unit tests
96 * to check for leaks.
97 *
98 * Last reviewed on 2006-08-11 (0.10.10)
99 */
101 #include "gst_private.h"
102 #include "gstconfig.h"
103 #include <stdlib.h>
104 #include <stdio.h>
105 #include <sys/types.h>
106 #ifdef HAVE_SYS_UTSNAME_H
107 #include <sys/utsname.h>
108 #endif
109 #ifdef HAVE_UNISTD_H
110 #include <unistd.h>
111 #endif
112 #ifdef G_OS_WIN32
113 #define WIN32_LEAN_AND_MEAN /* prevents from including too many things */
114 #include <windows.h> /* GetStdHandle, windows console */
115 #endif
117 #include "gst-i18n-lib.h"
118 #include <locale.h> /* for LC_ALL */
120 #include "gst.h"
122 #define GST_CAT_DEFAULT GST_CAT_GST_INIT
124 #define MAX_PATH_SPLIT 16
125 #define GST_PLUGIN_SEPARATOR ","
127 static gboolean gst_initialized = FALSE;
128 static gboolean gst_deinitialized = FALSE;
130 #ifdef G_OS_WIN32
131 HMODULE _priv_gst_dll_handle = NULL;
132 #endif
134 #ifndef GST_DISABLE_REGISTRY
135 GList *_priv_gst_plugin_paths = NULL; /* for delayed processing in post_init */
137 extern gboolean _priv_gst_disable_registry_update;
138 #endif
140 #ifndef GST_DISABLE_GST_DEBUG
141 extern const gchar *priv_gst_dump_dot_dir;
142 #endif
144 /* defaults */
146 /* set to TRUE when segfaults need to be left as is */
147 static gboolean _gst_disable_segtrap = FALSE;
149 static gboolean init_pre (GOptionContext * context, GOptionGroup * group,
150 gpointer data, GError ** error);
151 static gboolean init_post (GOptionContext * context, GOptionGroup * group,
152 gpointer data, GError ** error);
153 #ifndef GST_DISABLE_OPTION_PARSING
154 static gboolean parse_goption_arg (const gchar * s_opt,
155 const gchar * arg, gpointer data, GError ** err);
156 #endif
158 GSList *_priv_gst_preload_plugins = NULL;
160 const gchar g_log_domain_gstreamer[] = "GStreamer";
162 static void
163 debug_log_handler (const gchar * log_domain,
164 GLogLevelFlags log_level, const gchar * message, gpointer user_data)
165 {
166 g_log_default_handler (log_domain, log_level, message, user_data);
167 /* FIXME: do we still need this ? fatal errors these days are all
168 * other than core errors */
169 /* g_on_error_query (NULL); */
170 }
172 enum
173 {
174 ARG_VERSION = 1,
175 ARG_FATAL_WARNINGS,
176 #ifndef GST_DISABLE_GST_DEBUG
177 ARG_DEBUG_LEVEL,
178 ARG_DEBUG,
179 ARG_DEBUG_DISABLE,
180 ARG_DEBUG_NO_COLOR,
181 ARG_DEBUG_HELP,
182 #endif
183 ARG_PLUGIN_SPEW,
184 ARG_PLUGIN_PATH,
185 ARG_PLUGIN_LOAD,
186 ARG_SEGTRAP_DISABLE,
187 ARG_REGISTRY_UPDATE_DISABLE,
188 ARG_REGISTRY_FORK_DISABLE
189 };
191 /* debug-spec ::= category-spec [, category-spec]*
192 * category-spec ::= category:val | val
193 * category ::= [^:]+
194 * val ::= [0-5]
195 */
197 #ifndef NUL
198 #define NUL '\0'
199 #endif
201 #ifndef GST_DISABLE_GST_DEBUG
202 static gboolean
203 parse_debug_category (gchar * str, const gchar ** category)
204 {
205 if (!str)
206 return FALSE;
208 /* works in place */
209 g_strstrip (str);
211 if (str[0] != NUL) {
212 *category = str;
213 return TRUE;
214 }
216 return FALSE;
217 }
219 static gboolean
220 parse_debug_level (gchar * str, GstDebugLevel * level)
221 {
222 if (!str)
223 return FALSE;
225 /* works in place */
226 g_strstrip (str);
228 if (str[0] != NUL && str[1] == NUL
229 && str[0] >= '0' && str[0] < '0' + GST_LEVEL_COUNT) {
230 *level = (GstDebugLevel) (str[0] - '0');
231 return TRUE;
232 }
234 return FALSE;
235 }
237 static void
238 parse_debug_list (const gchar * list)
239 {
240 gchar **split;
241 gchar **walk;
243 g_assert (list);
245 split = g_strsplit (list, ",", 0);
247 for (walk = split; *walk; walk++) {
248 if (strchr (*walk, ':')) {
249 gchar **values = g_strsplit (*walk, ":", 2);
251 if (values[0] && values[1]) {
252 GstDebugLevel level;
253 const gchar *category;
255 if (parse_debug_category (values[0], &category)
256 && parse_debug_level (values[1], &level))
257 gst_debug_set_threshold_for_name (category, level);
258 }
260 g_strfreev (values);
261 } else {
262 GstDebugLevel level;
264 if (parse_debug_level (*walk, &level))
265 gst_debug_set_default_threshold (level);
266 }
267 }
269 g_strfreev (split);
270 }
271 #endif
273 #ifdef G_OS_WIN32
274 BOOL WINAPI DllMain (HINSTANCE hinstDLL, DWORD fdwReason, LPVOID lpvReserved);
275 BOOL WINAPI
276 DllMain (HINSTANCE hinstDLL, DWORD fdwReason, LPVOID lpvReserved)
277 {
278 if (fdwReason == DLL_PROCESS_ATTACH)
279 _priv_gst_dll_handle = (HMODULE) hinstDLL;
280 return TRUE;
281 }
283 #endif
285 /**
286 * gst_init_get_option_group:
287 *
288 * Returns a #GOptionGroup with GStreamer's argument specifications. The
289 * group is set up to use standard GOption callbacks, so when using this
290 * group in combination with GOption parsing methods, all argument parsing
291 * and initialization is automated.
292 *
293 * This function is useful if you want to integrate GStreamer with other
294 * libraries that use GOption (see g_option_context_add_group() ).
295 *
296 * If you use this function, you should make sure you initialise the GLib
297 * threading system as one of the very first things in your program
298 * (see the example at the beginning of this section).
299 *
300 * Returns: (transfer full): a pointer to GStreamer's option group.
301 */
303 GOptionGroup *
304 gst_init_get_option_group (void)
305 {
306 #ifndef GST_DISABLE_OPTION_PARSING
307 GOptionGroup *group;
308 static const GOptionEntry gst_args[] = {
309 {"gst-version", 0, G_OPTION_FLAG_NO_ARG, G_OPTION_ARG_CALLBACK,
310 (gpointer) parse_goption_arg, N_("Print the GStreamer version"), NULL},
311 {"gst-fatal-warnings", 0, G_OPTION_FLAG_NO_ARG, G_OPTION_ARG_CALLBACK,
312 (gpointer) parse_goption_arg, N_("Make all warnings fatal"), NULL},
313 #ifndef GST_DISABLE_GST_DEBUG
314 {"gst-debug-help", 0, G_OPTION_FLAG_NO_ARG, G_OPTION_ARG_CALLBACK,
315 (gpointer) parse_goption_arg,
316 N_("Print available debug categories and exit"),
317 NULL},
318 {"gst-debug-level", 0, 0, G_OPTION_ARG_CALLBACK,
319 (gpointer) parse_goption_arg,
320 N_("Default debug level from 1 (only error) to 5 (anything) or "
321 "0 for no output"),
322 N_("LEVEL")},
323 {"gst-debug", 0, 0, G_OPTION_ARG_CALLBACK, (gpointer) parse_goption_arg,
324 N_("Comma-separated list of category_name:level pairs to set "
325 "specific levels for the individual categories. Example: "
326 "GST_AUTOPLUG:5,GST_ELEMENT_*:3"),
327 N_("LIST")},
328 {"gst-debug-no-color", 0, G_OPTION_FLAG_NO_ARG, G_OPTION_ARG_CALLBACK,
329 (gpointer) parse_goption_arg, N_("Disable colored debugging output"),
330 NULL},
331 {"gst-debug-disable", 0, G_OPTION_FLAG_NO_ARG, G_OPTION_ARG_CALLBACK,
332 (gpointer) parse_goption_arg, N_("Disable debugging"), NULL},
333 #endif
334 {"gst-plugin-spew", 0, G_OPTION_FLAG_NO_ARG, G_OPTION_ARG_CALLBACK,
335 (gpointer) parse_goption_arg,
336 N_("Enable verbose plugin loading diagnostics"),
337 NULL},
338 {"gst-plugin-path", 0, 0, G_OPTION_ARG_CALLBACK,
339 (gpointer) parse_goption_arg,
340 N_("Colon-separated paths containing plugins"), N_("PATHS")},
341 {"gst-plugin-load", 0, 0, G_OPTION_ARG_CALLBACK,
342 (gpointer) parse_goption_arg,
343 N_("Comma-separated list of plugins to preload in addition to the "
344 "list stored in environment variable GST_PLUGIN_PATH"),
345 N_("PLUGINS")},
346 {"gst-disable-segtrap", 0, G_OPTION_FLAG_NO_ARG, G_OPTION_ARG_CALLBACK,
347 (gpointer) parse_goption_arg,
348 N_("Disable trapping of segmentation faults during plugin loading"),
349 NULL},
350 {"gst-disable-registry-update", 0, G_OPTION_FLAG_NO_ARG,
351 G_OPTION_ARG_CALLBACK,
352 (gpointer) parse_goption_arg,
353 N_("Disable updating the registry"),
354 NULL},
355 {"gst-disable-registry-fork", 0, G_OPTION_FLAG_NO_ARG,
356 G_OPTION_ARG_CALLBACK,
357 (gpointer) parse_goption_arg,
358 N_("Disable spawning a helper process while scanning the registry"),
359 NULL},
360 {NULL}
361 };
363 /* Since GLib 2.31.0 threading is always enabled and g_thread_init()
364 * is not needed any longer and deprecated */
365 #if !GLIB_CHECK_VERSION (2, 31, 0)
366 /* Since GLib 2.23.2 calling g_thread_init() 'late' is allowed and is
367 * automatically done as part of g_type_init() */
368 if (glib_check_version (2, 23, 3)) {
369 /* The GLib threading system must be initialised before calling any other
370 * GLib function according to the documentation; if the application hasn't
371 * called gst_init() yet or initialised the threading system otherwise, we
372 * better issue a warning here (since chances are high that the application
373 * has already called other GLib functions such as g_option_context_new() */
374 if (!g_thread_get_initialized ()) {
375 g_warning ("The GStreamer function gst_init_get_option_group() was\n"
376 "\tcalled, but the GLib threading system has not been initialised\n"
377 "\tyet, something that must happen before any other GLib function\n"
378 "\tis called. The application needs to be fixed so that it calls\n"
379 "\t if (!g_thread_get_initialized ()) g_thread_init(NULL);\n"
380 "\tas very first thing in its main() function. Please file a bug\n"
381 "\tagainst this application.");
382 g_thread_init (NULL);
383 }
384 } else {
385 /* GLib >= 2.23.2 */
386 }
387 #endif
389 group = g_option_group_new ("gst", _("GStreamer Options"),
390 _("Show GStreamer Options"), NULL, NULL);
391 g_option_group_set_parse_hooks (group, (GOptionParseFunc) init_pre,
392 (GOptionParseFunc) init_post);
394 g_option_group_add_entries (group, gst_args);
395 g_option_group_set_translation_domain (group, GETTEXT_PACKAGE);
397 return group;
398 #else
399 return NULL;
400 #endif
401 }
403 /**
404 * gst_init_check:
405 * @argc: (inout) (allow-none): pointer to application's argc
406 * @argv: (inout) (array length=argc) (allow-none): pointer to application's argv
407 * @err: pointer to a #GError to which a message will be posted on error
408 *
409 * Initializes the GStreamer library, setting up internal path lists,
410 * registering built-in elements, and loading standard plugins.
411 *
412 * This function will return %FALSE if GStreamer could not be initialized
413 * for some reason. If you want your program to fail fatally,
414 * use gst_init() instead.
415 *
416 * This function should be called before calling any other GLib functions. If
417 * this is not an option, your program must initialise the GLib thread system
418 * using g_thread_init() before any other GLib functions are called.
419 *
420 * Returns: %TRUE if GStreamer could be initialized.
421 */
422 gboolean
423 gst_init_check (int *argc, char **argv[], GError ** err)
424 {
425 #ifndef GST_DISABLE_OPTION_PARSING
426 GOptionGroup *group;
427 GOptionContext *ctx;
428 #endif
429 gboolean res;
431 #if !GLIB_CHECK_VERSION (2, 31, 0)
432 if (!g_thread_get_initialized ())
433 g_thread_init (NULL);
434 #endif
436 if (gst_initialized) {
437 GST_DEBUG ("already initialized gst");
438 return TRUE;
439 }
440 #ifndef GST_DISABLE_OPTION_PARSING
441 ctx = g_option_context_new ("- GStreamer initialization");
442 g_option_context_set_ignore_unknown_options (ctx, TRUE);
443 group = gst_init_get_option_group ();
444 g_option_context_add_group (ctx, group);
445 res = g_option_context_parse (ctx, argc, argv, err);
446 g_option_context_free (ctx);
447 #else
448 init_pre (NULL, NULL, NULL, NULL);
449 init_post (NULL, NULL, NULL, NULL);
450 res = TRUE;
451 #endif
453 gst_initialized = res;
455 if (res) {
456 GST_INFO ("initialized GStreamer successfully");
457 } else {
458 GST_INFO ("failed to initialize GStreamer");
459 }
461 return res;
462 }
464 /**
465 * gst_init:
466 * @argc: (inout) (allow-none): pointer to application's argc
467 * @argv: (inout) (array length=argc) (allow-none): pointer to application's argv
468 *
469 * Initializes the GStreamer library, setting up internal path lists,
470 * registering built-in elements, and loading standard plugins.
471 *
472 * Unless the plugin registry is disabled at compile time, the registry will be
473 * loaded. By default this will also check if the registry cache needs to be
474 * updated and rescan all plugins if needed. See gst_update_registry() for
475 * details and section
476 * <link linkend="gst-running">Running GStreamer Applications</link>
477 * for how to disable automatic registry updates.
478 *
479 * This function should be called before calling any other GLib functions. If
480 * this is not an option, your program must initialise the GLib thread system
481 * using g_thread_init() before any other GLib functions are called.
482 *
483 * <note><para>
484 * This function will terminate your program if it was unable to initialize
485 * GStreamer for some reason. If you want your program to fall back,
486 * use gst_init_check() instead.
487 * </para></note>
488 *
489 * WARNING: This function does not work in the same way as corresponding
490 * functions in other glib-style libraries, such as gtk_init(). In
491 * particular, unknown command line options cause this function to
492 * abort program execution.
493 */
494 void
495 gst_init (int *argc, char **argv[])
496 {
497 GError *err = NULL;
499 if (!gst_init_check (argc, argv, &err)) {
500 g_print ("Could not initialize GStreamer: %s\n",
501 err ? err->message : "unknown error occurred");
502 if (err) {
503 g_error_free (err);
504 }
505 exit (1);
506 }
507 }
509 /**
510 * gst_is_initialized:
511 *
512 * Use this function to check if GStreamer has been initialized with gst_init()
513 * or gst_init_check().
514 *
515 * Returns: TRUE if initialization has been done, FALSE otherwise.
516 *
517 * Since: 0.10.31
518 */
519 gboolean
520 gst_is_initialized (void)
521 {
522 return gst_initialized;
523 }
525 #ifndef GST_DISABLE_REGISTRY
526 static void
527 add_path_func (gpointer data, gpointer user_data)
528 {
529 GST_INFO ("Adding plugin path: \"%s\", will scan later", (gchar *) data);
530 _priv_gst_plugin_paths =
531 g_list_append (_priv_gst_plugin_paths, g_strdup (data));
532 }
533 #endif
535 #ifndef GST_DISABLE_OPTION_PARSING
536 static void
537 prepare_for_load_plugin_func (gpointer data, gpointer user_data)
538 {
539 _priv_gst_preload_plugins =
540 g_slist_prepend (_priv_gst_preload_plugins, g_strdup (data));
541 }
542 #endif
544 #ifndef GST_DISABLE_OPTION_PARSING
545 static void
546 split_and_iterate (const gchar * stringlist, const gchar * separator,
547 GFunc iterator, gpointer user_data)
548 {
549 gchar **strings;
550 gint j = 0;
551 gchar *lastlist = g_strdup (stringlist);
553 while (lastlist) {
554 strings = g_strsplit (lastlist, separator, MAX_PATH_SPLIT);
555 g_free (lastlist);
556 lastlist = NULL;
558 while (strings[j]) {
559 iterator (strings[j], user_data);
560 if (++j == MAX_PATH_SPLIT) {
561 lastlist = g_strdup (strings[j]);
562 j = 0;
563 break;
564 }
565 }
566 g_strfreev (strings);
567 }
568 }
569 #endif
571 /* we have no fail cases yet, but maybe in the future */
572 static gboolean
573 init_pre (GOptionContext * context, GOptionGroup * group, gpointer data,
574 GError ** error)
575 {
576 if (gst_initialized) {
577 GST_DEBUG ("already initialized");
578 return TRUE;
579 }
581 g_type_init ();
583 #if !GLIB_CHECK_VERSION (2, 31, 0)
584 /* we need threading to be enabled right here */
585 g_assert (g_thread_get_initialized ());
586 #endif
588 _gst_debug_init ();
590 #ifdef ENABLE_NLS
591 setlocale (LC_ALL, "");
592 bindtextdomain (GETTEXT_PACKAGE, LOCALEDIR);
593 bind_textdomain_codeset (GETTEXT_PACKAGE, "UTF-8");
594 #endif /* ENABLE_NLS */
596 #ifndef GST_DISABLE_GST_DEBUG
597 {
598 const gchar *debug_list;
600 if (g_getenv ("GST_DEBUG_NO_COLOR") != NULL)
601 gst_debug_set_colored (FALSE);
603 debug_list = g_getenv ("GST_DEBUG");
604 if (debug_list) {
605 parse_debug_list (debug_list);
606 }
607 }
609 priv_gst_dump_dot_dir = g_getenv ("GST_DEBUG_DUMP_DOT_DIR");
610 #endif
611 /* This is the earliest we can make stuff show up in the logs.
612 * So give some useful info about GStreamer here */
613 GST_INFO ("Initializing GStreamer Core Library version %s", VERSION);
614 GST_INFO ("Using library installed in %s", LIBDIR);
616 /* Print some basic system details if possible (OS/architecture) */
617 #ifdef HAVE_SYS_UTSNAME_H
618 {
619 struct utsname sys_details;
621 if (uname (&sys_details) == 0) {
622 GST_INFO ("%s %s %s %s %s", sys_details.sysname,
623 sys_details.nodename, sys_details.release, sys_details.version,
624 sys_details.machine);
625 }
626 }
627 #endif
629 return TRUE;
630 }
632 static gboolean
633 gst_register_core_elements (GstPlugin * plugin)
634 {
635 /* register some standard builtin types */
636 if (!gst_element_register (plugin, "bin", GST_RANK_PRIMARY,
637 GST_TYPE_BIN) ||
638 !gst_element_register (plugin, "pipeline", GST_RANK_PRIMARY,
639 GST_TYPE_PIPELINE)
640 )
641 g_assert_not_reached ();
643 return TRUE;
644 }
646 /*
647 * this bit handles:
648 * - initalization of threads if we use them
649 * - log handler
650 * - initial output
651 * - initializes gst_format
652 * - registers a bunch of types for gst_objects
653 *
654 * - we don't have cases yet where this fails, but in the future
655 * we might and then it's nice to be able to return that
656 */
657 static gboolean
658 init_post (GOptionContext * context, GOptionGroup * group, gpointer data,
659 GError ** error)
660 {
661 GLogLevelFlags llf;
663 #ifndef GST_DISABLE_TRACE
664 GstTrace *gst_trace;
665 #endif /* GST_DISABLE_TRACE */
667 if (gst_initialized) {
668 GST_DEBUG ("already initialized");
669 return TRUE;
670 }
672 llf = G_LOG_LEVEL_CRITICAL | G_LOG_LEVEL_ERROR | G_LOG_FLAG_FATAL;
673 g_log_set_handler (g_log_domain_gstreamer, llf, debug_log_handler, NULL);
675 _priv_gst_quarks_initialize ();
676 _gst_format_initialize ();
677 _gst_query_initialize ();
678 g_type_class_ref (gst_object_get_type ());
679 g_type_class_ref (gst_pad_get_type ());
680 g_type_class_ref (gst_element_factory_get_type ());
681 g_type_class_ref (gst_element_get_type ());
682 g_type_class_ref (gst_type_find_factory_get_type ());
683 g_type_class_ref (gst_bin_get_type ());
684 g_type_class_ref (gst_bus_get_type ());
685 g_type_class_ref (gst_task_get_type ());
686 g_type_class_ref (gst_clock_get_type ());
688 g_type_class_ref (gst_index_factory_get_type ());
689 gst_uri_handler_get_type ();
691 g_type_class_ref (gst_object_flags_get_type ());
692 g_type_class_ref (gst_bin_flags_get_type ());
693 g_type_class_ref (gst_buffer_flag_get_type ());
694 g_type_class_ref (gst_buffer_copy_flags_get_type ());
695 g_type_class_ref (gst_buffer_list_item_get_type ());
696 g_type_class_ref (gst_bus_flags_get_type ());
697 g_type_class_ref (gst_bus_sync_reply_get_type ());
698 g_type_class_ref (gst_caps_flags_get_type ());
699 g_type_class_ref (gst_clock_return_get_type ());
700 g_type_class_ref (gst_clock_entry_type_get_type ());
701 g_type_class_ref (gst_clock_flags_get_type ());
702 g_type_class_ref (gst_clock_type_get_type ());
703 g_type_class_ref (gst_debug_graph_details_get_type ());
704 g_type_class_ref (gst_state_get_type ());
705 g_type_class_ref (gst_state_change_return_get_type ());
706 g_type_class_ref (gst_state_change_get_type ());
707 g_type_class_ref (gst_element_flags_get_type ());
708 g_type_class_ref (gst_core_error_get_type ());
709 g_type_class_ref (gst_library_error_get_type ());
710 g_type_class_ref (gst_resource_error_get_type ());
711 g_type_class_ref (gst_stream_error_get_type ());
712 g_type_class_ref (gst_event_type_flags_get_type ());
713 g_type_class_ref (gst_event_type_get_type ());
714 g_type_class_ref (gst_seek_type_get_type ());
715 g_type_class_ref (gst_seek_flags_get_type ());
716 g_type_class_ref (gst_qos_type_get_type ());
717 g_type_class_ref (gst_format_get_type ());
718 g_type_class_ref (gst_index_certainty_get_type ());
719 g_type_class_ref (gst_index_entry_type_get_type ());
720 g_type_class_ref (gst_index_lookup_method_get_type ());
721 g_type_class_ref (gst_assoc_flags_get_type ());
722 g_type_class_ref (gst_index_resolver_method_get_type ());
723 g_type_class_ref (gst_index_flags_get_type ());
724 g_type_class_ref (gst_debug_level_get_type ());
725 g_type_class_ref (gst_debug_color_flags_get_type ());
726 g_type_class_ref (gst_iterator_result_get_type ());
727 g_type_class_ref (gst_iterator_item_get_type ());
728 g_type_class_ref (gst_message_type_get_type ());
729 g_type_class_ref (gst_mini_object_flags_get_type ());
730 g_type_class_ref (gst_pad_link_return_get_type ());
731 g_type_class_ref (gst_pad_link_check_get_type ());
732 g_type_class_ref (gst_flow_return_get_type ());
733 g_type_class_ref (gst_activate_mode_get_type ());
734 g_type_class_ref (gst_pad_direction_get_type ());
735 g_type_class_ref (gst_pad_flags_get_type ());
736 g_type_class_ref (gst_pad_presence_get_type ());
737 g_type_class_ref (gst_pad_template_flags_get_type ());
738 g_type_class_ref (gst_pipeline_flags_get_type ());
739 g_type_class_ref (gst_plugin_error_get_type ());
740 g_type_class_ref (gst_plugin_flags_get_type ());
741 g_type_class_ref (gst_plugin_dependency_flags_get_type ());
742 g_type_class_ref (gst_rank_get_type ());
743 g_type_class_ref (gst_query_type_get_type ());
744 g_type_class_ref (gst_buffering_mode_get_type ());
745 g_type_class_ref (gst_stream_status_type_get_type ());
746 g_type_class_ref (gst_structure_change_type_get_type ());
747 g_type_class_ref (gst_tag_merge_mode_get_type ());
748 g_type_class_ref (gst_tag_flag_get_type ());
749 g_type_class_ref (gst_task_pool_get_type ());
750 g_type_class_ref (gst_task_state_get_type ());
751 g_type_class_ref (gst_alloc_trace_flags_get_type ());
752 g_type_class_ref (gst_type_find_probability_get_type ());
753 g_type_class_ref (gst_uri_type_get_type ());
754 g_type_class_ref (gst_parse_error_get_type ());
755 g_type_class_ref (gst_parse_flags_get_type ());
756 g_type_class_ref (gst_search_mode_get_type ());
757 g_type_class_ref (gst_progress_type_get_type ());
758 g_type_class_ref (gst_caps_intersect_mode_get_type ());
760 gst_structure_get_type ();
761 _gst_value_initialize ();
762 g_type_class_ref (gst_param_spec_fraction_get_type ());
763 gst_caps_get_type ();
764 _gst_event_initialize ();
765 _gst_buffer_initialize ();
766 _gst_buffer_list_initialize ();
767 gst_buffer_list_iterator_get_type ();
768 _gst_message_initialize ();
769 _gst_tag_initialize ();
770 gst_parse_context_get_type ();
772 _gst_plugin_initialize ();
774 gst_g_error_get_type ();
776 /* register core plugins */
777 gst_plugin_register_static (GST_VERSION_MAJOR, GST_VERSION_MINOR,
778 "staticelements", "core elements linked into the GStreamer library",
779 gst_register_core_elements, VERSION, GST_LICENSE, PACKAGE,
780 GST_PACKAGE_NAME, GST_PACKAGE_ORIGIN);
782 /*
783 * Any errors happening below this point are non-fatal, we therefore mark
784 * gstreamer as being initialized, since it is the case from a plugin point of
785 * view.
786 *
787 * If anything fails, it will be put back to FALSE in gst_init_check().
788 * This allows some special plugins that would call gst_init() to not cause a
789 * looping effect (i.e. initializing GStreamer twice).
790 */
791 gst_initialized = TRUE;
793 if (!gst_update_registry ())
794 return FALSE;
796 #ifndef GST_DISABLE_TRACE
797 _gst_trace_on = 0;
798 if (_gst_trace_on) {
799 gst_trace = gst_trace_new ("gst.trace", 1024);
800 gst_trace_set_default (gst_trace);
801 }
802 #endif /* GST_DISABLE_TRACE */
804 GST_INFO ("GLib runtime version: %d.%d.%d", glib_major_version,
805 glib_minor_version, glib_micro_version);
806 GST_INFO ("GLib headers version: %d.%d.%d", GLIB_MAJOR_VERSION,
807 GLIB_MINOR_VERSION, GLIB_MICRO_VERSION);
809 return TRUE;
810 }
812 #ifndef GST_DISABLE_GST_DEBUG
813 static gboolean
814 select_all (GstPlugin * plugin, gpointer user_data)
815 {
816 return TRUE;
817 }
819 static gint
820 sort_by_category_name (gconstpointer a, gconstpointer b)
821 {
822 return strcmp (gst_debug_category_get_name ((GstDebugCategory *) a),
823 gst_debug_category_get_name ((GstDebugCategory *) b));
824 }
826 static void
827 gst_debug_help (void)
828 {
829 GSList *list, *walk;
830 GList *list2, *g;
832 /* Need to ensure the registry is loaded to get debug categories */
833 if (!init_post (NULL, NULL, NULL, NULL))
834 exit (1);
836 list2 = gst_registry_plugin_filter (gst_registry_get_default (),
837 select_all, FALSE, NULL);
839 /* FIXME this is gross. why don't debug have categories PluginFeatures? */
840 for (g = list2; g; g = g_list_next (g)) {
841 GstPlugin *plugin = GST_PLUGIN_CAST (g->data);
843 gst_plugin_load (plugin);
844 }
845 g_list_free (list2);
847 list = gst_debug_get_all_categories ();
848 walk = list = g_slist_sort (list, sort_by_category_name);
850 g_print ("\n");
851 g_print ("name level description\n");
852 g_print ("---------------------+--------+--------------------------------\n");
854 while (walk) {
855 GstDebugCategory *cat = (GstDebugCategory *) walk->data;
857 if (gst_debug_is_colored ()) {
858 #ifdef G_OS_WIN32
859 gint color = gst_debug_construct_win_color (cat->color);
860 const gint clear = FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE;
862 SetConsoleTextAttribute (GetStdHandle (STD_OUTPUT_HANDLE), color);
863 g_print ("%-20s", gst_debug_category_get_name (cat));
864 SetConsoleTextAttribute (GetStdHandle (STD_OUTPUT_HANDLE), clear);
865 g_print (" %1d %s ", gst_debug_category_get_threshold (cat),
866 gst_debug_level_get_name (gst_debug_category_get_threshold (cat)));
867 SetConsoleTextAttribute (GetStdHandle (STD_OUTPUT_HANDLE), color);
868 g_print ("%s", gst_debug_category_get_description (cat));
869 SetConsoleTextAttribute (GetStdHandle (STD_OUTPUT_HANDLE), clear);
870 g_print ("\n");
871 #else /* G_OS_WIN32 */
872 gchar *color = gst_debug_construct_term_color (cat->color);
874 g_print ("%s%-20s\033[00m %1d %s %s%s\033[00m\n",
875 color,
876 gst_debug_category_get_name (cat),
877 gst_debug_category_get_threshold (cat),
878 gst_debug_level_get_name (gst_debug_category_get_threshold (cat)),
879 color, gst_debug_category_get_description (cat));
880 g_free (color);
881 #endif /* G_OS_WIN32 */
882 } else {
883 g_print ("%-20s %1d %s %s\n", gst_debug_category_get_name (cat),
884 gst_debug_category_get_threshold (cat),
885 gst_debug_level_get_name (gst_debug_category_get_threshold (cat)),
886 gst_debug_category_get_description (cat));
887 }
888 walk = g_slist_next (walk);
889 }
890 g_slist_free (list);
891 g_print ("\n");
892 }
893 #endif
895 #ifndef GST_DISABLE_OPTION_PARSING
896 static gboolean
897 parse_one_option (gint opt, const gchar * arg, GError ** err)
898 {
899 switch (opt) {
900 case ARG_VERSION:
901 g_print ("GStreamer Core Library version %s\n", PACKAGE_VERSION);
902 exit (0);
903 case ARG_FATAL_WARNINGS:{
904 GLogLevelFlags fatal_mask;
906 fatal_mask = g_log_set_always_fatal (G_LOG_FATAL_MASK);
907 fatal_mask |= G_LOG_LEVEL_WARNING | G_LOG_LEVEL_CRITICAL;
908 g_log_set_always_fatal (fatal_mask);
909 break;
910 }
911 #ifndef GST_DISABLE_GST_DEBUG
912 case ARG_DEBUG_LEVEL:{
913 GstDebugLevel tmp = GST_LEVEL_NONE;
915 tmp = (GstDebugLevel) strtol (arg, NULL, 0);
916 if (tmp >= 0 && tmp < GST_LEVEL_COUNT) {
917 gst_debug_set_default_threshold (tmp);
918 }
919 break;
920 }
921 case ARG_DEBUG:
922 parse_debug_list (arg);
923 break;
924 case ARG_DEBUG_NO_COLOR:
925 gst_debug_set_colored (FALSE);
926 break;
927 case ARG_DEBUG_DISABLE:
928 gst_debug_set_active (FALSE);
929 break;
930 case ARG_DEBUG_HELP:
931 gst_debug_help ();
932 exit (0);
933 #endif
934 case ARG_PLUGIN_SPEW:
935 break;
936 case ARG_PLUGIN_PATH:
937 #ifndef GST_DISABLE_REGISTRY
938 split_and_iterate (arg, G_SEARCHPATH_SEPARATOR_S, add_path_func, NULL);
939 #endif /* GST_DISABLE_REGISTRY */
940 break;
941 case ARG_PLUGIN_LOAD:
942 split_and_iterate (arg, ",", prepare_for_load_plugin_func, NULL);
943 break;
944 case ARG_SEGTRAP_DISABLE:
945 _gst_disable_segtrap = TRUE;
946 break;
947 case ARG_REGISTRY_UPDATE_DISABLE:
948 #ifndef GST_DISABLE_REGISTRY
949 _priv_gst_disable_registry_update = TRUE;
950 #endif
951 break;
952 case ARG_REGISTRY_FORK_DISABLE:
953 gst_registry_fork_set_enabled (FALSE);
954 break;
955 default:
956 g_set_error (err, G_OPTION_ERROR, G_OPTION_ERROR_UNKNOWN_OPTION,
957 _("Unknown option"));
958 return FALSE;
959 }
961 return TRUE;
962 }
964 static gboolean
965 parse_goption_arg (const gchar * opt,
966 const gchar * arg, gpointer data, GError ** err)
967 {
968 static const struct
969 {
970 const gchar *opt;
971 int val;
972 } options[] = {
973 {
974 "--gst-version", ARG_VERSION}, {
975 "--gst-fatal-warnings", ARG_FATAL_WARNINGS},
976 #ifndef GST_DISABLE_GST_DEBUG
977 {
978 "--gst-debug-level", ARG_DEBUG_LEVEL}, {
979 "--gst-debug", ARG_DEBUG}, {
980 "--gst-debug-disable", ARG_DEBUG_DISABLE}, {
981 "--gst-debug-no-color", ARG_DEBUG_NO_COLOR}, {
982 "--gst-debug-help", ARG_DEBUG_HELP},
983 #endif
984 {
985 "--gst-plugin-spew", ARG_PLUGIN_SPEW}, {
986 "--gst-plugin-path", ARG_PLUGIN_PATH}, {
987 "--gst-plugin-load", ARG_PLUGIN_LOAD}, {
988 "--gst-disable-segtrap", ARG_SEGTRAP_DISABLE}, {
989 "--gst-disable-registry-update", ARG_REGISTRY_UPDATE_DISABLE}, {
990 "--gst-disable-registry-fork", ARG_REGISTRY_FORK_DISABLE}, {
991 NULL}
992 };
993 gint val = 0, n;
995 for (n = 0; options[n].opt; n++) {
996 if (!strcmp (opt, options[n].opt)) {
997 val = options[n].val;
998 break;
999 }
1000 }
1002 return parse_one_option (val, arg, err);
1003 }
1004 #endif
1006 /**
1007 * gst_deinit:
1008 *
1009 * Clean up any resources created by GStreamer in gst_init().
1010 *
1011 * It is normally not needed to call this function in a normal application
1012 * as the resources will automatically be freed when the program terminates.
1013 * This function is therefore mostly used by testsuites and other memory
1014 * profiling tools.
1015 *
1016 * After this call GStreamer (including this method) should not be used anymore.
1017 */
1018 void
1019 gst_deinit (void)
1020 {
1021 GstClock *clock;
1023 GST_INFO ("deinitializing GStreamer");
1025 if (gst_deinitialized) {
1026 GST_DEBUG ("already deinitialized");
1027 return;
1028 }
1030 g_slist_foreach (_priv_gst_preload_plugins, (GFunc) g_free, NULL);
1031 g_slist_free (_priv_gst_preload_plugins);
1032 _priv_gst_preload_plugins = NULL;
1034 #ifndef GST_DISABLE_REGISTRY
1035 g_list_foreach (_priv_gst_plugin_paths, (GFunc) g_free, NULL);
1036 g_list_free (_priv_gst_plugin_paths);
1037 _priv_gst_plugin_paths = NULL;
1038 #endif
1040 clock = gst_system_clock_obtain ();
1041 gst_object_unref (clock);
1042 gst_object_unref (clock);
1044 _priv_gst_registry_cleanup ();
1046 g_type_class_unref (g_type_class_peek (gst_object_get_type ()));
1047 g_type_class_unref (g_type_class_peek (gst_pad_get_type ()));
1048 g_type_class_unref (g_type_class_peek (gst_element_factory_get_type ()));
1049 g_type_class_unref (g_type_class_peek (gst_element_get_type ()));
1050 g_type_class_unref (g_type_class_peek (gst_type_find_factory_get_type ()));
1051 g_type_class_unref (g_type_class_peek (gst_bin_get_type ()));
1052 g_type_class_unref (g_type_class_peek (gst_bus_get_type ()));
1053 g_type_class_unref (g_type_class_peek (gst_task_get_type ()));
1054 g_type_class_unref (g_type_class_peek (gst_index_factory_get_type ()));
1055 g_type_class_unref (g_type_class_peek (gst_object_flags_get_type ()));
1056 g_type_class_unref (g_type_class_peek (gst_bin_flags_get_type ()));
1057 g_type_class_unref (g_type_class_peek (gst_buffer_flag_get_type ()));
1058 g_type_class_unref (g_type_class_peek (gst_buffer_copy_flags_get_type ()));
1059 g_type_class_unref (g_type_class_peek (gst_buffer_list_item_get_type ()));
1060 g_type_class_unref (g_type_class_peek (gst_bus_flags_get_type ()));
1061 g_type_class_unref (g_type_class_peek (gst_bus_sync_reply_get_type ()));
1062 g_type_class_unref (g_type_class_peek (gst_caps_flags_get_type ()));
1063 g_type_class_unref (g_type_class_peek (gst_clock_type_get_type ()));
1064 g_type_class_unref (g_type_class_peek (gst_clock_return_get_type ()));
1065 g_type_class_unref (g_type_class_peek (gst_clock_entry_type_get_type ()));
1066 g_type_class_unref (g_type_class_peek (gst_clock_flags_get_type ()));
1067 g_type_class_unref (g_type_class_peek (gst_debug_graph_details_get_type ()));
1068 g_type_class_unref (g_type_class_peek (gst_state_get_type ()));
1069 g_type_class_unref (g_type_class_peek (gst_state_change_return_get_type ()));
1070 g_type_class_unref (g_type_class_peek (gst_state_change_get_type ()));
1071 g_type_class_unref (g_type_class_peek (gst_element_flags_get_type ()));
1072 g_type_class_unref (g_type_class_peek (gst_core_error_get_type ()));
1073 g_type_class_unref (g_type_class_peek (gst_library_error_get_type ()));
1074 g_type_class_unref (g_type_class_peek (gst_plugin_dependency_flags_get_type
1075 ()));
1076 g_type_class_unref (g_type_class_peek (gst_parse_flags_get_type ()));
1077 g_type_class_unref (g_type_class_peek (gst_resource_error_get_type ()));
1078 g_type_class_unref (g_type_class_peek (gst_search_mode_get_type ()));
1079 g_type_class_unref (g_type_class_peek (gst_stream_error_get_type ()));
1080 g_type_class_unref (g_type_class_peek (gst_stream_status_type_get_type ()));
1081 g_type_class_unref (g_type_class_peek (gst_structure_change_type_get_type
1082 ()));
1083 g_type_class_unref (g_type_class_peek (gst_event_type_flags_get_type ()));
1084 g_type_class_unref (g_type_class_peek (gst_event_type_get_type ()));
1085 g_type_class_unref (g_type_class_peek (gst_seek_type_get_type ()));
1086 g_type_class_unref (g_type_class_peek (gst_seek_flags_get_type ()));
1087 g_type_class_unref (g_type_class_peek (gst_qos_type_get_type ()));
1088 g_type_class_unref (g_type_class_peek (gst_format_get_type ()));
1089 g_type_class_unref (g_type_class_peek (gst_index_certainty_get_type ()));
1090 g_type_class_unref (g_type_class_peek (gst_index_entry_type_get_type ()));
1091 g_type_class_unref (g_type_class_peek (gst_index_lookup_method_get_type ()));
1092 g_type_class_unref (g_type_class_peek (gst_assoc_flags_get_type ()));
1093 g_type_class_unref (g_type_class_peek (gst_index_resolver_method_get_type
1094 ()));
1095 g_type_class_unref (g_type_class_peek (gst_index_flags_get_type ()));
1096 g_type_class_unref (g_type_class_peek (gst_debug_level_get_type ()));
1097 g_type_class_unref (g_type_class_peek (gst_debug_color_flags_get_type ()));
1098 g_type_class_unref (g_type_class_peek (gst_iterator_result_get_type ()));
1099 g_type_class_unref (g_type_class_peek (gst_iterator_item_get_type ()));
1100 g_type_class_unref (g_type_class_peek (gst_message_type_get_type ()));
1101 g_type_class_unref (g_type_class_peek (gst_mini_object_flags_get_type ()));
1102 g_type_class_unref (g_type_class_peek (gst_pad_link_return_get_type ()));
1103 g_type_class_unref (g_type_class_peek (gst_pad_link_check_get_type ()));
1104 g_type_class_unref (g_type_class_peek (gst_flow_return_get_type ()));
1105 g_type_class_unref (g_type_class_peek (gst_activate_mode_get_type ()));
1106 g_type_class_unref (g_type_class_peek (gst_pad_direction_get_type ()));
1107 g_type_class_unref (g_type_class_peek (gst_pad_flags_get_type ()));
1108 g_type_class_unref (g_type_class_peek (gst_pad_presence_get_type ()));
1109 g_type_class_unref (g_type_class_peek (gst_pad_template_flags_get_type ()));
1110 g_type_class_unref (g_type_class_peek (gst_pipeline_flags_get_type ()));
1111 g_type_class_unref (g_type_class_peek (gst_plugin_error_get_type ()));
1112 g_type_class_unref (g_type_class_peek (gst_plugin_flags_get_type ()));
1113 g_type_class_unref (g_type_class_peek (gst_rank_get_type ()));
1114 g_type_class_unref (g_type_class_peek (gst_query_type_get_type ()));
1115 g_type_class_unref (g_type_class_peek (gst_buffering_mode_get_type ()));
1116 g_type_class_unref (g_type_class_peek (gst_tag_merge_mode_get_type ()));
1117 g_type_class_unref (g_type_class_peek (gst_tag_flag_get_type ()));
1118 g_type_class_unref (g_type_class_peek (gst_task_state_get_type ()));
1119 g_type_class_unref (g_type_class_peek (gst_alloc_trace_flags_get_type ()));
1120 g_type_class_unref (g_type_class_peek (gst_type_find_probability_get_type
1121 ()));
1122 g_type_class_unref (g_type_class_peek (gst_uri_type_get_type ()));
1123 g_type_class_unref (g_type_class_peek (gst_parse_error_get_type ()));
1124 g_type_class_unref (g_type_class_peek (gst_param_spec_fraction_get_type ()));
1125 g_type_class_unref (g_type_class_peek (gst_progress_type_get_type ()));
1126 g_type_class_unref (g_type_class_peek (gst_caps_intersect_mode_get_type ()));
1128 gst_deinitialized = TRUE;
1129 GST_INFO ("deinitialized GStreamer");
1130 }
1132 /**
1133 * gst_version:
1134 * @major: (out): pointer to a guint to store the major version number
1135 * @minor: (out): pointer to a guint to store the minor version number
1136 * @micro: (out): pointer to a guint to store the micro version number
1137 * @nano: (out): pointer to a guint to store the nano version number
1138 *
1139 * Gets the version number of the GStreamer library.
1140 */
1141 void
1142 gst_version (guint * major, guint * minor, guint * micro, guint * nano)
1143 {
1144 g_return_if_fail (major);
1145 g_return_if_fail (minor);
1146 g_return_if_fail (micro);
1147 g_return_if_fail (nano);
1149 *major = GST_VERSION_MAJOR;
1150 *minor = GST_VERSION_MINOR;
1151 *micro = GST_VERSION_MICRO;
1152 *nano = GST_VERSION_NANO;
1153 }
1155 /**
1156 * gst_version_string:
1157 *
1158 * This function returns a string that is useful for describing this version
1159 * of GStreamer to the outside world: user agent strings, logging, ...
1160 *
1161 * Returns: (transfer full): a newly allocated string describing this version
1162 * of GStreamer.
1163 */
1165 gchar *
1166 gst_version_string (void)
1167 {
1168 guint major, minor, micro, nano;
1170 gst_version (&major, &minor, µ, &nano);
1171 if (nano == 0)
1172 return g_strdup_printf ("GStreamer %d.%d.%d", major, minor, micro);
1173 else if (nano == 1)
1174 return g_strdup_printf ("GStreamer %d.%d.%d (GIT)", major, minor, micro);
1175 else
1176 return g_strdup_printf ("GStreamer %d.%d.%d (prerelease)", major, minor,
1177 micro);
1178 }
1180 /**
1181 * gst_segtrap_is_enabled:
1182 *
1183 * Some functions in the GStreamer core might install a custom SIGSEGV handler
1184 * to better catch and report errors to the application. Currently this feature
1185 * is enabled by default when loading plugins.
1186 *
1187 * Applications might want to disable this behaviour with the
1188 * gst_segtrap_set_enabled() function. This is typically done if the application
1189 * wants to install its own handler without GStreamer interfering.
1190 *
1191 * Returns: %TRUE if GStreamer is allowed to install a custom SIGSEGV handler.
1192 *
1193 * Since: 0.10.10
1194 */
1195 gboolean
1196 gst_segtrap_is_enabled (void)
1197 {
1198 /* yeps, it's enabled when it's not disabled */
1199 return !_gst_disable_segtrap;
1200 }
1202 /**
1203 * gst_segtrap_set_enabled:
1204 * @enabled: whether a custom SIGSEGV handler should be installed.
1205 *
1206 * Applications might want to disable/enable the SIGSEGV handling of
1207 * the GStreamer core. See gst_segtrap_is_enabled() for more information.
1208 *
1209 * Since: 0.10.10
1210 */
1211 void
1212 gst_segtrap_set_enabled (gboolean enabled)
1213 {
1214 _gst_disable_segtrap = !enabled;
1215 }