266feed04a5bb54d80926dbf925565bf4d5e2649
1 /* GStreamer
2 * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3 * 2000 Wim Taymans <wtay@chello.be>
4 * 2003 Benjamin Otte <in7y118@public.uni-hamburg.de>
5 * Copyright (C) 2008-2009 Tim-Philipp Müller <tim centricular net>
6 *
7 * gstinfo.c: debugging functions
8 *
9 * This library is free software; you can redistribute it and/or
10 * modify it under the terms of the GNU Library General Public
11 * License as published by the Free Software Foundation; either
12 * version 2 of the License, or (at your option) any later version.
13 *
14 * This library is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
17 * Library General Public License for more details.
18 *
19 * You should have received a copy of the GNU Library General Public
20 * License along with this library; if not, write to the
21 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
22 * Boston, MA 02111-1307, USA.
23 */
25 /**
26 * SECTION:gstinfo
27 * @short_description: Debugging and logging facilities
28 * @see_also: #gstreamer-gstconfig, #gstreamer-Gst for command line parameters
29 * and environment variables that affect the debugging output.
30 *
31 * GStreamer's debugging subsystem is an easy way to get information about what
32 * the application is doing. It is not meant for programming errors. Use GLib
33 * methods (g_warning and friends) for that.
34 *
35 * The debugging subsystem works only after GStreamer has been initialized
36 * - for example by calling gst_init().
37 *
38 * The debugging subsystem is used to log informational messages while the
39 * application runs. Each messages has some properties attached to it. Among
40 * these properties are the debugging category, the severity (called "level"
41 * here) and an optional #GObject it belongs to. Each of these messages is sent
42 * to all registered debugging handlers, which then handle the messages.
43 * GStreamer attaches a default handler on startup, which outputs requested
44 * messages to stderr.
45 *
46 * Messages are output by using shortcut macros like #GST_DEBUG,
47 * #GST_CAT_ERROR_OBJECT or similar. These all expand to calling gst_debug_log()
48 * with the right parameters.
49 * The only thing a developer will probably want to do is define his own
50 * categories. This is easily done with 3 lines. At the top of your code,
51 * declare
52 * the variables and set the default category.
53 * <informalexample>
54 * <programlisting>
55 * GST_DEBUG_CATEGORY_STATIC (my_category); // define category (statically)
56 * &hash;define GST_CAT_DEFAULT my_category // set as default
57 * </programlisting>
58 * </informalexample>
59 * After that you only need to initialize the category.
60 * <informalexample>
61 * <programlisting>
62 * GST_DEBUG_CATEGORY_INIT (my_category, "my category",
63 * 0, "This is my very own");
64 * </programlisting>
65 * </informalexample>
66 * Initialization must be done before the category is used first.
67 * Plugins do this
68 * in their plugin_init function, libraries and applications should do that
69 * during their initialization.
70 *
71 * The whole debugging subsystem can be disabled at build time with passing the
72 * --disable-gst-debug switch to configure. If this is done, every function,
73 * macro and even structs described in this file evaluate to default values or
74 * nothing at all.
75 * So don't take addresses of these functions or use other tricks.
76 * If you must do that for some reason, there is still an option.
77 * If the debugging
78 * subsystem was compiled out, #GST_DISABLE_GST_DEBUG is defined in
79 * <gst/gst.h>,
80 * so you can check that before doing your trick.
81 * Disabling the debugging subsystem will give you a slight (read: unnoticeable)
82 * speed increase and will reduce the size of your compiled code. The GStreamer
83 * library itself becomes around 10% smaller.
84 *
85 * Please note that there are naming conventions for the names of debugging
86 * categories. These are explained at GST_DEBUG_CATEGORY_INIT().
87 */
89 #define GST_INFO_C
90 #include "gst_private.h"
91 #include "gstinfo.h"
93 #undef gst_debug_remove_log_function
94 #undef gst_debug_add_log_function
96 #ifndef GST_DISABLE_GST_DEBUG
98 #ifdef HAVE_DLFCN_H
99 # include <dlfcn.h>
100 #endif
101 #ifdef HAVE_PRINTF_EXTENSION
102 # include <printf.h>
103 #endif
104 #include <stdio.h> /* fprintf */
105 #include <glib/gstdio.h>
106 #include <errno.h>
107 #ifdef HAVE_UNISTD_H
108 # include <unistd.h> /* getpid on UNIX */
109 #endif
110 #ifdef HAVE_PROCESS_H
111 # include <process.h> /* getpid on win32 */
112 #endif
113 #include <string.h> /* G_VA_COPY */
114 #ifdef G_OS_WIN32
115 # define WIN32_LEAN_AND_MEAN /* prevents from including too many things */
116 # include <windows.h> /* GetStdHandle, windows console */
117 #endif
119 #include "gst_private.h"
120 #include "gstutils.h"
121 #include "gstquark.h"
122 #include "gstsegment.h"
123 #ifdef HAVE_VALGRIND_VALGRIND_H
124 # include <valgrind/valgrind.h>
125 #endif
126 #include <glib/gprintf.h> /* g_sprintf */
128 #endif /* !GST_DISABLE_GST_DEBUG */
130 /* we want these symbols exported even if debug is disabled, to maintain
131 * ABI compatibility. Unless GST_REMOVE_DISABLED is defined. */
132 #if !defined(GST_DISABLE_GST_DEBUG) || !defined(GST_REMOVE_DISABLED)
134 /* disabled by default, as soon as some threshold is set > NONE,
135 * it becomes enabled. */
136 gboolean __gst_debug_enabled = FALSE;
137 GstDebugLevel __gst_debug_min = GST_LEVEL_NONE;
139 GstDebugCategory *GST_CAT_DEFAULT = NULL;
141 GstDebugCategory *GST_CAT_GST_INIT = NULL;
142 GstDebugCategory *GST_CAT_AUTOPLUG = NULL;
143 GstDebugCategory *GST_CAT_AUTOPLUG_ATTEMPT = NULL;
144 GstDebugCategory *GST_CAT_PARENTAGE = NULL;
145 GstDebugCategory *GST_CAT_STATES = NULL;
146 GstDebugCategory *GST_CAT_SCHEDULING = NULL;
148 GstDebugCategory *GST_CAT_BUFFER = NULL;
149 GstDebugCategory *GST_CAT_BUFFER_LIST = NULL;
150 GstDebugCategory *GST_CAT_BUS = NULL;
151 GstDebugCategory *GST_CAT_CAPS = NULL;
152 GstDebugCategory *GST_CAT_CLOCK = NULL;
153 GstDebugCategory *GST_CAT_ELEMENT_PADS = NULL;
154 GstDebugCategory *GST_CAT_PADS = NULL;
155 GstDebugCategory *GST_CAT_PERFORMANCE = NULL;
156 GstDebugCategory *GST_CAT_PIPELINE = NULL;
157 GstDebugCategory *GST_CAT_PLUGIN_LOADING = NULL;
158 GstDebugCategory *GST_CAT_PLUGIN_INFO = NULL;
159 GstDebugCategory *GST_CAT_PROPERTIES = NULL;
160 GstDebugCategory *GST_CAT_TYPES = NULL;
161 GstDebugCategory *GST_CAT_XML = NULL;
162 GstDebugCategory *GST_CAT_NEGOTIATION = NULL;
163 GstDebugCategory *GST_CAT_REFCOUNTING = NULL;
164 GstDebugCategory *GST_CAT_ERROR_SYSTEM = NULL;
165 GstDebugCategory *GST_CAT_EVENT = NULL;
166 GstDebugCategory *GST_CAT_MESSAGE = NULL;
167 GstDebugCategory *GST_CAT_PARAMS = NULL;
168 GstDebugCategory *GST_CAT_CALL_TRACE = NULL;
169 GstDebugCategory *GST_CAT_SIGNAL = NULL;
170 GstDebugCategory *GST_CAT_PROBE = NULL;
171 GstDebugCategory *GST_CAT_REGISTRY = NULL;
172 GstDebugCategory *GST_CAT_QOS = NULL;
173 GstDebugCategory *_priv_GST_CAT_POLL = NULL;
176 #endif /* !defined(GST_DISABLE_GST_DEBUG) || !defined(GST_REMOVE_DISABLED) */
178 #ifndef GST_DISABLE_GST_DEBUG
180 /* underscore is to prevent conflict with GST_CAT_DEBUG define */
181 GST_DEBUG_CATEGORY_STATIC (_GST_CAT_DEBUG);
183 /* time of initialization, so we get useful debugging output times
184 * FIXME: we use this in gstdebugutils.c, what about a function + macro to
185 * get the running time: GST_DEBUG_RUNNING_TIME
186 */
187 GstClockTime _priv_gst_info_start_time;
189 #if 0
190 #if defined __sgi__
191 #include <rld_interface.h>
192 typedef struct DL_INFO
193 {
194 const char *dli_fname;
195 void *dli_fbase;
196 const char *dli_sname;
197 void *dli_saddr;
198 int dli_version;
199 int dli_reserved1;
200 long dli_reserved[4];
201 }
202 Dl_info;
204 #define _RLD_DLADDR 14
205 int dladdr (void *address, Dl_info * dl);
207 int
208 dladdr (void *address, Dl_info * dl)
209 {
210 void *v;
212 v = _rld_new_interface (_RLD_DLADDR, address, dl);
213 return (int) v;
214 }
215 #endif /* __sgi__ */
216 #endif
218 static void gst_debug_reset_threshold (gpointer category, gpointer unused);
219 static void gst_debug_reset_all_thresholds (void);
221 #ifdef HAVE_PRINTF_EXTENSION
222 static int _gst_info_printf_extension_ptr (FILE * stream,
223 const struct printf_info *info, const void *const *args);
224 static int _gst_info_printf_extension_segment (FILE * stream,
225 const struct printf_info *info, const void *const *args);
226 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
227 static int _gst_info_printf_extension_arginfo (const struct printf_info *info,
228 size_t n, int *argtypes, int *size);
229 #else
230 static int _gst_info_printf_extension_arginfo (const struct printf_info *info,
231 size_t n, int *argtypes);
232 #endif
233 #endif
235 struct _GstDebugMessage
236 {
237 gchar *message;
238 const gchar *format;
239 va_list arguments;
240 };
242 /* list of all name/level pairs from --gst-debug and GST_DEBUG */
243 static GStaticMutex __level_name_mutex = G_STATIC_MUTEX_INIT;
244 static GSList *__level_name = NULL;
245 typedef struct
246 {
247 GPatternSpec *pat;
248 GstDebugLevel level;
249 }
250 LevelNameEntry;
252 /* list of all categories */
253 static GStaticMutex __cat_mutex = G_STATIC_MUTEX_INIT;
254 static GSList *__categories = NULL;
256 /* all registered debug handlers */
257 typedef struct
258 {
259 GstLogFunction func;
260 gpointer user_data;
261 }
262 LogFuncEntry;
263 static GStaticMutex __log_func_mutex = G_STATIC_MUTEX_INIT;
264 static GSList *__log_functions = NULL;
266 #define PRETTY_TAGS_DEFAULT TRUE
267 static gboolean pretty_tags = PRETTY_TAGS_DEFAULT;
269 static volatile gint G_GNUC_MAY_ALIAS __default_level = GST_LEVEL_DEFAULT;
270 static volatile gint G_GNUC_MAY_ALIAS __use_color = 1;
272 static FILE *log_file;
274 /* FIXME: export this? */
275 gboolean
276 _priv_gst_in_valgrind (void)
277 {
278 static enum
279 {
280 GST_VG_UNCHECKED,
281 GST_VG_NO_VALGRIND,
282 GST_VG_INSIDE
283 }
284 in_valgrind = GST_VG_UNCHECKED;
286 if (in_valgrind == GST_VG_UNCHECKED) {
287 #ifdef HAVE_VALGRIND_VALGRIND_H
288 if (RUNNING_ON_VALGRIND) {
289 GST_CAT_INFO (GST_CAT_GST_INIT, "we're running inside valgrind");
290 printf ("GStreamer has detected that it is running inside valgrind.\n");
291 printf ("It might now take different code paths to ease debugging.\n");
292 printf ("Of course, this may also lead to different bugs.\n");
293 in_valgrind = GST_VG_INSIDE;
294 } else {
295 GST_CAT_LOG (GST_CAT_GST_INIT, "not doing extra valgrind stuff");
296 in_valgrind = GST_VG_NO_VALGRIND;
297 }
298 #else
299 in_valgrind = GST_VG_NO_VALGRIND;
300 #endif
301 g_assert (in_valgrind == GST_VG_NO_VALGRIND ||
302 in_valgrind == GST_VG_INSIDE);
303 }
304 return (in_valgrind == GST_VG_INSIDE);
305 }
307 /**
308 * _gst_debug_init:
309 *
310 * Initializes the debugging system.
311 * Normally you don't want to call this, because gst_init() does it for you.
312 */
313 void
314 _gst_debug_init (void)
315 {
316 const gchar *env;
318 env = g_getenv ("GST_DEBUG_FILE");
319 if (env != NULL && *env != '\0') {
320 if (strcmp (env, "-") == 0) {
321 log_file = stdout;
322 } else {
323 log_file = g_fopen (env, "w");
324 if (log_file == NULL) {
325 g_printerr ("Could not open log file '%s' for writing: %s\n", env,
326 g_strerror (errno));
327 log_file = stderr;
328 }
329 }
330 } else {
331 log_file = stderr;
332 }
334 /* get time we started for debugging messages */
335 _priv_gst_info_start_time = gst_util_get_timestamp ();
337 #ifdef HAVE_PRINTF_EXTENSION
338 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
339 register_printf_specifier (GST_PTR_FORMAT[0], _gst_info_printf_extension_ptr,
340 _gst_info_printf_extension_arginfo);
341 register_printf_specifier (GST_SEGMENT_FORMAT[0],
342 _gst_info_printf_extension_segment, _gst_info_printf_extension_arginfo);
343 #else
344 register_printf_function (GST_PTR_FORMAT[0], _gst_info_printf_extension_ptr,
345 _gst_info_printf_extension_arginfo);
346 register_printf_function (GST_SEGMENT_FORMAT[0],
347 _gst_info_printf_extension_segment, _gst_info_printf_extension_arginfo);
348 #endif
349 #endif
351 /* do NOT use a single debug function before this line has been run */
352 GST_CAT_DEFAULT = _gst_debug_category_new ("default",
353 GST_DEBUG_UNDERLINE, NULL);
354 _GST_CAT_DEBUG = _gst_debug_category_new ("GST_DEBUG",
355 GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, "debugging subsystem");
357 gst_debug_add_log_function (gst_debug_log_default, NULL);
359 /* FIXME: add descriptions here */
360 GST_CAT_GST_INIT = _gst_debug_category_new ("GST_INIT",
361 GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
362 GST_CAT_AUTOPLUG = _gst_debug_category_new ("GST_AUTOPLUG",
363 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
364 GST_CAT_AUTOPLUG_ATTEMPT = _gst_debug_category_new ("GST_AUTOPLUG_ATTEMPT",
365 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN | GST_DEBUG_BG_BLUE, NULL);
366 GST_CAT_PARENTAGE = _gst_debug_category_new ("GST_PARENTAGE",
367 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
368 GST_CAT_STATES = _gst_debug_category_new ("GST_STATES",
369 GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
370 GST_CAT_SCHEDULING = _gst_debug_category_new ("GST_SCHEDULING",
371 GST_DEBUG_BOLD | GST_DEBUG_FG_MAGENTA, NULL);
372 GST_CAT_BUFFER = _gst_debug_category_new ("GST_BUFFER",
373 GST_DEBUG_BOLD | GST_DEBUG_BG_GREEN, NULL);
374 GST_CAT_BUFFER_LIST = _gst_debug_category_new ("GST_BUFFER_LIST",
375 GST_DEBUG_BOLD | GST_DEBUG_BG_GREEN, NULL);
376 GST_CAT_BUS = _gst_debug_category_new ("GST_BUS", GST_DEBUG_BG_YELLOW, NULL);
377 GST_CAT_CAPS = _gst_debug_category_new ("GST_CAPS",
378 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
379 GST_CAT_CLOCK = _gst_debug_category_new ("GST_CLOCK",
380 GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, NULL);
381 GST_CAT_ELEMENT_PADS = _gst_debug_category_new ("GST_ELEMENT_PADS",
382 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
383 GST_CAT_PADS = _gst_debug_category_new ("GST_PADS",
384 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_RED, NULL);
385 GST_CAT_PERFORMANCE = _gst_debug_category_new ("GST_PERFORMANCE",
386 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
387 GST_CAT_PIPELINE = _gst_debug_category_new ("GST_PIPELINE",
388 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
389 GST_CAT_PLUGIN_LOADING = _gst_debug_category_new ("GST_PLUGIN_LOADING",
390 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
391 GST_CAT_PLUGIN_INFO = _gst_debug_category_new ("GST_PLUGIN_INFO",
392 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
393 GST_CAT_PROPERTIES = _gst_debug_category_new ("GST_PROPERTIES",
394 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_BLUE, NULL);
395 GST_CAT_TYPES = _gst_debug_category_new ("GST_TYPES",
396 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
397 GST_CAT_XML = _gst_debug_category_new ("GST_XML",
398 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
399 GST_CAT_NEGOTIATION = _gst_debug_category_new ("GST_NEGOTIATION",
400 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
401 GST_CAT_REFCOUNTING = _gst_debug_category_new ("GST_REFCOUNTING",
402 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_BLUE, NULL);
403 GST_CAT_ERROR_SYSTEM = _gst_debug_category_new ("GST_ERROR_SYSTEM",
404 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_WHITE, NULL);
406 GST_CAT_EVENT = _gst_debug_category_new ("GST_EVENT",
407 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
408 GST_CAT_MESSAGE = _gst_debug_category_new ("GST_MESSAGE",
409 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
410 GST_CAT_PARAMS = _gst_debug_category_new ("GST_PARAMS",
411 GST_DEBUG_BOLD | GST_DEBUG_FG_BLACK | GST_DEBUG_BG_YELLOW, NULL);
412 GST_CAT_CALL_TRACE = _gst_debug_category_new ("GST_CALL_TRACE",
413 GST_DEBUG_BOLD, NULL);
414 GST_CAT_SIGNAL = _gst_debug_category_new ("GST_SIGNAL",
415 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
416 GST_CAT_PROBE = _gst_debug_category_new ("GST_PROBE",
417 GST_DEBUG_BOLD | GST_DEBUG_FG_GREEN, "pad probes");
418 GST_CAT_REGISTRY = _gst_debug_category_new ("GST_REGISTRY", 0, "registry");
419 GST_CAT_QOS = _gst_debug_category_new ("GST_QOS", 0, "QoS");
420 _priv_GST_CAT_POLL = _gst_debug_category_new ("GST_POLL", 0, "poll");
423 /* print out the valgrind message if we're in valgrind */
424 _priv_gst_in_valgrind ();
426 env = g_getenv ("GST_DEBUG_OPTIONS");
427 if (env != NULL) {
428 if (strstr (env, "full_tags") || strstr (env, "full-tags"))
429 pretty_tags = FALSE;
430 else if (strstr (env, "pretty_tags") || strstr (env, "pretty-tags"))
431 pretty_tags = TRUE;
432 }
433 }
435 /* we can't do this further above, because we initialize the GST_CAT_DEFAULT struct */
436 #define GST_CAT_DEFAULT _GST_CAT_DEBUG
438 /**
439 * gst_debug_log:
440 * @category: category to log
441 * @level: level of the message is in
442 * @file: the file that emitted the message, usually the __FILE__ identifier
443 * @function: the function that emitted the message
444 * @line: the line from that the message was emitted, usually __LINE__
445 * @object: (transfer none) (allow-none): the object this message relates to,
446 * or NULL if none
447 * @format: a printf style format string
448 * @...: optional arguments for the format
449 *
450 * Logs the given message using the currently registered debugging handlers.
451 */
452 void
453 gst_debug_log (GstDebugCategory * category, GstDebugLevel level,
454 const gchar * file, const gchar * function, gint line,
455 GObject * object, const gchar * format, ...)
456 {
457 va_list var_args;
459 va_start (var_args, format);
460 gst_debug_log_valist (category, level, file, function, line, object, format,
461 var_args);
462 va_end (var_args);
463 }
465 #ifdef _MSC_VER
466 /* based on g_basename(), which we can't use because it was deprecated */
467 static inline const gchar *
468 gst_path_basename (const gchar * file_name)
469 {
470 register const gchar *base;
472 base = strrchr (file_name, G_DIR_SEPARATOR);
474 {
475 const gchar *q = strrchr (file_name, '/');
476 if (base == NULL || (q != NULL && q > base))
477 base = q;
478 }
480 if (base)
481 return base + 1;
483 if (g_ascii_isalpha (file_name[0]) && file_name[1] == ':')
484 return file_name + 2;
486 return file_name;
487 }
488 #endif
490 /**
491 * gst_debug_log_valist:
492 * @category: category to log
493 * @level: level of the message is in
494 * @file: the file that emitted the message, usually the __FILE__ identifier
495 * @function: the function that emitted the message
496 * @line: the line from that the message was emitted, usually __LINE__
497 * @object: (transfer none) (allow-none): the object this message relates to,
498 * or NULL if none
499 * @format: a printf style format string
500 * @args: optional arguments for the format
501 *
502 * Logs the given message using the currently registered debugging handlers.
503 */
504 void
505 gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level,
506 const gchar * file, const gchar * function, gint line,
507 GObject * object, const gchar * format, va_list args)
508 {
509 GstDebugMessage message;
510 LogFuncEntry *entry;
511 GSList *handler;
513 g_return_if_fail (category != NULL);
514 g_return_if_fail (file != NULL);
515 g_return_if_fail (function != NULL);
516 g_return_if_fail (format != NULL);
518 /* The predefined macro __FILE__ is always the exact path given to the
519 * compiler with MSVC, which may or may not be the basename. We work
520 * around it at runtime to improve the readability. */
521 #ifdef _MSC_VER
522 file = gst_path_basename (file);
523 #endif
525 message.message = NULL;
526 message.format = format;
527 G_VA_COPY (message.arguments, args);
529 handler = __log_functions;
530 while (handler) {
531 entry = handler->data;
532 handler = g_slist_next (handler);
533 entry->func (category, level, file, function, line, object, &message,
534 entry->user_data);
535 }
536 g_free (message.message);
537 va_end (message.arguments);
538 }
540 /**
541 * gst_debug_message_get:
542 * @message: a debug message
543 *
544 * Gets the string representation of a #GstDebugMessage. This function is used
545 * in debug handlers to extract the message.
546 *
547 * Returns: the string representation of a #GstDebugMessage.
548 */
549 const gchar *
550 gst_debug_message_get (GstDebugMessage * message)
551 {
552 if (message->message == NULL) {
553 message->message = g_strdup_vprintf (message->format, message->arguments);
554 }
555 return message->message;
556 }
558 #define MAX_BUFFER_DUMP_STRING_LEN 100
560 /* structure_to_pretty_string:
561 * @structure: a #GstStructure
562 *
563 * Converts @structure to a human-readable string representation. Basically
564 * the same as gst_structure_to_string(), but if the structure contains large
565 * buffers such as images the hex representation of those buffers will be
566 * shortened so that the string remains readable.
567 *
568 * Returns: a newly-allocated string. g_free() when no longer needed.
569 */
570 static gchar *
571 structure_to_pretty_string (const GstStructure * s)
572 {
573 gchar *str, *pos, *end;
575 str = gst_structure_to_string (s);
576 if (str == NULL)
577 return NULL;
579 pos = str;
580 while ((pos = strstr (pos, "(buffer)"))) {
581 guint count = 0;
583 pos += strlen ("(buffer)");
584 for (end = pos; *end != '\0' && *end != ';' && *end != ' '; ++end)
585 ++count;
586 if (count > MAX_BUFFER_DUMP_STRING_LEN) {
587 memcpy (pos + MAX_BUFFER_DUMP_STRING_LEN - 6, "..", 2);
588 memcpy (pos + MAX_BUFFER_DUMP_STRING_LEN - 4, pos + count - 4, 4);
589 g_memmove (pos + MAX_BUFFER_DUMP_STRING_LEN, pos + count,
590 strlen (pos + count) + 1);
591 pos += MAX_BUFFER_DUMP_STRING_LEN;
592 }
593 }
595 return str;
596 }
598 static inline gchar *
599 gst_info_structure_to_string (GstStructure * s)
600 {
601 if (G_UNLIKELY (pretty_tags && s->name == GST_QUARK (TAGLIST)))
602 return structure_to_pretty_string (s);
603 else
604 return gst_structure_to_string (s);
605 }
607 static gchar *
608 gst_debug_print_object (gpointer ptr)
609 {
610 GObject *object = (GObject *) ptr;
612 #ifdef unused
613 /* This is a cute trick to detect unmapped memory, but is unportable,
614 * slow, screws around with madvise, and not actually that useful. */
615 {
616 int ret;
618 ret = madvise ((void *) ((unsigned long) ptr & (~0xfff)), 4096, 0);
619 if (ret == -1 && errno == ENOMEM) {
620 buffer = g_strdup_printf ("%p (unmapped memory)", ptr);
621 }
622 }
623 #endif
625 /* nicely printed object */
626 if (object == NULL) {
627 return g_strdup ("(NULL)");
628 }
629 if (*(GType *) ptr == GST_TYPE_CAPS) {
630 return gst_caps_to_string ((GstCaps *) ptr);
631 }
632 if (*(GType *) ptr == GST_TYPE_STRUCTURE) {
633 return gst_info_structure_to_string ((GstStructure *) ptr);
634 }
635 if (GST_IS_BUFFER (ptr)) {
636 GstBuffer *buf = (GstBuffer *) ptr;
637 gchar *caps, *ret;
639 caps = gst_caps_to_string (GST_BUFFER_CAPS (buf));
640 ret =
641 g_strdup_printf ("%p, data %p, malloc %p, ts %" GST_TIME_FORMAT
642 ", dur %" GST_TIME_FORMAT ", size %u, offset %" G_GUINT64_FORMAT
643 ", offset_end %" G_GUINT64_FORMAT ", caps: %s", buf,
644 GST_BUFFER_DATA (buf), GST_BUFFER_MALLOCDATA (buf),
645 GST_TIME_ARGS (GST_BUFFER_TIMESTAMP (buf)),
646 GST_TIME_ARGS (GST_BUFFER_DURATION (buf)), GST_BUFFER_SIZE (buf),
647 GST_BUFFER_OFFSET (buf), GST_BUFFER_OFFSET_END (buf), caps);
649 g_free (caps);
650 return ret;
651 }
652 #ifdef USE_POISONING
653 if (*(guint32 *) ptr == 0xffffffff) {
654 return g_strdup_printf ("<poisoned@%p>", ptr);
655 }
656 #endif
657 if (GST_IS_PAD (object) && GST_OBJECT_NAME (object)) {
658 return g_strdup_printf ("<%s:%s>", GST_DEBUG_PAD_NAME (object));
659 }
660 if (GST_IS_OBJECT (object) && GST_OBJECT_NAME (object)) {
661 return g_strdup_printf ("<%s>", GST_OBJECT_NAME (object));
662 }
663 if (G_IS_OBJECT (object)) {
664 return g_strdup_printf ("<%s@%p>", G_OBJECT_TYPE_NAME (object), object);
665 }
666 if (GST_IS_MESSAGE (object)) {
667 GstMessage *msg = GST_MESSAGE_CAST (object);
668 gchar *s, *ret;
670 if (msg->structure) {
671 s = gst_info_structure_to_string (msg->structure);
672 } else {
673 s = g_strdup ("(NULL)");
674 }
676 ret = g_strdup_printf ("%s message from element '%s': %s",
677 GST_MESSAGE_TYPE_NAME (msg), (msg->src != NULL) ?
678 GST_ELEMENT_NAME (msg->src) : "(NULL)", s);
679 g_free (s);
680 return ret;
681 }
682 if (GST_IS_QUERY (object)) {
683 GstQuery *query = GST_QUERY_CAST (object);
685 if (query->structure) {
686 return gst_info_structure_to_string (query->structure);
687 } else {
688 const gchar *query_type_name;
690 query_type_name = gst_query_type_get_name (query->type);
691 if (G_LIKELY (query_type_name != NULL)) {
692 return g_strdup_printf ("%s query", query_type_name);
693 } else {
694 return g_strdup_printf ("query of unknown type %d", query->type);
695 }
696 }
697 }
698 if (GST_IS_EVENT (object)) {
699 GstEvent *event = GST_EVENT_CAST (object);
700 gchar *s, *ret;
702 if (event->structure) {
703 s = gst_info_structure_to_string (event->structure);
704 } else {
705 s = g_strdup ("(NULL)");
706 }
708 ret = g_strdup_printf ("%s event from '%s' at time %"
709 GST_TIME_FORMAT ": %s",
710 GST_EVENT_TYPE_NAME (event), (event->src != NULL) ?
711 GST_OBJECT_NAME (event->src) : "(NULL)",
712 GST_TIME_ARGS (event->timestamp), s);
713 g_free (s);
714 return ret;
715 }
717 return g_strdup_printf ("%p", ptr);
718 }
720 #ifdef HAVE_PRINTF_EXTENSION
722 static gchar *
723 gst_debug_print_segment (gpointer ptr)
724 {
725 GstSegment *segment = (GstSegment *) ptr;
727 /* nicely printed segment */
728 if (segment == NULL) {
729 return g_strdup ("(NULL)");
730 }
732 switch (segment->format) {
733 case GST_FORMAT_UNDEFINED:{
734 return g_strdup_printf ("UNDEFINED segment");
735 }
736 case GST_FORMAT_TIME:{
737 return g_strdup_printf ("time segment start=%" GST_TIME_FORMAT
738 ", stop=%" GST_TIME_FORMAT ", last_stop=%" GST_TIME_FORMAT
739 ", duration=%" GST_TIME_FORMAT ", rate=%f, applied_rate=%f"
740 ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
741 GST_TIME_ARGS (segment->start), GST_TIME_ARGS (segment->stop),
742 GST_TIME_ARGS (segment->last_stop), GST_TIME_ARGS (segment->duration),
743 segment->rate, segment->applied_rate, (guint) segment->flags,
744 GST_TIME_ARGS (segment->time), GST_TIME_ARGS (segment->accum));
745 }
746 default:{
747 const gchar *format_name;
749 format_name = gst_format_get_name (segment->format);
750 if (G_UNLIKELY (format_name == NULL))
751 format_name = "(UNKNOWN FORMAT)";
752 return g_strdup_printf ("%s segment start=%" G_GINT64_FORMAT
753 ", stop=%" G_GINT64_FORMAT ", last_stop=%" G_GINT64_FORMAT
754 ", duration=%" G_GINT64_FORMAT ", rate=%f, applied_rate=%f"
755 ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
756 format_name, segment->start, segment->stop, segment->last_stop,
757 segment->duration, segment->rate, segment->applied_rate,
758 (guint) segment->flags, GST_TIME_ARGS (segment->time),
759 GST_TIME_ARGS (segment->accum));
760 }
761 }
762 }
764 #endif /* HAVE_PRINTF_EXTENSION */
766 /**
767 * gst_debug_construct_term_color:
768 * @colorinfo: the color info
769 *
770 * Constructs a string that can be used for getting the desired color in color
771 * terminals.
772 * You need to free the string after use.
773 *
774 * Returns: (transfer full) (type gchar*): a string containing the color
775 * definition
776 */
777 gchar *
778 gst_debug_construct_term_color (guint colorinfo)
779 {
780 GString *color;
782 color = g_string_new ("\033[00");
784 if (colorinfo & GST_DEBUG_BOLD) {
785 g_string_append_len (color, ";01", 3);
786 }
787 if (colorinfo & GST_DEBUG_UNDERLINE) {
788 g_string_append_len (color, ";04", 3);
789 }
790 if (colorinfo & GST_DEBUG_FG_MASK) {
791 g_string_append_printf (color, ";3%1d", colorinfo & GST_DEBUG_FG_MASK);
792 }
793 if (colorinfo & GST_DEBUG_BG_MASK) {
794 g_string_append_printf (color, ";4%1d",
795 (colorinfo & GST_DEBUG_BG_MASK) >> 4);
796 }
797 g_string_append_c (color, 'm');
799 return g_string_free (color, FALSE);
800 }
802 /**
803 * gst_debug_construct_win_color:
804 * @colorinfo: the color info
805 *
806 * Constructs an integer that can be used for getting the desired color in
807 * windows' terminals (cmd.exe). As there is no mean to underline, we simply
808 * ignore this attribute.
809 *
810 * This function returns 0 on non-windows machines.
811 *
812 * Returns: an integer containing the color definition
813 *
814 * Since: 0.10.23
815 */
816 gint
817 gst_debug_construct_win_color (guint colorinfo)
818 {
819 gint color = 0;
820 #ifdef G_OS_WIN32
821 static const guchar ansi_to_win_fg[8] = {
822 0, /* black */
823 FOREGROUND_RED, /* red */
824 FOREGROUND_GREEN, /* green */
825 FOREGROUND_RED | FOREGROUND_GREEN, /* yellow */
826 FOREGROUND_BLUE, /* blue */
827 FOREGROUND_RED | FOREGROUND_BLUE, /* magenta */
828 FOREGROUND_GREEN | FOREGROUND_BLUE, /* cyan */
829 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE /* white */
830 };
831 static const guchar ansi_to_win_bg[8] = {
832 0,
833 BACKGROUND_RED,
834 BACKGROUND_GREEN,
835 BACKGROUND_RED | BACKGROUND_GREEN,
836 BACKGROUND_BLUE,
837 BACKGROUND_RED | BACKGROUND_BLUE,
838 BACKGROUND_GREEN | FOREGROUND_BLUE,
839 BACKGROUND_RED | BACKGROUND_GREEN | BACKGROUND_BLUE
840 };
842 /* we draw black as white, as cmd.exe can only have black bg */
843 if (colorinfo == 0) {
844 return ansi_to_win_fg[7];
845 }
847 if (colorinfo & GST_DEBUG_BOLD) {
848 color |= FOREGROUND_INTENSITY;
849 }
850 if (colorinfo & GST_DEBUG_FG_MASK) {
851 color |= ansi_to_win_fg[colorinfo & GST_DEBUG_FG_MASK];
852 }
853 if (colorinfo & GST_DEBUG_BG_MASK) {
854 color |= ansi_to_win_bg[(colorinfo & GST_DEBUG_BG_MASK) >> 4];
855 }
856 #endif
857 return color;
858 }
860 /* width of %p varies depending on actual value of pointer, which can make
861 * output unevenly aligned if multiple threads are involved, hence the %14p
862 * (should really be %18p, but %14p seems a good compromise between too many
863 * white spaces and likely unalignment on my system) */
864 #if defined (GLIB_SIZEOF_VOID_P) && GLIB_SIZEOF_VOID_P == 8
865 #define PTR_FMT "%14p"
866 #else
867 #define PTR_FMT "%10p"
868 #endif
869 #define PID_FMT "%5d"
870 #define CAT_FMT "%20s %s:%d:%s:%s"
872 #ifdef G_OS_WIN32
873 static const guchar levelcolormap[GST_LEVEL_COUNT] = {
874 /* GST_LEVEL_NONE */
875 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
876 /* GST_LEVEL_ERROR */
877 FOREGROUND_RED | FOREGROUND_INTENSITY,
878 /* GST_LEVEL_WARNING */
879 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_INTENSITY,
880 /* GST_LEVEL_INFO */
881 FOREGROUND_GREEN | FOREGROUND_INTENSITY,
882 /* GST_LEVEL_DEBUG */
883 FOREGROUND_GREEN | FOREGROUND_BLUE,
884 /* GST_LEVEL_LOG */
885 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
886 /* GST_LEVEL_FIXME */
887 FOREGROUND_RED | FOREGROUND_GREEN,
888 /* GST_LEVEL_TRACE */
889 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
890 /* placeholder for log level 8 */
891 0,
892 /* GST_LEVEL_MEMDUMP */
893 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE
894 };
896 static const guchar available_colors[] = {
897 FOREGROUND_RED, FOREGROUND_GREEN, FOREGROUND_RED | FOREGROUND_GREEN,
898 FOREGROUND_BLUE, FOREGROUND_RED | FOREGROUND_BLUE,
899 FOREGROUND_GREEN | FOREGROUND_BLUE,
900 };
901 #else
902 static const gchar *levelcolormap[GST_LEVEL_COUNT] = {
903 "\033[37m", /* GST_LEVEL_NONE */
904 "\033[31;01m", /* GST_LEVEL_ERROR */
905 "\033[33;01m", /* GST_LEVEL_WARNING */
906 "\033[32;01m", /* GST_LEVEL_INFO */
907 "\033[36m", /* GST_LEVEL_DEBUG */
908 "\033[37m", /* GST_LEVEL_LOG */
909 "\033[33;01m", /* GST_LEVEL_FIXME */
910 "\033[37m", /* GST_LEVEL_TRACE */
911 "\033[37m", /* placeholder for log level 8 */
912 "\033[37m" /* GST_LEVEL_MEMDUMP */
913 };
914 #endif
916 /**
917 * gst_debug_log_default:
918 * @category: category to log
919 * @level: level of the message
920 * @file: the file that emitted the message, usually the __FILE__ identifier
921 * @function: the function that emitted the message
922 * @line: the line from that the message was emitted, usually __LINE__
923 * @message: the actual message
924 * @object: (transfer none) (allow-none): the object this message relates to,
925 * or NULL if none
926 * @unused: an unused variable, reserved for some user_data.
927 *
928 * The default logging handler used by GStreamer. Logging functions get called
929 * whenever a macro like GST_DEBUG or similar is used. This function outputs the
930 * message and additional info to stderr (or the log file specified via the
931 * GST_DEBUG_FILE environment variable).
932 *
933 * You can add other handlers by using gst_debug_add_log_function().
934 * And you can remove this handler by calling
935 * gst_debug_remove_log_function(gst_debug_log_default);
936 */
937 void
938 gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level,
939 const gchar * file, const gchar * function, gint line,
940 GObject * object, GstDebugMessage * message, gpointer unused)
941 {
942 gint pid;
943 GstClockTime elapsed;
944 gchar *obj = NULL;
945 gboolean is_colored;
947 if (level > gst_debug_category_get_threshold (category))
948 return;
950 pid = getpid ();
951 is_colored = gst_debug_is_colored ();
953 if (object) {
954 obj = gst_debug_print_object (object);
955 } else {
956 obj = g_strdup ("");
957 }
959 elapsed = GST_CLOCK_DIFF (_priv_gst_info_start_time,
960 gst_util_get_timestamp ());
962 if (is_colored) {
963 #ifndef G_OS_WIN32
964 /* colors, non-windows */
965 gchar *color = NULL;
966 const gchar *clear;
967 gchar pidcolor[10];
968 const gchar *levelcolor;
970 color = gst_debug_construct_term_color (gst_debug_category_get_color
971 (category));
972 clear = "\033[00m";
973 g_sprintf (pidcolor, "\033[3%1dm", pid % 6 + 31);
974 levelcolor = levelcolormap[level];
976 #define PRINT_FMT " %s"PID_FMT"%s "PTR_FMT" %s%s%s %s"CAT_FMT"%s %s\n"
977 fprintf (log_file, "%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed),
978 pidcolor, pid, clear, g_thread_self (), levelcolor,
979 gst_debug_level_get_name (level), clear, color,
980 gst_debug_category_get_name (category), file, line, function, obj,
981 clear, gst_debug_message_get (message));
982 fflush (log_file);
983 #undef PRINT_FMT
984 g_free (color);
985 #else
986 /* colors, windows. We take a lock to keep colors and content together.
987 * Maybe there is a better way but for now this will do the right
988 * thing. */
989 static GStaticMutex win_print_mutex = G_STATIC_MUTEX_INIT;
990 const gint clear = FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE;
991 #define SET_COLOR(c) G_STMT_START { \
992 if (log_file == stderr) \
993 SetConsoleTextAttribute (GetStdHandle (STD_ERROR_HANDLE), (c)); \
994 } G_STMT_END
995 g_static_mutex_lock (&win_print_mutex);
996 /* timestamp */
997 fprintf (log_file, "%" GST_TIME_FORMAT " ", GST_TIME_ARGS (elapsed));
998 fflush (log_file);
999 /* pid */
1000 SET_COLOR (available_colors[pid % G_N_ELEMENTS (available_colors)]);
1001 fprintf (log_file, PID_FMT, pid);
1002 fflush (log_file);
1003 /* thread */
1004 SET_COLOR (clear);
1005 fprintf (log_file, " " PTR_FMT " ", g_thread_self ());
1006 fflush (log_file);
1007 /* level */
1008 SET_COLOR (levelcolormap[level]);
1009 fprintf (log_file, "%s ", gst_debug_level_get_name (level));
1010 fflush (log_file);
1011 /* category */
1012 SET_COLOR (gst_debug_construct_win_color (gst_debug_category_get_color
1013 (category)));
1014 fprintf (log_file, CAT_FMT, gst_debug_category_get_name (category),
1015 file, line, function, obj);
1016 fflush (log_file);
1017 /* message */
1018 SET_COLOR (clear);
1019 fprintf (log_file, " %s\n", gst_debug_message_get (message));
1020 fflush (log_file);
1021 g_static_mutex_unlock (&win_print_mutex);
1022 #endif
1023 } else {
1024 /* no color, all platforms */
1025 #define PRINT_FMT " "PID_FMT" "PTR_FMT" %s "CAT_FMT" %s\n"
1026 fprintf (log_file, "%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed),
1027 pid, g_thread_self (), gst_debug_level_get_name (level),
1028 gst_debug_category_get_name (category), file, line, function, obj,
1029 gst_debug_message_get (message));
1030 fflush (log_file);
1031 #undef PRINT_FMT
1032 }
1034 g_free (obj);
1035 }
1037 /**
1038 * gst_debug_level_get_name:
1039 * @level: the level to get the name for
1040 *
1041 * Get the string representation of a debugging level
1042 *
1043 * Returns: the name
1044 */
1045 const gchar *
1046 gst_debug_level_get_name (GstDebugLevel level)
1047 {
1048 switch (level) {
1049 case GST_LEVEL_NONE:
1050 return "";
1051 case GST_LEVEL_ERROR:
1052 return "ERROR ";
1053 case GST_LEVEL_WARNING:
1054 return "WARN ";
1055 case GST_LEVEL_INFO:
1056 return "INFO ";
1057 case GST_LEVEL_DEBUG:
1058 return "DEBUG ";
1059 case GST_LEVEL_LOG:
1060 return "LOG ";
1061 case GST_LEVEL_FIXME:
1062 return "FIXME ";
1063 case GST_LEVEL_TRACE:
1064 return "TRACE ";
1065 case GST_LEVEL_MEMDUMP:
1066 return "MEMDUMP";
1067 default:
1068 g_warning ("invalid level specified for gst_debug_level_get_name");
1069 return "";
1070 }
1071 }
1073 /**
1074 * gst_debug_add_log_function:
1075 * @func: the function to use
1076 * @data: (closure): user data
1077 *
1078 * Adds the logging function to the list of logging functions.
1079 * Be sure to use #G_GNUC_NO_INSTRUMENT on that function, it is needed.
1080 */
1081 void
1082 gst_debug_add_log_function (GstLogFunction func, gpointer data)
1083 {
1084 LogFuncEntry *entry;
1085 GSList *list;
1087 if (func == NULL)
1088 func = gst_debug_log_default;
1090 entry = g_slice_new (LogFuncEntry);
1091 entry->func = func;
1092 entry->user_data = data;
1093 /* FIXME: we leak the old list here - other threads might access it right now
1094 * in gst_debug_logv. Another solution is to lock the mutex in gst_debug_logv,
1095 * but that is waaay costly.
1096 * It'd probably be clever to use some kind of RCU here, but I don't know
1097 * anything about that.
1098 */
1099 g_static_mutex_lock (&__log_func_mutex);
1100 list = g_slist_copy (__log_functions);
1101 __log_functions = g_slist_prepend (list, entry);
1102 g_static_mutex_unlock (&__log_func_mutex);
1104 GST_DEBUG ("prepended log function %p (user data %p) to log functions",
1105 func, data);
1106 }
1108 static gint
1109 gst_debug_compare_log_function_by_func (gconstpointer entry, gconstpointer func)
1110 {
1111 gpointer entryfunc = (gpointer) (((LogFuncEntry *) entry)->func);
1113 return (entryfunc < func) ? -1 : (entryfunc > func) ? 1 : 0;
1114 }
1116 static gint
1117 gst_debug_compare_log_function_by_data (gconstpointer entry, gconstpointer data)
1118 {
1119 gpointer entrydata = ((LogFuncEntry *) entry)->user_data;
1121 return (entrydata < data) ? -1 : (entrydata > data) ? 1 : 0;
1122 }
1124 static guint
1125 gst_debug_remove_with_compare_func (GCompareFunc func, gpointer data)
1126 {
1127 GSList *found;
1128 GSList *new;
1129 guint removals = 0;
1131 g_static_mutex_lock (&__log_func_mutex);
1132 new = __log_functions;
1133 while ((found = g_slist_find_custom (new, data, func))) {
1134 if (new == __log_functions) {
1135 /* make a copy when we have the first hit, so that we modify the copy and
1136 * make that the new list later */
1137 new = g_slist_copy (new);
1138 continue;
1139 }
1140 g_slice_free (LogFuncEntry, found->data);
1141 new = g_slist_delete_link (new, found);
1142 removals++;
1143 }
1144 /* FIXME: We leak the old list here. See _add_log_function for why. */
1145 __log_functions = new;
1146 g_static_mutex_unlock (&__log_func_mutex);
1148 return removals;
1149 }
1151 /**
1152 * gst_debug_remove_log_function:
1153 * @func: the log function to remove
1154 *
1155 * Removes all registered instances of the given logging functions.
1156 *
1157 * Returns: How many instances of the function were removed
1158 */
1159 guint
1160 gst_debug_remove_log_function (GstLogFunction func)
1161 {
1162 guint removals;
1164 if (func == NULL)
1165 func = gst_debug_log_default;
1167 removals =
1168 gst_debug_remove_with_compare_func
1169 (gst_debug_compare_log_function_by_func, (gpointer) func);
1170 GST_DEBUG ("removed log function %p %d times from log function list", func,
1171 removals);
1173 return removals;
1174 }
1176 /**
1177 * gst_debug_remove_log_function_by_data:
1178 * @data: user data of the log function to remove
1179 *
1180 * Removes all registered instances of log functions with the given user data.
1181 *
1182 * Returns: How many instances of the function were removed
1183 */
1184 guint
1185 gst_debug_remove_log_function_by_data (gpointer data)
1186 {
1187 guint removals;
1189 removals =
1190 gst_debug_remove_with_compare_func
1191 (gst_debug_compare_log_function_by_data, data);
1192 GST_DEBUG
1193 ("removed %d log functions with user data %p from log function list",
1194 removals, data);
1196 return removals;
1197 }
1199 /**
1200 * gst_debug_set_colored:
1201 * @colored: Whether to use colored output or not
1202 *
1203 * Sets or unsets the use of coloured debugging output.
1204 *
1205 * This function may be called before gst_init().
1206 */
1207 void
1208 gst_debug_set_colored (gboolean colored)
1209 {
1210 g_atomic_int_set (&__use_color, (gint) colored);
1211 }
1213 /**
1214 * gst_debug_is_colored:
1215 *
1216 * Checks if the debugging output should be colored.
1217 *
1218 * Returns: TRUE, if the debug output should be colored.
1219 */
1220 gboolean
1221 gst_debug_is_colored (void)
1222 {
1223 return (gboolean) g_atomic_int_get (&__use_color);
1224 }
1226 /**
1227 * gst_debug_set_active:
1228 * @active: Whether to use debugging output or not
1229 *
1230 * If activated, debugging messages are sent to the debugging
1231 * handlers.
1232 * It makes sense to deactivate it for speed issues.
1233 * <note><para>This function is not threadsafe. It makes sense to only call it
1234 * during initialization.</para></note>
1235 */
1236 void
1237 gst_debug_set_active (gboolean active)
1238 {
1239 __gst_debug_enabled = active;
1240 if (active)
1241 __gst_debug_min = GST_LEVEL_COUNT;
1242 else
1243 __gst_debug_min = GST_LEVEL_NONE;
1244 }
1246 /**
1247 * gst_debug_is_active:
1248 *
1249 * Checks if debugging output is activated.
1250 *
1251 * Returns: TRUE, if debugging is activated
1252 */
1253 gboolean
1254 gst_debug_is_active (void)
1255 {
1256 return __gst_debug_enabled;
1257 }
1259 /**
1260 * gst_debug_set_default_threshold:
1261 * @level: level to set
1262 *
1263 * Sets the default threshold to the given level and updates all categories to
1264 * use this threshold.
1265 *
1266 * This function may be called before gst_init().
1267 */
1268 void
1269 gst_debug_set_default_threshold (GstDebugLevel level)
1270 {
1271 g_atomic_int_set (&__default_level, level);
1272 gst_debug_reset_all_thresholds ();
1273 }
1275 /**
1276 * gst_debug_get_default_threshold:
1277 *
1278 * Returns the default threshold that is used for new categories.
1279 *
1280 * Returns: the default threshold level
1281 */
1282 GstDebugLevel
1283 gst_debug_get_default_threshold (void)
1284 {
1285 return (GstDebugLevel) g_atomic_int_get (&__default_level);
1286 }
1288 static void
1289 gst_debug_reset_threshold (gpointer category, gpointer unused)
1290 {
1291 GstDebugCategory *cat = (GstDebugCategory *) category;
1292 GSList *walk;
1294 g_static_mutex_lock (&__level_name_mutex);
1295 walk = __level_name;
1296 while (walk) {
1297 LevelNameEntry *entry = walk->data;
1299 walk = g_slist_next (walk);
1300 if (g_pattern_match_string (entry->pat, cat->name)) {
1301 GST_LOG ("category %s matches pattern %p - gets set to level %d",
1302 cat->name, entry->pat, entry->level);
1303 gst_debug_category_set_threshold (cat, entry->level);
1304 goto exit;
1305 }
1306 }
1307 gst_debug_category_set_threshold (cat, gst_debug_get_default_threshold ());
1309 exit:
1310 g_static_mutex_unlock (&__level_name_mutex);
1311 }
1313 static void
1314 gst_debug_reset_all_thresholds (void)
1315 {
1316 g_static_mutex_lock (&__cat_mutex);
1317 g_slist_foreach (__categories, gst_debug_reset_threshold, NULL);
1318 g_static_mutex_unlock (&__cat_mutex);
1319 }
1321 static void
1322 for_each_threshold_by_entry (gpointer data, gpointer user_data)
1323 {
1324 GstDebugCategory *cat = (GstDebugCategory *) data;
1325 LevelNameEntry *entry = (LevelNameEntry *) user_data;
1327 if (g_pattern_match_string (entry->pat, cat->name)) {
1328 GST_LOG ("category %s matches pattern %p - gets set to level %d",
1329 cat->name, entry->pat, entry->level);
1330 gst_debug_category_set_threshold (cat, entry->level);
1331 }
1332 }
1334 /**
1335 * gst_debug_set_threshold_for_name:
1336 * @name: name of the categories to set
1337 * @level: level to set them to
1338 *
1339 * Sets all categories which match the given glob style pattern to the given
1340 * level.
1341 */
1342 void
1343 gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level)
1344 {
1345 GPatternSpec *pat;
1346 LevelNameEntry *entry;
1348 g_return_if_fail (name != NULL);
1350 pat = g_pattern_spec_new (name);
1351 entry = g_slice_new (LevelNameEntry);
1352 entry->pat = pat;
1353 entry->level = level;
1354 g_static_mutex_lock (&__level_name_mutex);
1355 __level_name = g_slist_prepend (__level_name, entry);
1356 g_static_mutex_unlock (&__level_name_mutex);
1357 g_static_mutex_lock (&__cat_mutex);
1358 g_slist_foreach (__categories, for_each_threshold_by_entry, entry);
1359 g_static_mutex_unlock (&__cat_mutex);
1360 }
1362 /**
1363 * gst_debug_unset_threshold_for_name:
1364 * @name: name of the categories to set
1365 *
1366 * Resets all categories with the given name back to the default level.
1367 */
1368 void
1369 gst_debug_unset_threshold_for_name (const gchar * name)
1370 {
1371 GSList *walk;
1372 GPatternSpec *pat;
1374 g_return_if_fail (name != NULL);
1376 pat = g_pattern_spec_new (name);
1377 g_static_mutex_lock (&__level_name_mutex);
1378 walk = __level_name;
1379 /* improve this if you want, it's mighty slow */
1380 while (walk) {
1381 LevelNameEntry *entry = walk->data;
1383 if (g_pattern_spec_equal (entry->pat, pat)) {
1384 __level_name = g_slist_remove_link (__level_name, walk);
1385 g_pattern_spec_free (entry->pat);
1386 g_slice_free (LevelNameEntry, entry);
1387 g_slist_free_1 (walk);
1388 walk = __level_name;
1389 }
1390 }
1391 g_static_mutex_unlock (&__level_name_mutex);
1392 g_pattern_spec_free (pat);
1393 gst_debug_reset_all_thresholds ();
1394 }
1396 GstDebugCategory *
1397 _gst_debug_category_new (const gchar * name, guint color,
1398 const gchar * description)
1399 {
1400 GstDebugCategory *cat;
1402 g_return_val_if_fail (name != NULL, NULL);
1404 cat = g_slice_new (GstDebugCategory);
1405 cat->name = g_strdup (name);
1406 cat->color = color;
1407 if (description != NULL) {
1408 cat->description = g_strdup (description);
1409 } else {
1410 cat->description = g_strdup ("no description");
1411 }
1412 g_atomic_int_set (&cat->threshold, 0);
1413 gst_debug_reset_threshold (cat, NULL);
1415 /* add to category list */
1416 g_static_mutex_lock (&__cat_mutex);
1417 __categories = g_slist_prepend (__categories, cat);
1418 g_static_mutex_unlock (&__cat_mutex);
1420 return cat;
1421 }
1423 /**
1424 * gst_debug_category_free:
1425 * @category: #GstDebugCategory to free.
1426 *
1427 * Removes and frees the category and all associated resources.
1428 */
1429 void
1430 gst_debug_category_free (GstDebugCategory * category)
1431 {
1432 if (category == NULL)
1433 return;
1435 /* remove from category list */
1436 g_static_mutex_lock (&__cat_mutex);
1437 __categories = g_slist_remove (__categories, category);
1438 g_static_mutex_unlock (&__cat_mutex);
1440 g_free ((gpointer) category->name);
1441 g_free ((gpointer) category->description);
1442 g_slice_free (GstDebugCategory, category);
1443 }
1445 /**
1446 * gst_debug_category_set_threshold:
1447 * @category: a #GstDebugCategory to set threshold of.
1448 * @level: the #GstDebugLevel threshold to set.
1449 *
1450 * Sets the threshold of the category to the given level. Debug information will
1451 * only be output if the threshold is lower or equal to the level of the
1452 * debugging message.
1453 * <note><para>
1454 * Do not use this function in production code, because other functions may
1455 * change the threshold of categories as side effect. It is however a nice
1456 * function to use when debugging (even from gdb).
1457 * </para></note>
1458 */
1459 void
1460 gst_debug_category_set_threshold (GstDebugCategory * category,
1461 GstDebugLevel level)
1462 {
1463 g_return_if_fail (category != NULL);
1465 if (level > __gst_debug_min) {
1466 __gst_debug_enabled = TRUE;
1467 __gst_debug_min = level;
1468 }
1470 g_atomic_int_set (&category->threshold, level);
1471 }
1473 /**
1474 * gst_debug_category_reset_threshold:
1475 * @category: a #GstDebugCategory to reset threshold of.
1476 *
1477 * Resets the threshold of the category to the default level. Debug information
1478 * will only be output if the threshold is lower or equal to the level of the
1479 * debugging message.
1480 * Use this function to set the threshold back to where it was after using
1481 * gst_debug_category_set_threshold().
1482 */
1483 void
1484 gst_debug_category_reset_threshold (GstDebugCategory * category)
1485 {
1486 gst_debug_reset_threshold (category, NULL);
1487 }
1489 /**
1490 * gst_debug_category_get_threshold:
1491 * @category: a #GstDebugCategory to get threshold of.
1492 *
1493 * Returns the threshold of a #GstDebugCategory.
1494 *
1495 * Returns: the #GstDebugLevel that is used as threshold.
1496 */
1497 GstDebugLevel
1498 gst_debug_category_get_threshold (GstDebugCategory * category)
1499 {
1500 return (GstDebugLevel) g_atomic_int_get (&category->threshold);
1501 }
1503 /**
1504 * gst_debug_category_get_name:
1505 * @category: a #GstDebugCategory to get name of.
1506 *
1507 * Returns the name of a debug category.
1508 *
1509 * Returns: the name of the category.
1510 */
1511 const gchar *
1512 gst_debug_category_get_name (GstDebugCategory * category)
1513 {
1514 return category->name;
1515 }
1517 /**
1518 * gst_debug_category_get_color:
1519 * @category: a #GstDebugCategory to get the color of.
1520 *
1521 * Returns the color of a debug category used when printing output in this
1522 * category.
1523 *
1524 * Returns: the color of the category.
1525 */
1526 guint
1527 gst_debug_category_get_color (GstDebugCategory * category)
1528 {
1529 return category->color;
1530 }
1532 /**
1533 * gst_debug_category_get_description:
1534 * @category: a #GstDebugCategory to get the description of.
1535 *
1536 * Returns the description of a debug category.
1537 *
1538 * Returns: the description of the category.
1539 */
1540 const gchar *
1541 gst_debug_category_get_description (GstDebugCategory * category)
1542 {
1543 return category->description;
1544 }
1546 /**
1547 * gst_debug_get_all_categories:
1548 *
1549 * Returns a snapshot of a all categories that are currently in use . This list
1550 * may change anytime.
1551 * The caller has to free the list after use.
1552 *
1553 * Returns: (transfer container) (element-type Gst.DebugCategory): the list of
1554 * debug categories
1555 */
1556 GSList *
1557 gst_debug_get_all_categories (void)
1558 {
1559 GSList *ret;
1561 g_static_mutex_lock (&__cat_mutex);
1562 ret = g_slist_copy (__categories);
1563 g_static_mutex_unlock (&__cat_mutex);
1565 return ret;
1566 }
1568 GstDebugCategory *
1569 _gst_debug_get_category (const gchar * name)
1570 {
1571 GstDebugCategory *ret = NULL;
1572 GSList *node;
1574 for (node = __categories; node; node = g_slist_next (node)) {
1575 ret = (GstDebugCategory *) node->data;
1576 if (!strcmp (name, ret->name)) {
1577 return ret;
1578 }
1579 }
1580 return NULL;
1581 }
1583 /*** FUNCTION POINTERS ********************************************************/
1585 static GHashTable *__gst_function_pointers; /* NULL */
1586 static GStaticMutex __dbg_functions_mutex = G_STATIC_MUTEX_INIT;
1588 /* This function MUST NOT return NULL */
1589 const gchar *
1590 _gst_debug_nameof_funcptr (GstDebugFuncPtr func)
1591 {
1592 gchar *ptrname;
1594 #ifdef HAVE_DLADDR
1595 Dl_info dl_info;
1596 #endif
1598 if (G_UNLIKELY (func == NULL))
1599 return "(NULL)";
1601 g_static_mutex_lock (&__dbg_functions_mutex);
1602 if (G_LIKELY (__gst_function_pointers)) {
1603 ptrname = g_hash_table_lookup (__gst_function_pointers, (gpointer) func);
1604 g_static_mutex_unlock (&__dbg_functions_mutex);
1605 if (G_LIKELY (ptrname))
1606 return ptrname;
1607 } else {
1608 g_static_mutex_unlock (&__dbg_functions_mutex);
1609 }
1610 /* we need to create an entry in the hash table for this one so we don't leak
1611 * the name */
1612 #ifdef HAVE_DLADDR
1613 if (dladdr ((gpointer) func, &dl_info) && dl_info.dli_sname) {
1614 gchar *name = g_strdup (dl_info.dli_sname);
1616 _gst_debug_register_funcptr (func, name);
1617 return name;
1618 } else
1619 #endif
1620 {
1621 gchar *name = g_strdup_printf ("%p", (gpointer) func);
1623 _gst_debug_register_funcptr (func, name);
1624 return name;
1625 }
1626 }
1628 void
1629 _gst_debug_register_funcptr (GstDebugFuncPtr func, const gchar * ptrname)
1630 {
1631 gpointer ptr = (gpointer) func;
1633 g_static_mutex_lock (&__dbg_functions_mutex);
1635 if (!__gst_function_pointers)
1636 __gst_function_pointers = g_hash_table_new (g_direct_hash, g_direct_equal);
1637 if (!g_hash_table_lookup (__gst_function_pointers, ptr))
1638 g_hash_table_insert (__gst_function_pointers, ptr, (gpointer) ptrname);
1640 g_static_mutex_unlock (&__dbg_functions_mutex);
1641 }
1643 /*** PRINTF EXTENSIONS ********************************************************/
1645 #ifdef HAVE_PRINTF_EXTENSION
1646 static int
1647 _gst_info_printf_extension_ptr (FILE * stream, const struct printf_info *info,
1648 const void *const *args)
1649 {
1650 char *buffer;
1651 int len;
1652 void *ptr;
1654 buffer = NULL;
1655 ptr = *(void **) args[0];
1657 buffer = gst_debug_print_object (ptr);
1658 len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1659 buffer);
1661 g_free (buffer);
1662 return len;
1663 }
1665 static int
1666 _gst_info_printf_extension_segment (FILE * stream,
1667 const struct printf_info *info, const void *const *args)
1668 {
1669 char *buffer;
1670 int len;
1671 void *ptr;
1673 buffer = NULL;
1674 ptr = *(void **) args[0];
1676 buffer = gst_debug_print_segment (ptr);
1677 len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1678 buffer);
1680 g_free (buffer);
1681 return len;
1682 }
1684 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
1685 static int
1686 _gst_info_printf_extension_arginfo (const struct printf_info *info, size_t n,
1687 int *argtypes, int *size)
1688 #else
1689 static int
1690 _gst_info_printf_extension_arginfo (const struct printf_info *info, size_t n,
1691 int *argtypes)
1692 #endif
1693 {
1694 if (n > 0) {
1695 argtypes[0] = PA_POINTER;
1696 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
1697 *size = sizeof (gpointer);
1698 #endif
1699 }
1700 return 1;
1701 }
1702 #endif /* HAVE_PRINTF_EXTENSION */
1704 static void
1705 gst_info_dump_mem_line (gchar * linebuf, gsize linebuf_size,
1706 const guint8 * mem, gsize mem_offset, gsize mem_size)
1707 {
1708 gchar hexstr[50], ascstr[18], digitstr[4];
1710 if (mem_size > 16)
1711 mem_size = 16;
1713 hexstr[0] = '\0';
1714 ascstr[0] = '\0';
1716 if (mem != NULL) {
1717 guint i = 0;
1719 mem += mem_offset;
1720 while (i < mem_size) {
1721 ascstr[i] = (g_ascii_isprint (mem[i])) ? mem[i] : '.';
1722 g_snprintf (digitstr, sizeof (digitstr), "%02x ", mem[i]);
1723 g_strlcat (hexstr, digitstr, sizeof (hexstr));
1724 ++i;
1725 }
1726 ascstr[i] = '\0';
1727 }
1729 g_snprintf (linebuf, linebuf_size, "%08x: %-48.48s %-16.16s",
1730 (guint) mem_offset, hexstr, ascstr);
1731 }
1733 void
1734 _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
1735 const gchar * func, gint line, GObject * obj, const gchar * msg,
1736 const guint8 * data, guint length)
1737 {
1738 guint off = 0;
1740 gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "--------"
1741 "-------------------------------------------------------------------");
1743 if (msg != NULL && *msg != '\0') {
1744 gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "%s", msg);
1745 }
1747 while (off < length) {
1748 gchar buf[128];
1750 /* gst_info_dump_mem_line will process 16 bytes at most */
1751 gst_info_dump_mem_line (buf, sizeof (buf), data, off, length - off);
1752 gst_debug_log (cat, GST_LEVEL_MEMDUMP, file, func, line, obj, "%s", buf);
1753 off += 16;
1754 }
1756 gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "--------"
1757 "-------------------------------------------------------------------");
1758 }
1760 #else /* !GST_DISABLE_GST_DEBUG */
1761 #ifndef GST_REMOVE_DISABLED
1763 GstDebugCategory *
1764 _gst_debug_category_new (const gchar * name, guint color,
1765 const gchar * description)
1766 {
1767 return NULL;
1768 }
1770 void
1771 _gst_debug_register_funcptr (GstDebugFuncPtr func, const gchar * ptrname)
1772 {
1773 }
1775 /* This function MUST NOT return NULL */
1776 const gchar *
1777 _gst_debug_nameof_funcptr (GstDebugFuncPtr func)
1778 {
1779 return "(NULL)";
1780 }
1782 void
1783 gst_debug_log (GstDebugCategory * category, GstDebugLevel level,
1784 const gchar * file, const gchar * function, gint line,
1785 GObject * object, const gchar * format, ...)
1786 {
1787 }
1789 void
1790 gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level,
1791 const gchar * file, const gchar * function, gint line,
1792 GObject * object, const gchar * format, va_list args)
1793 {
1794 }
1796 const gchar *
1797 gst_debug_message_get (GstDebugMessage * message)
1798 {
1799 return "";
1800 }
1802 void
1803 gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level,
1804 const gchar * file, const gchar * function, gint line,
1805 GObject * object, GstDebugMessage * message, gpointer unused)
1806 {
1807 }
1809 const gchar *
1810 gst_debug_level_get_name (GstDebugLevel level)
1811 {
1812 return "NONE";
1813 }
1815 void
1816 gst_debug_add_log_function (GstLogFunction func, gpointer data)
1817 {
1818 }
1820 guint
1821 gst_debug_remove_log_function (GstLogFunction func)
1822 {
1823 return 0;
1824 }
1826 guint
1827 gst_debug_remove_log_function_by_data (gpointer data)
1828 {
1829 return 0;
1830 }
1832 void
1833 gst_debug_set_active (gboolean active)
1834 {
1835 }
1837 gboolean
1838 gst_debug_is_active (void)
1839 {
1840 return FALSE;
1841 }
1843 void
1844 gst_debug_set_colored (gboolean colored)
1845 {
1846 }
1848 gboolean
1849 gst_debug_is_colored (void)
1850 {
1851 return FALSE;
1852 }
1854 void
1855 gst_debug_set_default_threshold (GstDebugLevel level)
1856 {
1857 }
1859 GstDebugLevel
1860 gst_debug_get_default_threshold (void)
1861 {
1862 return GST_LEVEL_NONE;
1863 }
1865 void
1866 gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level)
1867 {
1868 }
1870 void
1871 gst_debug_unset_threshold_for_name (const gchar * name)
1872 {
1873 }
1875 void
1876 gst_debug_category_free (GstDebugCategory * category)
1877 {
1878 }
1880 void
1881 gst_debug_category_set_threshold (GstDebugCategory * category,
1882 GstDebugLevel level)
1883 {
1884 }
1886 void
1887 gst_debug_category_reset_threshold (GstDebugCategory * category)
1888 {
1889 }
1891 GstDebugLevel
1892 gst_debug_category_get_threshold (GstDebugCategory * category)
1893 {
1894 return GST_LEVEL_NONE;
1895 }
1897 const gchar *
1898 gst_debug_category_get_name (GstDebugCategory * category)
1899 {
1900 return "";
1901 }
1903 guint
1904 gst_debug_category_get_color (GstDebugCategory * category)
1905 {
1906 return 0;
1907 }
1909 const gchar *
1910 gst_debug_category_get_description (GstDebugCategory * category)
1911 {
1912 return "";
1913 }
1915 GSList *
1916 gst_debug_get_all_categories (void)
1917 {
1918 return NULL;
1919 }
1921 GstDebugCategory *
1922 _gst_debug_get_category (const gchar * name)
1923 {
1924 return NULL;
1925 }
1927 gchar *
1928 gst_debug_construct_term_color (guint colorinfo)
1929 {
1930 return g_strdup ("00");
1931 }
1933 gint
1934 gst_debug_construct_win_color (guint colorinfo)
1935 {
1936 return 0;
1937 }
1939 gboolean
1940 _priv_gst_in_valgrind (void)
1941 {
1942 return FALSE;
1943 }
1945 void
1946 _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
1947 const gchar * func, gint line, GObject * obj, const gchar * msg,
1948 const guint8 * data, guint length)
1949 {
1950 }
1951 #endif /* GST_REMOVE_DISABLED */
1952 #endif /* GST_DISABLE_GST_DEBUG */
1955 #ifdef GST_ENABLE_FUNC_INSTRUMENTATION
1956 /* FIXME make this thread specific */
1957 static GSList *stack_trace = NULL;
1959 void
1960 __cyg_profile_func_enter (void *this_fn, void *call_site)
1961 G_GNUC_NO_INSTRUMENT;
1962 void __cyg_profile_func_enter (void *this_fn, void *call_site)
1963 {
1964 gchar *name = _gst_debug_nameof_funcptr (this_fn);
1965 gchar *site = _gst_debug_nameof_funcptr (call_site);
1967 GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "entering function %s from %s", name,
1968 site);
1969 stack_trace =
1970 g_slist_prepend (stack_trace, g_strdup_printf ("%8p in %s from %p (%s)",
1971 this_fn, name, call_site, site));
1973 g_free (name);
1974 g_free (site);
1975 }
1977 void
1978 __cyg_profile_func_exit (void *this_fn, void *call_site)
1979 G_GNUC_NO_INSTRUMENT;
1980 void __cyg_profile_func_exit (void *this_fn, void *call_site)
1981 {
1982 gchar *name = _gst_debug_nameof_funcptr (this_fn);
1984 GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "leaving function %s", name);
1985 g_free (stack_trace->data);
1986 stack_trace = g_slist_delete_link (stack_trace, stack_trace);
1988 g_free (name);
1989 }
1991 /**
1992 * gst_debug_print_stack_trace:
1993 *
1994 * If GST_ENABLE_FUNC_INSTRUMENTATION is defined a stacktrace is available for
1995 * gstreamer code, which can be printed with this function.
1996 */
1997 void
1998 gst_debug_print_stack_trace (void)
1999 {
2000 GSList *walk = stack_trace;
2001 gint count = 0;
2003 if (walk)
2004 walk = g_slist_next (walk);
2006 while (walk) {
2007 gchar *name = (gchar *) walk->data;
2009 g_print ("#%-2d %s\n", count++, name);
2011 walk = g_slist_next (walk);
2012 }
2013 }
2014 #else
2015 void
2016 gst_debug_print_stack_trace (void)
2017 {
2018 /* nothing because it's compiled out */
2019 }
2021 #endif /* GST_ENABLE_FUNC_INSTRUMENTATION */