1 /* GStreamer
2 * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3 * 2000 Wim Taymans <wtay@chello.be>
4 * 2003 Benjamin Otte <in7y118@public.uni-hamburg.de>
5 * Copyright (C) 2008-2009 Tim-Philipp Müller <tim centricular net>
6 *
7 * gstinfo.c: debugging functions
8 *
9 * This library is free software; you can redistribute it and/or
10 * modify it under the terms of the GNU Library General Public
11 * License as published by the Free Software Foundation; either
12 * version 2 of the License, or (at your option) any later version.
13 *
14 * This library is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
17 * Library General Public License for more details.
18 *
19 * You should have received a copy of the GNU Library General Public
20 * License along with this library; if not, write to the
21 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
22 * Boston, MA 02111-1307, USA.
23 */
25 /**
26 * SECTION:gstinfo
27 * @short_description: Debugging and logging facilities
28 * @see_also: #GstConfig, #Gst for command line parameters
29 * and environment variables that affect the debugging output.
30 *
31 * GStreamer's debugging subsystem is an easy way to get information about what
32 * the application is doing. It is not meant for programming errors. Use GLib
33 * methods (g_warning and friends) for that.
34 *
35 * The debugging subsystem works only after GStreamer has been initialized
36 * - for example by calling gst_init().
37 *
38 * The debugging subsystem is used to log informational messages while the
39 * application runs. Each messages has some properties attached to it. Among
40 * these properties are the debugging category, the severity (called "level"
41 * here) and an optional #GObject it belongs to. Each of these messages is sent
42 * to all registered debugging handlers, which then handle the messages.
43 * GStreamer attaches a default handler on startup, which outputs requested
44 * messages to stderr.
45 *
46 * Messages are output by using shortcut macros like #GST_DEBUG,
47 * #GST_CAT_ERROR_OBJECT or similar. These all expand to calling gst_debug_log()
48 * with the right parameters.
49 * The only thing a developer will probably want to do is define his own
50 * categories. This is easily done with 3 lines. At the top of your code,
51 * declare
52 * the variables and set the default category.
53 * <informalexample>
54 * <programlisting>
55 * GST_DEBUG_CATEGORY_STATIC (my_category); // define category (statically)
56 * &hash;define GST_CAT_DEFAULT my_category // set as default
57 * </programlisting>
58 * </informalexample>
59 * After that you only need to initialize the category.
60 * <informalexample>
61 * <programlisting>
62 * GST_DEBUG_CATEGORY_INIT (my_category, "my category",
63 * 0, "This is my very own");
64 * </programlisting>
65 * </informalexample>
66 * Initialization must be done before the category is used first.
67 * Plugins do this
68 * in their plugin_init function, libraries and applications should do that
69 * during their initialization.
70 *
71 * The whole debugging subsystem can be disabled at build time with passing the
72 * --disable-gst-debug switch to configure. If this is done, every function,
73 * macro and even structs described in this file evaluate to default values or
74 * nothing at all.
75 * So don't take addresses of these functions or use other tricks.
76 * If you must do that for some reason, there is still an option.
77 * If the debugging
78 * subsystem was compiled out, #GST_DISABLE_GST_DEBUG is defined in
79 * <gst/gst.h>,
80 * so you can check that before doing your trick.
81 * Disabling the debugging subsystem will give you a slight (read: unnoticeable)
82 * speed increase and will reduce the size of your compiled code. The GStreamer
83 * library itself becomes around 10% smaller.
84 *
85 * Please note that there are naming conventions for the names of debugging
86 * categories. These are explained at GST_DEBUG_CATEGORY_INIT().
87 */
89 #define GST_INFO_C
90 #include "gst_private.h"
91 #include "gstinfo.h"
93 #ifndef GST_DISABLE_GST_DEBUG
95 #ifdef HAVE_DLFCN_H
96 # include <dlfcn.h>
97 #endif
98 #ifdef HAVE_PRINTF_EXTENSION
99 # include <printf.h>
100 #endif
101 #include <stdio.h> /* fprintf */
102 #ifdef HAVE_UNISTD_H
103 # include <unistd.h> /* getpid on UNIX */
104 #endif
105 #ifdef HAVE_PROCESS_H
106 # include <process.h> /* getpid on win32 */
107 #endif
108 #include <string.h> /* G_VA_COPY */
109 #ifdef G_OS_WIN32
110 # define WIN32_LEAN_AND_MEAN /* prevents from including too many things */
111 # include <windows.h> /* GetStdHandle, windows console */
112 #endif
114 #include "gst_private.h"
115 #include "gstutils.h"
116 #include "gstquark.h"
117 #include "gstsegment.h"
118 #ifdef HAVE_VALGRIND_H
119 # include <valgrind/valgrind.h>
120 #endif
121 #include <glib/gprintf.h> /* g_sprintf */
123 #endif /* !GST_DISABLE_GST_DEBUG */
125 /* we want these symbols exported even if debug is disabled, to maintain
126 * ABI compatibility. Unless GST_REMOVE_DISABLED is defined. */
127 #if !defined(GST_DISABLE_GST_DEBUG) || !defined(GST_REMOVE_DISABLED)
129 /* disabled by default, as soon as some threshold is set > NONE,
130 * it becomes enabled. */
131 gboolean __gst_debug_enabled = FALSE;
132 GstDebugLevel __gst_debug_min = GST_LEVEL_NONE;
134 GstDebugCategory *GST_CAT_DEFAULT = NULL;
136 GstDebugCategory *GST_CAT_GST_INIT = NULL;
137 GstDebugCategory *GST_CAT_AUTOPLUG = NULL;
138 GstDebugCategory *GST_CAT_AUTOPLUG_ATTEMPT = NULL;
139 GstDebugCategory *GST_CAT_PARENTAGE = NULL;
140 GstDebugCategory *GST_CAT_STATES = NULL;
141 GstDebugCategory *GST_CAT_SCHEDULING = NULL;
143 GstDebugCategory *GST_CAT_BUFFER = NULL;
144 GstDebugCategory *GST_CAT_BUFFER_LIST = NULL;
145 GstDebugCategory *GST_CAT_BUS = NULL;
146 GstDebugCategory *GST_CAT_CAPS = NULL;
147 GstDebugCategory *GST_CAT_CLOCK = NULL;
148 GstDebugCategory *GST_CAT_ELEMENT_PADS = NULL;
149 GstDebugCategory *GST_CAT_PADS = NULL;
150 GstDebugCategory *GST_CAT_PERFORMANCE = NULL;
151 GstDebugCategory *GST_CAT_PIPELINE = NULL;
152 GstDebugCategory *GST_CAT_PLUGIN_LOADING = NULL;
153 GstDebugCategory *GST_CAT_PLUGIN_INFO = NULL;
154 GstDebugCategory *GST_CAT_PROPERTIES = NULL;
155 GstDebugCategory *GST_CAT_TYPES = NULL;
156 GstDebugCategory *GST_CAT_XML = NULL;
157 GstDebugCategory *GST_CAT_NEGOTIATION = NULL;
158 GstDebugCategory *GST_CAT_REFCOUNTING = NULL;
159 GstDebugCategory *GST_CAT_ERROR_SYSTEM = NULL;
160 GstDebugCategory *GST_CAT_EVENT = NULL;
161 GstDebugCategory *GST_CAT_MESSAGE = NULL;
162 GstDebugCategory *GST_CAT_PARAMS = NULL;
163 GstDebugCategory *GST_CAT_CALL_TRACE = NULL;
164 GstDebugCategory *GST_CAT_SIGNAL = NULL;
165 GstDebugCategory *GST_CAT_PROBE = NULL;
166 GstDebugCategory *GST_CAT_REGISTRY = NULL;
167 GstDebugCategory *GST_CAT_QOS = NULL;
169 #endif /* !defined(GST_DISABLE_GST_DEBUG) || !defined(GST_REMOVE_DISABLED) */
171 #ifndef GST_DISABLE_GST_DEBUG
173 /* underscore is to prevent conflict with GST_CAT_DEBUG define */
174 GST_DEBUG_CATEGORY_STATIC (_GST_CAT_DEBUG);
176 /* time of initialization, so we get useful debugging output times
177 * FIXME: we use this in gstdebugutils.c, what about a function + macro to
178 * get the running time: GST_DEBUG_RUNNING_TIME
179 */
180 GstClockTime _priv_gst_info_start_time;
182 #if 0
183 #if defined __sgi__
184 #include <rld_interface.h>
185 typedef struct DL_INFO
186 {
187 const char *dli_fname;
188 void *dli_fbase;
189 const char *dli_sname;
190 void *dli_saddr;
191 int dli_version;
192 int dli_reserved1;
193 long dli_reserved[4];
194 }
195 Dl_info;
197 #define _RLD_DLADDR 14
198 int dladdr (void *address, Dl_info * dl);
200 int
201 dladdr (void *address, Dl_info * dl)
202 {
203 void *v;
205 v = _rld_new_interface (_RLD_DLADDR, address, dl);
206 return (int) v;
207 }
208 #endif /* __sgi__ */
209 #endif
211 static void gst_debug_reset_threshold (gpointer category, gpointer unused);
212 static void gst_debug_reset_all_thresholds (void);
214 #ifdef HAVE_PRINTF_EXTENSION
215 static int _gst_info_printf_extension_ptr (FILE * stream,
216 const struct printf_info *info, const void *const *args);
217 static int _gst_info_printf_extension_segment (FILE * stream,
218 const struct printf_info *info, const void *const *args);
219 #if HAVE_REGISTER_PRINTF_SPECIFIER
220 static int _gst_info_printf_extension_arginfo (const struct printf_info *info,
221 size_t n, int *argtypes, int *size);
222 #else
223 static int _gst_info_printf_extension_arginfo (const struct printf_info *info,
224 size_t n, int *argtypes);
225 #endif
226 #endif
228 struct _GstDebugMessage
229 {
230 gchar *message;
231 const gchar *format;
232 va_list arguments;
233 };
235 /* list of all name/level pairs from --gst-debug and GST_DEBUG */
236 static GStaticMutex __level_name_mutex = G_STATIC_MUTEX_INIT;
237 static GSList *__level_name = NULL;
238 typedef struct
239 {
240 GPatternSpec *pat;
241 GstDebugLevel level;
242 }
243 LevelNameEntry;
245 /* list of all categories */
246 static GStaticMutex __cat_mutex = G_STATIC_MUTEX_INIT;
247 static GSList *__categories = NULL;
249 /* all registered debug handlers */
250 typedef struct
251 {
252 GstLogFunction func;
253 gpointer user_data;
254 }
255 LogFuncEntry;
256 static GStaticMutex __log_func_mutex = G_STATIC_MUTEX_INIT;
257 static GSList *__log_functions = NULL;
259 #define PRETTY_TAGS_DEFAULT TRUE
260 static gboolean pretty_tags = PRETTY_TAGS_DEFAULT;
262 static gint __default_level;
263 static gint __use_color;
265 /* FIXME: export this? */
266 gboolean
267 _priv_gst_in_valgrind (void)
268 {
269 static enum
270 {
271 GST_VG_UNCHECKED,
272 GST_VG_NO_VALGRIND,
273 GST_VG_INSIDE
274 }
275 in_valgrind = GST_VG_UNCHECKED;
277 if (in_valgrind == GST_VG_UNCHECKED) {
278 #ifdef HAVE_VALGRIND_H
279 if (RUNNING_ON_VALGRIND) {
280 GST_CAT_INFO (GST_CAT_GST_INIT, "we're running inside valgrind");
281 printf ("GStreamer has detected that it is running inside valgrind.\n");
282 printf ("It might now take different code paths to ease debugging.\n");
283 printf ("Of course, this may also lead to different bugs.\n");
284 in_valgrind = GST_VG_INSIDE;
285 } else {
286 GST_CAT_LOG (GST_CAT_GST_INIT, "not doing extra valgrind stuff");
287 in_valgrind = GST_VG_NO_VALGRIND;
288 }
289 #else
290 in_valgrind = GST_VG_NO_VALGRIND;
291 #endif
292 g_assert (in_valgrind == GST_VG_NO_VALGRIND ||
293 in_valgrind == GST_VG_INSIDE);
294 }
295 return (in_valgrind == GST_VG_INSIDE) ? TRUE : FALSE;
296 }
298 /**
299 * _gst_debug_init:
300 *
301 * Initializes the debugging system.
302 * Normally you don't want to call this, because gst_init() does it for you.
303 */
304 void
305 _gst_debug_init (void)
306 {
307 const gchar *env;
309 g_atomic_int_set (&__default_level, GST_LEVEL_DEFAULT);
310 g_atomic_int_set (&__use_color, 1);
312 /* get time we started for debugging messages */
313 _priv_gst_info_start_time = gst_util_get_timestamp ();
315 #ifdef HAVE_PRINTF_EXTENSION
316 #if HAVE_REGISTER_PRINTF_SPECIFIER
317 register_printf_specifier (GST_PTR_FORMAT[0], _gst_info_printf_extension_ptr,
318 _gst_info_printf_extension_arginfo);
319 register_printf_specifier (GST_SEGMENT_FORMAT[0],
320 _gst_info_printf_extension_segment, _gst_info_printf_extension_arginfo);
321 #else
322 register_printf_function (GST_PTR_FORMAT[0], _gst_info_printf_extension_ptr,
323 _gst_info_printf_extension_arginfo);
324 register_printf_function (GST_SEGMENT_FORMAT[0],
325 _gst_info_printf_extension_segment, _gst_info_printf_extension_arginfo);
326 #endif
327 #endif
329 /* do NOT use a single debug function before this line has been run */
330 GST_CAT_DEFAULT = _gst_debug_category_new ("default",
331 GST_DEBUG_UNDERLINE, NULL);
332 _GST_CAT_DEBUG = _gst_debug_category_new ("GST_DEBUG",
333 GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, "debugging subsystem");
335 gst_debug_add_log_function (gst_debug_log_default, NULL);
337 /* FIXME: add descriptions here */
338 GST_CAT_GST_INIT = _gst_debug_category_new ("GST_INIT",
339 GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
340 GST_CAT_AUTOPLUG = _gst_debug_category_new ("GST_AUTOPLUG",
341 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
342 GST_CAT_AUTOPLUG_ATTEMPT = _gst_debug_category_new ("GST_AUTOPLUG_ATTEMPT",
343 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN | GST_DEBUG_BG_BLUE, NULL);
344 GST_CAT_PARENTAGE = _gst_debug_category_new ("GST_PARENTAGE",
345 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
346 GST_CAT_STATES = _gst_debug_category_new ("GST_STATES",
347 GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
348 GST_CAT_SCHEDULING = _gst_debug_category_new ("GST_SCHEDULING",
349 GST_DEBUG_BOLD | GST_DEBUG_FG_MAGENTA, NULL);
350 GST_CAT_BUFFER = _gst_debug_category_new ("GST_BUFFER",
351 GST_DEBUG_BOLD | GST_DEBUG_BG_GREEN, NULL);
352 GST_CAT_BUFFER_LIST = _gst_debug_category_new ("GST_BUFFER_LIST",
353 GST_DEBUG_BOLD | GST_DEBUG_BG_GREEN, NULL);
354 GST_CAT_BUS = _gst_debug_category_new ("GST_BUS", GST_DEBUG_BG_YELLOW, NULL);
355 GST_CAT_CAPS = _gst_debug_category_new ("GST_CAPS",
356 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
357 GST_CAT_CLOCK = _gst_debug_category_new ("GST_CLOCK",
358 GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, NULL);
359 GST_CAT_ELEMENT_PADS = _gst_debug_category_new ("GST_ELEMENT_PADS",
360 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
361 GST_CAT_PADS = _gst_debug_category_new ("GST_PADS",
362 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_RED, NULL);
363 GST_CAT_PERFORMANCE = _gst_debug_category_new ("GST_PERFORMANCE",
364 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
365 GST_CAT_PIPELINE = _gst_debug_category_new ("GST_PIPELINE",
366 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
367 GST_CAT_PLUGIN_LOADING = _gst_debug_category_new ("GST_PLUGIN_LOADING",
368 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
369 GST_CAT_PLUGIN_INFO = _gst_debug_category_new ("GST_PLUGIN_INFO",
370 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
371 GST_CAT_PROPERTIES = _gst_debug_category_new ("GST_PROPERTIES",
372 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_BLUE, NULL);
373 GST_CAT_TYPES = _gst_debug_category_new ("GST_TYPES",
374 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
375 GST_CAT_XML = _gst_debug_category_new ("GST_XML",
376 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
377 GST_CAT_NEGOTIATION = _gst_debug_category_new ("GST_NEGOTIATION",
378 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
379 GST_CAT_REFCOUNTING = _gst_debug_category_new ("GST_REFCOUNTING",
380 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_BLUE, NULL);
381 GST_CAT_ERROR_SYSTEM = _gst_debug_category_new ("GST_ERROR_SYSTEM",
382 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_WHITE, NULL);
384 GST_CAT_EVENT = _gst_debug_category_new ("GST_EVENT",
385 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
386 GST_CAT_MESSAGE = _gst_debug_category_new ("GST_MESSAGE",
387 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
388 GST_CAT_PARAMS = _gst_debug_category_new ("GST_PARAMS",
389 GST_DEBUG_BOLD | GST_DEBUG_FG_BLACK | GST_DEBUG_BG_YELLOW, NULL);
390 GST_CAT_CALL_TRACE = _gst_debug_category_new ("GST_CALL_TRACE",
391 GST_DEBUG_BOLD, NULL);
392 GST_CAT_SIGNAL = _gst_debug_category_new ("GST_SIGNAL",
393 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
394 GST_CAT_PROBE = _gst_debug_category_new ("GST_PROBE",
395 GST_DEBUG_BOLD | GST_DEBUG_FG_GREEN, "pad probes");
396 GST_CAT_REGISTRY = _gst_debug_category_new ("GST_REGISTRY", 0, "registry");
397 GST_CAT_QOS = _gst_debug_category_new ("GST_QOS", 0, "QoS");
400 /* print out the valgrind message if we're in valgrind */
401 _priv_gst_in_valgrind ();
403 env = g_getenv ("GST_DEBUG_OPTIONS");
404 if (env != NULL) {
405 if (strstr (env, "full_tags") || strstr (env, "full-tags"))
406 pretty_tags = FALSE;
407 else if (strstr (env, "pretty_tags") || strstr (env, "pretty-tags"))
408 pretty_tags = TRUE;
409 }
410 }
412 /* we can't do this further above, because we initialize the GST_CAT_DEFAULT struct */
413 #define GST_CAT_DEFAULT _GST_CAT_DEBUG
415 /**
416 * gst_debug_log:
417 * @category: category to log
418 * @level: level of the message is in
419 * @file: the file that emitted the message, usually the __FILE__ identifier
420 * @function: the function that emitted the message
421 * @line: the line from that the message was emitted, usually __LINE__
422 * @object: the object this message relates to or NULL if none
423 * @format: a printf style format string
424 * @...: optional arguments for the format
425 *
426 * Logs the given message using the currently registered debugging handlers.
427 */
428 void
429 gst_debug_log (GstDebugCategory * category, GstDebugLevel level,
430 const gchar * file, const gchar * function, gint line,
431 GObject * object, const gchar * format, ...)
432 {
433 va_list var_args;
435 va_start (var_args, format);
436 gst_debug_log_valist (category, level, file, function, line, object, format,
437 var_args);
438 va_end (var_args);
439 }
441 /**
442 * gst_debug_log_valist:
443 * @category: category to log
444 * @level: level of the message is in
445 * @file: the file that emitted the message, usually the __FILE__ identifier
446 * @function: the function that emitted the message
447 * @line: the line from that the message was emitted, usually __LINE__
448 * @object: the object this message relates to or NULL if none
449 * @format: a printf style format string
450 * @args: optional arguments for the format
451 *
452 * Logs the given message using the currently registered debugging handlers.
453 */
454 void
455 gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level,
456 const gchar * file, const gchar * function, gint line,
457 GObject * object, const gchar * format, va_list args)
458 {
459 GstDebugMessage message;
460 LogFuncEntry *entry;
461 GSList *handler;
463 #ifdef _MSC_VER
464 gchar *file_basename;
465 #endif
467 g_return_if_fail (category != NULL);
468 g_return_if_fail (file != NULL);
469 g_return_if_fail (function != NULL);
470 g_return_if_fail (format != NULL);
472 #ifdef _MSC_VER
473 /*
474 * The predefined macro __FILE__ is always the exact path given to the
475 * compiler with MSVC, which may or may not be the basename. We work
476 * around it at runtime to improve the readability.
477 */
478 file = file_basename = g_path_get_basename (file);
479 #endif
481 message.message = NULL;
482 message.format = format;
483 G_VA_COPY (message.arguments, args);
485 handler = __log_functions;
486 while (handler) {
487 entry = handler->data;
488 handler = g_slist_next (handler);
489 entry->func (category, level, file, function, line, object, &message,
490 entry->user_data);
491 }
492 g_free (message.message);
493 va_end (message.arguments);
495 #ifdef _MSC_VER
496 g_free (file_basename);
497 #endif
498 }
500 /**
501 * gst_debug_message_get:
502 * @message: a debug message
503 *
504 * Gets the string representation of a #GstDebugMessage. This function is used
505 * in debug handlers to extract the message.
506 *
507 * Returns: the string representation of a #GstDebugMessage.
508 */
509 const gchar *
510 gst_debug_message_get (GstDebugMessage * message)
511 {
512 if (message->message == NULL) {
513 message->message = g_strdup_vprintf (message->format, message->arguments);
514 }
515 return message->message;
516 }
518 #define MAX_BUFFER_DUMP_STRING_LEN 100
520 /* structure_to_pretty_string:
521 * @structure: a #GstStructure
522 *
523 * Converts @structure to a human-readable string representation. Basically
524 * the same as gst_structure_to_string(), but if the structure contains large
525 * buffers such as images the hex representation of those buffers will be
526 * shortened so that the string remains readable.
527 *
528 * Returns: a newly-allocated string. g_free() when no longer needed.
529 */
530 static gchar *
531 structure_to_pretty_string (const GstStructure * s)
532 {
533 gchar *str, *pos, *end;
535 str = gst_structure_to_string (s);
536 if (str == NULL)
537 return NULL;
539 pos = str;
540 while ((pos = strstr (pos, "(buffer)"))) {
541 guint count = 0;
543 pos += strlen ("(buffer)");
544 for (end = pos; *end != '\0' && *end != ';' && *end != ' '; ++end)
545 ++count;
546 if (count > MAX_BUFFER_DUMP_STRING_LEN) {
547 memcpy (pos + MAX_BUFFER_DUMP_STRING_LEN - 6, "..", 2);
548 memcpy (pos + MAX_BUFFER_DUMP_STRING_LEN - 4, pos + count - 4, 4);
549 g_memmove (pos + MAX_BUFFER_DUMP_STRING_LEN, pos + count,
550 strlen (pos + count) + 1);
551 pos += MAX_BUFFER_DUMP_STRING_LEN;
552 }
553 }
555 return str;
556 }
558 static inline gchar *
559 gst_info_structure_to_string (GstStructure * s)
560 {
561 if (G_UNLIKELY (pretty_tags && s->name == GST_QUARK (TAGLIST)))
562 return structure_to_pretty_string (s);
563 else
564 return gst_structure_to_string (s);
565 }
567 static gchar *
568 gst_debug_print_object (gpointer ptr)
569 {
570 GObject *object = (GObject *) ptr;
572 #ifdef unused
573 /* This is a cute trick to detect unmapped memory, but is unportable,
574 * slow, screws around with madvise, and not actually that useful. */
575 {
576 int ret;
578 ret = madvise ((void *) ((unsigned long) ptr & (~0xfff)), 4096, 0);
579 if (ret == -1 && errno == ENOMEM) {
580 buffer = g_strdup_printf ("%p (unmapped memory)", ptr);
581 }
582 }
583 #endif
585 /* nicely printed object */
586 if (object == NULL) {
587 return g_strdup ("(NULL)");
588 }
589 if (*(GType *) ptr == GST_TYPE_CAPS) {
590 return gst_caps_to_string ((GstCaps *) ptr);
591 }
592 if (*(GType *) ptr == GST_TYPE_STRUCTURE) {
593 return gst_info_structure_to_string ((GstStructure *) ptr);
594 }
595 #ifdef USE_POISONING
596 if (*(guint32 *) ptr == 0xffffffff) {
597 return g_strdup_printf ("<poisoned@%p>", ptr);
598 }
599 #endif
600 if (GST_IS_PAD (object) && GST_OBJECT_NAME (object)) {
601 return g_strdup_printf ("<%s:%s>", GST_DEBUG_PAD_NAME (object));
602 }
603 if (GST_IS_OBJECT (object) && GST_OBJECT_NAME (object)) {
604 return g_strdup_printf ("<%s>", GST_OBJECT_NAME (object));
605 }
606 if (G_IS_OBJECT (object)) {
607 return g_strdup_printf ("<%s@%p>", G_OBJECT_TYPE_NAME (object), object);
608 }
609 if (GST_IS_MESSAGE (object)) {
610 GstMessage *msg = GST_MESSAGE_CAST (object);
611 gchar *s, *ret;
613 if (msg->structure) {
614 s = gst_info_structure_to_string (msg->structure);
615 } else {
616 s = g_strdup ("(NULL)");
617 }
619 ret = g_strdup_printf ("%s message from element '%s': %s",
620 GST_MESSAGE_TYPE_NAME (msg), (msg->src != NULL) ?
621 GST_ELEMENT_NAME (msg->src) : "(NULL)", s);
622 g_free (s);
623 return ret;
624 }
625 if (GST_IS_QUERY (object)) {
626 GstQuery *query = GST_QUERY_CAST (object);
628 if (query->structure) {
629 return gst_info_structure_to_string (query->structure);
630 } else {
631 const gchar *query_type_name;
633 query_type_name = gst_query_type_get_name (query->type);
634 if (G_LIKELY (query_type_name != NULL)) {
635 return g_strdup_printf ("%s query", query_type_name);
636 } else {
637 return g_strdup_printf ("query of unknown type %d", query->type);
638 }
639 }
640 }
642 return g_strdup_printf ("%p", ptr);
643 }
645 #ifdef HAVE_PRINTF_EXTENSION
647 static gchar *
648 gst_debug_print_segment (gpointer ptr)
649 {
650 GstSegment *segment = (GstSegment *) ptr;
652 /* nicely printed segment */
653 if (segment == NULL) {
654 return g_strdup ("(NULL)");
655 }
657 switch (segment->format) {
658 case GST_FORMAT_UNDEFINED:{
659 return g_strdup_printf ("UNDEFINED segment");
660 }
661 case GST_FORMAT_TIME:{
662 return g_strdup_printf ("time segment start=%" GST_TIME_FORMAT
663 ", stop=%" GST_TIME_FORMAT ", last_stop=%" GST_TIME_FORMAT
664 ", duration=%" GST_TIME_FORMAT ", rate=%f, applied_rate=%f"
665 ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
666 GST_TIME_ARGS (segment->start), GST_TIME_ARGS (segment->stop),
667 GST_TIME_ARGS (segment->last_stop), GST_TIME_ARGS (segment->duration),
668 segment->rate, segment->applied_rate, (guint) segment->flags,
669 GST_TIME_ARGS (segment->time), GST_TIME_ARGS (segment->accum));
670 }
671 default:{
672 const gchar *format_name;
674 format_name = gst_format_get_name (segment->format);
675 if (G_UNLIKELY (format_name == NULL))
676 format_name = "(UNKNOWN FORMAT)";
677 return g_strdup_printf ("%s segment start=%" G_GINT64_FORMAT
678 ", stop=%" G_GINT64_FORMAT ", last_stop=%" G_GINT64_FORMAT
679 ", duration=%" G_GINT64_FORMAT ", rate=%f, applied_rate=%f"
680 ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
681 format_name, segment->start, segment->stop, segment->last_stop,
682 segment->duration, segment->rate, segment->applied_rate,
683 (guint) segment->flags, GST_TIME_ARGS (segment->time),
684 GST_TIME_ARGS (segment->accum));
685 }
686 }
687 }
689 #endif /* HAVE_PRINTF_EXTENSION */
691 /**
692 * gst_debug_construct_term_color:
693 * @colorinfo: the color info
694 *
695 * Constructs a string that can be used for getting the desired color in color
696 * terminals.
697 * You need to free the string after use.
698 *
699 * Returns: a string containing the color definition
700 */
701 gchar *
702 gst_debug_construct_term_color (guint colorinfo)
703 {
704 GString *color;
706 color = g_string_new ("\033[00");
708 if (colorinfo & GST_DEBUG_BOLD) {
709 g_string_append_len (color, ";01", 3);
710 }
711 if (colorinfo & GST_DEBUG_UNDERLINE) {
712 g_string_append_len (color, ";04", 3);
713 }
714 if (colorinfo & GST_DEBUG_FG_MASK) {
715 g_string_append_printf (color, ";3%1d", colorinfo & GST_DEBUG_FG_MASK);
716 }
717 if (colorinfo & GST_DEBUG_BG_MASK) {
718 g_string_append_printf (color, ";4%1d",
719 (colorinfo & GST_DEBUG_BG_MASK) >> 4);
720 }
721 g_string_append_c (color, 'm');
723 return g_string_free (color, FALSE);
724 }
726 /**
727 * gst_debug_construct_win_color:
728 * @colorinfo: the color info
729 *
730 * Constructs an integer that can be used for getting the desired color in
731 * windows' terminals (cmd.exe). As there is no mean to underline, we simply
732 * ignore this attribute.
733 *
734 * This function returns 0 on non-windows machines.
735 *
736 * Returns: an integer containing the color definition
737 *
738 * Since: 0.10.23
739 */
740 gint
741 gst_debug_construct_win_color (guint colorinfo)
742 {
743 gint color = 0;
744 #ifdef G_OS_WIN32
745 static const guchar ansi_to_win_fg[8] = {
746 0, /* black */
747 FOREGROUND_RED, /* red */
748 FOREGROUND_GREEN, /* green */
749 FOREGROUND_RED | FOREGROUND_GREEN, /* yellow */
750 FOREGROUND_BLUE, /* blue */
751 FOREGROUND_RED | FOREGROUND_BLUE, /* magenta */
752 FOREGROUND_GREEN | FOREGROUND_BLUE, /* cyan */
753 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE /* white */
754 };
755 static const guchar ansi_to_win_bg[8] = {
756 0,
757 BACKGROUND_RED,
758 BACKGROUND_GREEN,
759 BACKGROUND_RED | BACKGROUND_GREEN,
760 BACKGROUND_BLUE,
761 BACKGROUND_RED | BACKGROUND_BLUE,
762 BACKGROUND_GREEN | FOREGROUND_BLUE,
763 BACKGROUND_RED | BACKGROUND_GREEN | BACKGROUND_BLUE
764 };
766 /* we draw black as white, as cmd.exe can only have black bg */
767 if (colorinfo == 0) {
768 return ansi_to_win_fg[7];
769 }
771 if (colorinfo & GST_DEBUG_BOLD) {
772 color |= FOREGROUND_INTENSITY;
773 }
774 if (colorinfo & GST_DEBUG_FG_MASK) {
775 color |= ansi_to_win_fg[colorinfo & GST_DEBUG_FG_MASK];
776 }
777 if (colorinfo & GST_DEBUG_BG_MASK) {
778 color |= ansi_to_win_bg[(colorinfo & GST_DEBUG_BG_MASK) >> 4];
779 }
780 #endif
781 return color;
782 }
784 /* width of %p varies depending on actual value of pointer, which can make
785 * output unevenly aligned if multiple threads are involved, hence the %14p
786 * (should really be %18p, but %14p seems a good compromise between too many
787 * white spaces and likely unalignment on my system) */
788 #if defined (GLIB_SIZEOF_VOID_P) && GLIB_SIZEOF_VOID_P == 8
789 #define PTR_FMT "%14p"
790 #else
791 #define PTR_FMT "%10p"
792 #endif
793 #define PID_FMT "%5d"
794 #define CAT_FMT "%20s %s:%d:%s:%s"
796 #ifdef G_OS_WIN32
797 static const guchar levelcolormap[GST_LEVEL_COUNT] = {
798 /* GST_LEVEL_NONE */
799 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
800 /* GST_LEVEL_ERROR */
801 FOREGROUND_RED | FOREGROUND_INTENSITY,
802 /* GST_LEVEL_WARNING */
803 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_INTENSITY,
804 /* GST_LEVEL_INFO */
805 FOREGROUND_GREEN | FOREGROUND_INTENSITY,
806 /* GST_LEVEL_DEBUG */
807 FOREGROUND_GREEN | FOREGROUND_BLUE,
808 /* GST_LEVEL_LOG */
809 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
810 /* GST_LEVEL_FIXME */
811 FOREGROUND_RED | FOREGROUND_GREEN,
812 /* placeholder for log level 7 */
813 0,
814 /* placeholder for log level 8 */
815 0,
816 /* GST_LEVEL_MEMDUMP */
817 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE
818 };
820 static const guchar available_colors[] = {
821 FOREGROUND_RED, FOREGROUND_GREEN, FOREGROUND_RED | FOREGROUND_GREEN,
822 FOREGROUND_BLUE, FOREGROUND_RED | FOREGROUND_BLUE,
823 FOREGROUND_GREEN | FOREGROUND_BLUE,
824 };
825 #else
826 static const gchar *levelcolormap[GST_LEVEL_COUNT] = {
827 "\033[37m", /* GST_LEVEL_NONE */
828 "\033[31;01m", /* GST_LEVEL_ERROR */
829 "\033[33;01m", /* GST_LEVEL_WARNING */
830 "\033[32;01m", /* GST_LEVEL_INFO */
831 "\033[36m", /* GST_LEVEL_DEBUG */
832 "\033[37m", /* GST_LEVEL_LOG */
833 "\033[33;01m", /* GST_LEVEL_FIXME */
834 "\033[37m", /* placeholder for log level 7 */
835 "\033[37m", /* placeholder for log level 8 */
836 "\033[37m" /* GST_LEVEL_MEMDUMP */
837 };
838 #endif
840 /**
841 * gst_debug_log_default:
842 * @category: category to log
843 * @level: level of the message
844 * @file: the file that emitted the message, usually the __FILE__ identifier
845 * @function: the function that emitted the message
846 * @line: the line from that the message was emitted, usually __LINE__
847 * @message: the actual message
848 * @object: the object this message relates to or NULL if none
849 * @unused: an unused variable, reserved for some user_data.
850 *
851 * The default logging handler used by GStreamer. Logging functions get called
852 * whenever a macro like GST_DEBUG or similar is used. This function outputs the
853 * message and additional info using the glib error handler.
854 * You can add other handlers by using gst_debug_add_log_function().
855 * And you can remove this handler by calling
856 * gst_debug_remove_log_function(gst_debug_log_default);
857 */
858 void
859 gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level,
860 const gchar * file, const gchar * function, gint line,
861 GObject * object, GstDebugMessage * message, gpointer unused)
862 {
863 gint pid;
864 GstClockTime elapsed;
865 gchar *obj = NULL;
866 gboolean free_obj = TRUE;
867 gboolean is_colored;
869 if (level > gst_debug_category_get_threshold (category))
870 return;
872 pid = getpid ();
873 is_colored = gst_debug_is_colored ();
875 elapsed = GST_CLOCK_DIFF (_priv_gst_info_start_time,
876 gst_util_get_timestamp ());
878 if (object) {
879 obj = gst_debug_print_object (object);
880 } else {
881 obj = "\0";
882 free_obj = FALSE;
883 }
885 if (is_colored) {
886 #ifndef G_OS_WIN32
887 /* colors, non-windows */
888 gchar *color = NULL;
889 gchar *clear;
890 gchar pidcolor[10];
891 const gchar *levelcolor;
893 color = gst_debug_construct_term_color (gst_debug_category_get_color
894 (category));
895 clear = "\033[00m";
896 g_sprintf (pidcolor, "\033[3%1dm", pid % 6 + 31);
897 levelcolor = levelcolormap[level];
899 #define PRINT_FMT " %s"PID_FMT"%s "PTR_FMT" %s%s%s %s"CAT_FMT"%s %s\n"
900 g_printerr ("%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed),
901 pidcolor, pid, clear, g_thread_self (), levelcolor,
902 gst_debug_level_get_name (level), clear, color,
903 gst_debug_category_get_name (category), file, line, function, obj,
904 clear, gst_debug_message_get (message));
905 #undef PRINT_FMT
906 g_free (color);
907 #else
908 /* colors, windows. We take a lock to keep colors and content together.
909 * Maybe there is a better way but for now this will do the right
910 * thing. */
911 static GStaticMutex win_print_mutex = G_STATIC_MUTEX_INIT;
912 const gint clear = FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE;
913 #define SET_COLOR(c) \
914 SetConsoleTextAttribute (GetStdHandle (STD_ERROR_HANDLE), (c));
915 g_static_mutex_lock (&win_print_mutex);
916 /* timestamp */
917 g_printerr ("%" GST_TIME_FORMAT " ", GST_TIME_ARGS (elapsed));
918 /* pid */
919 SET_COLOR (available_colors[pid % G_N_ELEMENTS (available_colors)]);
920 g_printerr (PID_FMT, pid);
921 /* thread */
922 SET_COLOR (clear);
923 g_printerr (" " PTR_FMT " ", g_thread_self ());
924 /* level */
925 SET_COLOR (levelcolormap[level]);
926 g_printerr ("%s ", gst_debug_level_get_name (level));
927 /* category */
928 SET_COLOR (gst_debug_construct_win_color (gst_debug_category_get_color
929 (category)));
930 g_printerr (CAT_FMT, gst_debug_category_get_name (category),
931 file, line, function, obj);
932 /* message */
933 SET_COLOR (clear);
934 g_printerr (" %s\n", gst_debug_message_get (message));
935 g_static_mutex_unlock (&win_print_mutex);
936 #endif
937 } else {
938 /* no color, all platforms */
939 #define PRINT_FMT " "PID_FMT" "PTR_FMT" %s "CAT_FMT" %s\n"
940 g_printerr ("%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed), pid,
941 g_thread_self (), gst_debug_level_get_name (level),
942 gst_debug_category_get_name (category), file, line, function, obj,
943 gst_debug_message_get (message));
944 #undef PRINT_FMT
945 }
947 if (free_obj)
948 g_free (obj);
949 }
951 /**
952 * gst_debug_level_get_name:
953 * @level: the level to get the name for
954 *
955 * Get the string representation of a debugging level
956 *
957 * Returns: the name
958 */
959 const gchar *
960 gst_debug_level_get_name (GstDebugLevel level)
961 {
962 switch (level) {
963 case GST_LEVEL_NONE:
964 return "";
965 case GST_LEVEL_ERROR:
966 return "ERROR ";
967 case GST_LEVEL_WARNING:
968 return "WARN ";
969 case GST_LEVEL_INFO:
970 return "INFO ";
971 case GST_LEVEL_DEBUG:
972 return "DEBUG ";
973 case GST_LEVEL_LOG:
974 return "LOG ";
975 case GST_LEVEL_FIXME:
976 return "FIXME ";
977 case GST_LEVEL_MEMDUMP:
978 return "MEMDUMP";
979 default:
980 g_warning ("invalid level specified for gst_debug_level_get_name");
981 return "";
982 }
983 }
985 /**
986 * gst_debug_add_log_function:
987 * @func: the function to use
988 * @data: user data
989 *
990 * Adds the logging function to the list of logging functions.
991 * Be sure to use G_GNUC_NO_INSTRUMENT on that function, it is needed.
992 */
993 void
994 gst_debug_add_log_function (GstLogFunction func, gpointer data)
995 {
996 LogFuncEntry *entry;
997 GSList *list;
999 g_return_if_fail (func != NULL);
1001 entry = g_new (LogFuncEntry, 1);
1002 entry->func = func;
1003 entry->user_data = data;
1004 /* FIXME: we leak the old list here - other threads might access it right now
1005 * in gst_debug_logv. Another solution is to lock the mutex in gst_debug_logv,
1006 * but that is waaay costly.
1007 * It'd probably be clever to use some kind of RCU here, but I don't know
1008 * anything about that.
1009 */
1010 g_static_mutex_lock (&__log_func_mutex);
1011 list = g_slist_copy (__log_functions);
1012 __log_functions = g_slist_prepend (list, entry);
1013 g_static_mutex_unlock (&__log_func_mutex);
1015 GST_DEBUG ("prepended log function %p (user data %p) to log functions",
1016 func, data);
1017 }
1019 static gint
1020 gst_debug_compare_log_function_by_func (gconstpointer entry, gconstpointer func)
1021 {
1022 gpointer entryfunc = (gpointer) (((LogFuncEntry *) entry)->func);
1024 return (entryfunc < func) ? -1 : (entryfunc > func) ? 1 : 0;
1025 }
1027 static gint
1028 gst_debug_compare_log_function_by_data (gconstpointer entry, gconstpointer data)
1029 {
1030 gpointer entrydata = ((LogFuncEntry *) entry)->user_data;
1032 return (entrydata < data) ? -1 : (entrydata > data) ? 1 : 0;
1033 }
1035 static guint
1036 gst_debug_remove_with_compare_func (GCompareFunc func, gpointer data)
1037 {
1038 GSList *found;
1039 GSList *new;
1040 guint removals = 0;
1042 g_static_mutex_lock (&__log_func_mutex);
1043 new = __log_functions;
1044 while ((found = g_slist_find_custom (new, data, func))) {
1045 if (new == __log_functions) {
1046 /* make a copy when we have the first hit, so that we modify the copy and
1047 * make that the new list later */
1048 new = g_slist_copy (new);
1049 continue;
1050 }
1051 g_free (found->data);
1052 new = g_slist_delete_link (new, found);
1053 removals++;
1054 }
1055 /* FIXME: We leak the old list here. See _add_log_function for why. */
1056 __log_functions = new;
1057 g_static_mutex_unlock (&__log_func_mutex);
1059 return removals;
1060 }
1062 /**
1063 * gst_debug_remove_log_function:
1064 * @func: the log function to remove
1065 *
1066 * Removes all registered instances of the given logging functions.
1067 *
1068 * Returns: How many instances of the function were removed
1069 */
1070 guint
1071 gst_debug_remove_log_function (GstLogFunction func)
1072 {
1073 guint removals;
1075 g_return_val_if_fail (func != NULL, 0);
1077 removals =
1078 gst_debug_remove_with_compare_func
1079 (gst_debug_compare_log_function_by_func, (gpointer) func);
1080 GST_DEBUG ("removed log function %p %d times from log function list", func,
1081 removals);
1083 return removals;
1084 }
1086 /**
1087 * gst_debug_remove_log_function_by_data:
1088 * @data: user data of the log function to remove
1089 *
1090 * Removes all registered instances of log functions with the given user data.
1091 *
1092 * Returns: How many instances of the function were removed
1093 */
1094 guint
1095 gst_debug_remove_log_function_by_data (gpointer data)
1096 {
1097 guint removals;
1099 removals =
1100 gst_debug_remove_with_compare_func
1101 (gst_debug_compare_log_function_by_data, data);
1102 GST_DEBUG
1103 ("removed %d log functions with user data %p from log function list",
1104 removals, data);
1106 return removals;
1107 }
1109 /**
1110 * gst_debug_set_colored:
1111 * @colored: Whether to use colored output or not
1112 *
1113 * Sets or unsets the use of coloured debugging output.
1114 */
1115 void
1116 gst_debug_set_colored (gboolean colored)
1117 {
1118 g_atomic_int_set (&__use_color, colored ? 1 : 0);
1119 }
1121 /**
1122 * gst_debug_is_colored:
1123 *
1124 * Checks if the debugging output should be colored.
1125 *
1126 * Returns: TRUE, if the debug output should be colored.
1127 */
1128 gboolean
1129 gst_debug_is_colored (void)
1130 {
1131 return g_atomic_int_get (&__use_color) == 0 ? FALSE : TRUE;
1132 }
1134 /**
1135 * gst_debug_set_active:
1136 * @active: Whether to use debugging output or not
1137 *
1138 * If activated, debugging messages are sent to the debugging
1139 * handlers.
1140 * It makes sense to deactivate it for speed issues.
1141 * <note><para>This function is not threadsafe. It makes sense to only call it
1142 * during initialization.</para></note>
1143 */
1144 void
1145 gst_debug_set_active (gboolean active)
1146 {
1147 __gst_debug_enabled = active;
1148 if (active)
1149 __gst_debug_min = GST_LEVEL_COUNT;
1150 else
1151 __gst_debug_min = GST_LEVEL_NONE;
1152 }
1154 /**
1155 * gst_debug_is_active:
1156 *
1157 * Checks if debugging output is activated.
1158 *
1159 * Returns: TRUE, if debugging is activated
1160 */
1161 gboolean
1162 gst_debug_is_active (void)
1163 {
1164 return __gst_debug_enabled;
1165 }
1167 /**
1168 * gst_debug_set_default_threshold:
1169 * @level: level to set
1170 *
1171 * Sets the default threshold to the given level and updates all categories to
1172 * use this threshold.
1173 */
1174 void
1175 gst_debug_set_default_threshold (GstDebugLevel level)
1176 {
1177 g_atomic_int_set (&__default_level, level);
1178 gst_debug_reset_all_thresholds ();
1179 }
1181 /**
1182 * gst_debug_get_default_threshold:
1183 *
1184 * Returns the default threshold that is used for new categories.
1185 *
1186 * Returns: the default threshold level
1187 */
1188 GstDebugLevel
1189 gst_debug_get_default_threshold (void)
1190 {
1191 return (GstDebugLevel) g_atomic_int_get (&__default_level);
1192 }
1194 static void
1195 gst_debug_reset_threshold (gpointer category, gpointer unused)
1196 {
1197 GstDebugCategory *cat = (GstDebugCategory *) category;
1198 GSList *walk;
1200 g_static_mutex_lock (&__level_name_mutex);
1201 walk = __level_name;
1202 while (walk) {
1203 LevelNameEntry *entry = walk->data;
1205 walk = g_slist_next (walk);
1206 if (g_pattern_match_string (entry->pat, cat->name)) {
1207 GST_LOG ("category %s matches pattern %p - gets set to level %d",
1208 cat->name, entry->pat, entry->level);
1209 gst_debug_category_set_threshold (cat, entry->level);
1210 goto exit;
1211 }
1212 }
1213 gst_debug_category_set_threshold (cat, gst_debug_get_default_threshold ());
1215 exit:
1216 g_static_mutex_unlock (&__level_name_mutex);
1217 }
1219 static void
1220 gst_debug_reset_all_thresholds (void)
1221 {
1222 g_static_mutex_lock (&__cat_mutex);
1223 g_slist_foreach (__categories, gst_debug_reset_threshold, NULL);
1224 g_static_mutex_unlock (&__cat_mutex);
1225 }
1227 static void
1228 for_each_threshold_by_entry (gpointer data, gpointer user_data)
1229 {
1230 GstDebugCategory *cat = (GstDebugCategory *) data;
1231 LevelNameEntry *entry = (LevelNameEntry *) user_data;
1233 if (g_pattern_match_string (entry->pat, cat->name)) {
1234 GST_LOG ("category %s matches pattern %p - gets set to level %d",
1235 cat->name, entry->pat, entry->level);
1236 gst_debug_category_set_threshold (cat, entry->level);
1237 }
1238 }
1240 /**
1241 * gst_debug_set_threshold_for_name:
1242 * @name: name of the categories to set
1243 * @level: level to set them to
1244 *
1245 * Sets all categories which match the given glob style pattern to the given
1246 * level.
1247 */
1248 void
1249 gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level)
1250 {
1251 GPatternSpec *pat;
1252 LevelNameEntry *entry;
1254 g_return_if_fail (name != NULL);
1256 pat = g_pattern_spec_new (name);
1257 entry = g_new (LevelNameEntry, 1);
1258 entry->pat = pat;
1259 entry->level = level;
1260 g_static_mutex_lock (&__level_name_mutex);
1261 __level_name = g_slist_prepend (__level_name, entry);
1262 g_static_mutex_unlock (&__level_name_mutex);
1263 g_static_mutex_lock (&__cat_mutex);
1264 g_slist_foreach (__categories, for_each_threshold_by_entry, entry);
1265 g_static_mutex_unlock (&__cat_mutex);
1266 }
1268 /**
1269 * gst_debug_unset_threshold_for_name:
1270 * @name: name of the categories to set
1271 *
1272 * Resets all categories with the given name back to the default level.
1273 */
1274 void
1275 gst_debug_unset_threshold_for_name (const gchar * name)
1276 {
1277 GSList *walk;
1278 GPatternSpec *pat;
1280 g_return_if_fail (name != NULL);
1282 pat = g_pattern_spec_new (name);
1283 g_static_mutex_lock (&__level_name_mutex);
1284 walk = __level_name;
1285 /* improve this if you want, it's mighty slow */
1286 while (walk) {
1287 LevelNameEntry *entry = walk->data;
1289 if (g_pattern_spec_equal (entry->pat, pat)) {
1290 __level_name = g_slist_remove_link (__level_name, walk);
1291 g_pattern_spec_free (entry->pat);
1292 g_free (entry);
1293 g_slist_free_1 (walk);
1294 walk = __level_name;
1295 }
1296 }
1297 g_static_mutex_unlock (&__level_name_mutex);
1298 g_pattern_spec_free (pat);
1299 gst_debug_reset_all_thresholds ();
1300 }
1302 GstDebugCategory *
1303 _gst_debug_category_new (const gchar * name, guint color,
1304 const gchar * description)
1305 {
1306 GstDebugCategory *cat;
1308 g_return_val_if_fail (name != NULL, NULL);
1310 cat = g_new (GstDebugCategory, 1);
1311 cat->name = g_strdup (name);
1312 cat->color = color;
1313 if (description != NULL) {
1314 cat->description = g_strdup (description);
1315 } else {
1316 cat->description = g_strdup ("no description");
1317 }
1318 g_atomic_int_set (&cat->threshold, 0);
1319 gst_debug_reset_threshold (cat, NULL);
1321 /* add to category list */
1322 g_static_mutex_lock (&__cat_mutex);
1323 __categories = g_slist_prepend (__categories, cat);
1324 g_static_mutex_unlock (&__cat_mutex);
1326 return cat;
1327 }
1329 /**
1330 * gst_debug_category_free:
1331 * @category: #GstDebugCategory to free.
1332 *
1333 * Removes and frees the category and all associated resources.
1334 */
1335 void
1336 gst_debug_category_free (GstDebugCategory * category)
1337 {
1338 if (category == NULL)
1339 return;
1341 /* remove from category list */
1342 g_static_mutex_lock (&__cat_mutex);
1343 __categories = g_slist_remove (__categories, category);
1344 g_static_mutex_unlock (&__cat_mutex);
1346 g_free ((gpointer) category->name);
1347 g_free ((gpointer) category->description);
1348 g_free (category);
1349 }
1351 /**
1352 * gst_debug_category_set_threshold:
1353 * @category: a #GstDebugCategory to set threshold of.
1354 * @level: the #GstDebugLevel threshold to set.
1355 *
1356 * Sets the threshold of the category to the given level. Debug information will
1357 * only be output if the threshold is lower or equal to the level of the
1358 * debugging message.
1359 * <note><para>
1360 * Do not use this function in production code, because other functions may
1361 * change the threshold of categories as side effect. It is however a nice
1362 * function to use when debugging (even from gdb).
1363 * </para></note>
1364 */
1365 void
1366 gst_debug_category_set_threshold (GstDebugCategory * category,
1367 GstDebugLevel level)
1368 {
1369 g_return_if_fail (category != NULL);
1371 if (level > __gst_debug_min) {
1372 __gst_debug_enabled = TRUE;
1373 __gst_debug_min = level;
1374 }
1376 g_atomic_int_set (&category->threshold, level);
1377 }
1379 /**
1380 * gst_debug_category_reset_threshold:
1381 * @category: a #GstDebugCategory to reset threshold of.
1382 *
1383 * Resets the threshold of the category to the default level. Debug information
1384 * will only be output if the threshold is lower or equal to the level of the
1385 * debugging message.
1386 * Use this function to set the threshold back to where it was after using
1387 * gst_debug_category_set_threshold().
1388 */
1389 void
1390 gst_debug_category_reset_threshold (GstDebugCategory * category)
1391 {
1392 gst_debug_reset_threshold (category, NULL);
1393 }
1395 /**
1396 * gst_debug_category_get_threshold:
1397 * @category: a #GstDebugCategory to get threshold of.
1398 *
1399 * Returns the threshold of a #GstDebugCategory.
1400 *
1401 * Returns: the #GstDebugLevel that is used as threshold.
1402 */
1403 GstDebugLevel
1404 gst_debug_category_get_threshold (GstDebugCategory * category)
1405 {
1406 return g_atomic_int_get (&category->threshold);
1407 }
1409 /**
1410 * gst_debug_category_get_name:
1411 * @category: a #GstDebugCategory to get name of.
1412 *
1413 * Returns the name of a debug category.
1414 *
1415 * Returns: the name of the category.
1416 */
1417 const gchar *
1418 gst_debug_category_get_name (GstDebugCategory * category)
1419 {
1420 return category->name;
1421 }
1423 /**
1424 * gst_debug_category_get_color:
1425 * @category: a #GstDebugCategory to get the color of.
1426 *
1427 * Returns the color of a debug category used when printing output in this
1428 * category.
1429 *
1430 * Returns: the color of the category.
1431 */
1432 guint
1433 gst_debug_category_get_color (GstDebugCategory * category)
1434 {
1435 return category->color;
1436 }
1438 /**
1439 * gst_debug_category_get_description:
1440 * @category: a #GstDebugCategory to get the description of.
1441 *
1442 * Returns the description of a debug category.
1443 *
1444 * Returns: the description of the category.
1445 */
1446 const gchar *
1447 gst_debug_category_get_description (GstDebugCategory * category)
1448 {
1449 return category->description;
1450 }
1452 /**
1453 * gst_debug_get_all_categories:
1454 *
1455 * Returns a snapshot of a all categories that are currently in use . This list
1456 * may change anytime.
1457 * The caller has to free the list after use.
1458 *
1459 * Returns: the list of categories
1460 */
1461 GSList *
1462 gst_debug_get_all_categories (void)
1463 {
1464 GSList *ret;
1466 g_static_mutex_lock (&__cat_mutex);
1467 ret = g_slist_copy (__categories);
1468 g_static_mutex_unlock (&__cat_mutex);
1470 return ret;
1471 }
1473 GstDebugCategory *
1474 _gst_debug_get_category (const gchar * name)
1475 {
1476 GstDebugCategory *ret = NULL;
1477 GSList *node;
1479 for (node = __categories; node; node = g_slist_next (node)) {
1480 ret = (GstDebugCategory *) node->data;
1481 if (!strcmp (name, ret->name)) {
1482 return ret;
1483 }
1484 }
1485 return NULL;
1486 }
1488 /*** FUNCTION POINTERS ********************************************************/
1490 static GHashTable *__gst_function_pointers; /* NULL */
1491 static GStaticMutex __dbg_functions_mutex = G_STATIC_MUTEX_INIT;
1493 const gchar *
1494 _gst_debug_nameof_funcptr (GstDebugFuncPtr ptr)
1495 G_GNUC_NO_INSTRUMENT;
1497 /* This function MUST NOT return NULL */
1498 const gchar *_gst_debug_nameof_funcptr (GstDebugFuncPtr func)
1499 {
1500 gchar *ptrname;
1502 #ifdef HAVE_DLADDR
1503 Dl_info dl_info;
1504 #endif
1506 if (G_UNLIKELY (func == NULL))
1507 return "(NULL)";
1509 g_static_mutex_lock (&__dbg_functions_mutex);
1510 if (G_LIKELY (__gst_function_pointers)) {
1511 ptrname = g_hash_table_lookup (__gst_function_pointers, (gpointer) func);
1512 g_static_mutex_unlock (&__dbg_functions_mutex);
1513 if (G_LIKELY (ptrname))
1514 return ptrname;
1515 } else {
1516 g_static_mutex_unlock (&__dbg_functions_mutex);
1517 }
1518 /* we need to create an entry in the hash table for this one so we don't leak
1519 * the name */
1520 #ifdef HAVE_DLADDR
1521 if (dladdr ((gpointer) func, &dl_info) && dl_info.dli_sname) {
1522 gchar *name = g_strdup (dl_info.dli_sname);
1524 _gst_debug_register_funcptr (func, name);
1525 return name;
1526 } else
1527 #endif
1528 {
1529 gchar *name = g_strdup_printf ("%p", (gpointer) func);
1531 _gst_debug_register_funcptr (func, name);
1532 return name;
1533 }
1534 }
1536 void
1537 _gst_debug_register_funcptr (GstDebugFuncPtr func, const gchar * ptrname)
1538 {
1539 gpointer ptr = (gpointer) func;
1541 g_static_mutex_lock (&__dbg_functions_mutex);
1543 if (!__gst_function_pointers)
1544 __gst_function_pointers = g_hash_table_new (g_direct_hash, g_direct_equal);
1545 if (!g_hash_table_lookup (__gst_function_pointers, ptr))
1546 g_hash_table_insert (__gst_function_pointers, ptr, (gpointer) ptrname);
1548 g_static_mutex_unlock (&__dbg_functions_mutex);
1549 }
1551 /*** PRINTF EXTENSIONS ********************************************************/
1553 #ifdef HAVE_PRINTF_EXTENSION
1554 static int
1555 _gst_info_printf_extension_ptr (FILE * stream, const struct printf_info *info,
1556 const void *const *args)
1557 {
1558 char *buffer;
1559 int len;
1560 void *ptr;
1562 buffer = NULL;
1563 ptr = *(void **) args[0];
1565 buffer = gst_debug_print_object (ptr);
1566 len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1567 buffer);
1569 g_free (buffer);
1570 return len;
1571 }
1573 static int
1574 _gst_info_printf_extension_segment (FILE * stream,
1575 const struct printf_info *info, const void *const *args)
1576 {
1577 char *buffer;
1578 int len;
1579 void *ptr;
1581 buffer = NULL;
1582 ptr = *(void **) args[0];
1584 buffer = gst_debug_print_segment (ptr);
1585 len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1586 buffer);
1588 g_free (buffer);
1589 return len;
1590 }
1592 #if HAVE_REGISTER_PRINTF_SPECIFIER
1593 static int
1594 _gst_info_printf_extension_arginfo (const struct printf_info *info, size_t n,
1595 int *argtypes, int *size)
1596 #else
1597 static int
1598 _gst_info_printf_extension_arginfo (const struct printf_info *info, size_t n,
1599 int *argtypes)
1600 #endif
1601 {
1602 if (n > 0) {
1603 argtypes[0] = PA_POINTER;
1604 #if HAVE_REGISTER_PRINTF_SPECIFIER
1605 *size = sizeof (gpointer);
1606 #endif
1607 }
1608 return 1;
1609 }
1610 #endif /* HAVE_PRINTF_EXTENSION */
1612 static void
1613 gst_info_dump_mem_line (gchar * linebuf, gsize linebuf_size,
1614 const guint8 * mem, gsize mem_offset, gsize mem_size)
1615 {
1616 gchar hexstr[50], ascstr[18], digitstr[4];
1618 if (mem_size > 16)
1619 mem_size = 16;
1621 hexstr[0] = '\0';
1622 ascstr[0] = '\0';
1624 if (mem != NULL) {
1625 guint i = 0;
1627 mem += mem_offset;
1628 while (i < mem_size) {
1629 ascstr[i] = (g_ascii_isprint (mem[i])) ? mem[i] : '.';
1630 g_snprintf (digitstr, sizeof (digitstr), "%02x ", mem[i]);
1631 g_strlcat (hexstr, digitstr, sizeof (hexstr));
1632 ++i;
1633 }
1634 ascstr[i] = '\0';
1635 }
1637 g_snprintf (linebuf, linebuf_size, "%08x: %-48.48s %-16.16s",
1638 (guint) mem_offset, hexstr, ascstr);
1639 }
1641 void
1642 _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
1643 const gchar * func, gint line, GObject * obj, const gchar * msg,
1644 const guint8 * data, guint length)
1645 {
1646 guint off = 0;
1648 gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "--------"
1649 "-------------------------------------------------------------------");
1651 if (msg != NULL && *msg != '\0') {
1652 gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, msg);
1653 }
1655 while (off < length) {
1656 gchar buf[128];
1658 /* gst_info_dump_mem_line will process 16 bytes at most */
1659 gst_info_dump_mem_line (buf, sizeof (buf), data, off, length - off);
1660 gst_debug_log (cat, GST_LEVEL_MEMDUMP, file, func, line, obj, "%s", buf);
1661 off += 16;
1662 }
1664 gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "--------"
1665 "-------------------------------------------------------------------");
1666 }
1668 #else /* !GST_DISABLE_GST_DEBUG */
1669 #ifndef GST_REMOVE_DISABLED
1671 GstDebugCategory *
1672 _gst_debug_category_new (const gchar * name, guint color,
1673 const gchar * description)
1674 {
1675 return NULL;
1676 }
1678 void
1679 _gst_debug_register_funcptr (gpointer func, const gchar * ptrname)
1680 {
1681 }
1683 /* This function MUST NOT return NULL */
1684 const gchar *
1685 _gst_debug_nameof_funcptr (gpointer func)
1686 {
1687 return "(NULL)";
1688 }
1690 void
1691 gst_debug_log (GstDebugCategory * category, GstDebugLevel level,
1692 const gchar * file, const gchar * function, gint line,
1693 GObject * object, const gchar * format, ...)
1694 {
1695 }
1697 void
1698 gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level,
1699 const gchar * file, const gchar * function, gint line,
1700 GObject * object, const gchar * format, va_list args)
1701 {
1702 }
1704 const gchar *
1705 gst_debug_message_get (GstDebugMessage * message)
1706 {
1707 return "";
1708 }
1710 void
1711 gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level,
1712 const gchar * file, const gchar * function, gint line,
1713 GObject * object, GstDebugMessage * message, gpointer unused)
1714 {
1715 }
1717 G_CONST_RETURN gchar *
1718 gst_debug_level_get_name (GstDebugLevel level)
1719 {
1720 return "NONE";
1721 }
1723 void
1724 gst_debug_add_log_function (GstLogFunction func, gpointer data)
1725 {
1726 }
1728 guint
1729 gst_debug_remove_log_function (GstLogFunction func)
1730 {
1731 return 0;
1732 }
1734 guint
1735 gst_debug_remove_log_function_by_data (gpointer data)
1736 {
1737 return 0;
1738 }
1740 void
1741 gst_debug_set_active (gboolean active)
1742 {
1743 }
1745 gboolean
1746 gst_debug_is_active (void)
1747 {
1748 return FALSE;
1749 }
1751 void
1752 gst_debug_set_colored (gboolean colored)
1753 {
1754 }
1756 gboolean
1757 gst_debug_is_colored (void)
1758 {
1759 return FALSE;
1760 }
1762 void
1763 gst_debug_set_default_threshold (GstDebugLevel level)
1764 {
1765 }
1767 GstDebugLevel
1768 gst_debug_get_default_threshold (void)
1769 {
1770 return GST_LEVEL_NONE;
1771 }
1773 void
1774 gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level)
1775 {
1776 }
1778 void
1779 gst_debug_unset_threshold_for_name (const gchar * name)
1780 {
1781 }
1783 void
1784 gst_debug_category_free (GstDebugCategory * category)
1785 {
1786 }
1788 void
1789 gst_debug_category_set_threshold (GstDebugCategory * category,
1790 GstDebugLevel level)
1791 {
1792 }
1794 void
1795 gst_debug_category_reset_threshold (GstDebugCategory * category)
1796 {
1797 }
1799 GstDebugLevel
1800 gst_debug_category_get_threshold (GstDebugCategory * category)
1801 {
1802 return GST_LEVEL_NONE;
1803 }
1805 G_CONST_RETURN gchar *
1806 gst_debug_category_get_name (GstDebugCategory * category)
1807 {
1808 return "";
1809 }
1811 guint
1812 gst_debug_category_get_color (GstDebugCategory * category)
1813 {
1814 return 0;
1815 }
1817 G_CONST_RETURN gchar *
1818 gst_debug_category_get_description (GstDebugCategory * category)
1819 {
1820 return "";
1821 }
1823 GSList *
1824 gst_debug_get_all_categories (void)
1825 {
1826 return NULL;
1827 }
1829 gchar *
1830 gst_debug_construct_term_color (guint colorinfo)
1831 {
1832 return g_strdup ("00");
1833 }
1835 gint
1836 gst_debug_construct_win_color (guint colorinfo)
1837 {
1838 return 0;
1839 }
1841 gboolean
1842 _priv_gst_in_valgrind (void)
1843 {
1844 return FALSE;
1845 }
1847 void
1848 _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
1849 const gchar * func, gint line, GObject * obj, const gchar * msg,
1850 const guint8 * data, guint length)
1851 {
1852 }
1853 #endif /* GST_REMOVE_DISABLED */
1854 #endif /* GST_DISABLE_GST_DEBUG */
1857 #ifdef GST_ENABLE_FUNC_INSTRUMENTATION
1858 /* FIXME make this thread specific */
1859 static GSList *stack_trace = NULL;
1861 void
1862 __cyg_profile_func_enter (void *this_fn, void *call_site)
1863 G_GNUC_NO_INSTRUMENT;
1864 void __cyg_profile_func_enter (void *this_fn, void *call_site)
1865 {
1866 gchar *name = _gst_debug_nameof_funcptr (this_fn);
1867 gchar *site = _gst_debug_nameof_funcptr (call_site);
1869 GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "entering function %s from %s", name,
1870 site);
1871 stack_trace =
1872 g_slist_prepend (stack_trace, g_strdup_printf ("%8p in %s from %p (%s)",
1873 this_fn, name, call_site, site));
1875 g_free (name);
1876 g_free (site);
1877 }
1879 void
1880 __cyg_profile_func_exit (void *this_fn, void *call_site)
1881 G_GNUC_NO_INSTRUMENT;
1882 void __cyg_profile_func_exit (void *this_fn, void *call_site)
1883 {
1884 gchar *name = _gst_debug_nameof_funcptr (this_fn);
1886 GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "leaving function %s", name);
1887 g_free (stack_trace->data);
1888 stack_trace = g_slist_delete_link (stack_trace, stack_trace);
1890 g_free (name);
1891 }
1893 /**
1894 * gst_debug_print_stack_trace:
1895 *
1896 * If GST_ENABLE_FUNC_INSTRUMENTATION is defined a stacktrace is available for
1897 * gstreamer code, which can be printed with this function.
1898 */
1899 void
1900 gst_debug_print_stack_trace (void)
1901 {
1902 GSList *walk = stack_trace;
1903 gint count = 0;
1905 if (walk)
1906 walk = g_slist_next (walk);
1908 while (walk) {
1909 gchar *name = (gchar *) walk->data;
1911 g_print ("#%-2d %s\n", count++, name);
1913 walk = g_slist_next (walk);
1914 }
1915 }
1916 #else
1917 void
1918 gst_debug_print_stack_trace (void)
1919 {
1920 /* nothing because it's compiled out */
1921 }
1923 #endif /* GST_ENABLE_FUNC_INSTRUMENTATION */