1 /* GStreamer
2 * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3 * 2000 Wim Taymans <wtay@chello.be>
4 * 2003 Benjamin Otte <in7y118@public.uni-hamburg.de>
5 *
6 * gstinfo.c: debugging functions
7 *
8 * This library is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU Library General Public
10 * License as published by the Free Software Foundation; either
11 * version 2 of the License, or (at your option) any later version.
12 *
13 * This library is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
16 * Library General Public License for more details.
17 *
18 * You should have received a copy of the GNU Library General Public
19 * License along with this library; if not, write to the
20 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
21 * Boston, MA 02111-1307, USA.
22 */
24 /**
25 * SECTION:gstinfo
26 * @short_description: Debugging and logging facilities
27 * @see_also: #GstConfig, #Gst for command line parameters
28 * and environment variables that affect the debugging output.
29 *
30 * GStreamer's debugging subsystem is an easy way to get information about what
31 * the application is doing. It is not meant for programming errors. Use GLib
32 * methods (g_warning and friends) for that.
33 *
34 * The debugging subsystem works only after GStreamer has been initialized
35 * - for example by calling gst_init().
36 *
37 * The debugging subsystem is used to log informational messages while the
38 * application runs. Each messages has some properties attached to it. Among
39 * these properties are the debugging category, the severity (called "level"
40 * here) and an optional #GObject it belongs to. Each of these messages is sent
41 * to all registered debugging handlers, which then handle the messages.
42 * GStreamer attaches a default handler on startup, which outputs requested
43 * messages to stderr.
44 *
45 * Messages are output by using shortcut macros like #GST_DEBUG,
46 * #GST_CAT_ERROR_OBJECT or similar. These all expand to calling gst_debug_log()
47 * with the right parameters.
48 * The only thing a developer will probably want to do is define his own
49 * categories. This is easily done with 3 lines. At the top of your code,
50 * declare
51 * the variables and set the default category.
52 * <informalexample>
53 * <programlisting>
54 * GST_DEBUG_CATEGORY_STATIC (my_category); // define category (statically)
55 * &hash;define GST_CAT_DEFAULT my_category // set as default
56 * </programlisting>
57 * </informalexample>
58 * After that you only need to initialize the category.
59 * <informalexample>
60 * <programlisting>
61 * GST_DEBUG_CATEGORY_INIT (my_category, "my category",
62 * 0, "This is my very own");
63 * </programlisting>
64 * </informalexample>
65 * Initialization must be done before the category is used first.
66 * Plugins do this
67 * in their plugin_init function, libraries and applications should do that
68 * during their initialization.
69 *
70 * The whole debugging subsystem can be disabled at build time with passing the
71 * --disable-gst-debug switch to configure. If this is done, every function,
72 * macro and even structs described in this file evaluate to default values or
73 * nothing at all.
74 * So don't take addresses of these functions or use other tricks.
75 * If you must do that for some reason, there is still an option.
76 * If the debugging
77 * subsystem was compiled out, #GST_DISABLE_GST_DEBUG is defined in
78 * <gst/gst.h>,
79 * so you can check that before doing your trick.
80 * Disabling the debugging subsystem will give you a slight (read: unnoticeable)
81 * speed increase and will reduce the size of your compiled code. The GStreamer
82 * library itself becomes around 10% smaller.
83 *
84 * Please note that there are naming conventions for the names of debugging
85 * categories. These are explained at GST_DEBUG_CATEGORY_INIT().
86 */
88 #include "gst_private.h"
89 #include "gstinfo.h"
91 #ifndef GST_DISABLE_GST_DEBUG
93 #ifdef HAVE_DLFCN_H
94 # include <dlfcn.h>
95 #endif
96 #ifdef HAVE_PRINTF_EXTENSION
97 # include <printf.h>
98 #endif
99 #include <stdio.h> /* fprintf */
100 #ifdef HAVE_UNISTD_H
101 # include <unistd.h> /* getpid on UNIX */
102 #endif
103 #ifdef HAVE_PROCESS_H
104 # include <process.h> /* getpid on win32 */
105 #endif
106 #include <string.h> /* G_VA_COPY */
107 #ifdef G_OS_WIN32
108 # define WIN32_LEAN_AND_MEAN /* prevents from including too many things */
109 # include <windows.h> /* GetStdHandle, windows console */
110 #endif
112 #include "gst_private.h"
113 #include "gstutils.h"
114 #include "gstsegment.h"
115 #ifdef HAVE_VALGRIND_H
116 # include <valgrind/valgrind.h>
117 #endif
118 #include <glib/gprintf.h> /* g_sprintf */
120 /* underscore is to prevent conflict with GST_CAT_DEBUG define */
121 GST_DEBUG_CATEGORY_STATIC (_GST_CAT_DEBUG);
123 /* time of initialization, so we get useful debugging output times
124 * FIXME: we use this in gstdebugutils.c, what about a function + macro to
125 * get the running time: GST_DEBUG_RUNNING_TIME
126 */
127 GstClockTime _priv_gst_info_start_time;
129 #if 0
130 #if defined __sgi__
131 #include <rld_interface.h>
132 typedef struct DL_INFO
133 {
134 const char *dli_fname;
135 void *dli_fbase;
136 const char *dli_sname;
137 void *dli_saddr;
138 int dli_version;
139 int dli_reserved1;
140 long dli_reserved[4];
141 }
142 Dl_info;
144 #define _RLD_DLADDR 14
145 int dladdr (void *address, Dl_info * dl);
147 int
148 dladdr (void *address, Dl_info * dl)
149 {
150 void *v;
152 v = _rld_new_interface (_RLD_DLADDR, address, dl);
153 return (int) v;
154 }
155 #endif /* __sgi__ */
156 #endif
158 static void gst_debug_reset_threshold (gpointer category, gpointer unused);
159 static void gst_debug_reset_all_thresholds (void);
161 #ifdef HAVE_PRINTF_EXTENSION
162 static int _gst_info_printf_extension_ptr (FILE * stream,
163 const struct printf_info *info, const void *const *args);
164 static int _gst_info_printf_extension_segment (FILE * stream,
165 const struct printf_info *info, const void *const *args);
166 static int _gst_info_printf_extension_arginfo (const struct printf_info *info,
167 size_t n, int *argtypes);
168 #endif
170 struct _GstDebugMessage
171 {
172 gchar *message;
173 const gchar *format;
174 va_list arguments;
175 };
177 /* list of all name/level pairs from --gst-debug and GST_DEBUG */
178 static GStaticMutex __level_name_mutex = G_STATIC_MUTEX_INIT;
179 static GSList *__level_name = NULL;
180 typedef struct
181 {
182 GPatternSpec *pat;
183 GstDebugLevel level;
184 }
185 LevelNameEntry;
187 /* list of all categories */
188 static GStaticMutex __cat_mutex = G_STATIC_MUTEX_INIT;
189 static GSList *__categories = NULL;
191 /* all registered debug handlers */
192 typedef struct
193 {
194 GstLogFunction func;
195 gpointer user_data;
196 }
197 LogFuncEntry;
198 static GStaticMutex __log_func_mutex = G_STATIC_MUTEX_INIT;
199 static GSList *__log_functions = NULL;
201 static gint __default_level;
202 static gint __use_color;
204 /* disabled by default, as soon as some threshold is set > NONE,
205 * it becomes enabled. */
206 gboolean __gst_debug_enabled = FALSE;
207 GstDebugLevel __gst_debug_min = GST_LEVEL_NONE;
209 GstDebugCategory *GST_CAT_DEFAULT = NULL;
211 GstDebugCategory *GST_CAT_GST_INIT = NULL;
212 GstDebugCategory *GST_CAT_AUTOPLUG = NULL;
213 GstDebugCategory *GST_CAT_AUTOPLUG_ATTEMPT = NULL;
214 GstDebugCategory *GST_CAT_PARENTAGE = NULL;
215 GstDebugCategory *GST_CAT_STATES = NULL;
216 GstDebugCategory *GST_CAT_SCHEDULING = NULL;
218 GstDebugCategory *GST_CAT_BUFFER = NULL;
219 GstDebugCategory *GST_CAT_BUS = NULL;
220 GstDebugCategory *GST_CAT_CAPS = NULL;
221 GstDebugCategory *GST_CAT_CLOCK = NULL;
222 GstDebugCategory *GST_CAT_ELEMENT_PADS = NULL;
223 GstDebugCategory *GST_CAT_PADS = NULL;
224 GstDebugCategory *GST_CAT_PIPELINE = NULL;
225 GstDebugCategory *GST_CAT_PLUGIN_LOADING = NULL;
226 GstDebugCategory *GST_CAT_PLUGIN_INFO = NULL;
227 GstDebugCategory *GST_CAT_PROPERTIES = NULL;
228 GstDebugCategory *GST_CAT_TYPES = NULL;
229 GstDebugCategory *GST_CAT_XML = NULL;
230 GstDebugCategory *GST_CAT_NEGOTIATION = NULL;
231 GstDebugCategory *GST_CAT_REFCOUNTING = NULL;
232 GstDebugCategory *GST_CAT_ERROR_SYSTEM = NULL;
233 GstDebugCategory *GST_CAT_EVENT = NULL;
234 GstDebugCategory *GST_CAT_MESSAGE = NULL;
235 GstDebugCategory *GST_CAT_PARAMS = NULL;
236 GstDebugCategory *GST_CAT_CALL_TRACE = NULL;
237 GstDebugCategory *GST_CAT_SIGNAL = NULL;
238 GstDebugCategory *GST_CAT_PROBE = NULL;
239 GstDebugCategory *GST_CAT_REGISTRY = NULL;
240 GstDebugCategory *GST_CAT_QOS = NULL;
242 /* FIXME: export this? */
243 gboolean
244 _priv_gst_in_valgrind (void)
245 {
246 static enum
247 {
248 GST_VG_UNCHECKED,
249 GST_VG_NO_VALGRIND,
250 GST_VG_INSIDE
251 }
252 in_valgrind = GST_VG_UNCHECKED;
254 if (in_valgrind == GST_VG_UNCHECKED) {
255 #ifdef HAVE_VALGRIND_H
256 if (RUNNING_ON_VALGRIND) {
257 GST_CAT_INFO (GST_CAT_GST_INIT, "we're running inside valgrind");
258 printf ("GStreamer has detected that it is running inside valgrind.\n");
259 printf ("It might now take different code paths to ease debugging.\n");
260 printf ("Of course, this may also lead to different bugs.\n");
261 in_valgrind = GST_VG_INSIDE;
262 } else {
263 GST_CAT_LOG (GST_CAT_GST_INIT, "not doing extra valgrind stuff");
264 in_valgrind = GST_VG_NO_VALGRIND;
265 }
266 #else
267 in_valgrind = GST_VG_NO_VALGRIND;
268 #endif
269 g_assert (in_valgrind == GST_VG_NO_VALGRIND ||
270 in_valgrind == GST_VG_INSIDE);
271 }
272 return (in_valgrind == GST_VG_INSIDE) ? TRUE : FALSE;
273 }
275 /**
276 * _gst_debug_init:
277 *
278 * Initializes the debugging system.
279 * Normally you don't want to call this, because gst_init() does it for you.
280 */
281 void
282 _gst_debug_init (void)
283 {
284 g_atomic_int_set (&__default_level, GST_LEVEL_DEFAULT);
285 g_atomic_int_set (&__use_color, 1);
287 /* get time we started for debugging messages */
288 _priv_gst_info_start_time = gst_util_get_timestamp ();
290 #ifdef HAVE_PRINTF_EXTENSION
291 register_printf_function (GST_PTR_FORMAT[0], _gst_info_printf_extension_ptr,
292 _gst_info_printf_extension_arginfo);
293 register_printf_function (GST_SEGMENT_FORMAT[0],
294 _gst_info_printf_extension_segment, _gst_info_printf_extension_arginfo);
295 #endif
297 /* do NOT use a single debug function before this line has been run */
298 GST_CAT_DEFAULT = _gst_debug_category_new ("default",
299 GST_DEBUG_UNDERLINE, NULL);
300 _GST_CAT_DEBUG = _gst_debug_category_new ("GST_DEBUG",
301 GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, "debugging subsystem");
303 gst_debug_add_log_function (gst_debug_log_default, NULL);
305 /* FIXME: add descriptions here */
306 GST_CAT_GST_INIT = _gst_debug_category_new ("GST_INIT",
307 GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
308 GST_CAT_AUTOPLUG = _gst_debug_category_new ("GST_AUTOPLUG",
309 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
310 GST_CAT_AUTOPLUG_ATTEMPT = _gst_debug_category_new ("GST_AUTOPLUG_ATTEMPT",
311 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN | GST_DEBUG_BG_BLUE, NULL);
312 GST_CAT_PARENTAGE = _gst_debug_category_new ("GST_PARENTAGE",
313 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
314 GST_CAT_STATES = _gst_debug_category_new ("GST_STATES",
315 GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
316 GST_CAT_SCHEDULING = _gst_debug_category_new ("GST_SCHEDULING",
317 GST_DEBUG_BOLD | GST_DEBUG_FG_MAGENTA, NULL);
318 GST_CAT_BUFFER = _gst_debug_category_new ("GST_BUFFER",
319 GST_DEBUG_BOLD | GST_DEBUG_BG_GREEN, NULL);
320 GST_CAT_BUS = _gst_debug_category_new ("GST_BUS", GST_DEBUG_BG_YELLOW, NULL);
321 GST_CAT_CAPS = _gst_debug_category_new ("GST_CAPS",
322 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
323 GST_CAT_CLOCK = _gst_debug_category_new ("GST_CLOCK",
324 GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, NULL);
325 GST_CAT_ELEMENT_PADS = _gst_debug_category_new ("GST_ELEMENT_PADS",
326 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
327 GST_CAT_PADS = _gst_debug_category_new ("GST_PADS",
328 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
329 GST_CAT_PIPELINE = _gst_debug_category_new ("GST_PIPELINE",
330 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
331 GST_CAT_PLUGIN_LOADING = _gst_debug_category_new ("GST_PLUGIN_LOADING",
332 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
333 GST_CAT_PLUGIN_INFO = _gst_debug_category_new ("GST_PLUGIN_INFO",
334 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
335 GST_CAT_PROPERTIES = _gst_debug_category_new ("GST_PROPERTIES",
336 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_BLUE, NULL);
337 GST_CAT_TYPES = _gst_debug_category_new ("GST_TYPES",
338 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
339 GST_CAT_XML = _gst_debug_category_new ("GST_XML",
340 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
341 GST_CAT_NEGOTIATION = _gst_debug_category_new ("GST_NEGOTIATION",
342 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
343 GST_CAT_REFCOUNTING = _gst_debug_category_new ("GST_REFCOUNTING",
344 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_BLUE, NULL);
345 GST_CAT_ERROR_SYSTEM = _gst_debug_category_new ("GST_ERROR_SYSTEM",
346 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_WHITE, NULL);
348 GST_CAT_EVENT = _gst_debug_category_new ("GST_EVENT",
349 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
350 GST_CAT_MESSAGE = _gst_debug_category_new ("GST_MESSAGE",
351 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
352 GST_CAT_PARAMS = _gst_debug_category_new ("GST_PARAMS",
353 GST_DEBUG_BOLD | GST_DEBUG_FG_BLACK | GST_DEBUG_BG_YELLOW, NULL);
354 GST_CAT_CALL_TRACE = _gst_debug_category_new ("GST_CALL_TRACE",
355 GST_DEBUG_BOLD, NULL);
356 GST_CAT_SIGNAL = _gst_debug_category_new ("GST_SIGNAL",
357 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
358 GST_CAT_PROBE = _gst_debug_category_new ("GST_PROBE",
359 GST_DEBUG_BOLD | GST_DEBUG_FG_GREEN, "pad probes");
360 GST_CAT_REGISTRY = _gst_debug_category_new ("GST_REGISTRY", 0, "registry");
361 GST_CAT_QOS = _gst_debug_category_new ("GST_QOS", 0, "QoS");
364 /* print out the valgrind message if we're in valgrind */
365 _priv_gst_in_valgrind ();
366 }
368 /* we can't do this further above, because we initialize the GST_CAT_DEFAULT struct */
369 #define GST_CAT_DEFAULT _GST_CAT_DEBUG
371 /**
372 * gst_debug_log:
373 * @category: category to log
374 * @level: level of the message is in
375 * @file: the file that emitted the message, usually the __FILE__ identifier
376 * @function: the function that emitted the message
377 * @line: the line from that the message was emitted, usually __LINE__
378 * @object: the object this message relates to or NULL if none
379 * @format: a printf style format string
380 * @...: optional arguments for the format
381 *
382 * Logs the given message using the currently registered debugging handlers.
383 */
384 void
385 gst_debug_log (GstDebugCategory * category, GstDebugLevel level,
386 const gchar * file, const gchar * function, gint line,
387 GObject * object, const gchar * format, ...)
388 {
389 va_list var_args;
391 va_start (var_args, format);
392 gst_debug_log_valist (category, level, file, function, line, object, format,
393 var_args);
394 va_end (var_args);
395 }
397 /**
398 * gst_debug_log_valist:
399 * @category: category to log
400 * @level: level of the message is in
401 * @file: the file that emitted the message, usually the __FILE__ identifier
402 * @function: the function that emitted the message
403 * @line: the line from that the message was emitted, usually __LINE__
404 * @object: the object this message relates to or NULL if none
405 * @format: a printf style format string
406 * @args: optional arguments for the format
407 *
408 * Logs the given message using the currently registered debugging handlers.
409 */
410 void
411 gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level,
412 const gchar * file, const gchar * function, gint line,
413 GObject * object, const gchar * format, va_list args)
414 {
415 GstDebugMessage message;
416 LogFuncEntry *entry;
417 GSList *handler;
419 #ifdef _MSC_VER
420 gchar *file_basename;
421 #endif
423 g_return_if_fail (category != NULL);
424 g_return_if_fail (file != NULL);
425 g_return_if_fail (function != NULL);
426 g_return_if_fail (format != NULL);
428 #ifdef _MSC_VER
429 /*
430 * The predefined macro __FILE__ is always the exact path given to the
431 * compiler with MSVC, which may or may not be the basename. We work
432 * around it at runtime to improve the readability.
433 */
434 file = file_basename = g_path_get_basename (file);
435 #endif
437 message.message = NULL;
438 message.format = format;
439 G_VA_COPY (message.arguments, args);
441 handler = __log_functions;
442 while (handler) {
443 entry = handler->data;
444 handler = g_slist_next (handler);
445 entry->func (category, level, file, function, line, object, &message,
446 entry->user_data);
447 }
448 g_free (message.message);
449 va_end (message.arguments);
451 #ifdef _MSC_VER
452 g_free (file_basename);
453 #endif
454 }
456 /**
457 * gst_debug_message_get:
458 * @message: a debug message
459 *
460 * Gets the string representation of a #GstDebugMessage. This function is used
461 * in debug handlers to extract the message.
462 *
463 * Returns: the string representation of a #GstDebugMessage.
464 */
465 const gchar *
466 gst_debug_message_get (GstDebugMessage * message)
467 {
468 if (message->message == NULL) {
469 message->message = g_strdup_vprintf (message->format, message->arguments);
470 }
471 return message->message;
472 }
475 static gchar *
476 gst_debug_print_object (gpointer ptr)
477 {
478 GObject *object = (GObject *) ptr;
480 #ifdef unused
481 /* This is a cute trick to detect unmapped memory, but is unportable,
482 * slow, screws around with madvise, and not actually that useful. */
483 {
484 int ret;
486 ret = madvise ((void *) ((unsigned long) ptr & (~0xfff)), 4096, 0);
487 if (ret == -1 && errno == ENOMEM) {
488 buffer = g_strdup_printf ("%p (unmapped memory)", ptr);
489 }
490 }
491 #endif
493 /* nicely printed object */
494 if (object == NULL) {
495 return g_strdup ("(NULL)");
496 }
497 if (*(GType *) ptr == GST_TYPE_CAPS) {
498 return gst_caps_to_string ((GstCaps *) ptr);
499 }
500 if (*(GType *) ptr == GST_TYPE_STRUCTURE) {
501 return gst_structure_to_string ((GstStructure *) ptr);
502 }
503 #ifdef USE_POISONING
504 if (*(guint32 *) ptr == 0xffffffff) {
505 return g_strdup_printf ("<poisoned@%p>", ptr);
506 }
507 #endif
508 if (GST_IS_PAD (object) && GST_OBJECT_NAME (object)) {
509 return g_strdup_printf ("<%s:%s>", GST_DEBUG_PAD_NAME (object));
510 }
511 if (GST_IS_OBJECT (object) && GST_OBJECT_NAME (object)) {
512 return g_strdup_printf ("<%s>", GST_OBJECT_NAME (object));
513 }
514 if (G_IS_OBJECT (object)) {
515 return g_strdup_printf ("<%s@%p>", G_OBJECT_TYPE_NAME (object), object);
516 }
517 if (GST_IS_MESSAGE (object)) {
518 GstMessage *msg = GST_MESSAGE_CAST (object);
519 gchar *s, *ret;
521 if (msg->structure) {
522 s = gst_structure_to_string (msg->structure);
523 } else {
524 s = g_strdup ("(NULL)");
525 }
527 ret = g_strdup_printf ("%s message from element '%s': %s",
528 GST_MESSAGE_TYPE_NAME (msg), (msg->src != NULL) ?
529 GST_ELEMENT_NAME (msg->src) : "(NULL)", s);
530 g_free (s);
531 return ret;
532 }
534 return g_strdup_printf ("%p", ptr);
535 }
537 #ifdef HAVE_PRINTF_EXTENSION
539 static gchar *
540 gst_debug_print_segment (gpointer ptr)
541 {
542 GstSegment *segment = (GstSegment *) ptr;
544 /* nicely printed segment */
545 if (segment == NULL) {
546 return g_strdup ("(NULL)");
547 }
549 switch (segment->format) {
550 case GST_FORMAT_UNDEFINED:{
551 return g_strdup_printf ("UNDEFINED segment");
552 }
553 case GST_FORMAT_TIME:{
554 return g_strdup_printf ("time segment start=%" GST_TIME_FORMAT
555 ", stop=%" GST_TIME_FORMAT ", last_stop=%" GST_TIME_FORMAT
556 ", duration=%" GST_TIME_FORMAT ", rate=%f, applied_rate=%f"
557 ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
558 GST_TIME_ARGS (segment->start), GST_TIME_ARGS (segment->stop),
559 GST_TIME_ARGS (segment->last_stop), GST_TIME_ARGS (segment->duration),
560 segment->rate, segment->applied_rate, (guint) segment->flags,
561 GST_TIME_ARGS (segment->time), GST_TIME_ARGS (segment->accum));
562 }
563 default:{
564 const gchar *format_name;
566 format_name = gst_format_get_name (segment->format);
567 if (G_UNLIKELY (format_name == NULL))
568 format_name = "(UNKNOWN FORMAT)";
569 return g_strdup_printf ("%s segment start=%" G_GINT64_FORMAT
570 ", stop=%" G_GINT64_FORMAT ", last_stop=%" G_GINT64_FORMAT
571 ", duration=%" G_GINT64_FORMAT ", rate=%f, applied_rate=%f"
572 ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
573 format_name, segment->start, segment->stop, segment->last_stop,
574 segment->duration, segment->rate, segment->applied_rate,
575 (guint) segment->flags, GST_TIME_ARGS (segment->time),
576 GST_TIME_ARGS (segment->accum));
577 }
578 }
579 }
581 #endif /* HAVE_PRINTF_EXTENSION */
583 /**
584 * gst_debug_construct_term_color:
585 * @colorinfo: the color info
586 *
587 * Constructs a string that can be used for getting the desired color in color
588 * terminals.
589 * You need to free the string after use.
590 *
591 * Returns: a string containing the color definition
592 */
593 gchar *
594 gst_debug_construct_term_color (guint colorinfo)
595 {
596 GString *color;
598 color = g_string_new ("\033[00");
600 if (colorinfo & GST_DEBUG_BOLD) {
601 g_string_append_len (color, ";01", 3);
602 }
603 if (colorinfo & GST_DEBUG_UNDERLINE) {
604 g_string_append_len (color, ";04", 3);
605 }
606 if (colorinfo & GST_DEBUG_FG_MASK) {
607 g_string_append_printf (color, ";3%1d", colorinfo & GST_DEBUG_FG_MASK);
608 }
609 if (colorinfo & GST_DEBUG_BG_MASK) {
610 g_string_append_printf (color, ";4%1d",
611 (colorinfo & GST_DEBUG_BG_MASK) >> 4);
612 }
613 g_string_append_c (color, 'm');
615 return g_string_free (color, FALSE);
616 }
618 /**
619 * gst_debug_construct_win_color:
620 * @colorinfo: the color info
621 *
622 * Constructs an integer that can be used for getting the desired color in
623 * windows' terminals (cmd.exe). As there is no mean to underline, we simply
624 * ignore this attribute.
625 *
626 * This function returns 0 on non-windows machines.
627 *
628 * Returns: an integer containing the color definition
629 *
630 * Since: 0.10.23
631 */
632 gint
633 gst_debug_construct_win_color (guint colorinfo)
634 {
635 gint color = 0;
636 #ifdef G_OS_WIN32
637 static const guchar ansi_to_win_fg[8] = {
638 0, /* black */
639 FOREGROUND_RED, /* red */
640 FOREGROUND_GREEN, /* green */
641 FOREGROUND_RED | FOREGROUND_GREEN, /* yellow */
642 FOREGROUND_BLUE, /* blue */
643 FOREGROUND_RED | FOREGROUND_BLUE, /* magenta */
644 FOREGROUND_GREEN | FOREGROUND_BLUE, /* cyan */
645 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE /* white */
646 };
647 static const guchar ansi_to_win_bg[8] = {
648 0,
649 BACKGROUND_RED,
650 BACKGROUND_GREEN,
651 BACKGROUND_RED | BACKGROUND_GREEN,
652 BACKGROUND_BLUE,
653 BACKGROUND_RED | BACKGROUND_BLUE,
654 BACKGROUND_GREEN | FOREGROUND_BLUE,
655 BACKGROUND_RED | BACKGROUND_GREEN | BACKGROUND_BLUE
656 };
658 /* we draw black as white, as cmd.exe can only have black bg */
659 if (colorinfo == 0) {
660 return ansi_to_win_fg[7];
661 }
663 if (colorinfo & GST_DEBUG_BOLD) {
664 color |= FOREGROUND_INTENSITY;
665 }
666 if (colorinfo & GST_DEBUG_FG_MASK) {
667 color |= ansi_to_win_fg[colorinfo & GST_DEBUG_FG_MASK];
668 }
669 if (colorinfo & GST_DEBUG_BG_MASK) {
670 color |= ansi_to_win_bg[(colorinfo & GST_DEBUG_BG_MASK) >> 4];
671 }
672 #endif
673 return color;
674 }
676 /* width of %p varies depending on actual value of pointer, which can make
677 * output unevenly aligned if multiple threads are involved, hence the %14p
678 * (should really be %18p, but %14p seems a good compromise between too many
679 * white spaces and likely unalignment on my system) */
680 #if defined (GLIB_SIZEOF_VOID_P) && GLIB_SIZEOF_VOID_P == 8
681 #define PTR_FMT "%14p"
682 #else
683 #define PTR_FMT "%10p"
684 #endif
685 #define PID_FMT "%5d"
686 #define CAT_FMT "%20s %s:%d:%s:%s"
688 #ifdef G_OS_WIN32
689 static const guchar levelcolormap[] = {
690 /* GST_LEVEL_NONE */
691 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
692 /* GST_LEVEL_ERROR */
693 FOREGROUND_RED | FOREGROUND_INTENSITY,
694 /* GST_LEVEL_WARNING */
695 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_INTENSITY,
696 /* GST_LEVEL_INFO */
697 FOREGROUND_GREEN | FOREGROUND_INTENSITY,
698 /* GST_LEVEL_DEBUG */
699 FOREGROUND_GREEN | FOREGROUND_BLUE,
700 /* GST_LEVEL_LOG */
701 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE
702 };
704 static const guchar available_colors[6] = {
705 FOREGROUND_RED, FOREGROUND_GREEN, FOREGROUND_RED | FOREGROUND_GREEN,
706 FOREGROUND_BLUE, FOREGROUND_RED | FOREGROUND_BLUE,
707 FOREGROUND_GREEN | FOREGROUND_BLUE,
708 };
709 #else
710 static const gchar *levelcolormap[] = {
711 "\033[37m", /* GST_LEVEL_NONE */
712 "\033[31;01m", /* GST_LEVEL_ERROR */
713 "\033[33;01m", /* GST_LEVEL_WARNING */
714 "\033[32;01m", /* GST_LEVEL_INFO */
715 "\033[36m", /* GST_LEVEL_DEBUG */
716 "\033[37m" /* GST_LEVEL_LOG */
717 };
718 #endif
720 /**
721 * gst_debug_log_default:
722 * @category: category to log
723 * @level: level of the message
724 * @file: the file that emitted the message, usually the __FILE__ identifier
725 * @function: the function that emitted the message
726 * @line: the line from that the message was emitted, usually __LINE__
727 * @message: the actual message
728 * @object: the object this message relates to or NULL if none
729 * @unused: an unused variable, reserved for some user_data.
730 *
731 * The default logging handler used by GStreamer. Logging functions get called
732 * whenever a macro like GST_DEBUG or similar is used. This function outputs the
733 * message and additional info using the glib error handler.
734 * You can add other handlers by using gst_debug_add_log_function().
735 * And you can remove this handler by calling
736 * gst_debug_remove_log_function(gst_debug_log_default);
737 */
738 void
739 gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level,
740 const gchar * file, const gchar * function, gint line,
741 GObject * object, GstDebugMessage * message, gpointer unused)
742 {
743 gint pid;
744 GstClockTime elapsed;
745 gchar *obj = NULL;
746 gboolean free_obj = TRUE;
747 gboolean is_colored;
749 if (level > gst_debug_category_get_threshold (category))
750 return;
752 pid = getpid ();
753 is_colored = gst_debug_is_colored ();
755 elapsed = GST_CLOCK_DIFF (_priv_gst_info_start_time,
756 gst_util_get_timestamp ());
758 if (object) {
759 obj = gst_debug_print_object (object);
760 } else {
761 obj = "\0";
762 free_obj = FALSE;
763 }
765 if (is_colored) {
766 #ifndef G_OS_WIN32
767 gchar *color = NULL;
768 gchar *clear;
769 gchar pidcolor[10];
770 const gchar *levelcolor;
772 color = gst_debug_construct_term_color (gst_debug_category_get_color
773 (category));
774 clear = "\033[00m";
775 g_sprintf (pidcolor, "\033[3%1dm", pid % 6 + 31);
776 levelcolor = levelcolormap[level];
778 #define PRINT_FMT " %s"PID_FMT"%s "PTR_FMT" %s%s%s %s"CAT_FMT"%s %s\n"
779 g_printerr ("%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed),
780 pidcolor, pid, clear, g_thread_self (), levelcolor,
781 gst_debug_level_get_name (level), clear, color,
782 gst_debug_category_get_name (category), file, line, function, obj,
783 clear, gst_debug_message_get (message));
784 #undef PRINT_FMT
785 g_free (color);
786 #else
787 const gint clear = FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE;
788 #define SET_COLOR(c) \
789 SetConsoleTextAttribute (GetStdHandle (STD_ERROR_HANDLE), (c));
790 /* timestamp */
791 g_printerr ("%" GST_TIME_FORMAT " ", GST_TIME_ARGS (elapsed));
792 /* pid */
793 SET_COLOR (available_colors[pid % 6]);
794 g_printerr (PID_FMT, pid);
795 /* thread */
796 SET_COLOR (clear);
797 g_printerr (" " PTR_FMT " ", g_thread_self ());
798 /* level */
799 SET_COLOR (levelcolormap[level]);
800 g_printerr ("%s ", gst_debug_level_get_name (level));
801 /* category */
802 SET_COLOR (gst_debug_construct_win_color (gst_debug_category_get_color
803 (category)));
804 g_printerr (CAT_FMT, gst_debug_category_get_name (category),
805 file, line, function, obj);
806 /* message */
807 SET_COLOR (clear);
808 g_printerr (" %s\n", gst_debug_message_get (message));
809 #endif
810 } else {
811 #define PRINT_FMT " "PID_FMT" "PTR_FMT" %s "CAT_FMT" %s\n"
812 g_printerr ("%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed), pid,
813 g_thread_self (), gst_debug_level_get_name (level),
814 gst_debug_category_get_name (category), file, line, function, obj,
815 gst_debug_message_get (message));
816 #undef PRINT_FMT
817 }
819 if (free_obj)
820 g_free (obj);
821 }
823 /**
824 * gst_debug_level_get_name:
825 * @level: the level to get the name for
826 *
827 * Get the string representation of a debugging level
828 *
829 * Returns: the name
830 */
831 const gchar *
832 gst_debug_level_get_name (GstDebugLevel level)
833 {
834 switch (level) {
835 case GST_LEVEL_NONE:
836 return "";
837 case GST_LEVEL_ERROR:
838 return "ERROR";
839 case GST_LEVEL_WARNING:
840 return "WARN ";
841 case GST_LEVEL_INFO:
842 return "INFO ";
843 case GST_LEVEL_DEBUG:
844 return "DEBUG";
845 case GST_LEVEL_LOG:
846 return "LOG ";
847 default:
848 g_warning ("invalid level specified for gst_debug_level_get_name");
849 return "";
850 }
851 }
853 /**
854 * gst_debug_add_log_function:
855 * @func: the function to use
856 * @data: user data
857 *
858 * Adds the logging function to the list of logging functions.
859 * Be sure to use G_GNUC_NO_INSTRUMENT on that function, it is needed.
860 */
861 void
862 gst_debug_add_log_function (GstLogFunction func, gpointer data)
863 {
864 LogFuncEntry *entry;
865 GSList *list;
867 g_return_if_fail (func != NULL);
869 entry = g_new (LogFuncEntry, 1);
870 entry->func = func;
871 entry->user_data = data;
872 /* FIXME: we leak the old list here - other threads might access it right now
873 * in gst_debug_logv. Another solution is to lock the mutex in gst_debug_logv,
874 * but that is waaay costly.
875 * It'd probably be clever to use some kind of RCU here, but I don't know
876 * anything about that.
877 */
878 g_static_mutex_lock (&__log_func_mutex);
879 list = g_slist_copy (__log_functions);
880 __log_functions = g_slist_prepend (list, entry);
881 g_static_mutex_unlock (&__log_func_mutex);
883 GST_DEBUG ("prepended log function %p (user data %p) to log functions",
884 func, data);
885 }
887 static gint
888 gst_debug_compare_log_function_by_func (gconstpointer entry, gconstpointer func)
889 {
890 gpointer entryfunc = (gpointer) (((LogFuncEntry *) entry)->func);
892 return (entryfunc < func) ? -1 : (entryfunc > func) ? 1 : 0;
893 }
895 static gint
896 gst_debug_compare_log_function_by_data (gconstpointer entry, gconstpointer data)
897 {
898 gpointer entrydata = ((LogFuncEntry *) entry)->user_data;
900 return (entrydata < data) ? -1 : (entrydata > data) ? 1 : 0;
901 }
903 static guint
904 gst_debug_remove_with_compare_func (GCompareFunc func, gpointer data)
905 {
906 GSList *found;
907 GSList *new;
908 guint removals = 0;
910 g_static_mutex_lock (&__log_func_mutex);
911 new = __log_functions;
912 while ((found = g_slist_find_custom (new, data, func))) {
913 if (new == __log_functions) {
914 /* make a copy when we have the first hit, so that we modify the copy and
915 * make that the new list later */
916 new = g_slist_copy (new);
917 continue;
918 }
919 g_free (found->data);
920 new = g_slist_delete_link (new, found);
921 removals++;
922 }
923 /* FIXME: We leak the old list here. See _add_log_function for why. */
924 __log_functions = new;
925 g_static_mutex_unlock (&__log_func_mutex);
927 return removals;
928 }
930 /**
931 * gst_debug_remove_log_function:
932 * @func: the log function to remove
933 *
934 * Removes all registered instances of the given logging functions.
935 *
936 * Returns: How many instances of the function were removed
937 */
938 guint
939 gst_debug_remove_log_function (GstLogFunction func)
940 {
941 guint removals;
943 g_return_val_if_fail (func != NULL, 0);
945 removals =
946 gst_debug_remove_with_compare_func
947 (gst_debug_compare_log_function_by_func, (gpointer) func);
948 GST_DEBUG ("removed log function %p %d times from log function list", func,
949 removals);
951 return removals;
952 }
954 /**
955 * gst_debug_remove_log_function_by_data:
956 * @data: user data of the log function to remove
957 *
958 * Removes all registered instances of log functions with the given user data.
959 *
960 * Returns: How many instances of the function were removed
961 */
962 guint
963 gst_debug_remove_log_function_by_data (gpointer data)
964 {
965 guint removals;
967 removals =
968 gst_debug_remove_with_compare_func
969 (gst_debug_compare_log_function_by_data, data);
970 GST_DEBUG
971 ("removed %d log functions with user data %p from log function list",
972 removals, data);
974 return removals;
975 }
977 /**
978 * gst_debug_set_colored:
979 * @colored: Whether to use colored output or not
980 *
981 * Sets or unsets the use of coloured debugging output.
982 */
983 void
984 gst_debug_set_colored (gboolean colored)
985 {
986 g_atomic_int_set (&__use_color, colored ? 1 : 0);
987 }
989 /**
990 * gst_debug_is_colored:
991 *
992 * Checks if the debugging output should be colored.
993 *
994 * Returns: TRUE, if the debug output should be colored.
995 */
996 gboolean
997 gst_debug_is_colored (void)
998 {
999 return g_atomic_int_get (&__use_color) == 0 ? FALSE : TRUE;
1000 }
1002 /**
1003 * gst_debug_set_active:
1004 * @active: Whether to use debugging output or not
1005 *
1006 * If activated, debugging messages are sent to the debugging
1007 * handlers.
1008 * It makes sense to deactivate it for speed issues.
1009 * <note><para>This function is not threadsafe. It makes sense to only call it
1010 * during initialization.</para></note>
1011 */
1012 void
1013 gst_debug_set_active (gboolean active)
1014 {
1015 __gst_debug_enabled = active;
1016 if (active)
1017 __gst_debug_min = GST_LEVEL_COUNT;
1018 else
1019 __gst_debug_min = GST_LEVEL_NONE;
1020 }
1022 /**
1023 * gst_debug_is_active:
1024 *
1025 * Checks if debugging output is activated.
1026 *
1027 * Returns: TRUE, if debugging is activated
1028 */
1029 gboolean
1030 gst_debug_is_active (void)
1031 {
1032 return __gst_debug_enabled;
1033 }
1035 /**
1036 * gst_debug_set_default_threshold:
1037 * @level: level to set
1038 *
1039 * Sets the default threshold to the given level and updates all categories to
1040 * use this threshold.
1041 */
1042 void
1043 gst_debug_set_default_threshold (GstDebugLevel level)
1044 {
1045 g_atomic_int_set (&__default_level, level);
1046 gst_debug_reset_all_thresholds ();
1047 }
1049 /**
1050 * gst_debug_get_default_threshold:
1051 *
1052 * Returns the default threshold that is used for new categories.
1053 *
1054 * Returns: the default threshold level
1055 */
1056 GstDebugLevel
1057 gst_debug_get_default_threshold (void)
1058 {
1059 return (GstDebugLevel) g_atomic_int_get (&__default_level);
1060 }
1062 static void
1063 gst_debug_reset_threshold (gpointer category, gpointer unused)
1064 {
1065 GstDebugCategory *cat = (GstDebugCategory *) category;
1066 GSList *walk;
1068 g_static_mutex_lock (&__level_name_mutex);
1069 walk = __level_name;
1070 while (walk) {
1071 LevelNameEntry *entry = walk->data;
1073 walk = g_slist_next (walk);
1074 if (g_pattern_match_string (entry->pat, cat->name)) {
1075 GST_LOG ("category %s matches pattern %p - gets set to level %d",
1076 cat->name, entry->pat, entry->level);
1077 gst_debug_category_set_threshold (cat, entry->level);
1078 goto exit;
1079 }
1080 }
1081 gst_debug_category_set_threshold (cat, gst_debug_get_default_threshold ());
1083 exit:
1084 g_static_mutex_unlock (&__level_name_mutex);
1085 }
1087 static void
1088 gst_debug_reset_all_thresholds (void)
1089 {
1090 g_static_mutex_lock (&__cat_mutex);
1091 g_slist_foreach (__categories, gst_debug_reset_threshold, NULL);
1092 g_static_mutex_unlock (&__cat_mutex);
1093 }
1095 static void
1096 for_each_threshold_by_entry (gpointer data, gpointer user_data)
1097 {
1098 GstDebugCategory *cat = (GstDebugCategory *) data;
1099 LevelNameEntry *entry = (LevelNameEntry *) user_data;
1101 if (g_pattern_match_string (entry->pat, cat->name)) {
1102 GST_LOG ("category %s matches pattern %p - gets set to level %d",
1103 cat->name, entry->pat, entry->level);
1104 gst_debug_category_set_threshold (cat, entry->level);
1105 }
1106 }
1108 /**
1109 * gst_debug_set_threshold_for_name:
1110 * @name: name of the categories to set
1111 * @level: level to set them to
1112 *
1113 * Sets all categories which match the given glob style pattern to the given
1114 * level.
1115 */
1116 void
1117 gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level)
1118 {
1119 GPatternSpec *pat;
1120 LevelNameEntry *entry;
1122 g_return_if_fail (name != NULL);
1124 pat = g_pattern_spec_new (name);
1125 entry = g_new (LevelNameEntry, 1);
1126 entry->pat = pat;
1127 entry->level = level;
1128 g_static_mutex_lock (&__level_name_mutex);
1129 __level_name = g_slist_prepend (__level_name, entry);
1130 g_static_mutex_unlock (&__level_name_mutex);
1131 g_static_mutex_lock (&__cat_mutex);
1132 g_slist_foreach (__categories, for_each_threshold_by_entry, entry);
1133 g_static_mutex_unlock (&__cat_mutex);
1134 }
1136 /**
1137 * gst_debug_unset_threshold_for_name:
1138 * @name: name of the categories to set
1139 *
1140 * Resets all categories with the given name back to the default level.
1141 */
1142 void
1143 gst_debug_unset_threshold_for_name (const gchar * name)
1144 {
1145 GSList *walk;
1146 GPatternSpec *pat;
1148 g_return_if_fail (name != NULL);
1150 pat = g_pattern_spec_new (name);
1151 g_static_mutex_lock (&__level_name_mutex);
1152 walk = __level_name;
1153 /* improve this if you want, it's mighty slow */
1154 while (walk) {
1155 LevelNameEntry *entry = walk->data;
1157 if (g_pattern_spec_equal (entry->pat, pat)) {
1158 __level_name = g_slist_remove_link (__level_name, walk);
1159 g_pattern_spec_free (entry->pat);
1160 g_free (entry);
1161 g_slist_free_1 (walk);
1162 walk = __level_name;
1163 }
1164 }
1165 g_static_mutex_unlock (&__level_name_mutex);
1166 g_pattern_spec_free (pat);
1167 gst_debug_reset_all_thresholds ();
1168 }
1170 GstDebugCategory *
1171 _gst_debug_category_new (const gchar * name, guint color,
1172 const gchar * description)
1173 {
1174 GstDebugCategory *cat;
1176 g_return_val_if_fail (name != NULL, NULL);
1178 cat = g_new (GstDebugCategory, 1);
1179 cat->name = g_strdup (name);
1180 cat->color = color;
1181 if (description != NULL) {
1182 cat->description = g_strdup (description);
1183 } else {
1184 cat->description = g_strdup ("no description");
1185 }
1186 g_atomic_int_set (&cat->threshold, 0);
1187 gst_debug_reset_threshold (cat, NULL);
1189 /* add to category list */
1190 g_static_mutex_lock (&__cat_mutex);
1191 __categories = g_slist_prepend (__categories, cat);
1192 g_static_mutex_unlock (&__cat_mutex);
1194 return cat;
1195 }
1197 /**
1198 * gst_debug_category_free:
1199 * @category: #GstDebugCategory to free.
1200 *
1201 * Removes and frees the category and all associated resources.
1202 */
1203 void
1204 gst_debug_category_free (GstDebugCategory * category)
1205 {
1206 if (category == NULL)
1207 return;
1209 /* remove from category list */
1210 g_static_mutex_lock (&__cat_mutex);
1211 __categories = g_slist_remove (__categories, category);
1212 g_static_mutex_unlock (&__cat_mutex);
1214 g_free ((gpointer) category->name);
1215 g_free ((gpointer) category->description);
1216 g_free (category);
1217 }
1219 /**
1220 * gst_debug_category_set_threshold:
1221 * @category: a #GstDebugCategory to set threshold of.
1222 * @level: the #GstDebugLevel threshold to set.
1223 *
1224 * Sets the threshold of the category to the given level. Debug information will
1225 * only be output if the threshold is lower or equal to the level of the
1226 * debugging message.
1227 * <note><para>
1228 * Do not use this function in production code, because other functions may
1229 * change the threshold of categories as side effect. It is however a nice
1230 * function to use when debugging (even from gdb).
1231 * </para></note>
1232 */
1233 void
1234 gst_debug_category_set_threshold (GstDebugCategory * category,
1235 GstDebugLevel level)
1236 {
1237 g_return_if_fail (category != NULL);
1239 if (level > __gst_debug_min) {
1240 __gst_debug_enabled = TRUE;
1241 __gst_debug_min = level;
1242 }
1244 g_atomic_int_set (&category->threshold, level);
1245 }
1247 /**
1248 * gst_debug_category_reset_threshold:
1249 * @category: a #GstDebugCategory to reset threshold of.
1250 *
1251 * Resets the threshold of the category to the default level. Debug information
1252 * will only be output if the threshold is lower or equal to the level of the
1253 * debugging message.
1254 * Use this function to set the threshold back to where it was after using
1255 * gst_debug_category_set_threshold().
1256 */
1257 void
1258 gst_debug_category_reset_threshold (GstDebugCategory * category)
1259 {
1260 gst_debug_reset_threshold (category, NULL);
1261 }
1263 /**
1264 * gst_debug_category_get_threshold:
1265 * @category: a #GstDebugCategory to get threshold of.
1266 *
1267 * Returns the threshold of a #GstDebugCategory.
1268 *
1269 * Returns: the #GstDebugLevel that is used as threshold.
1270 */
1271 GstDebugLevel
1272 gst_debug_category_get_threshold (GstDebugCategory * category)
1273 {
1274 return g_atomic_int_get (&category->threshold);
1275 }
1277 /**
1278 * gst_debug_category_get_name:
1279 * @category: a #GstDebugCategory to get name of.
1280 *
1281 * Returns the name of a debug category.
1282 *
1283 * Returns: the name of the category.
1284 */
1285 const gchar *
1286 gst_debug_category_get_name (GstDebugCategory * category)
1287 {
1288 return category->name;
1289 }
1291 /**
1292 * gst_debug_category_get_color:
1293 * @category: a #GstDebugCategory to get the color of.
1294 *
1295 * Returns the color of a debug category used when printing output in this
1296 * category.
1297 *
1298 * Returns: the color of the category.
1299 */
1300 guint
1301 gst_debug_category_get_color (GstDebugCategory * category)
1302 {
1303 return category->color;
1304 }
1306 /**
1307 * gst_debug_category_get_description:
1308 * @category: a #GstDebugCategory to get the description of.
1309 *
1310 * Returns the description of a debug category.
1311 *
1312 * Returns: the description of the category.
1313 */
1314 const gchar *
1315 gst_debug_category_get_description (GstDebugCategory * category)
1316 {
1317 return category->description;
1318 }
1320 /**
1321 * gst_debug_get_all_categories:
1322 *
1323 * Returns a snapshot of a all categories that are currently in use . This list
1324 * may change anytime.
1325 * The caller has to free the list after use.
1326 *
1327 * Returns: the list of categories
1328 */
1329 GSList *
1330 gst_debug_get_all_categories (void)
1331 {
1332 GSList *ret;
1334 g_static_mutex_lock (&__cat_mutex);
1335 ret = g_slist_copy (__categories);
1336 g_static_mutex_unlock (&__cat_mutex);
1338 return ret;
1339 }
1341 /*** FUNCTION POINTERS ********************************************************/
1343 static GHashTable *__gst_function_pointers; /* NULL */
1344 static GStaticMutex __dbg_functions_mutex = G_STATIC_MUTEX_INIT;
1346 const gchar *
1347 _gst_debug_nameof_funcptr (GstDebugFuncPtr ptr)
1348 G_GNUC_NO_INSTRUMENT;
1350 /* This function MUST NOT return NULL */
1351 const gchar *_gst_debug_nameof_funcptr (GstDebugFuncPtr func)
1352 {
1353 gchar *ptrname;
1355 #ifdef HAVE_DLADDR
1356 Dl_info dl_info;
1357 #endif
1359 if (G_UNLIKELY (func == NULL))
1360 return "(NULL)";
1362 g_static_mutex_lock (&__dbg_functions_mutex);
1363 if (G_LIKELY (__gst_function_pointers)) {
1364 ptrname = g_hash_table_lookup (__gst_function_pointers, (gpointer) func);
1365 g_static_mutex_unlock (&__dbg_functions_mutex);
1366 if (G_LIKELY (ptrname))
1367 return ptrname;
1368 } else {
1369 g_static_mutex_unlock (&__dbg_functions_mutex);
1370 }
1371 /* we need to create an entry in the hash table for this one so we don't leak
1372 * the name */
1373 #ifdef HAVE_DLADDR
1374 if (dladdr ((gpointer) func, &dl_info) && dl_info.dli_sname) {
1375 gchar *name = g_strdup (dl_info.dli_sname);
1377 _gst_debug_register_funcptr (func, name);
1378 return name;
1379 } else
1380 #endif
1381 {
1382 gchar *name = g_strdup_printf ("%p", (gpointer) func);
1384 _gst_debug_register_funcptr (func, name);
1385 return name;
1386 }
1387 }
1389 void
1390 _gst_debug_register_funcptr (GstDebugFuncPtr func, const gchar * ptrname)
1391 {
1392 gpointer ptr = (gpointer) func;
1394 g_static_mutex_lock (&__dbg_functions_mutex);
1396 if (!__gst_function_pointers)
1397 __gst_function_pointers = g_hash_table_new (g_direct_hash, g_direct_equal);
1398 if (!g_hash_table_lookup (__gst_function_pointers, ptr))
1399 g_hash_table_insert (__gst_function_pointers, ptr, (gpointer) ptrname);
1401 g_static_mutex_unlock (&__dbg_functions_mutex);
1402 }
1404 /*** PRINTF EXTENSIONS ********************************************************/
1406 #ifdef HAVE_PRINTF_EXTENSION
1407 static int
1408 _gst_info_printf_extension_ptr (FILE * stream, const struct printf_info *info,
1409 const void *const *args)
1410 {
1411 char *buffer;
1412 int len;
1413 void *ptr;
1415 buffer = NULL;
1416 ptr = *(void **) args[0];
1418 buffer = gst_debug_print_object (ptr);
1419 len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1420 buffer);
1422 g_free (buffer);
1423 return len;
1424 }
1426 static int
1427 _gst_info_printf_extension_segment (FILE * stream,
1428 const struct printf_info *info, const void *const *args)
1429 {
1430 char *buffer;
1431 int len;
1432 void *ptr;
1434 buffer = NULL;
1435 ptr = *(void **) args[0];
1437 buffer = gst_debug_print_segment (ptr);
1438 len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1439 buffer);
1441 g_free (buffer);
1442 return len;
1443 }
1445 static int
1446 _gst_info_printf_extension_arginfo (const struct printf_info *info, size_t n,
1447 int *argtypes)
1448 {
1449 if (n > 0)
1450 argtypes[0] = PA_POINTER;
1451 return 1;
1452 }
1453 #endif /* HAVE_PRINTF_EXTENSION */
1455 #else /* !GST_DISABLE_GST_DEBUG */
1456 guint
1457 gst_debug_remove_log_function (GstLogFunction func)
1458 {
1459 return 0;
1460 }
1462 guint
1463 gst_debug_remove_log_function_by_data (gpointer data)
1464 {
1465 return 0;
1466 }
1468 gboolean
1469 _priv_gst_in_valgrind (void)
1470 {
1471 return FALSE;
1472 }
1474 #endif /* GST_DISABLE_GST_DEBUG */
1477 #ifdef GST_ENABLE_FUNC_INSTRUMENTATION
1478 /* FIXME make this thread specific */
1479 static GSList *stack_trace = NULL;
1481 void
1482 __cyg_profile_func_enter (void *this_fn, void *call_site)
1483 G_GNUC_NO_INSTRUMENT;
1484 void __cyg_profile_func_enter (void *this_fn, void *call_site)
1485 {
1486 gchar *name = _gst_debug_nameof_funcptr (this_fn);
1487 gchar *site = _gst_debug_nameof_funcptr (call_site);
1489 GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "entering function %s from %s", name,
1490 site);
1491 stack_trace =
1492 g_slist_prepend (stack_trace, g_strdup_printf ("%8p in %s from %p (%s)",
1493 this_fn, name, call_site, site));
1495 g_free (name);
1496 g_free (site);
1497 }
1499 void
1500 __cyg_profile_func_exit (void *this_fn, void *call_site)
1501 G_GNUC_NO_INSTRUMENT;
1502 void __cyg_profile_func_exit (void *this_fn, void *call_site)
1503 {
1504 gchar *name = _gst_debug_nameof_funcptr (this_fn);
1506 GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "leaving function %s", name);
1507 g_free (stack_trace->data);
1508 stack_trace = g_slist_delete_link (stack_trace, stack_trace);
1510 g_free (name);
1511 }
1513 /**
1514 * gst_debug_print_stack_trace:
1515 *
1516 * If GST_ENABLE_FUNC_INSTRUMENTATION is defined a stacktrace is available for
1517 * gstreamer code, which can be printed with this function.
1518 */
1519 void
1520 gst_debug_print_stack_trace (void)
1521 {
1522 GSList *walk = stack_trace;
1523 gint count = 0;
1525 if (walk)
1526 walk = g_slist_next (walk);
1528 while (walk) {
1529 gchar *name = (gchar *) walk->data;
1531 g_print ("#%-2d %s\n", count++, name);
1533 walk = g_slist_next (walk);
1534 }
1535 }
1536 #else
1537 void
1538 gst_debug_print_stack_trace (void)
1539 {
1540 /* nothing because it's compiled out */
1541 }
1543 #endif /* GST_ENABLE_FUNC_INSTRUMENTATION */