1 /* GStreamer
2 * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3 * 2000 Wim Taymans <wtay@chello.be>
4 * 2003 Benjamin Otte <in7y118@public.uni-hamburg.de>
5 * Copyright (C) 2008-2009 Tim-Philipp Müller <tim centricular net>
6 *
7 * gstinfo.c: debugging functions
8 *
9 * This library is free software; you can redistribute it and/or
10 * modify it under the terms of the GNU Library General Public
11 * License as published by the Free Software Foundation; either
12 * version 2 of the License, or (at your option) any later version.
13 *
14 * This library is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
17 * Library General Public License for more details.
18 *
19 * You should have received a copy of the GNU Library General Public
20 * License along with this library; if not, write to the
21 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
22 * Boston, MA 02111-1307, USA.
23 */
25 /**
26 * SECTION:gstinfo
27 * @short_description: Debugging and logging facilities
28 * @see_also: #gstreamer-gstconfig, #gstreamer-Gst for command line parameters
29 * and environment variables that affect the debugging output.
30 *
31 * GStreamer's debugging subsystem is an easy way to get information about what
32 * the application is doing. It is not meant for programming errors. Use GLib
33 * methods (g_warning and friends) for that.
34 *
35 * The debugging subsystem works only after GStreamer has been initialized
36 * - for example by calling gst_init().
37 *
38 * The debugging subsystem is used to log informational messages while the
39 * application runs. Each messages has some properties attached to it. Among
40 * these properties are the debugging category, the severity (called "level"
41 * here) and an optional #GObject it belongs to. Each of these messages is sent
42 * to all registered debugging handlers, which then handle the messages.
43 * GStreamer attaches a default handler on startup, which outputs requested
44 * messages to stderr.
45 *
46 * Messages are output by using shortcut macros like #GST_DEBUG,
47 * #GST_CAT_ERROR_OBJECT or similar. These all expand to calling gst_debug_log()
48 * with the right parameters.
49 * The only thing a developer will probably want to do is define his own
50 * categories. This is easily done with 3 lines. At the top of your code,
51 * declare
52 * the variables and set the default category.
53 * <informalexample>
54 * <programlisting>
55 * GST_DEBUG_CATEGORY_STATIC (my_category); // define category (statically)
56 * &hash;define GST_CAT_DEFAULT my_category // set as default
57 * </programlisting>
58 * </informalexample>
59 * After that you only need to initialize the category.
60 * <informalexample>
61 * <programlisting>
62 * GST_DEBUG_CATEGORY_INIT (my_category, "my category",
63 * 0, "This is my very own");
64 * </programlisting>
65 * </informalexample>
66 * Initialization must be done before the category is used first.
67 * Plugins do this
68 * in their plugin_init function, libraries and applications should do that
69 * during their initialization.
70 *
71 * The whole debugging subsystem can be disabled at build time with passing the
72 * --disable-gst-debug switch to configure. If this is done, every function,
73 * macro and even structs described in this file evaluate to default values or
74 * nothing at all.
75 * So don't take addresses of these functions or use other tricks.
76 * If you must do that for some reason, there is still an option.
77 * If the debugging
78 * subsystem was compiled out, #GST_DISABLE_GST_DEBUG is defined in
79 * <gst/gst.h>,
80 * so you can check that before doing your trick.
81 * Disabling the debugging subsystem will give you a slight (read: unnoticeable)
82 * speed increase and will reduce the size of your compiled code. The GStreamer
83 * library itself becomes around 10% smaller.
84 *
85 * Please note that there are naming conventions for the names of debugging
86 * categories. These are explained at GST_DEBUG_CATEGORY_INIT().
87 */
89 #define GST_INFO_C
90 #include "gst_private.h"
91 #include "gstinfo.h"
93 #ifndef GST_DISABLE_GST_DEBUG
95 #ifdef HAVE_DLFCN_H
96 # include <dlfcn.h>
97 #endif
98 #ifdef HAVE_PRINTF_EXTENSION
99 # include <printf.h>
100 #endif
101 #include <stdio.h> /* fprintf */
102 #include <glib/gstdio.h>
103 #include <errno.h>
104 #ifdef HAVE_UNISTD_H
105 # include <unistd.h> /* getpid on UNIX */
106 #endif
107 #ifdef HAVE_PROCESS_H
108 # include <process.h> /* getpid on win32 */
109 #endif
110 #include <string.h> /* G_VA_COPY */
111 #ifdef G_OS_WIN32
112 # define WIN32_LEAN_AND_MEAN /* prevents from including too many things */
113 # include <windows.h> /* GetStdHandle, windows console */
114 #endif
116 #include "gst_private.h"
117 #include "gstutils.h"
118 #include "gstquark.h"
119 #include "gstsegment.h"
120 #ifdef HAVE_VALGRIND_H
121 # include <valgrind/valgrind.h>
122 #endif
123 #include <glib/gprintf.h> /* g_sprintf */
125 #endif /* !GST_DISABLE_GST_DEBUG */
127 /* we want these symbols exported even if debug is disabled, to maintain
128 * ABI compatibility. Unless GST_REMOVE_DISABLED is defined. */
129 #if !defined(GST_DISABLE_GST_DEBUG) || !defined(GST_REMOVE_DISABLED)
131 /* disabled by default, as soon as some threshold is set > NONE,
132 * it becomes enabled. */
133 gboolean __gst_debug_enabled = FALSE;
134 GstDebugLevel __gst_debug_min = GST_LEVEL_NONE;
136 GstDebugCategory *GST_CAT_DEFAULT = NULL;
138 GstDebugCategory *GST_CAT_GST_INIT = NULL;
139 GstDebugCategory *GST_CAT_AUTOPLUG = NULL;
140 GstDebugCategory *GST_CAT_AUTOPLUG_ATTEMPT = NULL;
141 GstDebugCategory *GST_CAT_PARENTAGE = NULL;
142 GstDebugCategory *GST_CAT_STATES = NULL;
143 GstDebugCategory *GST_CAT_SCHEDULING = NULL;
145 GstDebugCategory *GST_CAT_BUFFER = NULL;
146 GstDebugCategory *GST_CAT_BUFFER_LIST = NULL;
147 GstDebugCategory *GST_CAT_BUS = NULL;
148 GstDebugCategory *GST_CAT_CAPS = NULL;
149 GstDebugCategory *GST_CAT_CLOCK = NULL;
150 GstDebugCategory *GST_CAT_ELEMENT_PADS = NULL;
151 GstDebugCategory *GST_CAT_PADS = NULL;
152 GstDebugCategory *GST_CAT_PERFORMANCE = NULL;
153 GstDebugCategory *GST_CAT_PIPELINE = NULL;
154 GstDebugCategory *GST_CAT_PLUGIN_LOADING = NULL;
155 GstDebugCategory *GST_CAT_PLUGIN_INFO = NULL;
156 GstDebugCategory *GST_CAT_PROPERTIES = NULL;
157 GstDebugCategory *GST_CAT_TYPES = NULL;
158 GstDebugCategory *GST_CAT_XML = NULL;
159 GstDebugCategory *GST_CAT_NEGOTIATION = NULL;
160 GstDebugCategory *GST_CAT_REFCOUNTING = NULL;
161 GstDebugCategory *GST_CAT_ERROR_SYSTEM = NULL;
162 GstDebugCategory *GST_CAT_EVENT = NULL;
163 GstDebugCategory *GST_CAT_MESSAGE = NULL;
164 GstDebugCategory *GST_CAT_PARAMS = NULL;
165 GstDebugCategory *GST_CAT_CALL_TRACE = NULL;
166 GstDebugCategory *GST_CAT_SIGNAL = NULL;
167 GstDebugCategory *GST_CAT_PROBE = NULL;
168 GstDebugCategory *GST_CAT_REGISTRY = NULL;
169 GstDebugCategory *GST_CAT_QOS = NULL;
170 GstDebugCategory *_priv_GST_CAT_POLL = NULL;
173 #endif /* !defined(GST_DISABLE_GST_DEBUG) || !defined(GST_REMOVE_DISABLED) */
175 #ifndef GST_DISABLE_GST_DEBUG
177 /* underscore is to prevent conflict with GST_CAT_DEBUG define */
178 GST_DEBUG_CATEGORY_STATIC (_GST_CAT_DEBUG);
180 /* time of initialization, so we get useful debugging output times
181 * FIXME: we use this in gstdebugutils.c, what about a function + macro to
182 * get the running time: GST_DEBUG_RUNNING_TIME
183 */
184 GstClockTime _priv_gst_info_start_time;
186 #if 0
187 #if defined __sgi__
188 #include <rld_interface.h>
189 typedef struct DL_INFO
190 {
191 const char *dli_fname;
192 void *dli_fbase;
193 const char *dli_sname;
194 void *dli_saddr;
195 int dli_version;
196 int dli_reserved1;
197 long dli_reserved[4];
198 }
199 Dl_info;
201 #define _RLD_DLADDR 14
202 int dladdr (void *address, Dl_info * dl);
204 int
205 dladdr (void *address, Dl_info * dl)
206 {
207 void *v;
209 v = _rld_new_interface (_RLD_DLADDR, address, dl);
210 return (int) v;
211 }
212 #endif /* __sgi__ */
213 #endif
215 static void gst_debug_reset_threshold (gpointer category, gpointer unused);
216 static void gst_debug_reset_all_thresholds (void);
218 #ifdef HAVE_PRINTF_EXTENSION
219 static int _gst_info_printf_extension_ptr (FILE * stream,
220 const struct printf_info *info, const void *const *args);
221 static int _gst_info_printf_extension_segment (FILE * stream,
222 const struct printf_info *info, const void *const *args);
223 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
224 static int _gst_info_printf_extension_arginfo (const struct printf_info *info,
225 size_t n, int *argtypes, int *size);
226 #else
227 static int _gst_info_printf_extension_arginfo (const struct printf_info *info,
228 size_t n, int *argtypes);
229 #endif
230 #endif
232 struct _GstDebugMessage
233 {
234 gchar *message;
235 const gchar *format;
236 va_list arguments;
237 };
239 /* list of all name/level pairs from --gst-debug and GST_DEBUG */
240 static GStaticMutex __level_name_mutex = G_STATIC_MUTEX_INIT;
241 static GSList *__level_name = NULL;
242 typedef struct
243 {
244 GPatternSpec *pat;
245 GstDebugLevel level;
246 }
247 LevelNameEntry;
249 /* list of all categories */
250 static GStaticMutex __cat_mutex = G_STATIC_MUTEX_INIT;
251 static GSList *__categories = NULL;
253 /* all registered debug handlers */
254 typedef struct
255 {
256 GstLogFunction func;
257 gpointer user_data;
258 }
259 LogFuncEntry;
260 static GStaticMutex __log_func_mutex = G_STATIC_MUTEX_INIT;
261 static GSList *__log_functions = NULL;
263 #define PRETTY_TAGS_DEFAULT TRUE
264 static gboolean pretty_tags = PRETTY_TAGS_DEFAULT;
266 static gint __default_level;
267 static gint __use_color;
269 static FILE *log_file;
271 /* FIXME: export this? */
272 gboolean
273 _priv_gst_in_valgrind (void)
274 {
275 static enum
276 {
277 GST_VG_UNCHECKED,
278 GST_VG_NO_VALGRIND,
279 GST_VG_INSIDE
280 }
281 in_valgrind = GST_VG_UNCHECKED;
283 if (in_valgrind == GST_VG_UNCHECKED) {
284 #ifdef HAVE_VALGRIND_H
285 if (RUNNING_ON_VALGRIND) {
286 GST_CAT_INFO (GST_CAT_GST_INIT, "we're running inside valgrind");
287 printf ("GStreamer has detected that it is running inside valgrind.\n");
288 printf ("It might now take different code paths to ease debugging.\n");
289 printf ("Of course, this may also lead to different bugs.\n");
290 in_valgrind = GST_VG_INSIDE;
291 } else {
292 GST_CAT_LOG (GST_CAT_GST_INIT, "not doing extra valgrind stuff");
293 in_valgrind = GST_VG_NO_VALGRIND;
294 }
295 #else
296 in_valgrind = GST_VG_NO_VALGRIND;
297 #endif
298 g_assert (in_valgrind == GST_VG_NO_VALGRIND ||
299 in_valgrind == GST_VG_INSIDE);
300 }
301 return (in_valgrind == GST_VG_INSIDE) ? TRUE : FALSE;
302 }
304 /**
305 * _gst_debug_init:
306 *
307 * Initializes the debugging system.
308 * Normally you don't want to call this, because gst_init() does it for you.
309 */
310 void
311 _gst_debug_init (void)
312 {
313 const gchar *env;
315 env = g_getenv ("GST_DEBUG_FILE");
316 if (env != NULL && *env != '\0') {
317 if (strcmp (env, "-") == 0) {
318 log_file = stdout;
319 } else {
320 log_file = g_fopen (env, "w");
321 if (log_file == NULL) {
322 g_printerr ("Could not open log file '%s' for writing: %s\n", env,
323 g_strerror (errno));
324 log_file = stderr;
325 }
326 }
327 } else {
328 log_file = stderr;
329 }
331 g_atomic_int_set (&__default_level, GST_LEVEL_DEFAULT);
332 g_atomic_int_set (&__use_color, 1);
334 /* get time we started for debugging messages */
335 _priv_gst_info_start_time = gst_util_get_timestamp ();
337 #ifdef HAVE_PRINTF_EXTENSION
338 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
339 register_printf_specifier (GST_PTR_FORMAT[0], _gst_info_printf_extension_ptr,
340 _gst_info_printf_extension_arginfo);
341 register_printf_specifier (GST_SEGMENT_FORMAT[0],
342 _gst_info_printf_extension_segment, _gst_info_printf_extension_arginfo);
343 #else
344 register_printf_function (GST_PTR_FORMAT[0], _gst_info_printf_extension_ptr,
345 _gst_info_printf_extension_arginfo);
346 register_printf_function (GST_SEGMENT_FORMAT[0],
347 _gst_info_printf_extension_segment, _gst_info_printf_extension_arginfo);
348 #endif
349 #endif
351 /* do NOT use a single debug function before this line has been run */
352 GST_CAT_DEFAULT = _gst_debug_category_new ("default",
353 GST_DEBUG_UNDERLINE, NULL);
354 _GST_CAT_DEBUG = _gst_debug_category_new ("GST_DEBUG",
355 GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, "debugging subsystem");
357 gst_debug_add_log_function (gst_debug_log_default, NULL);
359 /* FIXME: add descriptions here */
360 GST_CAT_GST_INIT = _gst_debug_category_new ("GST_INIT",
361 GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
362 GST_CAT_AUTOPLUG = _gst_debug_category_new ("GST_AUTOPLUG",
363 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
364 GST_CAT_AUTOPLUG_ATTEMPT = _gst_debug_category_new ("GST_AUTOPLUG_ATTEMPT",
365 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN | GST_DEBUG_BG_BLUE, NULL);
366 GST_CAT_PARENTAGE = _gst_debug_category_new ("GST_PARENTAGE",
367 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
368 GST_CAT_STATES = _gst_debug_category_new ("GST_STATES",
369 GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
370 GST_CAT_SCHEDULING = _gst_debug_category_new ("GST_SCHEDULING",
371 GST_DEBUG_BOLD | GST_DEBUG_FG_MAGENTA, NULL);
372 GST_CAT_BUFFER = _gst_debug_category_new ("GST_BUFFER",
373 GST_DEBUG_BOLD | GST_DEBUG_BG_GREEN, NULL);
374 GST_CAT_BUFFER_LIST = _gst_debug_category_new ("GST_BUFFER_LIST",
375 GST_DEBUG_BOLD | GST_DEBUG_BG_GREEN, NULL);
376 GST_CAT_BUS = _gst_debug_category_new ("GST_BUS", GST_DEBUG_BG_YELLOW, NULL);
377 GST_CAT_CAPS = _gst_debug_category_new ("GST_CAPS",
378 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
379 GST_CAT_CLOCK = _gst_debug_category_new ("GST_CLOCK",
380 GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, NULL);
381 GST_CAT_ELEMENT_PADS = _gst_debug_category_new ("GST_ELEMENT_PADS",
382 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
383 GST_CAT_PADS = _gst_debug_category_new ("GST_PADS",
384 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_RED, NULL);
385 GST_CAT_PERFORMANCE = _gst_debug_category_new ("GST_PERFORMANCE",
386 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
387 GST_CAT_PIPELINE = _gst_debug_category_new ("GST_PIPELINE",
388 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
389 GST_CAT_PLUGIN_LOADING = _gst_debug_category_new ("GST_PLUGIN_LOADING",
390 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
391 GST_CAT_PLUGIN_INFO = _gst_debug_category_new ("GST_PLUGIN_INFO",
392 GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
393 GST_CAT_PROPERTIES = _gst_debug_category_new ("GST_PROPERTIES",
394 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_BLUE, NULL);
395 GST_CAT_TYPES = _gst_debug_category_new ("GST_TYPES",
396 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
397 GST_CAT_XML = _gst_debug_category_new ("GST_XML",
398 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
399 GST_CAT_NEGOTIATION = _gst_debug_category_new ("GST_NEGOTIATION",
400 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
401 GST_CAT_REFCOUNTING = _gst_debug_category_new ("GST_REFCOUNTING",
402 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_BLUE, NULL);
403 GST_CAT_ERROR_SYSTEM = _gst_debug_category_new ("GST_ERROR_SYSTEM",
404 GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_WHITE, NULL);
406 GST_CAT_EVENT = _gst_debug_category_new ("GST_EVENT",
407 GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
408 GST_CAT_MESSAGE = _gst_debug_category_new ("GST_MESSAGE",
409 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
410 GST_CAT_PARAMS = _gst_debug_category_new ("GST_PARAMS",
411 GST_DEBUG_BOLD | GST_DEBUG_FG_BLACK | GST_DEBUG_BG_YELLOW, NULL);
412 GST_CAT_CALL_TRACE = _gst_debug_category_new ("GST_CALL_TRACE",
413 GST_DEBUG_BOLD, NULL);
414 GST_CAT_SIGNAL = _gst_debug_category_new ("GST_SIGNAL",
415 GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
416 GST_CAT_PROBE = _gst_debug_category_new ("GST_PROBE",
417 GST_DEBUG_BOLD | GST_DEBUG_FG_GREEN, "pad probes");
418 GST_CAT_REGISTRY = _gst_debug_category_new ("GST_REGISTRY", 0, "registry");
419 GST_CAT_QOS = _gst_debug_category_new ("GST_QOS", 0, "QoS");
420 _priv_GST_CAT_POLL = _gst_debug_category_new ("GST_POLL", 0, "poll");
423 /* print out the valgrind message if we're in valgrind */
424 _priv_gst_in_valgrind ();
426 env = g_getenv ("GST_DEBUG_OPTIONS");
427 if (env != NULL) {
428 if (strstr (env, "full_tags") || strstr (env, "full-tags"))
429 pretty_tags = FALSE;
430 else if (strstr (env, "pretty_tags") || strstr (env, "pretty-tags"))
431 pretty_tags = TRUE;
432 }
433 }
435 /* we can't do this further above, because we initialize the GST_CAT_DEFAULT struct */
436 #define GST_CAT_DEFAULT _GST_CAT_DEBUG
438 /**
439 * gst_debug_log:
440 * @category: category to log
441 * @level: level of the message is in
442 * @file: the file that emitted the message, usually the __FILE__ identifier
443 * @function: the function that emitted the message
444 * @line: the line from that the message was emitted, usually __LINE__
445 * @object: the object this message relates to or NULL if none
446 * @format: a printf style format string
447 * @...: optional arguments for the format
448 *
449 * Logs the given message using the currently registered debugging handlers.
450 */
451 void
452 gst_debug_log (GstDebugCategory * category, GstDebugLevel level,
453 const gchar * file, const gchar * function, gint line,
454 GObject * object, const gchar * format, ...)
455 {
456 va_list var_args;
458 va_start (var_args, format);
459 gst_debug_log_valist (category, level, file, function, line, object, format,
460 var_args);
461 va_end (var_args);
462 }
464 /**
465 * gst_debug_log_valist:
466 * @category: category to log
467 * @level: level of the message is in
468 * @file: the file that emitted the message, usually the __FILE__ identifier
469 * @function: the function that emitted the message
470 * @line: the line from that the message was emitted, usually __LINE__
471 * @object: the object this message relates to or NULL if none
472 * @format: a printf style format string
473 * @args: optional arguments for the format
474 *
475 * Logs the given message using the currently registered debugging handlers.
476 */
477 void
478 gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level,
479 const gchar * file, const gchar * function, gint line,
480 GObject * object, const gchar * format, va_list args)
481 {
482 GstDebugMessage message;
483 LogFuncEntry *entry;
484 GSList *handler;
486 #ifdef _MSC_VER
487 gchar *file_basename;
488 #endif
490 g_return_if_fail (category != NULL);
491 g_return_if_fail (file != NULL);
492 g_return_if_fail (function != NULL);
493 g_return_if_fail (format != NULL);
495 #ifdef _MSC_VER
496 /*
497 * The predefined macro __FILE__ is always the exact path given to the
498 * compiler with MSVC, which may or may not be the basename. We work
499 * around it at runtime to improve the readability.
500 */
501 file = file_basename = g_path_get_basename (file);
502 #endif
504 message.message = NULL;
505 message.format = format;
506 G_VA_COPY (message.arguments, args);
508 handler = __log_functions;
509 while (handler) {
510 entry = handler->data;
511 handler = g_slist_next (handler);
512 entry->func (category, level, file, function, line, object, &message,
513 entry->user_data);
514 }
515 g_free (message.message);
516 va_end (message.arguments);
518 #ifdef _MSC_VER
519 g_free (file_basename);
520 #endif
521 }
523 /**
524 * gst_debug_message_get:
525 * @message: a debug message
526 *
527 * Gets the string representation of a #GstDebugMessage. This function is used
528 * in debug handlers to extract the message.
529 *
530 * Returns: the string representation of a #GstDebugMessage.
531 */
532 const gchar *
533 gst_debug_message_get (GstDebugMessage * message)
534 {
535 if (message->message == NULL) {
536 message->message = g_strdup_vprintf (message->format, message->arguments);
537 }
538 return message->message;
539 }
541 #define MAX_BUFFER_DUMP_STRING_LEN 100
543 /* structure_to_pretty_string:
544 * @structure: a #GstStructure
545 *
546 * Converts @structure to a human-readable string representation. Basically
547 * the same as gst_structure_to_string(), but if the structure contains large
548 * buffers such as images the hex representation of those buffers will be
549 * shortened so that the string remains readable.
550 *
551 * Returns: a newly-allocated string. g_free() when no longer needed.
552 */
553 static gchar *
554 structure_to_pretty_string (const GstStructure * s)
555 {
556 gchar *str, *pos, *end;
558 str = gst_structure_to_string (s);
559 if (str == NULL)
560 return NULL;
562 pos = str;
563 while ((pos = strstr (pos, "(buffer)"))) {
564 guint count = 0;
566 pos += strlen ("(buffer)");
567 for (end = pos; *end != '\0' && *end != ';' && *end != ' '; ++end)
568 ++count;
569 if (count > MAX_BUFFER_DUMP_STRING_LEN) {
570 memcpy (pos + MAX_BUFFER_DUMP_STRING_LEN - 6, "..", 2);
571 memcpy (pos + MAX_BUFFER_DUMP_STRING_LEN - 4, pos + count - 4, 4);
572 g_memmove (pos + MAX_BUFFER_DUMP_STRING_LEN, pos + count,
573 strlen (pos + count) + 1);
574 pos += MAX_BUFFER_DUMP_STRING_LEN;
575 }
576 }
578 return str;
579 }
581 static inline gchar *
582 gst_info_structure_to_string (GstStructure * s)
583 {
584 if (G_UNLIKELY (pretty_tags && s->name == GST_QUARK (TAGLIST)))
585 return structure_to_pretty_string (s);
586 else
587 return gst_structure_to_string (s);
588 }
590 static gchar *
591 gst_debug_print_object (gpointer ptr)
592 {
593 GObject *object = (GObject *) ptr;
595 #ifdef unused
596 /* This is a cute trick to detect unmapped memory, but is unportable,
597 * slow, screws around with madvise, and not actually that useful. */
598 {
599 int ret;
601 ret = madvise ((void *) ((unsigned long) ptr & (~0xfff)), 4096, 0);
602 if (ret == -1 && errno == ENOMEM) {
603 buffer = g_strdup_printf ("%p (unmapped memory)", ptr);
604 }
605 }
606 #endif
608 /* nicely printed object */
609 if (object == NULL) {
610 return g_strdup ("(NULL)");
611 }
612 if (*(GType *) ptr == GST_TYPE_CAPS) {
613 return gst_caps_to_string ((GstCaps *) ptr);
614 }
615 if (*(GType *) ptr == GST_TYPE_STRUCTURE) {
616 return gst_info_structure_to_string ((GstStructure *) ptr);
617 }
618 #ifdef USE_POISONING
619 if (*(guint32 *) ptr == 0xffffffff) {
620 return g_strdup_printf ("<poisoned@%p>", ptr);
621 }
622 #endif
623 if (GST_IS_PAD (object) && GST_OBJECT_NAME (object)) {
624 return g_strdup_printf ("<%s:%s>", GST_DEBUG_PAD_NAME (object));
625 }
626 if (GST_IS_OBJECT (object) && GST_OBJECT_NAME (object)) {
627 return g_strdup_printf ("<%s>", GST_OBJECT_NAME (object));
628 }
629 if (G_IS_OBJECT (object)) {
630 return g_strdup_printf ("<%s@%p>", G_OBJECT_TYPE_NAME (object), object);
631 }
632 if (GST_IS_MESSAGE (object)) {
633 GstMessage *msg = GST_MESSAGE_CAST (object);
634 gchar *s, *ret;
636 if (msg->structure) {
637 s = gst_info_structure_to_string (msg->structure);
638 } else {
639 s = g_strdup ("(NULL)");
640 }
642 ret = g_strdup_printf ("%s message from element '%s': %s",
643 GST_MESSAGE_TYPE_NAME (msg), (msg->src != NULL) ?
644 GST_ELEMENT_NAME (msg->src) : "(NULL)", s);
645 g_free (s);
646 return ret;
647 }
648 if (GST_IS_QUERY (object)) {
649 GstQuery *query = GST_QUERY_CAST (object);
651 if (query->structure) {
652 return gst_info_structure_to_string (query->structure);
653 } else {
654 const gchar *query_type_name;
656 query_type_name = gst_query_type_get_name (query->type);
657 if (G_LIKELY (query_type_name != NULL)) {
658 return g_strdup_printf ("%s query", query_type_name);
659 } else {
660 return g_strdup_printf ("query of unknown type %d", query->type);
661 }
662 }
663 }
664 if (GST_IS_EVENT (object)) {
665 GstEvent *event = GST_EVENT_CAST (object);
666 gchar *s, *ret;
668 if (event->structure) {
669 s = gst_info_structure_to_string (event->structure);
670 } else {
671 s = g_strdup ("(NULL)");
672 }
674 ret = g_strdup_printf ("%s event from '%s' at time %"
675 GST_TIME_FORMAT ": %s",
676 GST_EVENT_TYPE_NAME (event), (event->src != NULL) ?
677 GST_OBJECT_NAME (event->src) : "(NULL)",
678 GST_TIME_ARGS (event->timestamp), s);
679 g_free (s);
680 return ret;
681 }
683 return g_strdup_printf ("%p", ptr);
684 }
686 #ifdef HAVE_PRINTF_EXTENSION
688 static gchar *
689 gst_debug_print_segment (gpointer ptr)
690 {
691 GstSegment *segment = (GstSegment *) ptr;
693 /* nicely printed segment */
694 if (segment == NULL) {
695 return g_strdup ("(NULL)");
696 }
698 switch (segment->format) {
699 case GST_FORMAT_UNDEFINED:{
700 return g_strdup_printf ("UNDEFINED segment");
701 }
702 case GST_FORMAT_TIME:{
703 return g_strdup_printf ("time segment start=%" GST_TIME_FORMAT
704 ", stop=%" GST_TIME_FORMAT ", last_stop=%" GST_TIME_FORMAT
705 ", duration=%" GST_TIME_FORMAT ", rate=%f, applied_rate=%f"
706 ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
707 GST_TIME_ARGS (segment->start), GST_TIME_ARGS (segment->stop),
708 GST_TIME_ARGS (segment->last_stop), GST_TIME_ARGS (segment->duration),
709 segment->rate, segment->applied_rate, (guint) segment->flags,
710 GST_TIME_ARGS (segment->time), GST_TIME_ARGS (segment->accum));
711 }
712 default:{
713 const gchar *format_name;
715 format_name = gst_format_get_name (segment->format);
716 if (G_UNLIKELY (format_name == NULL))
717 format_name = "(UNKNOWN FORMAT)";
718 return g_strdup_printf ("%s segment start=%" G_GINT64_FORMAT
719 ", stop=%" G_GINT64_FORMAT ", last_stop=%" G_GINT64_FORMAT
720 ", duration=%" G_GINT64_FORMAT ", rate=%f, applied_rate=%f"
721 ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
722 format_name, segment->start, segment->stop, segment->last_stop,
723 segment->duration, segment->rate, segment->applied_rate,
724 (guint) segment->flags, GST_TIME_ARGS (segment->time),
725 GST_TIME_ARGS (segment->accum));
726 }
727 }
728 }
730 #endif /* HAVE_PRINTF_EXTENSION */
732 /**
733 * gst_debug_construct_term_color:
734 * @colorinfo: the color info
735 *
736 * Constructs a string that can be used for getting the desired color in color
737 * terminals.
738 * You need to free the string after use.
739 *
740 * Returns: a string containing the color definition
741 */
742 gchar *
743 gst_debug_construct_term_color (guint colorinfo)
744 {
745 GString *color;
747 color = g_string_new ("\033[00");
749 if (colorinfo & GST_DEBUG_BOLD) {
750 g_string_append_len (color, ";01", 3);
751 }
752 if (colorinfo & GST_DEBUG_UNDERLINE) {
753 g_string_append_len (color, ";04", 3);
754 }
755 if (colorinfo & GST_DEBUG_FG_MASK) {
756 g_string_append_printf (color, ";3%1d", colorinfo & GST_DEBUG_FG_MASK);
757 }
758 if (colorinfo & GST_DEBUG_BG_MASK) {
759 g_string_append_printf (color, ";4%1d",
760 (colorinfo & GST_DEBUG_BG_MASK) >> 4);
761 }
762 g_string_append_c (color, 'm');
764 return g_string_free (color, FALSE);
765 }
767 /**
768 * gst_debug_construct_win_color:
769 * @colorinfo: the color info
770 *
771 * Constructs an integer that can be used for getting the desired color in
772 * windows' terminals (cmd.exe). As there is no mean to underline, we simply
773 * ignore this attribute.
774 *
775 * This function returns 0 on non-windows machines.
776 *
777 * Returns: an integer containing the color definition
778 *
779 * Since: 0.10.23
780 */
781 gint
782 gst_debug_construct_win_color (guint colorinfo)
783 {
784 gint color = 0;
785 #ifdef G_OS_WIN32
786 static const guchar ansi_to_win_fg[8] = {
787 0, /* black */
788 FOREGROUND_RED, /* red */
789 FOREGROUND_GREEN, /* green */
790 FOREGROUND_RED | FOREGROUND_GREEN, /* yellow */
791 FOREGROUND_BLUE, /* blue */
792 FOREGROUND_RED | FOREGROUND_BLUE, /* magenta */
793 FOREGROUND_GREEN | FOREGROUND_BLUE, /* cyan */
794 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE /* white */
795 };
796 static const guchar ansi_to_win_bg[8] = {
797 0,
798 BACKGROUND_RED,
799 BACKGROUND_GREEN,
800 BACKGROUND_RED | BACKGROUND_GREEN,
801 BACKGROUND_BLUE,
802 BACKGROUND_RED | BACKGROUND_BLUE,
803 BACKGROUND_GREEN | FOREGROUND_BLUE,
804 BACKGROUND_RED | BACKGROUND_GREEN | BACKGROUND_BLUE
805 };
807 /* we draw black as white, as cmd.exe can only have black bg */
808 if (colorinfo == 0) {
809 return ansi_to_win_fg[7];
810 }
812 if (colorinfo & GST_DEBUG_BOLD) {
813 color |= FOREGROUND_INTENSITY;
814 }
815 if (colorinfo & GST_DEBUG_FG_MASK) {
816 color |= ansi_to_win_fg[colorinfo & GST_DEBUG_FG_MASK];
817 }
818 if (colorinfo & GST_DEBUG_BG_MASK) {
819 color |= ansi_to_win_bg[(colorinfo & GST_DEBUG_BG_MASK) >> 4];
820 }
821 #endif
822 return color;
823 }
825 /* width of %p varies depending on actual value of pointer, which can make
826 * output unevenly aligned if multiple threads are involved, hence the %14p
827 * (should really be %18p, but %14p seems a good compromise between too many
828 * white spaces and likely unalignment on my system) */
829 #if defined (GLIB_SIZEOF_VOID_P) && GLIB_SIZEOF_VOID_P == 8
830 #define PTR_FMT "%14p"
831 #else
832 #define PTR_FMT "%10p"
833 #endif
834 #define PID_FMT "%5d"
835 #define CAT_FMT "%20s %s:%d:%s:%s"
837 #ifdef G_OS_WIN32
838 static const guchar levelcolormap[GST_LEVEL_COUNT] = {
839 /* GST_LEVEL_NONE */
840 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
841 /* GST_LEVEL_ERROR */
842 FOREGROUND_RED | FOREGROUND_INTENSITY,
843 /* GST_LEVEL_WARNING */
844 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_INTENSITY,
845 /* GST_LEVEL_INFO */
846 FOREGROUND_GREEN | FOREGROUND_INTENSITY,
847 /* GST_LEVEL_DEBUG */
848 FOREGROUND_GREEN | FOREGROUND_BLUE,
849 /* GST_LEVEL_LOG */
850 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
851 /* GST_LEVEL_FIXME */
852 FOREGROUND_RED | FOREGROUND_GREEN,
853 /* GST_LEVEL_TRACE */
854 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
855 /* placeholder for log level 8 */
856 0,
857 /* GST_LEVEL_MEMDUMP */
858 FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE
859 };
861 static const guchar available_colors[] = {
862 FOREGROUND_RED, FOREGROUND_GREEN, FOREGROUND_RED | FOREGROUND_GREEN,
863 FOREGROUND_BLUE, FOREGROUND_RED | FOREGROUND_BLUE,
864 FOREGROUND_GREEN | FOREGROUND_BLUE,
865 };
866 #else
867 static const gchar *levelcolormap[GST_LEVEL_COUNT] = {
868 "\033[37m", /* GST_LEVEL_NONE */
869 "\033[31;01m", /* GST_LEVEL_ERROR */
870 "\033[33;01m", /* GST_LEVEL_WARNING */
871 "\033[32;01m", /* GST_LEVEL_INFO */
872 "\033[36m", /* GST_LEVEL_DEBUG */
873 "\033[37m", /* GST_LEVEL_LOG */
874 "\033[33;01m", /* GST_LEVEL_FIXME */
875 "\033[37m", /* GST_LEVEL_TRACE */
876 "\033[37m", /* placeholder for log level 8 */
877 "\033[37m" /* GST_LEVEL_MEMDUMP */
878 };
879 #endif
881 /**
882 * gst_debug_log_default:
883 * @category: category to log
884 * @level: level of the message
885 * @file: the file that emitted the message, usually the __FILE__ identifier
886 * @function: the function that emitted the message
887 * @line: the line from that the message was emitted, usually __LINE__
888 * @message: the actual message
889 * @object: the object this message relates to or NULL if none
890 * @unused: an unused variable, reserved for some user_data.
891 *
892 * The default logging handler used by GStreamer. Logging functions get called
893 * whenever a macro like GST_DEBUG or similar is used. This function outputs the
894 * message and additional info to stderr (or the log file specified via the
895 * GST_DEBUG_FILE environment variable).
896 *
897 * You can add other handlers by using gst_debug_add_log_function().
898 * And you can remove this handler by calling
899 * gst_debug_remove_log_function(gst_debug_log_default);
900 */
901 void
902 gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level,
903 const gchar * file, const gchar * function, gint line,
904 GObject * object, GstDebugMessage * message, gpointer unused)
905 {
906 gint pid;
907 GstClockTime elapsed;
908 gchar *obj = NULL;
909 gboolean is_colored;
911 if (level > gst_debug_category_get_threshold (category))
912 return;
914 pid = getpid ();
915 is_colored = gst_debug_is_colored ();
917 elapsed = GST_CLOCK_DIFF (_priv_gst_info_start_time,
918 gst_util_get_timestamp ());
920 if (object) {
921 obj = gst_debug_print_object (object);
922 } else {
923 obj = g_strdup ("");
924 }
926 if (is_colored) {
927 #ifndef G_OS_WIN32
928 /* colors, non-windows */
929 gchar *color = NULL;
930 const gchar *clear;
931 gchar pidcolor[10];
932 const gchar *levelcolor;
934 color = gst_debug_construct_term_color (gst_debug_category_get_color
935 (category));
936 clear = "\033[00m";
937 g_sprintf (pidcolor, "\033[3%1dm", pid % 6 + 31);
938 levelcolor = levelcolormap[level];
940 #define PRINT_FMT " %s"PID_FMT"%s "PTR_FMT" %s%s%s %s"CAT_FMT"%s %s\n"
941 fprintf (log_file, "%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed),
942 pidcolor, pid, clear, g_thread_self (), levelcolor,
943 gst_debug_level_get_name (level), clear, color,
944 gst_debug_category_get_name (category), file, line, function, obj,
945 clear, gst_debug_message_get (message));
946 fflush (log_file);
947 #undef PRINT_FMT
948 g_free (color);
949 #else
950 /* colors, windows. We take a lock to keep colors and content together.
951 * Maybe there is a better way but for now this will do the right
952 * thing. */
953 static GStaticMutex win_print_mutex = G_STATIC_MUTEX_INIT;
954 const gint clear = FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE;
955 #define SET_COLOR(c) G_STMT_START { \
956 if (log_file == stderr) { \
957 SetConsoleTextAttribute (GetStdHandle (STD_ERROR_HANDLE), (c)); \
958 } G_STMT_END
959 g_static_mutex_lock (&win_print_mutex);
960 /* timestamp */
961 fprintf (log_file, "%" GST_TIME_FORMAT " ", GST_TIME_ARGS (elapsed));
962 fflush (log_file);
963 /* pid */
964 SET_COLOR (available_colors[pid % G_N_ELEMENTS (available_colors)]);
965 fprintf (log_file, PID_FMT, pid);
966 fflush (log_file);
967 /* thread */
968 SET_COLOR (clear);
969 fprintf (log_file, " " PTR_FMT " ", g_thread_self ());
970 fflush (log_file);
971 /* level */
972 SET_COLOR (levelcolormap[level]);
973 fprintf (log_file, "%s ", gst_debug_level_get_name (level));
974 fflush (log_file);
975 /* category */
976 SET_COLOR (gst_debug_construct_win_color (gst_debug_category_get_color
977 (category)));
978 fprintf (log_file, CAT_FMT, gst_debug_category_get_name (category),
979 file, line, function, obj);
980 fflush (log_file);
981 /* message */
982 SET_COLOR (clear);
983 fprintf (log_file, " %s\n", gst_debug_message_get (message));
984 fflush (log_file);
985 g_static_mutex_unlock (&win_print_mutex);
986 #endif
987 } else {
988 /* no color, all platforms */
989 #define PRINT_FMT " "PID_FMT" "PTR_FMT" %s "CAT_FMT" %s\n"
990 fprintf (log_file, "%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed),
991 pid, g_thread_self (), gst_debug_level_get_name (level),
992 gst_debug_category_get_name (category), file, line, function, obj,
993 gst_debug_message_get (message));
994 fflush (log_file);
995 #undef PRINT_FMT
996 }
998 g_free (obj);
999 }
1001 /**
1002 * gst_debug_level_get_name:
1003 * @level: the level to get the name for
1004 *
1005 * Get the string representation of a debugging level
1006 *
1007 * Returns: the name
1008 */
1009 const gchar *
1010 gst_debug_level_get_name (GstDebugLevel level)
1011 {
1012 switch (level) {
1013 case GST_LEVEL_NONE:
1014 return "";
1015 case GST_LEVEL_ERROR:
1016 return "ERROR ";
1017 case GST_LEVEL_WARNING:
1018 return "WARN ";
1019 case GST_LEVEL_INFO:
1020 return "INFO ";
1021 case GST_LEVEL_DEBUG:
1022 return "DEBUG ";
1023 case GST_LEVEL_LOG:
1024 return "LOG ";
1025 case GST_LEVEL_FIXME:
1026 return "FIXME ";
1027 case GST_LEVEL_TRACE:
1028 return "TRACE ";
1029 case GST_LEVEL_MEMDUMP:
1030 return "MEMDUMP";
1031 default:
1032 g_warning ("invalid level specified for gst_debug_level_get_name");
1033 return "";
1034 }
1035 }
1037 /**
1038 * gst_debug_add_log_function:
1039 * @func: the function to use
1040 * @data: user data
1041 *
1042 * Adds the logging function to the list of logging functions.
1043 * Be sure to use G_GNUC_NO_INSTRUMENT on that function, it is needed.
1044 */
1045 void
1046 gst_debug_add_log_function (GstLogFunction func, gpointer data)
1047 {
1048 LogFuncEntry *entry;
1049 GSList *list;
1051 g_return_if_fail (func != NULL);
1053 entry = g_slice_new (LogFuncEntry);
1054 entry->func = func;
1055 entry->user_data = data;
1056 /* FIXME: we leak the old list here - other threads might access it right now
1057 * in gst_debug_logv. Another solution is to lock the mutex in gst_debug_logv,
1058 * but that is waaay costly.
1059 * It'd probably be clever to use some kind of RCU here, but I don't know
1060 * anything about that.
1061 */
1062 g_static_mutex_lock (&__log_func_mutex);
1063 list = g_slist_copy (__log_functions);
1064 __log_functions = g_slist_prepend (list, entry);
1065 g_static_mutex_unlock (&__log_func_mutex);
1067 GST_DEBUG ("prepended log function %p (user data %p) to log functions",
1068 func, data);
1069 }
1071 static gint
1072 gst_debug_compare_log_function_by_func (gconstpointer entry, gconstpointer func)
1073 {
1074 gpointer entryfunc = (gpointer) (((LogFuncEntry *) entry)->func);
1076 return (entryfunc < func) ? -1 : (entryfunc > func) ? 1 : 0;
1077 }
1079 static gint
1080 gst_debug_compare_log_function_by_data (gconstpointer entry, gconstpointer data)
1081 {
1082 gpointer entrydata = ((LogFuncEntry *) entry)->user_data;
1084 return (entrydata < data) ? -1 : (entrydata > data) ? 1 : 0;
1085 }
1087 static guint
1088 gst_debug_remove_with_compare_func (GCompareFunc func, gpointer data)
1089 {
1090 GSList *found;
1091 GSList *new;
1092 guint removals = 0;
1094 g_static_mutex_lock (&__log_func_mutex);
1095 new = __log_functions;
1096 while ((found = g_slist_find_custom (new, data, func))) {
1097 if (new == __log_functions) {
1098 /* make a copy when we have the first hit, so that we modify the copy and
1099 * make that the new list later */
1100 new = g_slist_copy (new);
1101 continue;
1102 }
1103 g_slice_free (LogFuncEntry, found->data);
1104 new = g_slist_delete_link (new, found);
1105 removals++;
1106 }
1107 /* FIXME: We leak the old list here. See _add_log_function for why. */
1108 __log_functions = new;
1109 g_static_mutex_unlock (&__log_func_mutex);
1111 return removals;
1112 }
1114 /**
1115 * gst_debug_remove_log_function:
1116 * @func: the log function to remove
1117 *
1118 * Removes all registered instances of the given logging functions.
1119 *
1120 * Returns: How many instances of the function were removed
1121 */
1122 guint
1123 gst_debug_remove_log_function (GstLogFunction func)
1124 {
1125 guint removals;
1127 g_return_val_if_fail (func != NULL, 0);
1129 removals =
1130 gst_debug_remove_with_compare_func
1131 (gst_debug_compare_log_function_by_func, (gpointer) func);
1132 GST_DEBUG ("removed log function %p %d times from log function list", func,
1133 removals);
1135 return removals;
1136 }
1138 /**
1139 * gst_debug_remove_log_function_by_data:
1140 * @data: user data of the log function to remove
1141 *
1142 * Removes all registered instances of log functions with the given user data.
1143 *
1144 * Returns: How many instances of the function were removed
1145 */
1146 guint
1147 gst_debug_remove_log_function_by_data (gpointer data)
1148 {
1149 guint removals;
1151 removals =
1152 gst_debug_remove_with_compare_func
1153 (gst_debug_compare_log_function_by_data, data);
1154 GST_DEBUG
1155 ("removed %d log functions with user data %p from log function list",
1156 removals, data);
1158 return removals;
1159 }
1161 /**
1162 * gst_debug_set_colored:
1163 * @colored: Whether to use colored output or not
1164 *
1165 * Sets or unsets the use of coloured debugging output.
1166 */
1167 void
1168 gst_debug_set_colored (gboolean colored)
1169 {
1170 g_atomic_int_set (&__use_color, colored ? 1 : 0);
1171 }
1173 /**
1174 * gst_debug_is_colored:
1175 *
1176 * Checks if the debugging output should be colored.
1177 *
1178 * Returns: TRUE, if the debug output should be colored.
1179 */
1180 gboolean
1181 gst_debug_is_colored (void)
1182 {
1183 return g_atomic_int_get (&__use_color) == 0 ? FALSE : TRUE;
1184 }
1186 /**
1187 * gst_debug_set_active:
1188 * @active: Whether to use debugging output or not
1189 *
1190 * If activated, debugging messages are sent to the debugging
1191 * handlers.
1192 * It makes sense to deactivate it for speed issues.
1193 * <note><para>This function is not threadsafe. It makes sense to only call it
1194 * during initialization.</para></note>
1195 */
1196 void
1197 gst_debug_set_active (gboolean active)
1198 {
1199 __gst_debug_enabled = active;
1200 if (active)
1201 __gst_debug_min = GST_LEVEL_COUNT;
1202 else
1203 __gst_debug_min = GST_LEVEL_NONE;
1204 }
1206 /**
1207 * gst_debug_is_active:
1208 *
1209 * Checks if debugging output is activated.
1210 *
1211 * Returns: TRUE, if debugging is activated
1212 */
1213 gboolean
1214 gst_debug_is_active (void)
1215 {
1216 return __gst_debug_enabled;
1217 }
1219 /**
1220 * gst_debug_set_default_threshold:
1221 * @level: level to set
1222 *
1223 * Sets the default threshold to the given level and updates all categories to
1224 * use this threshold.
1225 */
1226 void
1227 gst_debug_set_default_threshold (GstDebugLevel level)
1228 {
1229 g_atomic_int_set (&__default_level, level);
1230 gst_debug_reset_all_thresholds ();
1231 }
1233 /**
1234 * gst_debug_get_default_threshold:
1235 *
1236 * Returns the default threshold that is used for new categories.
1237 *
1238 * Returns: the default threshold level
1239 */
1240 GstDebugLevel
1241 gst_debug_get_default_threshold (void)
1242 {
1243 return (GstDebugLevel) g_atomic_int_get (&__default_level);
1244 }
1246 static void
1247 gst_debug_reset_threshold (gpointer category, gpointer unused)
1248 {
1249 GstDebugCategory *cat = (GstDebugCategory *) category;
1250 GSList *walk;
1252 g_static_mutex_lock (&__level_name_mutex);
1253 walk = __level_name;
1254 while (walk) {
1255 LevelNameEntry *entry = walk->data;
1257 walk = g_slist_next (walk);
1258 if (g_pattern_match_string (entry->pat, cat->name)) {
1259 GST_LOG ("category %s matches pattern %p - gets set to level %d",
1260 cat->name, entry->pat, entry->level);
1261 gst_debug_category_set_threshold (cat, entry->level);
1262 goto exit;
1263 }
1264 }
1265 gst_debug_category_set_threshold (cat, gst_debug_get_default_threshold ());
1267 exit:
1268 g_static_mutex_unlock (&__level_name_mutex);
1269 }
1271 static void
1272 gst_debug_reset_all_thresholds (void)
1273 {
1274 g_static_mutex_lock (&__cat_mutex);
1275 g_slist_foreach (__categories, gst_debug_reset_threshold, NULL);
1276 g_static_mutex_unlock (&__cat_mutex);
1277 }
1279 static void
1280 for_each_threshold_by_entry (gpointer data, gpointer user_data)
1281 {
1282 GstDebugCategory *cat = (GstDebugCategory *) data;
1283 LevelNameEntry *entry = (LevelNameEntry *) user_data;
1285 if (g_pattern_match_string (entry->pat, cat->name)) {
1286 GST_LOG ("category %s matches pattern %p - gets set to level %d",
1287 cat->name, entry->pat, entry->level);
1288 gst_debug_category_set_threshold (cat, entry->level);
1289 }
1290 }
1292 /**
1293 * gst_debug_set_threshold_for_name:
1294 * @name: name of the categories to set
1295 * @level: level to set them to
1296 *
1297 * Sets all categories which match the given glob style pattern to the given
1298 * level.
1299 */
1300 void
1301 gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level)
1302 {
1303 GPatternSpec *pat;
1304 LevelNameEntry *entry;
1306 g_return_if_fail (name != NULL);
1308 pat = g_pattern_spec_new (name);
1309 entry = g_slice_new (LevelNameEntry);
1310 entry->pat = pat;
1311 entry->level = level;
1312 g_static_mutex_lock (&__level_name_mutex);
1313 __level_name = g_slist_prepend (__level_name, entry);
1314 g_static_mutex_unlock (&__level_name_mutex);
1315 g_static_mutex_lock (&__cat_mutex);
1316 g_slist_foreach (__categories, for_each_threshold_by_entry, entry);
1317 g_static_mutex_unlock (&__cat_mutex);
1318 }
1320 /**
1321 * gst_debug_unset_threshold_for_name:
1322 * @name: name of the categories to set
1323 *
1324 * Resets all categories with the given name back to the default level.
1325 */
1326 void
1327 gst_debug_unset_threshold_for_name (const gchar * name)
1328 {
1329 GSList *walk;
1330 GPatternSpec *pat;
1332 g_return_if_fail (name != NULL);
1334 pat = g_pattern_spec_new (name);
1335 g_static_mutex_lock (&__level_name_mutex);
1336 walk = __level_name;
1337 /* improve this if you want, it's mighty slow */
1338 while (walk) {
1339 LevelNameEntry *entry = walk->data;
1341 if (g_pattern_spec_equal (entry->pat, pat)) {
1342 __level_name = g_slist_remove_link (__level_name, walk);
1343 g_pattern_spec_free (entry->pat);
1344 g_slice_free (LevelNameEntry, entry);
1345 g_slist_free_1 (walk);
1346 walk = __level_name;
1347 }
1348 }
1349 g_static_mutex_unlock (&__level_name_mutex);
1350 g_pattern_spec_free (pat);
1351 gst_debug_reset_all_thresholds ();
1352 }
1354 GstDebugCategory *
1355 _gst_debug_category_new (const gchar * name, guint color,
1356 const gchar * description)
1357 {
1358 GstDebugCategory *cat;
1360 g_return_val_if_fail (name != NULL, NULL);
1362 cat = g_slice_new (GstDebugCategory);
1363 cat->name = g_strdup (name);
1364 cat->color = color;
1365 if (description != NULL) {
1366 cat->description = g_strdup (description);
1367 } else {
1368 cat->description = g_strdup ("no description");
1369 }
1370 g_atomic_int_set (&cat->threshold, 0);
1371 gst_debug_reset_threshold (cat, NULL);
1373 /* add to category list */
1374 g_static_mutex_lock (&__cat_mutex);
1375 __categories = g_slist_prepend (__categories, cat);
1376 g_static_mutex_unlock (&__cat_mutex);
1378 return cat;
1379 }
1381 /**
1382 * gst_debug_category_free:
1383 * @category: #GstDebugCategory to free.
1384 *
1385 * Removes and frees the category and all associated resources.
1386 */
1387 void
1388 gst_debug_category_free (GstDebugCategory * category)
1389 {
1390 if (category == NULL)
1391 return;
1393 /* remove from category list */
1394 g_static_mutex_lock (&__cat_mutex);
1395 __categories = g_slist_remove (__categories, category);
1396 g_static_mutex_unlock (&__cat_mutex);
1398 g_free ((gpointer) category->name);
1399 g_free ((gpointer) category->description);
1400 g_slice_free (GstDebugCategory, category);
1401 }
1403 /**
1404 * gst_debug_category_set_threshold:
1405 * @category: a #GstDebugCategory to set threshold of.
1406 * @level: the #GstDebugLevel threshold to set.
1407 *
1408 * Sets the threshold of the category to the given level. Debug information will
1409 * only be output if the threshold is lower or equal to the level of the
1410 * debugging message.
1411 * <note><para>
1412 * Do not use this function in production code, because other functions may
1413 * change the threshold of categories as side effect. It is however a nice
1414 * function to use when debugging (even from gdb).
1415 * </para></note>
1416 */
1417 void
1418 gst_debug_category_set_threshold (GstDebugCategory * category,
1419 GstDebugLevel level)
1420 {
1421 g_return_if_fail (category != NULL);
1423 if (level > __gst_debug_min) {
1424 __gst_debug_enabled = TRUE;
1425 __gst_debug_min = level;
1426 }
1428 g_atomic_int_set (&category->threshold, level);
1429 }
1431 /**
1432 * gst_debug_category_reset_threshold:
1433 * @category: a #GstDebugCategory to reset threshold of.
1434 *
1435 * Resets the threshold of the category to the default level. Debug information
1436 * will only be output if the threshold is lower or equal to the level of the
1437 * debugging message.
1438 * Use this function to set the threshold back to where it was after using
1439 * gst_debug_category_set_threshold().
1440 */
1441 void
1442 gst_debug_category_reset_threshold (GstDebugCategory * category)
1443 {
1444 gst_debug_reset_threshold (category, NULL);
1445 }
1447 /**
1448 * gst_debug_category_get_threshold:
1449 * @category: a #GstDebugCategory to get threshold of.
1450 *
1451 * Returns the threshold of a #GstDebugCategory.
1452 *
1453 * Returns: the #GstDebugLevel that is used as threshold.
1454 */
1455 GstDebugLevel
1456 gst_debug_category_get_threshold (GstDebugCategory * category)
1457 {
1458 return g_atomic_int_get (&category->threshold);
1459 }
1461 /**
1462 * gst_debug_category_get_name:
1463 * @category: a #GstDebugCategory to get name of.
1464 *
1465 * Returns the name of a debug category.
1466 *
1467 * Returns: the name of the category.
1468 */
1469 const gchar *
1470 gst_debug_category_get_name (GstDebugCategory * category)
1471 {
1472 return category->name;
1473 }
1475 /**
1476 * gst_debug_category_get_color:
1477 * @category: a #GstDebugCategory to get the color of.
1478 *
1479 * Returns the color of a debug category used when printing output in this
1480 * category.
1481 *
1482 * Returns: the color of the category.
1483 */
1484 guint
1485 gst_debug_category_get_color (GstDebugCategory * category)
1486 {
1487 return category->color;
1488 }
1490 /**
1491 * gst_debug_category_get_description:
1492 * @category: a #GstDebugCategory to get the description of.
1493 *
1494 * Returns the description of a debug category.
1495 *
1496 * Returns: the description of the category.
1497 */
1498 const gchar *
1499 gst_debug_category_get_description (GstDebugCategory * category)
1500 {
1501 return category->description;
1502 }
1504 /**
1505 * gst_debug_get_all_categories:
1506 *
1507 * Returns a snapshot of a all categories that are currently in use . This list
1508 * may change anytime.
1509 * The caller has to free the list after use.
1510 *
1511 * Returns: the list of categories
1512 */
1513 GSList *
1514 gst_debug_get_all_categories (void)
1515 {
1516 GSList *ret;
1518 g_static_mutex_lock (&__cat_mutex);
1519 ret = g_slist_copy (__categories);
1520 g_static_mutex_unlock (&__cat_mutex);
1522 return ret;
1523 }
1525 GstDebugCategory *
1526 _gst_debug_get_category (const gchar * name)
1527 {
1528 GstDebugCategory *ret = NULL;
1529 GSList *node;
1531 for (node = __categories; node; node = g_slist_next (node)) {
1532 ret = (GstDebugCategory *) node->data;
1533 if (!strcmp (name, ret->name)) {
1534 return ret;
1535 }
1536 }
1537 return NULL;
1538 }
1540 /*** FUNCTION POINTERS ********************************************************/
1542 static GHashTable *__gst_function_pointers; /* NULL */
1543 static GStaticMutex __dbg_functions_mutex = G_STATIC_MUTEX_INIT;
1545 /* This function MUST NOT return NULL */
1546 const gchar *
1547 _gst_debug_nameof_funcptr (GstDebugFuncPtr func)
1548 {
1549 gchar *ptrname;
1551 #ifdef HAVE_DLADDR
1552 Dl_info dl_info;
1553 #endif
1555 if (G_UNLIKELY (func == NULL))
1556 return "(NULL)";
1558 g_static_mutex_lock (&__dbg_functions_mutex);
1559 if (G_LIKELY (__gst_function_pointers)) {
1560 ptrname = g_hash_table_lookup (__gst_function_pointers, (gpointer) func);
1561 g_static_mutex_unlock (&__dbg_functions_mutex);
1562 if (G_LIKELY (ptrname))
1563 return ptrname;
1564 } else {
1565 g_static_mutex_unlock (&__dbg_functions_mutex);
1566 }
1567 /* we need to create an entry in the hash table for this one so we don't leak
1568 * the name */
1569 #ifdef HAVE_DLADDR
1570 if (dladdr ((gpointer) func, &dl_info) && dl_info.dli_sname) {
1571 gchar *name = g_strdup (dl_info.dli_sname);
1573 _gst_debug_register_funcptr (func, name);
1574 return name;
1575 } else
1576 #endif
1577 {
1578 gchar *name = g_strdup_printf ("%p", (gpointer) func);
1580 _gst_debug_register_funcptr (func, name);
1581 return name;
1582 }
1583 }
1585 void
1586 _gst_debug_register_funcptr (GstDebugFuncPtr func, const gchar * ptrname)
1587 {
1588 gpointer ptr = (gpointer) func;
1590 g_static_mutex_lock (&__dbg_functions_mutex);
1592 if (!__gst_function_pointers)
1593 __gst_function_pointers = g_hash_table_new (g_direct_hash, g_direct_equal);
1594 if (!g_hash_table_lookup (__gst_function_pointers, ptr))
1595 g_hash_table_insert (__gst_function_pointers, ptr, (gpointer) ptrname);
1597 g_static_mutex_unlock (&__dbg_functions_mutex);
1598 }
1600 /*** PRINTF EXTENSIONS ********************************************************/
1602 #ifdef HAVE_PRINTF_EXTENSION
1603 static int
1604 _gst_info_printf_extension_ptr (FILE * stream, const struct printf_info *info,
1605 const void *const *args)
1606 {
1607 char *buffer;
1608 int len;
1609 void *ptr;
1611 buffer = NULL;
1612 ptr = *(void **) args[0];
1614 buffer = gst_debug_print_object (ptr);
1615 len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1616 buffer);
1618 g_free (buffer);
1619 return len;
1620 }
1622 static int
1623 _gst_info_printf_extension_segment (FILE * stream,
1624 const struct printf_info *info, const void *const *args)
1625 {
1626 char *buffer;
1627 int len;
1628 void *ptr;
1630 buffer = NULL;
1631 ptr = *(void **) args[0];
1633 buffer = gst_debug_print_segment (ptr);
1634 len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1635 buffer);
1637 g_free (buffer);
1638 return len;
1639 }
1641 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
1642 static int
1643 _gst_info_printf_extension_arginfo (const struct printf_info *info, size_t n,
1644 int *argtypes, int *size)
1645 #else
1646 static int
1647 _gst_info_printf_extension_arginfo (const struct printf_info *info, size_t n,
1648 int *argtypes)
1649 #endif
1650 {
1651 if (n > 0) {
1652 argtypes[0] = PA_POINTER;
1653 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
1654 *size = sizeof (gpointer);
1655 #endif
1656 }
1657 return 1;
1658 }
1659 #endif /* HAVE_PRINTF_EXTENSION */
1661 static void
1662 gst_info_dump_mem_line (gchar * linebuf, gsize linebuf_size,
1663 const guint8 * mem, gsize mem_offset, gsize mem_size)
1664 {
1665 gchar hexstr[50], ascstr[18], digitstr[4];
1667 if (mem_size > 16)
1668 mem_size = 16;
1670 hexstr[0] = '\0';
1671 ascstr[0] = '\0';
1673 if (mem != NULL) {
1674 guint i = 0;
1676 mem += mem_offset;
1677 while (i < mem_size) {
1678 ascstr[i] = (g_ascii_isprint (mem[i])) ? mem[i] : '.';
1679 g_snprintf (digitstr, sizeof (digitstr), "%02x ", mem[i]);
1680 g_strlcat (hexstr, digitstr, sizeof (hexstr));
1681 ++i;
1682 }
1683 ascstr[i] = '\0';
1684 }
1686 g_snprintf (linebuf, linebuf_size, "%08x: %-48.48s %-16.16s",
1687 (guint) mem_offset, hexstr, ascstr);
1688 }
1690 void
1691 _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
1692 const gchar * func, gint line, GObject * obj, const gchar * msg,
1693 const guint8 * data, guint length)
1694 {
1695 guint off = 0;
1697 gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "--------"
1698 "-------------------------------------------------------------------");
1700 if (msg != NULL && *msg != '\0') {
1701 gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "%s", msg);
1702 }
1704 while (off < length) {
1705 gchar buf[128];
1707 /* gst_info_dump_mem_line will process 16 bytes at most */
1708 gst_info_dump_mem_line (buf, sizeof (buf), data, off, length - off);
1709 gst_debug_log (cat, GST_LEVEL_MEMDUMP, file, func, line, obj, "%s", buf);
1710 off += 16;
1711 }
1713 gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "--------"
1714 "-------------------------------------------------------------------");
1715 }
1717 #else /* !GST_DISABLE_GST_DEBUG */
1718 #ifndef GST_REMOVE_DISABLED
1720 GstDebugCategory *
1721 _gst_debug_category_new (const gchar * name, guint color,
1722 const gchar * description)
1723 {
1724 return NULL;
1725 }
1727 void
1728 _gst_debug_register_funcptr (GstDebugFuncPtr func, const gchar * ptrname)
1729 {
1730 }
1732 /* This function MUST NOT return NULL */
1733 const gchar *
1734 _gst_debug_nameof_funcptr (GstDebugFuncPtr func)
1735 {
1736 return "(NULL)";
1737 }
1739 void
1740 gst_debug_log (GstDebugCategory * category, GstDebugLevel level,
1741 const gchar * file, const gchar * function, gint line,
1742 GObject * object, const gchar * format, ...)
1743 {
1744 }
1746 void
1747 gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level,
1748 const gchar * file, const gchar * function, gint line,
1749 GObject * object, const gchar * format, va_list args)
1750 {
1751 }
1753 const gchar *
1754 gst_debug_message_get (GstDebugMessage * message)
1755 {
1756 return "";
1757 }
1759 void
1760 gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level,
1761 const gchar * file, const gchar * function, gint line,
1762 GObject * object, GstDebugMessage * message, gpointer unused)
1763 {
1764 }
1766 G_CONST_RETURN gchar *
1767 gst_debug_level_get_name (GstDebugLevel level)
1768 {
1769 return "NONE";
1770 }
1772 void
1773 gst_debug_add_log_function (GstLogFunction func, gpointer data)
1774 {
1775 }
1777 guint
1778 gst_debug_remove_log_function (GstLogFunction func)
1779 {
1780 return 0;
1781 }
1783 guint
1784 gst_debug_remove_log_function_by_data (gpointer data)
1785 {
1786 return 0;
1787 }
1789 void
1790 gst_debug_set_active (gboolean active)
1791 {
1792 }
1794 gboolean
1795 gst_debug_is_active (void)
1796 {
1797 return FALSE;
1798 }
1800 void
1801 gst_debug_set_colored (gboolean colored)
1802 {
1803 }
1805 gboolean
1806 gst_debug_is_colored (void)
1807 {
1808 return FALSE;
1809 }
1811 void
1812 gst_debug_set_default_threshold (GstDebugLevel level)
1813 {
1814 }
1816 GstDebugLevel
1817 gst_debug_get_default_threshold (void)
1818 {
1819 return GST_LEVEL_NONE;
1820 }
1822 void
1823 gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level)
1824 {
1825 }
1827 void
1828 gst_debug_unset_threshold_for_name (const gchar * name)
1829 {
1830 }
1832 void
1833 gst_debug_category_free (GstDebugCategory * category)
1834 {
1835 }
1837 void
1838 gst_debug_category_set_threshold (GstDebugCategory * category,
1839 GstDebugLevel level)
1840 {
1841 }
1843 void
1844 gst_debug_category_reset_threshold (GstDebugCategory * category)
1845 {
1846 }
1848 GstDebugLevel
1849 gst_debug_category_get_threshold (GstDebugCategory * category)
1850 {
1851 return GST_LEVEL_NONE;
1852 }
1854 G_CONST_RETURN gchar *
1855 gst_debug_category_get_name (GstDebugCategory * category)
1856 {
1857 return "";
1858 }
1860 guint
1861 gst_debug_category_get_color (GstDebugCategory * category)
1862 {
1863 return 0;
1864 }
1866 G_CONST_RETURN gchar *
1867 gst_debug_category_get_description (GstDebugCategory * category)
1868 {
1869 return "";
1870 }
1872 GSList *
1873 gst_debug_get_all_categories (void)
1874 {
1875 return NULL;
1876 }
1878 GstDebugCategory *
1879 _gst_debug_get_category (const gchar * name)
1880 {
1881 return NULL;
1882 }
1884 gchar *
1885 gst_debug_construct_term_color (guint colorinfo)
1886 {
1887 return g_strdup ("00");
1888 }
1890 gint
1891 gst_debug_construct_win_color (guint colorinfo)
1892 {
1893 return 0;
1894 }
1896 gboolean
1897 _priv_gst_in_valgrind (void)
1898 {
1899 return FALSE;
1900 }
1902 void
1903 _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
1904 const gchar * func, gint line, GObject * obj, const gchar * msg,
1905 const guint8 * data, guint length)
1906 {
1907 }
1908 #endif /* GST_REMOVE_DISABLED */
1909 #endif /* GST_DISABLE_GST_DEBUG */
1912 #ifdef GST_ENABLE_FUNC_INSTRUMENTATION
1913 /* FIXME make this thread specific */
1914 static GSList *stack_trace = NULL;
1916 void
1917 __cyg_profile_func_enter (void *this_fn, void *call_site)
1918 G_GNUC_NO_INSTRUMENT;
1919 void __cyg_profile_func_enter (void *this_fn, void *call_site)
1920 {
1921 gchar *name = _gst_debug_nameof_funcptr (this_fn);
1922 gchar *site = _gst_debug_nameof_funcptr (call_site);
1924 GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "entering function %s from %s", name,
1925 site);
1926 stack_trace =
1927 g_slist_prepend (stack_trace, g_strdup_printf ("%8p in %s from %p (%s)",
1928 this_fn, name, call_site, site));
1930 g_free (name);
1931 g_free (site);
1932 }
1934 void
1935 __cyg_profile_func_exit (void *this_fn, void *call_site)
1936 G_GNUC_NO_INSTRUMENT;
1937 void __cyg_profile_func_exit (void *this_fn, void *call_site)
1938 {
1939 gchar *name = _gst_debug_nameof_funcptr (this_fn);
1941 GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "leaving function %s", name);
1942 g_free (stack_trace->data);
1943 stack_trace = g_slist_delete_link (stack_trace, stack_trace);
1945 g_free (name);
1946 }
1948 /**
1949 * gst_debug_print_stack_trace:
1950 *
1951 * If GST_ENABLE_FUNC_INSTRUMENTATION is defined a stacktrace is available for
1952 * gstreamer code, which can be printed with this function.
1953 */
1954 void
1955 gst_debug_print_stack_trace (void)
1956 {
1957 GSList *walk = stack_trace;
1958 gint count = 0;
1960 if (walk)
1961 walk = g_slist_next (walk);
1963 while (walk) {
1964 gchar *name = (gchar *) walk->data;
1966 g_print ("#%-2d %s\n", count++, name);
1968 walk = g_slist_next (walk);
1969 }
1970 }
1971 #else
1972 void
1973 gst_debug_print_stack_trace (void)
1974 {
1975 /* nothing because it's compiled out */
1976 }
1978 #endif /* GST_ENABLE_FUNC_INSTRUMENTATION */