]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blob - gst/gstinfo.c
Allow gst_debug_set_default_threshold() before gst_init()
[glsdk/gstreamer0-10.git] / gst / gstinfo.c
1 /* GStreamer
2  * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3  *                    2000 Wim Taymans <wtay@chello.be>
4  *                    2003 Benjamin Otte <in7y118@public.uni-hamburg.de>
5  * Copyright (C) 2008-2009 Tim-Philipp Müller <tim centricular net>
6  *
7  * gstinfo.c: debugging functions
8  *
9  * This library is free software; you can redistribute it and/or
10  * modify it under the terms of the GNU Library General Public
11  * License as published by the Free Software Foundation; either
12  * version 2 of the License, or (at your option) any later version.
13  *
14  * This library is distributed in the hope that it will be useful,
15  * but WITHOUT ANY WARRANTY; without even the implied warranty of
16  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
17  * Library General Public License for more details.
18  *
19  * You should have received a copy of the GNU Library General Public
20  * License along with this library; if not, write to the
21  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
22  * Boston, MA 02111-1307, USA.
23  */
25 /**
26  * SECTION:gstinfo
27  * @short_description: Debugging and logging facilities
28  * @see_also: #gstreamer-gstconfig, #gstreamer-Gst for command line parameters
29  * and environment variables that affect the debugging output.
30  *
31  * GStreamer's debugging subsystem is an easy way to get information about what
32  * the application is doing.  It is not meant for programming errors. Use GLib
33  * methods (g_warning and friends) for that.
34  *
35  * The debugging subsystem works only after GStreamer has been initialized
36  * - for example by calling gst_init().
37  *
38  * The debugging subsystem is used to log informational messages while the
39  * application runs.  Each messages has some properties attached to it. Among
40  * these properties are the debugging category, the severity (called "level"
41  * here) and an optional #GObject it belongs to. Each of these messages is sent
42  * to all registered debugging handlers, which then handle the messages.
43  * GStreamer attaches a default handler on startup, which outputs requested
44  * messages to stderr.
45  *
46  * Messages are output by using shortcut macros like #GST_DEBUG,
47  * #GST_CAT_ERROR_OBJECT or similar. These all expand to calling gst_debug_log()
48  * with the right parameters.
49  * The only thing a developer will probably want to do is define his own
50  * categories. This is easily done with 3 lines. At the top of your code,
51  * declare
52  * the variables and set the default category.
53  * <informalexample>
54  * <programlisting>
55  * GST_DEBUG_CATEGORY_STATIC (my_category);     // define category (statically)
56  * &hash;define GST_CAT_DEFAULT my_category     // set as default
57  * </programlisting>
58  * </informalexample>
59  * After that you only need to initialize the category.
60  * <informalexample>
61  * <programlisting>
62  * GST_DEBUG_CATEGORY_INIT (my_category, "my category",
63  *                          0, "This is my very own");
64  * </programlisting>
65  * </informalexample>
66  * Initialization must be done before the category is used first.
67  * Plugins do this
68  * in their plugin_init function, libraries and applications should do that
69  * during their initialization.
70  *
71  * The whole debugging subsystem can be disabled at build time with passing the
72  * --disable-gst-debug switch to configure. If this is done, every function,
73  * macro and even structs described in this file evaluate to default values or
74  * nothing at all.
75  * So don't take addresses of these functions or use other tricks.
76  * If you must do that for some reason, there is still an option.
77  * If the debugging
78  * subsystem was compiled out, #GST_DISABLE_GST_DEBUG is defined in
79  * &lt;gst/gst.h&gt;,
80  * so you can check that before doing your trick.
81  * Disabling the debugging subsystem will give you a slight (read: unnoticeable)
82  * speed increase and will reduce the size of your compiled code. The GStreamer
83  * library itself becomes around 10% smaller.
84  *
85  * Please note that there are naming conventions for the names of debugging
86  * categories. These are explained at GST_DEBUG_CATEGORY_INIT().
87  */
89 #define GST_INFO_C
90 #include "gst_private.h"
91 #include "gstinfo.h"
93 #ifndef GST_DISABLE_GST_DEBUG
95 #ifdef HAVE_DLFCN_H
96 #  include <dlfcn.h>
97 #endif
98 #ifdef HAVE_PRINTF_EXTENSION
99 #  include <printf.h>
100 #endif
101 #include <stdio.h>              /* fprintf */
102 #include <glib/gstdio.h>
103 #include <errno.h>
104 #ifdef HAVE_UNISTD_H
105 #  include <unistd.h>           /* getpid on UNIX */
106 #endif
107 #ifdef HAVE_PROCESS_H
108 #  include <process.h>          /* getpid on win32 */
109 #endif
110 #include <string.h>             /* G_VA_COPY */
111 #ifdef G_OS_WIN32
112 #  define WIN32_LEAN_AND_MEAN   /* prevents from including too many things */
113 #  include <windows.h>          /* GetStdHandle, windows console */
114 #endif
116 #include "gst_private.h"
117 #include "gstutils.h"
118 #include "gstquark.h"
119 #include "gstsegment.h"
120 #ifdef HAVE_VALGRIND_H
121 #  include <valgrind/valgrind.h>
122 #endif
123 #include <glib/gprintf.h>       /* g_sprintf */
125 #endif /* !GST_DISABLE_GST_DEBUG */
127 /* we want these symbols exported even if debug is disabled, to maintain
128  * ABI compatibility. Unless GST_REMOVE_DISABLED is defined. */
129 #if !defined(GST_DISABLE_GST_DEBUG) || !defined(GST_REMOVE_DISABLED)
131 /* disabled by default, as soon as some threshold is set > NONE,
132  * it becomes enabled. */
133 gboolean __gst_debug_enabled = FALSE;
134 GstDebugLevel __gst_debug_min = GST_LEVEL_NONE;
136 GstDebugCategory *GST_CAT_DEFAULT = NULL;
138 GstDebugCategory *GST_CAT_GST_INIT = NULL;
139 GstDebugCategory *GST_CAT_AUTOPLUG = NULL;
140 GstDebugCategory *GST_CAT_AUTOPLUG_ATTEMPT = NULL;
141 GstDebugCategory *GST_CAT_PARENTAGE = NULL;
142 GstDebugCategory *GST_CAT_STATES = NULL;
143 GstDebugCategory *GST_CAT_SCHEDULING = NULL;
145 GstDebugCategory *GST_CAT_BUFFER = NULL;
146 GstDebugCategory *GST_CAT_BUFFER_LIST = NULL;
147 GstDebugCategory *GST_CAT_BUS = NULL;
148 GstDebugCategory *GST_CAT_CAPS = NULL;
149 GstDebugCategory *GST_CAT_CLOCK = NULL;
150 GstDebugCategory *GST_CAT_ELEMENT_PADS = NULL;
151 GstDebugCategory *GST_CAT_PADS = NULL;
152 GstDebugCategory *GST_CAT_PERFORMANCE = NULL;
153 GstDebugCategory *GST_CAT_PIPELINE = NULL;
154 GstDebugCategory *GST_CAT_PLUGIN_LOADING = NULL;
155 GstDebugCategory *GST_CAT_PLUGIN_INFO = NULL;
156 GstDebugCategory *GST_CAT_PROPERTIES = NULL;
157 GstDebugCategory *GST_CAT_TYPES = NULL;
158 GstDebugCategory *GST_CAT_XML = NULL;
159 GstDebugCategory *GST_CAT_NEGOTIATION = NULL;
160 GstDebugCategory *GST_CAT_REFCOUNTING = NULL;
161 GstDebugCategory *GST_CAT_ERROR_SYSTEM = NULL;
162 GstDebugCategory *GST_CAT_EVENT = NULL;
163 GstDebugCategory *GST_CAT_MESSAGE = NULL;
164 GstDebugCategory *GST_CAT_PARAMS = NULL;
165 GstDebugCategory *GST_CAT_CALL_TRACE = NULL;
166 GstDebugCategory *GST_CAT_SIGNAL = NULL;
167 GstDebugCategory *GST_CAT_PROBE = NULL;
168 GstDebugCategory *GST_CAT_REGISTRY = NULL;
169 GstDebugCategory *GST_CAT_QOS = NULL;
170 GstDebugCategory *_priv_GST_CAT_POLL = NULL;
173 #endif /* !defined(GST_DISABLE_GST_DEBUG) || !defined(GST_REMOVE_DISABLED) */
175 #ifndef GST_DISABLE_GST_DEBUG
177 /* underscore is to prevent conflict with GST_CAT_DEBUG define */
178 GST_DEBUG_CATEGORY_STATIC (_GST_CAT_DEBUG);
180 /* time of initialization, so we get useful debugging output times
181  * FIXME: we use this in gstdebugutils.c, what about a function + macro to
182  * get the running time: GST_DEBUG_RUNNING_TIME
183  */
184 GstClockTime _priv_gst_info_start_time;
186 #if 0
187 #if defined __sgi__
188 #include <rld_interface.h>
189 typedef struct DL_INFO
191   const char *dli_fname;
192   void *dli_fbase;
193   const char *dli_sname;
194   void *dli_saddr;
195   int dli_version;
196   int dli_reserved1;
197   long dli_reserved[4];
199 Dl_info;
201 #define _RLD_DLADDR             14
202 int dladdr (void *address, Dl_info * dl);
204 int
205 dladdr (void *address, Dl_info * dl)
207   void *v;
209   v = _rld_new_interface (_RLD_DLADDR, address, dl);
210   return (int) v;
212 #endif /* __sgi__ */
213 #endif
215 static void gst_debug_reset_threshold (gpointer category, gpointer unused);
216 static void gst_debug_reset_all_thresholds (void);
218 #ifdef HAVE_PRINTF_EXTENSION
219 static int _gst_info_printf_extension_ptr (FILE * stream,
220     const struct printf_info *info, const void *const *args);
221 static int _gst_info_printf_extension_segment (FILE * stream,
222     const struct printf_info *info, const void *const *args);
223 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
224 static int _gst_info_printf_extension_arginfo (const struct printf_info *info,
225     size_t n, int *argtypes, int *size);
226 #else
227 static int _gst_info_printf_extension_arginfo (const struct printf_info *info,
228     size_t n, int *argtypes);
229 #endif
230 #endif
232 struct _GstDebugMessage
234   gchar *message;
235   const gchar *format;
236   va_list arguments;
237 };
239 /* list of all name/level pairs from --gst-debug and GST_DEBUG */
240 static GStaticMutex __level_name_mutex = G_STATIC_MUTEX_INIT;
241 static GSList *__level_name = NULL;
242 typedef struct
244   GPatternSpec *pat;
245   GstDebugLevel level;
247 LevelNameEntry;
249 /* list of all categories */
250 static GStaticMutex __cat_mutex = G_STATIC_MUTEX_INIT;
251 static GSList *__categories = NULL;
253 /* all registered debug handlers */
254 typedef struct
256   GstLogFunction func;
257   gpointer user_data;
259 LogFuncEntry;
260 static GStaticMutex __log_func_mutex = G_STATIC_MUTEX_INIT;
261 static GSList *__log_functions = NULL;
263 #define PRETTY_TAGS_DEFAULT  TRUE
264 static gboolean pretty_tags = PRETTY_TAGS_DEFAULT;
266 static volatile gint G_GNUC_MAY_ALIAS __default_level = GST_LEVEL_DEFAULT;
267 static volatile gint G_GNUC_MAY_ALIAS __use_color;
269 static FILE *log_file;
271 /* FIXME: export this? */
272 gboolean
273 _priv_gst_in_valgrind (void)
275   static enum
276   {
277     GST_VG_UNCHECKED,
278     GST_VG_NO_VALGRIND,
279     GST_VG_INSIDE
280   }
281   in_valgrind = GST_VG_UNCHECKED;
283   if (in_valgrind == GST_VG_UNCHECKED) {
284 #ifdef HAVE_VALGRIND_H
285     if (RUNNING_ON_VALGRIND) {
286       GST_CAT_INFO (GST_CAT_GST_INIT, "we're running inside valgrind");
287       printf ("GStreamer has detected that it is running inside valgrind.\n");
288       printf ("It might now take different code paths to ease debugging.\n");
289       printf ("Of course, this may also lead to different bugs.\n");
290       in_valgrind = GST_VG_INSIDE;
291     } else {
292       GST_CAT_LOG (GST_CAT_GST_INIT, "not doing extra valgrind stuff");
293       in_valgrind = GST_VG_NO_VALGRIND;
294     }
295 #else
296     in_valgrind = GST_VG_NO_VALGRIND;
297 #endif
298     g_assert (in_valgrind == GST_VG_NO_VALGRIND ||
299         in_valgrind == GST_VG_INSIDE);
300   }
301   return (in_valgrind == GST_VG_INSIDE) ? TRUE : FALSE;
304 /**
305  * _gst_debug_init:
306  *
307  * Initializes the debugging system.
308  * Normally you don't want to call this, because gst_init() does it for you.
309  */
310 void
311 _gst_debug_init (void)
313   const gchar *env;
315   env = g_getenv ("GST_DEBUG_FILE");
316   if (env != NULL && *env != '\0') {
317     if (strcmp (env, "-") == 0) {
318       log_file = stdout;
319     } else {
320       log_file = g_fopen (env, "w");
321       if (log_file == NULL) {
322         g_printerr ("Could not open log file '%s' for writing: %s\n", env,
323             g_strerror (errno));
324         log_file = stderr;
325       }
326     }
327   } else {
328     log_file = stderr;
329   }
331   /* get time we started for debugging messages */
332   _priv_gst_info_start_time = gst_util_get_timestamp ();
334 #ifdef HAVE_PRINTF_EXTENSION
335 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
336   register_printf_specifier (GST_PTR_FORMAT[0], _gst_info_printf_extension_ptr,
337       _gst_info_printf_extension_arginfo);
338   register_printf_specifier (GST_SEGMENT_FORMAT[0],
339       _gst_info_printf_extension_segment, _gst_info_printf_extension_arginfo);
340 #else
341   register_printf_function (GST_PTR_FORMAT[0], _gst_info_printf_extension_ptr,
342       _gst_info_printf_extension_arginfo);
343   register_printf_function (GST_SEGMENT_FORMAT[0],
344       _gst_info_printf_extension_segment, _gst_info_printf_extension_arginfo);
345 #endif
346 #endif
348   /* do NOT use a single debug function before this line has been run */
349   GST_CAT_DEFAULT = _gst_debug_category_new ("default",
350       GST_DEBUG_UNDERLINE, NULL);
351   _GST_CAT_DEBUG = _gst_debug_category_new ("GST_DEBUG",
352       GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, "debugging subsystem");
354   gst_debug_add_log_function (gst_debug_log_default, NULL);
356   /* FIXME: add descriptions here */
357   GST_CAT_GST_INIT = _gst_debug_category_new ("GST_INIT",
358       GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
359   GST_CAT_AUTOPLUG = _gst_debug_category_new ("GST_AUTOPLUG",
360       GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
361   GST_CAT_AUTOPLUG_ATTEMPT = _gst_debug_category_new ("GST_AUTOPLUG_ATTEMPT",
362       GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN | GST_DEBUG_BG_BLUE, NULL);
363   GST_CAT_PARENTAGE = _gst_debug_category_new ("GST_PARENTAGE",
364       GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
365   GST_CAT_STATES = _gst_debug_category_new ("GST_STATES",
366       GST_DEBUG_BOLD | GST_DEBUG_FG_RED, NULL);
367   GST_CAT_SCHEDULING = _gst_debug_category_new ("GST_SCHEDULING",
368       GST_DEBUG_BOLD | GST_DEBUG_FG_MAGENTA, NULL);
369   GST_CAT_BUFFER = _gst_debug_category_new ("GST_BUFFER",
370       GST_DEBUG_BOLD | GST_DEBUG_BG_GREEN, NULL);
371   GST_CAT_BUFFER_LIST = _gst_debug_category_new ("GST_BUFFER_LIST",
372       GST_DEBUG_BOLD | GST_DEBUG_BG_GREEN, NULL);
373   GST_CAT_BUS = _gst_debug_category_new ("GST_BUS", GST_DEBUG_BG_YELLOW, NULL);
374   GST_CAT_CAPS = _gst_debug_category_new ("GST_CAPS",
375       GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
376   GST_CAT_CLOCK = _gst_debug_category_new ("GST_CLOCK",
377       GST_DEBUG_BOLD | GST_DEBUG_FG_YELLOW, NULL);
378   GST_CAT_ELEMENT_PADS = _gst_debug_category_new ("GST_ELEMENT_PADS",
379       GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
380   GST_CAT_PADS = _gst_debug_category_new ("GST_PADS",
381       GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_RED, NULL);
382   GST_CAT_PERFORMANCE = _gst_debug_category_new ("GST_PERFORMANCE",
383       GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
384   GST_CAT_PIPELINE = _gst_debug_category_new ("GST_PIPELINE",
385       GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
386   GST_CAT_PLUGIN_LOADING = _gst_debug_category_new ("GST_PLUGIN_LOADING",
387       GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
388   GST_CAT_PLUGIN_INFO = _gst_debug_category_new ("GST_PLUGIN_INFO",
389       GST_DEBUG_BOLD | GST_DEBUG_FG_CYAN, NULL);
390   GST_CAT_PROPERTIES = _gst_debug_category_new ("GST_PROPERTIES",
391       GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_BLUE, NULL);
392   GST_CAT_TYPES = _gst_debug_category_new ("GST_TYPES",
393       GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
394   GST_CAT_XML = _gst_debug_category_new ("GST_XML",
395       GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
396   GST_CAT_NEGOTIATION = _gst_debug_category_new ("GST_NEGOTIATION",
397       GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
398   GST_CAT_REFCOUNTING = _gst_debug_category_new ("GST_REFCOUNTING",
399       GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_BLUE, NULL);
400   GST_CAT_ERROR_SYSTEM = _gst_debug_category_new ("GST_ERROR_SYSTEM",
401       GST_DEBUG_BOLD | GST_DEBUG_FG_RED | GST_DEBUG_BG_WHITE, NULL);
403   GST_CAT_EVENT = _gst_debug_category_new ("GST_EVENT",
404       GST_DEBUG_BOLD | GST_DEBUG_FG_BLUE, NULL);
405   GST_CAT_MESSAGE = _gst_debug_category_new ("GST_MESSAGE",
406       GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
407   GST_CAT_PARAMS = _gst_debug_category_new ("GST_PARAMS",
408       GST_DEBUG_BOLD | GST_DEBUG_FG_BLACK | GST_DEBUG_BG_YELLOW, NULL);
409   GST_CAT_CALL_TRACE = _gst_debug_category_new ("GST_CALL_TRACE",
410       GST_DEBUG_BOLD, NULL);
411   GST_CAT_SIGNAL = _gst_debug_category_new ("GST_SIGNAL",
412       GST_DEBUG_BOLD | GST_DEBUG_FG_WHITE | GST_DEBUG_BG_RED, NULL);
413   GST_CAT_PROBE = _gst_debug_category_new ("GST_PROBE",
414       GST_DEBUG_BOLD | GST_DEBUG_FG_GREEN, "pad probes");
415   GST_CAT_REGISTRY = _gst_debug_category_new ("GST_REGISTRY", 0, "registry");
416   GST_CAT_QOS = _gst_debug_category_new ("GST_QOS", 0, "QoS");
417   _priv_GST_CAT_POLL = _gst_debug_category_new ("GST_POLL", 0, "poll");
420   /* print out the valgrind message if we're in valgrind */
421   _priv_gst_in_valgrind ();
423   env = g_getenv ("GST_DEBUG_OPTIONS");
424   if (env != NULL) {
425     if (strstr (env, "full_tags") || strstr (env, "full-tags"))
426       pretty_tags = FALSE;
427     else if (strstr (env, "pretty_tags") || strstr (env, "pretty-tags"))
428       pretty_tags = TRUE;
429   }
432 /* we can't do this further above, because we initialize the GST_CAT_DEFAULT struct */
433 #define GST_CAT_DEFAULT _GST_CAT_DEBUG
435 /**
436  * gst_debug_log:
437  * @category: category to log
438  * @level: level of the message is in
439  * @file: the file that emitted the message, usually the __FILE__ identifier
440  * @function: the function that emitted the message
441  * @line: the line from that the message was emitted, usually __LINE__
442  * @object: the object this message relates to or NULL if none
443  * @format: a printf style format string
444  * @...: optional arguments for the format
445  *
446  * Logs the given message using the currently registered debugging handlers.
447  */
448 void
449 gst_debug_log (GstDebugCategory * category, GstDebugLevel level,
450     const gchar * file, const gchar * function, gint line,
451     GObject * object, const gchar * format, ...)
453   va_list var_args;
455   va_start (var_args, format);
456   gst_debug_log_valist (category, level, file, function, line, object, format,
457       var_args);
458   va_end (var_args);
461 /**
462  * gst_debug_log_valist:
463  * @category: category to log
464  * @level: level of the message is in
465  * @file: the file that emitted the message, usually the __FILE__ identifier
466  * @function: the function that emitted the message
467  * @line: the line from that the message was emitted, usually __LINE__
468  * @object: the object this message relates to or NULL if none
469  * @format: a printf style format string
470  * @args: optional arguments for the format
471  *
472  * Logs the given message using the currently registered debugging handlers.
473  */
474 void
475 gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level,
476     const gchar * file, const gchar * function, gint line,
477     GObject * object, const gchar * format, va_list args)
479   GstDebugMessage message;
480   LogFuncEntry *entry;
481   GSList *handler;
483 #ifdef _MSC_VER
484   gchar *file_basename;
485 #endif
487   g_return_if_fail (category != NULL);
488   g_return_if_fail (file != NULL);
489   g_return_if_fail (function != NULL);
490   g_return_if_fail (format != NULL);
492 #ifdef _MSC_VER
493   /*
494    * The predefined macro __FILE__ is always the exact path given to the
495    * compiler with MSVC, which may or may not be the basename.  We work
496    * around it at runtime to improve the readability.
497    */
498   file = file_basename = g_path_get_basename (file);
499 #endif
501   message.message = NULL;
502   message.format = format;
503   G_VA_COPY (message.arguments, args);
505   handler = __log_functions;
506   while (handler) {
507     entry = handler->data;
508     handler = g_slist_next (handler);
509     entry->func (category, level, file, function, line, object, &message,
510         entry->user_data);
511   }
512   g_free (message.message);
513   va_end (message.arguments);
515 #ifdef _MSC_VER
516   g_free (file_basename);
517 #endif
520 /**
521  * gst_debug_message_get:
522  * @message: a debug message
523  *
524  * Gets the string representation of a #GstDebugMessage. This function is used
525  * in debug handlers to extract the message.
526  *
527  * Returns: the string representation of a #GstDebugMessage.
528  */
529 const gchar *
530 gst_debug_message_get (GstDebugMessage * message)
532   if (message->message == NULL) {
533     message->message = g_strdup_vprintf (message->format, message->arguments);
534   }
535   return message->message;
538 #define MAX_BUFFER_DUMP_STRING_LEN  100
540 /* structure_to_pretty_string:
541  * @structure: a #GstStructure
542  *
543  * Converts @structure to a human-readable string representation. Basically
544  * the same as gst_structure_to_string(), but if the structure contains large
545  * buffers such as images the hex representation of those buffers will be
546  * shortened so that the string remains readable.
547  *
548  * Returns: a newly-allocated string. g_free() when no longer needed.
549  */
550 static gchar *
551 structure_to_pretty_string (const GstStructure * s)
553   gchar *str, *pos, *end;
555   str = gst_structure_to_string (s);
556   if (str == NULL)
557     return NULL;
559   pos = str;
560   while ((pos = strstr (pos, "(buffer)"))) {
561     guint count = 0;
563     pos += strlen ("(buffer)");
564     for (end = pos; *end != '\0' && *end != ';' && *end != ' '; ++end)
565       ++count;
566     if (count > MAX_BUFFER_DUMP_STRING_LEN) {
567       memcpy (pos + MAX_BUFFER_DUMP_STRING_LEN - 6, "..", 2);
568       memcpy (pos + MAX_BUFFER_DUMP_STRING_LEN - 4, pos + count - 4, 4);
569       g_memmove (pos + MAX_BUFFER_DUMP_STRING_LEN, pos + count,
570           strlen (pos + count) + 1);
571       pos += MAX_BUFFER_DUMP_STRING_LEN;
572     }
573   }
575   return str;
578 static inline gchar *
579 gst_info_structure_to_string (GstStructure * s)
581   if (G_UNLIKELY (pretty_tags && s->name == GST_QUARK (TAGLIST)))
582     return structure_to_pretty_string (s);
583   else
584     return gst_structure_to_string (s);
587 static gchar *
588 gst_debug_print_object (gpointer ptr)
590   GObject *object = (GObject *) ptr;
592 #ifdef unused
593   /* This is a cute trick to detect unmapped memory, but is unportable,
594    * slow, screws around with madvise, and not actually that useful. */
595   {
596     int ret;
598     ret = madvise ((void *) ((unsigned long) ptr & (~0xfff)), 4096, 0);
599     if (ret == -1 && errno == ENOMEM) {
600       buffer = g_strdup_printf ("%p (unmapped memory)", ptr);
601     }
602   }
603 #endif
605   /* nicely printed object */
606   if (object == NULL) {
607     return g_strdup ("(NULL)");
608   }
609   if (*(GType *) ptr == GST_TYPE_CAPS) {
610     return gst_caps_to_string ((GstCaps *) ptr);
611   }
612   if (*(GType *) ptr == GST_TYPE_STRUCTURE) {
613     return gst_info_structure_to_string ((GstStructure *) ptr);
614   }
615 #ifdef USE_POISONING
616   if (*(guint32 *) ptr == 0xffffffff) {
617     return g_strdup_printf ("<poisoned@%p>", ptr);
618   }
619 #endif
620   if (GST_IS_PAD (object) && GST_OBJECT_NAME (object)) {
621     return g_strdup_printf ("<%s:%s>", GST_DEBUG_PAD_NAME (object));
622   }
623   if (GST_IS_OBJECT (object) && GST_OBJECT_NAME (object)) {
624     return g_strdup_printf ("<%s>", GST_OBJECT_NAME (object));
625   }
626   if (G_IS_OBJECT (object)) {
627     return g_strdup_printf ("<%s@%p>", G_OBJECT_TYPE_NAME (object), object);
628   }
629   if (GST_IS_MESSAGE (object)) {
630     GstMessage *msg = GST_MESSAGE_CAST (object);
631     gchar *s, *ret;
633     if (msg->structure) {
634       s = gst_info_structure_to_string (msg->structure);
635     } else {
636       s = g_strdup ("(NULL)");
637     }
639     ret = g_strdup_printf ("%s message from element '%s': %s",
640         GST_MESSAGE_TYPE_NAME (msg), (msg->src != NULL) ?
641         GST_ELEMENT_NAME (msg->src) : "(NULL)", s);
642     g_free (s);
643     return ret;
644   }
645   if (GST_IS_QUERY (object)) {
646     GstQuery *query = GST_QUERY_CAST (object);
648     if (query->structure) {
649       return gst_info_structure_to_string (query->structure);
650     } else {
651       const gchar *query_type_name;
653       query_type_name = gst_query_type_get_name (query->type);
654       if (G_LIKELY (query_type_name != NULL)) {
655         return g_strdup_printf ("%s query", query_type_name);
656       } else {
657         return g_strdup_printf ("query of unknown type %d", query->type);
658       }
659     }
660   }
661   if (GST_IS_EVENT (object)) {
662     GstEvent *event = GST_EVENT_CAST (object);
663     gchar *s, *ret;
665     if (event->structure) {
666       s = gst_info_structure_to_string (event->structure);
667     } else {
668       s = g_strdup ("(NULL)");
669     }
671     ret = g_strdup_printf ("%s event from '%s' at time %"
672         GST_TIME_FORMAT ": %s",
673         GST_EVENT_TYPE_NAME (event), (event->src != NULL) ?
674         GST_OBJECT_NAME (event->src) : "(NULL)",
675         GST_TIME_ARGS (event->timestamp), s);
676     g_free (s);
677     return ret;
678   }
680   return g_strdup_printf ("%p", ptr);
683 #ifdef HAVE_PRINTF_EXTENSION
685 static gchar *
686 gst_debug_print_segment (gpointer ptr)
688   GstSegment *segment = (GstSegment *) ptr;
690   /* nicely printed segment */
691   if (segment == NULL) {
692     return g_strdup ("(NULL)");
693   }
695   switch (segment->format) {
696     case GST_FORMAT_UNDEFINED:{
697       return g_strdup_printf ("UNDEFINED segment");
698     }
699     case GST_FORMAT_TIME:{
700       return g_strdup_printf ("time segment start=%" GST_TIME_FORMAT
701           ", stop=%" GST_TIME_FORMAT ", last_stop=%" GST_TIME_FORMAT
702           ", duration=%" GST_TIME_FORMAT ", rate=%f, applied_rate=%f"
703           ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
704           GST_TIME_ARGS (segment->start), GST_TIME_ARGS (segment->stop),
705           GST_TIME_ARGS (segment->last_stop), GST_TIME_ARGS (segment->duration),
706           segment->rate, segment->applied_rate, (guint) segment->flags,
707           GST_TIME_ARGS (segment->time), GST_TIME_ARGS (segment->accum));
708     }
709     default:{
710       const gchar *format_name;
712       format_name = gst_format_get_name (segment->format);
713       if (G_UNLIKELY (format_name == NULL))
714         format_name = "(UNKNOWN FORMAT)";
715       return g_strdup_printf ("%s segment start=%" G_GINT64_FORMAT
716           ", stop=%" G_GINT64_FORMAT ", last_stop=%" G_GINT64_FORMAT
717           ", duration=%" G_GINT64_FORMAT ", rate=%f, applied_rate=%f"
718           ", flags=0x%02x, time=%" GST_TIME_FORMAT ", accum=%" GST_TIME_FORMAT,
719           format_name, segment->start, segment->stop, segment->last_stop,
720           segment->duration, segment->rate, segment->applied_rate,
721           (guint) segment->flags, GST_TIME_ARGS (segment->time),
722           GST_TIME_ARGS (segment->accum));
723     }
724   }
727 #endif /* HAVE_PRINTF_EXTENSION */
729 /**
730  * gst_debug_construct_term_color:
731  * @colorinfo: the color info
732  *
733  * Constructs a string that can be used for getting the desired color in color
734  * terminals.
735  * You need to free the string after use.
736  *
737  * Returns: a string containing the color definition
738  */
739 gchar *
740 gst_debug_construct_term_color (guint colorinfo)
742   GString *color;
744   color = g_string_new ("\033[00");
746   if (colorinfo & GST_DEBUG_BOLD) {
747     g_string_append_len (color, ";01", 3);
748   }
749   if (colorinfo & GST_DEBUG_UNDERLINE) {
750     g_string_append_len (color, ";04", 3);
751   }
752   if (colorinfo & GST_DEBUG_FG_MASK) {
753     g_string_append_printf (color, ";3%1d", colorinfo & GST_DEBUG_FG_MASK);
754   }
755   if (colorinfo & GST_DEBUG_BG_MASK) {
756     g_string_append_printf (color, ";4%1d",
757         (colorinfo & GST_DEBUG_BG_MASK) >> 4);
758   }
759   g_string_append_c (color, 'm');
761   return g_string_free (color, FALSE);
764 /**
765  * gst_debug_construct_win_color:
766  * @colorinfo: the color info
767  *
768  * Constructs an integer that can be used for getting the desired color in
769  * windows' terminals (cmd.exe). As there is no mean to underline, we simply
770  * ignore this attribute.
771  *
772  * This function returns 0 on non-windows machines.
773  *
774  * Returns: an integer containing the color definition
775  *
776  * Since: 0.10.23
777  */
778 gint
779 gst_debug_construct_win_color (guint colorinfo)
781   gint color = 0;
782 #ifdef G_OS_WIN32
783   static const guchar ansi_to_win_fg[8] = {
784     0,                          /* black   */
785     FOREGROUND_RED,             /* red     */
786     FOREGROUND_GREEN,           /* green   */
787     FOREGROUND_RED | FOREGROUND_GREEN,  /* yellow  */
788     FOREGROUND_BLUE,            /* blue    */
789     FOREGROUND_RED | FOREGROUND_BLUE,   /* magenta */
790     FOREGROUND_GREEN | FOREGROUND_BLUE, /* cyan    */
791     FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE /* white   */
792   };
793   static const guchar ansi_to_win_bg[8] = {
794     0,
795     BACKGROUND_RED,
796     BACKGROUND_GREEN,
797     BACKGROUND_RED | BACKGROUND_GREEN,
798     BACKGROUND_BLUE,
799     BACKGROUND_RED | BACKGROUND_BLUE,
800     BACKGROUND_GREEN | FOREGROUND_BLUE,
801     BACKGROUND_RED | BACKGROUND_GREEN | BACKGROUND_BLUE
802   };
804   /* we draw black as white, as cmd.exe can only have black bg */
805   if (colorinfo == 0) {
806     return ansi_to_win_fg[7];
807   }
809   if (colorinfo & GST_DEBUG_BOLD) {
810     color |= FOREGROUND_INTENSITY;
811   }
812   if (colorinfo & GST_DEBUG_FG_MASK) {
813     color |= ansi_to_win_fg[colorinfo & GST_DEBUG_FG_MASK];
814   }
815   if (colorinfo & GST_DEBUG_BG_MASK) {
816     color |= ansi_to_win_bg[(colorinfo & GST_DEBUG_BG_MASK) >> 4];
817   }
818 #endif
819   return color;
822 /* width of %p varies depending on actual value of pointer, which can make
823  * output unevenly aligned if multiple threads are involved, hence the %14p
824  * (should really be %18p, but %14p seems a good compromise between too many
825  * white spaces and likely unalignment on my system) */
826 #if defined (GLIB_SIZEOF_VOID_P) && GLIB_SIZEOF_VOID_P == 8
827 #define PTR_FMT "%14p"
828 #else
829 #define PTR_FMT "%10p"
830 #endif
831 #define PID_FMT "%5d"
832 #define CAT_FMT "%20s %s:%d:%s:%s"
834 #ifdef G_OS_WIN32
835 static const guchar levelcolormap[GST_LEVEL_COUNT] = {
836   /* GST_LEVEL_NONE */
837   FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
838   /* GST_LEVEL_ERROR */
839   FOREGROUND_RED | FOREGROUND_INTENSITY,
840   /* GST_LEVEL_WARNING */
841   FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_INTENSITY,
842   /* GST_LEVEL_INFO */
843   FOREGROUND_GREEN | FOREGROUND_INTENSITY,
844   /* GST_LEVEL_DEBUG */
845   FOREGROUND_GREEN | FOREGROUND_BLUE,
846   /* GST_LEVEL_LOG */
847   FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
848   /* GST_LEVEL_FIXME */
849   FOREGROUND_RED | FOREGROUND_GREEN,
850   /* GST_LEVEL_TRACE */
851   FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE,
852   /* placeholder for log level 8 */
853   0,
854   /* GST_LEVEL_MEMDUMP */
855   FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE
856 };
858 static const guchar available_colors[] = {
859   FOREGROUND_RED, FOREGROUND_GREEN, FOREGROUND_RED | FOREGROUND_GREEN,
860   FOREGROUND_BLUE, FOREGROUND_RED | FOREGROUND_BLUE,
861   FOREGROUND_GREEN | FOREGROUND_BLUE,
862 };
863 #else
864 static const gchar *levelcolormap[GST_LEVEL_COUNT] = {
865   "\033[37m",                   /* GST_LEVEL_NONE */
866   "\033[31;01m",                /* GST_LEVEL_ERROR */
867   "\033[33;01m",                /* GST_LEVEL_WARNING */
868   "\033[32;01m",                /* GST_LEVEL_INFO */
869   "\033[36m",                   /* GST_LEVEL_DEBUG */
870   "\033[37m",                   /* GST_LEVEL_LOG */
871   "\033[33;01m",                /* GST_LEVEL_FIXME */
872   "\033[37m",                   /* GST_LEVEL_TRACE */
873   "\033[37m",                   /* placeholder for log level 8 */
874   "\033[37m"                    /* GST_LEVEL_MEMDUMP */
875 };
876 #endif
878 /**
879  * gst_debug_log_default:
880  * @category: category to log
881  * @level: level of the message
882  * @file: the file that emitted the message, usually the __FILE__ identifier
883  * @function: the function that emitted the message
884  * @line: the line from that the message was emitted, usually __LINE__
885  * @message: the actual message
886  * @object: the object this message relates to or NULL if none
887  * @unused: an unused variable, reserved for some user_data.
888  *
889  * The default logging handler used by GStreamer. Logging functions get called
890  * whenever a macro like GST_DEBUG or similar is used. This function outputs the
891  * message and additional info to stderr (or the log file specified via the
892  * GST_DEBUG_FILE environment variable).
893  *
894  * You can add other handlers by using gst_debug_add_log_function().
895  * And you can remove this handler by calling
896  * gst_debug_remove_log_function(gst_debug_log_default);
897  */
898 void
899 gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level,
900     const gchar * file, const gchar * function, gint line,
901     GObject * object, GstDebugMessage * message, gpointer unused)
903   gint pid;
904   GstClockTime elapsed;
905   gchar *obj = NULL;
906   gboolean is_colored;
908   if (level > gst_debug_category_get_threshold (category))
909     return;
911   pid = getpid ();
912   is_colored = gst_debug_is_colored ();
914   if (object) {
915     obj = gst_debug_print_object (object);
916   } else {
917     obj = g_strdup ("");
918   }
920   elapsed = GST_CLOCK_DIFF (_priv_gst_info_start_time,
921       gst_util_get_timestamp ());
923   if (is_colored) {
924 #ifndef G_OS_WIN32
925     /* colors, non-windows */
926     gchar *color = NULL;
927     const gchar *clear;
928     gchar pidcolor[10];
929     const gchar *levelcolor;
931     color = gst_debug_construct_term_color (gst_debug_category_get_color
932         (category));
933     clear = "\033[00m";
934     g_sprintf (pidcolor, "\033[3%1dm", pid % 6 + 31);
935     levelcolor = levelcolormap[level];
937 #define PRINT_FMT " %s"PID_FMT"%s "PTR_FMT" %s%s%s %s"CAT_FMT"%s %s\n"
938     fprintf (log_file, "%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed),
939         pidcolor, pid, clear, g_thread_self (), levelcolor,
940         gst_debug_level_get_name (level), clear, color,
941         gst_debug_category_get_name (category), file, line, function, obj,
942         clear, gst_debug_message_get (message));
943     fflush (log_file);
944 #undef PRINT_FMT
945     g_free (color);
946 #else
947     /* colors, windows. We take a lock to keep colors and content together.
948      * Maybe there is a better way but for now this will do the right
949      * thing. */
950     static GStaticMutex win_print_mutex = G_STATIC_MUTEX_INIT;
951     const gint clear = FOREGROUND_RED | FOREGROUND_GREEN | FOREGROUND_BLUE;
952 #define SET_COLOR(c) G_STMT_START { \
953   if (log_file == stderr) \
954     SetConsoleTextAttribute (GetStdHandle (STD_ERROR_HANDLE), (c)); \
955   } G_STMT_END
956     g_static_mutex_lock (&win_print_mutex);
957     /* timestamp */
958     fprintf (log_file, "%" GST_TIME_FORMAT " ", GST_TIME_ARGS (elapsed));
959     fflush (log_file);
960     /* pid */
961     SET_COLOR (available_colors[pid % G_N_ELEMENTS (available_colors)]);
962     fprintf (log_file, PID_FMT, pid);
963     fflush (log_file);
964     /* thread */
965     SET_COLOR (clear);
966     fprintf (log_file, " " PTR_FMT " ", g_thread_self ());
967     fflush (log_file);
968     /* level */
969     SET_COLOR (levelcolormap[level]);
970     fprintf (log_file, "%s ", gst_debug_level_get_name (level));
971     fflush (log_file);
972     /* category */
973     SET_COLOR (gst_debug_construct_win_color (gst_debug_category_get_color
974             (category)));
975     fprintf (log_file, CAT_FMT, gst_debug_category_get_name (category),
976         file, line, function, obj);
977     fflush (log_file);
978     /* message */
979     SET_COLOR (clear);
980     fprintf (log_file, " %s\n", gst_debug_message_get (message));
981     fflush (log_file);
982     g_static_mutex_unlock (&win_print_mutex);
983 #endif
984   } else {
985     /* no color, all platforms */
986 #define PRINT_FMT " "PID_FMT" "PTR_FMT" %s "CAT_FMT" %s\n"
987     fprintf (log_file, "%" GST_TIME_FORMAT PRINT_FMT, GST_TIME_ARGS (elapsed),
988         pid, g_thread_self (), gst_debug_level_get_name (level),
989         gst_debug_category_get_name (category), file, line, function, obj,
990         gst_debug_message_get (message));
991     fflush (log_file);
992 #undef PRINT_FMT
993   }
995   g_free (obj);
998 /**
999  * gst_debug_level_get_name:
1000  * @level: the level to get the name for
1001  *
1002  * Get the string representation of a debugging level
1003  *
1004  * Returns: the name
1005  */
1006 const gchar *
1007 gst_debug_level_get_name (GstDebugLevel level)
1009   switch (level) {
1010     case GST_LEVEL_NONE:
1011       return "";
1012     case GST_LEVEL_ERROR:
1013       return "ERROR  ";
1014     case GST_LEVEL_WARNING:
1015       return "WARN   ";
1016     case GST_LEVEL_INFO:
1017       return "INFO   ";
1018     case GST_LEVEL_DEBUG:
1019       return "DEBUG  ";
1020     case GST_LEVEL_LOG:
1021       return "LOG    ";
1022     case GST_LEVEL_FIXME:
1023       return "FIXME  ";
1024     case GST_LEVEL_TRACE:
1025       return "TRACE  ";
1026     case GST_LEVEL_MEMDUMP:
1027       return "MEMDUMP";
1028     default:
1029       g_warning ("invalid level specified for gst_debug_level_get_name");
1030       return "";
1031   }
1034 /**
1035  * gst_debug_add_log_function:
1036  * @func: the function to use
1037  * @data: user data
1038  *
1039  * Adds the logging function to the list of logging functions.
1040  * Be sure to use #G_GNUC_NO_INSTRUMENT on that function, it is needed.
1041  */
1042 void
1043 gst_debug_add_log_function (GstLogFunction func, gpointer data)
1045   LogFuncEntry *entry;
1046   GSList *list;
1048   g_return_if_fail (func != NULL);
1050   entry = g_slice_new (LogFuncEntry);
1051   entry->func = func;
1052   entry->user_data = data;
1053   /* FIXME: we leak the old list here - other threads might access it right now
1054    * in gst_debug_logv. Another solution is to lock the mutex in gst_debug_logv,
1055    * but that is waaay costly.
1056    * It'd probably be clever to use some kind of RCU here, but I don't know
1057    * anything about that.
1058    */
1059   g_static_mutex_lock (&__log_func_mutex);
1060   list = g_slist_copy (__log_functions);
1061   __log_functions = g_slist_prepend (list, entry);
1062   g_static_mutex_unlock (&__log_func_mutex);
1064   GST_DEBUG ("prepended log function %p (user data %p) to log functions",
1065       func, data);
1068 static gint
1069 gst_debug_compare_log_function_by_func (gconstpointer entry, gconstpointer func)
1071   gpointer entryfunc = (gpointer) (((LogFuncEntry *) entry)->func);
1073   return (entryfunc < func) ? -1 : (entryfunc > func) ? 1 : 0;
1076 static gint
1077 gst_debug_compare_log_function_by_data (gconstpointer entry, gconstpointer data)
1079   gpointer entrydata = ((LogFuncEntry *) entry)->user_data;
1081   return (entrydata < data) ? -1 : (entrydata > data) ? 1 : 0;
1084 static guint
1085 gst_debug_remove_with_compare_func (GCompareFunc func, gpointer data)
1087   GSList *found;
1088   GSList *new;
1089   guint removals = 0;
1091   g_static_mutex_lock (&__log_func_mutex);
1092   new = __log_functions;
1093   while ((found = g_slist_find_custom (new, data, func))) {
1094     if (new == __log_functions) {
1095       /* make a copy when we have the first hit, so that we modify the copy and
1096        * make that the new list later */
1097       new = g_slist_copy (new);
1098       continue;
1099     }
1100     g_slice_free (LogFuncEntry, found->data);
1101     new = g_slist_delete_link (new, found);
1102     removals++;
1103   }
1104   /* FIXME: We leak the old list here. See _add_log_function for why. */
1105   __log_functions = new;
1106   g_static_mutex_unlock (&__log_func_mutex);
1108   return removals;
1111 /**
1112  * gst_debug_remove_log_function:
1113  * @func: the log function to remove
1114  *
1115  * Removes all registered instances of the given logging functions.
1116  *
1117  * Returns: How many instances of the function were removed
1118  */
1119 guint
1120 gst_debug_remove_log_function (GstLogFunction func)
1122   guint removals;
1124   g_return_val_if_fail (func != NULL, 0);
1126   removals =
1127       gst_debug_remove_with_compare_func
1128       (gst_debug_compare_log_function_by_func, (gpointer) func);
1129   GST_DEBUG ("removed log function %p %d times from log function list", func,
1130       removals);
1132   return removals;
1135 /**
1136  * gst_debug_remove_log_function_by_data:
1137  * @data: user data of the log function to remove
1138  *
1139  * Removes all registered instances of log functions with the given user data.
1140  *
1141  * Returns: How many instances of the function were removed
1142  */
1143 guint
1144 gst_debug_remove_log_function_by_data (gpointer data)
1146   guint removals;
1148   removals =
1149       gst_debug_remove_with_compare_func
1150       (gst_debug_compare_log_function_by_data, data);
1151   GST_DEBUG
1152       ("removed %d log functions with user data %p from log function list",
1153       removals, data);
1155   return removals;
1158 /**
1159  * gst_debug_set_colored:
1160  * @colored: Whether to use colored output or not
1161  *
1162  * Sets or unsets the use of coloured debugging output.
1163  *
1164  * This function may be called before gst_init().
1165  */
1166 void
1167 gst_debug_set_colored (gboolean colored)
1169   g_atomic_int_set (&__use_color, colored ? 1 : 0);
1172 /**
1173  * gst_debug_is_colored:
1174  *
1175  * Checks if the debugging output should be colored.
1176  *
1177  * Returns: TRUE, if the debug output should be colored.
1178  */
1179 gboolean
1180 gst_debug_is_colored (void)
1182   return g_atomic_int_get (&__use_color) == 0 ? FALSE : TRUE;
1185 /**
1186  * gst_debug_set_active:
1187  * @active: Whether to use debugging output or not
1188  *
1189  * If activated, debugging messages are sent to the debugging
1190  * handlers.
1191  * It makes sense to deactivate it for speed issues.
1192  * <note><para>This function is not threadsafe. It makes sense to only call it
1193  * during initialization.</para></note>
1194  */
1195 void
1196 gst_debug_set_active (gboolean active)
1198   __gst_debug_enabled = active;
1199   if (active)
1200     __gst_debug_min = GST_LEVEL_COUNT;
1201   else
1202     __gst_debug_min = GST_LEVEL_NONE;
1205 /**
1206  * gst_debug_is_active:
1207  *
1208  * Checks if debugging output is activated.
1209  *
1210  * Returns: TRUE, if debugging is activated
1211  */
1212 gboolean
1213 gst_debug_is_active (void)
1215   return __gst_debug_enabled;
1218 /**
1219  * gst_debug_set_default_threshold:
1220  * @level: level to set
1221  *
1222  * Sets the default threshold to the given level and updates all categories to
1223  * use this threshold.
1224  *
1225  * This function may be called before gst_init().
1226  */
1227 void
1228 gst_debug_set_default_threshold (GstDebugLevel level)
1230   g_atomic_int_set (&__default_level, level);
1231   gst_debug_reset_all_thresholds ();
1234 /**
1235  * gst_debug_get_default_threshold:
1236  *
1237  * Returns the default threshold that is used for new categories.
1238  *
1239  * Returns: the default threshold level
1240  */
1241 GstDebugLevel
1242 gst_debug_get_default_threshold (void)
1244   return (GstDebugLevel) g_atomic_int_get (&__default_level);
1247 static void
1248 gst_debug_reset_threshold (gpointer category, gpointer unused)
1250   GstDebugCategory *cat = (GstDebugCategory *) category;
1251   GSList *walk;
1253   g_static_mutex_lock (&__level_name_mutex);
1254   walk = __level_name;
1255   while (walk) {
1256     LevelNameEntry *entry = walk->data;
1258     walk = g_slist_next (walk);
1259     if (g_pattern_match_string (entry->pat, cat->name)) {
1260       GST_LOG ("category %s matches pattern %p - gets set to level %d",
1261           cat->name, entry->pat, entry->level);
1262       gst_debug_category_set_threshold (cat, entry->level);
1263       goto exit;
1264     }
1265   }
1266   gst_debug_category_set_threshold (cat, gst_debug_get_default_threshold ());
1268 exit:
1269   g_static_mutex_unlock (&__level_name_mutex);
1272 static void
1273 gst_debug_reset_all_thresholds (void)
1275   g_static_mutex_lock (&__cat_mutex);
1276   g_slist_foreach (__categories, gst_debug_reset_threshold, NULL);
1277   g_static_mutex_unlock (&__cat_mutex);
1280 static void
1281 for_each_threshold_by_entry (gpointer data, gpointer user_data)
1283   GstDebugCategory *cat = (GstDebugCategory *) data;
1284   LevelNameEntry *entry = (LevelNameEntry *) user_data;
1286   if (g_pattern_match_string (entry->pat, cat->name)) {
1287     GST_LOG ("category %s matches pattern %p - gets set to level %d",
1288         cat->name, entry->pat, entry->level);
1289     gst_debug_category_set_threshold (cat, entry->level);
1290   }
1293 /**
1294  * gst_debug_set_threshold_for_name:
1295  * @name: name of the categories to set
1296  * @level: level to set them to
1297  *
1298  * Sets all categories which match the given glob style pattern to the given
1299  * level.
1300  */
1301 void
1302 gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level)
1304   GPatternSpec *pat;
1305   LevelNameEntry *entry;
1307   g_return_if_fail (name != NULL);
1309   pat = g_pattern_spec_new (name);
1310   entry = g_slice_new (LevelNameEntry);
1311   entry->pat = pat;
1312   entry->level = level;
1313   g_static_mutex_lock (&__level_name_mutex);
1314   __level_name = g_slist_prepend (__level_name, entry);
1315   g_static_mutex_unlock (&__level_name_mutex);
1316   g_static_mutex_lock (&__cat_mutex);
1317   g_slist_foreach (__categories, for_each_threshold_by_entry, entry);
1318   g_static_mutex_unlock (&__cat_mutex);
1321 /**
1322  * gst_debug_unset_threshold_for_name:
1323  * @name: name of the categories to set
1324  *
1325  * Resets all categories with the given name back to the default level.
1326  */
1327 void
1328 gst_debug_unset_threshold_for_name (const gchar * name)
1330   GSList *walk;
1331   GPatternSpec *pat;
1333   g_return_if_fail (name != NULL);
1335   pat = g_pattern_spec_new (name);
1336   g_static_mutex_lock (&__level_name_mutex);
1337   walk = __level_name;
1338   /* improve this if you want, it's mighty slow */
1339   while (walk) {
1340     LevelNameEntry *entry = walk->data;
1342     if (g_pattern_spec_equal (entry->pat, pat)) {
1343       __level_name = g_slist_remove_link (__level_name, walk);
1344       g_pattern_spec_free (entry->pat);
1345       g_slice_free (LevelNameEntry, entry);
1346       g_slist_free_1 (walk);
1347       walk = __level_name;
1348     }
1349   }
1350   g_static_mutex_unlock (&__level_name_mutex);
1351   g_pattern_spec_free (pat);
1352   gst_debug_reset_all_thresholds ();
1355 GstDebugCategory *
1356 _gst_debug_category_new (const gchar * name, guint color,
1357     const gchar * description)
1359   GstDebugCategory *cat;
1361   g_return_val_if_fail (name != NULL, NULL);
1363   cat = g_slice_new (GstDebugCategory);
1364   cat->name = g_strdup (name);
1365   cat->color = color;
1366   if (description != NULL) {
1367     cat->description = g_strdup (description);
1368   } else {
1369     cat->description = g_strdup ("no description");
1370   }
1371   g_atomic_int_set (&cat->threshold, 0);
1372   gst_debug_reset_threshold (cat, NULL);
1374   /* add to category list */
1375   g_static_mutex_lock (&__cat_mutex);
1376   __categories = g_slist_prepend (__categories, cat);
1377   g_static_mutex_unlock (&__cat_mutex);
1379   return cat;
1382 /**
1383  * gst_debug_category_free:
1384  * @category: #GstDebugCategory to free.
1385  *
1386  * Removes and frees the category and all associated resources.
1387  */
1388 void
1389 gst_debug_category_free (GstDebugCategory * category)
1391   if (category == NULL)
1392     return;
1394   /* remove from category list */
1395   g_static_mutex_lock (&__cat_mutex);
1396   __categories = g_slist_remove (__categories, category);
1397   g_static_mutex_unlock (&__cat_mutex);
1399   g_free ((gpointer) category->name);
1400   g_free ((gpointer) category->description);
1401   g_slice_free (GstDebugCategory, category);
1404 /**
1405  * gst_debug_category_set_threshold:
1406  * @category: a #GstDebugCategory to set threshold of.
1407  * @level: the #GstDebugLevel threshold to set.
1408  *
1409  * Sets the threshold of the category to the given level. Debug information will
1410  * only be output if the threshold is lower or equal to the level of the
1411  * debugging message.
1412  * <note><para>
1413  * Do not use this function in production code, because other functions may
1414  * change the threshold of categories as side effect. It is however a nice
1415  * function to use when debugging (even from gdb).
1416  * </para></note>
1417  */
1418 void
1419 gst_debug_category_set_threshold (GstDebugCategory * category,
1420     GstDebugLevel level)
1422   g_return_if_fail (category != NULL);
1424   if (level > __gst_debug_min) {
1425     __gst_debug_enabled = TRUE;
1426     __gst_debug_min = level;
1427   }
1429   g_atomic_int_set (&category->threshold, level);
1432 /**
1433  * gst_debug_category_reset_threshold:
1434  * @category: a #GstDebugCategory to reset threshold of.
1435  *
1436  * Resets the threshold of the category to the default level. Debug information
1437  * will only be output if the threshold is lower or equal to the level of the
1438  * debugging message.
1439  * Use this function to set the threshold back to where it was after using
1440  * gst_debug_category_set_threshold().
1441  */
1442 void
1443 gst_debug_category_reset_threshold (GstDebugCategory * category)
1445   gst_debug_reset_threshold (category, NULL);
1448 /**
1449  * gst_debug_category_get_threshold:
1450  * @category: a #GstDebugCategory to get threshold of.
1451  *
1452  * Returns the threshold of a #GstDebugCategory.
1453  *
1454  * Returns: the #GstDebugLevel that is used as threshold.
1455  */
1456 GstDebugLevel
1457 gst_debug_category_get_threshold (GstDebugCategory * category)
1459   return g_atomic_int_get (&category->threshold);
1462 /**
1463  * gst_debug_category_get_name:
1464  * @category: a #GstDebugCategory to get name of.
1465  *
1466  * Returns the name of a debug category.
1467  *
1468  * Returns: the name of the category.
1469  */
1470 const gchar *
1471 gst_debug_category_get_name (GstDebugCategory * category)
1473   return category->name;
1476 /**
1477  * gst_debug_category_get_color:
1478  * @category: a #GstDebugCategory to get the color of.
1479  *
1480  * Returns the color of a debug category used when printing output in this
1481  * category.
1482  *
1483  * Returns: the color of the category.
1484  */
1485 guint
1486 gst_debug_category_get_color (GstDebugCategory * category)
1488   return category->color;
1491 /**
1492  * gst_debug_category_get_description:
1493  * @category: a #GstDebugCategory to get the description of.
1494  *
1495  * Returns the description of a debug category.
1496  *
1497  * Returns: the description of the category.
1498  */
1499 const gchar *
1500 gst_debug_category_get_description (GstDebugCategory * category)
1502   return category->description;
1505 /**
1506  * gst_debug_get_all_categories:
1507  *
1508  * Returns a snapshot of a all categories that are currently in use . This list
1509  * may change anytime.
1510  * The caller has to free the list after use.
1511  *
1512  * Returns: the list of categories
1513  */
1514 GSList *
1515 gst_debug_get_all_categories (void)
1517   GSList *ret;
1519   g_static_mutex_lock (&__cat_mutex);
1520   ret = g_slist_copy (__categories);
1521   g_static_mutex_unlock (&__cat_mutex);
1523   return ret;
1526 GstDebugCategory *
1527 _gst_debug_get_category (const gchar * name)
1529   GstDebugCategory *ret = NULL;
1530   GSList *node;
1532   for (node = __categories; node; node = g_slist_next (node)) {
1533     ret = (GstDebugCategory *) node->data;
1534     if (!strcmp (name, ret->name)) {
1535       return ret;
1536     }
1537   }
1538   return NULL;
1541 /*** FUNCTION POINTERS ********************************************************/
1543 static GHashTable *__gst_function_pointers;     /* NULL */
1544 static GStaticMutex __dbg_functions_mutex = G_STATIC_MUTEX_INIT;
1546 /* This function MUST NOT return NULL */
1547 const gchar *
1548 _gst_debug_nameof_funcptr (GstDebugFuncPtr func)
1550   gchar *ptrname;
1552 #ifdef HAVE_DLADDR
1553   Dl_info dl_info;
1554 #endif
1556   if (G_UNLIKELY (func == NULL))
1557     return "(NULL)";
1559   g_static_mutex_lock (&__dbg_functions_mutex);
1560   if (G_LIKELY (__gst_function_pointers)) {
1561     ptrname = g_hash_table_lookup (__gst_function_pointers, (gpointer) func);
1562     g_static_mutex_unlock (&__dbg_functions_mutex);
1563     if (G_LIKELY (ptrname))
1564       return ptrname;
1565   } else {
1566     g_static_mutex_unlock (&__dbg_functions_mutex);
1567   }
1568   /* we need to create an entry in the hash table for this one so we don't leak
1569    * the name */
1570 #ifdef HAVE_DLADDR
1571   if (dladdr ((gpointer) func, &dl_info) && dl_info.dli_sname) {
1572     gchar *name = g_strdup (dl_info.dli_sname);
1574     _gst_debug_register_funcptr (func, name);
1575     return name;
1576   } else
1577 #endif
1578   {
1579     gchar *name = g_strdup_printf ("%p", (gpointer) func);
1581     _gst_debug_register_funcptr (func, name);
1582     return name;
1583   }
1586 void
1587 _gst_debug_register_funcptr (GstDebugFuncPtr func, const gchar * ptrname)
1589   gpointer ptr = (gpointer) func;
1591   g_static_mutex_lock (&__dbg_functions_mutex);
1593   if (!__gst_function_pointers)
1594     __gst_function_pointers = g_hash_table_new (g_direct_hash, g_direct_equal);
1595   if (!g_hash_table_lookup (__gst_function_pointers, ptr))
1596     g_hash_table_insert (__gst_function_pointers, ptr, (gpointer) ptrname);
1598   g_static_mutex_unlock (&__dbg_functions_mutex);
1601 /*** PRINTF EXTENSIONS ********************************************************/
1603 #ifdef HAVE_PRINTF_EXTENSION
1604 static int
1605 _gst_info_printf_extension_ptr (FILE * stream, const struct printf_info *info,
1606     const void *const *args)
1608   char *buffer;
1609   int len;
1610   void *ptr;
1612   buffer = NULL;
1613   ptr = *(void **) args[0];
1615   buffer = gst_debug_print_object (ptr);
1616   len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1617       buffer);
1619   g_free (buffer);
1620   return len;
1623 static int
1624 _gst_info_printf_extension_segment (FILE * stream,
1625     const struct printf_info *info, const void *const *args)
1627   char *buffer;
1628   int len;
1629   void *ptr;
1631   buffer = NULL;
1632   ptr = *(void **) args[0];
1634   buffer = gst_debug_print_segment (ptr);
1635   len = fprintf (stream, "%*s", (info->left ? -info->width : info->width),
1636       buffer);
1638   g_free (buffer);
1639   return len;
1642 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
1643 static int
1644 _gst_info_printf_extension_arginfo (const struct printf_info *info, size_t n,
1645     int *argtypes, int *size)
1646 #else
1647 static int
1648 _gst_info_printf_extension_arginfo (const struct printf_info *info, size_t n,
1649     int *argtypes)
1650 #endif
1652   if (n > 0) {
1653     argtypes[0] = PA_POINTER;
1654 #ifdef HAVE_REGISTER_PRINTF_SPECIFIER
1655     *size = sizeof (gpointer);
1656 #endif
1657   }
1658   return 1;
1660 #endif /* HAVE_PRINTF_EXTENSION */
1662 static void
1663 gst_info_dump_mem_line (gchar * linebuf, gsize linebuf_size,
1664     const guint8 * mem, gsize mem_offset, gsize mem_size)
1666   gchar hexstr[50], ascstr[18], digitstr[4];
1668   if (mem_size > 16)
1669     mem_size = 16;
1671   hexstr[0] = '\0';
1672   ascstr[0] = '\0';
1674   if (mem != NULL) {
1675     guint i = 0;
1677     mem += mem_offset;
1678     while (i < mem_size) {
1679       ascstr[i] = (g_ascii_isprint (mem[i])) ? mem[i] : '.';
1680       g_snprintf (digitstr, sizeof (digitstr), "%02x ", mem[i]);
1681       g_strlcat (hexstr, digitstr, sizeof (hexstr));
1682       ++i;
1683     }
1684     ascstr[i] = '\0';
1685   }
1687   g_snprintf (linebuf, linebuf_size, "%08x: %-48.48s %-16.16s",
1688       (guint) mem_offset, hexstr, ascstr);
1691 void
1692 _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
1693     const gchar * func, gint line, GObject * obj, const gchar * msg,
1694     const guint8 * data, guint length)
1696   guint off = 0;
1698   gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "--------"
1699       "-------------------------------------------------------------------");
1701   if (msg != NULL && *msg != '\0') {
1702     gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "%s", msg);
1703   }
1705   while (off < length) {
1706     gchar buf[128];
1708     /* gst_info_dump_mem_line will process 16 bytes at most */
1709     gst_info_dump_mem_line (buf, sizeof (buf), data, off, length - off);
1710     gst_debug_log (cat, GST_LEVEL_MEMDUMP, file, func, line, obj, "%s", buf);
1711     off += 16;
1712   }
1714   gst_debug_log ((cat), GST_LEVEL_MEMDUMP, file, func, line, obj, "--------"
1715       "-------------------------------------------------------------------");
1718 #else /* !GST_DISABLE_GST_DEBUG */
1719 #ifndef GST_REMOVE_DISABLED
1721 GstDebugCategory *
1722 _gst_debug_category_new (const gchar * name, guint color,
1723     const gchar * description)
1725   return NULL;
1728 void
1729 _gst_debug_register_funcptr (GstDebugFuncPtr func, const gchar * ptrname)
1733 /* This function MUST NOT return NULL */
1734 const gchar *
1735 _gst_debug_nameof_funcptr (GstDebugFuncPtr func)
1737   return "(NULL)";
1740 void
1741 gst_debug_log (GstDebugCategory * category, GstDebugLevel level,
1742     const gchar * file, const gchar * function, gint line,
1743     GObject * object, const gchar * format, ...)
1747 void
1748 gst_debug_log_valist (GstDebugCategory * category, GstDebugLevel level,
1749     const gchar * file, const gchar * function, gint line,
1750     GObject * object, const gchar * format, va_list args)
1754 const gchar *
1755 gst_debug_message_get (GstDebugMessage * message)
1757   return "";
1760 void
1761 gst_debug_log_default (GstDebugCategory * category, GstDebugLevel level,
1762     const gchar * file, const gchar * function, gint line,
1763     GObject * object, GstDebugMessage * message, gpointer unused)
1767 G_CONST_RETURN gchar *
1768 gst_debug_level_get_name (GstDebugLevel level)
1770   return "NONE";
1773 void
1774 gst_debug_add_log_function (GstLogFunction func, gpointer data)
1778 guint
1779 gst_debug_remove_log_function (GstLogFunction func)
1781   return 0;
1784 guint
1785 gst_debug_remove_log_function_by_data (gpointer data)
1787   return 0;
1790 void
1791 gst_debug_set_active (gboolean active)
1795 gboolean
1796 gst_debug_is_active (void)
1798   return FALSE;
1801 void
1802 gst_debug_set_colored (gboolean colored)
1806 gboolean
1807 gst_debug_is_colored (void)
1809   return FALSE;
1812 void
1813 gst_debug_set_default_threshold (GstDebugLevel level)
1817 GstDebugLevel
1818 gst_debug_get_default_threshold (void)
1820   return GST_LEVEL_NONE;
1823 void
1824 gst_debug_set_threshold_for_name (const gchar * name, GstDebugLevel level)
1828 void
1829 gst_debug_unset_threshold_for_name (const gchar * name)
1833 void
1834 gst_debug_category_free (GstDebugCategory * category)
1838 void
1839 gst_debug_category_set_threshold (GstDebugCategory * category,
1840     GstDebugLevel level)
1844 void
1845 gst_debug_category_reset_threshold (GstDebugCategory * category)
1849 GstDebugLevel
1850 gst_debug_category_get_threshold (GstDebugCategory * category)
1852   return GST_LEVEL_NONE;
1855 G_CONST_RETURN gchar *
1856 gst_debug_category_get_name (GstDebugCategory * category)
1858   return "";
1861 guint
1862 gst_debug_category_get_color (GstDebugCategory * category)
1864   return 0;
1867 G_CONST_RETURN gchar *
1868 gst_debug_category_get_description (GstDebugCategory * category)
1870   return "";
1873 GSList *
1874 gst_debug_get_all_categories (void)
1876   return NULL;
1879 GstDebugCategory *
1880 _gst_debug_get_category (const gchar * name)
1882   return NULL;
1885 gchar *
1886 gst_debug_construct_term_color (guint colorinfo)
1888   return g_strdup ("00");
1891 gint
1892 gst_debug_construct_win_color (guint colorinfo)
1894   return 0;
1897 gboolean
1898 _priv_gst_in_valgrind (void)
1900   return FALSE;
1903 void
1904 _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
1905     const gchar * func, gint line, GObject * obj, const gchar * msg,
1906     const guint8 * data, guint length)
1909 #endif /* GST_REMOVE_DISABLED */
1910 #endif /* GST_DISABLE_GST_DEBUG */
1913 #ifdef GST_ENABLE_FUNC_INSTRUMENTATION
1914 /* FIXME make this thread specific */
1915 static GSList *stack_trace = NULL;
1917 void
1918 __cyg_profile_func_enter (void *this_fn, void *call_site)
1919     G_GNUC_NO_INSTRUMENT;
1920      void __cyg_profile_func_enter (void *this_fn, void *call_site)
1922   gchar *name = _gst_debug_nameof_funcptr (this_fn);
1923   gchar *site = _gst_debug_nameof_funcptr (call_site);
1925   GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "entering function %s from %s", name,
1926       site);
1927   stack_trace =
1928       g_slist_prepend (stack_trace, g_strdup_printf ("%8p in %s from %p (%s)",
1929           this_fn, name, call_site, site));
1931   g_free (name);
1932   g_free (site);
1935 void
1936 __cyg_profile_func_exit (void *this_fn, void *call_site)
1937     G_GNUC_NO_INSTRUMENT;
1938      void __cyg_profile_func_exit (void *this_fn, void *call_site)
1940   gchar *name = _gst_debug_nameof_funcptr (this_fn);
1942   GST_CAT_DEBUG (GST_CAT_CALL_TRACE, "leaving function %s", name);
1943   g_free (stack_trace->data);
1944   stack_trace = g_slist_delete_link (stack_trace, stack_trace);
1946   g_free (name);
1949 /**
1950  * gst_debug_print_stack_trace:
1951  *
1952  * If GST_ENABLE_FUNC_INSTRUMENTATION is defined a stacktrace is available for
1953  * gstreamer code, which can be printed with this function.
1954  */
1955 void
1956 gst_debug_print_stack_trace (void)
1958   GSList *walk = stack_trace;
1959   gint count = 0;
1961   if (walk)
1962     walk = g_slist_next (walk);
1964   while (walk) {
1965     gchar *name = (gchar *) walk->data;
1967     g_print ("#%-2d %s\n", count++, name);
1969     walk = g_slist_next (walk);
1970   }
1972 #else
1973 void
1974 gst_debug_print_stack_trace (void)
1976   /* nothing because it's compiled out */
1979 #endif /* GST_ENABLE_FUNC_INSTRUMENTATION */