3abdb2dd42512de0733a3ca29224fa11169f9762
1 /* GStreamer
2 * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3 * 2000 Wim Taymans <wtay@chello.be>
4 * 2003 Benjamin Otte <in7y118@public.uni-hamburg.de>
5 *
6 * gstinfo.h: debugging functions
7 *
8 * This library is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU Library General Public
10 * License as published by the Free Software Foundation; either
11 * version 2 of the License, or (at your option) any later version.
12 *
13 * This library is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
16 * Library General Public License for more details.
17 *
18 * You should have received a copy of the GNU Library General Public
19 * License along with this library; if not, write to the
20 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
21 * Boston, MA 02111-1307, USA.
22 */
24 #ifndef __GSTINFO_H__
25 #define __GSTINFO_H__
27 #include <glib.h>
28 #include <glib-object.h>
29 #include <gst/gstconfig.h>
31 G_BEGIN_DECLS
33 /**
34 * GstDebugLevel:
35 * @GST_LEVEL_NONE: No debugging level specified or desired. Used to deactivate
36 * debugging output.
37 * @GST_LEVEL_ERROR: Error messages are to be used only when an error occured
38 * that stops the application from keeping working correctly.
39 * An examples is gst_element_error, which outputs a message with this priority.
40 * It does not mean that the application is terminating as with g_errror.
41 * @GST_LEVEL_WARNING: Warning messages are to inform about abnormal behaviour
42 * that could lead to problems or weird behaviour later on. An example of this
43 * would be clocking issues ("your computer is pretty slow") or broken input
44 * data ("Can't synchronize to stream.")
45 * @GST_LEVEL_INFO: Informational messages should be used to keep the developer
46 * updated about what is happening.
47 * Examples where this should be used are when a typefind function has
48 * successfully determined the type of the stream or when an mp3 plugin detects
49 * the format to be used. ("This file has mono sound.")
50 * @GST_LEVEL_DEBUG: Debugging messages should be used when something common
51 * happens that is not the expected default behavior, or something that's
52 * useful to know but doesn't happen all the time (ie. per loop iteration or
53 * buffer processed or event handled).
54 * An example would be notifications about state changes or receiving/sending
55 * of events.
56 * @GST_LEVEL_LOG: Log messages are messages that are very common but might be
57 * useful to know. As a rule of thumb a pipeline that is iterating as expected
58 * should never output anything else but LOG messages. Use this log level to
59 * log recurring information in chain functions and loop functions, for
60 * example.
61 * @GST_LEVEL_FIXME: Fixme messages are messages that indicate that something
62 * in the executed code path is not fully implemented or handled yet. Note
63 * that this does not replace proper error handling in any way, the purpose
64 * of this message is to make it easier to spot incomplete/unfinished pieces
65 * of code when reading the debug log. (Since: 0.10.23)
66 * @GST_LEVEL_TRACE: Tracing-related messages (Since: 0.10.30)
67 * Examples for this are referencing/dereferencing of objects.
68 * @GST_LEVEL_MEMDUMP: memory dump messages are used to log (small) chunks of
69 * data as memory dumps in the log. They will be displayed as hexdump with
70 * ASCII characters. (Since: 0.10.23)
71 * @GST_LEVEL_COUNT: The number of defined debugging levels.
72 *
73 * The level defines the importance of a debugging message. The more important a
74 * message is, the greater the probability that the debugging system outputs it.
75 */
76 typedef enum {
77 GST_LEVEL_NONE = 0,
78 GST_LEVEL_ERROR,
79 GST_LEVEL_WARNING,
80 GST_LEVEL_INFO,
81 GST_LEVEL_DEBUG,
82 GST_LEVEL_LOG,
83 GST_LEVEL_FIXME = 6,
84 GST_LEVEL_TRACE = 7,
85 /* add more */
86 GST_LEVEL_MEMDUMP = 9,
87 /* add more */
88 GST_LEVEL_COUNT
89 } GstDebugLevel;
91 /**
92 * GST_LEVEL_DEFAULT:
93 *
94 * Defines the default debugging level to be used with GStreamer. It is normally
95 * set to #GST_LEVEL_NONE so nothing get printed.
96 * As it can be configured at compile time, developer builds may chose to
97 * override that though.
98 * You can use this as an argument to gst_debug_set_default_threshold() to
99 * reset the debugging output to default behaviour.
100 */
101 #ifndef GST_LEVEL_DEFAULT
102 #define GST_LEVEL_DEFAULT GST_LEVEL_NONE
103 #endif
105 /* defines for format (colors etc)
106 * don't change them around, it uses terminal layout
107 * Terminal color strings:
108 * 00=none 01=bold 04=underscore 05=blink 07=reverse 08=concealed
109 * Text color codes:
110 * 30=black 31=red 32=green 33=yellow 34=blue 35=magenta 36=cyan 37=white
111 * Background color codes:
112 * 40=black 41=red 42=green 43=yellow 44=blue 45=magenta 46=cyan 47=white
113 */
114 /**
115 * GstDebugColorFlags:
116 * @GST_DEBUG_FG_BLACK: Use black as foreground color.
117 * @GST_DEBUG_FG_RED: Use red as foreground color.
118 * @GST_DEBUG_FG_GREEN: Use green as foreground color.
119 * @GST_DEBUG_FG_YELLOW: Use yellow as foreground color.
120 * @GST_DEBUG_FG_BLUE: Use blue as foreground color.
121 * @GST_DEBUG_FG_MAGENTA: Use magenta as foreground color.
122 * @GST_DEBUG_FG_CYAN: Use cyan as foreground color.
123 * @GST_DEBUG_FG_WHITE: Use white as foreground color.
124 * @GST_DEBUG_BG_BLACK: Use black as background color.
125 * @GST_DEBUG_BG_RED: Use red as background color.
126 * @GST_DEBUG_BG_GREEN: Use green as background color.
127 * @GST_DEBUG_BG_YELLOW: Use yellow as background color.
128 * @GST_DEBUG_BG_BLUE: Use blue as background color.
129 * @GST_DEBUG_BG_MAGENTA: Use magenta as background color.
130 * @GST_DEBUG_BG_CYAN: Use cyan as background color.
131 * @GST_DEBUG_BG_WHITE: Use white as background color.
132 * @GST_DEBUG_BOLD: Make the output bold.
133 * @GST_DEBUG_UNDERLINE: Underline the output.
134 *
135 * These are some terminal style flags you can use when creating your
136 * debugging categories to make them stand out in debugging output.
137 */
138 typedef enum {
139 /* colors */
140 GST_DEBUG_FG_BLACK = 0x0000,
141 GST_DEBUG_FG_RED = 0x0001,
142 GST_DEBUG_FG_GREEN = 0x0002,
143 GST_DEBUG_FG_YELLOW = 0x0003,
144 GST_DEBUG_FG_BLUE = 0x0004,
145 GST_DEBUG_FG_MAGENTA = 0x0005,
146 GST_DEBUG_FG_CYAN = 0x0006,
147 GST_DEBUG_FG_WHITE = 0x0007,
148 /* background colors */
149 GST_DEBUG_BG_BLACK = 0x0000,
150 GST_DEBUG_BG_RED = 0x0010,
151 GST_DEBUG_BG_GREEN = 0x0020,
152 GST_DEBUG_BG_YELLOW = 0x0030,
153 GST_DEBUG_BG_BLUE = 0x0040,
154 GST_DEBUG_BG_MAGENTA = 0x0050,
155 GST_DEBUG_BG_CYAN = 0x0060,
156 GST_DEBUG_BG_WHITE = 0x0070,
157 /* other formats */
158 GST_DEBUG_BOLD = 0x0100,
159 GST_DEBUG_UNDERLINE = 0x0200
160 } GstDebugColorFlags;
162 #define GST_DEBUG_FG_MASK (0x000F)
163 #define GST_DEBUG_BG_MASK (0x00F0)
164 #define GST_DEBUG_FORMAT_MASK (0xFF00)
166 typedef struct _GstDebugCategory GstDebugCategory;
167 /**
168 * GstDebugCategory:
169 *
170 * This is the struct that describes the categories. Once initialized with
171 * #GST_DEBUG_CATEGORY_INIT, its values can't be changed anymore.
172 */
173 struct _GstDebugCategory {
174 /*< private >*/
175 gint threshold;
176 guint color; /* see defines above */
178 const gchar * name;
179 const gchar * description;
181 void *ext; /**< for use by LD_PRELOADED trace extension */
182 };
184 /********** some convenience macros for debugging **********/
186 /**
187 * GST_STR_NULL:
188 * @str: The string to check.
189 *
190 * Macro to use when a string must not be NULL, but may be NULL. If the string
191 * is NULL, "(NULL)" is printed instead.
192 * In GStreamer printf string arguments may not be NULL, because on some
193 * platforms (ie Solaris) the libc crashes in that case. This includes debugging
194 * strings.
195 */
196 #define GST_STR_NULL(str) ((str) ? (str) : "(NULL)")
198 /* FIXME, not MT safe */
199 /**
200 * GST_DEBUG_PAD_NAME:
201 * @pad: The pad to debug.
202 *
203 * Evaluates to 2 strings, that describe the pad. Often used in debugging
204 * statements.
205 */
206 #define GST_DEBUG_PAD_NAME(pad) \
207 (pad != NULL) ? \
208 ((GST_OBJECT_PARENT(pad) != NULL) ? \
209 GST_STR_NULL (GST_OBJECT_NAME (GST_OBJECT_PARENT(pad))) : \
210 "''" ) : "''", \
211 (pad != NULL) ? GST_STR_NULL (GST_OBJECT_NAME (pad)) : "''"
213 /**
214 * GST_FUNCTION:
215 *
216 * This macro should evaluate to the name of the current function and be should
217 * be defined when configuring your project, as it is compiler dependant. If it
218 * is not defined, some default value is used. It is used to provide debugging
219 * output with the function name of the message.
220 *
221 * Note that this is different from G_STRFUNC as we do not want the full
222 * function signature in C++ code.
223 */
224 #ifndef GST_FUNCTION
225 #if defined (__GNUC__) || (defined (_MSC_VER) && _MSC_VER >= 1300)
226 # define GST_FUNCTION ((const char*) (__FUNCTION__))
227 #elif defined (__STDC__) && defined (__STDC_VERSION__) && __STDC_VERSION__ >= 199901L
228 # define GST_FUNCTION ((const char*) (__func__))
229 #else
230 # define GST_FUNCTION ((const char*) ("???"))
231 #endif
232 #endif /* ifndef GST_FUNCTION */
235 typedef struct _GstDebugMessage GstDebugMessage;
237 /**
238 * GstLogFunction:
239 * @category: a #GstDebugCategory
240 * @level: a #GstDebugLevel
241 * @file: file name
242 * @function: function name
243 * @line: line number
244 * @object: a #GObject
245 * @message: the message
246 * @data: user data for the log function
247 *
248 * Function prototype for a logging function that can be registered with
249 * gst_debug_add_log_function().
250 * Use G_GNUC_NO_INSTRUMENT on that function.
251 */
252 typedef void (*GstLogFunction) (GstDebugCategory * category,
253 GstDebugLevel level,
254 const gchar * file,
255 const gchar * function,
256 gint line,
257 GObject * object,
258 GstDebugMessage * message,
259 gpointer data);
262 /* FIXME 0.11: move this into private headers */
263 void _gst_debug_init (void);
265 typedef struct {
266 const gchar *file;
267 const gchar *function;
268 const gint line;
269 } GstDebugTraceLocation;
271 #define GST_DEBUG_TRACE_LOCATION() \
272 { __FILE__, GST_FUNCTION, __LINE__ }
274 #ifdef GST_USING_PRINTF_EXTENSION
276 /* not using G_GNUC_PRINTF, since gcc will choke on GST_PTR_FORMAT being %P */
277 void gst_debug_log (GstDebugCategory * category,
278 GstDebugLevel level,
279 const gchar * file,
280 const gchar * function,
281 gint line,
282 GObject * object,
283 const gchar * format,
284 ...) G_GNUC_NO_INSTRUMENT;
286 void gst_debug_log2 (GstDebugCategory * category,
287 GstDebugLevel level,
288 const GstDebugTraceLocation *location,
289 GObject * object,
290 const gchar * format,
291 ...) G_GNUC_NO_INSTRUMENT;
293 #else /* GST_USING_PRINTF_EXTENSION */
295 void gst_debug_log (GstDebugCategory * category,
296 GstDebugLevel level,
297 const gchar * file,
298 const gchar * function,
299 gint line,
300 GObject * object,
301 const gchar * format,
302 ...) G_GNUC_PRINTF (7, 8) G_GNUC_NO_INSTRUMENT;
304 void gst_debug_log2 (GstDebugCategory * category,
305 GstDebugLevel level,
306 const GstDebugTraceLocation *location,
307 GObject * object,
308 const gchar * format,
309 ...) G_GNUC_PRINTF (5, 6) G_GNUC_NO_INSTRUMENT;
311 #endif /* GST_USING_PRINTF_EXTENSION */
313 void gst_debug_log_valist (GstDebugCategory * category,
314 GstDebugLevel level,
315 const gchar * file,
316 const gchar * function,
317 gint line,
318 GObject * object,
319 const gchar * format,
320 va_list args) G_GNUC_NO_INSTRUMENT;
322 /* do not use this function, use the GST_DEBUG_CATEGORY_INIT macro */
323 GstDebugCategory *_gst_debug_category_new (const gchar * name,
324 guint color,
325 const gchar * description);
326 /* do not use this function, use the GST_DEBUG_CATEGORY_GET macro */
327 GstDebugCategory *_gst_debug_get_category (const gchar *name);
330 /* do not use this function, use the GST_CAT_MEMDUMP_* macros */
331 void _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
332 const gchar * func, gint line, GObject * obj, const gchar * msg,
333 const guint8 * data, guint length);
335 /* we define this to avoid a compiler warning regarding a cast from a function
336 * pointer to a void pointer
337 * (see https://bugzilla.gnome.org/show_bug.cgi?id=309253)
338 */
339 typedef void (* GstDebugFuncPtr) (void);
341 /* do no use these functions, use the GST_DEBUG*_FUNCPTR macros */
342 void _gst_debug_register_funcptr (GstDebugFuncPtr func,
343 const gchar * ptrname);
344 const gchar *
345 _gst_debug_nameof_funcptr (GstDebugFuncPtr func) G_GNUC_NO_INSTRUMENT;
348 void gst_debug_log_valist2 (GstDebugCategory * category,
349 GstDebugLevel level,
350 const GstDebugTraceLocation *location,
351 GObject * object,
352 const gchar * format,
353 va_list args) G_GNUC_NO_INSTRUMENT;
355 const gchar * gst_debug_message_get (GstDebugMessage * message);
357 gchar * gst_debug_print_object (gpointer ptr);
359 #ifdef HAVE_PRINTF_EXTENSION
360 gchar * gst_debug_print_segment (gpointer ptr);
361 #endif
363 void gst_debug_log_default (GstDebugCategory * category,
364 GstDebugLevel level,
365 const gchar * file,
366 const gchar * function,
367 gint line,
368 GObject * object,
369 GstDebugMessage * message,
370 gpointer unused) G_GNUC_NO_INSTRUMENT;
372 const gchar * gst_debug_level_get_name (GstDebugLevel level);
374 void gst_debug_add_log_function (GstLogFunction func,
375 gpointer data);
377 guint gst_debug_remove_log_function (GstLogFunction func);
378 guint gst_debug_remove_log_function_by_data (gpointer data);
380 void gst_debug_set_active (gboolean active);
381 gboolean gst_debug_is_active (void);
383 void gst_debug_set_colored (gboolean colored);
384 gboolean gst_debug_is_colored (void);
386 void gst_debug_set_default_threshold (GstDebugLevel level);
387 GstDebugLevel gst_debug_get_default_threshold (void);
388 void gst_debug_set_threshold_for_name (const gchar * name,
389 GstDebugLevel level);
390 void gst_debug_unset_threshold_for_name (const gchar * name);
393 void gst_debug_category_free (GstDebugCategory * category);
394 void gst_debug_category_set_threshold (GstDebugCategory * category,
395 GstDebugLevel level);
396 void gst_debug_category_reset_threshold (GstDebugCategory * category);
397 GstDebugLevel gst_debug_category_get_threshold (GstDebugCategory * category);
398 const gchar * gst_debug_category_get_name (GstDebugCategory * category);
399 guint gst_debug_category_get_color (GstDebugCategory * category);
400 const gchar * gst_debug_category_get_description (GstDebugCategory * category);
401 GSList * gst_debug_get_all_categories (void);
404 gchar * gst_debug_construct_term_color (guint colorinfo);
405 gint gst_debug_construct_win_color (guint colorinfo);
408 #ifndef GST_DISABLE_GST_DEBUG
410 #define gst_debug_add_log_function(func,data) \
411 G_STMT_START{ \
412 if (func == gst_debug_log_default) { \
413 gst_debug_add_log_function(NULL,data); \
414 } else { \
415 gst_debug_add_log_function(func,data); \
416 } \
417 }G_STMT_END
419 #define gst_debug_remove_log_function(func) \
420 (func == gst_debug_log_default) ? \
421 gst_debug_remove_log_function(NULL) : \
422 gst_debug_remove_log_function(func)
424 /**
425 * GST_DEBUG_CATEGORY:
426 * @cat: the category
427 *
428 * Defines a GstDebugCategory variable.
429 * This macro expands to nothing if debugging is disabled.
430 */
431 #define GST_DEBUG_CATEGORY(cat) GstDebugCategory *cat = NULL
432 /**
433 * GST_DEBUG_CATEGORY_EXTERN:
434 * @cat: the category
435 *
436 * Declares a GstDebugCategory variable as extern. Use in header files.
437 * This macro expands to nothing if debugging is disabled.
438 */
439 #define GST_DEBUG_CATEGORY_EXTERN(cat) extern GstDebugCategory *cat
441 /**
442 * GST_DEBUG_CATEGORY_STATIC:
443 * @cat: the category
444 *
445 * Defines a static GstDebugCategory variable.
446 * This macro expands to nothing if debugging is disabled.
447 */
448 #define GST_DEBUG_CATEGORY_STATIC(cat) static GstDebugCategory *cat = NULL
450 /**
451 * GST_DEBUG_CATEGORY_INIT:
452 * @cat: the category to initialize.
453 * @name: the name of the category.
454 * @color: the colors to use for a color representation or 0 for no color.
455 * @description: optional description of the category.
456 *
457 * Initializes a new #GstDebugCategory with the given properties and set to
458 * the default threshold.
459 *
460 * <note>
461 * <para>
462 * This macro expands to nothing if debugging is disabled.
463 * </para>
464 * <para>
465 * When naming your category, please follow the following conventions to ensure
466 * that the pattern matching for categories works as expected. It is not
467 * earth-shattering if you don't follow these conventions, but it would be nice
468 * for everyone.
469 * </para>
470 * <para>
471 * If you define a category for a plugin or a feature of it, name the category
472 * like the feature. So if you wanted to write a "filesrc" element, you would
473 * name the category "filesrc". Use lowercase letters only.
474 * If you define more than one category for the same element, append an
475 * underscore and an identifier to your categories, like this: "filesrc_cache"
476 * </para>
477 * <para>
478 * If you create a library or an application using debugging categories, use a
479 * common prefix followed by an underscore for all your categories. GStreamer
480 * uses the GST prefix so GStreamer categories look like "GST_STATES". Be sure
481 * to include uppercase letters.
482 * </para>
483 * </note>
484 */
485 #define GST_DEBUG_CATEGORY_INIT(cat,name,color,description) G_STMT_START{\
486 if (cat == NULL) \
487 cat = _gst_debug_category_new (name,color,description); \
488 }G_STMT_END
490 /**
491 * GST_DEBUG_CATEGORY_GET:
492 * @cat: the category to initialize.
493 * @name: log category name
494 *
495 * Looks up an existing #GstDebugCategory by its @name and sets @cat. If the
496 * category is not found, but GST_CAT_DEFAULT is defined, that is assigned to
497 * @cat. Otherwise @cat will be NULL.
498 *
499 * |[
500 * GST_DEBUG_CATEGORY_STATIC (gst_myplugin_debug);
501 * #define GST_CAT_DEFAULT gst_myplugin_debug
502 * GST_DEBUG_CATEGORY_STATIC (GST_CAT_PERFORMANCE);
503 * ...
504 * GST_DEBUG_CATEGORY_INIT (gst_myplugin_debug, "myplugin", 0, "nice element");
505 * GST_DEBUG_CATEGORY_GET (GST_CAT_PERFORMANCE, "GST_PERFORMANCE");
506 * ]|
507 *
508 * Since: 0.10.24
509 */
510 #ifdef GST_CAT_DEFAULT
511 #define GST_DEBUG_CATEGORY_GET(cat,name) G_STMT_START{\
512 cat = _gst_debug_get_category (name); \
513 if (!cat) { \
514 cat = GST_CAT_DEFAULT; \
515 } \
516 }G_STMT_END
517 #else
518 #define GST_DEBUG_CATEGORY_GET(cat,name) G_STMT_START{\
519 cat = _gst_debug_get_category (name); \
520 }G_STMT_END
521 #endif
523 /**
524 * GST_CAT_DEFAULT:
525 *
526 * Default gstreamer core debug log category. Please define your own.
527 */
528 GST_EXPORT GstDebugCategory * GST_CAT_DEFAULT;
529 /* this symbol may not be used */
530 extern gboolean __gst_debug_enabled;
532 /* since 0.10.7, the min debug level, used for quickly discarding debug
533 * messages that fall under the threshold. */
534 GST_EXPORT GstDebugLevel __gst_debug_min;
536 /**
537 * GST_CAT_LEVEL_LOG:
538 * @cat: category to use
539 * @level: the severity of the message
540 * @object: the #GObject the message belongs to or NULL if none
541 * @...: A printf-style message to output
542 *
543 * Outputs a debugging message. This is the most general macro for outputting
544 * debugging messages. You will probably want to use one of the ones described
545 * below.
546 */
547 #if defined(GST_USING_PRINTF_EXTENSION) && defined(G_HAVE_GNUC_VARARGS)
548 #define GST_CAT_LEVEL_LOG_obj(cat,level,object,str,args...) G_STMT_START{ \
549 if (G_UNLIKELY (level <= __gst_debug_min)) { \
550 const GstDebugTraceLocation loc = GST_DEBUG_TRACE_LOCATION(); \
551 gst_debug_log2 ((cat), (level), &loc, NULL, "%"GST_PTR_FORMAT" "str, \
552 (object), ##args ); \
553 } \
554 }G_STMT_END
555 #define GST_CAT_LEVEL_LOG_noobj(cat,level,object,str,args...) G_STMT_START{\
556 if (G_UNLIKELY (level <= __gst_debug_min)) { \
557 const GstDebugTraceLocation loc = GST_DEBUG_TRACE_LOCATION(); \
558 gst_debug_log2 ((cat), (level), &loc, NULL, (str), ##args ); \
559 } \
560 }G_STMT_END
561 #else
562 # define GST_CAT_LEVEL_LOG_obj GST_CAT_LEVEL_LOG
563 # define GST_CAT_LEVEL_LOG_noobj GST_CAT_LEVEL_LOG
564 #endif
567 #ifdef G_HAVE_ISO_VARARGS
568 #define GST_CAT_LEVEL_LOG(cat,level,object,...) G_STMT_START{ \
569 if (G_UNLIKELY (level <= __gst_debug_min)) { \
570 const GstDebugTraceLocation loc = GST_DEBUG_TRACE_LOCATION(); \
571 gst_debug_log2 ((cat), (level), &loc, (GObject *) (object), \
572 __VA_ARGS__); \
573 } \
574 }G_STMT_END
575 #else /* G_HAVE_GNUC_VARARGS */
576 #ifdef G_HAVE_GNUC_VARARGS
577 #define GST_CAT_LEVEL_LOG(cat,level,object,args...) G_STMT_START{ \
578 if (G_UNLIKELY (level <= __gst_debug_min)) { \
579 const GstDebugTraceLocation loc = GST_DEBUG_TRACE_LOCATION(); \
580 gst_debug_log2 ((cat), (level), &loc, (GObject *) (object), \
581 ##args ); \
582 } \
583 }G_STMT_END
584 #else /* no variadic macros, use inline */
585 static inline void
586 GST_CAT_LEVEL_LOG_valist (GstDebugCategory * cat,
587 GstDebugLevel level, gpointer object, const char *format, va_list varargs)
588 {
589 if (G_UNLIKELY (level <= __gst_debug_min)) {
590 gst_debug_log_valist (cat, level, "", "", 0, (GObject *) object, format,
591 varargs);
592 }
593 }
595 static inline void
596 GST_CAT_LEVEL_LOG (GstDebugCategory * cat, GstDebugLevel level,
597 gpointer object, const char *format, ...)
598 {
599 va_list varargs;
601 va_start (varargs, format);
602 GST_CAT_LEVEL_LOG_valist (cat, level, object, format, varargs);
603 va_end (varargs);
604 }
605 #endif
606 #endif /* G_HAVE_ISO_VARARGS */
608 /* This one doesn't have varargs in the macro, so it's different than all the
609 * other macros and hence in a separate block right here. Docs chunks are
610 * with the other doc chunks below though. */
611 #define __GST_CAT_MEMDUMP_LOG(cat,object,msg,data,length) G_STMT_START{ \
612 if (G_UNLIKELY (GST_LEVEL_MEMDUMP <= __gst_debug_min)) { \
613 _gst_debug_dump_mem ((cat), __FILE__, GST_FUNCTION, __LINE__, \
614 (GObject *) (object), (msg), (data), (length)); \
615 } \
616 }G_STMT_END
618 #define GST_CAT_MEMDUMP_OBJECT(cat,obj,msg,data,length) \
619 __GST_CAT_MEMDUMP_LOG(cat,obj,msg,data,length)
620 #define GST_CAT_MEMDUMP(cat,msg,data,length) \
621 __GST_CAT_MEMDUMP_LOG(cat,NULL,msg,data,length)
622 #define GST_MEMDUMP_OBJECT(obj,msg,data,length) \
623 __GST_CAT_MEMDUMP_LOG(GST_CAT_DEFAULT,obj,msg,data,length)
624 #define GST_MEMDUMP(msg,data,length) \
625 __GST_CAT_MEMDUMP_LOG(GST_CAT_DEFAULT,NULL,msg,data,length)
627 /**
628 * GST_CAT_ERROR_OBJECT:
629 * @cat: category to use
630 * @obj: the #GObject the message belongs to
631 * @...: printf-style message to output
632 *
633 * Output an error message belonging to the given object in the given category.
634 */
635 /**
636 * GST_CAT_WARNING_OBJECT:
637 * @cat: category to use
638 * @obj: the #GObject the message belongs to
639 * @...: printf-style message to output
640 *
641 * Output a warning message belonging to the given object in the given category.
642 */
643 /**
644 * GST_CAT_INFO_OBJECT:
645 * @cat: category to use
646 * @obj: the #GObject the message belongs to
647 * @...: printf-style message to output
648 *
649 * Output an informational message belonging to the given object in the given
650 * category.
651 */
652 /**
653 * GST_CAT_DEBUG_OBJECT:
654 * @cat: category to use
655 * @obj: the #GObject the message belongs to
656 * @...: printf-style message to output
657 *
658 * Output an debugging message belonging to the given object in the given category.
659 */
660 /**
661 * GST_CAT_LOG_OBJECT:
662 * @cat: category to use
663 * @obj: the #GObject the message belongs to
664 * @...: printf-style message to output
665 *
666 * Output an logging message belonging to the given object in the given category.
667 */
668 /**
669 * GST_CAT_FIXME_OBJECT:
670 * @cat: category to use
671 * @obj: the #GObject the message belongs to
672 * @...: printf-style message to output
673 *
674 * Output a fixme message belonging to the given object in the given category.
675 *
676 * Since: 0.10.23
677 */
678 /**
679 * GST_CAT_TRACE_OBJECT:
680 * @cat: category to use
681 * @obj: the #GObject the message belongs to
682 * @...: printf-style message to output
683 *
684 * Output a tracing message belonging to the given object in the given
685 * category.
686 *
687 * Since: 0.10.30
688 */
689 /**
690 * GST_CAT_MEMDUMP_OBJECT:
691 * @cat: category to use
692 * @obj: the #GObject the message belongs to
693 * @msg: message string to log with the data
694 * @data: pointer to the data to output
695 * @length: length of the data to output
696 *
697 * Output a hexdump of @data relating to the given object in the given
698 * category.
699 *
700 * Since: 0.10.23
701 */
704 /**
705 * GST_CAT_ERROR:
706 * @cat: category to use
707 * @...: printf-style message to output
708 *
709 * Output an error message in the given category.
710 */
711 /**
712 * GST_CAT_WARNING:
713 * @cat: category to use
714 * @...: printf-style message to output
715 *
716 * Output an warning message in the given category.
717 */
718 /**
719 * GST_CAT_INFO:
720 * @cat: category to use
721 * @...: printf-style message to output
722 *
723 * Output an informational message in the given category.
724 */
725 /**
726 * GST_CAT_DEBUG:
727 * @cat: category to use
728 * @...: printf-style message to output
729 *
730 * Output an debugging message in the given category.
731 */
732 /**
733 * GST_CAT_LOG:
734 * @cat: category to use
735 * @...: printf-style message to output
736 *
737 * Output an logging message in the given category.
738 */
739 /**
740 * GST_CAT_FIXME:
741 * @cat: category to use
742 * @...: printf-style message to output
743 *
744 * Output an fixme message in the given category.
745 *
746 * Since: 0.10.23
747 */
748 /**
749 * GST_CAT_TRACE:
750 * @cat: category to use
751 * @...: printf-style message to output
752 *
753 * Output a tracing message in the given category.
754 *
755 * Since: 0.10.30
756 */
757 /**
758 * GST_CAT_MEMDUMP:
759 * @cat: category to use
760 * @msg: message string to log with the data
761 * @data: pointer to the data to output
762 * @length: length of the data to output
763 *
764 * Output a hexdump of @data in the given category.
765 *
766 * Since: 0.10.23
767 */
770 /**
771 * GST_ERROR_OBJECT:
772 * @obj: the #GObject the message belongs to
773 * @...: printf-style message to output
774 *
775 * Output an error message belonging to the given object in the default category.
776 */
777 /**
778 * GST_WARNING_OBJECT:
779 * @obj: the #GObject the message belongs to
780 * @...: printf-style message to output
781 *
782 * Output a warning message belonging to the given object in the default category.
783 */
784 /**
785 * GST_INFO_OBJECT:
786 * @obj: the #GObject the message belongs to
787 * @...: printf-style message to output
788 *
789 * Output an informational message belonging to the given object in the default
790 * category.
791 */
792 /**
793 * GST_DEBUG_OBJECT:
794 * @obj: the #GObject the message belongs to
795 * @...: printf-style message to output
796 *
797 * Output a debugging message belonging to the given object in the default
798 * category.
799 */
800 /**
801 * GST_LOG_OBJECT:
802 * @obj: the #GObject the message belongs to
803 * @...: printf-style message to output
804 *
805 * Output a logging message belonging to the given object in the default category.
806 */
807 /**
808 * GST_FIXME_OBJECT:
809 * @obj: the #GObject the message belongs to
810 * @...: printf-style message to output
811 *
812 * Output a fixme message belonging to the given object in the default category.
813 *
814 * Since: 0.10.23
815 */
816 /**
817 * GST_TRACE_OBJECT:
818 * @obj: the #GObject the message belongs to
819 * @...: printf-style message to output
820 *
821 * Output a tracing message belonging to the given object in the default category.
822 *
823 * Since: 0.10.30
824 */
825 /**
826 * GST_MEMDUMP_OBJECT:
827 * @obj: the #GObject the message belongs to
828 * @msg: message string to log with the data
829 * @data: pointer to the data to output
830 * @length: length of the data to output
831 *
832 * Output a logging message belonging to the given object in the default category.
833 *
834 * Since: 0.10.23
835 */
838 /**
839 * GST_ERROR:
840 * @...: printf-style message to output
841 *
842 * Output an error message in the default category.
843 */
844 /**
845 * GST_WARNING:
846 * @...: printf-style message to output
847 *
848 * Output a warning message in the default category.
849 */
850 /**
851 * GST_INFO:
852 * @...: printf-style message to output
853 *
854 * Output an informational message in the default category.
855 */
856 /**
857 * GST_DEBUG:
858 * @...: printf-style message to output
859 *
860 * Output a debugging message in the default category.
861 */
862 /**
863 * GST_LOG:
864 * @...: printf-style message to output
865 *
866 * Output a logging message in the default category.
867 */
868 /**
869 * GST_FIXME:
870 * @...: printf-style message to output
871 *
872 * Output a fixme message in the default category.
873 *
874 * Since: 0.10.23
875 */
876 /**
877 * GST_TRACE:
878 * @...: printf-style message to output
879 *
880 * Output a tracing message in the default category.
881 *
882 * Since: 0.10.30
883 */
884 /**
885 * GST_MEMDUMP:
886 * @msg: message string to log with the data
887 * @data: pointer to the data to output
888 * @length: length of the data to output
889 *
890 * Output a hexdump of @data.
891 *
892 * Since: 0.10.23
893 */
895 #ifdef G_HAVE_ISO_VARARGS
897 #define GST_CAT_ERROR_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR, obj, __VA_ARGS__)
898 #define GST_CAT_WARNING_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, obj, __VA_ARGS__)
899 #define GST_CAT_INFO_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO, obj, __VA_ARGS__)
900 #define GST_CAT_DEBUG_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG, obj, __VA_ARGS__)
901 #define GST_CAT_LOG_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG, obj, __VA_ARGS__)
902 #define GST_CAT_FIXME_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME, obj, __VA_ARGS__)
903 #define GST_CAT_TRACE_OBJECT(cat,obj,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE, obj, __VA_ARGS__)
905 #define GST_CAT_ERROR(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR, NULL, __VA_ARGS__)
906 #define GST_CAT_WARNING(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, NULL, __VA_ARGS__)
907 #define GST_CAT_INFO(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO, NULL, __VA_ARGS__)
908 #define GST_CAT_DEBUG(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG, NULL, __VA_ARGS__)
909 #define GST_CAT_LOG(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG, NULL, __VA_ARGS__)
910 #define GST_CAT_FIXME(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME, NULL, __VA_ARGS__)
911 #define GST_CAT_TRACE(cat,...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE, NULL, __VA_ARGS__)
913 #define GST_ERROR_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR, obj, __VA_ARGS__)
914 #define GST_WARNING_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, obj, __VA_ARGS__)
915 #define GST_INFO_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO, obj, __VA_ARGS__)
916 #define GST_DEBUG_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, obj, __VA_ARGS__)
917 #define GST_LOG_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG, obj, __VA_ARGS__)
918 #define GST_FIXME_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME, obj, __VA_ARGS__)
919 #define GST_TRACE_OBJECT(obj,...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE, obj, __VA_ARGS__)
921 #define GST_ERROR(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR, NULL, __VA_ARGS__)
922 #define GST_WARNING(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, NULL, __VA_ARGS__)
923 #define GST_INFO(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO, NULL, __VA_ARGS__)
924 #define GST_DEBUG(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, NULL, __VA_ARGS__)
925 #define GST_LOG(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG, NULL, __VA_ARGS__)
926 #define GST_FIXME(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME, NULL, __VA_ARGS__)
927 #define GST_TRACE(...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE, NULL, __VA_ARGS__)
929 #else
930 #ifdef G_HAVE_GNUC_VARARGS
932 #define GST_CAT_ERROR_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR, obj, ##args )
933 #define GST_CAT_WARNING_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, obj, ##args )
934 #define GST_CAT_INFO_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO, obj, ##args )
935 #define GST_CAT_DEBUG_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG, obj, ##args )
936 #define GST_CAT_LOG_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG, obj, ##args )
937 #define GST_CAT_FIXME_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME, obj, ##args )
938 #define GST_CAT_TRACE_OBJECT(cat,obj,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE, obj, ##args )
940 #define GST_CAT_ERROR(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR, NULL, ##args )
941 #define GST_CAT_WARNING(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, NULL, ##args )
942 #define GST_CAT_INFO(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO, NULL, ##args )
943 #define GST_CAT_DEBUG(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG, NULL, ##args )
944 #define GST_CAT_LOG(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG, NULL, ##args )
945 #define GST_CAT_FIXME(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME, NULL, ##args )
946 #define GST_CAT_TRACE(cat,args...) GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE, NULL, ##args )
948 #define GST_ERROR_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR, obj, ##args )
949 #define GST_WARNING_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, obj, ##args )
950 #define GST_INFO_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO, obj, ##args )
951 #define GST_DEBUG_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, obj, ##args )
952 #define GST_LOG_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG, obj, ##args )
953 #define GST_FIXME_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME, obj, ##args )
954 #define GST_TRACE_OBJECT(obj,args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE, obj, ##args )
956 #define GST_ERROR(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR, NULL, ##args )
957 #define GST_WARNING(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, NULL, ##args )
958 #define GST_INFO(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO, NULL, ##args )
959 #define GST_DEBUG(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, NULL, ##args )
960 #define GST_LOG(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG, NULL, ##args )
961 #define GST_FIXME(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME, NULL, ##args )
962 #define GST_TRACE(args...) GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE, NULL, ##args )
964 #else
965 /* no variadic macros, use inline */
966 static inline void
967 GST_CAT_ERROR_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
968 ...)
969 {
970 va_list varargs;
972 va_start (varargs, format);
973 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_ERROR, obj, format, varargs);
974 va_end (varargs);
975 }
977 static inline void
978 GST_CAT_WARNING_OBJECT (GstDebugCategory * cat, gpointer obj,
979 const char *format, ...)
980 {
981 va_list varargs;
983 va_start (varargs, format);
984 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_WARNING, obj, format, varargs);
985 va_end (varargs);
986 }
988 static inline void
989 GST_CAT_INFO_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
990 ...)
991 {
992 va_list varargs;
994 va_start (varargs, format);
995 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_INFO, obj, format, varargs);
996 va_end (varargs);
997 }
999 static inline void
1000 GST_CAT_DEBUG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1001 ...)
1002 {
1003 va_list varargs;
1005 va_start (varargs, format);
1006 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_DEBUG, obj, format, varargs);
1007 va_end (varargs);
1008 }
1010 static inline void
1011 GST_CAT_LOG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1012 ...)
1013 {
1014 va_list varargs;
1016 va_start (varargs, format);
1017 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_LOG, obj, format, varargs);
1018 va_end (varargs);
1019 }
1021 static inline void
1022 GST_CAT_FIXME_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1023 ...)
1024 {
1025 va_list varargs;
1027 va_start (varargs, format);
1028 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_FIXME, obj, format, varargs);
1029 va_end (varargs);
1030 }
1032 static inline void
1033 GST_CAT_TRACE_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1034 ...)
1035 {
1036 va_list varargs;
1038 va_start (varargs, format);
1039 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_TRACE, obj, format, varargs);
1040 va_end (varargs);
1041 }
1043 static inline void
1044 GST_CAT_ERROR (GstDebugCategory * cat, const char *format, ...)
1045 {
1046 va_list varargs;
1048 va_start (varargs, format);
1049 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_ERROR, NULL, format, varargs);
1050 va_end (varargs);
1051 }
1053 static inline void
1054 GST_CAT_WARNING (GstDebugCategory * cat, const char *format, ...)
1055 {
1056 va_list varargs;
1058 va_start (varargs, format);
1059 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_WARNING, NULL, format, varargs);
1060 va_end (varargs);
1061 }
1063 static inline void
1064 GST_CAT_INFO (GstDebugCategory * cat, const char *format, ...)
1065 {
1066 va_list varargs;
1068 va_start (varargs, format);
1069 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_INFO, NULL, format, varargs);
1070 va_end (varargs);
1071 }
1073 static inline void
1074 GST_CAT_DEBUG (GstDebugCategory * cat, const char *format, ...)
1075 {
1076 va_list varargs;
1078 va_start (varargs, format);
1079 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_DEBUG, NULL, format, varargs);
1080 va_end (varargs);
1081 }
1083 static inline void
1084 GST_CAT_LOG (GstDebugCategory * cat, const char *format, ...)
1085 {
1086 va_list varargs;
1088 va_start (varargs, format);
1089 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_LOG, NULL, format, varargs);
1090 va_end (varargs);
1091 }
1093 static inline void
1094 GST_CAT_FIXME (GstDebugCategory * cat, const char *format, ...)
1095 {
1096 va_list varargs;
1098 va_start (varargs, format);
1099 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_FIXME, NULL, format, varargs);
1100 va_end (varargs);
1101 }
1103 static inline void
1104 GST_CAT_TRACE (GstDebugCategory * cat, const char *format, ...)
1105 {
1106 va_list varargs;
1108 va_start (varargs, format);
1109 GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_TRACE, NULL, format, varargs);
1110 va_end (varargs);
1111 }
1113 static inline void
1114 GST_ERROR_OBJECT (gpointer obj, const char *format, ...)
1115 {
1116 va_list varargs;
1118 va_start (varargs, format);
1119 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_ERROR, obj, format,
1120 varargs);
1121 va_end (varargs);
1122 }
1124 static inline void
1125 GST_WARNING_OBJECT (gpointer obj, const char *format, ...)
1126 {
1127 va_list varargs;
1129 va_start (varargs, format);
1130 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_WARNING, obj, format,
1131 varargs);
1132 va_end (varargs);
1133 }
1135 static inline void
1136 GST_INFO_OBJECT (gpointer obj, const char *format, ...)
1137 {
1138 va_list varargs;
1140 va_start (varargs, format);
1141 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_INFO, obj, format,
1142 varargs);
1143 va_end (varargs);
1144 }
1146 static inline void
1147 GST_DEBUG_OBJECT (gpointer obj, const char *format, ...)
1148 {
1149 va_list varargs;
1151 va_start (varargs, format);
1152 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, obj, format,
1153 varargs);
1154 va_end (varargs);
1155 }
1157 static inline void
1158 GST_LOG_OBJECT (gpointer obj, const char *format, ...)
1159 {
1160 va_list varargs;
1162 va_start (varargs, format);
1163 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_LOG, obj, format,
1164 varargs);
1165 va_end (varargs);
1166 }
1168 static inline void
1169 GST_FIXME_OBJECT (gpointer obj, const char *format, ...)
1170 {
1171 va_list varargs;
1173 va_start (varargs, format);
1174 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_FIXME, obj, format,
1175 varargs);
1176 va_end (varargs);
1177 }
1179 static inline void
1180 GST_TRACE_OBJECT (gpointer obj, const char *format, ...)
1181 {
1182 va_list varargs;
1184 va_start (varargs, format);
1185 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_TRACE, obj, format,
1186 varargs);
1187 va_end (varargs);
1188 }
1190 static inline void
1191 GST_ERROR (const char *format, ...)
1192 {
1193 va_list varargs;
1195 va_start (varargs, format);
1196 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_ERROR, NULL, format,
1197 varargs);
1198 va_end (varargs);
1199 }
1201 static inline void
1202 GST_WARNING (const char *format, ...)
1203 {
1204 va_list varargs;
1206 va_start (varargs, format);
1207 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_WARNING, NULL, format,
1208 varargs);
1209 va_end (varargs);
1210 }
1212 static inline void
1213 GST_INFO (const char *format, ...)
1214 {
1215 va_list varargs;
1217 va_start (varargs, format);
1218 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_INFO, NULL, format,
1219 varargs);
1220 va_end (varargs);
1221 }
1223 static inline void
1224 GST_DEBUG (const char *format, ...)
1225 {
1226 va_list varargs;
1228 va_start (varargs, format);
1229 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, NULL, format,
1230 varargs);
1231 va_end (varargs);
1232 }
1234 static inline void
1235 GST_LOG (const char *format, ...)
1236 {
1237 va_list varargs;
1239 va_start (varargs, format);
1240 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_LOG, NULL,
1241 format, varargs);
1242 va_end (varargs);
1243 }
1245 static inline void
1246 GST_FIXME (const char *format, ...)
1247 {
1248 va_list varargs;
1250 va_start (varargs, format);
1251 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_FIXME, NULL, format,
1252 varargs);
1253 va_end (varargs);
1254 }
1256 static inline void
1257 GST_TRACE (const char *format, ...)
1258 {
1259 va_list varargs;
1261 va_start (varargs, format);
1262 GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_TRACE, NULL, format,
1263 varargs);
1264 va_end (varargs);
1265 }
1266 #endif
1267 #endif
1270 /********** function pointer stuff **********/
1272 /**
1273 * GST_DEBUG_REGISTER_FUNCPTR:
1274 * @ptr: pointer to the function to register
1275 *
1276 * Register a pointer to a function with its name, so it can later be used by
1277 * GST_DEBUG_FUNCPTR_NAME().
1278 *
1279 * Use this variant of #GST_DEBUG_FUNCPTR if you do not need to use @ptr.
1280 *
1281 * Since: 0.10.26
1282 */
1283 #define GST_DEBUG_REGISTER_FUNCPTR(ptr) \
1284 _gst_debug_register_funcptr((GstDebugFuncPtr)(ptr), #ptr)
1285 /**
1286 * GST_DEBUG_FUNCPTR:
1287 * @ptr: pointer to the function to register
1288 *
1289 * Register a pointer to a function with its name, so it can later be used by
1290 * GST_DEBUG_FUNCPTR_NAME().
1291 *
1292 * Returns: the value passed to @ptr.
1293 */
1294 #define GST_DEBUG_FUNCPTR(ptr) \
1295 (_gst_debug_register_funcptr((GstDebugFuncPtr)(ptr), #ptr) , ptr)
1297 /**
1298 * GST_DEBUG_FUNCPTR_NAME:
1299 * @ptr: address of the function of which to look up the name
1300 *
1301 * Retrieves the name of the function, if it was previously registered with
1302 * GST_DEBUG_FUNCPTR(). If not, it returns a description of the pointer.
1303 *
1304 * This macro returns a constant string which must not be modified or
1305 * freed by the caller.
1306 */
1307 #define GST_DEBUG_FUNCPTR_NAME(ptr) \
1308 _gst_debug_nameof_funcptr((GstDebugFuncPtr)ptr)
1311 #else /* GST_DISABLE_GST_DEBUG */
1314 #ifndef GST_INFO_C
1316 #if defined(__GNUC__) && __GNUC__ >= 3
1317 # pragma GCC poison gst_debug_log
1318 # pragma GCC poison gst_debug_log2
1319 # pragma GCC poison gst_debug_log_valist
1320 # pragma GCC poison _gst_debug_category_new
1321 #endif
1323 #define __gst_debug_min GST_LEVEL_NONE
1325 #define _gst_debug_init() G_STMT_START{ }G_STMT_END
1327 #define gst_debug_set_default_threshold(level) G_STMT_START{ }G_STMT_END
1328 #define gst_debug_get_default_threshold() (GST_LEVEL_NONE)
1330 #define gst_debug_level_get_name(level) ("NONE")
1331 #define gst_debug_message_get(message) ("")
1332 #define gst_debug_add_log_function(func,data) G_STMT_START{ }G_STMT_END
1333 #define gst_debug_set_active(active) G_STMT_START{ }G_STMT_END
1334 #define gst_debug_is_active() (FALSE)
1335 #define gst_debug_set_colored(colored) G_STMT_START{ }G_STMT_END
1336 #define gst_debug_is_colored() (FALSE)
1337 #define gst_debug_set_default_threshold(level) G_STMT_START{ }G_STMT_END
1338 #define gst_debug_get_default_threshold() (GST_LEVEL_NONE)
1339 #define gst_debug_set_threshold_for_name(name,level) G_STMT_START{ }G_STMT_END
1340 #define gst_debug_unset_threshold_for_name(name) G_STMT_START{ }G_STMT_END
1342 /* we are using dummy function prototypes here to eat ';' as these macros are
1343 * used outside of functions */
1344 #define GST_DEBUG_CATEGORY(var) void _gst_debug_dummy_##var (void)
1345 #define GST_DEBUG_CATEGORY_EXTERN(var) void _gst_debug_dummy_extern_##var (void)
1346 #define GST_DEBUG_CATEGORY_STATIC(var) void _gst_debug_dummy_static_##var (void)
1348 #define GST_DEBUG_CATEGORY_INIT(var,name,color,desc) G_STMT_START{ }G_STMT_END
1349 #define GST_DEBUG_CATEGORY_GET(var,name) G_STMT_START{ }G_STMT_END
1350 #define gst_debug_category_free(category) G_STMT_START{ }G_STMT_END
1351 #define gst_debug_category_set_threshold(category,level) G_STMT_START{ }G_STMT_END
1352 #define gst_debug_category_reset_threshold(category) G_STMT_START{ }G_STMT_END
1353 #define gst_debug_category_get_threshold(category) (GST_LEVEL_NONE)
1354 #define gst_debug_category_get_name(cat) ("")
1355 #define gst_debug_category_get_color(cat) (0)
1356 #define gst_debug_category_get_description(cat) ("")
1357 #define gst_debug_get_all_categories() (NULL)
1358 #define gst_debug_construct_term_color(colorinfo) (g_strdup ("00"))
1359 #define gst_debug_construct_win_color(colorinfo) (0)
1361 #endif /* !GST_INFO_C */
1363 #ifdef G_HAVE_ISO_VARARGS
1365 #define GST_CAT_LEVEL_LOG(cat,level,...) G_STMT_START{ }G_STMT_END
1367 #define GST_CAT_ERROR_OBJECT(...) G_STMT_START{ }G_STMT_END
1368 #define GST_CAT_WARNING_OBJECT(...) G_STMT_START{ }G_STMT_END
1369 #define GST_CAT_INFO_OBJECT(...) G_STMT_START{ }G_STMT_END
1370 #define GST_CAT_DEBUG_OBJECT(...) G_STMT_START{ }G_STMT_END
1371 #define GST_CAT_LOG_OBJECT(...) G_STMT_START{ }G_STMT_END
1372 #define GST_CAT_FIXME_OBJECT(...) G_STMT_START{ }G_STMT_END
1373 #define GST_CAT_TRACE_OBJECT(...) G_STMT_START{ }G_STMT_END
1375 #define GST_CAT_ERROR(...) G_STMT_START{ }G_STMT_END
1376 #define GST_CAT_WARNING(...) G_STMT_START{ }G_STMT_END
1377 #define GST_CAT_INFO(...) G_STMT_START{ }G_STMT_END
1378 #define GST_CAT_DEBUG(...) G_STMT_START{ }G_STMT_END
1379 #define GST_CAT_LOG(...) G_STMT_START{ }G_STMT_END
1380 #define GST_CAT_FIXME(...) G_STMT_START{ }G_STMT_END
1381 #define GST_CAT_TRACE(...) G_STMT_START{ }G_STMT_END
1383 #define GST_ERROR_OBJECT(...) G_STMT_START{ }G_STMT_END
1384 #define GST_WARNING_OBJECT(...) G_STMT_START{ }G_STMT_END
1385 #define GST_INFO_OBJECT(...) G_STMT_START{ }G_STMT_END
1386 #define GST_DEBUG_OBJECT(...) G_STMT_START{ }G_STMT_END
1387 #define GST_LOG_OBJECT(...) G_STMT_START{ }G_STMT_END
1388 #define GST_FIXME_OBJECT(...) G_STMT_START{ }G_STMT_END
1389 #define GST_TRACE_OBJECT(...) G_STMT_START{ }G_STMT_END
1391 #define GST_ERROR(...) G_STMT_START{ }G_STMT_END
1392 #define GST_WARNING(...) G_STMT_START{ }G_STMT_END
1393 #define GST_INFO(...) G_STMT_START{ }G_STMT_END
1394 #define GST_DEBUG(...) G_STMT_START{ }G_STMT_END
1395 #define GST_LOG(...) G_STMT_START{ }G_STMT_END
1396 #define GST_FIXME(...) G_STMT_START{ }G_STMT_END
1397 #define GST_TRACE(...) G_STMT_START{ }G_STMT_END
1399 #else /* !G_HAVE_ISO_VARARGS */
1400 #ifdef G_HAVE_GNUC_VARARGS
1402 #define GST_CAT_LEVEL_LOG(cat,level,args...) G_STMT_START{ }G_STMT_END
1404 #define GST_CAT_ERROR_OBJECT(args...) G_STMT_START{ }G_STMT_END
1405 #define GST_CAT_WARNING_OBJECT(args...) G_STMT_START{ }G_STMT_END
1406 #define GST_CAT_INFO_OBJECT(args...) G_STMT_START{ }G_STMT_END
1407 #define GST_CAT_DEBUG_OBJECT(args...) G_STMT_START{ }G_STMT_END
1408 #define GST_CAT_LOG_OBJECT(args...) G_STMT_START{ }G_STMT_END
1409 #define GST_CAT_FIXME_OBJECT(args...) G_STMT_START{ }G_STMT_END
1410 #define GST_CAT_TRACE_OBJECT(args...) G_STMT_START{ }G_STMT_END
1412 #define GST_CAT_ERROR(args...) G_STMT_START{ }G_STMT_END
1413 #define GST_CAT_WARNING(args...) G_STMT_START{ }G_STMT_END
1414 #define GST_CAT_INFO(args...) G_STMT_START{ }G_STMT_END
1415 #define GST_CAT_DEBUG(args...) G_STMT_START{ }G_STMT_END
1416 #define GST_CAT_LOG(args...) G_STMT_START{ }G_STMT_END
1417 #define GST_CAT_FIXME(args...) G_STMT_START{ }G_STMT_END
1418 #define GST_CAT_TRACE(args...) G_STMT_START{ }G_STMT_END
1420 #define GST_ERROR_OBJECT(args...) G_STMT_START{ }G_STMT_END
1421 #define GST_WARNING_OBJECT(args...) G_STMT_START{ }G_STMT_END
1422 #define GST_INFO_OBJECT(args...) G_STMT_START{ }G_STMT_END
1423 #define GST_DEBUG_OBJECT(args...) G_STMT_START{ }G_STMT_END
1424 #define GST_LOG_OBJECT(args...) G_STMT_START{ }G_STMT_END
1425 #define GST_FIXME_OBJECT(args...) G_STMT_START{ }G_STMT_END
1426 #define GST_TRACE_OBJECT(args...) G_STMT_START{ }G_STMT_END
1428 #define GST_ERROR(args...) G_STMT_START{ }G_STMT_END
1429 #define GST_WARNING(args...) G_STMT_START{ }G_STMT_END
1430 #define GST_INFO(args...) G_STMT_START{ }G_STMT_END
1431 #define GST_DEBUG(args...) G_STMT_START{ }G_STMT_END
1432 #define GST_LOG(args...) G_STMT_START{ }G_STMT_END
1433 #define GST_FIXME(args...) G_STMT_START{ }G_STMT_END
1434 #define GST_TRACE(args...) G_STMT_START{ }G_STMT_END
1436 #else /* !G_HAVE_GNUC_VARARGS */
1437 static inline void
1438 GST_CAT_LEVEL_LOG_valist (GstDebugCategory * cat,
1439 GstDebugLevel level, gpointer object, const char *format, va_list varargs)
1440 {
1441 }
1443 static inline void
1444 GST_CAT_ERROR_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1445 ...)
1446 {
1447 }
1449 static inline void
1450 GST_CAT_WARNING_OBJECT (GstDebugCategory * cat, gpointer obj,
1451 const char *format, ...)
1452 {
1453 }
1455 static inline void
1456 GST_CAT_INFO_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1457 ...)
1458 {
1459 }
1461 static inline void
1462 GST_CAT_DEBUG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1463 ...)
1464 {
1465 }
1467 static inline void
1468 GST_CAT_LOG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1469 ...)
1470 {
1471 }
1473 static inline void
1474 GST_CAT_FIXME_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1475 ...)
1476 {
1477 }
1479 static inline void
1480 GST_CAT_TRACE_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
1481 ...)
1482 {
1483 }
1485 static inline void
1486 GST_CAT_ERROR (GstDebugCategory * cat, const char *format, ...)
1487 {
1488 }
1490 static inline void
1491 GST_CAT_WARNING (GstDebugCategory * cat, const char *format, ...)
1492 {
1493 }
1495 static inline void
1496 GST_CAT_INFO (GstDebugCategory * cat, const char *format, ...)
1497 {
1498 }
1500 static inline void
1501 GST_CAT_DEBUG (GstDebugCategory * cat, const char *format, ...)
1502 {
1503 }
1505 static inline void
1506 GST_CAT_LOG (GstDebugCategory * cat, const char *format, ...)
1507 {
1508 }
1510 static inline void
1511 GST_CAT_FIXME (GstDebugCategory * cat, const char *format, ...)
1512 {
1513 }
1515 static inline void
1516 GST_CAT_TRACE (GstDebugCategory * cat, const char *format, ...)
1517 {
1518 }
1520 static inline void
1521 GST_ERROR_OBJECT (gpointer obj, const char *format, ...)
1522 {
1523 }
1525 static inline void
1526 GST_WARNING_OBJECT (gpointer obj, const char *format, ...)
1527 {
1528 }
1530 static inline void
1531 GST_INFO_OBJECT (gpointer obj, const char *format, ...)
1532 {
1533 }
1535 static inline void
1536 GST_DEBUG_OBJECT (gpointer obj, const char *format, ...)
1537 {
1538 }
1540 static inline void
1541 GST_LOG_OBJECT (gpointer obj, const char *format, ...)
1542 {
1543 }
1545 static inline void
1546 GST_FIXME_OBJECT (gpointer obj, const char *format, ...)
1547 {
1548 }
1550 static inline void
1551 GST_TRACE_OBJECT (gpointer obj, const char *format, ...)
1552 {
1553 }
1555 static inline void
1556 GST_ERROR (const char *format, ...)
1557 {
1558 }
1560 static inline void
1561 GST_WARNING (const char *format, ...)
1562 {
1563 }
1565 static inline void
1566 GST_INFO (const char *format, ...)
1567 {
1568 }
1570 static inline void
1571 GST_DEBUG (const char *format, ...)
1572 {
1573 }
1575 static inline void
1576 GST_LOG (const char *format, ...)
1577 {
1578 }
1580 static inline void
1581 GST_FIXME (const char *format, ...)
1582 {
1583 }
1585 static inline void
1586 GST_TRACE (const char *format, ...)
1587 {
1588 }
1590 #endif /* G_HAVE_GNUC_VARARGS */
1591 #endif /* G_HAVE_ISO_VARARGS */
1593 #define GST_DEBUG_REGISTER_FUNCPTR(ptr) G_STMT_START{ }G_STMT_END
1594 #define GST_DEBUG_FUNCPTR(ptr) (ptr)
1595 #define GST_DEBUG_FUNCPTR_NAME(ptr) (g_strdup_printf ("%p", ptr))
1597 #define GST_CAT_MEMDUMP_OBJECT(cat,obj,msg,data,length) G_STMT_START{ }G_STMT_END
1598 #define GST_CAT_MEMDUMP(cat,msg,data,length) G_STMT_START{ }G_STMT_END
1599 #define GST_MEMDUMP_OBJECT(obj,msg,data,length) G_STMT_START{ }G_STMT_END
1600 #define GST_MEMDUMP(msg,data,length) G_STMT_START{ }G_STMT_END
1602 #endif /* GST_DISABLE_GST_DEBUG */
1605 void gst_debug_print_stack_trace (void);
1607 G_END_DECLS
1609 #endif /* __GSTINFO_H__ */