gst/gstbin.c: Some documentation updates.
[glsdk/gstreamer0-10.git] / gst / gstobject.c
1 /* GStreamer
2  * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3  *                    2000 Wim Taymans <wtay@chello.be>
4  *                    2005 Wim Taymans <wim@fluendo.com>
5  *
6  * gstobject.c: Fundamental class used for all of GStreamer
7  *
8  * This library is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU Library General Public
10  * License as published by the Free Software Foundation; either
11  * version 2 of the License, or (at your option) any later version.
12  *
13  * This library is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
16  * Library General Public License for more details.
17  *
18  * You should have received a copy of the GNU Library General Public
19  * License along with this library; if not, write to the
20  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
21  * Boston, MA 02111-1307, USA.
22  */
23 /**
24  * SECTION:gstobject
25  * @short_description: Base class for the GStreamer object hierarchy
26  *
27  * GstObject provides a root for the object hierarchy tree filed in by the
28  * GST library.  It is currently a thin wrapper on top of
29  * #GObject. It is an abstract class that is not very usable on its own.
30  *
31  * GstObject gives us basic refcounting, parenting functionality and locking.
32  * Most of the function are just extended for special gstreamer needs and can be
33  * found under the same name in the base class of GstObject which is GObject
34  * (e.g. g_object_ref() becomes gst_object_ref()).
35  *
36  * The most interesting difference between GstObject and GObject is the "floating"
37  * reference count. A GObject is created with a reference count of 1, owned by the
38  * creator of the GObject. (The owner of a reference is the code section that has
39  * the right to call gst_object_unref() in order to remove that reference.)
40  * A GstObject is created with a reference count of 1 also, but it isn't owned by
41  * anyone; calling gst_object_unref() on the newly-created GtkObject is incorrect.
42  * Instead, the initial reference count of a GstObject is "floating". The floating
43  * reference can be removed by anyone at any time, by calling gst_object_sink().
44  * gst_object_sink() does nothing if an object is already sunk (has no floating
45  * reference).
46  * 
47  * When you add a GstElement to its parent container, the parent container will do
48  * this:
49  * <informalexample>
50  * <programlisting>
51  *   gst_object_ref (GST_OBJECT (child_element));
52  *   gst_object_sink (GST_OBJECT (child_element));
53  * </programlisting>
54  * </informalexample>
55  * This means that the container now owns a reference to the child element (since
56  * it called gst_object_ref()), and the child element has no floating reference.
57  *
58  * The purpose of the floating reference is to keep the child element alive until
59  * you add it to a parent container:
60  * <informalexample>
61  * <programlisting>
62  *    element = gst_element_factory_make (factoryname, name);
63  *    // element has one floating reference to keep it alive
64  *    gst_bin_add (GST_BIN (bin), element);
65  *    // element has one non-floating reference owned by the container
66  * </programlisting>
67  * </informalexample>
68  *
69  * Another effect of this is, that calling gst_object_unref() on a bin object, will
70  * also destoy all the GstElement objects in it. The same is true for calling
71  * gst_bin_remove().
72  * 
73  * In contrast to GObject instances GstObject add a name property. The functions
74  * gst_object_set_name() and gst_object_get_name() are used to set/get the name
75  * of the object.
76  */
78 #include "gst_private.h"
80 #include "gstobject.h"
81 #include "gstmarshal.h"
82 #include "gstinfo.h"
83 #include "gstutils.h"
85 #ifndef GST_DISABLE_TRACE
86 #include "gsttrace.h"
87 #endif
89 #define DEBUG_REFCOUNT
90 #ifndef GST_HAVE_GLIB_2_8
91 #define REFCOUNT_HACK
92 #endif
94 /* Refcount hack: since glib is not threadsafe, the glib refcounter can be
95  * screwed up and the object can be freed unexpectedly. We use an evil hack
96  * to work around this problem. We set the glib refcount to a high value so
97  * that glib will never unref the object under realistic circumstances. Then
98  * we use our own atomic refcounting to do proper MT safe refcounting.
99  *
100  * The hack has several side-effect. At first you should use
101  * gst_object_ref/unref() whenever you can. Next when using g_value_set/get_object();
102  * you need to manually fix the refcount.
103  *
104  * A proper fix is of course to make the glib refcounting threadsafe which is
105  * planned. Update: atomic refcounting is now in glib >= 2.7.3
106  */
107 #ifdef REFCOUNT_HACK
108 #define PATCH_REFCOUNT(obj)    ((GObject*)(obj))->ref_count = 100000;
109 #define PATCH_REFCOUNT1(obj)    ((GObject*)(obj))->ref_count = 1;
110 #else
111 #define PATCH_REFCOUNT(obj)
112 #define PATCH_REFCOUNT1(obj)
113 #endif
115 /* Object signals and args */
116 enum
118   PARENT_SET,
119   PARENT_UNSET,
120 #ifndef GST_DISABLE_LOADSAVE_REGISTRY
121   OBJECT_SAVED,
122 #endif
123   DEEP_NOTIFY,
124   LAST_SIGNAL
125 };
127 enum
129   ARG_0,
130   ARG_NAME
131       /* FILL ME */
132 };
134 enum
136   SO_OBJECT_LOADED,
137   SO_LAST_SIGNAL
138 };
140 GType _gst_object_type = 0;
141 static GHashTable *object_name_counts = NULL;
143 G_LOCK_DEFINE_STATIC (object_name_mutex);
145 typedef struct _GstSignalObject GstSignalObject;
146 typedef struct _GstSignalObjectClass GstSignalObjectClass;
148 static GType gst_signal_object_get_type (void);
149 static void gst_signal_object_class_init (GstSignalObjectClass * klass);
150 static void gst_signal_object_init (GstSignalObject * object);
152 #ifndef GST_DISABLE_LOADSAVE_REGISTRY
153 static guint gst_signal_object_signals[SO_LAST_SIGNAL] = { 0 };
154 #endif
156 static void gst_object_class_init (GstObjectClass * klass);
157 static void gst_object_init (GTypeInstance * instance, gpointer g_class);
159 #ifndef GST_DISABLE_TRACE
160 static GObject *gst_object_constructor (GType type,
161     guint n_construct_properties, GObjectConstructParam * construct_params);
162 #endif
164 static void gst_object_set_property (GObject * object, guint prop_id,
165     const GValue * value, GParamSpec * pspec);
166 static void gst_object_get_property (GObject * object, guint prop_id,
167     GValue * value, GParamSpec * pspec);
168 static void gst_object_dispatch_properties_changed (GObject * object,
169     guint n_pspecs, GParamSpec ** pspecs);
171 static void gst_object_dispose (GObject * object);
172 static void gst_object_finalize (GObject * object);
174 static gboolean gst_object_set_name_default (GstObject * object,
175     const gchar * type_name);
177 #ifndef GST_DISABLE_LOADSAVE_REGISTRY
178 static void gst_object_real_restore_thyself (GstObject * object,
179     xmlNodePtr self);
180 #endif
182 static GObjectClass *parent_class = NULL;
183 static guint gst_object_signals[LAST_SIGNAL] = { 0 };
185 GType
186 gst_object_get_type (void)
188   if (!_gst_object_type) {
189     static const GTypeInfo object_info = {
190       sizeof (GstObjectClass),
191       NULL,
192       NULL,
193       (GClassInitFunc) gst_object_class_init,
194       NULL,
195       NULL,
196       sizeof (GstObject),
197       0,
198       gst_object_init,
199       NULL
200     };
202     _gst_object_type =
203         g_type_register_static (G_TYPE_OBJECT, "GstObject", &object_info,
204         G_TYPE_FLAG_ABSTRACT);
205   }
206   return _gst_object_type;
209 static void
210 gst_object_class_init (GstObjectClass * klass)
212   GObjectClass *gobject_class;
214   gobject_class = (GObjectClass *) klass;
216   parent_class = g_type_class_ref (G_TYPE_OBJECT);
218   gobject_class->set_property = GST_DEBUG_FUNCPTR (gst_object_set_property);
219   gobject_class->get_property = GST_DEBUG_FUNCPTR (gst_object_get_property);
221   g_object_class_install_property (G_OBJECT_CLASS (klass), ARG_NAME,
222       g_param_spec_string ("name", "Name", "The name of the object",
223           NULL, G_PARAM_READWRITE | G_PARAM_CONSTRUCT));
225   /**
226    * GstObject::parent-set:
227    * @gstobject: the object which received the signal.
228    * @parent: the new parent
229    *
230    * Is emitted when the parent of an object is set.
231    */
232   gst_object_signals[PARENT_SET] =
233       g_signal_new ("parent-set", G_TYPE_FROM_CLASS (klass), G_SIGNAL_RUN_LAST,
234       G_STRUCT_OFFSET (GstObjectClass, parent_set), NULL, NULL,
235       g_cclosure_marshal_VOID__OBJECT, G_TYPE_NONE, 1, G_TYPE_OBJECT);
237   /**
238    * GstObject::parent-unset:
239    * @gstobject: the object which received the signal.
240    * @parent: the old parent
241    *
242    * Is emitted when the parent of an object is unset.
243    */
244   gst_object_signals[PARENT_UNSET] =
245       g_signal_new ("parent-unset", G_TYPE_FROM_CLASS (klass),
246       G_SIGNAL_RUN_LAST, G_STRUCT_OFFSET (GstObjectClass, parent_unset), NULL,
247       NULL, g_cclosure_marshal_VOID__OBJECT, G_TYPE_NONE, 1, G_TYPE_OBJECT);
249 #ifndef GST_DISABLE_LOADSAVE_REGISTRY
250   /**
251    * GstObject::object-saved:
252    * @gstobject: the object which received the signal.
253    * @xml_node: the xmlNodePtr of the parent node
254    *
255    * Is trigered whenever a new object is saved to XML. You can connect to this
256    * signal to insert custom XML tags into the core XML.
257    */
258   /* FIXME This should be the GType of xmlNodePtr instead of G_TYPE_POINTER
259    *       (if libxml would use GObject)
260    */
261   gst_object_signals[OBJECT_SAVED] =
262       g_signal_new ("object-saved", G_TYPE_FROM_CLASS (klass),
263       G_SIGNAL_RUN_LAST, G_STRUCT_OFFSET (GstObjectClass, object_saved), NULL,
264       NULL, g_cclosure_marshal_VOID__POINTER, G_TYPE_NONE, 1, G_TYPE_POINTER);
266   klass->restore_thyself = gst_object_real_restore_thyself;
267 #endif
269   /**
270    * GstObject::deep-notify:
271    * @gstobject: the object which received the signal.
272    * @prop_object: the object that originated the signal
273    * @prop: the property that changed
274    *
275    * The deep notify signal is used to be notified of property changes. It is
276    * typically attached to the toplevel bin to receive notifications from all
277    * the elements contained in that bin.
278    */
279   gst_object_signals[DEEP_NOTIFY] =
280       g_signal_new ("deep-notify", G_TYPE_FROM_CLASS (klass),
281       G_SIGNAL_RUN_FIRST | G_SIGNAL_NO_RECURSE | G_SIGNAL_DETAILED |
282       G_SIGNAL_NO_HOOKS, G_STRUCT_OFFSET (GstObjectClass, deep_notify), NULL,
283       NULL, gst_marshal_VOID__OBJECT_PARAM, G_TYPE_NONE, 2, G_TYPE_OBJECT,
284       G_TYPE_PARAM);
286   klass->path_string_separator = "/";
287   klass->lock = g_new0 (GStaticRecMutex, 1);
288   g_static_rec_mutex_init (klass->lock);
290   klass->signal_object = g_object_new (gst_signal_object_get_type (), NULL);
292   /* see the comments at gst_object_dispatch_properties_changed */
293   gobject_class->dispatch_properties_changed
294       = GST_DEBUG_FUNCPTR (gst_object_dispatch_properties_changed);
296   gobject_class->dispose = gst_object_dispose;
297   gobject_class->finalize = gst_object_finalize;
298 #ifndef GST_DISABLE_TRACE
299   gobject_class->constructor = gst_object_constructor;
300 #endif
303 static void
304 gst_object_init (GTypeInstance * instance, gpointer g_class)
306   GstObject *object = GST_OBJECT (instance);
308   object->lock = g_mutex_new ();
309   object->parent = NULL;
310   object->name = NULL;
311   GST_CAT_LOG_OBJECT (GST_CAT_REFCOUNTING, object, "%p new", object);
312 #ifdef REFCOUNT_HACK
313   gst_atomic_int_set (&object->refcount, 1);
314 #endif
315   PATCH_REFCOUNT (object);
317   object->flags = 0;
318   GST_FLAG_SET (object, GST_OBJECT_FLOATING);
321 #ifndef GST_DISABLE_TRACE
322 static GObject *
323 gst_object_constructor (GType type, guint n_construct_properties,
324     GObjectConstructParam * construct_params)
326   const gchar *name;
327   GstAllocTrace *trace;
328   GObject *obj =
329       G_OBJECT_CLASS (parent_class)->constructor (type, n_construct_properties,
330       construct_params);
332   name = g_type_name (type);
334   trace = gst_alloc_trace_get (name);
335   if (!trace) {
336     trace = gst_alloc_trace_register (name);
337   }
338   gst_alloc_trace_new (trace, obj);
340   return obj;
342 #endif
343 /**
344  * gst_object_ref:
345  * @object: GstObject to reference
346  *
347  * Increments the refence count on the object. This function
348  * does not take the lock on the object because it relies on
349  * atomic refcounting.
350  *
351  * This object returns the input parameter to ease writing
352  * constructs like :
353  *  result = gst_object_ref (object->parent);
354  *
355  * Returns: A pointer to the object
356  */
357 gpointer
358 gst_object_ref (gpointer object)
360   g_return_val_if_fail (GST_IS_OBJECT (object), NULL);
362 #ifdef DEBUG_REFCOUNT
363 #ifdef REFCOUNT_HACK
364   GST_CAT_LOG_OBJECT (GST_CAT_REFCOUNTING, object, "%p ref %d->%d",
365       object,
366       GST_OBJECT_REFCOUNT_VALUE (object),
367       GST_OBJECT_REFCOUNT_VALUE (object) + 1);
368 #else
369   GST_CAT_LOG_OBJECT (GST_CAT_REFCOUNTING, object, "%p ref %d->%d",
370       object,
371       ((GObject *) object)->ref_count, ((GObject *) object)->ref_count + 1);
372 #endif
373 #endif
375 #ifdef REFCOUNT_HACK
376   g_atomic_int_inc (&((GstObject *) object)->refcount);
377   PATCH_REFCOUNT (object);
378 #else
379   g_object_ref (object);
380 #endif
382   return object;
385 /**
386  * gst_object_unref:
387  * @object: GstObject to unreference
388  *
389  * Decrements the refence count on the object.  If reference count hits
390  * zero, destroy the object. This function does not take the lock
391  * on the object as it relies on atomic refcounting.
392  *
393  * The unref method should never be called with the LOCK held since
394  * this might deadlock the dispose function.
395  */
396 void
397 gst_object_unref (gpointer object)
399   g_return_if_fail (GST_IS_OBJECT (object));
401 #ifdef REFCOUNT_HACK
402   g_return_if_fail (GST_OBJECT_REFCOUNT_VALUE (object) > 0);
403 #else
404   g_return_if_fail (((GObject *) object)->ref_count > 0);
405 #endif
407 #ifdef DEBUG_REFCOUNT
408 #ifdef REFCOUNT_HACK
409   GST_CAT_LOG_OBJECT (GST_CAT_REFCOUNTING, object, "%p unref %d->%d",
410       object,
411       GST_OBJECT_REFCOUNT_VALUE (object),
412       GST_OBJECT_REFCOUNT_VALUE (object) - 1);
413 #else
414   GST_CAT_LOG_OBJECT (GST_CAT_REFCOUNTING, object, "%p unref %d->%d",
415       object,
416       ((GObject *) object)->ref_count, ((GObject *) object)->ref_count - 1);
417 #endif
418 #endif
420 #ifdef REFCOUNT_HACK
421   if (G_UNLIKELY (g_atomic_int_dec_and_test (&((GstObject *) object)->
422               refcount))) {
423     PATCH_REFCOUNT1 (object);
424     g_object_unref (object);
425   } else {
426     PATCH_REFCOUNT (object);
427   }
428 #else
429   g_object_unref (object);
430 #endif
433 /**
434  * gst_object_sink:
435  * @object: GstObject to sink
436  *
437  * Removes floating reference on an object.  Any newly created object has
438  * a refcount of 1 and is FLOATING.  This function should be used when
439  * creating a new object to symbolically 'take ownership' of the object.
440  * Use #gst_object_set_parent to have this done for you.
441  *
442  * MT safe. This function grabs and releases the object lock.
443  */
444 void
445 gst_object_sink (gpointer object)
447   g_return_if_fail (GST_IS_OBJECT (object));
449   GST_CAT_LOG_OBJECT (GST_CAT_REFCOUNTING, object, "sink");
451   GST_LOCK (object);
452   if (G_LIKELY (GST_OBJECT_IS_FLOATING (object))) {
453     GST_FLAG_UNSET (object, GST_OBJECT_FLOATING);
454     GST_UNLOCK (object);
455     gst_object_unref (object);
456   } else {
457     GST_UNLOCK (object);
458   }
461 /**
462  * gst_object_replace:
463  * @oldobj: pointer to place of old GstObject
464  * @newobj: new GstObject
465  *
466  * Unrefs the object pointer to by oldobj, refs the newobj and
467  * puts the newobj in *oldobj. Be carefull when calling this
468  * function, it does not take any locks. You might want to lock
469  * the object owning the oldobj pointer before calling this
470  * function.
471  *
472  * Make sure not to LOCK the oldobj because it might be unreffed
473  * which could cause a deadlock when it is disposed.
474  */
475 void
476 gst_object_replace (GstObject ** oldobj, GstObject * newobj)
478   g_return_if_fail (oldobj != NULL);
479   g_return_if_fail (*oldobj == NULL || GST_IS_OBJECT (*oldobj));
480   g_return_if_fail (newobj == NULL || GST_IS_OBJECT (newobj));
482 #ifdef DEBUG_REFCOUNT
483 #ifdef REFCOUNT_HACK
484   GST_CAT_LOG (GST_CAT_REFCOUNTING, "replace %s (%d) with %s (%d)",
485       *oldobj ? GST_STR_NULL (GST_OBJECT_NAME (*oldobj)) : "(NONE)",
486       *oldobj ? GST_OBJECT_REFCOUNT_VALUE (*oldobj) : 0,
487       newobj ? GST_STR_NULL (GST_OBJECT_NAME (newobj)) : "(NONE)",
488       newobj ? GST_OBJECT_REFCOUNT_VALUE (newobj) : 0);
489 #else
490   GST_CAT_LOG (GST_CAT_REFCOUNTING, "replace %s (%d) with %s (%d)",
491       *oldobj ? GST_STR_NULL (GST_OBJECT_NAME (*oldobj)) : "(NONE)",
492       *oldobj ? G_OBJECT (*oldobj)->ref_count : 0,
493       newobj ? GST_STR_NULL (GST_OBJECT_NAME (newobj)) : "(NONE)",
494       newobj ? G_OBJECT (newobj)->ref_count : 0);
495 #endif
496 #endif
498   if (G_LIKELY (*oldobj != newobj)) {
499     if (newobj)
500       gst_object_ref (newobj);
501     if (*oldobj)
502       gst_object_unref (*oldobj);
504     *oldobj = newobj;
505   }
508 /* dispose is called when the object has to release all links
509  * to other objects */
510 static void
511 gst_object_dispose (GObject * object)
513   GST_CAT_LOG_OBJECT (GST_CAT_REFCOUNTING, object, "dispose");
515   GST_LOCK (object);
516   GST_OBJECT_PARENT (object) = NULL;
517   GST_UNLOCK (object);
519   /* need to patch refcount so it is finalized */
520   PATCH_REFCOUNT1 (object);
522   parent_class->dispose (object);
525 /* finalize is called when the object has to free its resources */
526 static void
527 gst_object_finalize (GObject * object)
529   GstObject *gstobject = GST_OBJECT (object);
531   GST_CAT_LOG_OBJECT (GST_CAT_REFCOUNTING, object, "finalize");
533   g_signal_handlers_destroy (object);
535   g_free (gstobject->name);
536   g_mutex_free (gstobject->lock);
538 #ifndef GST_DISABLE_TRACE
539   {
540     const gchar *name;
541     GstAllocTrace *trace;
543     name = g_type_name (G_OBJECT_TYPE (object));
544     trace = gst_alloc_trace_get (name);
545     g_assert (trace);
546     gst_alloc_trace_free (trace, object);
547   }
548 #endif
550   parent_class->finalize (object);
553 /* Changing a GObject property of a GstObject will result in "deep_notify"
554  * signals being emitted by the object itself, as well as in each parent
555  * object. This is so that an application can connect a listener to the
556  * top-level bin to catch property-change notifications for all contained
557  * elements. 
558  *
559  * This function is not MT safe in glib so we need to lock it with a 
560  * classwide mutex.
561  *
562  * MT safe.
563  */
564 static void
565 gst_object_dispatch_properties_changed (GObject * object,
566     guint n_pspecs, GParamSpec ** pspecs)
568   GstObject *gst_object, *parent, *old_parent;
569   guint i;
570   gchar *name, *debug_name;
571   GstObjectClass *klass;
573   /* we fail when this is not a GstObject */
574   g_return_if_fail (GST_IS_OBJECT (object));
576   klass = GST_OBJECT_GET_CLASS (object);
578   GST_CLASS_LOCK (klass);
579   /* do the standard dispatching */
580   PATCH_REFCOUNT (object);
581   G_OBJECT_CLASS (parent_class)->dispatch_properties_changed (object, n_pspecs,
582       pspecs);
583   PATCH_REFCOUNT (object);
585   gst_object = GST_OBJECT_CAST (object);
586   name = gst_object_get_name (gst_object);
587   debug_name = GST_STR_NULL (name);
589   /* now let the parent dispatch those, too */
590   parent = gst_object_get_parent (gst_object);
591   while (parent) {
592     /* for debugging ... */
593     gchar *parent_name = gst_object_get_name (parent);
595 #ifndef GST_DISABLE_GST_DEBUG
596     gchar *debug_parent_name = GST_STR_NULL (parent_name);
597 #endif
599     /* need own category? */
600     for (i = 0; i < n_pspecs; i++) {
601       GST_CAT_LOG (GST_CAT_EVENT, "deep notification from %s to %s (%s)",
602           debug_name, debug_parent_name, pspecs[i]->name);
604       /* not MT safe because of glib, fixed by taking class lock higher up */
605       PATCH_REFCOUNT (parent);
606       PATCH_REFCOUNT (object);
607       g_signal_emit (parent, gst_object_signals[DEEP_NOTIFY],
608           g_quark_from_string (pspecs[i]->name), GST_OBJECT_CAST (object),
609           pspecs[i]);
610       PATCH_REFCOUNT (parent);
611       PATCH_REFCOUNT (object);
612     }
613     g_free (parent_name);
615     old_parent = parent;
616     parent = gst_object_get_parent (old_parent);
617     gst_object_unref (old_parent);
618   }
619   g_free (name);
620   GST_CLASS_UNLOCK (klass);
623 /** 
624  * gst_object_default_deep_notify:
625  * @object: the #GObject that signalled the notify.
626  * @orig: a #GstObject that initiated the notify.
627  * @pspec: a #GParamSpec of the property.
628  * @excluded_props: a set of user-specified properties to exclude or
629  *  NULL to show all changes.
630  *
631  * A default deep_notify signal callback for an element. The user data 
632  * should contain a pointer to an array of strings that should be excluded 
633  * from the notify. The default handler will print the new value of the property 
634  * using g_print.
635  *
636  * MT safe. This function grabs and releases the object's LOCK or getting the
637  *          path string of the object.
638  */
639 void
640 gst_object_default_deep_notify (GObject * object, GstObject * orig,
641     GParamSpec * pspec, gchar ** excluded_props)
643   GValue value = { 0, };        /* the important thing is that value.type = 0 */
644   gchar *str = NULL;
645   gchar *name = NULL;
647   if (pspec->flags & G_PARAM_READABLE) {
648     /* let's not print these out for excluded properties... */
649     while (excluded_props != NULL && *excluded_props != NULL) {
650       if (strcmp (pspec->name, *excluded_props) == 0)
651         return;
652       excluded_props++;
653     }
654     g_value_init (&value, G_PARAM_SPEC_VALUE_TYPE (pspec));
655     g_object_get_property (G_OBJECT (orig), pspec->name, &value);
657     if (G_IS_PARAM_SPEC_ENUM (pspec)) {
658       GEnumValue *enum_value;
660       enum_value =
661           g_enum_get_value (G_ENUM_CLASS (g_type_class_ref (pspec->value_type)),
662           g_value_get_enum (&value));
664       str = g_strdup_printf ("%s (%d)", enum_value->value_nick,
665           enum_value->value);
666     } else {
667       str = g_strdup_value_contents (&value);
668     }
669     name = gst_object_get_path_string (orig);
670     g_print ("%s: %s = %s\n", name, pspec->name, str);
671     g_free (name);
672     g_free (str);
673     g_value_unset (&value);
674   } else {
675     name = gst_object_get_path_string (orig);
676     g_warning ("Parameter %s not readable in %s.", pspec->name, name);
677     g_free (name);
678   }
681 static gboolean
682 gst_object_set_name_default (GstObject * object, const gchar * type_name)
684   gint count;
685   gchar *name, *tmp;
686   gboolean result;
688   /* to ensure guaranteed uniqueness across threads, only one thread
689    * may ever assign a name */
690   G_LOCK (object_name_mutex);
692   if (!object_name_counts) {
693     object_name_counts = g_hash_table_new_full (g_str_hash, g_str_equal,
694         g_free, NULL);
695   }
697   count = GPOINTER_TO_INT (g_hash_table_lookup (object_name_counts, type_name));
698   g_hash_table_insert (object_name_counts, g_strdup (type_name),
699       GINT_TO_POINTER (count + 1));
701   G_UNLOCK (object_name_mutex);
703   /* GstFooSink -> foosinkN */
704   if (strncmp (type_name, "Gst", 3) == 0)
705     type_name += 3;
706   tmp = g_strdup_printf ("%s%d", type_name, count);
707   name = g_ascii_strdown (tmp, strlen (tmp));
708   g_free (tmp);
710   result = gst_object_set_name (object, name);
711   g_free (name);
713   return result;
716 /**
717  * gst_object_set_name:
718  * @object: a #GstObject to set the name of
719  * @name:   new name of object
720  *
721  * Sets the name of the object, or gives the object a guaranteed unique
722  * name (if @name is NULL).
723  * This function makes a copy of the provided name, so the caller
724  * retains ownership of the name it sent.
725  *
726  * Returns: TRUE if the name could be set. Objects that have
727  * a parent cannot be renamed.
728  *
729  * MT safe.  This function grabs and releases the object's LOCK.
730  */
731 gboolean
732 gst_object_set_name (GstObject * object, const gchar * name)
734   gboolean result;
736   g_return_val_if_fail (GST_IS_OBJECT (object), FALSE);
738   GST_LOCK (object);
740   /* parented objects cannot be renamed */
741   if (G_UNLIKELY (object->parent != NULL))
742     goto had_parent;
744   if (name != NULL) {
745     g_free (object->name);
746     object->name = g_strdup (name);
747     GST_UNLOCK (object);
748     result = TRUE;
749   } else {
750     GST_UNLOCK (object);
751     result = gst_object_set_name_default (object, G_OBJECT_TYPE_NAME (object));
752   }
753   return result;
755   /* error */
756 had_parent:
757   {
758     GST_UNLOCK (object);
759     return FALSE;
760   }
763 /**
764  * gst_object_get_name:
765  * @object: a #GstObject to get the name of
766  *
767  * Returns a copy of the name of the object.
768  * Caller should g_free() the return value after usage.
769  * For a nameless object, this returns NULL, which you can safely g_free()
770  * as well.
771  *
772  * Returns: the name of the object. g_free() after usage.
773  *
774  * MT safe. This function grabs and releases the object's LOCK.
775  */
776 gchar *
777 gst_object_get_name (GstObject * object)
779   gchar *result = NULL;
781   g_return_val_if_fail (GST_IS_OBJECT (object), NULL);
783   GST_LOCK (object);
784   result = g_strdup (object->name);
785   GST_UNLOCK (object);
787   return result;
790 /**
791  * gst_object_set_name_prefix:
792  * @object:      a #GstObject to set the name prefix of
793  * @name_prefix: new name prefix of object
794  *
795  * Sets the name prefix of the object.
796  * This function makes a copy of the provided name prefix, so the caller
797  * retains ownership of the name prefix it sent.
798  *
799  * MT safe.  This function grabs and releases the object's LOCK.
800  */
801 void
802 gst_object_set_name_prefix (GstObject * object, const gchar * name_prefix)
804   g_return_if_fail (GST_IS_OBJECT (object));
806   GST_LOCK (object);
807   g_free (object->name_prefix);
808   object->name_prefix = g_strdup (name_prefix); /* NULL gives NULL */
809   GST_UNLOCK (object);
812 /**
813  * gst_object_get_name_prefix:
814  * @object: a #GstObject to get the name prefix of
815  *
816  * Returns a copy of the name prefix of the object.
817  * Caller should g_free() the return value after usage.
818  * For a prefixless object, this returns NULL, which you can safely g_free()
819  * as well.
820  *
821  * Returns: the name prefix of the object. g_free() after usage.
822  *
823  * MT safe. This function grabs and releases the object's LOCK.
824  */
825 gchar *
826 gst_object_get_name_prefix (GstObject * object)
828   gchar *result = NULL;
830   g_return_val_if_fail (GST_IS_OBJECT (object), NULL);
832   GST_LOCK (object);
833   result = g_strdup (object->name_prefix);
834   GST_UNLOCK (object);
836   return result;
839 /**
840  * gst_object_set_parent:
841  * @object: GstObject to set parent of
842  * @parent: new parent of object
843  *
844  * Sets the parent of @object. The object's reference count will be incremented,
845  * and any floating reference will be removed (see gst_object_sink()).
846  *
847  * Causes the parent-set signal to be emitted.
848  *
849  * Returns: TRUE if the parent could be set or FALSE when the object
850  * already had a parent, the object and parent are the same or wrong
851  * parameters were provided.
852  *
853  * MT safe. Grabs and releases the object's LOCK.
854  */
855 gboolean
856 gst_object_set_parent (GstObject * object, GstObject * parent)
858   g_return_val_if_fail (GST_IS_OBJECT (object), FALSE);
859   g_return_val_if_fail (GST_IS_OBJECT (parent), FALSE);
860   g_return_val_if_fail (object != parent, FALSE);
862   GST_CAT_DEBUG_OBJECT (GST_CAT_REFCOUNTING, object,
863       "set parent (ref and sink)");
865   GST_LOCK (object);
866   if (G_UNLIKELY (object->parent != NULL))
867     goto had_parent;
869   /* sink object, we don't call our own function because we don't
870    * need to release/acquire the lock needlessly or touch the refcount
871    * in the floating case. */
872   object->parent = parent;
873   if (G_LIKELY (GST_OBJECT_IS_FLOATING (object))) {
874     GST_FLAG_UNSET (object, GST_OBJECT_FLOATING);
875     GST_UNLOCK (object);
876   } else {
877     GST_UNLOCK (object);
878     gst_object_ref (object);
879   }
881   g_signal_emit (G_OBJECT (object), gst_object_signals[PARENT_SET], 0, parent);
883   return TRUE;
885   /* ERROR handling */
886 had_parent:
887   {
888     GST_UNLOCK (object);
889     return FALSE;
890   }
893 /**
894  * gst_object_get_parent:
895  * @object: GstObject to get parent of
896  *
897  * Returns the parent of @object. This function increases the refcount
898  * of the parent object so you should gst_object_unref() it after usage.
899  *
900  * Returns: parent of the object, this can be NULL if the object has no
901  *   parent. unref after usage.
902  *
903  * MT safe. Grabs and releases the object's LOCK.
904  */
905 GstObject *
906 gst_object_get_parent (GstObject * object)
908   GstObject *result = NULL;
910   g_return_val_if_fail (GST_IS_OBJECT (object), NULL);
912   GST_LOCK (object);
913   result = object->parent;
914   if (G_LIKELY (result))
915     gst_object_ref (result);
916   GST_UNLOCK (object);
918   return result;
921 /**
922  * gst_object_unparent:
923  * @object: GstObject to unparent
924  *
925  * Clear the parent of @object, removing the associated reference.
926  * This function decreases the refcount of the object so the object
927  * might not point to valid memory anymore after calling this function.
928  *
929  * MT safe. Grabs and releases the object's lock.
930  */
931 void
932 gst_object_unparent (GstObject * object)
934   GstObject *parent;
936   g_return_if_fail (GST_IS_OBJECT (object));
938   GST_LOCK (object);
939   parent = object->parent;
941   if (G_LIKELY (parent != NULL)) {
942     GST_CAT_LOG_OBJECT (GST_CAT_REFCOUNTING, object, "unparent");
943     object->parent = NULL;
944     GST_UNLOCK (object);
946     g_signal_emit (G_OBJECT (object), gst_object_signals[PARENT_UNSET], 0,
947         parent);
949     gst_object_unref (object);
950   } else {
951     GST_UNLOCK (object);
952   }
955 /**
956  * gst_object_has_ancestor:
957  * @object: GstObject to check
958  * @ancestor: GstObject to check as ancestor
959  *
960  * Check if @object has an ancestor @ancestor somewhere up in
961  * the hierarchy.
962  *
963  * Returns: TRUE if @ancestor is an ancestor of @object.
964  *
965  * MT safe. Grabs and releases the object's locks.
966  */
967 gboolean
968 gst_object_has_ancestor (GstObject * object, GstObject * ancestor)
970   GstObject *parent;
971   gboolean result = FALSE;
973   if (object == NULL)
974     return FALSE;
976   if (object == ancestor)
977     return TRUE;
979   parent = gst_object_get_parent (object);
980   result = gst_object_has_ancestor (parent, ancestor);
981   if (parent)
982     gst_object_unref (parent);
984   return result;
987 /**
988  * gst_object_check_uniqueness:
989  * @list: a list of #GstObject to check through
990  * @name: the name to search for
991  *
992  * Checks to see if there is any object named @name in @list. This function
993  * does not do any locking of any kind. You might want to protect the
994  * provided list with the lock of the owner of the list. This function
995  * will lock each GstObject in the list to compare the name, so be
996  * carefull when passing a list with a locked object.
997  *
998  * Returns: TRUE if the name does not appear in the list, FALSE if it does.
999  *
1000  * MT safe. Grabs and releases the LOCK of each object in the list.
1001  */
1002 gboolean
1003 gst_object_check_uniqueness (GList * list, const gchar * name)
1005   gboolean result = TRUE;
1007   g_return_val_if_fail (name != NULL, FALSE);
1009   for (; list; list = g_list_next (list)) {
1010     GstObject *child;
1011     gboolean eq;
1013     child = GST_OBJECT (list->data);
1015     GST_LOCK (child);
1016     eq = strcmp (GST_OBJECT_NAME (child), name) == 0;
1017     GST_UNLOCK (child);
1019     if (G_UNLIKELY (eq)) {
1020       result = FALSE;
1021       break;
1022     }
1023   }
1024   return result;
1028 #ifndef GST_DISABLE_LOADSAVE_REGISTRY
1029 /**
1030  * gst_object_save_thyself:
1031  * @object: GstObject to save
1032  * @parent: The parent XML node to save the object into
1033  *
1034  * Saves the given object into the parent XML node.
1035  *
1036  * Returns: the new xmlNodePtr with the saved object
1037  */
1038 xmlNodePtr
1039 gst_object_save_thyself (GstObject * object, xmlNodePtr parent)
1041   GstObjectClass *oclass;
1043   g_return_val_if_fail (GST_IS_OBJECT (object), parent);
1044   g_return_val_if_fail (parent != NULL, parent);
1046   oclass = GST_OBJECT_GET_CLASS (object);
1048   if (oclass->save_thyself)
1049     oclass->save_thyself (object, parent);
1051   g_signal_emit (G_OBJECT (object), gst_object_signals[OBJECT_SAVED], 0,
1052       parent);
1054   return parent;
1057 /**
1058  * gst_object_restore_thyself:
1059  * @object: GstObject to load into
1060  * @self: The XML node to load the object from
1061  *
1062  * Restores the given object with the data from the parent XML node.
1063  */
1064 void
1065 gst_object_restore_thyself (GstObject * object, xmlNodePtr self)
1067   GstObjectClass *oclass;
1069   g_return_if_fail (GST_IS_OBJECT (object));
1070   g_return_if_fail (self != NULL);
1072   oclass = GST_OBJECT_GET_CLASS (object);
1074   if (oclass->restore_thyself)
1075     oclass->restore_thyself (object, self);
1078 static void
1079 gst_object_real_restore_thyself (GstObject * object, xmlNodePtr self)
1081   g_return_if_fail (GST_IS_OBJECT (object));
1082   g_return_if_fail (self != NULL);
1084   gst_class_signal_emit_by_name (object, "object_loaded", self);
1086 #endif /* GST_DISABLE_LOADSAVE_REGISTRY */
1088 static void
1089 gst_object_set_property (GObject * object, guint prop_id,
1090     const GValue * value, GParamSpec * pspec)
1092   GstObject *gstobject;
1094   gstobject = GST_OBJECT (object);
1096   switch (prop_id) {
1097     case ARG_NAME:
1098       gst_object_set_name (gstobject, g_value_get_string (value));
1099       break;
1100     default:
1101       G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
1102       break;
1103   }
1106 static void
1107 gst_object_get_property (GObject * object, guint prop_id,
1108     GValue * value, GParamSpec * pspec)
1110   GstObject *gstobject;
1112   gstobject = GST_OBJECT (object);
1114   switch (prop_id) {
1115     case ARG_NAME:
1116       g_value_take_string (value, gst_object_get_name (gstobject));
1117       break;
1118     default:
1119       G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
1120       break;
1121   }
1124 /**
1125  * gst_object_get_path_string:
1126  * @object: GstObject to get the path from
1127  *
1128  * Generates a string describing the path of the object in
1129  * the object hierarchy. Only useful (or used) for debugging.
1130  *
1131  * Returns: a string describing the path of the object. You must
1132  *          g_free() the string after usage. 
1133  *
1134  * MT safe. Grabs and releases the object's LOCK for all objects
1135  *          in the hierarchy.
1136  */
1137 gchar *
1138 gst_object_get_path_string (GstObject * object)
1140   GSList *parentage;
1141   GSList *parents;
1142   void *parent;
1143   gchar *prevpath, *path;
1144   gchar *component;
1145   gchar *separator;
1147   /* ref object before adding to list */
1148   gst_object_ref (object);
1149   parentage = g_slist_prepend (NULL, object);
1151   path = g_strdup ("");
1153   /* first walk the object hierarchy to build a list of the parents,
1154    * be carefull here with refcounting. */
1155   do {
1156     if (GST_IS_OBJECT (object)) {
1157       parent = gst_object_get_parent (object);
1158       /* add parents to list, refcount remains increased while
1159        * we handle the object */
1160       if (parent)
1161         parentage = g_slist_prepend (parentage, parent);
1162     } else {
1163       break;
1164     }
1165     object = parent;
1166   } while (object != NULL);
1168   /* then walk the parent list and print them out. we need to
1169    * decrease the refcounting on each element after we handled
1170    * it. */
1171   for (parents = parentage; parents; parents = g_slist_next (parents)) {
1172     if (GST_IS_OBJECT (parents->data)) {
1173       GstObject *item = GST_OBJECT_CAST (parents->data);
1174       GstObjectClass *oclass = GST_OBJECT_GET_CLASS (item);
1176       component = gst_object_get_name (item);
1177       separator = oclass->path_string_separator;
1178       /* and unref now */
1179       gst_object_unref (item);
1180     } else {
1181       component = g_strdup_printf ("%p", parents->data);
1182       separator = "/";
1183     }
1185     prevpath = path;
1186     path = g_strjoin (separator, prevpath, component, NULL);
1187     g_free (prevpath);
1188     g_free (component);
1189   }
1191   g_slist_free (parentage);
1193   return path;
1196 struct _GstSignalObject
1198   GObject object;
1199 };
1201 struct _GstSignalObjectClass
1203   GObjectClass parent_class;
1205   /* signals */
1206 #ifndef GST_DISABLE_LOADSAVE_REGISTRY
1207   void (*object_loaded) (GstSignalObject * object, GstObject * new,
1208       xmlNodePtr self);
1209 #endif                          /* GST_DISABLE_LOADSAVE_REGISTRY */
1210 };
1212 static GType
1213 gst_signal_object_get_type (void)
1215   static GType signal_object_type = 0;
1217   if (!signal_object_type) {
1218     static const GTypeInfo signal_object_info = {
1219       sizeof (GstSignalObjectClass),
1220       NULL,
1221       NULL,
1222       (GClassInitFunc) gst_signal_object_class_init,
1223       NULL,
1224       NULL,
1225       sizeof (GstSignalObject),
1226       0,
1227       (GInstanceInitFunc) gst_signal_object_init,
1228       NULL
1229     };
1231     signal_object_type =
1232         g_type_register_static (G_TYPE_OBJECT, "GstSignalObject",
1233         &signal_object_info, 0);
1234   }
1235   return signal_object_type;
1238 static void
1239 gst_signal_object_class_init (GstSignalObjectClass * klass)
1241   GObjectClass *gobject_class;
1243   gobject_class = (GObjectClass *) klass;
1245   parent_class = g_type_class_ref (G_TYPE_OBJECT);
1247 #ifndef GST_DISABLE_LOADSAVE_REGISTRY
1248   gst_signal_object_signals[SO_OBJECT_LOADED] =
1249       g_signal_new ("object-loaded", G_TYPE_FROM_CLASS (klass),
1250       G_SIGNAL_RUN_LAST, G_STRUCT_OFFSET (GstSignalObjectClass, object_loaded),
1251       NULL, NULL, gst_marshal_VOID__OBJECT_POINTER, G_TYPE_NONE, 2,
1252       G_TYPE_OBJECT, G_TYPE_POINTER);
1253 #endif
1256 static void
1257 gst_signal_object_init (GstSignalObject * object)
1261 /**
1262  * gst_class_signal_connect
1263  * @klass: the GstObjectClass to attach the signal to
1264  * @name: the name of the signal to attach to
1265  * @func: the signal function
1266  * @func_data: a pointer to user data
1267  *
1268  * Connect to a class signal.
1269  *
1270  * Returns: the signal id.
1271  */
1272 guint
1273 gst_class_signal_connect (GstObjectClass * klass,
1274     const gchar * name, gpointer func, gpointer func_data)
1276   return g_signal_connect (klass->signal_object, name, func, func_data);
1279 #ifndef GST_DISABLE_LOADSAVE_REGISTRY
1280 /**
1281  * gst_class_signal_emit_by_name:
1282  * @object: the object that sends the signal
1283  * @name: the name of the signal to emit
1284  * @self: data for the signal
1285  *
1286  * emits the named class signal.
1287  */
1288 void
1289 gst_class_signal_emit_by_name (GstObject * object,
1290     const gchar * name, xmlNodePtr self)
1292   GstObjectClass *oclass;
1294   oclass = GST_OBJECT_GET_CLASS (object);
1296   g_signal_emit_by_name (oclass->signal_object, name, object, self);
1299 #endif /* GST_DISABLE_LOADSAVE_REGISTRY */