]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blob - gst/gstpipeline.c
d80a38aa1347729395a862f93be4f5031bef3ac3
[glsdk/gstreamer0-10.git] / gst / gstpipeline.c
1 /* GStreamer
2  * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3  *                    2004,2005 Wim Taymans <wim@fluendo.com>
4  *
5  * gstpipeline.c: Overall pipeline management element
6  *
7  * This library is free software; you can redistribute it and/or
8  * modify it under the terms of the GNU Library General Public
9  * License as published by the Free Software Foundation; either
10  * version 2 of the License, or (at your option) any later version.
11  *
12  * This library is distributed in the hope that it will be useful,
13  * but WITHOUT ANY WARRANTY; without even the implied warranty of
14  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
15  * Library General Public License for more details.
16  *
17  * You should have received a copy of the GNU Library General Public
18  * License along with this library; if not, write to the
19  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20  * Boston, MA 02111-1307, USA.
21  */
23 /**
24  * SECTION:gstpipeline
25  * @short_description: Top-level bin with clocking and bus management
26                        functionality.
27  * @see_also: #GstElement, #GstBin, #GstClock, #GstBus
28  *
29  * A #GstPipeline is a special #GstBin used as the toplevel container for
30  * the filter graph. The #GstPipeline will manage the selection and
31  * distribution of a global #GstClock as well as provide a #GstBus to the
32  * application. It will also implement a default behavour for managing
33  * seek events (see gst_element_seek()).
34  *
35  * gst_pipeline_new() is used to create a pipeline. when you are done with
36  * the pipeline, use gst_object_unref() to free its resources including all
37  * added #GstElement objects (if not otherwise referenced).
38  *
39  * Elements are added and removed from the pipeline using the #GstBin
40  * methods like gst_bin_add() and gst_bin_remove() (see #GstBin).
41  *
42  * Before changing the state of the #GstPipeline (see #GstElement) a #GstBus
43  * can be retrieved with gst_pipeline_get_bus(). This bus can then be
44  * used to receive #GstMessage from the elements in the pipeline.
45  *
46  * By default, a #GstPipeline will automatically flush the pending #GstBus
47  * messages when going to the NULL state to ensure that no circular
48  * references exist when no messages are read from the #GstBus. This
49  * behaviour can be changed with gst_pipeline_set_auto_flush_bus().
50  *
51  * When the #GstPipeline performs the PAUSED to PLAYING state change it will
52  * select a clock for the elements. The clock selection algorithm will by
53  * default select a clock provided by an element that is most upstream
54  * (closest to the source). For live pipelines (ones that return
55  * #GST_STATE_CHANGE_NO_PREROLL from the gst_element_set_state() call) this
56  * will select the clock provided by the live source. For normal pipelines
57  * this will select a clock provided by the sinks (most likely the audio
58  * sink). If no element provides a clock, a default #GstSystemClock is used.
59  *
60  * The clock selection can be controlled with the gst_pipeline_use_clock()
61  * method, which will enforce a given clock on the pipeline. With
62  * gst_pipeline_auto_clock() the default clock selection algorithm can be
63  * restored.
64  *
65  * A #GstPipeline maintains a running time for the elements. The running
66  * time is defined as the difference between the current clock time and
67  * the base time. When the pipeline goes to READY or a flushing seek is
68  * performed on it, the running time is reset to 0. When the pipeline is
69  * set from PLAYING to PAUSED, the current clock time is sampled and used to
70  * configure the base time for the elements when the pipeline is set
71  * to PLAYING again. The effect is that the running time (as the difference
72  * between the clock time and the base time) will count how much time was spent
73  * in the PLAYING state. This default behaviour can be changed with the
74  * gst_element_set_start_time() method.
75  *
76  * When sending a flushing seek event to a GstPipeline (see
77  * gst_element_seek()), it will make sure that the pipeline is properly
78  * PAUSED and resumed as well as set the new running time to 0 when the
79  * seek succeeded.
80  *
81  * Last reviewed on 2009-05-29 (0.10.24)
82  */
84 #include "gst_private.h"
85 #include "gsterror.h"
86 #include "gst-i18n-lib.h"
88 #include "gstpipeline.h"
89 #include "gstinfo.h"
90 #include "gstsystemclock.h"
91 #include "gstutils.h"
93 GST_DEBUG_CATEGORY_STATIC (pipeline_debug);
94 #define GST_CAT_DEFAULT pipeline_debug
96 /* Pipeline signals and args */
97 enum
98 {
99   /* FILL ME */
100   LAST_SIGNAL
101 };
103 #define DEFAULT_DELAY           0
104 #define DEFAULT_AUTO_FLUSH_BUS  TRUE
106 enum
108   PROP_0,
109   PROP_DELAY,
110   PROP_AUTO_FLUSH_BUS
111 };
113 #define GST_PIPELINE_GET_PRIVATE(obj)  \
114    (G_TYPE_INSTANCE_GET_PRIVATE ((obj), GST_TYPE_PIPELINE, GstPipelinePrivate))
116 struct _GstPipelinePrivate
118   /* with LOCK */
119   gboolean auto_flush_bus;
121   /* when we need to update stream_time or clock when going back to
122    * PLAYING*/
123   GstClockTime last_start_time;
124   gboolean update_clock;
125 };
128 static void gst_pipeline_dispose (GObject * object);
129 static void gst_pipeline_set_property (GObject * object, guint prop_id,
130     const GValue * value, GParamSpec * pspec);
131 static void gst_pipeline_get_property (GObject * object, guint prop_id,
132     GValue * value, GParamSpec * pspec);
134 static GstClock *gst_pipeline_provide_clock_func (GstElement * element);
135 static GstStateChangeReturn gst_pipeline_change_state (GstElement * element,
136     GstStateChange transition);
138 static void gst_pipeline_handle_message (GstBin * bin, GstMessage * message);
140 /* static guint gst_pipeline_signals[LAST_SIGNAL] = { 0 }; */
142 #define _do_init(type) \
143 { \
144   GST_DEBUG_CATEGORY_INIT (pipeline_debug, "pipeline", GST_DEBUG_BOLD, \
145       "debugging info for the 'pipeline' container element"); \
148 GST_BOILERPLATE_FULL (GstPipeline, gst_pipeline, GstBin, GST_TYPE_BIN,
149     _do_init);
151 static void
152 gst_pipeline_base_init (gpointer g_class)
154   GstElementClass *gstelement_class = GST_ELEMENT_CLASS (g_class);
156   gst_element_class_set_details_simple (gstelement_class, "Pipeline object",
157       "Generic/Bin",
158       "Complete pipeline object",
159       "Erik Walthinsen <omega@cse.ogi.edu>, Wim Taymans <wim@fluendo.com>");
162 static void
163 gst_pipeline_class_init (GstPipelineClass * klass)
165   GObjectClass *gobject_class = G_OBJECT_CLASS (klass);
166   GstElementClass *gstelement_class = GST_ELEMENT_CLASS (klass);
167   GstBinClass *gstbin_class = GST_BIN_CLASS (klass);
169   g_type_class_add_private (klass, sizeof (GstPipelinePrivate));
171   gobject_class->set_property = gst_pipeline_set_property;
172   gobject_class->get_property = gst_pipeline_get_property;
174   /**
175    * GstPipeline:delay
176    *
177    * The expected delay needed for elements to spin up to the
178    * PLAYING state expressed in nanoseconds.
179    * see gst_pipeline_set_delay() for more information on this option.
180    *
181    * Since: 0.10.5
182    **/
183   g_object_class_install_property (gobject_class, PROP_DELAY,
184       g_param_spec_uint64 ("delay", "Delay",
185           "Expected delay needed for elements "
186           "to spin up to PLAYING in nanoseconds", 0, G_MAXUINT64, DEFAULT_DELAY,
187           G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
189   /**
190    * GstPipeline:auto-flush-bus:
191    *
192    * Whether or not to automatically flush all messages on the
193    * pipeline's bus when going from READY to NULL state. Please see
194    * gst_pipeline_set_auto_flush_bus() for more information on this option.
195    *
196    * Since: 0.10.4
197    **/
198   g_object_class_install_property (gobject_class, PROP_AUTO_FLUSH_BUS,
199       g_param_spec_boolean ("auto-flush-bus", "Auto Flush Bus",
200           "Whether to automatically flush the pipeline's bus when going "
201           "from READY into NULL state", DEFAULT_AUTO_FLUSH_BUS,
202           G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
204   gobject_class->dispose = gst_pipeline_dispose;
206   gstelement_class->change_state =
207       GST_DEBUG_FUNCPTR (gst_pipeline_change_state);
208   gstelement_class->provide_clock =
209       GST_DEBUG_FUNCPTR (gst_pipeline_provide_clock_func);
210   gstbin_class->handle_message =
211       GST_DEBUG_FUNCPTR (gst_pipeline_handle_message);
214 static void
215 gst_pipeline_init (GstPipeline * pipeline, GstPipelineClass * klass)
217   GstBus *bus;
219   pipeline->priv = GST_PIPELINE_GET_PRIVATE (pipeline);
221   /* set default property values */
222   pipeline->priv->auto_flush_bus = DEFAULT_AUTO_FLUSH_BUS;
223   pipeline->delay = DEFAULT_DELAY;
225   /* create and set a default bus */
226   bus = gst_bus_new ();
227 #if 0
228   /* FIXME, disabled for 0.10.5 release as it caused to many regressions */
229   /* Start our bus in flushing if appropriate */
230   if (pipeline->priv->auto_flush_bus)
231     gst_bus_set_flushing (bus, TRUE);
232 #endif
234   gst_element_set_bus (GST_ELEMENT_CAST (pipeline), bus);
235   GST_DEBUG_OBJECT (pipeline, "set bus %" GST_PTR_FORMAT " on pipeline", bus);
236   gst_object_unref (bus);
239 static void
240 gst_pipeline_dispose (GObject * object)
242   GstPipeline *pipeline = GST_PIPELINE (object);
243   GstClock **clock_p = &pipeline->fixed_clock;
245   GST_CAT_DEBUG_OBJECT (GST_CAT_REFCOUNTING, pipeline, "dispose");
247   /* clear and unref any fixed clock */
248   gst_object_replace ((GstObject **) clock_p, NULL);
250   G_OBJECT_CLASS (parent_class)->dispose (object);
253 static void
254 gst_pipeline_set_property (GObject * object, guint prop_id,
255     const GValue * value, GParamSpec * pspec)
257   GstPipeline *pipeline = GST_PIPELINE (object);
259   switch (prop_id) {
260     case PROP_DELAY:
261       gst_pipeline_set_delay (pipeline, g_value_get_uint64 (value));
262       break;
263     case PROP_AUTO_FLUSH_BUS:
264       gst_pipeline_set_auto_flush_bus (pipeline, g_value_get_boolean (value));
265       break;
266     default:
267       G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
268       break;
269   }
272 static void
273 gst_pipeline_get_property (GObject * object, guint prop_id,
274     GValue * value, GParamSpec * pspec)
276   GstPipeline *pipeline = GST_PIPELINE (object);
278   switch (prop_id) {
279     case PROP_DELAY:
280       g_value_set_uint64 (value, gst_pipeline_get_delay (pipeline));
281       break;
282     case PROP_AUTO_FLUSH_BUS:
283       g_value_set_boolean (value, gst_pipeline_get_auto_flush_bus (pipeline));
284       break;
285     default:
286       G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
287       break;
288   }
291 /* set the start_time to 0, this will cause us to select a new base_time and
292  * make the running_time start from 0 again. */
293 static void
294 reset_start_time (GstPipeline * pipeline)
296   GST_OBJECT_LOCK (pipeline);
297   if (GST_ELEMENT_START_TIME (pipeline) != GST_CLOCK_TIME_NONE) {
298     GST_DEBUG_OBJECT (pipeline, "reset start_time to 0");
299     GST_ELEMENT_START_TIME (pipeline) = 0;
300     pipeline->priv->last_start_time = -1;
301   } else {
302     GST_DEBUG_OBJECT (pipeline, "application asked to not reset stream_time");
303   }
304   GST_OBJECT_UNLOCK (pipeline);
307 /**
308  * gst_pipeline_new:
309  * @name: name of new pipeline
310  *
311  * Create a new pipeline with the given name.
312  *
313  * Returns: (transfer full): newly created GstPipeline
314  *
315  * MT safe.
316  */
317 GstElement *
318 gst_pipeline_new (const gchar * name)
320   return gst_element_factory_make ("pipeline", name);
323 /* takes a snapshot of the running_time of the pipeline and store this as the
324  * element start_time. This is the time we will set as the running_time of the
325  * pipeline when we go to PLAYING next. */
326 static void
327 pipeline_update_start_time (GstElement * element)
329   GstPipeline *pipeline = GST_PIPELINE_CAST (element);
330   GstClock *clock;
332   GST_OBJECT_LOCK (element);
333   if ((clock = element->clock)) {
334     GstClockTime now;
336     gst_object_ref (clock);
337     GST_OBJECT_UNLOCK (element);
339     /* calculate the time when we stopped */
340     now = gst_clock_get_time (clock);
341     gst_object_unref (clock);
343     GST_OBJECT_LOCK (element);
344     /* store the current running time */
345     if (GST_ELEMENT_START_TIME (pipeline) != GST_CLOCK_TIME_NONE) {
346       if (now != GST_CLOCK_TIME_NONE)
347         GST_ELEMENT_START_TIME (pipeline) = now - element->base_time;
348       else
349         GST_WARNING_OBJECT (element,
350             "Clock %s returned invalid time, can't calculate "
351             "running_time when going to the PAUSED state",
352             GST_OBJECT_NAME (clock));
354       /* we went to PAUSED, when going to PLAYING select clock and new
355        * base_time */
356       pipeline->priv->update_clock = TRUE;
357     }
358     GST_DEBUG_OBJECT (element,
359         "start_time=%" GST_TIME_FORMAT ", now=%" GST_TIME_FORMAT
360         ", base_time %" GST_TIME_FORMAT,
361         GST_TIME_ARGS (GST_ELEMENT_START_TIME (pipeline)),
362         GST_TIME_ARGS (now), GST_TIME_ARGS (element->base_time));
363   }
364   GST_OBJECT_UNLOCK (element);
367 /* MT safe */
368 static GstStateChangeReturn
369 gst_pipeline_change_state (GstElement * element, GstStateChange transition)
371   GstStateChangeReturn result = GST_STATE_CHANGE_SUCCESS;
372   GstPipeline *pipeline = GST_PIPELINE_CAST (element);
373   GstClock *clock;
375   switch (transition) {
376     case GST_STATE_CHANGE_NULL_TO_READY:
377       GST_OBJECT_LOCK (element);
378       if (element->bus)
379         gst_bus_set_flushing (element->bus, FALSE);
380       GST_OBJECT_UNLOCK (element);
381       break;
382     case GST_STATE_CHANGE_READY_TO_PAUSED:
383       GST_OBJECT_LOCK (element);
384       pipeline->priv->update_clock = TRUE;
385       GST_OBJECT_UNLOCK (element);
386       break;
387     case GST_STATE_CHANGE_PAUSED_TO_PLAYING:
388     {
389       GstClockTime now, start_time, last_start_time, delay;
390       gboolean update_clock;
391       GstClock *cur_clock;
393       GST_DEBUG_OBJECT (element, "selecting clock and base_time");
395       GST_OBJECT_LOCK (element);
396       cur_clock = element->clock;
397       if (cur_clock)
398         gst_object_ref (cur_clock);
399       /* get the desired running_time of the first buffer aka the start_time */
400       start_time = GST_ELEMENT_START_TIME (pipeline);
401       last_start_time = pipeline->priv->last_start_time;
402       pipeline->priv->last_start_time = start_time;
403       /* see if we need to update the clock */
404       update_clock = pipeline->priv->update_clock;
405       pipeline->priv->update_clock = FALSE;
406       delay = pipeline->delay;
407       GST_OBJECT_UNLOCK (element);
409       /* running time changed, either with a PAUSED or a flush, we need to check
410        * if there is a new clock & update the base time */
411       if (update_clock || last_start_time != start_time) {
412         GST_DEBUG_OBJECT (pipeline, "Need to update start_time");
414         /* when going to PLAYING, select a clock when needed. If we just got
415          * flushed, we don't reselect the clock. */
416         if (update_clock) {
417           GST_DEBUG_OBJECT (pipeline, "Need to update clock.");
418           clock = gst_element_provide_clock (element);
419         } else {
420           GST_DEBUG_OBJECT (pipeline,
421               "Don't need to update clock, using old clock.");
422           clock = gst_object_ref (cur_clock);
423         }
425         if (clock) {
426           now = gst_clock_get_time (clock);
427         } else {
428           GST_DEBUG ("no clock, using base time of NONE");
429           now = GST_CLOCK_TIME_NONE;
430         }
432         if (clock != cur_clock) {
433           /* now distribute the clock (which could be NULL). If some
434            * element refuses the clock, this will return FALSE and
435            * we effectively fail the state change. */
436           if (!gst_element_set_clock (element, clock))
437             goto invalid_clock;
439           /* if we selected and distributed a new clock, let the app
440            * know about it */
441           gst_element_post_message (element,
442               gst_message_new_new_clock (GST_OBJECT_CAST (element), clock));
443         }
445         if (clock)
446           gst_object_unref (clock);
448         if (start_time != GST_CLOCK_TIME_NONE && now != GST_CLOCK_TIME_NONE) {
449           GstClockTime new_base_time = now - start_time + delay;
450           GST_DEBUG_OBJECT (element,
451               "start_time=%" GST_TIME_FORMAT ", now=%" GST_TIME_FORMAT
452               ", base_time %" GST_TIME_FORMAT,
453               GST_TIME_ARGS (start_time), GST_TIME_ARGS (now),
454               GST_TIME_ARGS (new_base_time));
456           gst_element_set_base_time (element, new_base_time);
457         } else {
458           GST_DEBUG_OBJECT (pipeline,
459               "NOT adjusting base_time because start_time is NONE");
460         }
461       } else {
462         GST_DEBUG_OBJECT (pipeline,
463             "NOT adjusting base_time because we selected one before");
464       }
466       if (cur_clock)
467         gst_object_unref (cur_clock);
468       break;
469     }
470     case GST_STATE_CHANGE_PLAYING_TO_PAUSED:
471     {
472       /* we take a start_time snapshot before calling the children state changes
473        * so that they know about when the pipeline PAUSED. */
474       pipeline_update_start_time (element);
475       break;
476     }
477     case GST_STATE_CHANGE_PAUSED_TO_READY:
478     case GST_STATE_CHANGE_READY_TO_NULL:
479       break;
480   }
482   result = GST_ELEMENT_CLASS (parent_class)->change_state (element, transition);
484   switch (transition) {
485     case GST_STATE_CHANGE_NULL_TO_READY:
486       break;
487     case GST_STATE_CHANGE_READY_TO_PAUSED:
488     {
489       reset_start_time (pipeline);
490       break;
491     }
492     case GST_STATE_CHANGE_PAUSED_TO_PLAYING:
493       break;
494     case GST_STATE_CHANGE_PLAYING_TO_PAUSED:
495     {
496       /* Take a new snapshot of the start_time after calling the state change on
497        * all children. This will be the running_time of the pipeline when we go
498        * back to PLAYING */
499       pipeline_update_start_time (element);
500       break;
501     }
502     case GST_STATE_CHANGE_PAUSED_TO_READY:
503       break;
504     case GST_STATE_CHANGE_READY_TO_NULL:
505     {
506       GstBus *bus;
507       gboolean auto_flush;
509       /* grab some stuff before we release the lock to flush out the bus */
510       GST_OBJECT_LOCK (element);
511       if ((bus = element->bus))
512         gst_object_ref (bus);
513       auto_flush = pipeline->priv->auto_flush_bus;
514       GST_OBJECT_UNLOCK (element);
516       if (bus) {
517         if (auto_flush) {
518           gst_bus_set_flushing (bus, TRUE);
519         } else {
520           GST_INFO_OBJECT (element, "not flushing bus, auto-flushing disabled");
521         }
522         gst_object_unref (bus);
523       }
524       break;
525     }
526   }
527   return result;
529   /* ERRORS */
530 invalid_clock:
531   {
532     /* we generate this error when the selected clock was not
533      * accepted by some element */
534     GST_ELEMENT_ERROR (pipeline, CORE, CLOCK,
535         (_("Selected clock cannot be used in pipeline.")),
536         ("Pipeline cannot operate with selected clock"));
537     GST_DEBUG_OBJECT (pipeline,
538         "Pipeline cannot operate with selected clock %p", clock);
539     if (clock)
540       gst_object_unref (clock);
541     return GST_STATE_CHANGE_FAILURE;
542   }
545 /* intercept the bus messages from our children. We watch for the ASYNC_START
546  * message with is posted by the elements (sinks) that require a reset of the
547  * running_time after a flush. ASYNC_START also brings the pipeline back into
548  * the PAUSED, pending PAUSED state. When the ASYNC_DONE message is received the
549  * pipeline will redistribute the new base_time and will bring the elements back
550  * to the desired state of the pipeline. */
551 static void
552 gst_pipeline_handle_message (GstBin * bin, GstMessage * message)
554   GstPipeline *pipeline = GST_PIPELINE_CAST (bin);
556   switch (GST_MESSAGE_TYPE (message)) {
557     case GST_MESSAGE_ASYNC_START:
558     {
559       gboolean new_base_time;
561       gst_message_parse_async_start (message, &new_base_time);
563       /* reset our running time if we need to distribute a new base_time to the
564        * children. */
565       if (new_base_time)
566         reset_start_time (pipeline);
568       break;
569     }
570     case GST_MESSAGE_CLOCK_LOST:
571     {
572       GstClock *clock;
574       gst_message_parse_clock_lost (message, &clock);
576       GST_OBJECT_LOCK (bin);
577       if (clock == GST_ELEMENT_CAST (bin)->clock) {
578         GST_DEBUG_OBJECT (bin, "Used clock '%s' got lost",
579             GST_OBJECT_NAME (clock));
580         pipeline->priv->update_clock = TRUE;
581       }
582       GST_OBJECT_UNLOCK (bin);
583     }
584     default:
585       break;
586   }
587   GST_BIN_CLASS (parent_class)->handle_message (bin, message);
590 /**
591  * gst_pipeline_get_bus:
592  * @pipeline: a #GstPipeline
593  *
594  * Gets the #GstBus of @pipeline. The bus allows applications to receive
595  * #GstMessage packets.
596  *
597  * Returns: (transfer full): a #GstBus, unref after usage.
598  *
599  * MT safe.
600  */
601 GstBus *
602 gst_pipeline_get_bus (GstPipeline * pipeline)
604   return gst_element_get_bus (GST_ELEMENT_CAST (pipeline));
607 /**
608  * gst_pipeline_set_new_stream_time:
609  * @pipeline: a #GstPipeline
610  * @time: the new running time to set
611  *
612  * Set the new start time of @pipeline to @time. The start time is used to
613  * set the base time on the elements (see gst_element_set_base_time())
614  * in the PAUSED->PLAYING state transition.
615  *
616  * Setting @time to #GST_CLOCK_TIME_NONE will disable the pipeline's management
617  * of element base time. The application will then be responsible for
618  * performing base time distribution. This is sometimes useful if you want to
619  * synchronize capture from multiple pipelines, and you can also ensure that the
620  * pipelines have the same clock.
621  *
622  * MT safe.
623  *
624  * Deprecated: This function has the wrong name and is equivalent to
625  * gst_element_set_start_time(). 
626  */
627 #ifndef GST_REMOVE_DEPRECATED
628 #ifdef GST_DISABLE_DEPRECATED
629 void
630 gst_pipeline_set_new_stream_time (GstPipeline * pipeline, GstClockTime time);
631 #endif
632 void
633 gst_pipeline_set_new_stream_time (GstPipeline * pipeline, GstClockTime time)
635   g_return_if_fail (GST_IS_PIPELINE (pipeline));
637   gst_element_set_start_time (GST_ELEMENT_CAST (pipeline), time);
639   if (time == GST_CLOCK_TIME_NONE)
640     GST_DEBUG_OBJECT (pipeline, "told not to adjust base_time");
642 #endif /* GST_REMOVE_DEPRECATED */
644 /**
645  * gst_pipeline_get_last_stream_time:
646  * @pipeline: a #GstPipeline
647  *
648  * Gets the last running time of @pipeline. If the pipeline is PLAYING,
649  * the returned time is the running time used to configure the element's
650  * base time in the PAUSED->PLAYING state. If the pipeline is PAUSED, the
651  * returned time is the running time when the pipeline was paused.
652  *
653  * This function returns #GST_CLOCK_TIME_NONE if the pipeline was
654  * configured to not handle the management of the element's base time
655  * (see gst_pipeline_set_new_stream_time()).
656  *
657  * MT safe.
658  *
659  * Returns: a #GstClockTime.
660  *
661  * Deprecated: This function has the wrong name and is equivalent to
662  * gst_element_get_start_time(). 
663  */
664 #ifndef GST_REMOVE_DEPRECATED
665 #ifdef GST_DISABLE_DEPRECATED
666 GstClockTime gst_pipeline_get_last_stream_time (GstPipeline * pipeline);
667 #endif
668 GstClockTime
669 gst_pipeline_get_last_stream_time (GstPipeline * pipeline)
671   GstClockTime result;
673   g_return_val_if_fail (GST_IS_PIPELINE (pipeline), GST_CLOCK_TIME_NONE);
675   result = gst_element_get_start_time (GST_ELEMENT_CAST (pipeline));
677   return result;
679 #endif /* GST_REMOVE_DEPRECATED */
681 static GstClock *
682 gst_pipeline_provide_clock_func (GstElement * element)
684   GstClock *clock = NULL;
685   GstPipeline *pipeline = GST_PIPELINE (element);
687   /* if we have a fixed clock, use that one */
688   GST_OBJECT_LOCK (pipeline);
689   if (GST_OBJECT_FLAG_IS_SET (pipeline, GST_PIPELINE_FLAG_FIXED_CLOCK)) {
690     clock = pipeline->fixed_clock;
691     if (clock)
692       gst_object_ref (clock);
693     GST_OBJECT_UNLOCK (pipeline);
695     GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline using fixed clock %p (%s)",
696         clock, clock ? GST_STR_NULL (GST_OBJECT_NAME (clock)) : "-");
697   } else {
698     GST_OBJECT_UNLOCK (pipeline);
699     /* let the parent bin select a clock */
700     clock =
701         GST_ELEMENT_CLASS (parent_class)->provide_clock (GST_ELEMENT
702         (pipeline));
703     /* no clock, use a system clock */
704     if (!clock) {
705       clock = gst_system_clock_obtain ();
707       GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline obtained system clock: %p (%s)",
708           clock, clock ? GST_STR_NULL (GST_OBJECT_NAME (clock)) : "-");
709     } else {
710       GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline obtained clock: %p (%s)",
711           clock, clock ? GST_STR_NULL (GST_OBJECT_NAME (clock)) : "-");
712     }
713   }
714   return clock;
717 /**
718  * gst_pipeline_get_clock:
719  * @pipeline: a #GstPipeline
720  *
721  * Gets the current clock used by @pipeline.
722  *
723  * Returns: (transfer full): a #GstClock, unref after usage.
724  */
725 GstClock *
726 gst_pipeline_get_clock (GstPipeline * pipeline)
728   g_return_val_if_fail (GST_IS_PIPELINE (pipeline), NULL);
730   return gst_pipeline_provide_clock_func (GST_ELEMENT_CAST (pipeline));
734 /**
735  * gst_pipeline_use_clock:
736  * @pipeline: a #GstPipeline
737  * @clock: (transfer none): the clock to use
738  *
739  * Force @pipeline to use the given @clock. The pipeline will
740  * always use the given clock even if new clock providers are added
741  * to this pipeline.
742  *
743  * If @clock is NULL all clocking will be disabled which will make
744  * the pipeline run as fast as possible.
745  *
746  * MT safe.
747  */
748 void
749 gst_pipeline_use_clock (GstPipeline * pipeline, GstClock * clock)
751   GstClock **clock_p;
753   g_return_if_fail (GST_IS_PIPELINE (pipeline));
755   GST_OBJECT_LOCK (pipeline);
756   GST_OBJECT_FLAG_SET (pipeline, GST_PIPELINE_FLAG_FIXED_CLOCK);
758   clock_p = &pipeline->fixed_clock;
759   gst_object_replace ((GstObject **) clock_p, (GstObject *) clock);
760   GST_OBJECT_UNLOCK (pipeline);
762   GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline using fixed clock %p (%s)", clock,
763       (clock ? GST_OBJECT_NAME (clock) : "nil"));
766 /**
767  * gst_pipeline_set_clock:
768  * @pipeline: a #GstPipeline
769  * @clock: (transfer none): the clock to set
770  *
771  * Set the clock for @pipeline. The clock will be distributed
772  * to all the elements managed by the pipeline.
773  *
774  * Returns: TRUE if the clock could be set on the pipeline. FALSE if
775  *   some element did not accept the clock.
776  *
777  * MT safe.
778  */
779 gboolean
780 gst_pipeline_set_clock (GstPipeline * pipeline, GstClock * clock)
782   g_return_val_if_fail (pipeline != NULL, FALSE);
783   g_return_val_if_fail (GST_IS_PIPELINE (pipeline), FALSE);
785   return
786       GST_ELEMENT_CLASS (parent_class)->set_clock (GST_ELEMENT_CAST (pipeline),
787       clock);
790 /**
791  * gst_pipeline_auto_clock:
792  * @pipeline: a #GstPipeline
793  *
794  * Let @pipeline select a clock automatically. This is the default
795  * behaviour.
796  *
797  * Use this function if you previous forced a fixed clock with
798  * gst_pipeline_use_clock() and want to restore the default
799  * pipeline clock selection algorithm.
800  *
801  * MT safe.
802  */
803 void
804 gst_pipeline_auto_clock (GstPipeline * pipeline)
806   GstClock **clock_p;
808   g_return_if_fail (pipeline != NULL);
809   g_return_if_fail (GST_IS_PIPELINE (pipeline));
811   GST_OBJECT_LOCK (pipeline);
812   GST_OBJECT_FLAG_UNSET (pipeline, GST_PIPELINE_FLAG_FIXED_CLOCK);
814   clock_p = &pipeline->fixed_clock;
815   gst_object_replace ((GstObject **) clock_p, NULL);
816   GST_OBJECT_UNLOCK (pipeline);
818   GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline using automatic clock");
821 /**
822  * gst_pipeline_set_delay:
823  * @pipeline: a #GstPipeline
824  * @delay: the delay
825  *
826  * Set the expected delay needed for all elements to perform the
827  * PAUSED to PLAYING state change. @delay will be added to the
828  * base time of the elements so that they wait an additional @delay
829  * amount of time before starting to process buffers and cannot be
830  * #GST_CLOCK_TIME_NONE.
831  *
832  * This option is used for tuning purposes and should normally not be
833  * used.
834  *
835  * MT safe.
836  *
837  * Since: 0.10.5
838  */
839 void
840 gst_pipeline_set_delay (GstPipeline * pipeline, GstClockTime delay)
842   g_return_if_fail (GST_IS_PIPELINE (pipeline));
843   g_return_if_fail (delay != GST_CLOCK_TIME_NONE);
845   GST_OBJECT_LOCK (pipeline);
846   pipeline->delay = delay;
847   GST_OBJECT_UNLOCK (pipeline);
850 /**
851  * gst_pipeline_get_delay:
852  * @pipeline: a #GstPipeline
853  *
854  * Get the configured delay (see gst_pipeline_set_delay()).
855  *
856  * Returns: The configured delay.
857  *
858  * MT safe.
859  *
860  * Since: 0.10.5
861  */
862 GstClockTime
863 gst_pipeline_get_delay (GstPipeline * pipeline)
865   GstClockTime res;
867   g_return_val_if_fail (GST_IS_PIPELINE (pipeline), GST_CLOCK_TIME_NONE);
869   GST_OBJECT_LOCK (pipeline);
870   res = pipeline->delay;
871   GST_OBJECT_UNLOCK (pipeline);
873   return res;
876 /**
877  * gst_pipeline_set_auto_flush_bus:
878  * @pipeline: a #GstPipeline
879  * @auto_flush: whether or not to automatically flush the bus when
880  * the pipeline goes from READY to NULL state
881  *
882  * Usually, when a pipeline goes from READY to NULL state, it automatically
883  * flushes all pending messages on the bus, which is done for refcounting
884  * purposes, to break circular references.
885  *
886  * This means that applications that update state using (async) bus messages
887  * (e.g. do certain things when a pipeline goes from PAUSED to READY) might
888  * not get to see messages when the pipeline is shut down, because they might
889  * be flushed before they can be dispatched in the main thread. This behaviour
890  * can be disabled using this function.
891  *
892  * It is important that all messages on the bus are handled when the
893  * automatic flushing is disabled else memory leaks will be introduced.
894  *
895  * MT safe.
896  *
897  * Since: 0.10.4
898  */
899 void
900 gst_pipeline_set_auto_flush_bus (GstPipeline * pipeline, gboolean auto_flush)
902   g_return_if_fail (GST_IS_PIPELINE (pipeline));
904   GST_OBJECT_LOCK (pipeline);
905   pipeline->priv->auto_flush_bus = auto_flush;
906   GST_OBJECT_UNLOCK (pipeline);
909 /**
910  * gst_pipeline_get_auto_flush_bus:
911  * @pipeline: a #GstPipeline
912  *
913  * Check if @pipeline will automatically flush messages when going to
914  * the NULL state.
915  *
916  * Returns: whether the pipeline will automatically flush its bus when
917  * going from READY to NULL state or not.
918  *
919  * MT safe.
920  *
921  * Since: 0.10.4
922  */
923 gboolean
924 gst_pipeline_get_auto_flush_bus (GstPipeline * pipeline)
926   gboolean res;
928   g_return_val_if_fail (GST_IS_PIPELINE (pipeline), FALSE);
930   GST_OBJECT_LOCK (pipeline);
931   res = pipeline->priv->auto_flush_bus;
932   GST_OBJECT_UNLOCK (pipeline);
934   return res;