1 /* GStreamer
2 * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3 * 2004,2005 Wim Taymans <wim@fluendo.com>
4 *
5 * gstpipeline.c: Overall pipeline management element
6 *
7 * This library is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU Library General Public
9 * License as published by the Free Software Foundation; either
10 * version 2 of the License, or (at your option) any later version.
11 *
12 * This library is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
15 * Library General Public License for more details.
16 *
17 * You should have received a copy of the GNU Library General Public
18 * License along with this library; if not, write to the
19 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20 * Boston, MA 02111-1307, USA.
21 */
22 /**
23 * SECTION:gstpipeline
24 * @short_description: Top-level bin with scheduling and pipeline management functionality.
25 * @see_also: #GstBin
26 *
27 * In almost all cases, you'll want to use a GstPipeline when creating a filter
28 * graph. The GstPipeline will manage all the scheduling issues, including
29 * threading, as well as provide simple interfaces to common functions, like
30 * 'Play'.
31 *
32 * gst_pipeline_new() is used to create a pipeline. when you are done with
33 * the pipeline, use gst_object_unref() to free its resources including all
34 * added #GstElement objects (if not otherwiese referenced).
35 */
37 #include "gst_private.h"
39 #include "gstpipeline.h"
40 #include "gstinfo.h"
41 #include "gstsystemclock.h"
43 static GstElementDetails gst_pipeline_details =
44 GST_ELEMENT_DETAILS ("Pipeline object",
45 "Generic/Bin",
46 "Complete pipeline object",
47 "Erik Walthinsen <omega@cse.ogi.edu>, Wim Taymans <wim@fluendo.com>");
49 /* Pipeline signals and args */
50 enum
51 {
52 /* FILL ME */
53 LAST_SIGNAL
54 };
56 #define DEFAULT_DELAY 0
57 #define DEFAULT_PLAY_TIMEOUT (2*GST_SECOND)
58 enum
59 {
60 ARG_0,
61 ARG_DELAY,
62 ARG_PLAY_TIMEOUT,
63 /* FILL ME */
64 };
67 static void gst_pipeline_base_init (gpointer g_class);
68 static void gst_pipeline_class_init (gpointer g_class, gpointer class_data);
69 static void gst_pipeline_init (GTypeInstance * instance, gpointer g_class);
71 static void gst_pipeline_dispose (GObject * object);
72 static void gst_pipeline_set_property (GObject * object, guint prop_id,
73 const GValue * value, GParamSpec * pspec);
74 static void gst_pipeline_get_property (GObject * object, guint prop_id,
75 GValue * value, GParamSpec * pspec);
77 static gboolean gst_pipeline_send_event (GstElement * element,
78 GstEvent * event);
80 static GstClock *gst_pipeline_get_clock_func (GstElement * element);
81 static GstStateChangeReturn gst_pipeline_change_state (GstElement * element,
82 GstStateChange transition);
84 static GstBinClass *parent_class = NULL;
86 /* static guint gst_pipeline_signals[LAST_SIGNAL] = { 0 }; */
88 GType
89 gst_pipeline_get_type (void)
90 {
91 static GType pipeline_type = 0;
93 if (!pipeline_type) {
94 static const GTypeInfo pipeline_info = {
95 sizeof (GstPipelineClass),
96 gst_pipeline_base_init,
97 NULL,
98 (GClassInitFunc) gst_pipeline_class_init,
99 NULL,
100 NULL,
101 sizeof (GstPipeline),
102 0,
103 gst_pipeline_init,
104 NULL
105 };
107 pipeline_type =
108 g_type_register_static (GST_TYPE_BIN, "GstPipeline", &pipeline_info, 0);
109 }
110 return pipeline_type;
111 }
113 static void
114 gst_pipeline_base_init (gpointer g_class)
115 {
116 GstElementClass *gstelement_class = GST_ELEMENT_CLASS (g_class);
118 gst_element_class_set_details (gstelement_class, &gst_pipeline_details);
119 }
121 static void
122 gst_pipeline_class_init (gpointer g_class, gpointer class_data)
123 {
124 GObjectClass *gobject_class = G_OBJECT_CLASS (g_class);
125 GstElementClass *gstelement_class = GST_ELEMENT_CLASS (g_class);
126 GstPipelineClass *klass = GST_PIPELINE_CLASS (g_class);
128 parent_class = g_type_class_peek_parent (klass);
130 gobject_class->set_property = GST_DEBUG_FUNCPTR (gst_pipeline_set_property);
131 gobject_class->get_property = GST_DEBUG_FUNCPTR (gst_pipeline_get_property);
133 g_object_class_install_property (G_OBJECT_CLASS (klass), ARG_DELAY,
134 g_param_spec_uint64 ("delay", "Delay",
135 "Expected delay needed for elements "
136 "to spin up to PLAYING in nanoseconds", 0, G_MAXUINT64, DEFAULT_DELAY,
137 G_PARAM_READWRITE));
138 g_object_class_install_property (G_OBJECT_CLASS (klass), ARG_PLAY_TIMEOUT,
139 g_param_spec_uint64 ("play-timeout", "Play Timeout",
140 "Max timeout for going to PLAYING in nanoseconds", 0, G_MAXUINT64,
141 DEFAULT_PLAY_TIMEOUT, G_PARAM_READWRITE));
143 gobject_class->dispose = GST_DEBUG_FUNCPTR (gst_pipeline_dispose);
145 gstelement_class->send_event = GST_DEBUG_FUNCPTR (gst_pipeline_send_event);
146 gstelement_class->change_state =
147 GST_DEBUG_FUNCPTR (gst_pipeline_change_state);
148 gstelement_class->get_clock = GST_DEBUG_FUNCPTR (gst_pipeline_get_clock_func);
149 }
151 static void
152 gst_pipeline_init (GTypeInstance * instance, gpointer g_class)
153 {
154 GstPipeline *pipeline = GST_PIPELINE (instance);
156 pipeline->delay = DEFAULT_DELAY;
157 pipeline->play_timeout = DEFAULT_PLAY_TIMEOUT;
158 }
160 static void
161 gst_pipeline_dispose (GObject * object)
162 {
163 GstPipeline *pipeline = GST_PIPELINE (object);
165 GST_CAT_DEBUG_OBJECT (GST_CAT_REFCOUNTING, pipeline, "dispose");
167 gst_object_replace ((GstObject **) & pipeline->fixed_clock, NULL);
169 G_OBJECT_CLASS (parent_class)->dispose (object);
170 }
172 static void
173 gst_pipeline_set_property (GObject * object, guint prop_id,
174 const GValue * value, GParamSpec * pspec)
175 {
176 GstPipeline *pipeline = GST_PIPELINE (object);
178 GST_LOCK (pipeline);
179 switch (prop_id) {
180 case ARG_DELAY:
181 pipeline->delay = g_value_get_uint64 (value);
182 break;
183 case ARG_PLAY_TIMEOUT:
184 pipeline->play_timeout = g_value_get_uint64 (value);
185 break;
186 default:
187 G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
188 break;
189 }
190 GST_UNLOCK (pipeline);
191 }
193 static void
194 gst_pipeline_get_property (GObject * object, guint prop_id,
195 GValue * value, GParamSpec * pspec)
196 {
197 GstPipeline *pipeline = GST_PIPELINE (object);
199 GST_LOCK (pipeline);
200 switch (prop_id) {
201 case ARG_DELAY:
202 g_value_set_uint64 (value, pipeline->delay);
203 break;
204 case ARG_PLAY_TIMEOUT:
205 g_value_set_uint64 (value, pipeline->play_timeout);
206 break;
207 default:
208 G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
209 break;
210 }
211 GST_UNLOCK (pipeline);
212 }
214 static gboolean
215 do_pipeline_seek (GstElement * element, GstEvent * event)
216 {
217 gdouble rate;
218 GstSeekFlags flags;
219 gboolean flush;
220 gboolean was_playing = FALSE;
221 gboolean res;
223 gst_event_parse_seek (event, &rate, NULL, &flags, NULL, NULL, NULL, NULL);
225 flush = flags & GST_SEEK_FLAG_FLUSH;
227 if (flush) {
228 GstState state;
229 GTimeVal timeout;
231 GST_TIME_TO_TIMEVAL (0, timeout);
232 /* need to call _get_state() since a bin state is only updated
233 * with this call. */
234 gst_element_get_state (element, &state, NULL, &timeout);
235 was_playing = state == GST_STATE_PLAYING;
237 if (was_playing)
238 gst_element_set_state (element, GST_STATE_PAUSED);
239 }
241 res = GST_ELEMENT_CLASS (parent_class)->send_event (element, event);
243 if (flush && res) {
244 /* need to reset the stream time to 0 after a flushing seek */
245 gst_pipeline_set_new_stream_time (GST_PIPELINE (element), 0);
246 if (was_playing) {
247 /* and continue playing */
248 gst_element_set_state (element, GST_STATE_PLAYING);
249 }
250 }
251 return res;
252 }
254 /* sending a seek event on the pipeline pauses the pipeline if it
255 * was playing.
256 */
257 static gboolean
258 gst_pipeline_send_event (GstElement * element, GstEvent * event)
259 {
260 gboolean res;
261 GstEventType event_type = GST_EVENT_TYPE (event);
263 switch (event_type) {
264 case GST_EVENT_SEEK:
265 res = do_pipeline_seek (element, event);
266 break;
267 default:
268 res = GST_ELEMENT_CLASS (parent_class)->send_event (element, event);
269 break;
270 }
272 return res;
273 }
275 /**
276 * gst_pipeline_new:
277 * @name: name of new pipeline
278 *
279 * Create a new pipeline with the given name.
280 *
281 * Returns: newly created GstPipeline
282 *
283 * MT safe.
284 */
285 GstElement *
286 gst_pipeline_new (const gchar * name)
287 {
288 return gst_element_factory_make ("pipeline", name);
289 }
291 /* MT safe */
292 static GstStateChangeReturn
293 gst_pipeline_change_state (GstElement * element, GstStateChange transition)
294 {
295 GstStateChangeReturn result = GST_STATE_CHANGE_SUCCESS;
296 GstPipeline *pipeline = GST_PIPELINE (element);
297 GstClockTime play_timeout;
298 GstClock *clock;
300 switch (transition) {
301 case GST_STATE_CHANGE_NULL_TO_READY:
302 GST_LOCK (element);
303 if (element->bus)
304 gst_bus_set_flushing (element->bus, FALSE);
305 GST_UNLOCK (element);
306 break;
307 case GST_STATE_CHANGE_READY_TO_PAUSED:
308 break;
309 case GST_STATE_CHANGE_PAUSED_TO_PLAYING:
310 /* when going to playing, select a clock */
311 if ((clock = gst_element_get_clock (element))) {
312 GstClockTime start_time;
314 /* distribute the clock */
315 gst_element_set_clock (element, clock);
317 /* get start time */
318 start_time = gst_clock_get_time (clock);
319 gst_object_unref (clock);
321 GST_LOCK (element);
322 element->base_time = start_time -
323 pipeline->stream_time + pipeline->delay;
324 GST_DEBUG ("stream_time=%" GST_TIME_FORMAT ", start_time=%"
325 GST_TIME_FORMAT ", base time %" GST_TIME_FORMAT,
326 GST_TIME_ARGS (pipeline->stream_time),
327 GST_TIME_ARGS (start_time), GST_TIME_ARGS (element->base_time));
328 GST_UNLOCK (element);
329 } else {
330 GST_DEBUG ("no clock, using base time of 0");
331 gst_element_set_base_time (element, 0);
332 }
333 break;
334 case GST_STATE_CHANGE_PLAYING_TO_PAUSED:
335 case GST_STATE_CHANGE_PAUSED_TO_READY:
336 case GST_STATE_CHANGE_READY_TO_NULL:
337 break;
338 }
340 result = GST_ELEMENT_CLASS (parent_class)->change_state (element, transition);
342 switch (transition) {
343 case GST_STATE_CHANGE_NULL_TO_READY:
344 break;
345 case GST_STATE_CHANGE_READY_TO_PAUSED:
346 gst_pipeline_set_new_stream_time (pipeline, 0);
347 break;
348 case GST_STATE_CHANGE_PAUSED_TO_PLAYING:
349 break;
350 case GST_STATE_CHANGE_PLAYING_TO_PAUSED:
351 GST_LOCK (element);
352 if ((clock = element->clock)) {
353 GstClockTime now;
355 gst_object_ref (clock);
356 GST_UNLOCK (element);
358 /* calculate the time when we stopped */
359 now = gst_clock_get_time (clock);
360 gst_object_unref (clock);
362 GST_LOCK (element);
363 /* store the current stream time */
364 pipeline->stream_time = now - element->base_time;
365 GST_DEBUG ("stream_time=%" GST_TIME_FORMAT ", now=%" GST_TIME_FORMAT
366 ", base time %" GST_TIME_FORMAT,
367 GST_TIME_ARGS (pipeline->stream_time),
368 GST_TIME_ARGS (now), GST_TIME_ARGS (element->base_time));
369 }
370 GST_UNLOCK (element);
371 break;
372 case GST_STATE_CHANGE_PAUSED_TO_READY:
373 break;
374 case GST_STATE_CHANGE_READY_TO_NULL:
375 GST_LOCK (element);
376 if (element->bus) {
377 gst_bus_set_flushing (element->bus, TRUE);
378 }
379 GST_UNLOCK (element);
380 break;
381 }
383 if (result == GST_STATE_CHANGE_ASYNC) {
384 GST_LOCK (pipeline);
385 play_timeout = pipeline->play_timeout;
386 GST_UNLOCK (pipeline);
387 } else {
388 play_timeout = 0;
389 }
391 /* we wait for async state changes ourselves when we are in an
392 * intermediate state. */
393 if (play_timeout > 0) {
394 GTimeVal *timeval, timeout;
396 GST_STATE_UNLOCK (pipeline);
398 if (play_timeout == G_MAXUINT64) {
399 timeval = NULL;
400 } else {
401 GST_TIME_TO_TIMEVAL (play_timeout, timeout);
402 timeval = &timeout;
403 }
405 result = gst_element_get_state (element, NULL, NULL, timeval);
406 if (result == GST_STATE_CHANGE_ASYNC) {
407 GST_WARNING_OBJECT (pipeline,
408 "timeout in PREROLL, forcing next state change");
409 g_warning ("timeout in PREROLL, forcing next state change");
410 result = GST_STATE_CHANGE_SUCCESS;
411 }
413 GST_STATE_LOCK (pipeline);
414 }
416 return result;
417 }
419 /**
420 * gst_pipeline_get_bus:
421 * @pipeline: the pipeline
422 *
423 * Gets the #GstBus of this pipeline.
424 *
425 * Returns: a GstBus
426 *
427 * MT safe.
428 */
429 GstBus *
430 gst_pipeline_get_bus (GstPipeline * pipeline)
431 {
432 return gst_element_get_bus (GST_ELEMENT (pipeline));
433 }
435 /**
436 * gst_pipeline_set_new_stream_time:
437 * @pipeline: the pipeline
438 * @time: the new stream time to set
439 *
440 * Set the new stream time of the pipeline. The stream time is used to
441 * set the base time on the elements (see @gst_element_set_base_time())
442 * in the PAUSED->PLAYING state transition.
443 *
444 * MT safe.
445 */
446 void
447 gst_pipeline_set_new_stream_time (GstPipeline * pipeline, GstClockTime time)
448 {
449 g_return_if_fail (GST_IS_PIPELINE (pipeline));
451 GST_LOCK (pipeline);
452 pipeline->stream_time = time;
453 GST_DEBUG ("%s: set new stream_time to %" GST_TIME_FORMAT,
454 GST_ELEMENT_NAME (pipeline), GST_TIME_ARGS (time));
455 GST_UNLOCK (pipeline);
456 }
458 /**
459 * gst_pipeline_get_last_stream_time:
460 * @pipeline: the pipeline
461 *
462 * Gets the last stream time of the pipeline. If the pipeline is PLAYING,
463 * the returned time is the stream time used to configure the elements
464 * in the PAUSED->PLAYING state. If the pipeline is PAUSED, the returned
465 * time is the stream time when the pipeline was paused.
466 *
467 * Returns: a GstClockTime
468 *
469 * MT safe.
470 */
471 GstClockTime
472 gst_pipeline_get_last_stream_time (GstPipeline * pipeline)
473 {
474 GstClockTime result;
476 g_return_val_if_fail (GST_IS_PIPELINE (pipeline), GST_CLOCK_TIME_NONE);
478 GST_LOCK (pipeline);
479 result = pipeline->stream_time;
480 GST_UNLOCK (pipeline);
482 return result;
483 }
485 static GstClock *
486 gst_pipeline_get_clock_func (GstElement * element)
487 {
488 GstClock *clock = NULL;
489 GstPipeline *pipeline = GST_PIPELINE (element);
491 /* if we have a fixed clock, use that one */
492 GST_LOCK (pipeline);
493 if (GST_FLAG_IS_SET (pipeline, GST_PIPELINE_FLAG_FIXED_CLOCK)) {
494 clock = pipeline->fixed_clock;
495 gst_object_ref (clock);
496 GST_UNLOCK (pipeline);
498 GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline using fixed clock %p (%s)",
499 clock, clock ? GST_STR_NULL (GST_OBJECT_NAME (clock)) : "-");
500 } else {
501 GST_UNLOCK (pipeline);
502 clock =
503 GST_ELEMENT_CLASS (parent_class)->get_clock (GST_ELEMENT (pipeline));
504 /* no clock, use a system clock */
505 if (!clock) {
506 clock = gst_system_clock_obtain ();
508 GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline obtained system clock: %p (%s)",
509 clock, clock ? GST_STR_NULL (GST_OBJECT_NAME (clock)) : "-");
510 } else {
511 GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline obtained clock: %p (%s)",
512 clock, clock ? GST_STR_NULL (GST_OBJECT_NAME (clock)) : "-");
513 }
514 }
515 return clock;
516 }
518 /**
519 * gst_pipeline_get_clock:
520 * @pipeline: the pipeline
521 *
522 * Gets the current clock used by the pipeline.
523 *
524 * Returns: a GstClock
525 */
526 GstClock *
527 gst_pipeline_get_clock (GstPipeline * pipeline)
528 {
529 g_return_val_if_fail (GST_IS_PIPELINE (pipeline), NULL);
531 return gst_pipeline_get_clock_func (GST_ELEMENT (pipeline));
532 }
535 /**
536 * gst_pipeline_use_clock:
537 * @pipeline: the pipeline
538 * @clock: the clock to use
539 *
540 * Force the pipeline to use the given clock. The pipeline will
541 * always use the given clock even if new clock providers are added
542 * to this pipeline.
543 *
544 * MT safe.
545 */
546 void
547 gst_pipeline_use_clock (GstPipeline * pipeline, GstClock * clock)
548 {
549 g_return_if_fail (GST_IS_PIPELINE (pipeline));
551 GST_LOCK (pipeline);
552 GST_FLAG_SET (pipeline, GST_PIPELINE_FLAG_FIXED_CLOCK);
554 gst_object_replace ((GstObject **) & pipeline->fixed_clock,
555 (GstObject *) clock);
556 GST_UNLOCK (pipeline);
558 GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline using fixed clock %p (%s)", clock,
559 (clock ? GST_OBJECT_NAME (clock) : "nil"));
560 }
562 /**
563 * gst_pipeline_set_clock:
564 * @pipeline: the pipeline
565 * @clock: the clock to set
566 *
567 * Set the clock for the pipeline. The clock will be distributed
568 * to all the elements managed by the pipeline.
569 *
570 * MT safe.
571 */
572 void
573 gst_pipeline_set_clock (GstPipeline * pipeline, GstClock * clock)
574 {
575 g_return_if_fail (pipeline != NULL);
576 g_return_if_fail (GST_IS_PIPELINE (pipeline));
578 GST_ELEMENT_CLASS (parent_class)->set_clock (GST_ELEMENT (pipeline), clock);
579 }
581 /**
582 * gst_pipeline_auto_clock:
583 * @pipeline: the pipeline
584 *
585 * Let the pipeline select a clock automatically.
586 *
587 * MT safe.
588 */
589 void
590 gst_pipeline_auto_clock (GstPipeline * pipeline)
591 {
592 g_return_if_fail (pipeline != NULL);
593 g_return_if_fail (GST_IS_PIPELINE (pipeline));
595 GST_LOCK (pipeline);
596 GST_FLAG_UNSET (pipeline, GST_PIPELINE_FLAG_FIXED_CLOCK);
598 gst_object_replace ((GstObject **) & pipeline->fixed_clock, NULL);
599 GST_UNLOCK (pipeline);
601 GST_CAT_DEBUG (GST_CAT_CLOCK, "pipeline using automatic clock");
602 }