]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blob - gst/gstquery.h
Changes to make it possible to LD_PRELOAD libttif
[glsdk/gstreamer0-10.git] / gst / gstquery.h
1 /* GStreamer
2  * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3  *                    2000 Wim Taymans <wim.taymans@chello.be>
4  *                    2005 Wim Taymans <wim@fluendo.com>
5  *
6  * gstquery.h: GstQuery API declaration
7  *
8  * This library is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU Library General Public
10  * License as published by the Free Software Foundation; either
11  * version 2 of the License, or (at your option) any later version.
12  *
13  * This library is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
16  * Library General Public License for more details.
17  *
18  * You should have received a copy of the GNU Library General Public
19  * License along with this library; if not, write to the
20  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
21  * Boston, MA 02111-1307, USA.
22  */
25 #ifndef __GST_QUERY_H__
26 #define __GST_QUERY_H__
28 #include <glib.h>
30 #include <gst/gstiterator.h>
31 #include <gst/gstminiobject.h>
32 #include <gst/gststructure.h>
33 #include <gst/gstformat.h>
35 G_BEGIN_DECLS
37 /**
38  * GstQueryType:
39  * @GST_QUERY_NONE: invalid query type
40  * @GST_QUERY_POSITION: current position in stream
41  * @GST_QUERY_DURATION: total duration of the stream
42  * @GST_QUERY_LATENCY: latency of stream
43  * @GST_QUERY_JITTER: current jitter of stream
44  * @GST_QUERY_RATE: current rate of the stream
45  * @GST_QUERY_SEEKING: seeking capabilities
46  * @GST_QUERY_SEGMENT: segment start/stop positions
47  * @GST_QUERY_CONVERT: convert values between formats
48  * @GST_QUERY_FORMATS: query supported formats for convert
49  * @GST_QUERY_BUFFERING: query available media for efficient seeking. Since
50  * 0.10.20.
51  * @GST_QUERY_CUSTOM: a custom application or element defined query. Since
52  * 0.10.22.
53  * @GST_QUERY_URI: query the URI of the source or sink. Since 0.10.22.
54  *
55  * Standard predefined Query types
56  */
57 /* NOTE: don't forget to update the table in gstquery.c when changing
58  * this enum */
59 typedef enum {
60   GST_QUERY_NONE = 0,
61   GST_QUERY_POSITION,
62   GST_QUERY_DURATION,
63   GST_QUERY_LATENCY,
64   GST_QUERY_JITTER,     /* not in draft-query, necessary? */
65   GST_QUERY_RATE,
66   GST_QUERY_SEEKING,
67   GST_QUERY_SEGMENT,
68   GST_QUERY_CONVERT,
69   GST_QUERY_FORMATS,
70   GST_QUERY_BUFFERING,
71   GST_QUERY_CUSTOM,
72   GST_QUERY_URI
73 } GstQueryType;
75 /**
76  * GstBufferingMode:
77  * @GST_BUFFERING_STREAM: a small amount of data is buffered
78  * @GST_BUFFERING_DOWNLOAD: the stream is being downloaded
79  * @GST_BUFFERING_TIMESHIFT: the stream is being downloaded in a ringbuffer
80  * @GST_BUFFERING_LIVE: the stream is a live stream
81  *
82  * The different types of buffering methods.
83  */
84 typedef enum {
85   GST_BUFFERING_STREAM,
86   GST_BUFFERING_DOWNLOAD,
87   GST_BUFFERING_TIMESHIFT,
88   GST_BUFFERING_LIVE
89 } GstBufferingMode;
91 typedef struct _GstQueryTypeDefinition GstQueryTypeDefinition;
92 typedef struct _GstQuery GstQuery;
93 typedef struct _GstQueryClass GstQueryClass;
95 /**
96  * GstQueryTypeDefinition:
97  * @value: the unique id of the Query type
98  * @nick: a short nick
99  * @description: a longer description of the query type
100  * @quark: the quark for the nick
101  *
102  * A Query Type definition
103  */
104 struct _GstQueryTypeDefinition
106   GstQueryType   value;
107   const gchar   *nick;
108   const gchar   *description;
109   GQuark         quark;
110 };
112 #define GST_TYPE_QUERY                          (gst_query_get_type())
113 #define GST_IS_QUERY(obj)                      (G_TYPE_CHECK_INSTANCE_TYPE ((obj), GST_TYPE_QUERY))
114 #define GST_IS_QUERY_CLASS(klass)              (G_TYPE_CHECK_CLASS_TYPE ((klass), GST_TYPE_QUERY))
115 #define GST_QUERY_GET_CLASS(obj)               (G_TYPE_INSTANCE_GET_CLASS ((obj), GST_TYPE_QUERY, GstQueryClass))
116 #define GST_QUERY(obj)                         (G_TYPE_CHECK_INSTANCE_CAST ((obj), GST_TYPE_QUERY, GstQuery))
117 #define GST_QUERY_CAST(obj)                    ((GstQuery*)(obj)) /* only since 0.10.23 */
118 #define GST_QUERY_CLASS(klass)                 (G_TYPE_CHECK_CLASS_CAST ((klass), GST_TYPE_QUERY, GstQueryClass))
121 /**
122  * GST_QUERY_TYPE:
123  * @query: the query to query
124  *
125  * Get the #GstQueryType of the query.
126  */
127 #define GST_QUERY_TYPE(query)  (((GstQuery*)(query))->type)
129 /**
130  * GST_QUERY_TYPE_NAME:
131  * @query: the query to query
132  *
133  * Get a constant string representation of the #GstQueryType of the query.
134  *
135  * Since: 0.10.4
136  */
137 #define GST_QUERY_TYPE_NAME(query) (gst_query_type_get_name(GST_QUERY_TYPE(query)))
140 /**
141  * GstQuery:
142  * @mini_object: The parent #GstMiniObject type
143  * @type: the #GstQueryType
144  * @structure: the #GstStructure containing the query details.
145  *
146  * The #GstQuery structure.
147  */
148 struct _GstQuery
150   GstMiniObject mini_object;
152   /*< public > *//* with COW */
153   GstQueryType type;
155   GstStructure *structure;
157   /*< private >*/
158   gpointer _gst_reserved;
159 };
161 struct _GstQueryClass {
162   GstMiniObjectClass mini_object_class;
164   /*< private >*/
165   gpointer _gst_reserved[GST_PADDING];
166 };
168 const gchar*    gst_query_type_get_name        (GstQueryType query);
169 GQuark          gst_query_type_to_quark        (GstQueryType query);
171 GType           gst_query_get_type             (void);
173 /* register a new query */
174 GstQueryType    gst_query_type_register        (const gchar *nick,
175                                                 const gchar *description);
176 GstQueryType    gst_query_type_get_by_nick     (const gchar *nick);
178 /* check if a query is in an array of querys */
179 gboolean        gst_query_types_contains       (const GstQueryType *types,
180                                                 GstQueryType type);
182 /* query for query details */
184 const GstQueryTypeDefinition*
185                 gst_query_type_get_details         (GstQueryType type);
186 GstIterator*    gst_query_type_iterate_definitions (void) G_GNUC_MALLOC;
188 /* refcounting */
189 /**
190  * gst_query_ref:
191  * @q: a #GstQuery to increase the refcount of.
192  *
193  * Increases the refcount of the given query by one.
194  *
195  * Returns: @q
196  */
197 #ifdef _FOOL_GTK_DOC_
198 G_INLINE_FUNC GstQuery * gst_query_ref (GstQuery * q);
199 #endif
201 static inline GstQuery *
202 gst_query_ref (GstQuery * q)
204   return GST_QUERY_CAST (gst_mini_object_ref (GST_MINI_OBJECT_CAST (q)));
207 /**
208  * gst_query_unref:
209  * @q: a #GstQuery to decrease the refcount of.
210  *
211  * Decreases the refcount of the query. If the refcount reaches 0, the query
212  * will be freed.
213  */
214 #ifdef _FOOL_GTK_DOC_
215 G_INLINE_FUNC void gst_query_unref (GstQuery * q);
216 #endif
218 static inline void
219 gst_query_unref (GstQuery * q)
221   gst_mini_object_unref (GST_MINI_OBJECT_CAST (q));
224 /* copy query */
225 /**
226  * gst_query_copy:
227  * @q: a #GstQuery to copy.
228  *
229  * Copies the given query using the copy function of the parent #GstStructure.
230  *
231  * Free-function: gst_query_unref
232  *
233  * Returns: (transfer full): a new copy of @q.
234  */
235 #ifdef _FOOL_GTK_DOC_
236 G_INLINE_FUNC GstQuery * gst_query_copy (const GstQuery * q);
237 #endif
239 static inline GstQuery *
240 gst_query_copy (const GstQuery * q)
242   return GST_QUERY_CAST (gst_mini_object_copy (GST_MINI_OBJECT_CONST_CAST (q)));
245 /**
246  * gst_query_make_writable:
247  * @q: (transfer full): a #GstQuery to make writable
248  *
249  * Makes a writable query from the given query.
250  *
251  * Returns: (transfer full): a new writable query (possibly same as @q)
252  */
253 #define         gst_query_make_writable(q)      GST_QUERY_CAST (gst_mini_object_make_writable (GST_MINI_OBJECT_CAST (q)))
255 /* position query */
256 GstQuery*       gst_query_new_position          (GstFormat format) G_GNUC_MALLOC;
257 void            gst_query_set_position          (GstQuery *query, GstFormat format, gint64 cur);
258 void            gst_query_parse_position        (GstQuery *query, GstFormat *format, gint64 *cur);
260 /* duration query */
261 GstQuery*       gst_query_new_duration          (GstFormat format) G_GNUC_MALLOC;
262 void            gst_query_set_duration          (GstQuery *query, GstFormat format, gint64 duration);
263 void            gst_query_parse_duration        (GstQuery *query, GstFormat *format, gint64 *duration);
265 /* latency query */
266 GstQuery*       gst_query_new_latency           (void) G_GNUC_MALLOC;
267 void            gst_query_set_latency           (GstQuery *query, gboolean live, GstClockTime min_latency,
268                                                  GstClockTime max_latency);
269 void            gst_query_parse_latency         (GstQuery *query, gboolean *live, GstClockTime *min_latency,
270                                                  GstClockTime *max_latency);
272 /* convert query */
273 GstQuery*       gst_query_new_convert           (GstFormat src_format, gint64 value, GstFormat dest_format) G_GNUC_MALLOC;
274 void            gst_query_set_convert           (GstQuery *query, GstFormat src_format, gint64 src_value,
275                                                  GstFormat dest_format, gint64 dest_value);
276 void            gst_query_parse_convert         (GstQuery *query, GstFormat *src_format, gint64 *src_value,
277                                                  GstFormat *dest_format, gint64 *dest_value);
278 /* segment query */
279 GstQuery*       gst_query_new_segment           (GstFormat format) G_GNUC_MALLOC;
280 void            gst_query_set_segment           (GstQuery *query, gdouble rate, GstFormat format,
281                                                  gint64 start_value, gint64 stop_value);
282 void            gst_query_parse_segment         (GstQuery *query, gdouble *rate, GstFormat *format,
283                                                  gint64 *start_value, gint64 *stop_value);
285 /* application specific query */
286 GstQuery *      gst_query_new_application       (GstQueryType type,
287                                                  GstStructure *structure) G_GNUC_MALLOC;
288 GstStructure *  gst_query_get_structure         (GstQuery *query);
290 /* seeking query */
291 GstQuery*       gst_query_new_seeking           (GstFormat format) G_GNUC_MALLOC;
292 void            gst_query_set_seeking           (GstQuery *query, GstFormat format,
293                                                  gboolean seekable,
294                                                  gint64 segment_start,
295                                                  gint64 segment_end);
296 void            gst_query_parse_seeking         (GstQuery *query, GstFormat *format,
297                                                  gboolean *seekable,
298                                                  gint64 *segment_start,
299                                                  gint64 *segment_end);
300 /* formats query */
301 GstQuery*       gst_query_new_formats           (void) G_GNUC_MALLOC;
302 void            gst_query_set_formats           (GstQuery *query, gint n_formats, ...);
303 void            gst_query_set_formatsv          (GstQuery *query, gint n_formats, const GstFormat *formats);
304 void            gst_query_parse_formats_length  (GstQuery *query, guint *n_formats);
305 void            gst_query_parse_formats_nth     (GstQuery *query, guint nth, GstFormat *format);
307 /* buffering query */
308 GstQuery*       gst_query_new_buffering           (GstFormat format) G_GNUC_MALLOC;
309 void            gst_query_set_buffering_percent   (GstQuery *query, gboolean busy, gint percent);
310 void            gst_query_parse_buffering_percent (GstQuery *query, gboolean *busy, gint *percent);
312 void            gst_query_set_buffering_stats     (GstQuery *query, GstBufferingMode mode,
313                                                    gint avg_in, gint avg_out,
314                                                    gint64 buffering_left);
315 void            gst_query_parse_buffering_stats    (GstQuery *query, GstBufferingMode *mode,
316                                                    gint *avg_in, gint *avg_out,
317                                                    gint64 *buffering_left);
319 void            gst_query_set_buffering_range     (GstQuery *query, GstFormat format,
320                                                    gint64 start, gint64 stop,
321                                                    gint64 estimated_total);
322 void            gst_query_parse_buffering_range   (GstQuery *query, GstFormat *format,
323                                                    gint64 *start, gint64 *stop,
324                                                    gint64 *estimated_total);
325 gboolean        gst_query_add_buffering_range     (GstQuery *query,
326                                                    gint64 start, gint64 stop);
328 guint           gst_query_get_n_buffering_ranges  (GstQuery *query);
330 gboolean        gst_query_parse_nth_buffering_range (GstQuery *query,
331                                                      guint index, gint64 *start,
332                                                      gint64 *stop);
334 /* URI query */
335 GstQuery *      gst_query_new_uri                 (void) G_GNUC_MALLOC;
336 void            gst_query_parse_uri               (GstQuery *query, gchar **uri);
337 void            gst_query_set_uri                 (GstQuery *query, const gchar *uri);
339 G_END_DECLS
341 #endif /* __GST_QUERY_H__ */