e6f6f19ec64e64fe0d219804eeb7f02b95fa603c
1 /* GStreamer
2 * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3 * 2000 Wim Taymans <wtay@chello.be>
4 * 2005 David A. Schleef <ds@schleef.org>
5 *
6 * gstregistry.c: handle registry
7 *
8 * This library is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU Library General Public
10 * License as published by the Free Software Foundation; either
11 * version 2 of the License, or (at your option) any later version.
12 *
13 * This library is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
16 * Library General Public License for more details.
17 *
18 * You should have received a copy of the GNU Library General Public
19 * License along with this library; if not, write to the
20 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
21 * Boston, MA 02111-1307, USA.
22 */
24 /**
25 * SECTION:gstregistry
26 * @short_description: Abstract base class for management of #GstPlugin objects
27 * @see_also: #GstPlugin, #GstPluginFeature
28 *
29 * One registry holds the metadata of a set of plugins.
30 *
31 * <emphasis role="bold">Design:</emphasis>
32 *
33 * The #GstRegistry object is a list of plugins and some functions for dealing
34 * with them. Each #GstPlugin is matched 1-1 with a file on disk, and may or may
35 * not be loaded at a given time. There may be multiple #GstRegistry objects,
36 * but the "default registry" is the only object that has any meaning to the
37 * core.
38 *
39 * The registry file is actually a cache of plugin information. This is
40 * unlike versions prior to 0.10, where the registry file was the primary source
41 * of plugin information, and was created by the gst-register command.
42 *
43 * The primary source, at all times, of plugin information is each plugin file
44 * itself. Thus, if an application wants information about a particular plugin,
45 * or wants to search for a feature that satisfies given criteria, the primary
46 * means of doing so is to load every plugin and look at the resulting
47 * information that is gathered in the default registry. Clearly, this is a time
48 * consuming process, so we cache information in the registry file. The format
49 * and location of the cache file is internal to gstreamer.
50 *
51 * On startup, plugins are searched for in the plugin search path. The following
52 * locations are checked in this order:
53 * <itemizedlist>
54 * <listitem>
55 * <para>location from --gst-plugin-path commandline option.</para>
56 * </listitem>
57 * <listitem>
58 * <para>the GST_PLUGIN_PATH environment variable.</para>
59 * </listitem>
60 * <listitem>
61 * <para>the GST_PLUGIN_SYSTEM_PATH environment variable.</para>
62 * </listitem>
63 * <listitem>
64 * <para>default locations (if GST_PLUGIN_SYSTEM_PATH is not set). Those
65 * default locations are:
66 * <filename>~/.gstreamer-$GST_MAJORMINOR/plugins/</filename>
67 * and <filename>$prefix/libs/gstreamer-$GST_MAJORMINOR/</filename>.
68 * </para>
69 * </listitem>
70 * </itemizedlist>
71 * The registry cache file is loaded from
72 * <filename>~/.gstreamer-$GST_MAJORMINOR/registry-$ARCH.bin</filename> or the
73 * file listed in the GST_REGISTRY env var. One reason to change the registry
74 * location is for testing.
75 *
76 * For each plugin that is found in the plugin search path, there could be 3
77 * possibilities for cached information:
78 * <itemizedlist>
79 * <listitem>
80 * <para>the cache may not contain information about a given file.</para>
81 * </listitem>
82 * <listitem>
83 * <para>the cache may have stale information.</para>
84 * </listitem>
85 * <listitem>
86 * <para>the cache may have current information.</para>
87 * </listitem>
88 * </itemizedlist>
89 *
90 * In the first two cases, the plugin is loaded and the cache updated. In
91 * addition to these cases, the cache may have entries for plugins that are not
92 * relevant to the current process. These are marked as not available to the
93 * current process. If the cache is updated for whatever reason, it is marked
94 * dirty.
95 *
96 * A dirty cache is written out at the end of initialization. Each entry is
97 * checked to make sure the information is minimally valid. If not, the entry is
98 * simply dropped.
99 *
100 * <emphasis role="bold">Implementation notes:</emphasis>
101 *
102 * The "cache" and "default registry" are different concepts and can represent
103 * different sets of plugins. For various reasons, at init time, the cache is
104 * stored in the default registry, and plugins not relevant to the current
105 * process are marked with the %GST_PLUGIN_FLAG_CACHED bit. These plugins are
106 * removed at the end of initialization.
107 */
109 #ifdef HAVE_CONFIG_H
110 #include "config.h"
111 #endif
112 #include "gstconfig.h"
113 #include "gst_private.h"
114 #include <glib.h>
115 #include <sys/types.h>
116 #include <sys/stat.h>
117 #ifdef HAVE_UNISTD_H
118 #include <unistd.h>
119 #endif
120 #include <errno.h>
121 #include <stdio.h>
122 #include <string.h>
124 /* For g_stat () */
125 #include <glib/gstdio.h>
127 #include "gstinfo.h"
128 #include "gsterror.h"
129 #include "gstregistry.h"
130 #include "gstmarshal.h"
131 #include "gstfilter.h"
133 #include "gstpluginloader.h"
135 #include "gst-i18n-lib.h"
137 #include "gst.h"
138 #include "glib-compat-private.h"
140 #ifdef G_OS_WIN32
141 #include <windows.h>
142 extern HMODULE _priv_gst_dll_handle;
143 #endif
145 #define GST_CAT_DEFAULT GST_CAT_REGISTRY
147 struct _GstRegistryPrivate
148 {
149 /* updated whenever the feature list changes */
150 guint32 cookie;
151 /* speedup for searching features */
152 GList *element_factory_list;
153 guint32 efl_cookie;
154 GList *typefind_factory_list;
155 guint32 tfl_cookie;
156 };
158 /* the one instance of the default registry and the mutex protecting the
159 * variable. */
160 static GStaticMutex _gst_registry_mutex = G_STATIC_MUTEX_INIT;
161 static GstRegistry *_gst_registry_default = NULL;
163 /* defaults */
164 #define DEFAULT_FORK TRUE
166 /* control the behaviour of registry rebuild */
167 static gboolean _gst_enable_registry_fork = DEFAULT_FORK;
168 /* List of plugins that need preloading/reloading after scanning registry */
169 extern GSList *_priv_gst_preload_plugins;
171 #ifndef GST_DISABLE_REGISTRY
172 /*set to TRUE when registry needn't to be updated */
173 gboolean _priv_gst_disable_registry_update = FALSE;
174 extern GList *_priv_gst_plugin_paths;
176 /* Set to TRUE when the registry cache should be disabled */
177 gboolean _gst_disable_registry_cache = FALSE;
179 static gboolean __registry_reuse_plugin_scanner = TRUE;
180 #endif
182 /* Element signals and args */
183 enum
184 {
185 PLUGIN_ADDED,
186 FEATURE_ADDED,
187 LAST_SIGNAL
188 };
190 static void gst_registry_finalize (GObject * object);
192 static guint gst_registry_signals[LAST_SIGNAL] = { 0 };
194 static GstPluginFeature *gst_registry_lookup_feature_locked (GstRegistry *
195 registry, const char *name);
196 static GstPlugin *gst_registry_lookup_bn_locked (GstRegistry * registry,
197 const char *basename);
199 G_DEFINE_TYPE (GstRegistry, gst_registry, GST_TYPE_OBJECT);
200 static GstObjectClass *parent_class = NULL;
202 static void
203 gst_registry_class_init (GstRegistryClass * klass)
204 {
205 GObjectClass *gobject_class;
207 gobject_class = (GObjectClass *) klass;
209 parent_class = g_type_class_peek_parent (klass);
210 g_type_class_add_private (klass, sizeof (GstRegistryPrivate));
212 /**
213 * GstRegistry::plugin-added:
214 * @registry: the registry that emitted the signal
215 * @plugin: the plugin that has been added
216 *
217 * Signals that a plugin has been added to the registry (possibly
218 * replacing a previously-added one by the same name)
219 */
220 gst_registry_signals[PLUGIN_ADDED] =
221 g_signal_new ("plugin-added", G_TYPE_FROM_CLASS (klass),
222 G_SIGNAL_RUN_LAST, G_STRUCT_OFFSET (GstRegistryClass, plugin_added), NULL,
223 NULL, gst_marshal_VOID__POINTER, G_TYPE_NONE, 1, G_TYPE_POINTER);
225 /**
226 * GstRegistry::feature-added:
227 * @registry: the registry that emitted the signal
228 * @feature: the feature that has been added
229 *
230 * Signals that a feature has been added to the registry (possibly
231 * replacing a previously-added one by the same name)
232 */
233 gst_registry_signals[FEATURE_ADDED] =
234 g_signal_new ("feature-added", G_TYPE_FROM_CLASS (klass),
235 G_SIGNAL_RUN_LAST, G_STRUCT_OFFSET (GstRegistryClass, feature_added),
236 NULL, NULL, gst_marshal_VOID__POINTER, G_TYPE_NONE, 1, G_TYPE_POINTER);
238 gobject_class->finalize = gst_registry_finalize;
239 }
241 static void
242 gst_registry_init (GstRegistry * registry)
243 {
244 registry->feature_hash = g_hash_table_new (g_str_hash, g_str_equal);
245 registry->basename_hash = g_hash_table_new (g_str_hash, g_str_equal);
246 registry->priv =
247 G_TYPE_INSTANCE_GET_PRIVATE (registry, GST_TYPE_REGISTRY,
248 GstRegistryPrivate);
249 }
251 static void
252 gst_registry_finalize (GObject * object)
253 {
254 GstRegistry *registry = GST_REGISTRY (object);
255 GList *plugins, *p;
256 GList *features, *f;
258 plugins = registry->plugins;
259 registry->plugins = NULL;
261 GST_DEBUG_OBJECT (registry, "registry finalize");
262 p = plugins;
263 while (p) {
264 GstPlugin *plugin = p->data;
266 if (plugin) {
267 GST_LOG_OBJECT (registry, "removing plugin %s",
268 gst_plugin_get_name (plugin));
269 gst_object_unref (plugin);
270 }
271 p = g_list_next (p);
272 }
273 g_list_free (plugins);
275 features = registry->features;
276 registry->features = NULL;
278 f = features;
279 while (f) {
280 GstPluginFeature *feature = f->data;
282 if (feature) {
283 GST_LOG_OBJECT (registry, "removing feature %p (%s)",
284 feature, gst_plugin_feature_get_name (feature));
285 gst_object_unparent (GST_OBJECT_CAST (feature));
286 }
287 f = g_list_next (f);
288 }
289 g_list_free (features);
291 g_hash_table_destroy (registry->feature_hash);
292 registry->feature_hash = NULL;
293 g_hash_table_destroy (registry->basename_hash);
294 registry->basename_hash = NULL;
296 if (registry->priv->element_factory_list) {
297 GST_DEBUG_OBJECT (registry, "Cleaning up cached element factory list");
298 gst_plugin_feature_list_free (registry->priv->element_factory_list);
299 }
301 if (registry->priv->typefind_factory_list) {
302 GST_DEBUG_OBJECT (registry, "Cleaning up cached typefind factory list");
303 gst_plugin_feature_list_free (registry->priv->typefind_factory_list);
304 }
306 G_OBJECT_CLASS (parent_class)->finalize (object);
307 }
309 /**
310 * gst_registry_get_default:
311 *
312 * Retrieves the default registry. The caller does not own a reference on the
313 * registry, as it is alive as long as GStreamer is initialized.
314 *
315 * Returns: (transfer none): The default #GstRegistry.
316 */
317 GstRegistry *
318 gst_registry_get_default (void)
319 {
320 GstRegistry *registry;
322 g_static_mutex_lock (&_gst_registry_mutex);
323 if (G_UNLIKELY (!_gst_registry_default)) {
324 _gst_registry_default = g_object_newv (GST_TYPE_REGISTRY, 0, NULL);
325 gst_object_ref_sink (GST_OBJECT_CAST (_gst_registry_default));
326 }
327 registry = _gst_registry_default;
328 g_static_mutex_unlock (&_gst_registry_mutex);
330 return registry;
331 }
333 /**
334 * gst_registry_add_path:
335 * @registry: the registry to add the path to
336 * @path: the path to add to the registry
337 *
338 * Add the given path to the registry. The syntax of the
339 * path is specific to the registry. If the path has already been
340 * added, do nothing.
341 */
342 void
343 gst_registry_add_path (GstRegistry * registry, const gchar * path)
344 {
345 g_return_if_fail (GST_IS_REGISTRY (registry));
346 g_return_if_fail (path != NULL);
348 if (strlen (path) == 0)
349 goto empty_path;
351 GST_OBJECT_LOCK (registry);
352 if (g_list_find_custom (registry->paths, path, (GCompareFunc) strcmp))
353 goto was_added;
355 GST_INFO ("Adding plugin path: \"%s\"", path);
356 registry->paths = g_list_append (registry->paths, g_strdup (path));
357 GST_OBJECT_UNLOCK (registry);
359 return;
361 empty_path:
362 {
363 GST_INFO ("Ignoring empty plugin path");
364 return;
365 }
366 was_added:
367 {
368 g_warning ("path %s already added to registry", path);
369 GST_OBJECT_UNLOCK (registry);
370 return;
371 }
372 }
374 /**
375 * gst_registry_get_path_list:
376 * @registry: the registry to get the pathlist of
377 *
378 * Get the list of paths for the given registry.
379 *
380 * Returns: (transfer container) (element-type char*): A #GList of paths as
381 * strings. g_list_free after use.
382 *
383 * MT safe.
384 */
385 GList *
386 gst_registry_get_path_list (GstRegistry * registry)
387 {
388 GList *list;
390 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
392 GST_OBJECT_LOCK (registry);
393 /* We don't need to copy the strings, because they won't be deleted
394 * as long as the GstRegistry is around */
395 list = g_list_copy (registry->paths);
396 GST_OBJECT_UNLOCK (registry);
398 return list;
399 }
402 /**
403 * gst_registry_add_plugin:
404 * @registry: the registry to add the plugin to
405 * @plugin: (transfer full): the plugin to add
406 *
407 * Add the plugin to the registry. The plugin-added signal will be emitted.
408 * This function will sink @plugin.
409 *
410 * Returns: TRUE on success.
411 *
412 * MT safe.
413 */
414 gboolean
415 gst_registry_add_plugin (GstRegistry * registry, GstPlugin * plugin)
416 {
417 GstPlugin *existing_plugin;
419 g_return_val_if_fail (GST_IS_REGISTRY (registry), FALSE);
420 g_return_val_if_fail (GST_IS_PLUGIN (plugin), FALSE);
422 GST_OBJECT_LOCK (registry);
423 if (G_LIKELY (plugin->basename)) {
424 /* we have a basename, see if we find the plugin */
425 existing_plugin =
426 gst_registry_lookup_bn_locked (registry, plugin->basename);
427 if (existing_plugin) {
428 GST_DEBUG_OBJECT (registry,
429 "Replacing existing plugin \"%s\" %p with new plugin %p for filename \"%s\"",
430 GST_STR_NULL (existing_plugin->filename), existing_plugin, plugin,
431 GST_STR_NULL (plugin->filename));
432 /* If the new plugin is blacklisted and the existing one isn't cached, do not
433 * accept if it's from a different location than the existing one */
434 if ((plugin->flags & GST_PLUGIN_FLAG_BLACKLISTED) &&
435 strcmp (plugin->filename, existing_plugin->filename)) {
436 GST_WARNING_OBJECT (registry,
437 "Not replacing plugin because new one (%s) is blacklisted but for a different location than existing one (%s)",
438 plugin->filename, existing_plugin->filename);
439 gst_object_unref (plugin);
440 GST_OBJECT_UNLOCK (registry);
441 return FALSE;
442 }
443 registry->plugins = g_list_remove (registry->plugins, existing_plugin);
444 if (G_LIKELY (existing_plugin->basename))
445 g_hash_table_remove (registry->basename_hash,
446 existing_plugin->basename);
447 gst_object_unref (existing_plugin);
448 }
449 }
451 GST_DEBUG_OBJECT (registry, "adding plugin %p for filename \"%s\"",
452 plugin, GST_STR_NULL (plugin->filename));
454 registry->plugins = g_list_prepend (registry->plugins, plugin);
455 if (G_LIKELY (plugin->basename))
456 g_hash_table_replace (registry->basename_hash, plugin->basename, plugin);
458 gst_object_ref_sink (plugin);
459 GST_OBJECT_UNLOCK (registry);
461 GST_LOG_OBJECT (registry, "emitting plugin-added for filename \"%s\"",
462 GST_STR_NULL (plugin->filename));
463 g_signal_emit (registry, gst_registry_signals[PLUGIN_ADDED], 0, plugin);
465 return TRUE;
466 }
468 static void
469 gst_registry_remove_features_for_plugin_unlocked (GstRegistry * registry,
470 GstPlugin * plugin)
471 {
472 GList *f;
474 g_return_if_fail (GST_IS_REGISTRY (registry));
475 g_return_if_fail (GST_IS_PLUGIN (plugin));
477 /* Remove all features for this plugin */
478 f = registry->features;
479 while (f != NULL) {
480 GList *next = g_list_next (f);
481 GstPluginFeature *feature = f->data;
483 if (G_UNLIKELY (feature && feature->plugin == plugin)) {
484 GST_DEBUG_OBJECT (registry, "removing feature %p (%s) for plugin %p (%s)",
485 feature, gst_plugin_feature_get_name (feature), plugin,
486 plugin->desc.name);
488 registry->features = g_list_delete_link (registry->features, f);
489 g_hash_table_remove (registry->feature_hash, feature->name);
490 gst_object_unparent (GST_OBJECT_CAST (feature));
491 }
492 f = next;
493 }
494 registry->priv->cookie++;
495 }
497 /**
498 * gst_registry_remove_plugin:
499 * @registry: the registry to remove the plugin from
500 * @plugin: (transfer none): the plugin to remove
501 *
502 * Remove the plugin from the registry.
503 *
504 * MT safe.
505 */
506 void
507 gst_registry_remove_plugin (GstRegistry * registry, GstPlugin * plugin)
508 {
509 g_return_if_fail (GST_IS_REGISTRY (registry));
510 g_return_if_fail (GST_IS_PLUGIN (plugin));
512 GST_DEBUG_OBJECT (registry, "removing plugin %p (%s)",
513 plugin, gst_plugin_get_name (plugin));
515 GST_OBJECT_LOCK (registry);
516 registry->plugins = g_list_remove (registry->plugins, plugin);
517 if (G_LIKELY (plugin->basename))
518 g_hash_table_remove (registry->basename_hash, plugin->basename);
519 gst_registry_remove_features_for_plugin_unlocked (registry, plugin);
520 GST_OBJECT_UNLOCK (registry);
521 gst_object_unref (plugin);
522 }
524 /**
525 * gst_registry_add_feature:
526 * @registry: the registry to add the plugin to
527 * @feature: (transfer full): the feature to add
528 *
529 * Add the feature to the registry. The feature-added signal will be emitted.
530 * This function sinks @feature.
531 *
532 * Returns: TRUE on success.
533 *
534 * MT safe.
535 */
536 gboolean
537 gst_registry_add_feature (GstRegistry * registry, GstPluginFeature * feature)
538 {
539 GstPluginFeature *existing_feature;
541 g_return_val_if_fail (GST_IS_REGISTRY (registry), FALSE);
542 g_return_val_if_fail (GST_IS_PLUGIN_FEATURE (feature), FALSE);
543 g_return_val_if_fail (feature->name != NULL, FALSE);
544 g_return_val_if_fail (feature->plugin_name != NULL, FALSE);
546 GST_OBJECT_LOCK (registry);
547 existing_feature = gst_registry_lookup_feature_locked (registry,
548 feature->name);
549 if (G_UNLIKELY (existing_feature)) {
550 GST_DEBUG_OBJECT (registry, "replacing existing feature %p (%s)",
551 existing_feature, feature->name);
552 /* Remove the existing feature from the list now, before we insert the new
553 * one, but don't unref yet because the hash is still storing a reference to
554 * it. */
555 registry->features = g_list_remove (registry->features, existing_feature);
556 }
558 GST_DEBUG_OBJECT (registry, "adding feature %p (%s)", feature, feature->name);
560 registry->features = g_list_prepend (registry->features, feature);
561 g_hash_table_replace (registry->feature_hash, feature->name, feature);
563 if (G_UNLIKELY (existing_feature)) {
564 /* We unref now. No need to remove the feature name from the hash table, it
565 * got replaced by the new feature */
566 gst_object_unparent (GST_OBJECT_CAST (existing_feature));
567 }
569 gst_object_set_parent (GST_OBJECT_CAST (feature), GST_OBJECT_CAST (registry));
571 registry->priv->cookie++;
572 GST_OBJECT_UNLOCK (registry);
574 GST_LOG_OBJECT (registry, "emitting feature-added for %s", feature->name);
575 g_signal_emit (registry, gst_registry_signals[FEATURE_ADDED], 0, feature);
577 return TRUE;
578 }
580 /**
581 * gst_registry_remove_feature:
582 * @registry: the registry to remove the feature from
583 * @feature: (transfer none): the feature to remove
584 *
585 * Remove the feature from the registry.
586 *
587 * MT safe.
588 */
589 void
590 gst_registry_remove_feature (GstRegistry * registry, GstPluginFeature * feature)
591 {
592 g_return_if_fail (GST_IS_REGISTRY (registry));
593 g_return_if_fail (GST_IS_PLUGIN_FEATURE (feature));
595 GST_DEBUG_OBJECT (registry, "removing feature %p (%s)",
596 feature, gst_plugin_feature_get_name (feature));
598 GST_OBJECT_LOCK (registry);
599 registry->features = g_list_remove (registry->features, feature);
600 g_hash_table_remove (registry->feature_hash, feature->name);
601 registry->priv->cookie++;
602 GST_OBJECT_UNLOCK (registry);
604 gst_object_unparent ((GstObject *) feature);
605 }
607 /**
608 * gst_registry_plugin_filter:
609 * @registry: registry to query
610 * @filter: (scope call): the filter to use
611 * @first: only return first match
612 * @user_data: (closure): user data passed to the filter function
613 *
614 * Runs a filter against all plugins in the registry and returns a #GList with
615 * the results. If the first flag is set, only the first match is
616 * returned (as a list with a single object).
617 * Every plugin is reffed; use gst_plugin_list_free() after use, which
618 * will unref again.
619 *
620 * Returns: (transfer full) (element-type Gst.Plugin): a #GList of #GstPlugin.
621 * Use gst_plugin_list_free() after usage.
622 *
623 * MT safe.
624 */
625 GList *
626 gst_registry_plugin_filter (GstRegistry * registry,
627 GstPluginFilter filter, gboolean first, gpointer user_data)
628 {
629 GList *list = NULL;
631 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
633 GST_OBJECT_LOCK (registry);
634 {
635 const GList *walk;
637 for (walk = registry->plugins; walk != NULL; walk = walk->next) {
638 GstPlugin *plugin = walk->data;
640 if (filter == NULL || filter (plugin, user_data)) {
641 list = g_list_prepend (list, gst_object_ref (plugin));
643 if (first)
644 break;
645 }
646 }
647 }
648 GST_OBJECT_UNLOCK (registry);
650 return list;
651 }
653 #ifdef GST_DISABLE_DEPRECATED
654 typedef struct
655 {
656 const gchar *name;
657 GType type;
658 } GstTypeNameData;
659 static gboolean
660 gst_plugin_feature_type_name_filter (GstPluginFeature * feature,
661 GstTypeNameData * data)
662 {
663 g_assert (GST_IS_PLUGIN_FEATURE (feature));
665 return ((data->type == 0 || data->type == G_OBJECT_TYPE (feature)) &&
666 (data->name == NULL
667 || !strcmp (data->name, GST_PLUGIN_FEATURE_NAME (feature))));
668 }
669 #endif
671 /* returns TRUE if the list was changed
672 *
673 * Must be called with the object lock taken */
674 static gboolean
675 gst_registry_get_feature_list_or_create (GstRegistry * registry,
676 GList ** previous, guint32 * cookie, GType type)
677 {
678 gboolean res = FALSE;
679 GstRegistryPrivate *priv = registry->priv;
681 if (G_UNLIKELY (!*previous || priv->cookie != *cookie)) {
682 GstTypeNameData data;
683 const GList *walk;
685 if (*previous) {
686 gst_plugin_feature_list_free (*previous);
687 *previous = NULL;
688 }
690 data.type = type;
691 data.name = NULL;
693 for (walk = registry->features; walk != NULL; walk = walk->next) {
694 GstPluginFeature *feature = walk->data;
696 if (gst_plugin_feature_type_name_filter (feature, &data)) {
697 *previous = g_list_prepend (*previous, gst_object_ref (feature));
698 }
699 }
701 *cookie = priv->cookie;
702 res = TRUE;
703 }
705 return res;
706 }
708 static gint
709 type_find_factory_rank_cmp (const GstPluginFeature * fac1,
710 const GstPluginFeature * fac2)
711 {
712 if (G_LIKELY (fac1->rank != fac2->rank))
713 return fac2->rank - fac1->rank;
715 /* to make the order in which things happen more deterministic,
716 * sort by name when the ranks are the same. */
717 return strcmp (fac1->name, fac2->name);
718 }
720 static GList *
721 gst_registry_get_element_factory_list (GstRegistry * registry)
722 {
723 GList *list;
725 GST_OBJECT_LOCK (registry);
727 gst_registry_get_feature_list_or_create (registry,
728 ®istry->priv->element_factory_list, ®istry->priv->efl_cookie,
729 GST_TYPE_ELEMENT_FACTORY);
731 /* Return reffed copy */
732 list = gst_plugin_feature_list_copy (registry->priv->element_factory_list);
734 GST_OBJECT_UNLOCK (registry);
736 return list;
737 }
739 static GList *
740 gst_registry_get_typefind_factory_list (GstRegistry * registry)
741 {
742 GList *list;
744 GST_OBJECT_LOCK (registry);
746 if (G_UNLIKELY (gst_registry_get_feature_list_or_create (registry,
747 ®istry->priv->typefind_factory_list,
748 ®istry->priv->tfl_cookie, GST_TYPE_TYPE_FIND_FACTORY)))
749 registry->priv->typefind_factory_list =
750 g_list_sort (registry->priv->typefind_factory_list,
751 (GCompareFunc) type_find_factory_rank_cmp);
753 /* Return reffed copy */
754 list = gst_plugin_feature_list_copy (registry->priv->typefind_factory_list);
756 GST_OBJECT_UNLOCK (registry);
758 return list;
759 }
761 /**
762 * gst_registry_feature_filter:
763 * @registry: registry to query
764 * @filter: (scope call): the filter to use
765 * @first: only return first match
766 * @user_data: (closure): user data passed to the filter function
767 *
768 * Runs a filter against all features of the plugins in the registry
769 * and returns a GList with the results.
770 * If the first flag is set, only the first match is
771 * returned (as a list with a single object).
772 *
773 * Returns: (transfer full) (element-type Gst.PluginFeature): a #GList of
774 * #GstPluginFeature. Use gst_plugin_feature_list_free() after usage.
775 *
776 * MT safe.
777 */
778 GList *
779 gst_registry_feature_filter (GstRegistry * registry,
780 GstPluginFeatureFilter filter, gboolean first, gpointer user_data)
781 {
782 GList *list = NULL;
784 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
786 GST_OBJECT_LOCK (registry);
787 {
788 const GList *walk;
790 for (walk = registry->features; walk != NULL; walk = walk->next) {
791 GstPluginFeature *feature = walk->data;
793 if (filter == NULL || filter (feature, user_data)) {
794 list = g_list_prepend (list, gst_object_ref (feature));
796 if (first)
797 break;
798 }
799 }
800 }
801 GST_OBJECT_UNLOCK (registry);
803 return list;
804 }
806 /**
807 * gst_registry_find_plugin:
808 * @registry: the registry to search
809 * @name: the plugin name to find
810 *
811 * Find the plugin with the given name in the registry.
812 * The plugin will be reffed; caller is responsible for unreffing.
813 *
814 * Returns: (transfer full): the plugin with the given name or NULL if the
815 * plugin was not found. gst_object_unref() after usage.
816 *
817 * MT safe.
818 */
819 GstPlugin *
820 gst_registry_find_plugin (GstRegistry * registry, const gchar * name)
821 {
822 GList *walk;
823 GstPlugin *result = NULL;
825 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
826 g_return_val_if_fail (name != NULL, NULL);
828 walk = gst_registry_plugin_filter (registry,
829 (GstPluginFilter) gst_plugin_name_filter, TRUE, (gpointer) name);
830 if (walk) {
831 result = GST_PLUGIN_CAST (walk->data);
833 gst_object_ref (result);
834 gst_plugin_list_free (walk);
835 }
837 return result;
838 }
840 /**
841 * gst_registry_find_feature:
842 * @registry: the registry to search
843 * @name: the pluginfeature name to find
844 * @type: the pluginfeature type to find
845 *
846 * Find the pluginfeature with the given name and type in the registry.
847 *
848 * Returns: (transfer full): the pluginfeature with the given name and type
849 * or NULL if the plugin was not found. gst_object_unref() after usage.
850 *
851 * MT safe.
852 */
853 GstPluginFeature *
854 gst_registry_find_feature (GstRegistry * registry, const gchar * name,
855 GType type)
856 {
857 GstPluginFeature *feature = NULL;
859 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
860 g_return_val_if_fail (name != NULL, NULL);
861 g_return_val_if_fail (g_type_is_a (type, GST_TYPE_PLUGIN_FEATURE), NULL);
863 feature = gst_registry_lookup_feature (registry, name);
864 if (feature && !g_type_is_a (G_TYPE_FROM_INSTANCE (feature), type)) {
865 gst_object_unref (feature);
866 feature = NULL;
867 }
869 return feature;
870 }
872 /**
873 * gst_registry_get_feature_list:
874 * @registry: a #GstRegistry
875 * @type: a #GType.
876 *
877 * Retrieves a #GList of #GstPluginFeature of @type.
878 *
879 * Returns: (transfer full) (element-type Gst.PluginFeature): a #GList of
880 * #GstPluginFeature of @type. Use gst_plugin_feature_list_free() after use
881 *
882 * MT safe.
883 */
884 GList *
885 gst_registry_get_feature_list (GstRegistry * registry, GType type)
886 {
887 GstTypeNameData data;
889 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
890 g_return_val_if_fail (g_type_is_a (type, GST_TYPE_PLUGIN_FEATURE), NULL);
892 /* Speed up */
893 if (type == GST_TYPE_ELEMENT_FACTORY)
894 return gst_registry_get_element_factory_list (registry);
895 else if (type == GST_TYPE_TYPE_FIND_FACTORY)
896 return gst_registry_get_typefind_factory_list (registry);
898 data.type = type;
899 data.name = NULL;
901 return gst_registry_feature_filter (registry,
902 (GstPluginFeatureFilter) gst_plugin_feature_type_name_filter,
903 FALSE, &data);
904 }
906 /**
907 * gst_registry_get_plugin_list:
908 * @registry: the registry to search
909 *
910 * Get a copy of all plugins registered in the given registry. The refcount
911 * of each element in the list in incremented.
912 *
913 * Returns: (transfer full) (element-type Gst.Plugin): a #GList of #GstPlugin.
914 * Use gst_plugin_list_free() after usage.
915 *
916 * MT safe.
917 */
918 GList *
919 gst_registry_get_plugin_list (GstRegistry * registry)
920 {
921 GList *list;
922 GList *g;
924 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
926 GST_OBJECT_LOCK (registry);
927 list = g_list_copy (registry->plugins);
928 for (g = list; g; g = g->next) {
929 gst_object_ref (GST_PLUGIN_CAST (g->data));
930 }
931 GST_OBJECT_UNLOCK (registry);
933 return list;
934 }
936 static GstPluginFeature *
937 gst_registry_lookup_feature_locked (GstRegistry * registry, const char *name)
938 {
939 return g_hash_table_lookup (registry->feature_hash, name);
940 }
942 /**
943 * gst_registry_lookup_feature:
944 * @registry: a #GstRegistry
945 * @name: a #GstPluginFeature name
946 *
947 * Find a #GstPluginFeature with @name in @registry.
948 *
949 * Returns: (transfer full): a #GstPluginFeature with its refcount incremented,
950 * use gst_object_unref() after usage.
951 *
952 * MT safe.
953 */
954 GstPluginFeature *
955 gst_registry_lookup_feature (GstRegistry * registry, const char *name)
956 {
957 GstPluginFeature *feature;
959 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
960 g_return_val_if_fail (name != NULL, NULL);
962 GST_OBJECT_LOCK (registry);
963 feature = gst_registry_lookup_feature_locked (registry, name);
964 if (feature)
965 gst_object_ref (feature);
966 GST_OBJECT_UNLOCK (registry);
968 return feature;
969 }
971 static GstPlugin *
972 gst_registry_lookup_bn_locked (GstRegistry * registry, const char *basename)
973 {
974 return g_hash_table_lookup (registry->basename_hash, basename);
975 }
977 static GstPlugin *
978 gst_registry_lookup_bn (GstRegistry * registry, const char *basename)
979 {
980 GstPlugin *plugin;
982 GST_OBJECT_LOCK (registry);
983 plugin = gst_registry_lookup_bn_locked (registry, basename);
984 if (plugin)
985 gst_object_ref (plugin);
986 GST_OBJECT_UNLOCK (registry);
988 return plugin;
989 }
991 /**
992 * gst_registry_lookup:
993 * @registry: the registry to look up in
994 * @filename: the name of the file to look up
995 *
996 * Look up a plugin in the given registry with the given filename.
997 * If found, plugin is reffed.
998 *
999 * Returns: (transfer full): the #GstPlugin if found, or NULL if not.
1000 * gst_object_unref() after usage.
1001 */
1002 GstPlugin *
1003 gst_registry_lookup (GstRegistry * registry, const char *filename)
1004 {
1005 GstPlugin *plugin;
1006 gchar *basename;
1008 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
1009 g_return_val_if_fail (filename != NULL, NULL);
1011 basename = g_path_get_basename (filename);
1012 if (G_UNLIKELY (basename == NULL))
1013 return NULL;
1015 plugin = gst_registry_lookup_bn (registry, basename);
1017 g_free (basename);
1019 return plugin;
1020 }
1022 typedef enum
1023 {
1024 REGISTRY_SCAN_HELPER_NOT_STARTED = 0,
1025 REGISTRY_SCAN_HELPER_DISABLED,
1026 REGISTRY_SCAN_HELPER_RUNNING
1027 } GstRegistryScanHelperState;
1029 typedef struct
1030 {
1031 GstRegistry *registry;
1032 GstRegistryScanHelperState helper_state;
1033 GstPluginLoader *helper;
1034 gboolean changed;
1035 } GstRegistryScanContext;
1037 static void
1038 init_scan_context (GstRegistryScanContext * context, GstRegistry * registry)
1039 {
1040 gboolean do_fork;
1042 context->registry = registry;
1044 /* see if forking is enabled and set up the scan helper state accordingly */
1045 do_fork = _gst_enable_registry_fork;
1046 if (do_fork) {
1047 const gchar *fork_env;
1049 /* forking enabled, see if it is disabled with an env var */
1050 if ((fork_env = g_getenv ("GST_REGISTRY_FORK"))) {
1051 /* fork enabled for any value different from "no" */
1052 do_fork = strcmp (fork_env, "no") != 0;
1053 }
1054 }
1056 if (do_fork)
1057 context->helper_state = REGISTRY_SCAN_HELPER_NOT_STARTED;
1058 else
1059 context->helper_state = REGISTRY_SCAN_HELPER_DISABLED;
1061 context->helper = NULL;
1062 context->changed = FALSE;
1063 }
1065 static void
1066 clear_scan_context (GstRegistryScanContext * context)
1067 {
1068 if (context->helper) {
1069 context->changed |= _priv_gst_plugin_loader_funcs.destroy (context->helper);
1070 context->helper = NULL;
1071 }
1072 }
1074 static gboolean
1075 gst_registry_scan_plugin_file (GstRegistryScanContext * context,
1076 const gchar * filename, off_t file_size, time_t file_mtime)
1077 {
1078 gboolean changed = FALSE;
1079 GstPlugin *newplugin = NULL;
1081 #ifdef G_OS_WIN32
1082 /* Disable external plugin loader on Windows until it is ported properly. */
1083 context->helper_state = REGISTRY_SCAN_HELPER_DISABLED;
1084 #endif
1087 /* Have a plugin to load - see if the scan-helper needs starting */
1088 if (context->helper_state == REGISTRY_SCAN_HELPER_NOT_STARTED) {
1089 GST_DEBUG ("Starting plugin scanner for file %s", filename);
1090 context->helper = _priv_gst_plugin_loader_funcs.create (context->registry);
1091 if (context->helper != NULL)
1092 context->helper_state = REGISTRY_SCAN_HELPER_RUNNING;
1093 else {
1094 GST_WARNING ("Failed starting plugin scanner. Scanning in-process");
1095 context->helper_state = REGISTRY_SCAN_HELPER_DISABLED;
1096 }
1097 }
1099 if (context->helper_state == REGISTRY_SCAN_HELPER_RUNNING) {
1100 GST_DEBUG ("Using scan-helper to load plugin %s", filename);
1101 if (!_priv_gst_plugin_loader_funcs.load (context->helper,
1102 filename, file_size, file_mtime)) {
1103 g_warning ("External plugin loader failed. This most likely means that "
1104 "the plugin loader helper binary was not found or could not be run. "
1105 "%s", (g_getenv ("GST_PLUGIN_PATH") != NULL) ?
1106 "If you are running an uninstalled GStreamer setup, you might need "
1107 "to update your gst-uninstalled script so that the "
1108 "GST_PLUGIN_SCANNER environment variable gets set." : "");
1109 context->helper_state = REGISTRY_SCAN_HELPER_DISABLED;
1110 }
1111 }
1113 /* Check if the helper is disabled (or just got disabled above) */
1114 if (context->helper_state == REGISTRY_SCAN_HELPER_DISABLED) {
1115 /* Load plugin the old fashioned way... */
1117 /* We don't use a GError here because a failure to load some shared
1118 * objects as plugins is normal (particularly in the uninstalled case)
1119 */
1120 newplugin = gst_plugin_load_file (filename, NULL);
1121 }
1123 if (newplugin) {
1124 GST_DEBUG_OBJECT (context->registry, "marking new plugin %p as registered",
1125 newplugin);
1126 newplugin->registered = TRUE;
1127 gst_object_unref (newplugin);
1128 changed = TRUE;
1129 }
1130 #ifndef GST_DISABLE_REGISTRY
1131 if (!__registry_reuse_plugin_scanner) {
1132 clear_scan_context (context);
1133 context->helper_state = REGISTRY_SCAN_HELPER_NOT_STARTED;
1134 }
1135 #endif
1137 return changed;
1138 }
1140 static gboolean
1141 is_blacklisted_hidden_directory (const gchar * dirent)
1142 {
1143 if (G_LIKELY (dirent[0] != '.'))
1144 return FALSE;
1146 /* skip the .debug directory, these contain elf files that are not
1147 * useful or worse, can crash dlopen () */
1148 if (strcmp (dirent, ".debug") == 0)
1149 return TRUE;
1151 /* can also skip .git and .deps dirs, those won't contain useful files.
1152 * This speeds up scanning a bit in uninstalled setups. */
1153 if (strcmp (dirent, ".git") == 0 || strcmp (dirent, ".deps") == 0)
1154 return TRUE;
1156 return FALSE;
1157 }
1159 static gboolean
1160 gst_registry_scan_path_level (GstRegistryScanContext * context,
1161 const gchar * path, int level)
1162 {
1163 GDir *dir;
1164 const gchar *dirent;
1165 gchar *filename;
1166 GstPlugin *plugin;
1167 gboolean changed = FALSE;
1169 dir = g_dir_open (path, 0, NULL);
1170 if (!dir)
1171 return FALSE;
1173 while ((dirent = g_dir_read_name (dir))) {
1174 GStatBuf file_status;
1176 filename = g_build_filename (path, dirent, NULL);
1177 if (g_stat (filename, &file_status) < 0) {
1178 /* Plugin will be removed from cache after the scan completes if it
1179 * is still marked 'cached' */
1180 g_free (filename);
1181 continue;
1182 }
1184 if (file_status.st_mode & S_IFDIR) {
1185 if (G_UNLIKELY (is_blacklisted_hidden_directory (dirent))) {
1186 GST_TRACE_OBJECT (context->registry, "ignoring %s directory", dirent);
1187 g_free (filename);
1188 continue;
1189 }
1190 /* FIXME 0.11: Don't recurse into directories, this behaviour
1191 * is inconsistent with other PATH environment variables
1192 */
1193 if (level > 0) {
1194 GST_LOG_OBJECT (context->registry, "recursing into directory %s",
1195 filename);
1196 changed |= gst_registry_scan_path_level (context, filename, level - 1);
1197 } else {
1198 GST_LOG_OBJECT (context->registry, "not recursing into directory %s, "
1199 "recursion level too deep", filename);
1200 }
1201 g_free (filename);
1202 continue;
1203 }
1204 if (!(file_status.st_mode & S_IFREG)) {
1205 GST_TRACE_OBJECT (context->registry, "%s is not a regular file, ignoring",
1206 filename);
1207 g_free (filename);
1208 continue;
1209 }
1210 if (!g_str_has_suffix (dirent, G_MODULE_SUFFIX)
1211 #ifdef GST_EXTRA_MODULE_SUFFIX
1212 && !g_str_has_suffix (dirent, GST_EXTRA_MODULE_SUFFIX)
1213 #endif
1214 ) {
1215 GST_TRACE_OBJECT (context->registry,
1216 "extension is not recognized as module file, ignoring file %s",
1217 filename);
1218 g_free (filename);
1219 continue;
1220 }
1222 GST_LOG_OBJECT (context->registry, "file %s looks like a possible module",
1223 filename);
1225 /* try to avoid unnecessary plugin-move pain */
1226 if (g_str_has_prefix (dirent, "libgstvalve") ||
1227 g_str_has_prefix (dirent, "libgstselector")) {
1228 GST_WARNING_OBJECT (context->registry, "ignoring old plugin %s which "
1229 "has been merged into the corelements plugin", filename);
1230 /* Plugin will be removed from cache after the scan completes if it
1231 * is still marked 'cached' */
1232 g_free (filename);
1233 continue;
1234 }
1236 /* plug-ins are considered unique by basename; if the given name
1237 * was already seen by the registry, we ignore it */
1238 plugin = gst_registry_lookup_bn (context->registry, dirent);
1239 if (plugin) {
1240 gboolean env_vars_changed, deps_changed = FALSE;
1242 if (plugin->registered) {
1243 GST_DEBUG_OBJECT (context->registry,
1244 "plugin already registered from path \"%s\"",
1245 GST_STR_NULL (plugin->filename));
1246 g_free (filename);
1247 gst_object_unref (plugin);
1248 continue;
1249 }
1251 env_vars_changed = _priv_plugin_deps_env_vars_changed (plugin);
1253 /* If a file with a certain basename is seen on a different path,
1254 * update the plugin to ensure the registry cache will reflect up
1255 * to date information */
1257 if (plugin->file_mtime == file_status.st_mtime &&
1258 plugin->file_size == file_status.st_size && !env_vars_changed &&
1259 !(deps_changed = _priv_plugin_deps_files_changed (plugin)) &&
1260 !strcmp (plugin->filename, filename)) {
1261 GST_LOG_OBJECT (context->registry, "file %s cached", filename);
1262 plugin->flags &= ~GST_PLUGIN_FLAG_CACHED;
1263 GST_LOG_OBJECT (context->registry,
1264 "marking plugin %p as registered as %s", plugin, filename);
1265 plugin->registered = TRUE;
1266 } else {
1267 GST_INFO_OBJECT (context->registry, "cached info for %s is stale",
1268 filename);
1269 GST_DEBUG_OBJECT (context->registry, "mtime %" G_GINT64_FORMAT " != %"
1270 G_GINT64_FORMAT " or size %" G_GINT64_FORMAT " != %"
1271 G_GINT64_FORMAT " or external dependency env_vars changed: %d or"
1272 " external dependencies changed: %d or old path %s != new path %s",
1273 (gint64) plugin->file_mtime, (gint64) file_status.st_mtime,
1274 (gint64) plugin->file_size, (gint64) file_status.st_size,
1275 env_vars_changed, deps_changed, plugin->filename, filename);
1276 gst_registry_remove_plugin (context->registry, plugin);
1277 changed |= gst_registry_scan_plugin_file (context, filename,
1278 file_status.st_size, file_status.st_mtime);
1279 }
1280 gst_object_unref (plugin);
1282 } else {
1283 GST_DEBUG_OBJECT (context->registry, "file %s not yet in registry",
1284 filename);
1285 changed |= gst_registry_scan_plugin_file (context, filename,
1286 file_status.st_size, file_status.st_mtime);
1287 }
1289 g_free (filename);
1290 }
1292 g_dir_close (dir);
1294 return changed;
1295 }
1297 static gboolean
1298 gst_registry_scan_path_internal (GstRegistryScanContext * context,
1299 const gchar * path)
1300 {
1301 gboolean changed;
1303 GST_DEBUG_OBJECT (context->registry, "scanning path %s", path);
1304 changed = gst_registry_scan_path_level (context, path, 10);
1306 GST_DEBUG_OBJECT (context->registry, "registry changed in path %s: %d", path,
1307 changed);
1308 return changed;
1309 }
1311 /**
1312 * gst_registry_scan_path:
1313 * @registry: the registry to add found plugins to
1314 * @path: the path to scan
1315 *
1316 * Scan the given path for plugins to add to the registry. The syntax of the
1317 * path is specific to the registry.
1318 *
1319 * Returns: %TRUE if registry changed
1320 */
1321 gboolean
1322 gst_registry_scan_path (GstRegistry * registry, const gchar * path)
1323 {
1324 GstRegistryScanContext context;
1325 gboolean result;
1327 g_return_val_if_fail (GST_IS_REGISTRY (registry), FALSE);
1328 g_return_val_if_fail (path != NULL, FALSE);
1330 init_scan_context (&context, registry);
1332 result = gst_registry_scan_path_internal (&context, path);
1334 clear_scan_context (&context);
1335 result |= context.changed;
1337 return result;
1338 }
1340 static gboolean
1341 _gst_plugin_feature_filter_plugin_name (GstPluginFeature * feature,
1342 gpointer user_data)
1343 {
1344 return (strcmp (feature->plugin_name, (gchar *) user_data) == 0);
1345 }
1347 /**
1348 * gst_registry_get_feature_list_by_plugin:
1349 * @registry: a #GstRegistry.
1350 * @name: a plugin name.
1351 *
1352 * Retrieves a #GList of features of the plugin with name @name.
1353 *
1354 * Returns: (transfer full) (element-type Gst.PluginFeature): a #GList of
1355 * #GstPluginFeature. Use gst_plugin_feature_list_free() after usage.
1356 */
1357 GList *
1358 gst_registry_get_feature_list_by_plugin (GstRegistry * registry,
1359 const gchar * name)
1360 {
1361 g_return_val_if_fail (GST_IS_REGISTRY (registry), NULL);
1362 g_return_val_if_fail (name != NULL, NULL);
1364 return gst_registry_feature_filter (registry,
1365 _gst_plugin_feature_filter_plugin_name, FALSE, (gpointer) name);
1366 }
1368 /* Unref and delete the default registry */
1369 void
1370 _priv_gst_registry_cleanup (void)
1371 {
1372 GstRegistry *registry;
1374 g_static_mutex_lock (&_gst_registry_mutex);
1375 if ((registry = _gst_registry_default) != NULL) {
1376 _gst_registry_default = NULL;
1377 }
1378 g_static_mutex_unlock (&_gst_registry_mutex);
1380 /* unref outside of the lock because we can. */
1381 if (registry)
1382 gst_object_unref (registry);
1383 }
1385 /**
1386 * gst_default_registry_check_feature_version:
1387 * @feature_name: the name of the feature (e.g. "oggdemux")
1388 * @min_major: the minimum major version number
1389 * @min_minor: the minimum minor version number
1390 * @min_micro: the minimum micro version number
1391 *
1392 * Checks whether a plugin feature by the given name exists in the
1393 * default registry and whether its version is at least the
1394 * version required.
1395 *
1396 * Returns: #TRUE if the feature could be found and the version is
1397 * the same as the required version or newer, and #FALSE otherwise.
1398 */
1399 gboolean
1400 gst_default_registry_check_feature_version (const gchar * feature_name,
1401 guint min_major, guint min_minor, guint min_micro)
1402 {
1403 GstPluginFeature *feature;
1404 GstRegistry *registry;
1405 gboolean ret = FALSE;
1407 g_return_val_if_fail (feature_name != NULL, FALSE);
1409 GST_DEBUG ("Looking up plugin feature '%s'", feature_name);
1411 registry = gst_registry_get_default ();
1412 feature = gst_registry_lookup_feature (registry, feature_name);
1413 if (feature) {
1414 ret = gst_plugin_feature_check_version (feature, min_major, min_minor,
1415 min_micro);
1416 gst_object_unref (feature);
1417 } else {
1418 GST_DEBUG ("Could not find plugin feature '%s'", feature_name);
1419 }
1421 return ret;
1422 }
1424 static void
1425 load_plugin_func (gpointer data, gpointer user_data)
1426 {
1427 GstPlugin *plugin;
1428 const gchar *filename;
1429 GError *err = NULL;
1431 filename = (const gchar *) data;
1432 GST_DEBUG ("Pre-loading plugin %s", filename);
1434 plugin = gst_plugin_load_file (filename, &err);
1436 if (plugin) {
1437 GST_INFO ("Loaded plugin: \"%s\"", filename);
1439 gst_default_registry_add_plugin (plugin);
1440 } else {
1441 if (err) {
1442 /* Report error to user, and free error */
1443 GST_ERROR ("Failed to load plugin: %s", err->message);
1444 g_error_free (err);
1445 } else {
1446 GST_WARNING ("Failed to load plugin: \"%s\"", filename);
1447 }
1448 }
1449 }
1451 #ifndef GST_DISABLE_REGISTRY
1452 /* Unref all plugins marked 'cached', to clear old plugins that no
1453 * longer exist. Returns TRUE if any plugins were removed */
1454 static gboolean
1455 gst_registry_remove_cache_plugins (GstRegistry * registry)
1456 {
1457 GList *g;
1458 GList *g_next;
1459 GstPlugin *plugin;
1460 gboolean changed = FALSE;
1462 g_return_val_if_fail (GST_IS_REGISTRY (registry), FALSE);
1464 GST_OBJECT_LOCK (registry);
1466 GST_DEBUG_OBJECT (registry, "removing cached plugins");
1467 g = registry->plugins;
1468 while (g) {
1469 g_next = g->next;
1470 plugin = g->data;
1471 if (plugin->flags & GST_PLUGIN_FLAG_CACHED) {
1472 GST_DEBUG_OBJECT (registry, "removing cached plugin \"%s\"",
1473 GST_STR_NULL (plugin->filename));
1474 registry->plugins = g_list_delete_link (registry->plugins, g);
1475 if (G_LIKELY (plugin->basename))
1476 g_hash_table_remove (registry->basename_hash, plugin->basename);
1477 gst_registry_remove_features_for_plugin_unlocked (registry, plugin);
1478 gst_object_unref (plugin);
1479 changed = TRUE;
1480 }
1481 g = g_next;
1482 }
1484 GST_OBJECT_UNLOCK (registry);
1486 return changed;
1487 }
1489 typedef enum
1490 {
1491 REGISTRY_SCAN_AND_UPDATE_FAILURE = 0,
1492 REGISTRY_SCAN_AND_UPDATE_SUCCESS_NOT_CHANGED,
1493 REGISTRY_SCAN_AND_UPDATE_SUCCESS_UPDATED
1494 } GstRegistryScanAndUpdateResult;
1496 /*
1497 * scan_and_update_registry:
1498 * @default_registry: the #GstRegistry
1499 * @registry_file: registry filename
1500 * @write_changes: write registry if it has changed?
1501 *
1502 * Scans for registry changes and eventually updates the registry cache.
1503 *
1504 * Return: %REGISTRY_SCAN_AND_UPDATE_FAILURE if the registry could not scanned
1505 * or updated, %REGISTRY_SCAN_AND_UPDATE_SUCCESS_NOT_CHANGED if the
1506 * registry is clean and %REGISTRY_SCAN_AND_UPDATE_SUCCESS_UPDATED if
1507 * it has been updated and the cache needs to be re-read.
1508 */
1509 static GstRegistryScanAndUpdateResult
1510 scan_and_update_registry (GstRegistry * default_registry,
1511 const gchar * registry_file, gboolean write_changes, GError ** error)
1512 {
1513 const gchar *plugin_path;
1514 gboolean changed = FALSE;
1515 GList *l;
1516 GstRegistryScanContext context;
1518 GST_INFO ("Validating plugins from registry cache: %s", registry_file);
1520 init_scan_context (&context, default_registry);
1522 /* It sounds tempting to just compare the mtime of directories with the mtime
1523 * of the registry cache, but it does not work. It would not catch updated
1524 * plugins, which might bring more or less features.
1525 */
1527 /* scan paths specified via --gst-plugin-path */
1528 GST_DEBUG ("scanning paths added via --gst-plugin-path");
1529 for (l = _priv_gst_plugin_paths; l != NULL; l = l->next) {
1530 GST_INFO ("Scanning plugin path: \"%s\"", (gchar *) l->data);
1531 changed |= gst_registry_scan_path_internal (&context, (gchar *) l->data);
1532 }
1533 /* keep plugin_paths around in case a re-scan is forced later on */
1535 /* GST_PLUGIN_PATH specifies a list of directories to scan for
1536 * additional plugins. These take precedence over the system plugins */
1537 plugin_path = g_getenv ("GST_PLUGIN_PATH");
1538 if (plugin_path) {
1539 char **list;
1540 int i;
1542 GST_DEBUG ("GST_PLUGIN_PATH set to %s", plugin_path);
1543 list = g_strsplit (plugin_path, G_SEARCHPATH_SEPARATOR_S, 0);
1544 for (i = 0; list[i]; i++) {
1545 changed |= gst_registry_scan_path_internal (&context, list[i]);
1546 }
1547 g_strfreev (list);
1548 } else {
1549 GST_DEBUG ("GST_PLUGIN_PATH not set");
1550 }
1552 /* GST_PLUGIN_SYSTEM_PATH specifies a list of plugins that are always
1553 * loaded by default. If not set, this defaults to the system-installed
1554 * path, and the plugins installed in the user's home directory */
1555 plugin_path = g_getenv ("GST_PLUGIN_SYSTEM_PATH");
1556 if (plugin_path == NULL) {
1557 char *home_plugins;
1559 GST_DEBUG ("GST_PLUGIN_SYSTEM_PATH not set");
1561 /* plugins in the user's home directory take precedence over
1562 * system-installed ones */
1563 home_plugins = g_build_filename (g_get_home_dir (),
1564 ".gstreamer-" GST_MAJORMINOR, "plugins", NULL);
1565 GST_DEBUG ("scanning home plugins %s", home_plugins);
1566 changed |= gst_registry_scan_path_internal (&context, home_plugins);
1567 g_free (home_plugins);
1569 /* add the main (installed) library path */
1570 GST_DEBUG ("scanning main plugins %s", PLUGINDIR);
1571 changed |= gst_registry_scan_path_internal (&context, PLUGINDIR);
1573 #ifdef G_OS_WIN32
1574 {
1575 char *base_dir;
1576 char *dir;
1578 base_dir =
1579 g_win32_get_package_installation_directory_of_module
1580 (_priv_gst_dll_handle);
1582 dir = g_build_filename (base_dir, "lib", "gstreamer-0.10", NULL);
1583 GST_DEBUG ("scanning DLL dir %s", dir);
1585 changed |= gst_registry_scan_path_internal (&context, dir);
1587 g_free (dir);
1588 g_free (base_dir);
1589 }
1590 #endif
1591 } else {
1592 gchar **list;
1593 gint i;
1595 GST_DEBUG ("GST_PLUGIN_SYSTEM_PATH set to %s", plugin_path);
1596 list = g_strsplit (plugin_path, G_SEARCHPATH_SEPARATOR_S, 0);
1597 for (i = 0; list[i]; i++) {
1598 changed |= gst_registry_scan_path_internal (&context, list[i]);
1599 }
1600 g_strfreev (list);
1601 }
1603 clear_scan_context (&context);
1604 changed |= context.changed;
1606 /* Remove cached plugins so stale info is cleared. */
1607 changed |= gst_registry_remove_cache_plugins (default_registry);
1609 if (!changed) {
1610 GST_INFO ("Registry cache has not changed");
1611 return REGISTRY_SCAN_AND_UPDATE_SUCCESS_NOT_CHANGED;
1612 }
1614 if (!write_changes) {
1615 GST_INFO ("Registry cache changed, but writing is disabled. Not writing.");
1616 return REGISTRY_SCAN_AND_UPDATE_FAILURE;
1617 }
1619 GST_INFO ("Registry cache changed. Writing new registry cache");
1620 if (!gst_registry_binary_write_cache (default_registry, registry_file)) {
1621 g_set_error (error, GST_CORE_ERROR, GST_CORE_ERROR_FAILED,
1622 _("Error writing registry cache to %s: %s"),
1623 registry_file, g_strerror (errno));
1624 return REGISTRY_SCAN_AND_UPDATE_FAILURE;
1625 }
1627 GST_INFO ("Registry cache written successfully");
1628 return REGISTRY_SCAN_AND_UPDATE_SUCCESS_UPDATED;
1629 }
1631 static gboolean
1632 ensure_current_registry (GError ** error)
1633 {
1634 gchar *registry_file;
1635 GstRegistry *default_registry;
1636 gboolean ret = TRUE;
1637 gboolean do_update = TRUE;
1638 gboolean have_cache = TRUE;
1640 default_registry = gst_registry_get_default ();
1641 registry_file = g_strdup (g_getenv ("GST_REGISTRY"));
1642 if (registry_file == NULL) {
1643 registry_file = g_build_filename (g_get_home_dir (),
1644 ".gstreamer-" GST_MAJORMINOR, "registry." HOST_CPU ".bin", NULL);
1645 }
1647 if (!_gst_disable_registry_cache) {
1648 GST_INFO ("reading registry cache: %s", registry_file);
1649 have_cache = gst_registry_binary_read_cache (default_registry,
1650 registry_file);
1651 /* Only ever read the registry cache once, then disable it for
1652 * subsequent updates during the program lifetime */
1653 _gst_disable_registry_cache = TRUE;
1654 }
1656 if (have_cache) {
1657 do_update = !_priv_gst_disable_registry_update;
1658 if (do_update) {
1659 const gchar *update_env;
1661 if ((update_env = g_getenv ("GST_REGISTRY_UPDATE"))) {
1662 /* do update for any value different from "no" */
1663 do_update = (strcmp (update_env, "no") != 0);
1664 }
1665 }
1666 }
1668 if (do_update) {
1669 const gchar *reuse_env;
1671 if ((reuse_env = g_getenv ("GST_REGISTRY_REUSE_PLUGIN_SCANNER"))) {
1672 /* do reuse for any value different from "no" */
1673 __registry_reuse_plugin_scanner = (strcmp (reuse_env, "no") != 0);
1674 }
1675 /* now check registry */
1676 GST_DEBUG ("Updating registry cache");
1677 scan_and_update_registry (default_registry, registry_file, TRUE, error);
1678 } else {
1679 GST_DEBUG ("Not updating registry cache (disabled)");
1680 }
1682 g_free (registry_file);
1683 GST_INFO ("registry reading and updating done, result = %d", ret);
1685 return ret;
1686 }
1687 #endif /* GST_DISABLE_REGISTRY */
1689 /**
1690 * gst_registry_fork_is_enabled:
1691 *
1692 * By default GStreamer will perform scanning and rebuilding of the
1693 * registry file using a helper child process.
1694 *
1695 * Applications might want to disable this behaviour with the
1696 * gst_registry_fork_set_enabled() function, in which case new plugins
1697 * are scanned (and loaded) into the application process.
1698 *
1699 * Returns: %TRUE if GStreamer will use the child helper process when
1700 * rebuilding the registry.
1701 *
1702 * Since: 0.10.10
1703 */
1704 gboolean
1705 gst_registry_fork_is_enabled (void)
1706 {
1707 return _gst_enable_registry_fork;
1708 }
1710 /**
1711 * gst_registry_fork_set_enabled:
1712 * @enabled: whether rebuilding the registry can use a temporary child helper process.
1713 *
1714 * Applications might want to disable/enable spawning of a child helper process
1715 * when rebuilding the registry. See gst_registry_fork_is_enabled() for more
1716 * information.
1717 *
1718 * Since: 0.10.10
1719 */
1720 void
1721 gst_registry_fork_set_enabled (gboolean enabled)
1722 {
1723 _gst_enable_registry_fork = enabled;
1724 }
1726 /**
1727 * gst_update_registry:
1728 *
1729 * Forces GStreamer to re-scan its plugin paths and update the default
1730 * plugin registry.
1731 *
1732 * Applications will almost never need to call this function, it is only
1733 * useful if the application knows new plugins have been installed (or old
1734 * ones removed) since the start of the application (or, to be precise, the
1735 * first call to gst_init()) and the application wants to make use of any
1736 * newly-installed plugins without restarting the application.
1737 *
1738 * Applications should assume that the registry update is neither atomic nor
1739 * thread-safe and should therefore not have any dynamic pipelines running
1740 * (including the playbin and decodebin elements) and should also not create
1741 * any elements or access the GStreamer registry while the update is in
1742 * progress.
1743 *
1744 * Note that this function may block for a significant amount of time.
1745 *
1746 * Returns: %TRUE if the registry has been updated successfully (does not
1747 * imply that there were changes), otherwise %FALSE.
1748 *
1749 * Since: 0.10.12
1750 */
1751 gboolean
1752 gst_update_registry (void)
1753 {
1754 gboolean res;
1756 #ifndef GST_DISABLE_REGISTRY
1757 GError *err = NULL;
1759 res = ensure_current_registry (&err);
1760 if (err) {
1761 GST_WARNING ("registry update failed: %s", err->message);
1762 g_error_free (err);
1763 } else {
1764 GST_LOG ("registry update succeeded");
1765 }
1767 #else
1768 GST_WARNING ("registry update failed: %s", "registry disabled");
1769 res = TRUE;
1770 #endif /* GST_DISABLE_REGISTRY */
1772 if (_priv_gst_preload_plugins) {
1773 GST_DEBUG ("Preloading indicated plugins...");
1774 g_slist_foreach (_priv_gst_preload_plugins, load_plugin_func, NULL);
1775 }
1777 return res;
1778 }
1780 /**
1781 * gst_registry_get_feature_list_cookie:
1782 * @registry: the registry
1783 *
1784 * Returns the registrys feature list cookie. This changes
1785 * every time a feature is added or removed from the registry.
1786 *
1787 * Returns: the feature list cookie.
1788 *
1789 * Since: 0.10.26
1790 */
1791 guint32
1792 gst_registry_get_feature_list_cookie (GstRegistry * registry)
1793 {
1794 g_return_val_if_fail (GST_IS_REGISTRY (registry), 0);
1796 return registry->priv->cookie;
1797 }