ef691fd17de7ffc4b4ded24e245c8afd6d77d2b4
[glsdk/gstreamer0-10.git] / gst / gstsystemclock.c
1 /* GStreamer
2  * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3  *                    2004 Wim Taymans <wim@fluendo.com>
4  *
5  * gstsystemclock.c: Default clock, uses the system clock
6  *
7  * This library is free software; you can redistribute it and/or
8  * modify it under the terms of the GNU Library General Public
9  * License as published by the Free Software Foundation; either
10  * version 2 of the License, or (at your option) any later version.
11  *
12  * This library is distributed in the hope that it will be useful,
13  * but WITHOUT ANY WARRANTY; without even the implied warranty of
14  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
15  * Library General Public License for more details.
16  *
17  * You should have received a copy of the GNU Library General Public
18  * License along with this library; if not, write to the
19  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20  * Boston, MA 02111-1307, USA.
21  */
23 /**
24  * SECTION:gstsystemclock
25  * @short_description: Default clock that uses the current system time
26  * @see_also: #GstClock
27  *
28  * The GStreamer core provides a GstSystemClock based on the system time.
29  * Asynchronous callbacks are scheduled from an internal thread.
30  *
31  * Clock implementors are encouraged to subclass this systemclock as it
32  * implements the async notification.
33  *
34  * Subclasses can however override all of the important methods for sync and
35  * async notifications to implement their own callback methods or blocking
36  * wait operations.
37  *
38  * Last reviewed on 2006-03-08 (0.10.4)
39  */
41 #include "gst_private.h"
42 #include "gstinfo.h"
43 #include "gstsystemclock.h"
44 #include "gstenumtypes.h"
45 #include "gstpoll.h"
46 #include "gstutils.h"
47 #include "glib-compat-private.h"
49 #include <errno.h>
51 #ifdef G_OS_WIN32
52 #  define WIN32_LEAN_AND_MEAN   /* prevents from including too many things */
53 #  include <windows.h>          /* QueryPerformance* stuff */
54 #  undef WIN32_LEAN_AND_MEAN
55 #  define EWOULDBLOCK EAGAIN    /* This is just to placate gcc */
56 #endif /* G_OS_WIN32 */
58 #define GET_ENTRY_STATUS(e)          ((GstClockReturn) g_atomic_int_get(&GST_CLOCK_ENTRY_STATUS(e)))
59 #define SET_ENTRY_STATUS(e,val)      (g_atomic_int_set(&GST_CLOCK_ENTRY_STATUS(e),(val)))
60 #define CAS_ENTRY_STATUS(e,old,val)  (G_ATOMIC_INT_COMPARE_AND_EXCHANGE(\
61                                        (&GST_CLOCK_ENTRY_STATUS(e)), (old), (val)))
63 /* Define this to get some extra debug about jitter from each clock_wait */
64 #undef WAIT_DEBUGGING
66 struct _GstSystemClockPrivate
67 {
68   GstClockType clock_type;
69   GstPoll *timer;
70   gint wakeup_count;            /* the number of entries with a pending wakeup */
71   gboolean async_wakeup;        /* if the wakeup was because of a async list change */
73 #ifdef G_OS_WIN32
74   LARGE_INTEGER start;
75   LARGE_INTEGER frequency;
76 #endif                          /* G_OS_WIN32 */
77 };
79 #define GST_SYSTEM_CLOCK_GET_PRIVATE(obj)  \
80    (G_TYPE_INSTANCE_GET_PRIVATE ((obj), GST_TYPE_SYSTEM_CLOCK, \
81         GstSystemClockPrivate))
83 #ifdef HAVE_POSIX_TIMERS
84 # ifdef HAVE_MONOTONIC_CLOCK
85 #  define DEFAULT_CLOCK_TYPE GST_CLOCK_TYPE_MONOTONIC
86 # else
87 #  define DEFAULT_CLOCK_TYPE GST_CLOCK_TYPE_REALTIME
88 # endif
89 #else
90 #define DEFAULT_CLOCK_TYPE GST_CLOCK_TYPE_REALTIME
91 #endif
93 enum
94 {
95   PROP_0,
96   PROP_CLOCK_TYPE,
97   /* FILL ME */
98 };
100 /* the one instance of the systemclock */
101 static GstClock *_the_system_clock = NULL;
103 static void gst_system_clock_dispose (GObject * object);
104 static void gst_system_clock_set_property (GObject * object, guint prop_id,
105     const GValue * value, GParamSpec * pspec);
106 static void gst_system_clock_get_property (GObject * object, guint prop_id,
107     GValue * value, GParamSpec * pspec);
109 static GstClockTime gst_system_clock_get_internal_time (GstClock * clock);
110 static guint64 gst_system_clock_get_resolution (GstClock * clock);
111 static GstClockReturn gst_system_clock_id_wait_jitter (GstClock * clock,
112     GstClockEntry * entry, GstClockTimeDiff * jitter);
113 static GstClockReturn gst_system_clock_id_wait_jitter_unlocked
114     (GstClock * clock, GstClockEntry * entry, GstClockTimeDiff * jitter,
115     gboolean restart);
116 static GstClockReturn gst_system_clock_id_wait_async (GstClock * clock,
117     GstClockEntry * entry);
118 static void gst_system_clock_id_unschedule (GstClock * clock,
119     GstClockEntry * entry);
120 static void gst_system_clock_async_thread (GstClock * clock);
121 static gboolean gst_system_clock_start_async (GstSystemClock * clock);
122 static void gst_system_clock_add_wakeup (GstSystemClock * sysclock);
124 static GStaticMutex _gst_sysclock_mutex = G_STATIC_MUTEX_INIT;
126 static GstClockClass *parent_class = NULL;
128 /* static guint gst_system_clock_signals[LAST_SIGNAL] = { 0 }; */
130 G_DEFINE_TYPE (GstSystemClock, gst_system_clock, GST_TYPE_CLOCK);
132 static void
133 gst_system_clock_class_init (GstSystemClockClass * klass)
135   GObjectClass *gobject_class;
136   GstClockClass *gstclock_class;
138   gobject_class = (GObjectClass *) klass;
139   gstclock_class = (GstClockClass *) klass;
141   parent_class = g_type_class_peek_parent (klass);
143   g_type_class_add_private (klass, sizeof (GstSystemClockPrivate));
145   gobject_class->dispose = gst_system_clock_dispose;
146   gobject_class->set_property = gst_system_clock_set_property;
147   gobject_class->get_property = gst_system_clock_get_property;
149   g_object_class_install_property (gobject_class, PROP_CLOCK_TYPE,
150       g_param_spec_enum ("clock-type", "Clock type",
151           "The type of underlying clock implementation used",
152           GST_TYPE_CLOCK_TYPE, DEFAULT_CLOCK_TYPE,
153           G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
155   gstclock_class->get_internal_time = gst_system_clock_get_internal_time;
156   gstclock_class->get_resolution = gst_system_clock_get_resolution;
157   gstclock_class->wait_jitter = gst_system_clock_id_wait_jitter;
158   gstclock_class->wait_async = gst_system_clock_id_wait_async;
159   gstclock_class->unschedule = gst_system_clock_id_unschedule;
162 static void
163 gst_system_clock_init (GstSystemClock * clock)
165   GST_OBJECT_FLAG_SET (clock,
166       GST_CLOCK_FLAG_CAN_DO_SINGLE_SYNC |
167       GST_CLOCK_FLAG_CAN_DO_SINGLE_ASYNC |
168       GST_CLOCK_FLAG_CAN_DO_PERIODIC_SYNC |
169       GST_CLOCK_FLAG_CAN_DO_PERIODIC_ASYNC);
171   clock->priv = GST_SYSTEM_CLOCK_GET_PRIVATE (clock);
173   clock->priv->clock_type = DEFAULT_CLOCK_TYPE;
174   clock->priv->timer = gst_poll_new_timer ();
176 #ifdef G_OS_WIN32
177   QueryPerformanceFrequency (&clock->priv->frequency);
178   /* can be 0 if the hardware does not have hardware support */
179   if (clock->priv->frequency.QuadPart != 0)
180     /* we take a base time so that time starts from 0 to ease debugging */
181     QueryPerformanceCounter (&clock->priv->start);
182 #endif /* G_OS_WIN32 */
184 #if 0
185   /* Uncomment this to start the async clock thread straight away */
186   GST_OBJECT_LOCK (clock);
187   gst_system_clock_start_async (clock);
188   GST_OBJECT_UNLOCK (clock);
189 #endif
192 static void
193 gst_system_clock_dispose (GObject * object)
195   GstClock *clock = (GstClock *) object;
196   GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock);
197   GList *entries;
199   /* else we have to stop the thread */
200   GST_OBJECT_LOCK (clock);
201   sysclock->stopping = TRUE;
202   /* unschedule all entries */
203   for (entries = clock->entries; entries; entries = g_list_next (entries)) {
204     GstClockEntry *entry = (GstClockEntry *) entries->data;
206     GST_CAT_DEBUG (GST_CAT_CLOCK, "unscheduling entry %p", entry);
207     SET_ENTRY_STATUS (entry, GST_CLOCK_UNSCHEDULED);
208   }
209   GST_CLOCK_BROADCAST (clock);
210   gst_system_clock_add_wakeup (sysclock);
211   GST_OBJECT_UNLOCK (clock);
213   if (sysclock->thread)
214     g_thread_join (sysclock->thread);
215   sysclock->thread = NULL;
216   GST_CAT_DEBUG (GST_CAT_CLOCK, "joined thread");
218   g_list_foreach (clock->entries, (GFunc) gst_clock_id_unref, NULL);
219   g_list_free (clock->entries);
220   clock->entries = NULL;
222   gst_poll_free (sysclock->priv->timer);
224   G_OBJECT_CLASS (parent_class)->dispose (object);
226   if (_the_system_clock == clock) {
227     _the_system_clock = NULL;
228     GST_CAT_DEBUG (GST_CAT_CLOCK, "disposed system clock");
229   }
232 static void
233 gst_system_clock_set_property (GObject * object, guint prop_id,
234     const GValue * value, GParamSpec * pspec)
236   GstSystemClock *sysclock = GST_SYSTEM_CLOCK (object);
238   switch (prop_id) {
239     case PROP_CLOCK_TYPE:
240       sysclock->priv->clock_type = (GstClockType) g_value_get_enum (value);
241       GST_CAT_DEBUG (GST_CAT_CLOCK, "clock-type set to %d",
242           sysclock->priv->clock_type);
243       break;
244     default:
245       G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
246       break;
247   }
250 static void
251 gst_system_clock_get_property (GObject * object, guint prop_id, GValue * value,
252     GParamSpec * pspec)
254   GstSystemClock *sysclock = GST_SYSTEM_CLOCK (object);
256   switch (prop_id) {
257     case PROP_CLOCK_TYPE:
258       g_value_set_enum (value, sysclock->priv->clock_type);
259       break;
260     default:
261       G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
262       break;
263   }
266 /**
267  * gst_system_clock_obtain:
268  *
269  * Get a handle to the default system clock. The refcount of the
270  * clock will be increased so you need to unref the clock after
271  * usage.
272  *
273  * Returns: (transfer full): the default clock.
274  *
275  * MT safe.
276  */
277 GstClock *
278 gst_system_clock_obtain (void)
280   GstClock *clock;
282   g_static_mutex_lock (&_gst_sysclock_mutex);
283   clock = _the_system_clock;
285   if (clock == NULL) {
286     GST_CAT_DEBUG (GST_CAT_CLOCK, "creating new static system clock");
287     clock = g_object_new (GST_TYPE_SYSTEM_CLOCK,
288         "name", "GstSystemClock", NULL);
290     /* we created the global clock; take ownership so
291      * we can hand out instances later */
292     gst_object_ref_sink (clock);
294     _the_system_clock = clock;
295     g_static_mutex_unlock (&_gst_sysclock_mutex);
296   } else {
297     g_static_mutex_unlock (&_gst_sysclock_mutex);
298     GST_CAT_DEBUG (GST_CAT_CLOCK, "returning static system clock");
299   }
301   /* we ref it since we are a clock factory. */
302   gst_object_ref (clock);
303   return clock;
306 static void
307 gst_system_clock_remove_wakeup (GstSystemClock * sysclock)
309   g_return_if_fail (sysclock->priv->wakeup_count > 0);
311   sysclock->priv->wakeup_count--;
312   if (sysclock->priv->wakeup_count == 0) {
313     /* read the control socket byte when we removed the last wakeup count */
314     GST_CAT_DEBUG (GST_CAT_CLOCK, "reading control");
315     while (!gst_poll_read_control (sysclock->priv->timer)) {
316       g_warning ("gstsystemclock: read control failed, trying again\n");
317     }
318     GST_CLOCK_BROADCAST (sysclock);
319   }
320   GST_CAT_DEBUG (GST_CAT_CLOCK, "wakeup count %d",
321       sysclock->priv->wakeup_count);
324 static void
325 gst_system_clock_add_wakeup (GstSystemClock * sysclock)
327   /* only write the control socket for the first wakeup */
328   if (sysclock->priv->wakeup_count == 0) {
329     GST_CAT_DEBUG (GST_CAT_CLOCK, "writing control");
330     while (!gst_poll_write_control (sysclock->priv->timer)) {
331       if (errno == EAGAIN || errno == EWOULDBLOCK || errno == EINTR) {
332         g_warning
333             ("gstsystemclock: write control failed in wakeup_async, trying again: %d:%s\n",
334             errno, g_strerror (errno));
335       } else {
336         g_critical
337             ("gstsystemclock: write control failed in wakeup_async: %d:%s\n",
338             errno, g_strerror (errno));
339         return;
340       }
341     }
342   }
343   sysclock->priv->wakeup_count++;
344   GST_CAT_DEBUG (GST_CAT_CLOCK, "wakeup count %d",
345       sysclock->priv->wakeup_count);
348 static void
349 gst_system_clock_wait_wakeup (GstSystemClock * sysclock)
351   while (sysclock->priv->wakeup_count > 0) {
352     GST_CLOCK_WAIT (sysclock);
353   }
356 /* this thread reads the sorted clock entries from the queue.
357  *
358  * It waits on each of them and fires the callback when the timeout occurs.
359  *
360  * When an entry in the queue was canceled before we wait for it, it is
361  * simply skipped.
362  *
363  * When waiting for an entry, it can become canceled, in that case we don't
364  * call the callback but move to the next item in the queue.
365  *
366  * MT safe.
367  */
368 static void
369 gst_system_clock_async_thread (GstClock * clock)
371   GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock);
373   GST_CAT_DEBUG (GST_CAT_CLOCK, "enter system clock thread");
374   GST_OBJECT_LOCK (clock);
375   /* signal spinup */
376   GST_CLOCK_BROADCAST (clock);
377   /* now enter our (almost) infinite loop */
378   while (!sysclock->stopping) {
379     GstClockEntry *entry;
380     GstClockTime requested;
381     GstClockReturn res;
383     /* check if something to be done */
384     while (clock->entries == NULL) {
385       GST_CAT_DEBUG (GST_CAT_CLOCK, "no clock entries, waiting..");
386       /* wait for work to do */
387       GST_CLOCK_WAIT (clock);
388       GST_CAT_DEBUG (GST_CAT_CLOCK, "got signal");
389       /* clock was stopping, exit */
390       if (sysclock->stopping)
391         goto exit;
392     }
394     /* see if we have a pending wakeup because the order of the list
395      * changed. */
396     if (sysclock->priv->async_wakeup) {
397       GST_CAT_DEBUG (GST_CAT_CLOCK, "clear async wakeup");
398       gst_system_clock_remove_wakeup (sysclock);
399       sysclock->priv->async_wakeup = FALSE;
400     }
402     /* pick the next entry */
403     entry = clock->entries->data;
404     GST_OBJECT_UNLOCK (clock);
406     requested = entry->time;
408     /* now wait for the entry, we already hold the lock */
409     res =
410         gst_system_clock_id_wait_jitter_unlocked (clock, (GstClockID) entry,
411         NULL, FALSE);
413     GST_OBJECT_LOCK (clock);
415     switch (res) {
416       case GST_CLOCK_UNSCHEDULED:
417         /* entry was unscheduled, move to the next */
418         GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry %p unscheduled", entry);
419         goto next_entry;
420       case GST_CLOCK_OK:
421       case GST_CLOCK_EARLY:
422       {
423         /* entry timed out normally, fire the callback and move to the next
424          * entry */
425         GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry %p timed out", entry);
426         if (entry->func) {
427           /* unlock before firing the callback */
428           GST_OBJECT_UNLOCK (clock);
429           entry->func (clock, entry->time, (GstClockID) entry,
430               entry->user_data);
431           GST_OBJECT_LOCK (clock);
432         }
433         if (entry->type == GST_CLOCK_ENTRY_PERIODIC) {
434           GST_CAT_DEBUG (GST_CAT_CLOCK, "updating periodic entry %p", entry);
435           /* adjust time now */
436           entry->time = requested + entry->interval;
437           /* and resort the list now */
438           clock->entries =
439               g_list_sort (clock->entries, gst_clock_id_compare_func);
440           /* and restart */
441           continue;
442         } else {
443           GST_CAT_DEBUG (GST_CAT_CLOCK, "moving to next entry");
444           goto next_entry;
445         }
446       }
447       case GST_CLOCK_BUSY:
448         /* somebody unlocked the entry but is was not canceled, This means that
449          * either a new entry was added in front of the queue or some other entry
450          * was canceled. Whatever it is, pick the head entry of the list and
451          * continue waiting. */
452         GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry %p needs restart", entry);
454         /* we set the entry back to the OK state. This is needed so that the
455          * _unschedule() code can see if an entry is currently being waited
456          * on (when its state is BUSY). */
457         SET_ENTRY_STATUS (entry, GST_CLOCK_OK);
458         continue;
459       default:
460         GST_CAT_DEBUG (GST_CAT_CLOCK,
461             "strange result %d waiting for %p, skipping", res, entry);
462         g_warning ("%s: strange result %d waiting for %p, skipping",
463             GST_OBJECT_NAME (clock), res, entry);
464         goto next_entry;
465     }
466   next_entry:
467     /* we remove the current entry and unref it */
468     clock->entries = g_list_remove (clock->entries, entry);
469     gst_clock_id_unref ((GstClockID) entry);
470   }
471 exit:
472   /* signal exit */
473   GST_CLOCK_BROADCAST (clock);
474   GST_OBJECT_UNLOCK (clock);
475   GST_CAT_DEBUG (GST_CAT_CLOCK, "exit system clock thread");
478 #ifdef HAVE_POSIX_TIMERS
479 static inline clockid_t
480 clock_type_to_posix_id (GstClockType clock_type)
482 #ifdef HAVE_MONOTONIC_CLOCK
483   if (clock_type == GST_CLOCK_TYPE_MONOTONIC)
484     return CLOCK_MONOTONIC;
485   else
486 #endif
487     return CLOCK_REALTIME;
489 #endif
491 /* MT safe */
492 static GstClockTime
493 gst_system_clock_get_internal_time (GstClock * clock)
495 #ifdef G_OS_WIN32
496   GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock);
498   if (sysclock->priv->frequency.QuadPart != 0) {
499     LARGE_INTEGER now;
501     /* we prefer the highly accurate performance counters on windows */
502     QueryPerformanceCounter (&now);
504     return gst_util_uint64_scale (now.QuadPart - sysclock->priv->start.QuadPart,
505         GST_SECOND, sysclock->priv->frequency.QuadPart);
506   } else
507 #endif /* G_OS_WIN32 */
508 #if !defined HAVE_POSIX_TIMERS
509   {
510     GTimeVal timeval;
512     g_get_current_time (&timeval);
514     return GST_TIMEVAL_TO_TIME (timeval);
515   }
516 #else
517   {
518     GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock);
519     clockid_t ptype;
520     struct timespec ts;
522     ptype = clock_type_to_posix_id (sysclock->priv->clock_type);
524     if (G_UNLIKELY (clock_gettime (ptype, &ts)))
525       return GST_CLOCK_TIME_NONE;
527     return GST_TIMESPEC_TO_TIME (ts);
528   }
529 #endif
532 static guint64
533 gst_system_clock_get_resolution (GstClock * clock)
535 #ifdef G_OS_WIN32
536   GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock);
538   if (sysclock->priv->frequency.QuadPart != 0) {
539     return GST_SECOND / sysclock->priv->frequency.QuadPart;
540   } else
541 #endif /* G_OS_WIN32 */
542 #ifdef HAVE_POSIX_TIMERS
543   {
544     GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock);
545     clockid_t ptype;
546     struct timespec ts;
548     ptype = clock_type_to_posix_id (sysclock->priv->clock_type);
550     if (G_UNLIKELY (clock_getres (ptype, &ts)))
551       return GST_CLOCK_TIME_NONE;
553     return GST_TIMESPEC_TO_TIME (ts);
554   }
555 #else
556   {
557     return 1 * GST_USECOND;
558   }
559 #endif
562 /* synchronously wait on the given GstClockEntry.
563  *
564  * We do this by blocking on the global GstPoll timer with
565  * the requested timeout. This allows us to unblock the
566  * entry by writing on the control fd.
567  *
568  * Note that writing the global GstPoll unlocks all waiting entries. So
569  * we need to check if an unlocked entry has changed when it unlocks.
570  *
571  * Entries that arrive too late are simply not waited on and a
572  * GST_CLOCK_EARLY result is returned.
573  *
574  * MT safe.
575  */
576 static GstClockReturn
577 gst_system_clock_id_wait_jitter_unlocked (GstClock * clock,
578     GstClockEntry * entry, GstClockTimeDiff * jitter, gboolean restart)
580   GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock);
581   GstClockTime entryt, now;
582   GstClockTimeDiff diff;
583   GstClockReturn status;
585   if (G_UNLIKELY (GET_ENTRY_STATUS (entry) == GST_CLOCK_UNSCHEDULED))
586     return GST_CLOCK_UNSCHEDULED;
588   /* need to call the overridden method because we want to sync against the time
589    * of the clock, whatever the subclass uses as a clock. */
590   now = gst_clock_get_time (clock);
592   /* get the time of the entry */
593   entryt = GST_CLOCK_ENTRY_TIME (entry);
595   /* the diff of the entry with the clock is the amount of time we have to
596    * wait */
597   diff = GST_CLOCK_DIFF (now, entryt);
598   if (G_LIKELY (jitter))
599     *jitter = -diff;
601   GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p"
602       " time %" GST_TIME_FORMAT
603       " now %" GST_TIME_FORMAT
604       " diff (time-now) %" G_GINT64_FORMAT,
605       entry, GST_TIME_ARGS (entryt), GST_TIME_ARGS (now), diff);
607   if (G_LIKELY (diff > 0)) {
608 #ifdef WAIT_DEBUGGING
609     GstClockTime final;
610 #endif
612     while (TRUE) {
613       gint pollret;
615       do {
616         status = GET_ENTRY_STATUS (entry);
618         /* stop when we are unscheduled */
619         if (G_UNLIKELY (status == GST_CLOCK_UNSCHEDULED))
620           goto done;
622         /* mark the entry as busy but watch out for intermediate unscheduled
623          * statuses */
624       } while (G_UNLIKELY (!CAS_ENTRY_STATUS (entry, status, GST_CLOCK_BUSY)));
626       /* now wait on the entry, it either times out or the fd is written. The
627        * status of the entry is only BUSY around the poll. */
628       pollret = gst_poll_wait (sysclock->priv->timer, diff);
630       /* get the new status, mark as DONE. We do this so that the unschedule
631        * function knows when we left the poll and doesn't need to wakeup the
632        * poll anymore. */
633       do {
634         status = GET_ENTRY_STATUS (entry);
635         /* we were unscheduled, exit immediately */
636         if (G_UNLIKELY (status == GST_CLOCK_UNSCHEDULED))
637           break;
638       } while (G_UNLIKELY (!CAS_ENTRY_STATUS (entry, status, GST_CLOCK_DONE)));
640       GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p unlocked, status %d, ret %d",
641           entry, status, pollret);
643       if (G_UNLIKELY (status == GST_CLOCK_UNSCHEDULED)) {
644         /* try to clean up The unschedule function managed to set the status to
645          * unscheduled. We now take the lock and mark the entry as unscheduled.
646          * This makes sure that the unschedule function doesn't perform a
647          * wakeup anymore. If the unschedule function has a change to perform
648          * the wakeup before us, we clean up here */
649         GST_OBJECT_LOCK (sysclock);
650         entry->unscheduled = TRUE;
651         if (entry->woken_up) {
652           gst_system_clock_remove_wakeup (sysclock);
653         }
654         GST_OBJECT_UNLOCK (sysclock);
655         goto done;
656       } else {
657         if (G_UNLIKELY (pollret != 0)) {
658           /* some other id got unlocked */
659           if (!restart) {
660             /* this can happen if the entry got unlocked because of an async
661              * entry was added to the head of the async queue. */
662             GST_CAT_DEBUG (GST_CAT_CLOCK, "wakeup waiting for entry %p", entry);
663             goto done;
664           }
666           /* wait till all the entries got woken up */
667           GST_OBJECT_LOCK (sysclock);
668           gst_system_clock_wait_wakeup (sysclock);
669           GST_OBJECT_UNLOCK (sysclock);
671           GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p needs to be restarted",
672               entry);
673         } else {
674           GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p unlocked after timeout",
675               entry);
676         }
678         /* reschedule if gst_poll_wait returned early or we have to reschedule after
679          * an unlock*/
680         now = gst_clock_get_time (clock);
681         diff = GST_CLOCK_DIFF (now, entryt);
683         if (diff <= 0) {
684           /* timeout, this is fine, we can report success now */
685           status = GST_CLOCK_OK;
686           SET_ENTRY_STATUS (entry, status);
688           GST_CAT_DEBUG (GST_CAT_CLOCK,
689               "entry %p finished, diff %" G_GINT64_FORMAT, entry, diff);
691 #ifdef WAIT_DEBUGGING
692           final = gst_system_clock_get_internal_time (clock);
693           GST_CAT_DEBUG (GST_CAT_CLOCK, "Waited for %" G_GINT64_FORMAT
694               " got %" G_GINT64_FORMAT " diff %" G_GINT64_FORMAT
695               " %g target-offset %" G_GINT64_FORMAT " %g", entryt, now,
696               now - entryt,
697               (double) (GstClockTimeDiff) (now - entryt) / GST_SECOND,
698               (final - target),
699               ((double) (GstClockTimeDiff) (final - target)) / GST_SECOND);
700 #endif
701           goto done;
702         } else {
703           GST_CAT_DEBUG (GST_CAT_CLOCK,
704               "entry %p restart, diff %" G_GINT64_FORMAT, entry, diff);
705         }
706       }
707     }
708   } else {
709     /* we are right on time or too late */
710     if (G_UNLIKELY (diff == 0))
711       status = GST_CLOCK_OK;
712     else
713       status = GST_CLOCK_EARLY;
715     SET_ENTRY_STATUS (entry, status);
716   }
717 done:
718   return status;
721 static GstClockReturn
722 gst_system_clock_id_wait_jitter (GstClock * clock, GstClockEntry * entry,
723     GstClockTimeDiff * jitter)
725   return gst_system_clock_id_wait_jitter_unlocked (clock, entry, jitter, TRUE);
728 /* Start the async clock thread. Must be called with the object lock
729  * held */
730 static gboolean
731 gst_system_clock_start_async (GstSystemClock * clock)
733   GError *error = NULL;
735   if (G_LIKELY (clock->thread != NULL))
736     return TRUE;                /* Thread already running. Nothing to do */
738   clock->thread = g_thread_create ((GThreadFunc) gst_system_clock_async_thread,
739       clock, TRUE, &error);
740   if (G_UNLIKELY (error))
741     goto no_thread;
743   /* wait for it to spin up */
744   GST_CLOCK_WAIT (clock);
746   return TRUE;
748   /* ERRORS */
749 no_thread:
750   {
751     g_warning ("could not create async clock thread: %s", error->message);
752     g_error_free (error);
753   }
754   return FALSE;
757 /* Add an entry to the list of pending async waits. The entry is inserted
758  * in sorted order. If we inserted the entry at the head of the list, we
759  * need to signal the thread as it might either be waiting on it or waiting
760  * for a new entry.
761  *
762  * MT safe.
763  */
764 static GstClockReturn
765 gst_system_clock_id_wait_async (GstClock * clock, GstClockEntry * entry)
767   GstSystemClock *sysclock;
768   GstClockEntry *head;
770   sysclock = GST_SYSTEM_CLOCK_CAST (clock);
772   GST_CAT_DEBUG (GST_CAT_CLOCK, "adding async entry %p", entry);
774   GST_OBJECT_LOCK (clock);
775   /* Start the clock async thread if needed */
776   if (G_UNLIKELY (!gst_system_clock_start_async (sysclock)))
777     goto thread_error;
779   if (G_UNLIKELY (GET_ENTRY_STATUS (entry) == GST_CLOCK_UNSCHEDULED))
780     goto was_unscheduled;
782   if (clock->entries)
783     head = clock->entries->data;
784   else
785     head = NULL;
787   /* need to take a ref */
788   gst_clock_id_ref ((GstClockID) entry);
789   /* insert the entry in sorted order */
790   clock->entries = g_list_insert_sorted (clock->entries, entry,
791       gst_clock_id_compare_func);
793   /* only need to send the signal if the entry was added to the
794    * front, else the thread is just waiting for another entry and
795    * will get to this entry automatically. */
796   if (clock->entries->data == entry) {
797     GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry added to head %p", head);
798     if (head == NULL) {
799       /* the list was empty before, signal the cond so that the async thread can
800        * start taking a look at the queue */
801       GST_CAT_DEBUG (GST_CAT_CLOCK, "first entry, sending signal");
802       GST_CLOCK_BROADCAST (clock);
803     } else {
804       GstClockReturn status;
806       status = GET_ENTRY_STATUS (head);
807       GST_CAT_DEBUG (GST_CAT_CLOCK, "head entry %p status %d", head, status);
809       if (status == GST_CLOCK_BUSY) {
810         GST_CAT_DEBUG (GST_CAT_CLOCK, "head entry is busy");
811         /* the async thread was waiting for an entry, unlock the wait so that it
812          * looks at the new head entry instead, we only need to do this once */
813         if (!sysclock->priv->async_wakeup) {
814           GST_CAT_DEBUG (GST_CAT_CLOCK, "wakeup async thread");
815           sysclock->priv->async_wakeup = TRUE;
816           gst_system_clock_add_wakeup (sysclock);
817         }
818       }
819     }
820   }
821   GST_OBJECT_UNLOCK (clock);
823   return GST_CLOCK_OK;
825   /* ERRORS */
826 thread_error:
827   {
828     /* Could not start the async clock thread */
829     GST_OBJECT_UNLOCK (clock);
830     return GST_CLOCK_ERROR;
831   }
832 was_unscheduled:
833   {
834     GST_OBJECT_UNLOCK (clock);
835     return GST_CLOCK_UNSCHEDULED;
836   }
839 /* unschedule an entry. This will set the state of the entry to GST_CLOCK_UNSCHEDULED
840  * and will signal any thread waiting for entries to recheck their entry.
841  * We cannot really decide if the signal is needed or not because the entry
842  * could be waited on in async or sync mode.
843  *
844  * MT safe.
845  */
846 static void
847 gst_system_clock_id_unschedule (GstClock * clock, GstClockEntry * entry)
849   GstSystemClock *sysclock;
850   GstClockReturn status;
852   sysclock = GST_SYSTEM_CLOCK_CAST (clock);
854   GST_CAT_DEBUG (GST_CAT_CLOCK, "unscheduling entry %p", entry);
856   GST_OBJECT_LOCK (clock);
857   /* change the entry status to unscheduled */
858   do {
859     status = GET_ENTRY_STATUS (entry);
860   } while (G_UNLIKELY (!CAS_ENTRY_STATUS (entry, status,
861               GST_CLOCK_UNSCHEDULED)));
863   if (G_LIKELY (status == GST_CLOCK_BUSY)) {
864     /* the entry was being busy, wake up all entries so that they recheck their
865      * status. We cannot wake up just one entry because allocating such a
866      * datastructure for each entry would be too heavy and unlocking an entry
867      * is usually done when shutting down or some other exceptional case. */
868     GST_CAT_DEBUG (GST_CAT_CLOCK, "entry was BUSY, doing wakeup");
869     if (!entry->unscheduled && !entry->woken_up) {
870       gst_system_clock_add_wakeup (sysclock);
871       entry->woken_up = TRUE;
872     }
873   }
874   GST_OBJECT_UNLOCK (clock);