]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blob - libs/gst/base/gstbitreader.c
g_thread_create() is deprecated in GLib master, use g_thread_try_new() instead
[glsdk/gstreamer0-10.git] / libs / gst / base / gstbitreader.c
1 /* GStreamer
2  *
3  * Copyright (C) 2008 Sebastian Dröge <sebastian.droege@collabora.co.uk>.
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Library General Public
7  * License as published by the Free Software Foundation; either
8  * version 2 of the License, or (at your option) any later version.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
13  * Library General Public License for more details.
14  *
15  * You should have received a copy of the GNU Library General Public
16  * License along with this library; if not, write to the
17  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
18  * Boston, MA 02111-1307, USA.
19  */
21 #ifdef HAVE_CONFIG_H
22 #include "config.h"
23 #endif
25 #define GST_BIT_READER_DISABLE_INLINES
26 #include "gstbitreader.h"
28 #include <string.h>
30 /**
31  * SECTION:gstbitreader
32  * @short_description: Reads any number of bits from a memory buffer
33  *
34  * #GstBitReader provides a bit reader that can read any number of bits
35  * from a memory buffer. It provides functions for reading any number of bits
36  * into 8, 16, 32 and 64 bit variables.
37  */
39 /**
40  * gst_bit_reader_new:
41  * @data: Data from which the #GstBitReader should read
42  * @size: Size of @data in bytes
43  *
44  * Create a new #GstBitReader instance, which will read from @data.
45  *
46  * Free-function: gst_bit_reader_free
47  *
48  * Returns: (transfer full): a new #GstBitReader instance
49  *
50  * Since: 0.10.22
51  */
52 GstBitReader *
53 gst_bit_reader_new (const guint8 * data, guint size)
54 {
55   GstBitReader *ret = g_slice_new0 (GstBitReader);
57   ret->data = data;
58   ret->size = size;
60   return ret;
61 }
63 /**
64  * gst_bit_reader_new_from_buffer:
65  * @buffer: Buffer from which the #GstBitReader should read
66  *
67  * Create a new #GstBitReader instance, which will read from the
68  * #GstBuffer @buffer.
69  *
70  * Free-function: gst_bit_reader_free
71  *
72  * Returns: (transfer full): a new #GstBitReader instance
73  *
74  * Since: 0.10.22
75  */
76 GstBitReader *
77 gst_bit_reader_new_from_buffer (const GstBuffer * buffer)
78 {
79   g_return_val_if_fail (GST_IS_BUFFER (buffer), NULL);
81   return gst_bit_reader_new (GST_BUFFER_DATA (buffer),
82       GST_BUFFER_SIZE (buffer));
83 }
85 /**
86  * gst_bit_reader_free:
87  * @reader: (in) (transfer full): a #GstBitReader instance
88  *
89  * Frees a #GstBitReader instance, which was previously allocated by
90  * gst_bit_reader_new() or gst_bit_reader_new_from_buffer().
91  * 
92  * Since: 0.10.22
93  */
94 void
95 gst_bit_reader_free (GstBitReader * reader)
96 {
97   g_return_if_fail (reader != NULL);
99   g_slice_free (GstBitReader, reader);
102 /**
103  * gst_bit_reader_init:
104  * @reader: a #GstBitReader instance
105  * @data: (in) (array length=size): data from which the bit reader should read
106  * @size: Size of @data in bytes
107  *
108  * Initializes a #GstBitReader instance to read from @data. This function
109  * can be called on already initialized instances.
110  * 
111  * Since: 0.10.22
112  */
113 void
114 gst_bit_reader_init (GstBitReader * reader, const guint8 * data, guint size)
116   g_return_if_fail (reader != NULL);
118   reader->data = data;
119   reader->size = size;
120   reader->byte = reader->bit = 0;
123 /**
124  * gst_bit_reader_init_from_buffer:
125  * @reader: a #GstBitReader instance
126  * @buffer: (transfer none): Buffer from which the #GstBitReader should read
127  *
128  * Initializes a #GstBitReader instance to read from @buffer. This function
129  * can be called on already initialized instances.
130  * 
131  * Since: 0.10.22
132  */
133 void
134 gst_bit_reader_init_from_buffer (GstBitReader * reader,
135     const GstBuffer * buffer)
137   g_return_if_fail (GST_IS_BUFFER (buffer));
139   gst_bit_reader_init (reader, GST_BUFFER_DATA (buffer),
140       GST_BUFFER_SIZE (buffer));
143 /**
144  * gst_bit_reader_set_pos:
145  * @reader: a #GstBitReader instance
146  * @pos: The new position in bits
147  *
148  * Sets the new position of a #GstBitReader instance to @pos in bits.
149  *
150  * Returns: %TRUE if the position could be set successfully, %FALSE
151  * otherwise.
152  * 
153  * Since: 0.10.22
154  */
155 gboolean
156 gst_bit_reader_set_pos (GstBitReader * reader, guint pos)
158   g_return_val_if_fail (reader != NULL, FALSE);
160   if (pos > reader->size * 8)
161     return FALSE;
163   reader->byte = pos / 8;
164   reader->bit = pos % 8;
166   return TRUE;
169 /**
170  * gst_bit_reader_get_pos:
171  * @reader: a #GstBitReader instance
172  *
173  * Returns the current position of a #GstBitReader instance in bits.
174  *
175  * Returns: The current position of @reader in bits.
176  * 
177  * Since: 0.10.22
178  */
179 guint
180 gst_bit_reader_get_pos (const GstBitReader * reader)
182   return _gst_bit_reader_get_pos_inline (reader);
185 /**
186  * gst_bit_reader_get_remaining:
187  * @reader: a #GstBitReader instance
188  *
189  * Returns the remaining number of bits of a #GstBitReader instance.
190  *
191  * Returns: The remaining number of bits of @reader instance.
192  * 
193  * Since: 0.10.22
194  */
195 guint
196 gst_bit_reader_get_remaining (const GstBitReader * reader)
198   return _gst_bit_reader_get_remaining_inline (reader);
201 /**
202  * gst_bit_reader_get_size:
203  * @reader: a #GstBitReader instance
204  *
205  * Returns the total number of bits of a #GstBitReader instance.
206  *
207  * Returns: The total number of bits of @reader instance.
208  * 
209  * Since: 0.10.26
210  */
211 guint
212 gst_bit_reader_get_size (const GstBitReader * reader)
214   return _gst_bit_reader_get_size_inline (reader);
217 /**
218  * gst_bit_reader_skip:
219  * @reader: a #GstBitReader instance
220  * @nbits: the number of bits to skip
221  *
222  * Skips @nbits bits of the #GstBitReader instance.
223  *
224  * Returns: %TRUE if @nbits bits could be skipped, %FALSE otherwise.
225  * 
226  * Since: 0.10.22
227  */
228 gboolean
229 gst_bit_reader_skip (GstBitReader * reader, guint nbits)
231   return _gst_bit_reader_skip_inline (reader, nbits);
234 /**
235  * gst_bit_reader_skip_to_byte:
236  * @reader: a #GstBitReader instance
237  *
238  * Skips until the next byte.
239  *
240  * Returns: %TRUE if successful, %FALSE otherwise.
241  * 
242  * Since: 0.10.22
243  */
244 gboolean
245 gst_bit_reader_skip_to_byte (GstBitReader * reader)
247   return _gst_bit_reader_skip_to_byte_inline (reader);
250 /**
251  * gst_bit_reader_get_bits_uint8:
252  * @reader: a #GstBitReader instance
253  * @val: (out): Pointer to a #guint8 to store the result
254  * @nbits: number of bits to read
255  *
256  * Read @nbits bits into @val and update the current position.
257  *
258  * Returns: %TRUE if successful, %FALSE otherwise.
259  * 
260  * Since: 0.10.22
261  */
263 /**
264  * gst_bit_reader_get_bits_uint16:
265  * @reader: a #GstBitReader instance
266  * @val: (out): Pointer to a #guint16 to store the result
267  * @nbits: number of bits to read
268  *
269  * Read @nbits bits into @val and update the current position.
270  *
271  * Returns: %TRUE if successful, %FALSE otherwise.
272  * 
273  * Since: 0.10.22
274  */
276 /**
277  * gst_bit_reader_get_bits_uint32:
278  * @reader: a #GstBitReader instance
279  * @val: (out): Pointer to a #guint32 to store the result
280  * @nbits: number of bits to read
281  *
282  * Read @nbits bits into @val and update the current position.
283  *
284  * Returns: %TRUE if successful, %FALSE otherwise.
285  * 
286  * Since: 0.10.22
287  */
289 /**
290  * gst_bit_reader_get_bits_uint64:
291  * @reader: a #GstBitReader instance
292  * @val: (out): Pointer to a #guint64 to store the result
293  * @nbits: number of bits to read
294  *
295  * Read @nbits bits into @val and update the current position.
296  *
297  * Returns: %TRUE if successful, %FALSE otherwise.
298  * 
299  * Since: 0.10.22
300  */
302 /**
303  * gst_bit_reader_peek_bits_uint8:
304  * @reader: a #GstBitReader instance
305  * @val: (out): Pointer to a #guint8 to store the result
306  * @nbits: number of bits to read
307  *
308  * Read @nbits bits into @val but keep the current position.
309  *
310  * Returns: %TRUE if successful, %FALSE otherwise.
311  * 
312  * Since: 0.10.22
313  */
315 /**
316  * gst_bit_reader_peek_bits_uint16:
317  * @reader: a #GstBitReader instance
318  * @val: (out): Pointer to a #guint16 to store the result
319  * @nbits: number of bits to read
320  *
321  * Read @nbits bits into @val but keep the current position.
322  *
323  * Returns: %TRUE if successful, %FALSE otherwise.
324  * 
325  * Since: 0.10.22
326  */
328 /**
329  * gst_bit_reader_peek_bits_uint32:
330  * @reader: a #GstBitReader instance
331  * @val: (out): Pointer to a #guint32 to store the result
332  * @nbits: number of bits to read
333  *
334  * Read @nbits bits into @val but keep the current position.
335  *
336  * Returns: %TRUE if successful, %FALSE otherwise.
337  * 
338  * Since: 0.10.22
339  */
341 /**
342  * gst_bit_reader_peek_bits_uint64:
343  * @reader: a #GstBitReader instance
344  * @val: (out): Pointer to a #guint64 to store the result
345  * @nbits: number of bits to read
346  *
347  * Read @nbits bits into @val but keep the current position.
348  *
349  * Returns: %TRUE if successful, %FALSE otherwise.
350  * 
351  * Since: 0.10.22
352  */
354 #define GST_BIT_READER_READ_BITS(bits) \
355 gboolean \
356 gst_bit_reader_peek_bits_uint##bits (const GstBitReader *reader, guint##bits *val, guint nbits) \
357 { \
358   return _gst_bit_reader_peek_bits_uint##bits##_inline (reader, val, nbits); \
359 } \
361 gboolean \
362 gst_bit_reader_get_bits_uint##bits (GstBitReader *reader, guint##bits *val, guint nbits) \
363 { \
364   return _gst_bit_reader_get_bits_uint##bits##_inline (reader, val, nbits); \
367 GST_BIT_READER_READ_BITS (8);
368 GST_BIT_READER_READ_BITS (16);
369 GST_BIT_READER_READ_BITS (32);
370 GST_BIT_READER_READ_BITS (64);