Make gstcheck stuff show up in docs (still needs to be documented properly though).
[glsdk/gstreamer0-10.git] / libs / gst / check / gstbufferstraw.c
1 /* GStreamer
2  *
3  * unit testing helper lib
4  *
5  * Copyright (C) 2006 Andy Wingo <wingo at pobox.com>
6  *
7  * This library is free software; you can redistribute it and/or
8  * modify it under the terms of the GNU Library General Public
9  * License as published by the Free Software Foundation; either
10  * version 2 of the License, or (at your option) any later version.
11  *
12  * This library is distributed in the hope that it will be useful,
13  * but WITHOUT ANY WARRANTY; without even the implied warranty of
14  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
15  * Library General Public License for more details.
16  *
17  * You should have received a copy of the GNU Library General Public
18  * License along with this library; if not, write to the
19  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20  * Boston, MA 02111-1307, USA.
21  */
23 /**
24  * SECTION:gstcheckbufferstraw
25  * @short_description: Buffer interception code for GStreamer unit tests
26  *
27  * These macros and functions are for internal use of the unit tests found
28  * inside the 'check' directories of various GStreamer packages.
29  */
31 #include "gstbufferstraw.h"
33 static GCond *cond = NULL;
34 static GMutex *lock = NULL;
35 static GstBuffer *buf = NULL;
36 static gulong id;
38 /* called for every buffer.  Waits until the global "buf" variable is unset,
39  * then sets it to the buffer received, and signals. */
40 static gboolean
41 buffer_probe (GstPad * pad, GstBuffer * buffer, gpointer unused)
42 {
43   g_mutex_lock (lock);
45   while (buf != NULL)
46     g_cond_wait (cond, lock);
48   /* increase the refcount because we store it globally for others to use */
49   buf = gst_buffer_ref (buffer);
51   g_cond_signal (cond);
53   g_mutex_unlock (lock);
55   return TRUE;
56 }
58 /**
59  * gst_buffer_straw_start_pipeline:
60  * @bin: the pipeline to run
61  * @pad: a pad on an element in @bin
62  *
63  * Sets up a pipeline for buffer sucking. This will allow you to call
64  * gst_buffer_straw_get_buffer() to access buffers as they pass over @pad.
65  *
66  * This function is normally used in unit tests that want to verify that a
67  * particular element is outputting correct buffers. For example, you would make
68  * a pipeline via gst_parse_launch(), pull out the pad you want to monitor, then
69  * call gst_buffer_straw_get_buffer() to get the buffers that pass through @pad.
70  * The pipeline will block until you have sucked off the buffers.
71  *
72  * This function will set the state of @bin to PLAYING; to clean up, be sure to
73  * call gst_buffer_straw_stop_pipeline().
74  *
75  * Note that you may not start two buffer straws at the same time. This function
76  * is intended for unit tests, not general API use. In fact it calls fail_if
77  * from libcheck, so you cannot use it outside unit tests.
78  */
79 void
80 gst_buffer_straw_start_pipeline (GstElement * bin, GstPad * pad)
81 {
82   GstStateChangeReturn ret;
84   id = gst_pad_add_buffer_probe (pad, G_CALLBACK (buffer_probe), NULL);
86   cond = g_cond_new ();
87   lock = g_mutex_new ();
89   ret = gst_element_set_state (bin, GST_STATE_PLAYING);
90   fail_if (ret == GST_STATE_CHANGE_FAILURE, "Could not start test pipeline");
91   if (ret == GST_STATE_CHANGE_ASYNC) {
92     ret = gst_element_get_state (bin, NULL, NULL, GST_CLOCK_TIME_NONE);
93     fail_if (ret != GST_STATE_CHANGE_SUCCESS, "Could not start test pipeline");
94   }
95 }
97 /**
98  * gst_buffer_straw_get_buffer:
99  * @bin: the pipeline previously started via gst_buffer_straw_start_pipeline()
100  * @pad: the pad previously passed to gst_buffer_straw_start_pipeline()
101  *
102  * Get one buffer from @pad. Implemented via buffer probes. This function will
103  * block until the pipeline passes a buffer over @pad, so for robust behavior
104  * in unit tests, you need to use check's timeout to fail out in the case that a
105  * buffer never arrives.
106  *
107  * You must have previously called gst_buffer_straw_start_pipeline() on
108  * @pipeline and @pad.
109  */
110 GstBuffer *
111 gst_buffer_straw_get_buffer (GstElement * bin, GstPad * pad)
113   GstBuffer *ret;
115   g_mutex_lock (lock);
117   while (buf == NULL)
118     g_cond_wait (cond, lock);
120   ret = buf;
121   buf = NULL;
123   g_cond_signal (cond);
125   g_mutex_unlock (lock);
127   return ret;
130 /**
131  * gst_buffer_straw_stop_pipeline:
132  * @bin: the pipeline previously started via gst_buffer_straw_start_pipeline()
133  * @pad: the pad previously passed to gst_buffer_straw_start_pipeline()
134  *
135  * Set @bin to #GST_STATE_NULL and release resource allocated in
136  * gst_buffer_straw_start_pipeline().
137  *
138  * You must have previously called gst_buffer_straw_start_pipeline() on
139  * @pipeline and @pad.
140  */
141 void
142 gst_buffer_straw_stop_pipeline (GstElement * bin, GstPad * pad)
144   GstStateChangeReturn ret;
146   g_mutex_lock (lock);
147   if (buf)
148     gst_buffer_unref (buf);
149   buf = NULL;
150   gst_pad_remove_buffer_probe (pad, (guint) id);
151   id = 0;
152   g_cond_signal (cond);
153   g_mutex_unlock (lock);
155   ret = gst_element_set_state (bin, GST_STATE_NULL);
156   fail_if (ret == GST_STATE_CHANGE_FAILURE, "Could not stop test pipeline");
157   if (ret == GST_STATE_CHANGE_ASYNC) {
158     ret = gst_element_get_state (bin, NULL, NULL, GST_CLOCK_TIME_NONE);
159     fail_if (ret != GST_STATE_CHANGE_SUCCESS, "Could not stop test pipeline");
160   }
162   g_mutex_lock (lock);
163   if (buf)
164     gst_buffer_unref (buf);
165   buf = NULL;
166   g_mutex_unlock (lock);
168   g_mutex_free (lock);
169   g_cond_free (cond);
171   lock = NULL;
172   cond = NULL;