DEBIAN: Debianization
[glsdk/gstreamer0-10.git] / libs / gst / check / gstbufferstraw.h
1 /* GStreamer
2  *
3  * Copyright (C) 2006 Andy Wingo <wingo at pobox.com>
4  *
5  * This library is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU Library General Public
7  * License as published by the Free Software Foundation; either
8  * version 2 of the License, or (at your option) any later version.
9  *
10  * This library is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
13  * Library General Public License for more details.
14  *
15  * You should have received a copy of the GNU Library General Public
16  * License along with this library; if not, write to the
17  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
18  * Boston, MA 02111-1307, USA.
19  */
21 #ifndef __GST_BUFFER_STRAW_H__
22 #define __GST_BUFFER_STRAW_H__
25 #include <gst/check/gstcheck.h>
27 G_BEGIN_DECLS
29 void gst_buffer_straw_start_pipeline (GstElement * bin, GstPad * pad);
30 GstBuffer *gst_buffer_straw_get_buffer (GstElement * bin, GstPad * pad);
31 void gst_buffer_straw_stop_pipeline (GstElement * bin, GstPad * pad);
33 G_END_DECLS
35 #endif /* __GST_BUFFER_STRAW_H__ */