g_thread_create() is deprecated in GLib master, use g_thread_try_new() instead
[glsdk/gstreamer0-10.git] / libs / gst / check / gstcheck.c
1 /* GStreamer
2  *
3  * Common code for GStreamer unittests
4  *
5  * Copyright (C) 2004,2006 Thomas Vander Stichele <thomas at apestaart dot org>
6  * Copyright (C) 2008 Thijs Vermeir <thijsvermeir@gmail.com>
7  *
8  * This library is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU Library General Public
10  * License as published by the Free Software Foundation; either
11  * version 2 of the License, or (at your option) any later version.
12  *
13  * This library is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
16  * Library General Public License for more details.
17  *
18  * You should have received a copy of the GNU Library General Public
19  * License along with this library; if not, write to the
20  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
21  * Boston, MA 02111-1307, USA.
22  */
23 /**
24  * SECTION:gstcheck
25  * @short_description: Common code for GStreamer unit tests
26  *
27  * These macros and functions are for internal use of the unit tests found
28  * inside the 'check' directories of various GStreamer packages.
29  */
31 #include "gstcheck.h"
33 GST_DEBUG_CATEGORY (check_debug);
35 /* logging function for tests
36  * a test uses g_message() to log a debug line
37  * a gst unit test can be run with GST_TEST_DEBUG env var set to see the
38  * messages
39  */
41 gboolean _gst_check_threads_running = FALSE;
42 GList *thread_list = NULL;
43 GMutex *mutex;
44 GCond *start_cond;              /* used to notify main thread of thread startups */
45 GCond *sync_cond;               /* used to synchronize all threads and main thread */
47 GList *buffers = NULL;
48 GMutex *check_mutex = NULL;
49 GCond *check_cond = NULL;
51 /* FIXME 0.11: shouldn't _gst_check_debug be static? Not used anywhere */
52 gboolean _gst_check_debug = FALSE;
53 gboolean _gst_check_raised_critical = FALSE;
54 gboolean _gst_check_raised_warning = FALSE;
55 gboolean _gst_check_expecting_log = FALSE;
57 static void gst_check_log_message_func
58     (const gchar * log_domain, GLogLevelFlags log_level,
59     const gchar * message, gpointer user_data)
60 {
61   if (_gst_check_debug) {
62     g_print ("%s", message);
63   }
64 }
66 static void gst_check_log_critical_func
67     (const gchar * log_domain, GLogLevelFlags log_level,
68     const gchar * message, gpointer user_data)
69 {
70   if (!_gst_check_expecting_log) {
71     g_print ("\n\nUnexpected critical/warning: %s\n", message);
72     fail ("Unexpected critical/warning: %s", message);
73   }
75   if (_gst_check_debug) {
76     g_print ("\nExpected critical/warning: %s\n", message);
77   }
79   if (log_level & G_LOG_LEVEL_CRITICAL)
80     _gst_check_raised_critical = TRUE;
81   if (log_level & G_LOG_LEVEL_WARNING)
82     _gst_check_raised_warning = TRUE;
83 }
85 static gint
86 sort_plugins (GstPlugin * a, GstPlugin * b)
87 {
88   int ret;
90   ret = strcmp (gst_plugin_get_source (a), gst_plugin_get_source (b));
91   if (ret == 0)
92     ret = strcmp (gst_plugin_get_name (a), gst_plugin_get_name (b));
93   return ret;
94 }
96 static void
97 print_plugins (void)
98 {
99   GList *plugins, *l;
101   plugins = gst_default_registry_get_plugin_list ();
102   plugins = g_list_sort (plugins, (GCompareFunc) sort_plugins);
103   for (l = plugins; l != NULL; l = l->next) {
104     GstPlugin *plugin = GST_PLUGIN (l->data);
106     if (strcmp (gst_plugin_get_source (plugin), "BLACKLIST") != 0) {
107       GST_LOG ("%20s@%s", gst_plugin_get_name (plugin),
108           GST_STR_NULL (gst_plugin_get_filename (plugin)));
109     }
110   }
111   gst_plugin_list_free (plugins);
114 /* initialize GStreamer testing */
115 void
116 gst_check_init (int *argc, char **argv[])
118   gst_init (argc, argv);
120   GST_DEBUG_CATEGORY_INIT (check_debug, "check", 0, "check regression tests");
122   if (g_getenv ("GST_TEST_DEBUG"))
123     _gst_check_debug = TRUE;
125   g_log_set_handler (NULL, G_LOG_LEVEL_MESSAGE, gst_check_log_message_func,
126       NULL);
127   g_log_set_handler (NULL, G_LOG_LEVEL_CRITICAL | G_LOG_LEVEL_WARNING,
128       gst_check_log_critical_func, NULL);
129   g_log_set_handler ("GStreamer", G_LOG_LEVEL_CRITICAL | G_LOG_LEVEL_WARNING,
130       gst_check_log_critical_func, NULL);
131   g_log_set_handler ("GLib-GObject", G_LOG_LEVEL_CRITICAL | G_LOG_LEVEL_WARNING,
132       gst_check_log_critical_func, NULL);
133   g_log_set_handler ("Gst-Phonon", G_LOG_LEVEL_CRITICAL | G_LOG_LEVEL_WARNING,
134       gst_check_log_critical_func, NULL);
136   print_plugins ();
138   check_cond = g_cond_new ();
139   check_mutex = g_mutex_new ();
142 /* message checking */
143 void
144 gst_check_message_error (GstMessage * message, GstMessageType type,
145     GQuark domain, gint code)
147   GError *error;
148   gchar *debug;
150   fail_unless (GST_MESSAGE_TYPE (message) == type,
151       "message is of type %s instead of expected type %s",
152       gst_message_type_get_name (GST_MESSAGE_TYPE (message)),
153       gst_message_type_get_name (type));
154   gst_message_parse_error (message, &error, &debug);
155   fail_unless_equals_int (error->domain, domain);
156   fail_unless_equals_int (error->code, code);
157   g_error_free (error);
158   g_free (debug);
161 /* helper functions */
162 GstFlowReturn
163 gst_check_chain_func (GstPad * pad, GstBuffer * buffer)
165   GST_DEBUG ("chain_func: received buffer %p", buffer);
166   buffers = g_list_append (buffers, buffer);
168   g_mutex_lock (check_mutex);
169   g_cond_signal (check_cond);
170   g_mutex_unlock (check_mutex);
172   return GST_FLOW_OK;
175 /* setup an element for a filter test with mysrcpad and mysinkpad */
176 GstElement *
177 gst_check_setup_element (const gchar * factory)
179   GstElement *element;
181   GST_DEBUG ("setup_element");
183   element = gst_element_factory_make (factory, factory);
184   fail_if (element == NULL, "Could not create a '%s' element", factory);
185   ASSERT_OBJECT_REFCOUNT (element, factory, 1);
186   return element;
189 void
190 gst_check_teardown_element (GstElement * element)
192   GST_DEBUG ("teardown_element");
194   fail_unless (gst_element_set_state (element, GST_STATE_NULL) ==
195       GST_STATE_CHANGE_SUCCESS, "could not set to null");
196   ASSERT_OBJECT_REFCOUNT (element, "element", 1);
197   gst_object_unref (element);
200 /* FIXME: set_caps isn't that useful
201  */
202 GstPad *
203 gst_check_setup_src_pad (GstElement * element,
204     GstStaticPadTemplate * tmpl, GstCaps * caps)
206   GstPad *srcpad;
208   srcpad = gst_check_setup_src_pad_by_name (element, tmpl, "sink");
209   if (caps)
210     fail_unless (gst_pad_set_caps (srcpad, caps), "could not set caps on pad");
211   return srcpad;
214 GstPad *
215 gst_check_setup_src_pad_by_name (GstElement * element,
216     GstStaticPadTemplate * tmpl, const gchar * name)
218   GstPad *srcpad, *sinkpad;
220   /* sending pad */
221   srcpad = gst_pad_new_from_static_template (tmpl, "src");
222   GST_DEBUG_OBJECT (element, "setting up sending pad %p", srcpad);
223   fail_if (srcpad == NULL, "Could not create a srcpad");
224   ASSERT_OBJECT_REFCOUNT (srcpad, "srcpad", 1);
226   sinkpad = gst_element_get_static_pad (element, name);
227   if (sinkpad == NULL)
228     sinkpad = gst_element_get_request_pad (element, name);
229   fail_if (sinkpad == NULL, "Could not get sink pad from %s",
230       GST_ELEMENT_NAME (element));
231   ASSERT_OBJECT_REFCOUNT (sinkpad, "sinkpad", 2);
232   fail_unless (gst_pad_link (srcpad, sinkpad) == GST_PAD_LINK_OK,
233       "Could not link source and %s sink pads", GST_ELEMENT_NAME (element));
234   gst_object_unref (sinkpad);   /* because we got it higher up */
235   ASSERT_OBJECT_REFCOUNT (sinkpad, "sinkpad", 1);
237   return srcpad;
240 void
241 gst_check_teardown_pad_by_name (GstElement * element, const gchar * name)
243   GstPad *pad_peer, *pad_element;
245   /* clean up floating src pad */
246   pad_element = gst_element_get_static_pad (element, name);
247   /* We don't check the refcount here since there *might* be
248    * a pad cache holding an extra reference on pad_element.
249    * To get to a state where no pad cache will exist,
250    * we first unlink that pad. */
251   pad_peer = gst_pad_get_peer (pad_element);
253   if (pad_peer) {
254     if (gst_pad_get_direction (pad_element) == GST_PAD_SINK)
255       gst_pad_unlink (pad_peer, pad_element);
256     else
257       gst_pad_unlink (pad_element, pad_peer);
259     /* caps could have been set, make sure they get unset */
260     gst_pad_set_caps (pad_peer, NULL);
261   }
263   /* pad refs held by both creator and this function (through _get) */
264   ASSERT_OBJECT_REFCOUNT (pad_element, "element pad_element", 2);
265   gst_object_unref (pad_element);
266   /* one more ref is held by element itself */
268   if (pad_peer) {
269     /* pad refs held by both creator and this function (through _get_peer) */
270     ASSERT_OBJECT_REFCOUNT (pad_peer, "check pad_peer", 2);
271     gst_object_unref (pad_peer);
272     gst_object_unref (pad_peer);
273   }
276 void
277 gst_check_teardown_src_pad (GstElement * element)
279   gst_check_teardown_pad_by_name (element, "sink");
282 /* FIXME: set_caps isn't that useful; might want to check if fixed,
283  * then use set_use_fixed or somesuch */
284 GstPad *
285 gst_check_setup_sink_pad (GstElement * element, GstStaticPadTemplate * tmpl,
286     GstCaps * caps)
288   GstPad *sinkpad;
290   sinkpad = gst_check_setup_sink_pad_by_name (element, tmpl, "src");
291   if (caps)
292     fail_unless (gst_pad_set_caps (sinkpad, caps), "Could not set pad caps");
293   return sinkpad;
296 GstPad *
297 gst_check_setup_sink_pad_by_name (GstElement * element,
298     GstStaticPadTemplate * tmpl, const gchar * name)
300   GstPad *srcpad, *sinkpad;
302   /* receiving pad */
303   sinkpad = gst_pad_new_from_static_template (tmpl, "sink");
304   GST_DEBUG_OBJECT (element, "setting up receiving pad %p", sinkpad);
305   fail_if (sinkpad == NULL, "Could not create a sinkpad");
307   srcpad = gst_element_get_static_pad (element, name);
308   if (srcpad == NULL)
309     srcpad = gst_element_get_request_pad (element, name);
310   fail_if (srcpad == NULL, "Could not get source pad from %s",
311       GST_ELEMENT_NAME (element));
312   gst_pad_set_chain_function (sinkpad, gst_check_chain_func);
314   GST_DEBUG_OBJECT (element, "Linking element src pad and receiving sink pad");
315   fail_unless (gst_pad_link (srcpad, sinkpad) == GST_PAD_LINK_OK,
316       "Could not link %s source and sink pads", GST_ELEMENT_NAME (element));
317   gst_object_unref (srcpad);    /* because we got it higher up */
318   ASSERT_OBJECT_REFCOUNT (srcpad, "srcpad", 1);
320   GST_DEBUG_OBJECT (element, "set up srcpad, refcount is 1");
321   return sinkpad;
324 void
325 gst_check_teardown_sink_pad (GstElement * element)
327   gst_check_teardown_pad_by_name (element, "src");
330 /**
331  * gst_check_drop_buffers:
332  *
333  * Unref and remove all buffers that are in the global @buffers GList,
334  * emptying the list.
335  *
336  * Since: 0.10.18
337  */
338 void
339 gst_check_drop_buffers (void)
341   while (buffers != NULL) {
342     gst_buffer_unref (GST_BUFFER (buffers->data));
343     buffers = g_list_delete_link (buffers, buffers);
344   }
347 /**
348  * gst_check_caps_equal:
349  * @caps1: first caps to compare
350  * @caps2: second caps to compare
351  *
352  * Compare two caps with gst_caps_is_equal and fail unless they are
353  * equal.
354  *
355  * Since: 0.10.18
356  */
357 void
358 gst_check_caps_equal (GstCaps * caps1, GstCaps * caps2)
360   gchar *name1 = gst_caps_to_string (caps1);
361   gchar *name2 = gst_caps_to_string (caps2);
363   fail_unless (gst_caps_is_equal (caps1, caps2),
364       "caps ('%s') is not equal to caps ('%s')", name1, name2);
365   g_free (name1);
366   g_free (name2);
369 /**
370  * gst_check_element_push_buffer_list:
371  * @element_name: name of the element that needs to be created
372  * @buffer_in: a list of buffers that needs to be puched to the element
373  * @buffer_out: a list of buffers that we expect from the element
374  * @last_flow_return: the last buffer push needs to give this GstFlowReturn
375  *
376  * Create an @element with the factory with the name and push the buffers in
377  * @buffer_in to this element. The element should create the buffers equal to
378  * the buffers in @buffer_out. We only check the caps, size and the data of the
379  * buffers. This function unrefs the buffers in the two lists.
380  * The last_flow_return parameter indicates the expected flow return value from
381  * pushing the final buffer in the list.
382  * This can be used to set up a test which pushes some buffers and then an
383  * invalid buffer, when the final buffer is expected to fail, for example.
384  * 
385  * Since: 0.10.18
386  */
387 /* FIXME 0.11: rename this function now that there's GstBufferList? */
388 void
389 gst_check_element_push_buffer_list (const gchar * element_name,
390     GList * buffer_in, GList * buffer_out, GstFlowReturn last_flow_return)
392   GstCaps *sink_caps;
393   GstCaps *src_caps = NULL;
394   GstElement *element;
395   GstPad *pad_peer;
396   GstPad *sink_pad = NULL;
397   GstPad *src_pad;
398   GstBuffer *buffer;
400   /* check that there are no buffers waiting */
401   gst_check_drop_buffers ();
402   /* create the element */
403   element = gst_check_setup_element (element_name);
404   fail_if (element == NULL, "failed to create the element '%s'", element_name);
405   fail_unless (GST_IS_ELEMENT (element), "the element is no element");
406   /* create the src pad */
407   buffer = GST_BUFFER (buffer_in->data);
409   fail_unless (GST_IS_BUFFER (buffer), "There should be a buffer in buffer_in");
410   src_caps = GST_BUFFER_CAPS (buffer);
411   src_pad = gst_pad_new (NULL, GST_PAD_SRC);
412   gst_pad_set_caps (src_pad, src_caps);
413   pad_peer = gst_element_get_static_pad (element, "sink");
414   fail_if (pad_peer == NULL);
415   fail_unless (gst_pad_link (src_pad, pad_peer) == GST_PAD_LINK_OK,
416       "Could not link source and %s sink pads", GST_ELEMENT_NAME (element));
417   gst_object_unref (pad_peer);
418   /* activate the pad */
419   gst_pad_set_active (src_pad, TRUE);
420   GST_DEBUG ("src pad activated");
421   /* don't create the sink_pad if there is no buffer_out list */
422   if (buffer_out != NULL) {
423     gchar *temp;
425     GST_DEBUG ("buffer out detected, creating the sink pad");
426     /* get the sink caps */
427     sink_caps = GST_BUFFER_CAPS (GST_BUFFER (buffer_out->data));
428     fail_unless (GST_IS_CAPS (sink_caps), "buffer out don't have caps");
429     temp = gst_caps_to_string (sink_caps);
431     GST_DEBUG ("sink caps requested by buffer out: '%s'", temp);
432     g_free (temp);
433     fail_unless (gst_caps_is_fixed (sink_caps), "we need fixed caps");
434     /* get the sink pad */
435     sink_pad = gst_pad_new (NULL, GST_PAD_SINK);
436     fail_unless (GST_IS_PAD (sink_pad));
437     gst_pad_set_caps (sink_pad, sink_caps);
438     /* get the peer pad */
439     pad_peer = gst_element_get_static_pad (element, "src");
440     fail_unless (gst_pad_link (pad_peer, sink_pad) == GST_PAD_LINK_OK,
441         "Could not link sink and %s source pads", GST_ELEMENT_NAME (element));
442     gst_object_unref (pad_peer);
443     /* configure the sink pad */
444     gst_pad_set_chain_function (sink_pad, gst_check_chain_func);
445     gst_pad_set_active (sink_pad, TRUE);
446   }
447   fail_unless (gst_element_set_state (element,
448           GST_STATE_PLAYING) == GST_STATE_CHANGE_SUCCESS,
449       "could not set to playing");
450   /* push all the buffers in the buffer_in list */
451   fail_unless (g_list_length (buffer_in) > 0, "the buffer_in list is empty");
452   while (buffer_in != NULL) {
453     GstBuffer *next_buffer = GST_BUFFER (buffer_in->data);
455     fail_unless (GST_IS_BUFFER (next_buffer),
456         "data in buffer_in should be a buffer");
457     /* remove the buffer from the list */
458     buffer_in = g_list_remove (buffer_in, next_buffer);
459     if (buffer_in == NULL) {
460       fail_unless (gst_pad_push (src_pad, next_buffer) == last_flow_return,
461           "we expect something else from the last buffer");
462     } else {
463       fail_unless (gst_pad_push (src_pad, next_buffer) == GST_FLOW_OK,
464           "Failed to push buffer in");
465     }
466   }
467   fail_unless (gst_element_set_state (element,
468           GST_STATE_NULL) == GST_STATE_CHANGE_SUCCESS, "could not set to null");
469   /* check that there is a buffer out */
470   fail_unless_equals_int (g_list_length (buffers), g_list_length (buffer_out));
471   while (buffers != NULL) {
472     GstBuffer *new = GST_BUFFER (buffers->data);
473     GstBuffer *orig = GST_BUFFER (buffer_out->data);
475     GST_LOG ("orig buffer: size %u, caps %" GST_PTR_FORMAT,
476         GST_BUFFER_SIZE (orig), GST_BUFFER_CAPS (orig));
477     GST_LOG ("new  buffer: size %u, caps %" GST_PTR_FORMAT,
478         GST_BUFFER_SIZE (new), GST_BUFFER_CAPS (new));
479     GST_MEMDUMP ("orig buffer", GST_BUFFER_DATA (orig), GST_BUFFER_SIZE (orig));
480     GST_MEMDUMP ("new  buffer", GST_BUFFER_DATA (new), GST_BUFFER_SIZE (new));
482     /* remove the buffers */
483     buffers = g_list_remove (buffers, new);
484     buffer_out = g_list_remove (buffer_out, orig);
485     fail_unless (GST_BUFFER_SIZE (orig) == GST_BUFFER_SIZE (new),
486         "size of the buffers are not the same");
487     fail_unless (memcmp (GST_BUFFER_DATA (orig), GST_BUFFER_DATA (new),
488             GST_BUFFER_SIZE (new)) == 0, "data is not the same");
489     gst_check_caps_equal (GST_BUFFER_CAPS (orig), GST_BUFFER_CAPS (new));
490     gst_buffer_unref (new);
491     gst_buffer_unref (orig);
492   }
493   /* teardown the element and pads */
494   gst_pad_set_active (src_pad, FALSE);
495   gst_check_teardown_src_pad (element);
496   gst_pad_set_active (sink_pad, FALSE);
497   gst_check_teardown_sink_pad (element);
498   gst_check_teardown_element (element);
501 /**
502  * gst_check_element_push_buffer:
503  * @element_name: name of the element that needs to be created
504  * @buffer_in: push this buffer to the element
505  * @buffer_out: compare the result with this buffer
506  *
507  * Create an @element with the factory with the name and push the
508  * @buffer_in to this element. The element should create one buffer
509  * and this will be compared with @buffer_out. We only check the caps
510  * and the data of the buffers. This function unrefs the buffers.
511  * 
512  * Since: 0.10.18
513  */
514 void
515 gst_check_element_push_buffer (const gchar * element_name,
516     GstBuffer * buffer_in, GstBuffer * buffer_out)
518   GList *in = NULL;
519   GList *out = NULL;
521   in = g_list_append (in, buffer_in);
522   out = g_list_append (out, buffer_out);
524   gst_check_element_push_buffer_list (element_name, in, out, GST_FLOW_OK);
527 void
528 gst_check_abi_list (GstCheckABIStruct list[], gboolean have_abi_sizes)
530   if (have_abi_sizes) {
531     gboolean ok = TRUE;
532     gint i;
534     for (i = 0; list[i].name; i++) {
535       if (list[i].size != list[i].abi_size) {
536         ok = FALSE;
537         g_print ("sizeof(%s) is %d, expected %d\n",
538             list[i].name, list[i].size, list[i].abi_size);
539       }
540     }
541     fail_unless (ok, "failed ABI check");
542   } else {
543     const gchar *fn;
545     if ((fn = g_getenv ("GST_ABI"))) {
546       GError *err = NULL;
547       GString *s;
548       gint i;
550       s = g_string_new ("\nGstCheckABIStruct list[] = {\n");
551       for (i = 0; list[i].name; i++) {
552         g_string_append_printf (s, "  {\"%s\", sizeof (%s), %d},\n",
553             list[i].name, list[i].name, list[i].size);
554       }
555       g_string_append (s, "  {NULL, 0, 0}\n");
556       g_string_append (s, "};\n");
557       if (!g_file_set_contents (fn, s->str, s->len, &err)) {
558         g_print ("%s", s->str);
559         g_printerr ("\nFailed to write ABI information: %s\n", err->message);
560       } else {
561         g_print ("\nWrote ABI information to '%s'.\n", fn);
562       }
563       g_string_free (s, TRUE);
564     } else {
565       g_print ("No structure size list was generated for this architecture.\n");
566       g_print ("Run with GST_ABI environment variable set to output header.\n");
567     }
568   }
571 gint
572 gst_check_run_suite (Suite * suite, const gchar * name, const gchar * fname)
574   SRunner *sr;
575   gchar *xmlfilename = NULL;
576   gint nf;
578   sr = srunner_create (suite);
580   if (g_getenv ("GST_CHECK_XML")) {
581     /* how lucky we are to have __FILE__ end in .c */
582     xmlfilename = g_strdup_printf ("%sheck.xml", fname);
584     srunner_set_xml (sr, xmlfilename);
585   }
587   srunner_run_all (sr, CK_NORMAL);
588   nf = srunner_ntests_failed (sr);
589   g_free (xmlfilename);
590   srunner_free (sr);
591   return nf;
594 gboolean
595 _gst_check_run_test_func (const gchar * func_name)
597   const gchar *gst_checks;
598   gboolean res = FALSE;
599   gchar **funcs, **f;
601   gst_checks = g_getenv ("GST_CHECKS");
603   /* no filter specified => run all checks */
604   if (gst_checks == NULL || *gst_checks == '\0')
605     return TRUE;
607   /* only run specified functions */
608   funcs = g_strsplit (gst_checks, ",", -1);
609   for (f = funcs; f != NULL && *f != NULL; ++f) {
610     if (g_pattern_match_simple (*f, func_name)) {
611       res = TRUE;
612       break;
613     }
614   }
615   g_strfreev (funcs);
616   return res;