]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blob - libs/gst/check/gstconsistencychecker.c
affa6abd5e56e134c7b1dcbaaecba928ad125233
[glsdk/gstreamer0-10.git] / libs / gst / check / gstconsistencychecker.c
1 /* GStreamer
2  *
3  * unit testing helper lib
4  *
5  * Copyright (C) 2009 Edward Hervey <bilboed@bilboed.com>
6  *
7  * This library is free software; you can redistribute it and/or
8  * modify it under the terms of the GNU Library General Public
9  * License as published by the Free Software Foundation; either
10  * version 2 of the License, or (at your option) any later version.
11  *
12  * This library is distributed in the hope that it will be useful,
13  * but WITHOUT ANY WARRANTY; without even the implied warranty of
14  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
15  * Library General Public License for more details.
16  *
17  * You should have received a copy of the GNU Library General Public
18  * License along with this library; if not, write to the
19  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20  * Boston, MA 02111-1307, USA.
21  */
23 /**
24  * SECTION:gstcheckconsistencychecker
25  * @short_description: Data flow consistency checker for GStreamer unit tests.
26  *
27  * These macros and functions are for internal use of the unit tests found
28  * inside the 'check' directories of various GStreamer packages.
29  *
30  * Since: 0.10.24
31  */
33 #include "gstconsistencychecker.h"
35 static gboolean
36 source_pad_data_cb (GstPad * pad, GstMiniObject * data,
37     GstStreamConsistency * consist)
38 {
39   if (GST_IS_BUFFER (data)) {
40     GST_DEBUG_OBJECT (pad, "Buffer %" GST_TIME_FORMAT,
41         GST_TIME_ARGS (GST_BUFFER_TIMESTAMP (GST_BUFFER (data))));
42     /* If an EOS went through, a buffer would be invalid */
43     fail_if (consist->eos, "Buffer received after EOS");
44     /* Buffers need to be preceded by a newsegment event */
45     fail_unless (consist->newsegment, "Buffer received without newsegment");
46   } else {
47     GstEvent *event = (GstEvent *) data;
49     GST_DEBUG_OBJECT (pad, "%s", GST_EVENT_TYPE_NAME (event));
50     switch (GST_EVENT_TYPE (event)) {
51       case GST_EVENT_FLUSH_START:
52         consist->flushing = TRUE;
53         break;
54       case GST_EVENT_FLUSH_STOP:
55         /* Receiving a flush-stop is only valid after receiving a flush-start */
56         fail_unless (consist->flushing,
57             "Received a FLUSH_STOP without a FLUSH_START");
58         fail_if (consist->eos, "Received a FLUSH_STOP after an EOS");
59         consist->flushing = FALSE;
60         break;
61       case GST_EVENT_NEWSEGMENT:
62         consist->newsegment = TRUE;
63         consist->eos = FALSE;
64         break;
65       case GST_EVENT_EOS:
66         /* FIXME : not 100% sure about whether two eos in a row is valid */
67         fail_if (consist->eos, "Received EOS just after another EOS");
68         consist->eos = TRUE;
69         consist->newsegment = FALSE;
70         break;
71       case GST_EVENT_TAG:
72         GST_DEBUG_OBJECT (pad, "tag %" GST_PTR_FORMAT, event->structure);
73       default:
74         if (GST_EVENT_IS_SERIALIZED (event) && GST_EVENT_IS_DOWNSTREAM (event)) {
75           fail_if (consist->eos, "Event received after EOS");
76           fail_unless (consist->newsegment, "Event received before newsegment");
77         }
78         /* FIXME : Figure out what to do for other events */
79         break;
80     }
81   }
83   return TRUE;
84 }
86 /**
87  * gst_consistency_checker_new:
88  * @pad: The #GstPad on which the dataflow will be checked.
89  *
90  * Sets up a data probe on the given pad which will raise assertions if the
91  * data flow is inconsistent.
92  *
93  * Currently only works for source pads.
94  *
95  * Returns: A #GstStreamConsistency structure used to track data flow.
96  *
97  * Since: 0.10.24
98  */
100 GstStreamConsistency *
101 gst_consistency_checker_new (GstPad * pad)
103   GstStreamConsistency *consist;
105   g_return_val_if_fail (pad != NULL, NULL);
107   consist = g_new0 (GstStreamConsistency, 1);
108   consist->pad = g_object_ref (pad);
109   consist->probeid =
110       gst_pad_add_data_probe (pad, (GCallback) source_pad_data_cb, consist);
112   return consist;
115 /**
116  * gst_consistency_checker_reset:
117  * @consist: The #GstStreamConsistency to reset.
118  *
119  * Reset the stream checker's internal variables.
120  *
121  * Since: 0.10.24
122  */
124 void
125 gst_consistency_checker_reset (GstStreamConsistency * consist)
127   consist->eos = FALSE;
128   consist->flushing = FALSE;
129   consist->newsegment = FALSE;
132 /**
133  * gst_consistency_checker_free:
134  * @consist: The #GstStreamConsistency to free.
135  *
136  * Frees the allocated data and probe associated with @consist.
137  *
138  * Since: 0.10.24
139  */
141 void
142 gst_consistency_checker_free (GstStreamConsistency * consist)
144   /* Remove the data probe */
145   gst_pad_remove_data_probe (consist->pad, consist->probeid);
146   g_object_unref (consist->pad);
147   g_free (consist);