1 /* GStreamer
2 *
3 * unit testing helper lib
4 *
5 * Copyright (C) 2009 Edward Hervey <bilboed@bilboed.com>
6 *
7 * This library is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU Library General Public
9 * License as published by the Free Software Foundation; either
10 * version 2 of the License, or (at your option) any later version.
11 *
12 * This library is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
15 * Library General Public License for more details.
16 *
17 * You should have received a copy of the GNU Library General Public
18 * License along with this library; if not, write to the
19 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20 * Boston, MA 02111-1307, USA.
21 */
23 /**
24 * SECTION:gstcheckconsistencychecker
25 * @short_description: Data flow consistency checker for GStreamer unit tests.
26 *
27 * These macros and functions are for internal use of the unit tests found
28 * inside the 'check' directories of various GStreamer packages.
29 *
30 * Since: 0.10.24
31 */
33 #include "gstconsistencychecker.h"
35 struct _GstStreamConsistency
36 {
37 gboolean flushing;
38 gboolean newsegment;
39 gboolean eos;
40 gulong probeid;
41 GstPad *pad;
42 };
44 static gboolean
45 source_pad_data_cb (GstPad * pad, GstMiniObject * data,
46 GstStreamConsistency * consist)
47 {
48 if (GST_IS_BUFFER (data)) {
49 GST_DEBUG_OBJECT (pad, "Buffer %" GST_TIME_FORMAT,
50 GST_TIME_ARGS (GST_BUFFER_TIMESTAMP (GST_BUFFER (data))));
51 /* If an EOS went through, a buffer would be invalid */
52 fail_if (consist->eos, "Buffer received after EOS");
53 /* Buffers need to be preceded by a newsegment event */
54 fail_unless (consist->newsegment, "Buffer received without newsegment");
55 } else if (GST_IS_EVENT (data)) {
56 GstEvent *event = (GstEvent *) data;
58 GST_DEBUG_OBJECT (pad, "%s", GST_EVENT_TYPE_NAME (event));
59 switch (GST_EVENT_TYPE (event)) {
60 case GST_EVENT_FLUSH_START:
61 consist->flushing = TRUE;
62 break;
63 case GST_EVENT_FLUSH_STOP:
64 /* Receiving a flush-stop is only valid after receiving a flush-start */
65 fail_unless (consist->flushing,
66 "Received a FLUSH_STOP without a FLUSH_START");
67 fail_if (consist->eos, "Received a FLUSH_STOP after an EOS");
68 consist->flushing = FALSE;
69 break;
70 case GST_EVENT_NEWSEGMENT:
71 consist->newsegment = TRUE;
72 consist->eos = FALSE;
73 break;
74 case GST_EVENT_EOS:
75 /* FIXME : not 100% sure about whether two eos in a row is valid */
76 fail_if (consist->eos, "Received EOS just after another EOS");
77 consist->eos = TRUE;
78 consist->newsegment = FALSE;
79 break;
80 case GST_EVENT_TAG:
81 GST_DEBUG_OBJECT (pad, "tag %" GST_PTR_FORMAT, event->structure);
82 /* fall through */
83 default:
84 if (GST_EVENT_IS_SERIALIZED (event) && GST_EVENT_IS_DOWNSTREAM (event)) {
85 fail_if (consist->eos, "Event received after EOS");
86 fail_unless (consist->newsegment, "Event received before newsegment");
87 }
88 /* FIXME : Figure out what to do for other events */
89 break;
90 }
91 }
93 return TRUE;
94 }
96 /**
97 * gst_consistency_checker_new:
98 * @pad: The #GstPad on which the dataflow will be checked.
99 *
100 * Sets up a data probe on the given pad which will raise assertions if the
101 * data flow is inconsistent.
102 *
103 * Currently only works for source pads.
104 *
105 * Returns: A #GstStreamConsistency structure used to track data flow.
106 *
107 * Since: 0.10.24
108 */
110 GstStreamConsistency *
111 gst_consistency_checker_new (GstPad * pad)
112 {
113 GstStreamConsistency *consist;
115 g_return_val_if_fail (pad != NULL, NULL);
117 consist = g_new0 (GstStreamConsistency, 1);
118 consist->pad = g_object_ref (pad);
119 consist->probeid =
120 gst_pad_add_data_probe (pad, (GCallback) source_pad_data_cb, consist);
122 return consist;
123 }
125 /**
126 * gst_consistency_checker_reset:
127 * @consist: The #GstStreamConsistency to reset.
128 *
129 * Reset the stream checker's internal variables.
130 *
131 * Since: 0.10.24
132 */
134 void
135 gst_consistency_checker_reset (GstStreamConsistency * consist)
136 {
137 consist->eos = FALSE;
138 consist->flushing = FALSE;
139 consist->newsegment = FALSE;
140 }
142 /**
143 * gst_consistency_checker_free:
144 * @consist: The #GstStreamConsistency to free.
145 *
146 * Frees the allocated data and probe associated with @consist.
147 *
148 * Since: 0.10.24
149 */
151 void
152 gst_consistency_checker_free (GstStreamConsistency * consist)
153 {
154 /* Remove the data probe */
155 gst_pad_remove_data_probe (consist->pad, consist->probeid);
156 g_object_unref (consist->pad);
157 g_free (consist);
158 }