21bca4316eeeda34a583445371edd8c73df3fa77
1 /* GStreamer
2 * Copyright (C) <1999> Erik Walthinsen <omega@cse.ogi.edu>
3 * Copyright (C) <2004> Thomas Vander Stichele <thomas at apestaart dot org>
4 *
5 * dataprotocol.c: Functions implementing the GStreamer Data Protocol
6 *
7 * This library is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU Library General Public
9 * License as published by the Free Software Foundation; either
10 * version 2 of the License, or (at your option) any later version.
11 *
12 * This library is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
15 * Library General Public License for more details.
16 *
17 * You should have received a copy of the GNU Library General Public
18 * License along with this library; if not, write to the
19 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20 * Boston, MA 02111-1307, USA.
21 */
23 #ifdef HAVE_CONFIG_H
24 #include "config.h"
25 #endif
27 #include <gst/gst.h>
28 #include <gst/dataprotocol/dataprotocol.h>
29 #include <glib/gprintf.h> /* g_sprintf */
30 #include <string.h> /* strlen */
31 #include "dp-private.h"
33 /* debug category */
34 GST_DEBUG_CATEGORY (data_protocol_debug);
35 #define GST_CAT_DEFAULT data_protocol_debug
37 /* calculate a CCITT 16 bit CRC check value for a given byte array */
38 /*
39 * this code snippet is adapted from a web page I found
40 * it is identical except for cleanups, and a final XOR with 0xffff
41 * as outlined in the uecp spec
42 *
43 * XMODEM x^16 + x^12 + x^5 + 1
44 */
46 #define POLY 0x1021
47 #define CRC_INIT 0xFFFF
49 static guint16
50 gst_dp_crc (const guint8 * buffer, register guint length)
51 {
52 static gboolean initialized = FALSE;
53 static guint16 crc_table[256];
54 guint16 crc_register;
55 unsigned long i, j, k;
57 if (!initialized) {
58 for (i = 0; i < 256; i++) {
59 j = i << 8;
60 for (k = 8; k--;) {
61 j = j & 0x8000 ? (j << 1) ^ POLY : j << 1;
62 }
64 crc_table[i] = (guint16) j;
65 }
66 initialized = TRUE;
67 }
69 crc_register = CRC_INIT; /* always init register */
71 /* calc CRC */
72 for (; length--;) {
73 crc_register = (guint16) ((crc_register << 8) ^
74 crc_table[((crc_register >> 8) & 0x00ff) ^ *buffer++]);
75 }
76 return (0xffff ^ crc_register);
77 }
79 /* debugging function; dumps byte array values per 8 bytes */
80 /* FIXME: would be nice to merge this with gst_util_dump_mem () */
81 void
82 gst_dp_dump_byte_array (guint8 * array, guint length)
83 {
84 int i;
85 int n = 8; /* number of bytes per line */
86 gchar *line = g_malloc (3 * n + 1);
88 GST_LOG ("dumping byte array of length %d", length);
89 for (i = 0; i < length; ++i) {
90 g_sprintf (line + 3 * (i % n), "%02x ", array[i]);
91 if (i % n == (n - 1)) {
92 GST_LOG ("%03d: %s", i - (n - 1), line);
93 }
94 }
95 if (i % n != 0) {
96 GST_LOG ("%03d: %s", (i / n) * n, line);
97 }
98 g_free (line);
99 }
101 /**
102 * gst_dp_init:
103 *
104 * Initialize GStreamer Data Protocol library.
105 *
106 * Should be called before using these functions from source linking
107 * to this source file.
108 */
109 void
110 gst_dp_init (void)
111 {
112 static gboolean _gst_dp_initialized = FALSE;
114 if (_gst_dp_initialized)
115 return;
117 _gst_dp_initialized = TRUE;
119 GST_DEBUG_CATEGORY_INIT (data_protocol_debug, "gdp", 0,
120 "GStreamer Data Protocol");
121 }
123 /*** PUBLIC FUNCTIONS ***/
125 /**
126 * gst_dp_header_payload_length:
127 * @header: the byte header of the packet array
128 *
129 * Returns: the length of the payload this header describes.
130 */
131 guint32
132 gst_dp_header_payload_length (const guint8 * header)
133 {
134 return GST_DP_HEADER_PAYLOAD_LENGTH (header);
135 }
137 /**
138 * gst_dp_header_payload_type:
139 * @header: the byte header of the packet array
140 *
141 * Returns: the #GstDPPayloadType the payload this header describes.
142 */
143 GstDPPayloadType
144 gst_dp_header_payload_type (const guint8 * header)
145 {
146 return GST_DP_HEADER_PAYLOAD_TYPE (header);
147 }
149 /**
150 * gst_dp_header_from_buffer:
151 * @buffer: a #GstBuffer to create a header for
152 * @flags: the #GDPHeaderFlags to create the header with
153 * @length: a guint pointer to store the header length in
154 * @header: a guint8 * pointer to store a newly allocated header byte array in
155 *
156 * Creates a GDP header from the given buffer.
157 *
158 * Returns: %TRUE if the header was successfully created.
159 */
161 gboolean
162 gst_dp_header_from_buffer (const GstBuffer * buffer, GstDPHeaderFlag flags,
163 guint * length, guint8 ** header)
164 {
165 guint8 *h;
166 guint16 crc;
167 guint16 flags_mask;
169 g_return_val_if_fail (GST_IS_BUFFER (buffer), FALSE);
170 g_return_val_if_fail (header, FALSE);
172 *length = GST_DP_HEADER_LENGTH;
173 h = g_malloc (GST_DP_HEADER_LENGTH);
175 /* version, flags, type */
176 h[0] = (guint8) GST_DP_VERSION_MAJOR;
177 h[1] = (guint8) GST_DP_VERSION_MINOR;
178 h[2] = (guint8) flags;
179 h[3] = GST_DP_PAYLOAD_BUFFER;
181 /* buffer properties */
182 GST_WRITE_UINT32_BE (h + 4, GST_BUFFER_SIZE (buffer));
183 GST_WRITE_UINT64_BE (h + 8, GST_BUFFER_TIMESTAMP (buffer));
184 GST_WRITE_UINT64_BE (h + 16, GST_BUFFER_DURATION (buffer));
185 GST_WRITE_UINT64_BE (h + 24, GST_BUFFER_OFFSET (buffer));
186 GST_WRITE_UINT64_BE (h + 32, GST_BUFFER_OFFSET_END (buffer));
188 /* data flags */
189 /* we only copy KEY_UNIT,DELTA_UNIT and IN_CAPS flags */
190 flags_mask = GST_BUFFER_FLAG_PREROLL | GST_BUFFER_FLAG_IN_CAPS |
191 GST_BUFFER_FLAG_DELTA_UNIT;
193 GST_WRITE_UINT16_BE (h + 40, GST_BUFFER_FLAGS (buffer) & flags_mask);
195 /* ABI padding */
196 GST_WRITE_UINT16_BE (h + 42, (guint64) 0);
197 GST_WRITE_UINT32_BE (h + 44, (guint64) 0);
198 GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
200 /* CRC */
201 crc = 0;
202 if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
203 /* we don't crc the last four bytes of the header since they are crc's */
204 crc = gst_dp_crc (h, 56);
205 }
206 GST_WRITE_UINT16_BE (h + 56, crc);
208 crc = 0;
209 if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
210 crc = gst_dp_crc (GST_BUFFER_DATA (buffer), GST_BUFFER_SIZE (buffer));
211 }
212 GST_WRITE_UINT16_BE (h + 58, crc);
214 GST_LOG ("created header from buffer:");
215 gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
216 *header = h;
217 return TRUE;
218 }
220 /**
221 * gst_dp_packet_from_caps:
222 * @caps: a #GstCaps to create a packet for
223 * @flags: the #GDPHeaderFlags to create the header with
224 * @length: a guint pointer to store the header length in
225 * @header: a guint8 pointer to store a newly allocated header byte array in
226 * @payload: a guint8 pointer to store a newly allocated payload byte array in
227 *
228 * Creates a GDP packet from the given caps.
229 *
230 * Returns: %TRUE if the packet was successfully created.
231 */
232 gboolean
233 gst_dp_packet_from_caps (const GstCaps * caps, GstDPHeaderFlag flags,
234 guint * length, guint8 ** header, guint8 ** payload)
235 {
236 guint8 *h;
237 guint16 crc;
238 guchar *string;
240 /* FIXME: GST_IS_CAPS doesn't work
241 g_return_val_if_fail (GST_IS_CAPS (caps), FALSE); */
242 g_return_val_if_fail (caps, FALSE);
243 g_return_val_if_fail (header, FALSE);
244 g_return_val_if_fail (payload, FALSE);
246 *length = GST_DP_HEADER_LENGTH;
247 h = g_malloc (GST_DP_HEADER_LENGTH);
249 string = (guchar *) gst_caps_to_string (caps);
251 /* version, flags, type */
252 h[0] = (guint8) GST_DP_VERSION_MAJOR;
253 h[1] = (guint8) GST_DP_VERSION_MINOR;
254 h[2] = (guint8) flags;
255 h[3] = GST_DP_PAYLOAD_CAPS;
257 /* buffer properties */
258 GST_WRITE_UINT32_BE (h + 4, strlen ((gchar *) string) + 1); /* include trailing 0 */
259 GST_WRITE_UINT64_BE (h + 8, (guint64) 0);
260 GST_WRITE_UINT64_BE (h + 16, (guint64) 0);
261 GST_WRITE_UINT64_BE (h + 24, (guint64) 0);
262 GST_WRITE_UINT64_BE (h + 32, (guint64) 0);
264 /* ABI padding */
265 GST_WRITE_UINT64_BE (h + 40, (guint64) 0);
266 GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
268 /* CRC */
269 crc = 0;
270 if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
271 crc = gst_dp_crc (h, 56);
272 }
273 GST_WRITE_UINT16_BE (h + 56, crc);
275 crc = 0;
276 if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
277 crc = gst_dp_crc (string, strlen ((gchar *) string) + 1);
278 }
279 GST_WRITE_UINT16_BE (h + 58, crc);
281 GST_LOG ("created header from caps:");
282 gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
283 *header = h;
284 *payload = string;
285 return TRUE;
286 }
288 /**
289 * gst_dp_packet_from_event:
290 * @event: a #GstEvent to create a packet for
291 * @flags: the #GDPHeaderFlags to create the header with
292 * @length: a guint pointer to store the header length in
293 * @header: a guint8 pointer to store a newly allocated header byte array in
294 * @payload: a guint8 pointer to store a newly allocated payload byte array in
295 *
296 * Creates a GDP packet from the given event.
297 *
298 * Returns: %TRUE if the packet was successfully created.
299 */
300 gboolean
301 gst_dp_packet_from_event (const GstEvent * event, GstDPHeaderFlag flags,
302 guint * length, guint8 ** header, guint8 ** payload)
303 {
304 guint8 *h;
305 guint16 crc;
306 guint pl_length; /* length of payload */
308 g_return_val_if_fail (event, FALSE);
309 g_return_val_if_fail (GST_IS_EVENT (event), FALSE);
310 g_return_val_if_fail (header, FALSE);
311 g_return_val_if_fail (payload, FALSE);
313 *length = GST_DP_HEADER_LENGTH;
314 h = g_malloc0 (GST_DP_HEADER_LENGTH);
316 /* first construct payload, since we need the length */
317 switch (GST_EVENT_TYPE (event)) {
318 case GST_EVENT_UNKNOWN:
319 g_warning ("Unknown event, ignoring");
320 *length = 0;
321 g_free (h);
322 return FALSE;
323 case GST_EVENT_EOS:
324 case GST_EVENT_FLUSH_START:
325 case GST_EVENT_FLUSH_STOP:
326 case GST_EVENT_NEWSEGMENT:
327 GST_WRITE_UINT64_BE (h + 8, GST_EVENT_TIMESTAMP (event));
328 pl_length = 0;
329 *payload = NULL;
330 break;
331 case GST_EVENT_SEEK:
332 {
333 gdouble rate;
334 GstFormat format;
335 GstSeekFlags flags;
336 GstSeekType cur_type, stop_type;
337 gint64 cur, stop;
339 gst_event_parse_seek ((GstEvent *) event, &rate, &format, &flags,
340 &cur_type, &cur, &stop_type, &stop);
342 pl_length = 4 + 4 + 4 + 8 + 4 + 8;
343 *payload = g_malloc0 (pl_length);
344 /* FIXME write rate */
345 GST_WRITE_UINT32_BE (*payload, (guint32) format);
346 GST_WRITE_UINT32_BE (*payload + 4, (guint32) flags);
347 GST_WRITE_UINT32_BE (*payload + 8, (guint32) cur_type);
348 GST_WRITE_UINT64_BE (*payload + 12, (guint64) cur);
349 GST_WRITE_UINT32_BE (*payload + 20, (guint32) stop_type);
350 GST_WRITE_UINT64_BE (*payload + 24, (guint64) stop);
351 break;
352 }
353 case GST_EVENT_QOS:
354 case GST_EVENT_NAVIGATION:
355 case GST_EVENT_TAG:
356 g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event));
357 return FALSE;
358 default:
359 g_warning ("Unknown event type %d, ignoring", GST_EVENT_TYPE (event));
360 *length = 0;
361 g_free (h);
362 return FALSE;
363 }
365 /* version, flags, type */
366 h[0] = (guint8) GST_DP_VERSION_MAJOR;
367 h[1] = (guint8) GST_DP_VERSION_MINOR;
368 h[2] = (guint8) flags;
369 h[3] = GST_DP_PAYLOAD_EVENT_NONE + GST_EVENT_TYPE (event);
371 /* length */
372 GST_WRITE_UINT32_BE (h + 4, (guint32) pl_length);
373 /* timestamp */
374 GST_WRITE_UINT64_BE (h + 8, GST_EVENT_TIMESTAMP (event));
376 /* ABI padding */
377 GST_WRITE_UINT64_BE (h + 40, (guint64) 0);
378 GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
380 /* CRC */
381 crc = 0;
382 if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
383 crc = gst_dp_crc (h, 56);
384 }
385 GST_WRITE_UINT16_BE (h + 56, crc);
387 crc = 0;
388 /* events can have a NULL payload */
389 if (*payload && flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
390 crc = gst_dp_crc (*payload, strlen ((gchar *) * payload) + 1);
391 }
392 GST_WRITE_UINT16_BE (h + 58, crc);
394 GST_LOG ("created header from event:");
395 gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
396 *header = h;
397 return TRUE;
398 }
401 /**
402 * gst_dp_buffer_from_header:
403 * @header_length: the length of the packet header
404 * @header: the byte array of the packet header
405 *
406 * Creates a newly allocated #GstBuffer from the given header.
407 * The buffer data needs to be copied into it before validating.
408 *
409 * Use this function if you want to pre-allocate a buffer based on the
410 * packet header to read the packet payload in to.
411 *
412 * Returns: %TRUE if the buffer was successfully created.
413 */
414 GstBuffer *
415 gst_dp_buffer_from_header (guint header_length, const guint8 * header)
416 {
417 GstBuffer *buffer;
419 g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) ==
420 GST_DP_PAYLOAD_BUFFER, NULL);
421 buffer =
422 gst_buffer_new_and_alloc ((guint) GST_DP_HEADER_PAYLOAD_LENGTH (header));
423 GST_BUFFER_TIMESTAMP (buffer) = GST_DP_HEADER_TIMESTAMP (header);
424 GST_BUFFER_DURATION (buffer) = GST_DP_HEADER_DURATION (header);
425 GST_BUFFER_OFFSET (buffer) = GST_DP_HEADER_OFFSET (header);
426 GST_BUFFER_OFFSET_END (buffer) = GST_DP_HEADER_OFFSET_END (header);
427 GST_BUFFER_FLAGS (buffer) = GST_DP_HEADER_BUFFER_FLAGS (header);
429 return buffer;
430 }
432 /**
433 * gst_dp_caps_from_packet:
434 * @header_length: the length of the packet header
435 * @header: the byte array of the packet header
436 * @payload: the byte array of the packet payload
437 *
438 * Creates a newly allocated #GstCaps from the given packet.
439 *
440 * Returns: %TRUE if the caps was successfully created.
441 */
442 GstCaps *
443 gst_dp_caps_from_packet (guint header_length, const guint8 * header,
444 const guint8 * payload)
445 {
446 GstCaps *caps;
447 const gchar *string;
449 g_return_val_if_fail (header, NULL);
450 g_return_val_if_fail (payload, NULL);
451 g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) ==
452 GST_DP_PAYLOAD_CAPS, NULL);
454 string = (gchar *) payload;
455 caps = gst_caps_from_string (string);
456 return caps;
457 }
459 /**
460 * gst_dp_event_from_packet:
461 * @header_length: the length of the packet header
462 * @header: the byte array of the packet header
463 * @payload: the byte array of the packet payload
464 *
465 * Creates a newly allocated #GstEvent from the given packet.
466 *
467 * Returns: %TRUE if the event was successfully created.
468 */
469 GstEvent *
470 gst_dp_event_from_packet (guint header_length, const guint8 * header,
471 const guint8 * payload)
472 {
473 GstEvent *event = NULL;
474 GstEventType type;
476 g_return_val_if_fail (header, NULL);
477 /* payload can be NULL, e.g. for an EOS event */
479 type = GST_DP_HEADER_PAYLOAD_TYPE (header) - GST_DP_PAYLOAD_EVENT_NONE;
480 switch (type) {
481 case GST_EVENT_UNKNOWN:
482 g_warning ("Unknown event, ignoring");
483 return FALSE;
484 case GST_EVENT_EOS:
485 case GST_EVENT_FLUSH_START:
486 case GST_EVENT_FLUSH_STOP:
487 case GST_EVENT_NEWSEGMENT:
488 event = gst_event_new_custom (type, NULL);
489 GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header);
490 break;
491 case GST_EVENT_SEEK:
492 {
493 gdouble rate;
494 GstFormat format;
495 GstSeekFlags flags;
496 GstSeekType cur_type, stop_type;
497 gint64 cur, stop;
499 /* FIXME, read rate */
500 rate = 1.0;
501 format = (GstFormat) GST_READ_UINT32_BE (payload);
502 flags = (GstSeekFlags) GST_READ_UINT32_BE (payload + 4);
503 cur_type = (GstSeekType) GST_READ_UINT32_BE (payload + 8);
504 cur = (gint64) GST_READ_UINT64_BE (payload + 12);
505 stop_type = (GstSeekType) GST_READ_UINT32_BE (payload + 20);
506 stop = (gint64) GST_READ_UINT64_BE (payload + 24);
508 event = gst_event_new_seek (rate, format, flags, cur_type, cur,
509 stop_type, stop);
510 GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header);
511 break;
512 }
513 case GST_EVENT_QOS:
514 case GST_EVENT_NAVIGATION:
515 case GST_EVENT_TAG:
516 g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event));
517 return FALSE;
518 default:
519 g_warning ("Unknown event type %d, ignoring", GST_EVENT_TYPE (event));
520 return FALSE;
521 }
523 return event;
524 }
526 /**
527 * gst_dp_validate_header:
528 * @header_length: the length of the packet header
529 * @header: the byte array of the packet header
530 *
531 * Validates the given packet header by checking the CRC checksum.
532 *
533 * Returns: %TRUE if the CRC matches, or no CRC checksum is present.
534 */
535 gboolean
536 gst_dp_validate_header (guint header_length, const guint8 * header)
537 {
538 guint16 crc_read, crc_calculated;
540 if (!(GST_DP_HEADER_FLAGS (header) & GST_DP_HEADER_FLAG_CRC_HEADER))
541 return TRUE;
542 crc_read = GST_DP_HEADER_CRC_HEADER (header);
543 /* don't included the last two crc fields for the crc check */
544 crc_calculated = gst_dp_crc (header, header_length - 4);
545 if (crc_read != crc_calculated) {
546 GST_WARNING ("header crc mismatch: read %02x, calculated %02x", crc_read,
547 crc_calculated);
548 return FALSE;
549 }
550 GST_LOG ("header crc validation: %02x", crc_read);
551 return TRUE;
552 }
554 /**
555 * gst_dp_validate_payload:
556 * @header_length: the length of the packet header
557 * @header: the byte array of the packet header
558 * @payload: the byte array of the packet payload
559 *
560 * Validates the given packet payload using the given packet header
561 * by checking the CRC checksum.
562 *
563 * Returns: %TRUE if the CRC matches, or no CRC checksum is present.
564 */
565 gboolean
566 gst_dp_validate_payload (guint header_length, const guint8 * header,
567 const guint8 * payload)
568 {
569 guint16 crc_read, crc_calculated;
571 if (!(GST_DP_HEADER_FLAGS (header) & GST_DP_HEADER_FLAG_CRC_PAYLOAD))
572 return TRUE;
573 crc_read = GST_DP_HEADER_CRC_PAYLOAD (header);
574 crc_calculated = gst_dp_crc (payload, GST_DP_HEADER_PAYLOAD_LENGTH (header));
575 if (crc_read != crc_calculated) {
576 GST_WARNING ("payload crc mismatch: read %02x, calculated %02x", crc_read,
577 crc_calculated);
578 return FALSE;
579 }
580 GST_LOG ("payload crc validation: %02x", crc_read);
581 return TRUE;
582 }
584 /**
585 * gst_dp_validate_packet:
586 * @header_length: the length of the packet header
587 * @header: the byte array of the packet header
588 * @payload: the byte array of the packet payload
589 *
590 * Validates the given packet by checking version information and checksums.
591 *
592 * Returns: %TRUE if the packet validates.
593 */
594 gboolean
595 gst_dp_validate_packet (guint header_length, const guint8 * header,
596 const guint8 * payload)
597 {
598 if (!gst_dp_validate_header (header_length, header))
599 return FALSE;
600 if (!gst_dp_validate_payload (header_length, header, payload))
601 return FALSE;
603 return TRUE;
604 }