7c39492beaf0d7ead988a8b2a6e050a142a0f8ed
1 /* GStreamer
2 * Copyright (C) <1999> Erik Walthinsen <omega@cse.ogi.edu>
3 * Copyright (C) <2004> Thomas Vander Stichele <thomas at apestaart dot org>
4 *
5 * dataprotocol.c: Functions implementing the GStreamer Data Protocol
6 *
7 * This library is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU Library General Public
9 * License as published by the Free Software Foundation; either
10 * version 2 of the License, or (at your option) any later version.
11 *
12 * This library is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
15 * Library General Public License for more details.
16 *
17 * You should have received a copy of the GNU Library General Public
18 * License along with this library; if not, write to the
19 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20 * Boston, MA 02111-1307, USA.
21 */
23 #ifdef HAVE_CONFIG_H
24 #include "config.h"
25 #endif
27 #include <gst/gst.h>
28 #include <gst/dataprotocol/dataprotocol.h>
29 #include <glib/gprintf.h> /* g_sprintf */
30 #include <string.h> /* strlen */
31 #include "dp-private.h"
33 /* debug category */
34 GST_DEBUG_CATEGORY (data_protocol_debug);
35 #define GST_CAT_DEFAULT data_protocol_debug
37 /* calculate a CCITT 16 bit CRC check value for a given byte array */
38 /*
39 * this code snippet is adapted from a web page I found
40 * it is identical except for cleanups, and a final XOR with 0xffff
41 * as outlined in the uecp spec
42 *
43 * XMODEM x^16 + x^12 + x^5 + 1
44 */
46 #define POLY 0x1021
47 #define CRC_INIT 0xFFFF
49 static guint16
50 gst_dp_crc (const guint8 * buffer, register guint length)
51 {
52 static gboolean initialized = FALSE;
53 static guint16 crc_table[256];
54 guint16 crc_register;
55 unsigned long i, j, k;
57 if (!initialized) {
58 for (i = 0; i < 256; i++) {
59 j = i << 8;
60 for (k = 8; k--;) {
61 j = j & 0x8000 ? (j << 1) ^ POLY : j << 1;
62 }
64 crc_table[i] = (guint16) j;
65 }
66 initialized = TRUE;
67 }
69 crc_register = CRC_INIT; /* always init register */
71 /* calc CRC */
72 for (; length--;) {
73 crc_register = (guint16) ((crc_register << 8) ^
74 crc_table[((crc_register >> 8) & 0x00ff) ^ *buffer++]);
75 }
76 return (0xffff ^ crc_register);
77 }
79 /* debugging function; dumps byte array values per 8 bytes */
80 /* FIXME: would be nice to merge this with gst_util_dump_mem () */
81 void
82 gst_dp_dump_byte_array (guint8 * array, guint length)
83 {
84 int i;
85 int n = 8; /* number of bytes per line */
86 gchar *line = g_malloc (3 * n + 1);
88 GST_LOG ("dumping byte array of length %d", length);
89 for (i = 0; i < length; ++i) {
90 g_sprintf (line + 3 * (i % n), "%02x ", array[i]);
91 if (i % n == (n - 1)) {
92 GST_LOG ("%03d: %s", i - (n - 1), line);
93 }
94 }
95 if (i % n != 0) {
96 GST_LOG ("%03d: %s", (i / n) * n, line);
97 }
98 g_free (line);
99 }
101 /**
102 * gst_dp_init:
103 *
104 * Initialize GStreamer Data Protocol library.
105 *
106 * Should be called before using these functions from source linking
107 * to this source file.
108 */
109 void
110 gst_dp_init (void)
111 {
112 static gboolean _gst_dp_initialized = FALSE;
114 if (_gst_dp_initialized)
115 return;
117 _gst_dp_initialized = TRUE;
119 GST_DEBUG_CATEGORY_INIT (data_protocol_debug, "gdp", 0,
120 "GStreamer Data Protocol");
121 }
123 /*** PUBLIC FUNCTIONS ***/
125 /**
126 * gst_dp_header_payload_length:
127 * @header: the byte header of the packet array
128 *
129 * Returns: the length of the payload this header describes.
130 */
131 guint32
132 gst_dp_header_payload_length (const guint8 * header)
133 {
134 return GST_DP_HEADER_PAYLOAD_LENGTH (header);
135 }
137 /**
138 * gst_dp_header_payload_type:
139 * @header: the byte header of the packet array
140 *
141 * Returns: the #GstDPPayloadType the payload this header describes.
142 */
143 GstDPPayloadType
144 gst_dp_header_payload_type (const guint8 * header)
145 {
146 return GST_DP_HEADER_PAYLOAD_TYPE (header);
147 }
149 /**
150 * gst_dp_header_from_buffer:
151 * @buffer: a #GstBuffer to create a header for
152 * @flags: the #GDPHeaderFlags to create the header with
153 * @length: a guint pointer to store the header length in
154 * @header: a guint8 * pointer to store a newly allocated header byte array in
155 *
156 * Creates a GDP header from the given buffer.
157 *
158 * Returns: %TRUE if the header was successfully created.
159 */
161 gboolean
162 gst_dp_header_from_buffer (const GstBuffer * buffer, GstDPHeaderFlag flags,
163 guint * length, guint8 ** header)
164 {
165 guint8 *h;
166 guint16 crc;
167 guint16 flags_mask;
169 g_return_val_if_fail (GST_IS_BUFFER (buffer), FALSE);
170 g_return_val_if_fail (header, FALSE);
172 *length = GST_DP_HEADER_LENGTH;
173 h = g_malloc (GST_DP_HEADER_LENGTH);
175 /* version, flags, type */
176 h[0] = (guint8) GST_DP_VERSION_MAJOR;
177 h[1] = (guint8) GST_DP_VERSION_MINOR;
178 h[2] = (guint8) flags;
179 h[3] = 0; /* padding byte */
180 GST_WRITE_UINT16_BE (h + 4, GST_DP_PAYLOAD_BUFFER);
182 /* buffer properties */
183 GST_WRITE_UINT32_BE (h + 6, GST_BUFFER_SIZE (buffer));
184 GST_WRITE_UINT64_BE (h + 10, GST_BUFFER_TIMESTAMP (buffer));
185 GST_WRITE_UINT64_BE (h + 18, GST_BUFFER_DURATION (buffer));
186 GST_WRITE_UINT64_BE (h + 26, GST_BUFFER_OFFSET (buffer));
187 GST_WRITE_UINT64_BE (h + 34, GST_BUFFER_OFFSET_END (buffer));
189 /* data flags */
190 /* we only copy KEY_UNIT,DELTA_UNIT and IN_CAPS flags */
191 flags_mask = GST_BUFFER_FLAG_PREROLL | GST_BUFFER_FLAG_IN_CAPS |
192 GST_BUFFER_FLAG_DELTA_UNIT;
194 GST_WRITE_UINT16_BE (h + 42, GST_BUFFER_FLAGS (buffer) & flags_mask);
196 /* ABI padding */
197 GST_WRITE_UINT32_BE (h + 44, (guint64) 0);
198 GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
200 /* CRC */
201 crc = 0;
202 if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
203 /* we don't crc the last four bytes of the header since they are crc's */
204 crc = gst_dp_crc (h, 58);
205 }
206 GST_WRITE_UINT16_BE (h + 58, crc);
208 crc = 0;
209 if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
210 crc = gst_dp_crc (GST_BUFFER_DATA (buffer), GST_BUFFER_SIZE (buffer));
211 }
212 GST_WRITE_UINT16_BE (h + 60, crc);
214 GST_LOG ("created header from buffer:");
215 gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
216 *header = h;
217 return TRUE;
218 }
220 /**
221 * gst_dp_packet_from_caps:
222 * @caps: a #GstCaps to create a packet for
223 * @flags: the #GDPHeaderFlags to create the header with
224 * @length: a guint pointer to store the header length in
225 * @header: a guint8 pointer to store a newly allocated header byte array in
226 * @payload: a guint8 pointer to store a newly allocated payload byte array in
227 *
228 * Creates a GDP packet from the given caps.
229 *
230 * Returns: %TRUE if the packet was successfully created.
231 */
232 gboolean
233 gst_dp_packet_from_caps (const GstCaps * caps, GstDPHeaderFlag flags,
234 guint * length, guint8 ** header, guint8 ** payload)
235 {
236 guint8 *h;
237 guint16 crc;
238 guchar *string;
240 /* FIXME: GST_IS_CAPS doesn't work
241 g_return_val_if_fail (GST_IS_CAPS (caps), FALSE); */
242 g_return_val_if_fail (caps, FALSE);
243 g_return_val_if_fail (header, FALSE);
244 g_return_val_if_fail (payload, FALSE);
246 *length = GST_DP_HEADER_LENGTH;
247 h = g_malloc (GST_DP_HEADER_LENGTH);
249 string = (guchar *) gst_caps_to_string (caps);
251 /* version, flags, type */
252 h[0] = (guint8) GST_DP_VERSION_MAJOR;
253 h[1] = (guint8) GST_DP_VERSION_MINOR;
254 h[2] = (guint8) flags;
255 h[3] = 0; /* padding bytes */
256 GST_WRITE_UINT16_BE (h + 4, GST_DP_PAYLOAD_CAPS);
258 /* buffer properties */
259 GST_WRITE_UINT32_BE (h + 8, strlen ((gchar *) string) + 1); /* include trailing 0 */
260 GST_WRITE_UINT64_BE (h + 10, (guint64) 0);
261 GST_WRITE_UINT64_BE (h + 18, (guint64) 0);
262 GST_WRITE_UINT64_BE (h + 26, (guint64) 0);
263 GST_WRITE_UINT64_BE (h + 34, (guint64) 0);
265 /* ABI padding */
266 GST_WRITE_UINT64_BE (h + 42, (guint64) 0);
267 GST_WRITE_UINT64_BE (h + 50, (guint64) 0);
269 /* CRC */
270 crc = 0;
271 if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
272 crc = gst_dp_crc (h, 58);
273 }
274 GST_WRITE_UINT16_BE (h + 58, crc);
276 crc = 0;
277 if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
278 crc = gst_dp_crc (string, strlen ((gchar *) string) + 1);
279 }
280 GST_WRITE_UINT16_BE (h + 60, crc);
282 GST_LOG ("created header from caps:");
283 gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
284 *header = h;
285 *payload = string;
286 return TRUE;
287 }
289 /**
290 * gst_dp_packet_from_event:
291 * @event: a #GstEvent to create a packet for
292 * @flags: the #GDPHeaderFlags to create the header with
293 * @length: a guint pointer to store the header length in
294 * @header: a guint8 pointer to store a newly allocated header byte array in
295 * @payload: a guint8 pointer to store a newly allocated payload byte array in
296 *
297 * Creates a GDP packet from the given event.
298 *
299 * Returns: %TRUE if the packet was successfully created.
300 */
301 gboolean
302 gst_dp_packet_from_event (const GstEvent * event, GstDPHeaderFlag flags,
303 guint * length, guint8 ** header, guint8 ** payload)
304 {
305 guint8 *h;
306 guint16 crc;
307 guint pl_length; /* length of payload */
309 g_return_val_if_fail (event, FALSE);
310 g_return_val_if_fail (GST_IS_EVENT (event), FALSE);
311 g_return_val_if_fail (header, FALSE);
312 g_return_val_if_fail (payload, FALSE);
314 *length = GST_DP_HEADER_LENGTH;
315 h = g_malloc0 (GST_DP_HEADER_LENGTH);
317 /* first construct payload, since we need the length */
318 switch (GST_EVENT_TYPE (event)) {
319 case GST_EVENT_UNKNOWN:
320 g_warning ("Unknown event, ignoring");
321 *length = 0;
322 g_free (h);
323 return FALSE;
324 case GST_EVENT_EOS:
325 case GST_EVENT_FLUSH_START:
326 case GST_EVENT_FLUSH_STOP:
327 case GST_EVENT_NEWSEGMENT:
328 pl_length = 0;
329 *payload = NULL;
330 break;
331 case GST_EVENT_SEEK:
332 {
333 gdouble rate;
334 GstFormat format;
335 GstSeekFlags flags;
336 GstSeekType cur_type, stop_type;
337 gint64 cur, stop;
339 gst_event_parse_seek ((GstEvent *) event, &rate, &format, &flags,
340 &cur_type, &cur, &stop_type, &stop);
342 pl_length = 4 + 4 + 4 + 8 + 4 + 8;
343 *payload = g_malloc0 (pl_length);
344 /* FIXME write rate */
345 GST_WRITE_UINT32_BE (*payload, (guint32) format);
346 GST_WRITE_UINT32_BE (*payload + 4, (guint32) flags);
347 GST_WRITE_UINT32_BE (*payload + 8, (guint32) cur_type);
348 GST_WRITE_UINT64_BE (*payload + 12, (guint64) cur);
349 GST_WRITE_UINT32_BE (*payload + 20, (guint32) stop_type);
350 GST_WRITE_UINT64_BE (*payload + 24, (guint64) stop);
351 break;
352 }
353 case GST_EVENT_QOS:
354 case GST_EVENT_NAVIGATION:
355 case GST_EVENT_TAG:
356 g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event));
357 return FALSE;
358 default:
359 g_warning ("Unknown event type %d, ignoring", GST_EVENT_TYPE (event));
360 *length = 0;
361 g_free (h);
362 return FALSE;
363 }
365 /* version, flags, type */
366 h[0] = (guint8) GST_DP_VERSION_MAJOR;
367 h[1] = (guint8) GST_DP_VERSION_MINOR;
368 h[2] = (guint8) flags;
369 h[3] = 0; /* padding byte */
370 GST_WRITE_UINT16_BE (h + 4,
371 GST_DP_PAYLOAD_EVENT_NONE + GST_EVENT_TYPE (event));
373 /* length */
374 GST_WRITE_UINT32_BE (h + 6, (guint32) pl_length);
375 /* timestamp */
376 GST_WRITE_UINT64_BE (h + 10, GST_EVENT_TIMESTAMP (event));
378 /* ABI padding */
379 GST_WRITE_UINT64_BE (h + 42, (guint64) 0);
380 GST_WRITE_UINT64_BE (h + 50, (guint64) 0);
382 /* CRC */
383 crc = 0;
384 if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
385 crc = gst_dp_crc (h, 58);
386 }
387 GST_WRITE_UINT16_BE (h + 58, crc);
389 crc = 0;
390 /* events can have a NULL payload */
391 if (*payload && flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
392 crc = gst_dp_crc (*payload, strlen ((gchar *) * payload) + 1);
393 }
394 GST_WRITE_UINT16_BE (h + 60, crc);
396 GST_LOG ("created header from event:");
397 gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
398 *header = h;
399 return TRUE;
400 }
403 /**
404 * gst_dp_buffer_from_header:
405 * @header_length: the length of the packet header
406 * @header: the byte array of the packet header
407 *
408 * Creates a newly allocated #GstBuffer from the given header.
409 * The buffer data needs to be copied into it before validating.
410 *
411 * Use this function if you want to pre-allocate a buffer based on the
412 * packet header to read the packet payload in to.
413 *
414 * Returns: %TRUE if the buffer was successfully created.
415 */
416 GstBuffer *
417 gst_dp_buffer_from_header (guint header_length, const guint8 * header)
418 {
419 GstBuffer *buffer;
421 g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) ==
422 GST_DP_PAYLOAD_BUFFER, NULL);
423 buffer =
424 gst_buffer_new_and_alloc ((guint) GST_DP_HEADER_PAYLOAD_LENGTH (header));
425 GST_BUFFER_TIMESTAMP (buffer) = GST_DP_HEADER_TIMESTAMP (header);
426 GST_BUFFER_DURATION (buffer) = GST_DP_HEADER_DURATION (header);
427 GST_BUFFER_OFFSET (buffer) = GST_DP_HEADER_OFFSET (header);
428 GST_BUFFER_OFFSET_END (buffer) = GST_DP_HEADER_OFFSET_END (header);
429 GST_BUFFER_FLAGS (buffer) = GST_DP_HEADER_BUFFER_FLAGS (header);
431 return buffer;
432 }
434 /**
435 * gst_dp_caps_from_packet:
436 * @header_length: the length of the packet header
437 * @header: the byte array of the packet header
438 * @payload: the byte array of the packet payload
439 *
440 * Creates a newly allocated #GstCaps from the given packet.
441 *
442 * Returns: %TRUE if the caps was successfully created.
443 */
444 GstCaps *
445 gst_dp_caps_from_packet (guint header_length, const guint8 * header,
446 const guint8 * payload)
447 {
448 GstCaps *caps;
449 const gchar *string;
451 g_return_val_if_fail (header, NULL);
452 g_return_val_if_fail (payload, NULL);
453 g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) ==
454 GST_DP_PAYLOAD_CAPS, NULL);
456 string = (gchar *) payload;
457 caps = gst_caps_from_string (string);
458 return caps;
459 }
461 /**
462 * gst_dp_event_from_packet:
463 * @header_length: the length of the packet header
464 * @header: the byte array of the packet header
465 * @payload: the byte array of the packet payload
466 *
467 * Creates a newly allocated #GstEvent from the given packet.
468 *
469 * Returns: %TRUE if the event was successfully created.
470 */
471 GstEvent *
472 gst_dp_event_from_packet (guint header_length, const guint8 * header,
473 const guint8 * payload)
474 {
475 GstEvent *event = NULL;
476 GstEventType type;
478 g_return_val_if_fail (header, NULL);
479 /* payload can be NULL, e.g. for an EOS event */
481 type = GST_DP_HEADER_PAYLOAD_TYPE (header) - GST_DP_PAYLOAD_EVENT_NONE;
482 switch (type) {
483 case GST_EVENT_UNKNOWN:
484 g_warning ("Unknown event, ignoring");
485 return FALSE;
486 case GST_EVENT_EOS:
487 case GST_EVENT_FLUSH_START:
488 case GST_EVENT_FLUSH_STOP:
489 case GST_EVENT_NEWSEGMENT:
490 event = gst_event_new_custom (type, NULL);
491 GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header);
492 break;
493 case GST_EVENT_SEEK:
494 {
495 gdouble rate;
496 GstFormat format;
497 GstSeekFlags flags;
498 GstSeekType cur_type, stop_type;
499 gint64 cur, stop;
501 /* FIXME, read rate */
502 rate = 1.0;
503 format = (GstFormat) GST_READ_UINT32_BE (payload);
504 flags = (GstSeekFlags) GST_READ_UINT32_BE (payload + 4);
505 cur_type = (GstSeekType) GST_READ_UINT32_BE (payload + 8);
506 cur = (gint64) GST_READ_UINT64_BE (payload + 12);
507 stop_type = (GstSeekType) GST_READ_UINT32_BE (payload + 20);
508 stop = (gint64) GST_READ_UINT64_BE (payload + 24);
510 event = gst_event_new_seek (rate, format, flags, cur_type, cur,
511 stop_type, stop);
512 GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header);
513 break;
514 }
515 case GST_EVENT_QOS:
516 case GST_EVENT_NAVIGATION:
517 case GST_EVENT_TAG:
518 g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event));
519 return FALSE;
520 default:
521 g_warning ("Unknown event type %d, ignoring", GST_EVENT_TYPE (event));
522 return FALSE;
523 }
525 return event;
526 }
528 /**
529 * gst_dp_validate_header:
530 * @header_length: the length of the packet header
531 * @header: the byte array of the packet header
532 *
533 * Validates the given packet header by checking the CRC checksum.
534 *
535 * Returns: %TRUE if the CRC matches, or no CRC checksum is present.
536 */
537 gboolean
538 gst_dp_validate_header (guint header_length, const guint8 * header)
539 {
540 guint16 crc_read, crc_calculated;
542 if (!(GST_DP_HEADER_FLAGS (header) & GST_DP_HEADER_FLAG_CRC_HEADER))
543 return TRUE;
544 crc_read = GST_DP_HEADER_CRC_HEADER (header);
545 /* don't included the last two crc fields for the crc check */
546 crc_calculated = gst_dp_crc (header, header_length - 4);
547 if (crc_read != crc_calculated) {
548 GST_WARNING ("header crc mismatch: read %02x, calculated %02x", crc_read,
549 crc_calculated);
550 return FALSE;
551 }
552 GST_LOG ("header crc validation: %02x", crc_read);
553 return TRUE;
554 }
556 /**
557 * gst_dp_validate_payload:
558 * @header_length: the length of the packet header
559 * @header: the byte array of the packet header
560 * @payload: the byte array of the packet payload
561 *
562 * Validates the given packet payload using the given packet header
563 * by checking the CRC checksum.
564 *
565 * Returns: %TRUE if the CRC matches, or no CRC checksum is present.
566 */
567 gboolean
568 gst_dp_validate_payload (guint header_length, const guint8 * header,
569 const guint8 * payload)
570 {
571 guint16 crc_read, crc_calculated;
573 if (!(GST_DP_HEADER_FLAGS (header) & GST_DP_HEADER_FLAG_CRC_PAYLOAD))
574 return TRUE;
575 crc_read = GST_DP_HEADER_CRC_PAYLOAD (header);
576 crc_calculated = gst_dp_crc (payload, GST_DP_HEADER_PAYLOAD_LENGTH (header));
577 if (crc_read != crc_calculated) {
578 GST_WARNING ("payload crc mismatch: read %02x, calculated %02x", crc_read,
579 crc_calculated);
580 return FALSE;
581 }
582 GST_LOG ("payload crc validation: %02x", crc_read);
583 return TRUE;
584 }
586 /**
587 * gst_dp_validate_packet:
588 * @header_length: the length of the packet header
589 * @header: the byte array of the packet header
590 * @payload: the byte array of the packet payload
591 *
592 * Validates the given packet by checking version information and checksums.
593 *
594 * Returns: %TRUE if the packet validates.
595 */
596 gboolean
597 gst_dp_validate_packet (guint header_length, const guint8 * header,
598 const guint8 * payload)
599 {
600 if (!gst_dp_validate_header (header_length, header))
601 return FALSE;
602 if (!gst_dp_validate_payload (header_length, header, payload))
603 return FALSE;
605 return TRUE;
606 }