befd501b0ad33d7c91da81c9d123e22b035cc447
1 /* GStreamer
2 * Copyright (C) <1999> Erik Walthinsen <omega@cse.ogi.edu>
3 * Copyright (C) <2004> Thomas Vander Stichele <thomas at apestaart dot org>
4 *
5 * dp-private.h: private defines/macros for dataprotocol implementation
6 *
7 * This library is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU Library General Public
9 * License as published by the Free Software Foundation; either
10 * version 2 of the License, or (at your option) any later version.
11 *
12 * This library is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
15 * Library General Public License for more details.
16 *
17 * You should have received a copy of the GNU Library General Public
18 * License along with this library; if not, write to the
19 * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
20 * Boston, MA 02111-1307, USA.
21 */
23 #ifndef __GST_DP_PRIVATE_H__
24 #define __GST_DP_PRIVATE_H__
26 #include <gst/gstdata.h>
27 #include <gst/gstbuffer.h>
28 #include <gst/gstevent.h>
29 #include <gst/gstcaps.h>
31 G_BEGIN_DECLS
33 /* accessor defines */
34 #define GST_DP_HEADER_MAJOR_VERSION(x) ((x)[0])
35 #define GST_DP_HEADER_MINOR_VERSION(x) ((x)[1])
36 #define GST_DP_HEADER_FLAGS(x) ((x)[2])
37 #define GST_DP_HEADER_PAYLOAD_TYPE(x) ((x)[3])
38 #define GST_DP_HEADER_PAYLOAD_LENGTH(x) GST_READ_UINT32_BE (x + 4)
39 #define GST_DP_HEADER_TIMESTAMP(x) GST_READ_UINT64_BE (x + 8)
40 #define GST_DP_HEADER_DURATION(x) GST_READ_UINT64_BE (x + 16)
41 #define GST_DP_HEADER_OFFSET(x) GST_READ_UINT64_BE (x + 24)
42 #define GST_DP_HEADER_OFFSET_END(x) GST_READ_UINT64_BE (x + 32)
43 #define GST_DP_HEADER_BUFFER_FLAGS(x) GST_READ_UINT16_BE (x + 40)
44 #define GST_DP_HEADER_CRC_HEADER(x) GST_READ_UINT16_BE (x + 56)
45 #define GST_DP_HEADER_CRC_PAYLOAD(x) GST_READ_UINT16_BE (x + 58)
47 void gst_dp_init (void);
48 void gst_dp_dump_byte_array (guint8 *array, guint length);
50 G_END_DECLS
52 #endif /* __GST_DP_PRIVATE_H__ */