DEBIAN: Debianization
[glsdk/gstreamer0-10.git] / libs / gst / net / gstnetclientclock.h
1 /* GStreamer
2  * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
3  *                    2005 Wim Taymans <wim@fluendo.com>
4  *                    2005 Andy Wingo <wingo@pobox.com>
5  *
6  * gstnetclientclock.h: clock that synchronizes itself to a time provider over
7  * the network
8  *
9  * This library is free software; you can redistribute it and/or
10  * modify it under the terms of the GNU Library General Public
11  * License as published by the Free Software Foundation; either
12  * version 2 of the License, or (at your option) any later version.
13  *
14  * This library is distributed in the hope that it will be useful,
15  * but WITHOUT ANY WARRANTY; without even the implied warranty of
16  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
17  * Library General Public License for more details.
18  *
19  * You should have received a copy of the GNU Library General Public
20  * License along with this library; if not, write to the
21  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
22  * Boston, MA 02111-1307, USA.
23  */
26 #ifndef __GST_NET_CLIENT_CLOCK_H__
27 #define __GST_NET_CLIENT_CLOCK_H__
29 #include <gst/gst.h>
30 #include <gst/gstsystemclock.h>
32 G_BEGIN_DECLS
34 #include <errno.h>
35 #include <string.h>
36 #include <sys/types.h>
38 #ifdef G_OS_WIN32
39 # include <winsock2.h>
40 #else
41 # include <netdb.h>
42 # include <sys/socket.h>
43 # include <netinet/in.h>
44 # include <arpa/inet.h>
45 #endif /*G_OS_WIN32 */
47 #include <fcntl.h>
49 #define GST_TYPE_NET_CLIENT_CLOCK \
50   (gst_net_client_clock_get_type())
51 #define GST_NET_CLIENT_CLOCK(obj) \
52   (G_TYPE_CHECK_INSTANCE_CAST((obj),GST_TYPE_NET_CLIENT_CLOCK,GstNetClientClock))
53 #define GST_NET_CLIENT_CLOCK_CLASS(klass) \
54   (G_TYPE_CHECK_CLASS_CAST((klass),GST_TYPE_NET_CLIENT_CLOCK,GstNetClientClockClass))
55 #define GST_IS_NET_CLIENT_CLOCK(obj) \
56   (G_TYPE_CHECK_INSTANCE_TYPE((obj),GST_TYPE_NET_CLIENT_CLOCK))
57 #define GST_IS_NET_CLIENT_CLOCK_CLASS(klass) \
58   (G_TYPE_CHECK_CLASS_TYPE((klass),GST_TYPE_NET_CLIENT_CLOCK))
60 typedef struct _GstNetClientClock GstNetClientClock;
61 typedef struct _GstNetClientClockClass GstNetClientClockClass;
62 typedef struct _GstNetClientClockPrivate GstNetClientClockPrivate;
64 /**
65  * GstNetClientClock:
66  *
67  * Opaque #GstNetClientClock structure.
68  */
69 struct _GstNetClientClock {
70   GstSystemClock clock;
72   /*< protected >*/
73   gchar *address;
74   gint port;
76   /*< private >*/
77   int sock;
78   int control_sock[2];
80   GstClockTime current_timeout;
82   struct sockaddr_in *servaddr;
84   GThread *thread;
86   /*< private >*/
87   GstNetClientClockPrivate *priv;
89   gpointer _gst_reserved[GST_PADDING - 1];
90 };
92 struct _GstNetClientClockClass {
93   GstSystemClockClass parent_class;
95   /*< private >*/
96   gpointer _gst_reserved[GST_PADDING];
97 };
99 GType           gst_net_client_clock_get_type   (void);
100 GstClock*       gst_net_client_clock_new        (gchar *name, const gchar *remote_address,
101                                                  gint remote_port, GstClockTime base_time);
103 G_END_DECLS
105 #endif /* __GST_NET_CLIENT_CLOCK_H__ */