b04d28243ec1ca7eafb0404dac46587f4f0ec4a4
[glsdk/gstreamer0-10.git] / libs / gst / net / gstnettimeprovider.c
1 /* GStreamer
2  * Copyright (C) 2005 Andy Wingo <wingo@pobox.com>
3  *
4  * This library is free software; you can redistribute it and/or
5  * modify it under the terms of the GNU Library General Public
6  * License as published by the Free Software Foundation; either
7  * version 2 of the License, or (at your option) any later version.
8  *
9  * This library is distributed in the hope that it will be useful,
10  * but WITHOUT ANY WARRANTY; without even the implied warranty of
11  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
12  * Library General Public License for more details.
13  *
14  * You should have received a copy of the GNU Library General Public
15  * License along with this library; if not, write to the
16  * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
17  * Boston, MA 02111-1307, USA.
18  */
19 /**
20  * SECTION:gstnettimeprovider
21  * @short_description: Special object that exposed the time of a clock
22  *                     on the network.
23  * @see_also: #GstClock, #GstNetClientClock, #GstPipeline
24  *
25  * This object exposes the time of a #GstClock on the network.
26  *
27  * A #GstNetTimeProvider is created with gst_net_time_provider_new() which
28  * takes a #GstClock, an address and a port number as arguments.
29  *
30  * After creating the object, a client clock such as #GstNetClientClock can
31  * query the exposed clock over the network for its values.
32  *
33  * The #GstNetTimeProvider typically wraps the clock used by a #GstPipeline.
34  *
35  * Last reviewed on 2005-11-23 (0.9.5)
36  */
38 #ifdef HAVE_CONFIG_H
39 #include "config.h"
40 #endif
42 #include "gstnettimeprovider.h"
43 #include "gstnettimepacket.h"
45 #include <glib.h>
47 #ifdef HAVE_UNISTD_H
48 #include <unistd.h>
49 #endif
51 #if defined (_MSC_VER) && _MSC_VER >= 1400
52 #include <io.h>
53 #endif
55 #ifndef G_OS_WIN32
56 #include <sys/ioctl.h>
57 #endif
59 #ifdef HAVE_FIONREAD_IN_SYS_FILIO
60 #include <sys/filio.h>
61 #endif
63 GST_DEBUG_CATEGORY_STATIC (ntp_debug);
64 #define GST_CAT_DEFAULT (ntp_debug)
66 #ifdef G_OS_WIN32
67 #define close(sock) closesocket(sock)
68 #endif
70 #define DEFAULT_ADDRESS         "0.0.0.0"
71 #define DEFAULT_PORT            5637
73 #define IS_ACTIVE(self) (g_atomic_int_get (&((self)->active.active)))
75 #ifdef G_OS_WIN32
76 #define setsockopt(sock, sol_flags, reuse_flags, ru, sizeofru) setsockopt (sock, sol_flags, reuse_flags, (char *)ru, sizeofru)
77 #endif
78 enum
79 {
80   PROP_0,
81   PROP_PORT,
82   PROP_ADDRESS,
83   PROP_CLOCK,
84   PROP_ACTIVE
85       /* FILL ME */
86 };
88 #define GST_NET_TIME_PROVIDER_GET_PRIVATE(obj)  \
89    (G_TYPE_INSTANCE_GET_PRIVATE ((obj), GST_TYPE_NET_TIME_PROVIDER, GstNetTimeProviderPrivate))
91 struct _GstNetTimeProviderPrivate
92 {
93   GstPollFD sock;
94   GstPoll *fdset;
95 };
97 static gboolean gst_net_time_provider_start (GstNetTimeProvider * bself);
98 static void gst_net_time_provider_stop (GstNetTimeProvider * bself);
100 static gpointer gst_net_time_provider_thread (gpointer data);
102 static void gst_net_time_provider_finalize (GObject * object);
103 static void gst_net_time_provider_set_property (GObject * object, guint prop_id,
104     const GValue * value, GParamSpec * pspec);
105 static void gst_net_time_provider_get_property (GObject * object, guint prop_id,
106     GValue * value, GParamSpec * pspec);
108 #define _do_init(type) \
109   GST_DEBUG_CATEGORY_INIT (ntp_debug, "nettime", 0, "Network time provider");
111 GST_BOILERPLATE_FULL (GstNetTimeProvider, gst_net_time_provider, GstObject,
112     GST_TYPE_OBJECT, _do_init);
114 #ifdef G_OS_WIN32
115 static int
116 inet_aton (const char *c, struct in_addr *paddr)
118   paddr->s_addr = inet_addr (c);
119   if (paddr->s_addr == INADDR_NONE)
120     return 0;
122   return 1;
124 #endif
126 static void
127 gst_net_time_provider_base_init (gpointer g_class)
129   /* Do nothing here */
132 static void
133 gst_net_time_provider_class_init (GstNetTimeProviderClass * klass)
135   GObjectClass *gobject_class;
137   gobject_class = G_OBJECT_CLASS (klass);
139   g_assert (sizeof (GstClockTime) == 8);
141   g_type_class_add_private (klass, sizeof (GstNetTimeProviderPrivate));
143   gobject_class->finalize = gst_net_time_provider_finalize;
144   gobject_class->set_property = gst_net_time_provider_set_property;
145   gobject_class->get_property = gst_net_time_provider_get_property;
147   g_object_class_install_property (gobject_class, PROP_PORT,
148       g_param_spec_int ("port", "port",
149           "The port to receive the packets from, 0=allocate", 0, G_MAXUINT16,
150           DEFAULT_PORT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
151   g_object_class_install_property (gobject_class, PROP_ADDRESS,
152       g_param_spec_string ("address", "address",
153           "The address to bind on, as a dotted quad (x.x.x.x)",
154           DEFAULT_ADDRESS, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
155   g_object_class_install_property (gobject_class, PROP_CLOCK,
156       g_param_spec_object ("clock", "Clock",
157           "The clock to export over the network", GST_TYPE_CLOCK,
158           G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
159   g_object_class_install_property (gobject_class, PROP_ACTIVE,
160       g_param_spec_boolean ("active", "Active",
161           "TRUE if the clock will respond to queries over the network", TRUE,
162           G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
165 static void
166 gst_net_time_provider_init (GstNetTimeProvider * self,
167     GstNetTimeProviderClass * g_class)
169 #ifdef G_OS_WIN32
170   WSADATA w;
171   int error = WSAStartup (0x0202, &w);
173   if (error) {
174     GST_DEBUG_OBJECT (self, "Error on WSAStartup");
175   }
176   if (w.wVersion != 0x0202) {
177     WSACleanup ();
178   }
179 #endif
180   self->priv = GST_NET_TIME_PROVIDER_GET_PRIVATE (self);
182   self->port = DEFAULT_PORT;
183   self->priv->sock.fd = -1;
184   self->address = g_strdup (DEFAULT_ADDRESS);
185   self->thread = NULL;
186   self->active.active = TRUE;
189 static void
190 gst_net_time_provider_finalize (GObject * object)
192   GstNetTimeProvider *self = GST_NET_TIME_PROVIDER (object);
194   if (self->thread) {
195     gst_net_time_provider_stop (self);
196     g_assert (self->thread == NULL);
197   }
199   if (self->priv->fdset) {
200     gst_poll_free (self->priv->fdset);
201     self->priv->fdset = NULL;
202   }
204   g_free (self->address);
205   self->address = NULL;
207   if (self->clock)
208     gst_object_unref (self->clock);
209   self->clock = NULL;
211 #ifdef G_OS_WIN32
212   WSACleanup ();
213 #endif
215   G_OBJECT_CLASS (parent_class)->finalize (object);
218 static gpointer
219 gst_net_time_provider_thread (gpointer data)
221   GstNetTimeProvider *self = data;
222   struct sockaddr_in tmpaddr;
223   socklen_t len;
224   GstNetTimePacket *packet;
225   gint ret;
227   while (TRUE) {
228     GST_LOG_OBJECT (self, "doing select");
229     ret = gst_poll_wait (self->priv->fdset, GST_CLOCK_TIME_NONE);
230     GST_LOG_OBJECT (self, "select returned %d", ret);
232     if (ret <= 0) {
233       if (errno == EBUSY) {
234         GST_LOG_OBJECT (self, "stop");
235         goto stopped;
236       } else if (errno != EAGAIN && errno != EINTR)
237         goto select_error;
238       else
239         continue;
240     } else {
241       /* got data in */
242       len = sizeof (struct sockaddr);
244       packet = gst_net_time_packet_receive (self->priv->sock.fd,
245           (struct sockaddr *) &tmpaddr, &len);
247       if (!packet)
248         goto receive_error;
250       if (IS_ACTIVE (self)) {
251         /* do what we were asked to and send the packet back */
252         packet->remote_time = gst_clock_get_time (self->clock);
254         /* ignore errors */
255         gst_net_time_packet_send (packet, self->priv->sock.fd,
256             (struct sockaddr *) &tmpaddr, len);
257       }
259       g_free (packet);
261       continue;
262     }
264     g_assert_not_reached ();
266     /* log errors and keep going */
267   select_error:
268     {
269       GST_DEBUG_OBJECT (self, "select error %d: %s (%d)", ret,
270           g_strerror (errno), errno);
271       continue;
272     }
273   stopped:
274     {
275       GST_DEBUG_OBJECT (self, "shutting down");
276       /* close socket */
277       return NULL;
278     }
279   receive_error:
280     {
281       GST_DEBUG_OBJECT (self, "receive error");
282       continue;
283     }
285     g_assert_not_reached ();
287   }
289   g_assert_not_reached ();
291   return NULL;
294 static void
295 gst_net_time_provider_set_property (GObject * object, guint prop_id,
296     const GValue * value, GParamSpec * pspec)
298   GstNetTimeProvider *self = GST_NET_TIME_PROVIDER (object);
299   GstClock **clock_p = &self->clock;
301   switch (prop_id) {
302     case PROP_PORT:
303       self->port = g_value_get_int (value);
304       break;
305     case PROP_ADDRESS:
306       g_free (self->address);
307       if (g_value_get_string (value) == NULL)
308         self->address = g_strdup (DEFAULT_ADDRESS);
309       else
310         self->address = g_strdup (g_value_get_string (value));
311       break;
312     case PROP_CLOCK:
313       gst_object_replace ((GstObject **) clock_p,
314           (GstObject *) g_value_get_object (value));
315       break;
316     case PROP_ACTIVE:
317       g_atomic_int_set (&self->active.active, g_value_get_boolean (value));
318       break;
319     default:
320       G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
321       break;
322   }
325 static void
326 gst_net_time_provider_get_property (GObject * object, guint prop_id,
327     GValue * value, GParamSpec * pspec)
329   GstNetTimeProvider *self = GST_NET_TIME_PROVIDER (object);
331   switch (prop_id) {
332     case PROP_PORT:
333       g_value_set_int (value, self->port);
334       break;
335     case PROP_ADDRESS:
336       g_value_set_string (value, self->address);
337       break;
338     case PROP_CLOCK:
339       g_value_set_object (value, self->clock);
340       break;
341     case PROP_ACTIVE:
342       g_value_set_boolean (value, IS_ACTIVE (self));
343       break;
344     default:
345       G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
346       break;
347   }
350 static gboolean
351 gst_net_time_provider_start (GstNetTimeProvider * self)
353   gint ru;
354   struct sockaddr_in my_addr;
355   socklen_t len;
356   int port;
357   gint ret;
358   GError *error;
360   if ((ret = socket (AF_INET, SOCK_DGRAM, 0)) < 0)
361     goto no_socket;
363   self->priv->sock.fd = ret;
365   ru = 1;
366   ret =
367       setsockopt (self->priv->sock.fd, SOL_SOCKET, SO_REUSEADDR, &ru,
368       sizeof (ru));
369   if (ret < 0)
370     goto setsockopt_error;
372   memset (&my_addr, 0, sizeof (my_addr));
373   my_addr.sin_family = AF_INET; /* host byte order */
374   my_addr.sin_port = htons ((gint16) self->port);       /* short, network byte order */
375   my_addr.sin_addr.s_addr = INADDR_ANY;
376   if (self->address) {
377     ret = inet_aton (self->address, &my_addr.sin_addr);
378     if (ret == 0)
379       goto invalid_address_error;
380   }
382   GST_DEBUG_OBJECT (self, "binding on port %d", self->port);
383   ret =
384       bind (self->priv->sock.fd, (struct sockaddr *) &my_addr,
385       sizeof (my_addr));
386   if (ret < 0)
387     goto bind_error;
389   len = sizeof (my_addr);
390   ret = getsockname (self->priv->sock.fd, (struct sockaddr *) &my_addr, &len);
391   if (ret < 0)
392     goto getsockname_error;
394   port = ntohs (my_addr.sin_port);
395   GST_DEBUG_OBJECT (self, "bound, on port %d", port);
397   if (port != self->port) {
398     self->port = port;
399     GST_DEBUG_OBJECT (self, "notifying %d", port);
400     g_object_notify (G_OBJECT (self), "port");
401   }
403   gst_poll_add_fd (self->priv->fdset, &self->priv->sock);
404   gst_poll_fd_ctl_read (self->priv->fdset, &self->priv->sock, TRUE);
406   self->thread = g_thread_create (gst_net_time_provider_thread, self, TRUE,
407       &error);
408   if (!self->thread)
409     goto no_thread;
411   return TRUE;
413   /* ERRORS */
414 no_socket:
415   {
416     GST_ERROR_OBJECT (self, "socket failed %d: %s (%d)", ret,
417         g_strerror (errno), errno);
418     return FALSE;
419   }
420 setsockopt_error:
421   {
422     close (self->priv->sock.fd);
423     self->priv->sock.fd = -1;
424     GST_ERROR_OBJECT (self, "setsockopt failed %d: %s (%d)", ret,
425         g_strerror (errno), errno);
426     return FALSE;
427   }
428 invalid_address_error:
429   {
430     close (self->priv->sock.fd);
431     self->priv->sock.fd = -1;
432     GST_ERROR_OBJECT (self, "invalid network address %s: %s (%d)",
433         self->address, g_strerror (errno), errno);
434     return FALSE;
435   }
436 bind_error:
437   {
438     close (self->priv->sock.fd);
439     self->priv->sock.fd = -1;
440     GST_ERROR_OBJECT (self, "bind failed %d: %s (%d)", ret,
441         g_strerror (errno), errno);
442     return FALSE;
443   }
444 getsockname_error:
445   {
446     close (self->priv->sock.fd);
447     self->priv->sock.fd = -1;
448     GST_ERROR_OBJECT (self, "getsockname failed %d: %s (%d)", ret,
449         g_strerror (errno), errno);
450     return FALSE;
451   }
452 no_thread:
453   {
454     gst_poll_remove_fd (self->priv->fdset, &self->priv->sock);
455     close (self->priv->sock.fd);
456     self->priv->sock.fd = -1;
457     GST_ERROR_OBJECT (self, "could not create thread: %s", error->message);
458     g_error_free (error);
459     return FALSE;
460   }
463 static void
464 gst_net_time_provider_stop (GstNetTimeProvider * self)
466   gst_poll_set_flushing (self->priv->fdset, TRUE);
467   g_thread_join (self->thread);
468   self->thread = NULL;
470   if (self->priv->sock.fd != -1) {
471     gst_poll_remove_fd (self->priv->fdset, &self->priv->sock);
472     close (self->priv->sock.fd);
473     self->priv->sock.fd = -1;
474   }
477 /**
478  * gst_net_time_provider_new:
479  * @clock: a #GstClock to export over the network
480  * @address: an address to bind on as a dotted quad (xxx.xxx.xxx.xxx), or NULL
481  *           to bind to all addresses
482  * @port: a port to bind on, or 0 to let the kernel choose
483  *
484  * Allows network clients to get the current time of @clock.
485  *
486  * Returns: the new #GstNetTimeProvider, or NULL on error
487  */
488 GstNetTimeProvider *
489 gst_net_time_provider_new (GstClock * clock, const gchar * address, gint port)
491   GstNetTimeProvider *ret;
493   g_return_val_if_fail (clock && GST_IS_CLOCK (clock), NULL);
494   g_return_val_if_fail (port >= 0 && port <= G_MAXUINT16, NULL);
496   ret = g_object_new (GST_TYPE_NET_TIME_PROVIDER, "clock", clock, "address",
497       address, "port", port, NULL);
499   if ((ret->priv->fdset = gst_poll_new (TRUE)) == NULL)
500     goto no_fdset;
502   if (!gst_net_time_provider_start (ret))
503     goto failed_start;
505   /* all systems go, cap'n */
506   return ret;
508 no_fdset:
509   {
510     GST_ERROR_OBJECT (ret, "could not create an fdset: %s (%d)",
511         g_strerror (errno), errno);
512     gst_object_unref (ret);
513     return NULL;
514   }
515 failed_start:
516   {
517     /* already printed a nice error */
518     gst_object_unref (ret);
519     return NULL;
520   }